Updated OAR and PAF submodule.
PASDK-251:Fix uninitialized global variables (DSP params, numBufOverride
in PAF_AST_params_outBufStatus.
NOTE: This problem also exists in DA8x, DSPA (SB00) params.
in PAF_AST_params_outBufStatus.
NOTE: This problem also exists in DA8x, DSPA (SB00) params.
PASDK-216:Update tools
PASDK-258:Merge remote-tracking branch 'origin/dev_pasdk_frank_pasdk258Alpha4Release'
PASDK-258:Add comment to PASDK release notes describing incomplete functionality w.r.t. PASDK-242.
PASDK-258:Update build scripts to handle release notes
PASDK-258:Add Brandon's Release Notes for PASDK & Dolby IP
PASDK-258:Remove stale ReadMe.txt file
PASDK-258:Update PASDK setup guide (.doc & .pdf), Brandon's updates
PASDK-258:Update OS package creation script to handle tools as sub-module (remove 3rd party python tools, add tools setup script)
PASDK-258:Merge remote-tracking branch 'origin/dev_pasdk_pp_pasdk258HigherSampleRateSupport' into dev_pasdk_frank_pasdk258Alpha4Release
PASDK-258:Update Alpha command package (code cleanup + copyright change to 2017)
PASDK-258:Update copyright for files modified since Alpha-2 release.
PASDK-258:Update FD package version number.
PASDK258: Always use Input interface rate hard-coded to 192 kHz.
PASDK258: Updated PAF submodule for SRC fix.
PASDK-258:Update copyright for files modified since Alpha-2 release.
PASDK-258:Update copyright for files modified since Alpha-2 release.
PASDK-258:Update copyright for files modified since Alpha-2 release.
PASDK-258:Update PDK eng to 1.0.1.1. Using build number to differentiate PDK eng versions.
PASDK-258:Update PDK eng to 1.0.1.1. Using build number to differentiate PDK eng versions.
PASDK-258:Add FD package version number build scripts.
PASDK-258:Update PDK eng to 1.0.1.1. Using build number to differentiate PDK eng versions.
PASDK-258:Update PDK eng to 1.0.1.1. Using build number to differentiate PDK eng versions.
PASDK-258:Update PDK eng to 1.0.1.1. Using build number to differentiate PDK eng versions.
PASDK-258:Update PDK eng to 1.0.1.1. Using build number to differentiate PDK eng versions.
PASDK-258:Update PDK eng to 1.0.1.1. Using build number to differentiate PDK eng versions.
PASDK-258:Update PDK eng to 1.0.1.1. Using build number to differentiate PDK eng versions.
PASDK-258:Update PDK eng to 1.0.1.1. Using build number to differentiate PDK eng versions.
PASDK-258:Update build_os_pkg.bat to include config_cust.ini for pyalpha from tools for release.
PASDK-258:Update PASDK_VERSION in build_all.bat
PASDK-258:Remove TEST_MULTICHANNEL define from DSP application, IP packages build
PASDK-258:Add ML0 include path for DSP application, IP packages build
PASDK-258:Merge remote-tracking branch 'origin/dev_pasdk_govind_pasdk258Clean4Alpha4' into dev_pasdk_frank_pasdk258Alpha4Release
PASDK-258: Minor clean up removing dead wood from test_dsp application.
PASDK-258:Update tools submodule
PASDK-258:Update root installation folder to processor_audio_sdk_1_00_00_02
PASDK-258:Update code merged from 4573453 (PP PASDK-242).
Provide single header file to enable/disable and configure benchmarking
build (see PASDK-242 for details on benchmarking configurations).
Header file: common/dbgBenchmark.h
Build with benchmarking disabled is default (SIDK) build.
Provide single header file to enable/disable and configure benchmarking
build (see PASDK-242 for details on benchmarking configurations).
Header file: common/dbgBenchmark.h
Build with benchmarking disabled is default (SIDK) build.
PASDK-258:Update code merged from 4573453 (PP PASDK-242) for default build.
ASIT/ASOT maxFramelength==1024 results in malloc failure during system
intialization w/ CAR,OAR and BMDA in build.
ASIT/ASOT maxFramelength==1024 results in malloc failure during system
intialization w/ CAR,OAR and BMDA in build.
PASDK-258:Merge remote-tracking branch 'origin/dev_pasdk_pp_pasdk242HigherSamplingRate' into dev_pasdk_frank_pasdk258Alpha4Release
PASDK-258:Update Dolby DDP IP submodules to Harmony v1.3
PASDK-258:Update PAF submodule
PASDK-258:Update Dolby IP submodules to Harmony v1.3
PASDK242: Added BMDA and merged CB memset() fix.
PASDK-258:Update linker File Search Path for LibArch EDMA example code for PASDK custom PDK
PASDK-258:Add LibArch environment setup batch file
PASDK-258:Add LibArch release from Jianzhong
PASDK-258:Update OS package creation script:
1. Remove .doc version of setup guide in docs folder.
2. Retain .pdf version of setup guide in docs folder.
Note: release notes will replace "ReadMe.txt" in root folder.
1. Remove .doc version of setup guide in docs folder.
2. Retain .pdf version of setup guide in docs folder.
Note: release notes will replace "ReadMe.txt" in root folder.
PASDK-258:Add PASDK setup guide, .doc version. This will be removed by build/release scripts.
PASDK-258:Clean up PASDK docs. Docs relocated from paf/pa/docs folder.
PASDK-258:Update OS package creation script to handle tools as sub-module (don't include README.md in release).
PASDK-258:Update OS package creation script to handle tools as sub-module (don't include internal tools in release).
Add fil and src4 to paf build script
Update OS package creation script to handle tools as sub-module (don't
include internal tools in release.
Update ARM/DSP projects for high-sampling rate+SRC code changes.
Update OS package creation script to handle tools as sub-module (don't
include internal tools in release.
Update ARM/DSP projects for high-sampling rate+SRC code changes.
Update CCS projects
Update alpha package
Circular buffer read cleanup from Build #38 (work on PASDK-53).
GPIO debug.
This helps 192 kHz & SRC 4:1 to "work" in some circumstances w/ CAR
enabled for 7.1.4 upmix.
GPIO debug.
This helps 192 kHz & SRC 4:1 to "work" in some circumstances w/ CAR
enabled for 7.1.4 upmix.
PASDK242: Added PAF_SYS_FRAMELENGTH for system framelength.
Build #38: remove GPIO debug
Add third debug GPIO
Update ARM app to allow GPIO debug
Further cleanup of CB overflow handling
Further cleanup of CB underflow handling
Fix ASIT decodeInfo() to properly return error return to from ARM.
Remove ML0 from DSP build.
Remove ML0 from DSP build.
PASDK-53: Cleanup of CB underflow. Additional work needed as mentioned in comments.
Add comment
PASDK-53: Experimental code for circular buffer overflow/underflow handling
PASDK242: updated trigger of ASP profiling to sampling rate.
PASDK242: Added support for SRC4 and 96KHz.
PASDK-53: Experimental code, remove Dec Op CB reset on CB underflow.
This appears to fix:
1) Glitching for DDP, channel_sampling_rate_48k.ec3
2) MAT-THD causing system failure after 7x streams of
channel_sampling_rate_48k.mlp
This appears to fix:
1) Glitching for DDP, channel_sampling_rate_48k.ec3
2) MAT-THD causing system failure after 7x streams of
channel_sampling_rate_48k.mlp
Add 3p-ip-dts submodule
Remove tools directory.
Tools will be obtain directly from PASDK tools repository.
PASDK tools repository will be made into PASDK super-repo submodule.
Scripts will produce correct tools directory content for release.
(cherry picked from commit f99cba46f1dd0f578baf37962fcbee10f39b15f8)
Tools will be obtain directly from PASDK tools repository.
PASDK tools repository will be made into PASDK super-repo submodule.
Scripts will produce correct tools directory content for release.
(cherry picked from commit f99cba46f1dd0f578baf37962fcbee10f39b15f8)
PASDK-53: Experimental code,dynamically change Audio Stream Task priorities.
PASDK-53: Experimental code,dynamically change Audio Stream Task priorities.
ASIT is higher priority than ASOT during autodetection
ASIT is the same priority as ASOT during decoding
ASIT is higher priority than ASOT during autodetection
ASIT is the same priority as ASOT during decoding
PASDK209: Added post processing and CPU load profiler.
Update include files in DSP project for ML0 alpha header file
Update tools submodule
Add ML0 to DSP
Update tools submodule
Update PAF submodule
Update PAF submodule
Fix memset bugs.
Update oar submodule
Change at-boot output shortcut to execPAIOutAnalog
Merge remote-tracking branch 'origin/dev_pasdk_govind_pasdk53IpDataDebug' into dev_pasdk_frank
PASDK-53: This commit for cleaner input handling, also brings decoders back into the system.
BugFix in PAF_ASIT_decodeProcessing owing to the newer "statusOp_read"
BugFix in PAF_ASIT_decodeProcessing owing to the newer "statusOp_read"
Remove tabs
Remove SW_BREAKPOINT on ASIP due to Dec CB overflow returned to DSP
PASDK-53: Hard-coding 192 KHz as the IB SampleRate, to aid with SIDK progress.
Importantly, this helps side-step the I2C real-time issue, until the an efficient I2C option is found.
Importantly, this helps side-step the I2C real-time issue, until the an efficient I2C option is found.
PASDK-53: EDMA programming fix, to suit both 1-lane & 4-lane HDMI input handling + misc. Debug Logs.
PASDK-53: Reducing the arbitrary per-call time to invoke platform_delay with. Few other debug mods.
PASDK-53: Don't need the 2nd Memtab in IB anymore. The scratch memory tab was used primarily for paging of data from SDRAM->IRAM. Important when there was no D-cache.
PASDK-53: DIBERR_SYNC is NOT masked now in PAF_ASIT_autoProcessing, to consolidate all the Input Reset operations to the top of the ASIP state-machine.
PASDK-53: This commit for cleaner input handling, also brings decoders back into the system.
BugFix in PAF_ASIT_decodeProcessing owing to the newer "statusOp_read"
BugFix in PAF_ASIT_decodeProcessing owing to the newer "statusOp_read"
Update PAF submodule