Update CCS projects for resource table change
* Update CCS projects for PRU Labs and PRU Demos for updated
Resource Table header files
* Update CCS projects for PRU Labs and PRU Demos for updated
Resource Table header files
Update empty Resource Table header files
Update Software Manifest to v2.0
Update PRU_edmaConfig example to config EDMA clock
Updated access_const_table example
* Expand PRU_access_const_table to include 3 different types of memory accesses:
1. Access PRU peripherals using Constant Table & PRU header file
2. Access SoC peripherals using Constant Table
3. Access PRU Shared RAM using Constant Table
* Expand PRU_access_const_table to include 3 different types of memory accesses:
1. Access PRU peripherals using Constant Table & PRU header file
2. Access SoC peripherals using Constant Table
3. Access PRU Shared RAM using Constant Table
Update CCS projects for labs and demos
* Updated the PRU labs and demo CCS projects for the firmware updates made
with the linker cmd file changes.
* Updated the PRU labs and demo CCS projects for the firmware updates made
with the linker cmd file changes.
Update linker cmd files to standardized AM335x PRU cmd file
* The linker cmd files for all examples, labs, and demos are updated
to a standardized AM335x PRU cmd file.
* All PRU firmware updated for linker cmd file changes.
* The linker cmd files for all examples, labs, and demos are updated
to a standardized AM335x PRU cmd file.
* All PRU firmware updated for linker cmd file changes.
Update Resource Table header files
* Removed device specific details
* Included header file in all examples
* Updated PRU_IEP example to configure PRU INTC in resource table
* Removed device specific details
* Included header file in all examples
* Updated PRU_IEP example to configure PRU INTC in resource table
Define PRU_CTRL address to header file
* Define PRU_CTRL address in the PRU_CTRL header file to comply with remoteproc
driver.
* Update example code accessing PRU_CTRL registers.
* Define PRU_CTRL address in the PRU_CTRL header file to comply with remoteproc
driver.
* Update example code accessing PRU_CTRL registers.
Disable HDMI related features in BBB dtsi file
* Disable hdmi, mcasp0, and sound
* Disable hdmi, mcasp0, and sound
Add patches for linux-3.14.26 kernel
Remove LINUXEZSDK v7 patches
* Remove patches associated with LINUXEZSDK-AM335X v7.0 and
LINUXEZSDK-AM437X v7.1.
* Note these patches are already applied to the Linux kernel starting in
linux-3.14.26.
* Remove patches associated with LINUXEZSDK-AM335X v7.0 and
LINUXEZSDK-AM437X v7.1.
* Note these patches are already applied to the Linux kernel starting in
linux-3.14.26.
Update Lab 4 resource_table_1 header file
Add new PRU labs and demo
* Add Lab 3: Temperature Monitor Application
* Add Lab 4: Introduction to Linux Driver
* Add Temperature Sensor demo
* Add am335x-boneblack-prucape.dtsi
* Add am335x-bone-prucape.dtsi
* Add Lab 3: Temperature Monitor Application
* Add Lab 4: Introduction to Linux Driver
* Add Temperature Sensor demo
* Add am335x-boneblack-prucape.dtsi
* Add am335x-bone-prucape.dtsi
Add PRU labs and demos
* Labs include:
- Lab 1 Toggle LED with PRU GPO
- Lab 2 Read Push Button Switch on PRU0 GPI & Toggle LED with PRU1 GPO
* Demos include:
- LED
- Push Button Switch
- Audio
- UART
* Update Software Manifest
* Add ReadMe file
* Labs include:
- Lab 1 Toggle LED with PRU GPO
- Lab 2 Read Push Button Switch on PRU0 GPI & Toggle LED with PRU1 GPO
* Demos include:
- LED
- Push Button Switch
- Audio
- UART
* Update Software Manifest
* Add ReadMe file
Update PRU examples to use updated header files
Update PRU header files
Update patch set for Linux Kernel
PRU Software Support Package v1.0