1 # -*- coding: utf-8 -*-
2 #
3 # The Linux Kernel documentation build configuration file, created by
4 # sphinx-quickstart on Fri Feb 12 13:51:46 2016.
5 #
6 # This file is execfile()d with the current directory set to its
7 # containing dir.
8 #
9 # Note that not all possible configuration values are present in this
10 # autogenerated file.
11 #
12 # All configuration values have a default; values that are commented out
13 # serve to show the default.
15 import sys
16 import os
17 import sphinx
19 # Get Sphinx version
20 major, minor, patch = sphinx.version_info[:3]
23 # If extensions (or modules to document with autodoc) are in another directory,
24 # add these directories to sys.path here. If the directory is relative to the
25 # documentation root, use os.path.abspath to make it absolute, like shown here.
26 sys.path.insert(0, os.path.abspath('sphinx'))
27 from load_config import loadConfig
29 # -- General configuration ------------------------------------------------
31 # If your documentation needs a minimal Sphinx version, state it here.
32 needs_sphinx = '1.3'
34 # Add any Sphinx extension module names here, as strings. They can be
35 # extensions coming with Sphinx (named 'sphinx.ext.*') or your custom
36 # ones.
37 extensions = ['kerneldoc', 'rstFlatTable', 'kernel_include', 'cdomain', 'kfigure', 'sphinx.ext.ifconfig']
39 # The name of the math extension changed on Sphinx 1.4
40 if major == 1 and minor > 3:
41 extensions.append("sphinx.ext.imgmath")
42 else:
43 extensions.append("sphinx.ext.pngmath")
45 # Add any paths that contain templates here, relative to this directory.
46 templates_path = ['_templates']
48 # The suffix(es) of source filenames.
49 # You can specify multiple suffix as a list of string:
50 # source_suffix = ['.rst', '.md']
51 source_suffix = '.rst'
53 # The encoding of source files.
54 #source_encoding = 'utf-8-sig'
56 # The master toctree document.
57 master_doc = 'index'
59 # General information about the project.
60 project = 'The Linux Kernel'
61 copyright = 'The kernel development community'
62 author = 'The kernel development community'
64 # The version info for the project you're documenting, acts as replacement for
65 # |version| and |release|, also used in various other places throughout the
66 # built documents.
67 #
68 # In a normal build, version and release are are set to KERNELVERSION and
69 # KERNELRELEASE, respectively, from the Makefile via Sphinx command line
70 # arguments.
71 #
72 # The following code tries to extract the information by reading the Makefile,
73 # when Sphinx is run directly (e.g. by Read the Docs).
74 try:
75 makefile_version = None
76 makefile_patchlevel = None
77 for line in open('../Makefile'):
78 key, val = [x.strip() for x in line.split('=', 2)]
79 if key == 'VERSION':
80 makefile_version = val
81 elif key == 'PATCHLEVEL':
82 makefile_patchlevel = val
83 if makefile_version and makefile_patchlevel:
84 break
85 except:
86 pass
87 finally:
88 if makefile_version and makefile_patchlevel:
89 version = release = makefile_version + '.' + makefile_patchlevel
90 else:
91 version = release = "unknown version"
93 # The language for content autogenerated by Sphinx. Refer to documentation
94 # for a list of supported languages.
95 #
96 # This is also used if you do content translation via gettext catalogs.
97 # Usually you set "language" from the command line for these cases.
98 language = None
100 # There are two options for replacing |today|: either, you set today to some
101 # non-false value, then it is used:
102 #today = ''
103 # Else, today_fmt is used as the format for a strftime call.
104 #today_fmt = '%B %d, %Y'
106 # List of patterns, relative to source directory, that match files and
107 # directories to ignore when looking for source files.
108 exclude_patterns = ['output']
110 # The reST default role (used for this markup: `text`) to use for all
111 # documents.
112 #default_role = None
114 # If true, '()' will be appended to :func: etc. cross-reference text.
115 #add_function_parentheses = True
117 # If true, the current module name will be prepended to all description
118 # unit titles (such as .. function::).
119 #add_module_names = True
121 # If true, sectionauthor and moduleauthor directives will be shown in the
122 # output. They are ignored by default.
123 #show_authors = False
125 # The name of the Pygments (syntax highlighting) style to use.
126 pygments_style = 'sphinx'
128 # A list of ignored prefixes for module index sorting.
129 #modindex_common_prefix = []
131 # If true, keep warnings as "system message" paragraphs in the built documents.
132 #keep_warnings = False
134 # If true, `todo` and `todoList` produce output, else they produce nothing.
135 todo_include_todos = False
137 primary_domain = 'c'
138 highlight_language = 'none'
140 # -- Options for HTML output ----------------------------------------------
142 # The theme to use for HTML and HTML Help pages. See the documentation for
143 # a list of builtin themes.
145 # The Read the Docs theme is available from
146 # - https://github.com/snide/sphinx_rtd_theme
147 # - https://pypi.python.org/pypi/sphinx_rtd_theme
148 # - python-sphinx-rtd-theme package (on Debian)
149 try:
150 import sphinx_rtd_theme
151 html_theme = 'sphinx_rtd_theme'
152 html_theme_path = [sphinx_rtd_theme.get_html_theme_path()]
153 except ImportError:
154 sys.stderr.write('Warning: The Sphinx \'sphinx_rtd_theme\' HTML theme was not found. Make sure you have the theme installed to produce pretty HTML output. Falling back to the default theme.\n')
156 # Theme options are theme-specific and customize the look and feel of a theme
157 # further. For a list of options available for each theme, see the
158 # documentation.
159 #html_theme_options = {}
161 # Add any paths that contain custom themes here, relative to this directory.
162 #html_theme_path = []
164 # The name for this set of Sphinx documents. If None, it defaults to
165 # "<project> v<release> documentation".
166 #html_title = None
168 # A shorter title for the navigation bar. Default is the same as html_title.
169 #html_short_title = None
171 # The name of an image file (relative to this directory) to place at the top
172 # of the sidebar.
173 #html_logo = None
175 # The name of an image file (within the static path) to use as favicon of the
176 # docs. This file should be a Windows icon file (.ico) being 16x16 or 32x32
177 # pixels large.
178 #html_favicon = None
180 # Add any paths that contain custom static files (such as style sheets) here,
181 # relative to this directory. They are copied after the builtin static files,
182 # so a file named "default.css" will overwrite the builtin "default.css".
184 html_static_path = ['sphinx-static']
186 html_context = {
187 'css_files': [
188 '_static/theme_overrides.css',
189 ],
190 }
192 # Add any extra paths that contain custom files (such as robots.txt or
193 # .htaccess) here, relative to this directory. These files are copied
194 # directly to the root of the documentation.
195 #html_extra_path = []
197 # If not '', a 'Last updated on:' timestamp is inserted at every page bottom,
198 # using the given strftime format.
199 #html_last_updated_fmt = '%b %d, %Y'
201 # If true, SmartyPants will be used to convert quotes and dashes to
202 # typographically correct entities.
203 #html_use_smartypants = True
205 # Custom sidebar templates, maps document names to template names.
206 #html_sidebars = {}
208 # Additional templates that should be rendered to pages, maps page names to
209 # template names.
210 #html_additional_pages = {}
212 # If false, no module index is generated.
213 #html_domain_indices = True
215 # If false, no index is generated.
216 #html_use_index = True
218 # If true, the index is split into individual pages for each letter.
219 #html_split_index = False
221 # If true, links to the reST sources are added to the pages.
222 #html_show_sourcelink = True
224 # If true, "Created using Sphinx" is shown in the HTML footer. Default is True.
225 #html_show_sphinx = True
227 # If true, "(C) Copyright ..." is shown in the HTML footer. Default is True.
228 #html_show_copyright = True
230 # If true, an OpenSearch description file will be output, and all pages will
231 # contain a <link> tag referring to it. The value of this option must be the
232 # base URL from which the finished HTML is served.
233 #html_use_opensearch = ''
235 # This is the file name suffix for HTML files (e.g. ".xhtml").
236 #html_file_suffix = None
238 # Language to be used for generating the HTML full-text search index.
239 # Sphinx supports the following languages:
240 # 'da', 'de', 'en', 'es', 'fi', 'fr', 'h', 'it', 'ja'
241 # 'nl', 'no', 'pt', 'ro', 'r', 'sv', 'tr'
242 #html_search_language = 'en'
244 # A dictionary with options for the search language support, empty by default.
245 # Now only 'ja' uses this config value
246 #html_search_options = {'type': 'default'}
248 # The name of a javascript file (relative to the configuration directory) that
249 # implements a search results scorer. If empty, the default will be used.
250 #html_search_scorer = 'scorer.js'
252 # Output file base name for HTML help builder.
253 htmlhelp_basename = 'TheLinuxKerneldoc'
255 # -- Options for LaTeX output ---------------------------------------------
257 latex_elements = {
258 # The paper size ('letterpaper' or 'a4paper').
259 'papersize': 'a4paper',
261 # The font size ('10pt', '11pt' or '12pt').
262 'pointsize': '8pt',
264 # Latex figure (float) alignment
265 #'figure_align': 'htbp',
267 # Don't mangle with UTF-8 chars
268 'inputenc': '',
269 'utf8extra': '',
271 # Additional stuff for the LaTeX preamble.
272 'preamble': '''
273 % Use some font with UTF-8 support with XeLaTeX
274 \\usepackage{fontspec}
275 \\setsansfont{DejaVu Serif}
276 \\setromanfont{DejaVu Sans}
277 \\setmonofont{DejaVu Sans Mono}
279 '''
280 }
282 # Fix reference escape troubles with Sphinx 1.4.x
283 if major == 1 and minor > 3:
284 latex_elements['preamble'] += '\\renewcommand*{\\DUrole}[2]{ #2 }\n'
286 if major == 1 and minor <= 4:
287 latex_elements['preamble'] += '\\usepackage[margin=0.5in, top=1in, bottom=1in]{geometry}'
288 elif major == 1 and (minor > 5 or (minor == 5 and patch >= 3)):
289 latex_elements['sphinxsetup'] = 'hmargin=0.5in, vmargin=1in'
290 latex_elements['preamble'] += '\\fvset{fontsize=auto}\n'
292 # Customize notice background colors on Sphinx < 1.6:
293 if major == 1 and minor < 6:
294 latex_elements['preamble'] += '''
295 \\usepackage{ifthen}
297 % Put notes in color and let them be inside a table
298 \\definecolor{NoteColor}{RGB}{204,255,255}
299 \\definecolor{WarningColor}{RGB}{255,204,204}
300 \\definecolor{AttentionColor}{RGB}{255,255,204}
301 \\definecolor{ImportantColor}{RGB}{192,255,204}
302 \\definecolor{OtherColor}{RGB}{204,204,204}
303 \\newlength{\\mynoticelength}
304 \\makeatletter\\newenvironment{coloredbox}[1]{%
305 \\setlength{\\fboxrule}{1pt}
306 \\setlength{\\fboxsep}{7pt}
307 \\setlength{\\mynoticelength}{\\linewidth}
308 \\addtolength{\\mynoticelength}{-2\\fboxsep}
309 \\addtolength{\\mynoticelength}{-2\\fboxrule}
310 \\begin{lrbox}{\\@tempboxa}\\begin{minipage}{\\mynoticelength}}{\\end{minipage}\\end{lrbox}%
311 \\ifthenelse%
312 {\\equal{\\py@noticetype}{note}}%
313 {\\colorbox{NoteColor}{\\usebox{\\@tempboxa}}}%
314 {%
315 \\ifthenelse%
316 {\\equal{\\py@noticetype}{warning}}%
317 {\\colorbox{WarningColor}{\\usebox{\\@tempboxa}}}%
318 {%
319 \\ifthenelse%
320 {\\equal{\\py@noticetype}{attention}}%
321 {\\colorbox{AttentionColor}{\\usebox{\\@tempboxa}}}%
322 {%
323 \\ifthenelse%
324 {\\equal{\\py@noticetype}{important}}%
325 {\\colorbox{ImportantColor}{\\usebox{\\@tempboxa}}}%
326 {\\colorbox{OtherColor}{\\usebox{\\@tempboxa}}}%
327 }%
328 }%
329 }%
330 }\\makeatother
332 \\makeatletter
333 \\renewenvironment{notice}[2]{%
334 \\def\\py@noticetype{#1}
335 \\begin{coloredbox}{#1}
336 \\bf\\it
337 \\par\\strong{#2}
338 \\csname py@noticestart@#1\\endcsname
339 }
340 {
341 \\csname py@noticeend@\\py@noticetype\\endcsname
342 \\end{coloredbox}
343 }
344 \\makeatother
346 '''
348 # With Sphinx 1.6, it is possible to change the Bg color directly
349 # by using:
350 # \definecolor{sphinxnoteBgColor}{RGB}{204,255,255}
351 # \definecolor{sphinxwarningBgColor}{RGB}{255,204,204}
352 # \definecolor{sphinxattentionBgColor}{RGB}{255,255,204}
353 # \definecolor{sphinximportantBgColor}{RGB}{192,255,204}
354 #
355 # However, it require to use sphinx heavy box with:
356 #
357 # \renewenvironment{sphinxlightbox} {%
358 # \\begin{sphinxheavybox}
359 # }
360 # \\end{sphinxheavybox}
361 # }
362 #
363 # Unfortunately, the implementation is buggy: if a note is inside a
364 # table, it isn't displayed well. So, for now, let's use boring
365 # black and white notes.
367 # Grouping the document tree into LaTeX files. List of tuples
368 # (source start file, target name, title,
369 # author, documentclass [howto, manual, or own class]).
370 # Sorted in alphabetical order
371 latex_documents = [
372 ('admin-guide/index', 'linux-user.tex', 'Linux Kernel User Documentation',
373 'The kernel development community', 'manual'),
374 ('core-api/index', 'core-api.tex', 'The kernel core API manual',
375 'The kernel development community', 'manual'),
376 ('crypto/index', 'crypto-api.tex', 'Linux Kernel Crypto API manual',
377 'The kernel development community', 'manual'),
378 ('dev-tools/index', 'dev-tools.tex', 'Development tools for the Kernel',
379 'The kernel development community', 'manual'),
380 ('doc-guide/index', 'kernel-doc-guide.tex', 'Linux Kernel Documentation Guide',
381 'The kernel development community', 'manual'),
382 ('driver-api/index', 'driver-api.tex', 'The kernel driver API manual',
383 'The kernel development community', 'manual'),
384 ('filesystems/index', 'filesystems.tex', 'Linux Filesystems API',
385 'The kernel development community', 'manual'),
386 ('gpu/index', 'gpu.tex', 'Linux GPU Driver Developer\'s Guide',
387 'The kernel development community', 'manual'),
388 ('input/index', 'linux-input.tex', 'The Linux input driver subsystem',
389 'The kernel development community', 'manual'),
390 ('kernel-hacking/index', 'kernel-hacking.tex', 'Unreliable Guide To Hacking The Linux Kernel',
391 'The kernel development community', 'manual'),
392 ('media/index', 'media.tex', 'Linux Media Subsystem Documentation',
393 'The kernel development community', 'manual'),
394 ('networking/index', 'networking.tex', 'Linux Networking Documentation',
395 'The kernel development community', 'manual'),
396 ('process/index', 'development-process.tex', 'Linux Kernel Development Documentation',
397 'The kernel development community', 'manual'),
398 ('security/index', 'security.tex', 'The kernel security subsystem manual',
399 'The kernel development community', 'manual'),
400 ('sh/index', 'sh.tex', 'SuperH architecture implementation manual',
401 'The kernel development community', 'manual'),
402 ('sound/index', 'sound.tex', 'Linux Sound Subsystem Documentation',
403 'The kernel development community', 'manual'),
404 ('userspace-api/index', 'userspace-api.tex', 'The Linux kernel user-space API guide',
405 'The kernel development community', 'manual'),
406 ]
408 # The name of an image file (relative to this directory) to place at the top of
409 # the title page.
410 #latex_logo = None
412 # For "manual" documents, if this is true, then toplevel headings are parts,
413 # not chapters.
414 #latex_use_parts = False
416 # If true, show page references after internal links.
417 #latex_show_pagerefs = False
419 # If true, show URL addresses after external links.
420 #latex_show_urls = False
422 # Documents to append as an appendix to all manuals.
423 #latex_appendices = []
425 # If false, no module index is generated.
426 #latex_domain_indices = True
429 # -- Options for manual page output ---------------------------------------
431 # One entry per manual page. List of tuples
432 # (source start file, name, description, authors, manual section).
433 man_pages = [
434 (master_doc, 'thelinuxkernel', 'The Linux Kernel Documentation',
435 [author], 1)
436 ]
438 # If true, show URL addresses after external links.
439 #man_show_urls = False
442 # -- Options for Texinfo output -------------------------------------------
444 # Grouping the document tree into Texinfo files. List of tuples
445 # (source start file, target name, title, author,
446 # dir menu entry, description, category)
447 texinfo_documents = [
448 (master_doc, 'TheLinuxKernel', 'The Linux Kernel Documentation',
449 author, 'TheLinuxKernel', 'One line description of project.',
450 'Miscellaneous'),
451 ]
453 # Documents to append as an appendix to all manuals.
454 #texinfo_appendices = []
456 # If false, no module index is generated.
457 #texinfo_domain_indices = True
459 # How to display URL addresses: 'footnote', 'no', or 'inline'.
460 #texinfo_show_urls = 'footnote'
462 # If true, do not generate a @detailmenu in the "Top" node's menu.
463 #texinfo_no_detailmenu = False
466 # -- Options for Epub output ----------------------------------------------
468 # Bibliographic Dublin Core info.
469 epub_title = project
470 epub_author = author
471 epub_publisher = author
472 epub_copyright = copyright
474 # The basename for the epub file. It defaults to the project name.
475 #epub_basename = project
477 # The HTML theme for the epub output. Since the default themes are not
478 # optimized for small screen space, using the same theme for HTML and epub
479 # output is usually not wise. This defaults to 'epub', a theme designed to save
480 # visual space.
481 #epub_theme = 'epub'
483 # The language of the text. It defaults to the language option
484 # or 'en' if the language is not set.
485 #epub_language = ''
487 # The scheme of the identifier. Typical schemes are ISBN or URL.
488 #epub_scheme = ''
490 # The unique identifier of the text. This can be a ISBN number
491 # or the project homepage.
492 #epub_identifier = ''
494 # A unique identification for the text.
495 #epub_uid = ''
497 # A tuple containing the cover image and cover page html template filenames.
498 #epub_cover = ()
500 # A sequence of (type, uri, title) tuples for the guide element of content.opf.
501 #epub_guide = ()
503 # HTML files that should be inserted before the pages created by sphinx.
504 # The format is a list of tuples containing the path and title.
505 #epub_pre_files = []
507 # HTML files that should be inserted after the pages created by sphinx.
508 # The format is a list of tuples containing the path and title.
509 #epub_post_files = []
511 # A list of files that should not be packed into the epub file.
512 epub_exclude_files = ['search.html']
514 # The depth of the table of contents in toc.ncx.
515 #epub_tocdepth = 3
517 # Allow duplicate toc entries.
518 #epub_tocdup = True
520 # Choose between 'default' and 'includehidden'.
521 #epub_tocscope = 'default'
523 # Fix unsupported image types using the Pillow.
524 #epub_fix_images = False
526 # Scale large images.
527 #epub_max_image_width = 0
529 # How to display URL addresses: 'footnote', 'no', or 'inline'.
530 #epub_show_urls = 'inline'
532 # If false, no index is generated.
533 #epub_use_index = True
535 #=======
536 # rst2pdf
537 #
538 # Grouping the document tree into PDF files. List of tuples
539 # (source start file, target name, title, author, options).
540 #
541 # See the Sphinx chapter of http://ralsina.me/static/manual.pdf
542 #
543 # FIXME: Do not add the index file here; the result will be too big. Adding
544 # multiple PDF files here actually tries to get the cross-referencing right
545 # *between* PDF files.
546 pdf_documents = [
547 ('kernel-documentation', u'Kernel', u'Kernel', u'J. Random Bozo'),
548 ]
550 # kernel-doc extension configuration for running Sphinx directly (e.g. by Read
551 # the Docs). In a normal build, these are supplied from the Makefile via command
552 # line arguments.
553 kerneldoc_bin = '../scripts/kernel-doc'
554 kerneldoc_srctree = '..'
556 # ------------------------------------------------------------------------------
557 # Since loadConfig overwrites settings from the global namespace, it has to be
558 # the last statement in the conf.py file
559 # ------------------------------------------------------------------------------
560 loadConfig(globals())