]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/hwspinlock.git/blob - Documentation/devicetree/bindings/arm/cpus.txt
Merge branch 'userns-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/ebiederm...
[rpmsg/hwspinlock.git] / Documentation / devicetree / bindings / arm / cpus.txt
1 =================
2 ARM CPUs bindings
3 =================
5 The device tree allows to describe the layout of CPUs in a system through
6 the "cpus" node, which in turn contains a number of subnodes (ie "cpu")
7 defining properties for every cpu.
9 Bindings for CPU nodes follow the Devicetree Specification, available from:
11 https://www.devicetree.org/specifications/
13 with updates for 32-bit and 64-bit ARM systems provided in this document.
15 ================================
16 Convention used in this document
17 ================================
19 This document follows the conventions described in the Devicetree
20 Specification, with the addition:
22 - square brackets define bitfields, eg reg[7:0] value of the bitfield in
23   the reg property contained in bits 7 down to 0
25 =====================================
26 cpus and cpu node bindings definition
27 =====================================
29 The ARM architecture, in accordance with the Devicetree Specification,
30 requires the cpus and cpu nodes to be present and contain the properties
31 described below.
33 - cpus node
35         Description: Container of cpu nodes
37         The node name must be "cpus".
39         A cpus node must define the following properties:
41         - #address-cells
42                 Usage: required
43                 Value type: <u32>
45                 Definition depends on ARM architecture version and
46                 configuration:
48                         # On uniprocessor ARM architectures previous to v7
49                           value must be 1, to enable a simple enumeration
50                           scheme for processors that do not have a HW CPU
51                           identification register.
52                         # On 32-bit ARM 11 MPcore, ARM v7 or later systems
53                           value must be 1, that corresponds to CPUID/MPIDR
54                           registers sizes.
55                         # On ARM v8 64-bit systems value should be set to 2,
56                           that corresponds to the MPIDR_EL1 register size.
57                           If MPIDR_EL1[63:32] value is equal to 0 on all CPUs
58                           in the system, #address-cells can be set to 1, since
59                           MPIDR_EL1[63:32] bits are not used for CPUs
60                           identification.
61         - #size-cells
62                 Usage: required
63                 Value type: <u32>
64                 Definition: must be set to 0
66 - cpu node
68         Description: Describes a CPU in an ARM based system
70         PROPERTIES
72         - device_type
73                 Usage: required
74                 Value type: <string>
75                 Definition: must be "cpu"
76         - reg
77                 Usage and definition depend on ARM architecture version and
78                 configuration:
80                         # On uniprocessor ARM architectures previous to v7
81                           this property is required and must be set to 0.
83                         # On ARM 11 MPcore based systems this property is
84                           required and matches the CPUID[11:0] register bits.
86                           Bits [11:0] in the reg cell must be set to
87                           bits [11:0] in CPU ID register.
89                           All other bits in the reg cell must be set to 0.
91                         # On 32-bit ARM v7 or later systems this property is
92                           required and matches the CPU MPIDR[23:0] register
93                           bits.
95                           Bits [23:0] in the reg cell must be set to
96                           bits [23:0] in MPIDR.
98                           All other bits in the reg cell must be set to 0.
100                         # On ARM v8 64-bit systems this property is required
101                           and matches the MPIDR_EL1 register affinity bits.
103                           * If cpus node's #address-cells property is set to 2
105                             The first reg cell bits [7:0] must be set to
106                             bits [39:32] of MPIDR_EL1.
108                             The second reg cell bits [23:0] must be set to
109                             bits [23:0] of MPIDR_EL1.
111                           * If cpus node's #address-cells property is set to 1
113                             The reg cell bits [23:0] must be set to bits [23:0]
114                             of MPIDR_EL1.
116                           All other bits in the reg cells must be set to 0.
118         - compatible:
119                 Usage: required
120                 Value type: <string>
121                 Definition: should be one of:
122                             "arm,arm710t"
123                             "arm,arm720t"
124                             "arm,arm740t"
125                             "arm,arm7ej-s"
126                             "arm,arm7tdmi"
127                             "arm,arm7tdmi-s"
128                             "arm,arm9es"
129                             "arm,arm9ej-s"
130                             "arm,arm920t"
131                             "arm,arm922t"
132                             "arm,arm925"
133                             "arm,arm926e-s"
134                             "arm,arm926ej-s"
135                             "arm,arm940t"
136                             "arm,arm946e-s"
137                             "arm,arm966e-s"
138                             "arm,arm968e-s"
139                             "arm,arm9tdmi"
140                             "arm,arm1020e"
141                             "arm,arm1020t"
142                             "arm,arm1022e"
143                             "arm,arm1026ej-s"
144                             "arm,arm1136j-s"
145                             "arm,arm1136jf-s"
146                             "arm,arm1156t2-s"
147                             "arm,arm1156t2f-s"
148                             "arm,arm1176jzf"
149                             "arm,arm1176jz-s"
150                             "arm,arm1176jzf-s"
151                             "arm,arm11mpcore"
152                             "arm,cortex-a5"
153                             "arm,cortex-a7"
154                             "arm,cortex-a8"
155                             "arm,cortex-a9"
156                             "arm,cortex-a12"
157                             "arm,cortex-a15"
158                             "arm,cortex-a17"
159                             "arm,cortex-a53"
160                             "arm,cortex-a57"
161                             "arm,cortex-a72"
162                             "arm,cortex-a73"
163                             "arm,cortex-m0"
164                             "arm,cortex-m0+"
165                             "arm,cortex-m1"
166                             "arm,cortex-m3"
167                             "arm,cortex-m4"
168                             "arm,cortex-r4"
169                             "arm,cortex-r5"
170                             "arm,cortex-r7"
171                             "brcm,brahma-b15"
172                             "brcm,brahma-b53"
173                             "brcm,vulcan"
174                             "cavium,thunder"
175                             "cavium,thunder2"
176                             "faraday,fa526"
177                             "intel,sa110"
178                             "intel,sa1100"
179                             "marvell,feroceon"
180                             "marvell,mohawk"
181                             "marvell,pj4a"
182                             "marvell,pj4b"
183                             "marvell,sheeva-v5"
184                             "nvidia,tegra132-denver"
185                             "nvidia,tegra186-denver"
186                             "nvidia,tegra194-carmel"
187                             "qcom,krait"
188                             "qcom,kryo"
189                             "qcom,kryo385"
190                             "qcom,scorpion"
191         - enable-method
192                 Value type: <stringlist>
193                 Usage and definition depend on ARM architecture version.
194                         # On ARM v8 64-bit this property is required and must
195                           be one of:
196                              "psci"
197                              "spin-table"
198                         # On ARM 32-bit systems this property is optional and
199                           can be one of:
200                             "actions,s500-smp"
201                             "allwinner,sun6i-a31"
202                             "allwinner,sun8i-a23"
203                             "allwinner,sun9i-a80-smp"
204                             "amlogic,meson8-smp"
205                             "amlogic,meson8b-smp"
206                             "arm,realview-smp"
207                             "brcm,bcm11351-cpu-method"
208                             "brcm,bcm23550"
209                             "brcm,bcm2836-smp"
210                             "brcm,bcm-nsp-smp"
211                             "brcm,brahma-b15"
212                             "marvell,armada-375-smp"
213                             "marvell,armada-380-smp"
214                             "marvell,armada-390-smp"
215                             "marvell,armada-xp-smp"
216                             "marvell,98dx3236-smp"
217                             "mediatek,mt6589-smp"
218                             "mediatek,mt81xx-tz-smp"
219                             "qcom,gcc-msm8660"
220                             "qcom,kpss-acc-v1"
221                             "qcom,kpss-acc-v2"
222                             "renesas,apmu"
223                             "renesas,r9a06g032-smp"
224                             "rockchip,rk3036-smp"
225                             "rockchip,rk3066-smp"
226                             "ste,dbx500-smp"
228         - cpu-release-addr
229                 Usage: required for systems that have an "enable-method"
230                        property value of "spin-table".
231                 Value type: <prop-encoded-array>
232                 Definition:
233                         # On ARM v8 64-bit systems must be a two cell
234                           property identifying a 64-bit zero-initialised
235                           memory location.
237         - qcom,saw
238                 Usage: required for systems that have an "enable-method"
239                        property value of "qcom,kpss-acc-v1" or
240                        "qcom,kpss-acc-v2"
241                 Value type: <phandle>
242                 Definition: Specifies the SAW[1] node associated with this CPU.
244         - qcom,acc
245                 Usage: required for systems that have an "enable-method"
246                        property value of "qcom,kpss-acc-v1" or
247                        "qcom,kpss-acc-v2"
248                 Value type: <phandle>
249                 Definition: Specifies the ACC[2] node associated with this CPU.
251         - cpu-idle-states
252                 Usage: Optional
253                 Value type: <prop-encoded-array>
254                 Definition:
255                         # List of phandles to idle state nodes supported
256                           by this cpu [3].
258         - capacity-dmips-mhz
259                 Usage: Optional
260                 Value type: <u32>
261                 Definition:
262                         # u32 value representing CPU capacity [4] in
263                           DMIPS/MHz, relative to highest capacity-dmips-mhz
264                           in the system.
266         - rockchip,pmu
267                 Usage: optional for systems that have an "enable-method"
268                        property value of "rockchip,rk3066-smp"
269                        While optional, it is the preferred way to get access to
270                        the cpu-core power-domains.
271                 Value type: <phandle>
272                 Definition: Specifies the syscon node controlling the cpu core
273                             power domains.
275         - dynamic-power-coefficient
276                 Usage: optional
277                 Value type: <prop-encoded-array>
278                 Definition: A u32 value that represents the running time dynamic
279                             power coefficient in units of mW/MHz/uV^2. The
280                             coefficient can either be calculated from power
281                             measurements or derived by analysis.
283                             The dynamic power consumption of the CPU  is
284                             proportional to the square of the Voltage (V) and
285                             the clock frequency (f). The coefficient is used to
286                             calculate the dynamic power as below -
288                             Pdyn = dynamic-power-coefficient * V^2 * f
290                             where voltage is in uV, frequency is in MHz.
292 Example 1 (dual-cluster big.LITTLE system 32-bit):
294         cpus {
295                 #size-cells = <0>;
296                 #address-cells = <1>;
298                 cpu@0 {
299                         device_type = "cpu";
300                         compatible = "arm,cortex-a15";
301                         reg = <0x0>;
302                 };
304                 cpu@1 {
305                         device_type = "cpu";
306                         compatible = "arm,cortex-a15";
307                         reg = <0x1>;
308                 };
310                 cpu@100 {
311                         device_type = "cpu";
312                         compatible = "arm,cortex-a7";
313                         reg = <0x100>;
314                 };
316                 cpu@101 {
317                         device_type = "cpu";
318                         compatible = "arm,cortex-a7";
319                         reg = <0x101>;
320                 };
321         };
323 Example 2 (Cortex-A8 uniprocessor 32-bit system):
325         cpus {
326                 #size-cells = <0>;
327                 #address-cells = <1>;
329                 cpu@0 {
330                         device_type = "cpu";
331                         compatible = "arm,cortex-a8";
332                         reg = <0x0>;
333                 };
334         };
336 Example 3 (ARM 926EJ-S uniprocessor 32-bit system):
338         cpus {
339                 #size-cells = <0>;
340                 #address-cells = <1>;
342                 cpu@0 {
343                         device_type = "cpu";
344                         compatible = "arm,arm926ej-s";
345                         reg = <0x0>;
346                 };
347         };
349 Example 4 (ARM Cortex-A57 64-bit system):
351 cpus {
352         #size-cells = <0>;
353         #address-cells = <2>;
355         cpu@0 {
356                 device_type = "cpu";
357                 compatible = "arm,cortex-a57";
358                 reg = <0x0 0x0>;
359                 enable-method = "spin-table";
360                 cpu-release-addr = <0 0x20000000>;
361         };
363         cpu@1 {
364                 device_type = "cpu";
365                 compatible = "arm,cortex-a57";
366                 reg = <0x0 0x1>;
367                 enable-method = "spin-table";
368                 cpu-release-addr = <0 0x20000000>;
369         };
371         cpu@100 {
372                 device_type = "cpu";
373                 compatible = "arm,cortex-a57";
374                 reg = <0x0 0x100>;
375                 enable-method = "spin-table";
376                 cpu-release-addr = <0 0x20000000>;
377         };
379         cpu@101 {
380                 device_type = "cpu";
381                 compatible = "arm,cortex-a57";
382                 reg = <0x0 0x101>;
383                 enable-method = "spin-table";
384                 cpu-release-addr = <0 0x20000000>;
385         };
387         cpu@10000 {
388                 device_type = "cpu";
389                 compatible = "arm,cortex-a57";
390                 reg = <0x0 0x10000>;
391                 enable-method = "spin-table";
392                 cpu-release-addr = <0 0x20000000>;
393         };
395         cpu@10001 {
396                 device_type = "cpu";
397                 compatible = "arm,cortex-a57";
398                 reg = <0x0 0x10001>;
399                 enable-method = "spin-table";
400                 cpu-release-addr = <0 0x20000000>;
401         };
403         cpu@10100 {
404                 device_type = "cpu";
405                 compatible = "arm,cortex-a57";
406                 reg = <0x0 0x10100>;
407                 enable-method = "spin-table";
408                 cpu-release-addr = <0 0x20000000>;
409         };
411         cpu@10101 {
412                 device_type = "cpu";
413                 compatible = "arm,cortex-a57";
414                 reg = <0x0 0x10101>;
415                 enable-method = "spin-table";
416                 cpu-release-addr = <0 0x20000000>;
417         };
419         cpu@100000000 {
420                 device_type = "cpu";
421                 compatible = "arm,cortex-a57";
422                 reg = <0x1 0x0>;
423                 enable-method = "spin-table";
424                 cpu-release-addr = <0 0x20000000>;
425         };
427         cpu@100000001 {
428                 device_type = "cpu";
429                 compatible = "arm,cortex-a57";
430                 reg = <0x1 0x1>;
431                 enable-method = "spin-table";
432                 cpu-release-addr = <0 0x20000000>;
433         };
435         cpu@100000100 {
436                 device_type = "cpu";
437                 compatible = "arm,cortex-a57";
438                 reg = <0x1 0x100>;
439                 enable-method = "spin-table";
440                 cpu-release-addr = <0 0x20000000>;
441         };
443         cpu@100000101 {
444                 device_type = "cpu";
445                 compatible = "arm,cortex-a57";
446                 reg = <0x1 0x101>;
447                 enable-method = "spin-table";
448                 cpu-release-addr = <0 0x20000000>;
449         };
451         cpu@100010000 {
452                 device_type = "cpu";
453                 compatible = "arm,cortex-a57";
454                 reg = <0x1 0x10000>;
455                 enable-method = "spin-table";
456                 cpu-release-addr = <0 0x20000000>;
457         };
459         cpu@100010001 {
460                 device_type = "cpu";
461                 compatible = "arm,cortex-a57";
462                 reg = <0x1 0x10001>;
463                 enable-method = "spin-table";
464                 cpu-release-addr = <0 0x20000000>;
465         };
467         cpu@100010100 {
468                 device_type = "cpu";
469                 compatible = "arm,cortex-a57";
470                 reg = <0x1 0x10100>;
471                 enable-method = "spin-table";
472                 cpu-release-addr = <0 0x20000000>;
473         };
475         cpu@100010101 {
476                 device_type = "cpu";
477                 compatible = "arm,cortex-a57";
478                 reg = <0x1 0x10101>;
479                 enable-method = "spin-table";
480                 cpu-release-addr = <0 0x20000000>;
481         };
482 };
484 --
485 [1] arm/msm/qcom,saw2.txt
486 [2] arm/msm/qcom,kpss-acc.txt
487 [3] ARM Linux kernel documentation - idle states bindings
488     Documentation/devicetree/bindings/arm/idle-states.txt
489 [4] ARM Linux kernel documentation - cpu capacity bindings
490     Documentation/devicetree/bindings/arm/cpu-capacity.txt