]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/hwspinlock.git/blob - Documentation/kernel-per-CPU-kthreads.txt
soc: ti: wkup_m3_ipc: Add support for i2c voltage scaling
[rpmsg/hwspinlock.git] / Documentation / kernel-per-CPU-kthreads.txt
1 ==========================================
2 Reducing OS jitter due to per-cpu kthreads
3 ==========================================
5 This document lists per-CPU kthreads in the Linux kernel and presents
6 options to control their OS jitter.  Note that non-per-CPU kthreads are
7 not listed here.  To reduce OS jitter from non-per-CPU kthreads, bind
8 them to a "housekeeping" CPU dedicated to such work.
10 References
11 ==========
13 -       Documentation/IRQ-affinity.txt:  Binding interrupts to sets of CPUs.
15 -       Documentation/cgroup-v1:  Using cgroups to bind tasks to sets of CPUs.
17 -       man taskset:  Using the taskset command to bind tasks to sets
18         of CPUs.
20 -       man sched_setaffinity:  Using the sched_setaffinity() system
21         call to bind tasks to sets of CPUs.
23 -       /sys/devices/system/cpu/cpuN/online:  Control CPU N's hotplug state,
24         writing "0" to offline and "1" to online.
26 -       In order to locate kernel-generated OS jitter on CPU N:
28                 cd /sys/kernel/debug/tracing
29                 echo 1 > max_graph_depth # Increase the "1" for more detail
30                 echo function_graph > current_tracer
31                 # run workload
32                 cat per_cpu/cpuN/trace
34 kthreads
35 ========
37 Name:
38   ehca_comp/%u
40 Purpose:
41   Periodically process Infiniband-related work.
43 To reduce its OS jitter, do any of the following:
45 1.      Don't use eHCA Infiniband hardware, instead choosing hardware
46         that does not require per-CPU kthreads.  This will prevent these
47         kthreads from being created in the first place.  (This will
48         work for most people, as this hardware, though important, is
49         relatively old and is produced in relatively low unit volumes.)
50 2.      Do all eHCA-Infiniband-related work on other CPUs, including
51         interrupts.
52 3.      Rework the eHCA driver so that its per-CPU kthreads are
53         provisioned only on selected CPUs.
56 Name:
57   irq/%d-%s
59 Purpose:
60   Handle threaded interrupts.
62 To reduce its OS jitter, do the following:
64 1.      Use irq affinity to force the irq threads to execute on
65         some other CPU.
67 Name:
68   kcmtpd_ctr_%d
70 Purpose:
71   Handle Bluetooth work.
73 To reduce its OS jitter, do one of the following:
75 1.      Don't use Bluetooth, in which case these kthreads won't be
76         created in the first place.
77 2.      Use irq affinity to force Bluetooth-related interrupts to
78         occur on some other CPU and furthermore initiate all
79         Bluetooth activity on some other CPU.
81 Name:
82   ksoftirqd/%u
84 Purpose:
85   Execute softirq handlers when threaded or when under heavy load.
87 To reduce its OS jitter, each softirq vector must be handled
88 separately as follows:
90 TIMER_SOFTIRQ
91 -------------
93 Do all of the following:
95 1.      To the extent possible, keep the CPU out of the kernel when it
96         is non-idle, for example, by avoiding system calls and by forcing
97         both kernel threads and interrupts to execute elsewhere.
98 2.      Build with CONFIG_HOTPLUG_CPU=y.  After boot completes, force
99         the CPU offline, then bring it back online.  This forces
100         recurring timers to migrate elsewhere.  If you are concerned
101         with multiple CPUs, force them all offline before bringing the
102         first one back online.  Once you have onlined the CPUs in question,
103         do not offline any other CPUs, because doing so could force the
104         timer back onto one of the CPUs in question.
106 NET_TX_SOFTIRQ and NET_RX_SOFTIRQ
107 ---------------------------------
109 Do all of the following:
111 1.      Force networking interrupts onto other CPUs.
112 2.      Initiate any network I/O on other CPUs.
113 3.      Once your application has started, prevent CPU-hotplug operations
114         from being initiated from tasks that might run on the CPU to
115         be de-jittered.  (It is OK to force this CPU offline and then
116         bring it back online before you start your application.)
118 BLOCK_SOFTIRQ
119 -------------
121 Do all of the following:
123 1.      Force block-device interrupts onto some other CPU.
124 2.      Initiate any block I/O on other CPUs.
125 3.      Once your application has started, prevent CPU-hotplug operations
126         from being initiated from tasks that might run on the CPU to
127         be de-jittered.  (It is OK to force this CPU offline and then
128         bring it back online before you start your application.)
130 IRQ_POLL_SOFTIRQ
131 ----------------
133 Do all of the following:
135 1.      Force block-device interrupts onto some other CPU.
136 2.      Initiate any block I/O and block-I/O polling on other CPUs.
137 3.      Once your application has started, prevent CPU-hotplug operations
138         from being initiated from tasks that might run on the CPU to
139         be de-jittered.  (It is OK to force this CPU offline and then
140         bring it back online before you start your application.)
142 TASKLET_SOFTIRQ
143 ---------------
145 Do one or more of the following:
147 1.      Avoid use of drivers that use tasklets.  (Such drivers will contain
148         calls to things like tasklet_schedule().)
149 2.      Convert all drivers that you must use from tasklets to workqueues.
150 3.      Force interrupts for drivers using tasklets onto other CPUs,
151         and also do I/O involving these drivers on other CPUs.
153 SCHED_SOFTIRQ
154 -------------
156 Do all of the following:
158 1.      Avoid sending scheduler IPIs to the CPU to be de-jittered,
159         for example, ensure that at most one runnable kthread is present
160         on that CPU.  If a thread that expects to run on the de-jittered
161         CPU awakens, the scheduler will send an IPI that can result in
162         a subsequent SCHED_SOFTIRQ.
163 2.      CONFIG_NO_HZ_FULL=y and ensure that the CPU to be de-jittered
164         is marked as an adaptive-ticks CPU using the "nohz_full="
165         boot parameter.  This reduces the number of scheduler-clock
166         interrupts that the de-jittered CPU receives, minimizing its
167         chances of being selected to do the load balancing work that
168         runs in SCHED_SOFTIRQ context.
169 3.      To the extent possible, keep the CPU out of the kernel when it
170         is non-idle, for example, by avoiding system calls and by
171         forcing both kernel threads and interrupts to execute elsewhere.
172         This further reduces the number of scheduler-clock interrupts
173         received by the de-jittered CPU.
175 HRTIMER_SOFTIRQ
176 ---------------
178 Do all of the following:
180 1.      To the extent possible, keep the CPU out of the kernel when it
181         is non-idle.  For example, avoid system calls and force both
182         kernel threads and interrupts to execute elsewhere.
183 2.      Build with CONFIG_HOTPLUG_CPU=y.  Once boot completes, force the
184         CPU offline, then bring it back online.  This forces recurring
185         timers to migrate elsewhere.  If you are concerned with multiple
186         CPUs, force them all offline before bringing the first one
187         back online.  Once you have onlined the CPUs in question, do not
188         offline any other CPUs, because doing so could force the timer
189         back onto one of the CPUs in question.
191 RCU_SOFTIRQ
192 -----------
194 Do at least one of the following:
196 1.      Offload callbacks and keep the CPU in either dyntick-idle or
197         adaptive-ticks state by doing all of the following:
199         a.      CONFIG_NO_HZ_FULL=y and ensure that the CPU to be
200                 de-jittered is marked as an adaptive-ticks CPU using the
201                 "nohz_full=" boot parameter.  Bind the rcuo kthreads to
202                 housekeeping CPUs, which can tolerate OS jitter.
203         b.      To the extent possible, keep the CPU out of the kernel
204                 when it is non-idle, for example, by avoiding system
205                 calls and by forcing both kernel threads and interrupts
206                 to execute elsewhere.
208 2.      Enable RCU to do its processing remotely via dyntick-idle by
209         doing all of the following:
211         a.      Build with CONFIG_NO_HZ=y and CONFIG_RCU_FAST_NO_HZ=y.
212         b.      Ensure that the CPU goes idle frequently, allowing other
213                 CPUs to detect that it has passed through an RCU quiescent
214                 state.  If the kernel is built with CONFIG_NO_HZ_FULL=y,
215                 userspace execution also allows other CPUs to detect that
216                 the CPU in question has passed through a quiescent state.
217         c.      To the extent possible, keep the CPU out of the kernel
218                 when it is non-idle, for example, by avoiding system
219                 calls and by forcing both kernel threads and interrupts
220                 to execute elsewhere.
222 Name:
223   kworker/%u:%d%s (cpu, id, priority)
225 Purpose:
226   Execute workqueue requests
228 To reduce its OS jitter, do any of the following:
230 1.      Run your workload at a real-time priority, which will allow
231         preempting the kworker daemons.
232 2.      A given workqueue can be made visible in the sysfs filesystem
233         by passing the WQ_SYSFS to that workqueue's alloc_workqueue().
234         Such a workqueue can be confined to a given subset of the
235         CPUs using the ``/sys/devices/virtual/workqueue/*/cpumask`` sysfs
236         files.  The set of WQ_SYSFS workqueues can be displayed using
237         "ls sys/devices/virtual/workqueue".  That said, the workqueues
238         maintainer would like to caution people against indiscriminately
239         sprinkling WQ_SYSFS across all the workqueues.  The reason for
240         caution is that it is easy to add WQ_SYSFS, but because sysfs is
241         part of the formal user/kernel API, it can be nearly impossible
242         to remove it, even if its addition was a mistake.
243 3.      Do any of the following needed to avoid jitter that your
244         application cannot tolerate:
246         a.      Build your kernel with CONFIG_SLUB=y rather than
247                 CONFIG_SLAB=y, thus avoiding the slab allocator's periodic
248                 use of each CPU's workqueues to run its cache_reap()
249                 function.
250         b.      Avoid using oprofile, thus avoiding OS jitter from
251                 wq_sync_buffer().
252         c.      Limit your CPU frequency so that a CPU-frequency
253                 governor is not required, possibly enlisting the aid of
254                 special heatsinks or other cooling technologies.  If done
255                 correctly, and if you CPU architecture permits, you should
256                 be able to build your kernel with CONFIG_CPU_FREQ=n to
257                 avoid the CPU-frequency governor periodically running
258                 on each CPU, including cs_dbs_timer() and od_dbs_timer().
260                 WARNING:  Please check your CPU specifications to
261                 make sure that this is safe on your particular system.
262         d.      As of v3.18, Christoph Lameter's on-demand vmstat workers
263                 commit prevents OS jitter due to vmstat_update() on
264                 CONFIG_SMP=y systems.  Before v3.18, is not possible
265                 to entirely get rid of the OS jitter, but you can
266                 decrease its frequency by writing a large value to
267                 /proc/sys/vm/stat_interval.  The default value is HZ,
268                 for an interval of one second.  Of course, larger values
269                 will make your virtual-memory statistics update more
270                 slowly.  Of course, you can also run your workload at
271                 a real-time priority, thus preempting vmstat_update(),
272                 but if your workload is CPU-bound, this is a bad idea.
273                 However, there is an RFC patch from Christoph Lameter
274                 (based on an earlier one from Gilad Ben-Yossef) that
275                 reduces or even eliminates vmstat overhead for some
276                 workloads at https://lkml.org/lkml/2013/9/4/379.
277         e.      Boot with "elevator=noop" to avoid workqueue use by
278                 the block layer.
279         f.      If running on high-end powerpc servers, build with
280                 CONFIG_PPC_RTAS_DAEMON=n.  This prevents the RTAS
281                 daemon from running on each CPU every second or so.
282                 (This will require editing Kconfig files and will defeat
283                 this platform's RAS functionality.)  This avoids jitter
284                 due to the rtas_event_scan() function.
285                 WARNING:  Please check your CPU specifications to
286                 make sure that this is safe on your particular system.
287         g.      If running on Cell Processor, build your kernel with
288                 CBE_CPUFREQ_SPU_GOVERNOR=n to avoid OS jitter from
289                 spu_gov_work().
290                 WARNING:  Please check your CPU specifications to
291                 make sure that this is safe on your particular system.
292         h.      If running on PowerMAC, build your kernel with
293                 CONFIG_PMAC_RACKMETER=n to disable the CPU-meter,
294                 avoiding OS jitter from rackmeter_do_timer().
296 Name:
297   rcuc/%u
299 Purpose:
300   Execute RCU callbacks in CONFIG_RCU_BOOST=y kernels.
302 To reduce its OS jitter, do at least one of the following:
304 1.      Build the kernel with CONFIG_PREEMPT=n.  This prevents these
305         kthreads from being created in the first place, and also obviates
306         the need for RCU priority boosting.  This approach is feasible
307         for workloads that do not require high degrees of responsiveness.
308 2.      Build the kernel with CONFIG_RCU_BOOST=n.  This prevents these
309         kthreads from being created in the first place.  This approach
310         is feasible only if your workload never requires RCU priority
311         boosting, for example, if you ensure frequent idle time on all
312         CPUs that might execute within the kernel.
313 3.      Build with CONFIG_RCU_NOCB_CPU=y and boot with the rcu_nocbs=
314         boot parameter offloading RCU callbacks from all CPUs susceptible
315         to OS jitter.  This approach prevents the rcuc/%u kthreads from
316         having any work to do, so that they are never awakened.
317 4.      Ensure that the CPU never enters the kernel, and, in particular,
318         avoid initiating any CPU hotplug operations on this CPU.  This is
319         another way of preventing any callbacks from being queued on the
320         CPU, again preventing the rcuc/%u kthreads from having any work
321         to do.
323 Name:
324   rcuob/%d, rcuop/%d, and rcuos/%d
326 Purpose:
327   Offload RCU callbacks from the corresponding CPU.
329 To reduce its OS jitter, do at least one of the following:
331 1.      Use affinity, cgroups, or other mechanism to force these kthreads
332         to execute on some other CPU.
333 2.      Build with CONFIG_RCU_NOCB_CPU=n, which will prevent these
334         kthreads from being created in the first place.  However, please
335         note that this will not eliminate OS jitter, but will instead
336         shift it to RCU_SOFTIRQ.
338 Name:
339   watchdog/%u
341 Purpose:
342   Detect software lockups on each CPU.
344 To reduce its OS jitter, do at least one of the following:
346 1.      Build with CONFIG_LOCKUP_DETECTOR=n, which will prevent these
347         kthreads from being created in the first place.
348 2.      Boot with "nosoftlockup=0", which will also prevent these kthreads
349         from being created.  Other related watchdog and softlockup boot
350         parameters may be found in Documentation/admin-guide/kernel-parameters.rst
351         and Documentation/watchdog/watchdog-parameters.txt.
352 3.      Echo a zero to /proc/sys/kernel/watchdog to disable the
353         watchdog timer.
354 4.      Echo a large number of /proc/sys/kernel/watchdog_thresh in
355         order to reduce the frequency of OS jitter due to the watchdog
356         timer down to a level that is acceptable for your workload.