ARM: OMAP2+: omap_hwmod: Introduce HWMOD_NEEDS_REIDLE
[rpmsg/hwspinlock.git] / arch / arm / mach-omap2 / omap_device.c
1 /*
2  * omap_device implementation
3  *
4  * Copyright (C) 2009-2010 Nokia Corporation
5  * Paul Walmsley, Kevin Hilman
6  *
7  * Developed in collaboration with (alphabetical order): Benoit
8  * Cousson, Thara Gopinath, Tony Lindgren, Rajendra Nayak, Vikram
9  * Pandita, Sakari Poussa, Anand Sawant, Santosh Shilimkar, Richard
10  * Woodruff
11  *
12  * This program is free software; you can redistribute it and/or modify
13  * it under the terms of the GNU General Public License version 2 as
14  * published by the Free Software Foundation.
15  *
16  * This code provides a consistent interface for OMAP device drivers
17  * to control power management and interconnect properties of their
18  * devices.
19  *
20  * In the medium- to long-term, this code should be implemented as a
21  * proper omap_bus/omap_device in Linux, no more platform_data func
22  * pointers
23  *
24  *
25  */
26 #undef DEBUG
28 #include <linux/kernel.h>
29 #include <linux/platform_device.h>
30 #include <linux/slab.h>
31 #include <linux/err.h>
32 #include <linux/io.h>
33 #include <linux/clk.h>
34 #include <linux/clkdev.h>
35 #include <linux/pm_domain.h>
36 #include <linux/pm_runtime.h>
37 #include <linux/of.h>
38 #include <linux/of_address.h>
39 #include <linux/of_irq.h>
40 #include <linux/notifier.h>
42 #include "common.h"
43 #include "soc.h"
44 #include "omap_device.h"
45 #include "omap_hwmod.h"
47 /* Private functions */
49 static void _add_clkdev(struct omap_device *od, const char *clk_alias,
50                        const char *clk_name)
51 {
52         struct clk *r;
53         int rc;
55         if (!clk_alias || !clk_name)
56                 return;
58         dev_dbg(&od->pdev->dev, "Creating %s -> %s\n", clk_alias, clk_name);
60         r = clk_get_sys(dev_name(&od->pdev->dev), clk_alias);
61         if (!IS_ERR(r)) {
62                 dev_dbg(&od->pdev->dev,
63                          "alias %s already exists\n", clk_alias);
64                 clk_put(r);
65                 return;
66         }
68         r = clk_get_sys(NULL, clk_name);
70         if (IS_ERR(r)) {
71                 struct of_phandle_args clkspec;
73                 clkspec.np = of_find_node_by_name(NULL, clk_name);
75                 r = of_clk_get_from_provider(&clkspec);
77                 rc = clk_register_clkdev(r, clk_alias,
78                                          dev_name(&od->pdev->dev));
79         } else {
80                 rc = clk_add_alias(clk_alias, dev_name(&od->pdev->dev),
81                                    clk_name, NULL);
82         }
84         if (rc) {
85                 if (rc == -ENODEV || rc == -ENOMEM)
86                         dev_err(&od->pdev->dev,
87                                 "clkdev_alloc for %s failed\n", clk_alias);
88                 else
89                         dev_err(&od->pdev->dev,
90                                 "clk_get for %s failed\n", clk_name);
91         }
92 }
94 /**
95  * _add_hwmod_clocks_clkdev - Add clkdev entry for hwmod optional clocks
96  * and main clock
97  * @od: struct omap_device *od
98  * @oh: struct omap_hwmod *oh
99  *
100  * For the main clock and every optional clock present per hwmod per
101  * omap_device, this function adds an entry in the clkdev table of the
102  * form <dev-id=dev_name, con-id=role> if it does not exist already.
103  *
104  * The function is called from inside omap_device_build_ss(), after
105  * omap_device_register.
106  *
107  * This allows drivers to get a pointer to its optional clocks based on its role
108  * by calling clk_get(<dev*>, <role>).
109  * In the case of the main clock, a "fck" alias is used.
110  *
111  * No return value.
112  */
113 static void _add_hwmod_clocks_clkdev(struct omap_device *od,
114                                      struct omap_hwmod *oh)
116         int i;
118         _add_clkdev(od, "fck", oh->main_clk);
120         for (i = 0; i < oh->opt_clks_cnt; i++)
121                 _add_clkdev(od, oh->opt_clks[i].role, oh->opt_clks[i].clk);
125 /**
126  * omap_device_build_from_dt - build an omap_device with multiple hwmods
127  * @pdev_name: name of the platform_device driver to use
128  * @pdev_id: this platform_device's connection ID
129  * @oh: ptr to the single omap_hwmod that backs this omap_device
130  * @pdata: platform_data ptr to associate with the platform_device
131  * @pdata_len: amount of memory pointed to by @pdata
132  *
133  * Function for building an omap_device already registered from device-tree
134  *
135  * Returns 0 or PTR_ERR() on error.
136  */
137 static int omap_device_build_from_dt(struct platform_device *pdev)
139         struct omap_hwmod **hwmods;
140         struct omap_device *od;
141         struct omap_hwmod *oh;
142         struct device_node *node = pdev->dev.of_node;
143         struct resource res;
144         const char *oh_name;
145         int oh_cnt, i, ret = 0;
146         bool device_active = false, skip_pm_domain = false;
148         oh_cnt = of_property_count_strings(node, "ti,hwmods");
149         if (oh_cnt <= 0) {
150                 dev_dbg(&pdev->dev, "No 'hwmods' to build omap_device\n");
151                 return -ENODEV;
152         }
154         /* SDMA still needs special handling for omap_device_build() */
155         ret = of_property_read_string_index(node, "ti,hwmods", 0, &oh_name);
156         if (!ret && (!strncmp("dma_system", oh_name, 10) ||
157                      !strncmp("dma", oh_name, 3)))
158                 skip_pm_domain = true;
160         /* Use ti-sysc driver instead of omap_device? */
161         if (!skip_pm_domain &&
162             !omap_hwmod_parse_module_range(NULL, node, &res))
163                 return -ENODEV;
165         hwmods = kcalloc(oh_cnt, sizeof(struct omap_hwmod *), GFP_KERNEL);
166         if (!hwmods) {
167                 ret = -ENOMEM;
168                 goto odbfd_exit;
169         }
171         for (i = 0; i < oh_cnt; i++) {
172                 of_property_read_string_index(node, "ti,hwmods", i, &oh_name);
173                 oh = omap_hwmod_lookup(oh_name);
174                 if (!oh) {
175                         dev_err(&pdev->dev, "Cannot lookup hwmod '%s'\n",
176                                 oh_name);
177                         ret = -EINVAL;
178                         goto odbfd_exit1;
179                 }
180                 hwmods[i] = oh;
181                 if (oh->flags & HWMOD_INIT_NO_IDLE)
182                         device_active = true;
183         }
185         od = omap_device_alloc(pdev, hwmods, oh_cnt);
186         if (IS_ERR(od)) {
187                 dev_err(&pdev->dev, "Cannot allocate omap_device for :%s\n",
188                         oh_name);
189                 ret = PTR_ERR(od);
190                 goto odbfd_exit1;
191         }
193         /* Fix up missing resource names */
194         for (i = 0; i < pdev->num_resources; i++) {
195                 struct resource *r = &pdev->resource[i];
197                 if (r->name == NULL)
198                         r->name = dev_name(&pdev->dev);
199         }
201         if (!skip_pm_domain) {
202                 dev_pm_domain_set(&pdev->dev, &omap_device_pm_domain);
203                 if (device_active) {
204                         omap_device_enable(pdev);
205                         pm_runtime_set_active(&pdev->dev);
206                 }
207         }
209 odbfd_exit1:
210         kfree(hwmods);
211 odbfd_exit:
212         /* if data/we are at fault.. load up a fail handler */
213         if (ret)
214                 dev_pm_domain_set(&pdev->dev, &omap_device_fail_pm_domain);
216         return ret;
219 /**
220  * _omap_device_check_reidle_hwmods - check all hwmods in device for reidle flag
221  * @od: struct omap_device *od
222  *
223  * Checks underlying hwmods for reidle flag, if present, remove from hwmod
224  * list and set flag in omap_device to keep track.  Returns 0.
225  */
226 static int _omap_device_check_reidle_hwmods(struct omap_device *od)
228         int i;
230         for (i = 0; i < od->hwmods_cnt; i++) {
231                 if (od->hwmods[i]->flags & HWMOD_NEEDS_REIDLE) {
232                         od->flags |= OMAP_DEVICE_HAS_REIDLE_HWMODS;
233                         omap_hwmod_disable_reidle(od->hwmods[i]);
234                 }
235         }
237         return 0;
240 static int _omap_device_notifier_call(struct notifier_block *nb,
241                                       unsigned long event, void *dev)
243         struct platform_device *pdev = to_platform_device(dev);
244         struct omap_device *od;
245         int err;
247         switch (event) {
248         case BUS_NOTIFY_REMOVED_DEVICE:
249                 if (pdev->archdata.od)
250                         omap_device_delete(pdev->archdata.od);
251                 break;
252         case BUS_NOTIFY_UNBOUND_DRIVER:
253                 od = to_omap_device(pdev);
254                 if (od && (od->_state == OMAP_DEVICE_STATE_ENABLED)) {
255                         dev_info(dev, "enabled after unload, idling\n");
256                         err = omap_device_idle(pdev);
257                         if (err)
258                                 dev_err(dev, "failed to idle\n");
259                 }
260                 break;
261         case BUS_NOTIFY_BIND_DRIVER:
262                 od = to_omap_device(pdev);
263                 if (od && (od->_state == OMAP_DEVICE_STATE_ENABLED) &&
264                     pm_runtime_status_suspended(dev)) {
265                         od->_driver_status = BUS_NOTIFY_BIND_DRIVER;
266                         pm_runtime_set_active(dev);
267                 }
268                 break;
269         case BUS_NOTIFY_BOUND_DRIVER:
270                 od = to_omap_device(pdev);
271                 if (od) {
272                         od->_driver_status = BUS_NOTIFY_BOUND_DRIVER;
273                         _omap_device_check_reidle_hwmods(od);
274                 }
275                 break;
276         case BUS_NOTIFY_ADD_DEVICE:
277                 if (pdev->dev.of_node)
278                         omap_device_build_from_dt(pdev);
279                 omap_auxdata_legacy_init(dev);
280                 /* fall through */
281         default:
282                 od = to_omap_device(pdev);
283                 if (od)
284                         od->_driver_status = event;
285         }
287         return NOTIFY_DONE;
290 /**
291  * _omap_device_enable_hwmods - call omap_hwmod_enable() on all hwmods
292  * @od: struct omap_device *od
293  *
294  * Enable all underlying hwmods.  Returns 0.
295  */
296 static int _omap_device_enable_hwmods(struct omap_device *od)
298         int ret = 0;
299         int i;
301         for (i = 0; i < od->hwmods_cnt; i++)
302                 ret |= omap_hwmod_enable(od->hwmods[i]);
304         return ret;
307 /**
308  * _omap_device_idle_hwmods - call omap_hwmod_idle() on all hwmods
309  * @od: struct omap_device *od
310  *
311  * Idle all underlying hwmods.  Returns 0.
312  */
313 static int _omap_device_idle_hwmods(struct omap_device *od)
315         int ret = 0;
316         int i;
318         for (i = 0; i < od->hwmods_cnt; i++)
319                 ret |= omap_hwmod_idle(od->hwmods[i]);
321         return ret;
324 /**
325  * _omap_device_reidle_hwmods - call omap_hwmod_enable_reidle on all hwmods
326  * @od: struct omap_device *od
327  *
328  * Add all underlying hwmods to hwmod reidle list.  Returns 0.
329  */
330 static int _omap_device_reidle_hwmods(struct omap_device *od)
332         int i;
334         for (i = 0; i < od->hwmods_cnt; i++)
335                 if (od->hwmods[i]->flags | HWMOD_NEEDS_REIDLE)
336                         omap_hwmod_enable_reidle(od->hwmods[i]);
338         /* XXX pass along return value here? */
339         return 0;
342 /* Public functions for use by core code */
344 /**
345  * omap_device_get_context_loss_count - get lost context count
346  * @od: struct omap_device *
347  *
348  * Using the primary hwmod, query the context loss count for this
349  * device.
350  *
351  * Callers should consider context for this device lost any time this
352  * function returns a value different than the value the caller got
353  * the last time it called this function.
354  *
355  * If any hwmods exist for the omap_device associated with @pdev,
356  * return the context loss counter for that hwmod, otherwise return
357  * zero.
358  */
359 int omap_device_get_context_loss_count(struct platform_device *pdev)
361         struct omap_device *od;
362         u32 ret = 0;
364         od = to_omap_device(pdev);
366         if (od->hwmods_cnt)
367                 ret = omap_hwmod_get_context_loss_count(od->hwmods[0]);
369         return ret;
372 /**
373  * omap_device_alloc - allocate an omap_device
374  * @pdev: platform_device that will be included in this omap_device
375  * @oh: ptr to the single omap_hwmod that backs this omap_device
376  * @pdata: platform_data ptr to associate with the platform_device
377  * @pdata_len: amount of memory pointed to by @pdata
378  *
379  * Convenience function for allocating an omap_device structure and filling
380  * hwmods, and resources.
381  *
382  * Returns an struct omap_device pointer or ERR_PTR() on error;
383  */
384 struct omap_device *omap_device_alloc(struct platform_device *pdev,
385                                         struct omap_hwmod **ohs, int oh_cnt)
387         int ret = -ENOMEM;
388         struct omap_device *od;
389         int i;
390         struct omap_hwmod **hwmods;
392         od = kzalloc(sizeof(struct omap_device), GFP_KERNEL);
393         if (!od) {
394                 ret = -ENOMEM;
395                 goto oda_exit1;
396         }
397         od->hwmods_cnt = oh_cnt;
399         hwmods = kmemdup(ohs, sizeof(struct omap_hwmod *) * oh_cnt, GFP_KERNEL);
400         if (!hwmods)
401                 goto oda_exit2;
403         od->hwmods = hwmods;
404         od->pdev = pdev;
405         pdev->archdata.od = od;
407         for (i = 0; i < oh_cnt; i++) {
408                 hwmods[i]->od = od;
409                 _add_hwmod_clocks_clkdev(od, hwmods[i]);
410         }
412         return od;
414 oda_exit2:
415         kfree(od);
416 oda_exit1:
417         dev_err(&pdev->dev, "omap_device: build failed (%d)\n", ret);
419         return ERR_PTR(ret);
422 void omap_device_delete(struct omap_device *od)
424         if (!od)
425                 return;
427         if (od->flags & OMAP_DEVICE_HAS_REIDLE_HWMODS)
428                 _omap_device_reidle_hwmods(od);
430         od->pdev->archdata.od = NULL;
431         kfree(od->hwmods);
432         kfree(od);
435 /**
436  * omap_device_copy_resources - Add legacy IO and IRQ resources
437  * @oh: interconnect target module
438  * @pdev: platform device to copy resources to
439  *
440  * We still have legacy DMA and smartreflex needing resources.
441  * Let's populate what they need until we can eventually just
442  * remove this function. Note that there should be no need to
443  * call this from omap_device_build_from_dt(), nor should there
444  * be any need to call it for other devices.
445  */
446 static int
447 omap_device_copy_resources(struct omap_hwmod *oh,
448                            struct platform_device *pdev)
450         struct device_node *np, *child;
451         struct property *prop;
452         struct resource *res;
453         const char *name;
454         int error, irq = 0;
456         if (!oh || !oh->od || !oh->od->pdev)
457                 return -EINVAL;
459         np = oh->od->pdev->dev.of_node;
460         if (!np) {
461                 error = -ENODEV;
462                 goto error;
463         }
465         res = kcalloc(2, sizeof(*res), GFP_KERNEL);
466         if (!res)
467                 return -ENOMEM;
469         /* Do we have a dts range for the interconnect target module? */
470         error = omap_hwmod_parse_module_range(oh, np, res);
472         /* No ranges, rely on device reg entry */
473         if (error)
474                 error = of_address_to_resource(np, 0, res);
475         if (error)
476                 goto free;
478         /* SmartReflex needs first IO resource name to be "mpu" */
479         res[0].name = "mpu";
481         /*
482          * We may have a configured "ti,sysc" interconnect target with a
483          * dts child with the interrupt. If so use the first child's
484          * first interrupt for "ti-hwmods" legacy support.
485          */
486         of_property_for_each_string(np, "compatible", prop, name)
487                 if (!strncmp("ti,sysc-", name, 8))
488                         break;
490         child = of_get_next_available_child(np, NULL);
492         if (name)
493                 irq = irq_of_parse_and_map(child, 0);
494         if (!irq)
495                 irq = irq_of_parse_and_map(np, 0);
496         if (!irq) {
497                 error = -EINVAL;
498                 goto free;
499         }
501         /* Legacy DMA code needs interrupt name to be "0" */
502         res[1].start = irq;
503         res[1].end = irq;
504         res[1].flags = IORESOURCE_IRQ;
505         res[1].name = "0";
507         error = platform_device_add_resources(pdev, res, 2);
509 free:
510         kfree(res);
512 error:
513         WARN(error, "%s: %s device %s failed: %i\n",
514              __func__, oh->name, dev_name(&pdev->dev),
515              error);
517         return error;
520 /**
521  * omap_device_build - build and register an omap_device with one omap_hwmod
522  * @pdev_name: name of the platform_device driver to use
523  * @pdev_id: this platform_device's connection ID
524  * @oh: ptr to the single omap_hwmod that backs this omap_device
525  * @pdata: platform_data ptr to associate with the platform_device
526  * @pdata_len: amount of memory pointed to by @pdata
527  *
528  * Convenience function for building and registering a single
529  * omap_device record, which in turn builds and registers a
530  * platform_device record.  See omap_device_build_ss() for more
531  * information.  Returns ERR_PTR(-EINVAL) if @oh is NULL; otherwise,
532  * passes along the return value of omap_device_build_ss().
533  */
534 struct platform_device __init *omap_device_build(const char *pdev_name,
535                                                  int pdev_id,
536                                                  struct omap_hwmod *oh,
537                                                  void *pdata, int pdata_len)
539         int ret = -ENOMEM;
540         struct platform_device *pdev;
541         struct omap_device *od;
543         if (!oh || !pdev_name)
544                 return ERR_PTR(-EINVAL);
546         if (!pdata && pdata_len > 0)
547                 return ERR_PTR(-EINVAL);
549         if (strncmp(oh->name, "smartreflex", 11) &&
550             strncmp(oh->name, "dma", 3)) {
551                 pr_warn("%s need to update %s to probe with dt\na",
552                         __func__, pdev_name);
553                 ret = -ENODEV;
554                 goto odbs_exit;
555         }
557         pdev = platform_device_alloc(pdev_name, pdev_id);
558         if (!pdev) {
559                 ret = -ENOMEM;
560                 goto odbs_exit;
561         }
563         /* Set the dev_name early to allow dev_xxx in omap_device_alloc */
564         if (pdev->id != -1)
565                 dev_set_name(&pdev->dev, "%s.%d", pdev->name,  pdev->id);
566         else
567                 dev_set_name(&pdev->dev, "%s", pdev->name);
569         /*
570          * Must be called before omap_device_alloc() as oh->od
571          * only contains the currently registered omap_device
572          * and will get overwritten by omap_device_alloc().
573          */
574         ret = omap_device_copy_resources(oh, pdev);
575         if (ret)
576                 goto odbs_exit1;
578         od = omap_device_alloc(pdev, &oh, 1);
579         if (IS_ERR(od)) {
580                 ret = PTR_ERR(od);
581                 goto odbs_exit1;
582         }
584         ret = platform_device_add_data(pdev, pdata, pdata_len);
585         if (ret)
586                 goto odbs_exit2;
588         ret = omap_device_register(pdev);
589         if (ret)
590                 goto odbs_exit2;
592         return pdev;
594 odbs_exit2:
595         omap_device_delete(od);
596 odbs_exit1:
597         platform_device_put(pdev);
598 odbs_exit:
600         pr_err("omap_device: %s: build failed (%d)\n", pdev_name, ret);
602         return ERR_PTR(ret);
605 #ifdef CONFIG_PM
606 static int _od_runtime_suspend(struct device *dev)
608         struct platform_device *pdev = to_platform_device(dev);
609         int ret;
611         ret = pm_generic_runtime_suspend(dev);
612         if (ret)
613                 return ret;
615         return omap_device_idle(pdev);
618 static int _od_runtime_resume(struct device *dev)
620         struct platform_device *pdev = to_platform_device(dev);
621         int ret;
623         ret = omap_device_enable(pdev);
624         if (ret) {
625                 dev_err(dev, "use pm_runtime_put_sync_suspend() in driver?\n");
626                 return ret;
627         }
629         return pm_generic_runtime_resume(dev);
632 static int _od_fail_runtime_suspend(struct device *dev)
634         dev_warn(dev, "%s: FIXME: missing hwmod/omap_dev info\n", __func__);
635         return -ENODEV;
638 static int _od_fail_runtime_resume(struct device *dev)
640         dev_warn(dev, "%s: FIXME: missing hwmod/omap_dev info\n", __func__);
641         return -ENODEV;
644 #endif
646 #ifdef CONFIG_SUSPEND
647 static int _od_suspend_noirq(struct device *dev)
649         struct platform_device *pdev = to_platform_device(dev);
650         struct omap_device *od = to_omap_device(pdev);
651         int ret;
653         /* Don't attempt late suspend on a driver that is not bound */
654         if (od->_driver_status != BUS_NOTIFY_BOUND_DRIVER)
655                 return 0;
657         ret = pm_generic_suspend_noirq(dev);
659         if (!ret && !pm_runtime_status_suspended(dev)) {
660                 if (pm_generic_runtime_suspend(dev) == 0) {
661                         omap_device_idle(pdev);
662                         od->flags |= OMAP_DEVICE_SUSPENDED;
663                 }
664         }
666         return ret;
669 static int _od_resume_noirq(struct device *dev)
671         struct platform_device *pdev = to_platform_device(dev);
672         struct omap_device *od = to_omap_device(pdev);
674         if (od->flags & OMAP_DEVICE_SUSPENDED) {
675                 od->flags &= ~OMAP_DEVICE_SUSPENDED;
676                 omap_device_enable(pdev);
677                 pm_generic_runtime_resume(dev);
678         }
680         return pm_generic_resume_noirq(dev);
682 #else
683 #define _od_suspend_noirq NULL
684 #define _od_resume_noirq NULL
685 #endif
687 struct dev_pm_domain omap_device_fail_pm_domain = {
688         .ops = {
689                 SET_RUNTIME_PM_OPS(_od_fail_runtime_suspend,
690                                    _od_fail_runtime_resume, NULL)
691         }
692 };
694 struct dev_pm_domain omap_device_pm_domain = {
695         .ops = {
696                 SET_RUNTIME_PM_OPS(_od_runtime_suspend, _od_runtime_resume,
697                                    NULL)
698                 USE_PLATFORM_PM_SLEEP_OPS
699                 SET_NOIRQ_SYSTEM_SLEEP_PM_OPS(_od_suspend_noirq,
700                                               _od_resume_noirq)
701         }
702 };
704 /**
705  * omap_device_register - register an omap_device with one omap_hwmod
706  * @od: struct omap_device * to register
707  *
708  * Register the omap_device structure.  This currently just calls
709  * platform_device_register() on the underlying platform_device.
710  * Returns the return value of platform_device_register().
711  */
712 int omap_device_register(struct platform_device *pdev)
714         pr_debug("omap_device: %s: registering\n", pdev->name);
716         dev_pm_domain_set(&pdev->dev, &omap_device_pm_domain);
717         return platform_device_add(pdev);
721 /* Public functions for use by device drivers through struct platform_data */
723 /**
724  * omap_device_enable - fully activate an omap_device
725  * @od: struct omap_device * to activate
726  *
727  * Do whatever is necessary for the hwmods underlying omap_device @od
728  * to be accessible and ready to operate.  This generally involves
729  * enabling clocks, setting SYSCONFIG registers; and in the future may
730  * involve remuxing pins.  Device drivers should call this function
731  * indirectly via pm_runtime_get*().  Returns -EINVAL if called when
732  * the omap_device is already enabled, or passes along the return
733  * value of _omap_device_enable_hwmods().
734  */
735 int omap_device_enable(struct platform_device *pdev)
737         int ret;
738         struct omap_device *od;
740         od = to_omap_device(pdev);
742         if (od->_state == OMAP_DEVICE_STATE_ENABLED) {
743                 dev_warn(&pdev->dev,
744                          "omap_device: %s() called from invalid state %d\n",
745                          __func__, od->_state);
746                 return -EINVAL;
747         }
749         ret = _omap_device_enable_hwmods(od);
751         if (ret == 0)
752                 od->_state = OMAP_DEVICE_STATE_ENABLED;
754         return ret;
757 /**
758  * omap_device_idle - idle an omap_device
759  * @od: struct omap_device * to idle
760  *
761  * Idle omap_device @od.  Device drivers call this function indirectly
762  * via pm_runtime_put*().  Returns -EINVAL if the omap_device is not
763  * currently enabled, or passes along the return value of
764  * _omap_device_idle_hwmods().
765  */
766 int omap_device_idle(struct platform_device *pdev)
768         int ret;
769         struct omap_device *od;
771         od = to_omap_device(pdev);
773         if (od->_state != OMAP_DEVICE_STATE_ENABLED) {
774                 dev_warn(&pdev->dev,
775                          "omap_device: %s() called from invalid state %d\n",
776                          __func__, od->_state);
777                 return -EINVAL;
778         }
780         ret = _omap_device_idle_hwmods(od);
782         if (ret == 0)
783                 od->_state = OMAP_DEVICE_STATE_IDLE;
785         return ret;
788 /**
789  * omap_device_assert_hardreset - set a device's hardreset line
790  * @pdev: struct platform_device * to reset
791  * @name: const char * name of the reset line
792  *
793  * Set the hardreset line identified by @name on the IP blocks
794  * associated with the hwmods backing the platform_device @pdev.  All
795  * of the hwmods associated with @pdev must have the same hardreset
796  * line linked to them for this to work.  Passes along the return value
797  * of omap_hwmod_assert_hardreset() in the event of any failure, or
798  * returns 0 upon success.
799  */
800 int omap_device_assert_hardreset(struct platform_device *pdev, const char *name)
802         struct omap_device *od = to_omap_device(pdev);
803         int ret = 0;
804         int i;
806         for (i = 0; i < od->hwmods_cnt; i++) {
807                 ret = omap_hwmod_assert_hardreset(od->hwmods[i], name);
808                 if (ret)
809                         break;
810         }
812         return ret;
815 /**
816  * omap_device_deassert_hardreset - release a device's hardreset line
817  * @pdev: struct platform_device * to reset
818  * @name: const char * name of the reset line
819  *
820  * Release the hardreset line identified by @name on the IP blocks
821  * associated with the hwmods backing the platform_device @pdev.  All
822  * of the hwmods associated with @pdev must have the same hardreset
823  * line linked to them for this to work.  Passes along the return
824  * value of omap_hwmod_deassert_hardreset() in the event of any
825  * failure, or returns 0 upon success.
826  */
827 int omap_device_deassert_hardreset(struct platform_device *pdev,
828                                    const char *name)
830         struct omap_device *od = to_omap_device(pdev);
831         int ret = 0;
832         int i;
834         for (i = 0; i < od->hwmods_cnt; i++) {
835                 ret = omap_hwmod_deassert_hardreset(od->hwmods[i], name);
836                 if (ret)
837                         break;
838         }
840         return ret;
843 /**
844  * omap_device_get_by_hwmod_name() - convert a hwmod name to
845  * device pointer.
846  * @oh_name: name of the hwmod device
847  *
848  * Returns back a struct device * pointer associated with a hwmod
849  * device represented by a hwmod_name
850  */
851 struct device *omap_device_get_by_hwmod_name(const char *oh_name)
853         struct omap_hwmod *oh;
855         if (!oh_name) {
856                 WARN(1, "%s: no hwmod name!\n", __func__);
857                 return ERR_PTR(-EINVAL);
858         }
860         oh = omap_hwmod_lookup(oh_name);
861         if (!oh) {
862                 WARN(1, "%s: no hwmod for %s\n", __func__,
863                         oh_name);
864                 return ERR_PTR(-ENODEV);
865         }
866         if (!oh->od) {
867                 WARN(1, "%s: no omap_device for %s\n", __func__,
868                         oh_name);
869                 return ERR_PTR(-ENODEV);
870         }
872         return &oh->od->pdev->dev;
875 static struct notifier_block platform_nb = {
876         .notifier_call = _omap_device_notifier_call,
877 };
879 static int __init omap_device_init(void)
881         omap_hwmod_setup_reidle();
882         bus_register_notifier(&platform_bus_type, &platform_nb);
883         return 0;
885 omap_postcore_initcall(omap_device_init);
887 /**
888  * omap_device_late_idle - idle devices without drivers
889  * @dev: struct device * associated with omap_device
890  * @data: unused
891  *
892  * Check the driver bound status of this device, and idle it
893  * if there is no driver attached.
894  */
895 static int __init omap_device_late_idle(struct device *dev, void *data)
897         struct platform_device *pdev = to_platform_device(dev);
898         struct omap_device *od = to_omap_device(pdev);
899         int i;
901         if (!od)
902                 return 0;
904         /*
905          * If omap_device state is enabled, but has no driver bound,
906          * idle it.
907          */
909         /*
910          * Some devices (like memory controllers) are always kept
911          * enabled, and should not be idled even with no drivers.
912          */
913         for (i = 0; i < od->hwmods_cnt; i++)
914                 if (od->hwmods[i]->flags & HWMOD_INIT_NO_IDLE)
915                         return 0;
917         if (od->_driver_status != BUS_NOTIFY_BOUND_DRIVER &&
918             od->_driver_status != BUS_NOTIFY_BIND_DRIVER) {
919                 if (od->_state == OMAP_DEVICE_STATE_ENABLED) {
920                         dev_warn(dev, "%s: enabled but no driver.  Idling\n",
921                                  __func__);
922                         omap_device_idle(pdev);
923                 }
924         }
926         return 0;
929 static int __init omap_device_late_init(void)
931         bus_for_each_dev(&platform_bus_type, NULL, NULL, omap_device_late_idle);
933         return 0;
935 omap_late_initcall_sync(omap_device_late_init);