1 /*
2 * OMAP3/OMAP4 Voltage Management Routines
3 *
4 * Author: Thara Gopinath <thara@ti.com>
5 *
6 * Copyright (C) 2007 Texas Instruments, Inc.
7 * Rajendra Nayak <rnayak@ti.com>
8 * Lesly A M <x0080970@ti.com>
9 *
10 * Copyright (C) 2008, 2011 Nokia Corporation
11 * Kalle Jokiniemi
12 * Paul Walmsley
13 *
14 * Copyright (C) 2010 Texas Instruments, Inc.
15 * Thara Gopinath <thara@ti.com>
16 *
17 * This program is free software; you can redistribute it and/or modify
18 * it under the terms of the GNU General Public License version 2 as
19 * published by the Free Software Foundation.
20 */
22 #include <linux/delay.h>
23 #include <linux/io.h>
24 #include <linux/err.h>
25 #include <linux/export.h>
26 #include <linux/debugfs.h>
27 #include <linux/slab.h>
28 #include <linux/clk.h>
30 #include "common.h"
32 #include "prm-regbits-34xx.h"
33 #include "prm-regbits-44xx.h"
34 #include "prm44xx.h"
35 #include "prcm44xx.h"
36 #include "prminst44xx.h"
37 #include "control.h"
39 #include "voltage.h"
40 #include "powerdomain.h"
42 #include "vc.h"
43 #include "vp.h"
45 static LIST_HEAD(voltdm_list);
47 /* Public functions */
48 /**
49 * voltdm_get_voltage() - Gets the current non-auto-compensated voltage
50 * @voltdm: pointer to the voltdm for which current voltage info is needed
51 *
52 * API to get the current non-auto-compensated voltage for a voltage domain.
53 * Returns 0 in case of error else returns the current voltage.
54 */
55 unsigned long voltdm_get_voltage(struct voltagedomain *voltdm)
56 {
57 if (!voltdm || IS_ERR(voltdm)) {
58 pr_warn("%s: VDD specified does not exist!\n", __func__);
59 return 0;
60 }
62 return voltdm->nominal_volt;
63 }
65 /**
66 * voltdm_scale() - API to scale voltage of a particular voltage domain.
67 * @voltdm: pointer to the voltage domain which is to be scaled.
68 * @target_volt: The target voltage of the voltage domain
69 *
70 * This API should be called by the kernel to do the voltage scaling
71 * for a particular voltage domain during DVFS.
72 */
73 int voltdm_scale(struct voltagedomain *voltdm,
74 unsigned long target_volt)
75 {
76 int ret, i;
77 unsigned long volt = 0;
79 if (!voltdm || IS_ERR(voltdm)) {
80 pr_warn("%s: VDD specified does not exist!\n", __func__);
81 return -EINVAL;
82 }
84 if (!voltdm->scale) {
85 pr_err("%s: No voltage scale API registered for vdd_%s\n",
86 __func__, voltdm->name);
87 return -ENODATA;
88 }
90 if (!voltdm->volt_data) {
91 pr_err("%s: No voltage data defined for vdd_%s\n",
92 __func__, voltdm->name);
93 return -ENODATA;
94 }
96 /* Adjust voltage to the exact voltage from the OPP table */
97 for (i = 0; voltdm->volt_data[i].volt_nominal != 0; i++) {
98 if (voltdm->volt_data[i].volt_nominal >= target_volt) {
99 volt = voltdm->volt_data[i].volt_nominal;
100 break;
101 }
102 }
104 if (!volt) {
105 pr_warn("%s: not scaling. OPP voltage for %lu, not found.\n",
106 __func__, target_volt);
107 return -EINVAL;
108 }
110 ret = voltdm->scale(voltdm, volt);
111 if (!ret)
112 voltdm->nominal_volt = volt;
114 return ret;
115 }
117 /**
118 * voltdm_reset() - Resets the voltage of a particular voltage domain
119 * to that of the current OPP.
120 * @voltdm: pointer to the voltage domain whose voltage is to be reset.
121 *
122 * This API finds out the correct voltage the voltage domain is supposed
123 * to be at and resets the voltage to that level. Should be used especially
124 * while disabling any voltage compensation modules.
125 */
126 void voltdm_reset(struct voltagedomain *voltdm)
127 {
128 unsigned long target_volt;
130 if (!voltdm || IS_ERR(voltdm)) {
131 pr_warn("%s: VDD specified does not exist!\n", __func__);
132 return;
133 }
135 target_volt = voltdm_get_voltage(voltdm);
136 if (!target_volt) {
137 pr_err("%s: unable to find current voltage for vdd_%s\n",
138 __func__, voltdm->name);
139 return;
140 }
142 voltdm_scale(voltdm, target_volt);
143 }
145 /**
146 * omap_voltage_get_volttable() - API to get the voltage table associated with a
147 * particular voltage domain.
148 * @voltdm: pointer to the VDD for which the voltage table is required
149 * @volt_data: the voltage table for the particular vdd which is to be
150 * populated by this API
151 *
152 * This API populates the voltage table associated with a VDD into the
153 * passed parameter pointer. Returns the count of distinct voltages
154 * supported by this vdd.
155 *
156 */
157 void omap_voltage_get_volttable(struct voltagedomain *voltdm,
158 struct omap_volt_data **volt_data)
159 {
160 if (!voltdm || IS_ERR(voltdm)) {
161 pr_warn("%s: VDD specified does not exist!\n", __func__);
162 return;
163 }
165 *volt_data = voltdm->volt_data;
166 }
168 /**
169 * omap_voltage_get_voltdata() - API to get the voltage table entry for a
170 * particular voltage
171 * @voltdm: pointer to the VDD whose voltage table has to be searched
172 * @volt: the voltage to be searched in the voltage table
173 *
174 * This API searches through the voltage table for the required voltage
175 * domain and tries to find a matching entry for the passed voltage volt.
176 * If a matching entry is found volt_data is populated with that entry.
177 * This API searches only through the non-compensated voltages int the
178 * voltage table.
179 * Returns pointer to the voltage table entry corresponding to volt on
180 * success. Returns -ENODATA if no voltage table exisits for the passed voltage
181 * domain or if there is no matching entry.
182 */
183 struct omap_volt_data *omap_voltage_get_voltdata(struct voltagedomain *voltdm,
184 unsigned long volt)
185 {
186 int i;
188 if (!voltdm || IS_ERR(voltdm)) {
189 pr_warn("%s: VDD specified does not exist!\n", __func__);
190 return ERR_PTR(-EINVAL);
191 }
193 if (!voltdm->volt_data) {
194 pr_warn("%s: voltage table does not exist for vdd_%s\n",
195 __func__, voltdm->name);
196 return ERR_PTR(-ENODATA);
197 }
199 for (i = 0; voltdm->volt_data[i].volt_nominal != 0; i++) {
200 if (voltdm->volt_data[i].volt_nominal == volt)
201 return &voltdm->volt_data[i];
202 }
204 pr_notice("%s: Unable to match the current voltage with the voltage table for vdd_%s\n",
205 __func__, voltdm->name);
207 return ERR_PTR(-ENODATA);
208 }
210 /**
211 * omap_voltage_register_pmic() - API to register PMIC specific data
212 * @voltdm: pointer to the VDD for which the PMIC specific data is
213 * to be registered
214 * @pmic: the structure containing pmic info
215 *
216 * This API is to be called by the SOC/PMIC file to specify the
217 * pmic specific info as present in omap_voltdm_pmic structure.
218 */
219 int omap_voltage_register_pmic(struct voltagedomain *voltdm,
220 struct omap_voltdm_pmic *pmic)
221 {
222 if (!voltdm || IS_ERR(voltdm)) {
223 pr_warn("%s: VDD specified does not exist!\n", __func__);
224 return -EINVAL;
225 }
227 voltdm->pmic = pmic;
229 return 0;
230 }
232 /**
233 * omap_voltage_late_init() - Init the various voltage parameters
234 *
235 * This API is to be called in the later stages of the
236 * system boot to init the voltage controller and
237 * voltage processors.
238 */
239 int __init omap_voltage_late_init(void)
240 {
241 struct voltagedomain *voltdm;
243 if (list_empty(&voltdm_list)) {
244 pr_err("%s: Voltage driver support not added\n",
245 __func__);
246 return -EINVAL;
247 }
249 list_for_each_entry(voltdm, &voltdm_list, node) {
250 struct clk *sys_ck;
252 if (!voltdm->scalable)
253 continue;
255 sys_ck = clk_get(NULL, voltdm->sys_clk.name);
256 if (IS_ERR(sys_ck)) {
257 pr_warn("%s: Could not get sys clk.\n", __func__);
258 return -EINVAL;
259 }
260 voltdm->sys_clk.rate = clk_get_rate(sys_ck);
261 WARN_ON(!voltdm->sys_clk.rate);
262 clk_put(sys_ck);
264 if (voltdm->vc) {
265 voltdm->scale = omap_vc_bypass_scale;
266 omap_vc_init_channel(voltdm);
267 }
269 if (voltdm->vp) {
270 voltdm->scale = omap_vp_forceupdate_scale;
271 omap_vp_init(voltdm);
272 }
273 }
275 return 0;
276 }
278 static struct voltagedomain *_voltdm_lookup(const char *name)
279 {
280 struct voltagedomain *voltdm, *temp_voltdm;
282 voltdm = NULL;
284 list_for_each_entry(temp_voltdm, &voltdm_list, node) {
285 if (!strcmp(name, temp_voltdm->name)) {
286 voltdm = temp_voltdm;
287 break;
288 }
289 }
291 return voltdm;
292 }
294 static int _voltdm_register(struct voltagedomain *voltdm)
295 {
296 if (!voltdm || !voltdm->name)
297 return -EINVAL;
299 list_add(&voltdm->node, &voltdm_list);
301 pr_debug("voltagedomain: registered %s\n", voltdm->name);
303 return 0;
304 }
306 /**
307 * voltdm_lookup - look up a voltagedomain by name, return a pointer
308 * @name: name of voltagedomain
309 *
310 * Find a registered voltagedomain by its name @name. Returns a pointer
311 * to the struct voltagedomain if found, or NULL otherwise.
312 */
313 struct voltagedomain *voltdm_lookup(const char *name)
314 {
315 struct voltagedomain *voltdm ;
317 if (!name)
318 return NULL;
320 voltdm = _voltdm_lookup(name);
322 return voltdm;
323 }
325 /**
326 * voltdm_init - set up the voltagedomain layer
327 * @voltdm_list: array of struct voltagedomain pointers to register
328 *
329 * Loop through the array of voltagedomains @voltdm_list, registering all
330 * that are available on the current CPU. If voltdm_list is supplied
331 * and not null, all of the referenced voltagedomains will be
332 * registered. No return value.
333 */
334 void voltdm_init(struct voltagedomain **voltdms)
335 {
336 struct voltagedomain **v;
338 if (voltdms) {
339 for (v = voltdms; *v; v++)
340 _voltdm_register(*v);
341 }
342 }