1 /*
2 * Block device elevator/IO-scheduler.
3 *
4 * Copyright (C) 2000 Andrea Arcangeli <andrea@suse.de> SuSE
5 *
6 * 30042000 Jens Axboe <axboe@kernel.dk> :
7 *
8 * Split the elevator a bit so that it is possible to choose a different
9 * one or even write a new "plug in". There are three pieces:
10 * - elevator_fn, inserts a new request in the queue list
11 * - elevator_merge_fn, decides whether a new buffer can be merged with
12 * an existing request
13 * - elevator_dequeue_fn, called when a request is taken off the active list
14 *
15 * 20082000 Dave Jones <davej@suse.de> :
16 * Removed tests for max-bomb-segments, which was breaking elvtune
17 * when run without -bN
18 *
19 * Jens:
20 * - Rework again to work with bio instead of buffer_heads
21 * - loose bi_dev comparisons, partition handling is right now
22 * - completely modularize elevator setup and teardown
23 *
24 */
25 #include <linux/kernel.h>
26 #include <linux/fs.h>
27 #include <linux/blkdev.h>
28 #include <linux/elevator.h>
29 #include <linux/bio.h>
30 #include <linux/module.h>
31 #include <linux/slab.h>
32 #include <linux/init.h>
33 #include <linux/compiler.h>
34 #include <linux/blktrace_api.h>
35 #include <linux/hash.h>
36 #include <linux/uaccess.h>
37 #include <linux/pm_runtime.h>
38 #include <linux/blk-cgroup.h>
40 #include <trace/events/block.h>
42 #include "blk.h"
43 #include "blk-mq-sched.h"
44 #include "blk-wbt.h"
46 static DEFINE_SPINLOCK(elv_list_lock);
47 static LIST_HEAD(elv_list);
49 /*
50 * Merge hash stuff.
51 */
52 #define rq_hash_key(rq) (blk_rq_pos(rq) + blk_rq_sectors(rq))
54 /*
55 * Query io scheduler to see if the current process issuing bio may be
56 * merged with rq.
57 */
58 static int elv_iosched_allow_bio_merge(struct request *rq, struct bio *bio)
59 {
60 struct request_queue *q = rq->q;
61 struct elevator_queue *e = q->elevator;
63 if (e->uses_mq && e->type->ops.mq.allow_merge)
64 return e->type->ops.mq.allow_merge(q, rq, bio);
65 else if (!e->uses_mq && e->type->ops.sq.elevator_allow_bio_merge_fn)
66 return e->type->ops.sq.elevator_allow_bio_merge_fn(q, rq, bio);
68 return 1;
69 }
71 /*
72 * can we safely merge with this request?
73 */
74 bool elv_bio_merge_ok(struct request *rq, struct bio *bio)
75 {
76 if (!blk_rq_merge_ok(rq, bio))
77 return false;
79 if (!elv_iosched_allow_bio_merge(rq, bio))
80 return false;
82 return true;
83 }
84 EXPORT_SYMBOL(elv_bio_merge_ok);
86 static bool elevator_match(const struct elevator_type *e, const char *name)
87 {
88 if (!strcmp(e->elevator_name, name))
89 return true;
90 if (e->elevator_alias && !strcmp(e->elevator_alias, name))
91 return true;
93 return false;
94 }
96 /*
97 * Return scheduler with name 'name' and with matching 'mq capability
98 */
99 static struct elevator_type *elevator_find(const char *name, bool mq)
100 {
101 struct elevator_type *e;
103 list_for_each_entry(e, &elv_list, list) {
104 if (elevator_match(e, name) && (mq == e->uses_mq))
105 return e;
106 }
108 return NULL;
109 }
111 static void elevator_put(struct elevator_type *e)
112 {
113 module_put(e->elevator_owner);
114 }
116 static struct elevator_type *elevator_get(struct request_queue *q,
117 const char *name, bool try_loading)
118 {
119 struct elevator_type *e;
121 spin_lock(&elv_list_lock);
123 e = elevator_find(name, q->mq_ops != NULL);
124 if (!e && try_loading) {
125 spin_unlock(&elv_list_lock);
126 request_module("%s-iosched", name);
127 spin_lock(&elv_list_lock);
128 e = elevator_find(name, q->mq_ops != NULL);
129 }
131 if (e && !try_module_get(e->elevator_owner))
132 e = NULL;
134 spin_unlock(&elv_list_lock);
135 return e;
136 }
138 static char chosen_elevator[ELV_NAME_MAX];
140 static int __init elevator_setup(char *str)
141 {
142 /*
143 * Be backwards-compatible with previous kernels, so users
144 * won't get the wrong elevator.
145 */
146 strncpy(chosen_elevator, str, sizeof(chosen_elevator) - 1);
147 return 1;
148 }
150 __setup("elevator=", elevator_setup);
152 /* called during boot to load the elevator chosen by the elevator param */
153 void __init load_default_elevator_module(void)
154 {
155 struct elevator_type *e;
157 if (!chosen_elevator[0])
158 return;
160 /*
161 * Boot parameter is deprecated, we haven't supported that for MQ.
162 * Only look for non-mq schedulers from here.
163 */
164 spin_lock(&elv_list_lock);
165 e = elevator_find(chosen_elevator, false);
166 spin_unlock(&elv_list_lock);
168 if (!e)
169 request_module("%s-iosched", chosen_elevator);
170 }
172 static struct kobj_type elv_ktype;
174 struct elevator_queue *elevator_alloc(struct request_queue *q,
175 struct elevator_type *e)
176 {
177 struct elevator_queue *eq;
179 eq = kzalloc_node(sizeof(*eq), GFP_KERNEL, q->node);
180 if (unlikely(!eq))
181 return NULL;
183 eq->type = e;
184 kobject_init(&eq->kobj, &elv_ktype);
185 mutex_init(&eq->sysfs_lock);
186 hash_init(eq->hash);
187 eq->uses_mq = e->uses_mq;
189 return eq;
190 }
191 EXPORT_SYMBOL(elevator_alloc);
193 static void elevator_release(struct kobject *kobj)
194 {
195 struct elevator_queue *e;
197 e = container_of(kobj, struct elevator_queue, kobj);
198 elevator_put(e->type);
199 kfree(e);
200 }
202 /*
203 * Use the default elevator specified by config boot param for non-mq devices,
204 * or by config option. Don't try to load modules as we could be running off
205 * async and request_module() isn't allowed from async.
206 */
207 int elevator_init(struct request_queue *q)
208 {
209 struct elevator_type *e = NULL;
210 int err = 0;
212 /*
213 * q->sysfs_lock must be held to provide mutual exclusion between
214 * elevator_switch() and here.
215 */
216 mutex_lock(&q->sysfs_lock);
217 if (unlikely(q->elevator))
218 goto out_unlock;
220 if (*chosen_elevator) {
221 e = elevator_get(q, chosen_elevator, false);
222 if (!e)
223 printk(KERN_ERR "I/O scheduler %s not found\n",
224 chosen_elevator);
225 }
227 if (!e)
228 e = elevator_get(q, CONFIG_DEFAULT_IOSCHED, false);
229 if (!e) {
230 printk(KERN_ERR
231 "Default I/O scheduler not found. Using noop.\n");
232 e = elevator_get(q, "noop", false);
233 }
235 err = e->ops.sq.elevator_init_fn(q, e);
236 if (err)
237 elevator_put(e);
238 out_unlock:
239 mutex_unlock(&q->sysfs_lock);
240 return err;
241 }
243 void elevator_exit(struct request_queue *q, struct elevator_queue *e)
244 {
245 mutex_lock(&e->sysfs_lock);
246 if (e->uses_mq && e->type->ops.mq.exit_sched)
247 blk_mq_exit_sched(q, e);
248 else if (!e->uses_mq && e->type->ops.sq.elevator_exit_fn)
249 e->type->ops.sq.elevator_exit_fn(e);
250 mutex_unlock(&e->sysfs_lock);
252 kobject_put(&e->kobj);
253 }
255 static inline void __elv_rqhash_del(struct request *rq)
256 {
257 hash_del(&rq->hash);
258 rq->rq_flags &= ~RQF_HASHED;
259 }
261 void elv_rqhash_del(struct request_queue *q, struct request *rq)
262 {
263 if (ELV_ON_HASH(rq))
264 __elv_rqhash_del(rq);
265 }
266 EXPORT_SYMBOL_GPL(elv_rqhash_del);
268 void elv_rqhash_add(struct request_queue *q, struct request *rq)
269 {
270 struct elevator_queue *e = q->elevator;
272 BUG_ON(ELV_ON_HASH(rq));
273 hash_add(e->hash, &rq->hash, rq_hash_key(rq));
274 rq->rq_flags |= RQF_HASHED;
275 }
276 EXPORT_SYMBOL_GPL(elv_rqhash_add);
278 void elv_rqhash_reposition(struct request_queue *q, struct request *rq)
279 {
280 __elv_rqhash_del(rq);
281 elv_rqhash_add(q, rq);
282 }
284 struct request *elv_rqhash_find(struct request_queue *q, sector_t offset)
285 {
286 struct elevator_queue *e = q->elevator;
287 struct hlist_node *next;
288 struct request *rq;
290 hash_for_each_possible_safe(e->hash, rq, next, hash, offset) {
291 BUG_ON(!ELV_ON_HASH(rq));
293 if (unlikely(!rq_mergeable(rq))) {
294 __elv_rqhash_del(rq);
295 continue;
296 }
298 if (rq_hash_key(rq) == offset)
299 return rq;
300 }
302 return NULL;
303 }
305 /*
306 * RB-tree support functions for inserting/lookup/removal of requests
307 * in a sorted RB tree.
308 */
309 void elv_rb_add(struct rb_root *root, struct request *rq)
310 {
311 struct rb_node **p = &root->rb_node;
312 struct rb_node *parent = NULL;
313 struct request *__rq;
315 while (*p) {
316 parent = *p;
317 __rq = rb_entry(parent, struct request, rb_node);
319 if (blk_rq_pos(rq) < blk_rq_pos(__rq))
320 p = &(*p)->rb_left;
321 else if (blk_rq_pos(rq) >= blk_rq_pos(__rq))
322 p = &(*p)->rb_right;
323 }
325 rb_link_node(&rq->rb_node, parent, p);
326 rb_insert_color(&rq->rb_node, root);
327 }
328 EXPORT_SYMBOL(elv_rb_add);
330 void elv_rb_del(struct rb_root *root, struct request *rq)
331 {
332 BUG_ON(RB_EMPTY_NODE(&rq->rb_node));
333 rb_erase(&rq->rb_node, root);
334 RB_CLEAR_NODE(&rq->rb_node);
335 }
336 EXPORT_SYMBOL(elv_rb_del);
338 struct request *elv_rb_find(struct rb_root *root, sector_t sector)
339 {
340 struct rb_node *n = root->rb_node;
341 struct request *rq;
343 while (n) {
344 rq = rb_entry(n, struct request, rb_node);
346 if (sector < blk_rq_pos(rq))
347 n = n->rb_left;
348 else if (sector > blk_rq_pos(rq))
349 n = n->rb_right;
350 else
351 return rq;
352 }
354 return NULL;
355 }
356 EXPORT_SYMBOL(elv_rb_find);
358 /*
359 * Insert rq into dispatch queue of q. Queue lock must be held on
360 * entry. rq is sort instead into the dispatch queue. To be used by
361 * specific elevators.
362 */
363 void elv_dispatch_sort(struct request_queue *q, struct request *rq)
364 {
365 sector_t boundary;
366 struct list_head *entry;
368 if (q->last_merge == rq)
369 q->last_merge = NULL;
371 elv_rqhash_del(q, rq);
373 q->nr_sorted--;
375 boundary = q->end_sector;
376 list_for_each_prev(entry, &q->queue_head) {
377 struct request *pos = list_entry_rq(entry);
379 if (req_op(rq) != req_op(pos))
380 break;
381 if (rq_data_dir(rq) != rq_data_dir(pos))
382 break;
383 if (pos->rq_flags & (RQF_STARTED | RQF_SOFTBARRIER))
384 break;
385 if (blk_rq_pos(rq) >= boundary) {
386 if (blk_rq_pos(pos) < boundary)
387 continue;
388 } else {
389 if (blk_rq_pos(pos) >= boundary)
390 break;
391 }
392 if (blk_rq_pos(rq) >= blk_rq_pos(pos))
393 break;
394 }
396 list_add(&rq->queuelist, entry);
397 }
398 EXPORT_SYMBOL(elv_dispatch_sort);
400 /*
401 * Insert rq into dispatch queue of q. Queue lock must be held on
402 * entry. rq is added to the back of the dispatch queue. To be used by
403 * specific elevators.
404 */
405 void elv_dispatch_add_tail(struct request_queue *q, struct request *rq)
406 {
407 if (q->last_merge == rq)
408 q->last_merge = NULL;
410 elv_rqhash_del(q, rq);
412 q->nr_sorted--;
414 q->end_sector = rq_end_sector(rq);
415 q->boundary_rq = rq;
416 list_add_tail(&rq->queuelist, &q->queue_head);
417 }
418 EXPORT_SYMBOL(elv_dispatch_add_tail);
420 enum elv_merge elv_merge(struct request_queue *q, struct request **req,
421 struct bio *bio)
422 {
423 struct elevator_queue *e = q->elevator;
424 struct request *__rq;
426 /*
427 * Levels of merges:
428 * nomerges: No merges at all attempted
429 * noxmerges: Only simple one-hit cache try
430 * merges: All merge tries attempted
431 */
432 if (blk_queue_nomerges(q) || !bio_mergeable(bio))
433 return ELEVATOR_NO_MERGE;
435 /*
436 * First try one-hit cache.
437 */
438 if (q->last_merge && elv_bio_merge_ok(q->last_merge, bio)) {
439 enum elv_merge ret = blk_try_merge(q->last_merge, bio);
441 if (ret != ELEVATOR_NO_MERGE) {
442 *req = q->last_merge;
443 return ret;
444 }
445 }
447 if (blk_queue_noxmerges(q))
448 return ELEVATOR_NO_MERGE;
450 /*
451 * See if our hash lookup can find a potential backmerge.
452 */
453 __rq = elv_rqhash_find(q, bio->bi_iter.bi_sector);
454 if (__rq && elv_bio_merge_ok(__rq, bio)) {
455 *req = __rq;
456 return ELEVATOR_BACK_MERGE;
457 }
459 if (e->uses_mq && e->type->ops.mq.request_merge)
460 return e->type->ops.mq.request_merge(q, req, bio);
461 else if (!e->uses_mq && e->type->ops.sq.elevator_merge_fn)
462 return e->type->ops.sq.elevator_merge_fn(q, req, bio);
464 return ELEVATOR_NO_MERGE;
465 }
467 /*
468 * Attempt to do an insertion back merge. Only check for the case where
469 * we can append 'rq' to an existing request, so we can throw 'rq' away
470 * afterwards.
471 *
472 * Returns true if we merged, false otherwise
473 */
474 bool elv_attempt_insert_merge(struct request_queue *q, struct request *rq)
475 {
476 struct request *__rq;
477 bool ret;
479 if (blk_queue_nomerges(q))
480 return false;
482 /*
483 * First try one-hit cache.
484 */
485 if (q->last_merge && blk_attempt_req_merge(q, q->last_merge, rq))
486 return true;
488 if (blk_queue_noxmerges(q))
489 return false;
491 ret = false;
492 /*
493 * See if our hash lookup can find a potential backmerge.
494 */
495 while (1) {
496 __rq = elv_rqhash_find(q, blk_rq_pos(rq));
497 if (!__rq || !blk_attempt_req_merge(q, __rq, rq))
498 break;
500 /* The merged request could be merged with others, try again */
501 ret = true;
502 rq = __rq;
503 }
505 return ret;
506 }
508 void elv_merged_request(struct request_queue *q, struct request *rq,
509 enum elv_merge type)
510 {
511 struct elevator_queue *e = q->elevator;
513 if (e->uses_mq && e->type->ops.mq.request_merged)
514 e->type->ops.mq.request_merged(q, rq, type);
515 else if (!e->uses_mq && e->type->ops.sq.elevator_merged_fn)
516 e->type->ops.sq.elevator_merged_fn(q, rq, type);
518 if (type == ELEVATOR_BACK_MERGE)
519 elv_rqhash_reposition(q, rq);
521 q->last_merge = rq;
522 }
524 void elv_merge_requests(struct request_queue *q, struct request *rq,
525 struct request *next)
526 {
527 struct elevator_queue *e = q->elevator;
528 bool next_sorted = false;
530 if (e->uses_mq && e->type->ops.mq.requests_merged)
531 e->type->ops.mq.requests_merged(q, rq, next);
532 else if (e->type->ops.sq.elevator_merge_req_fn) {
533 next_sorted = (__force bool)(next->rq_flags & RQF_SORTED);
534 if (next_sorted)
535 e->type->ops.sq.elevator_merge_req_fn(q, rq, next);
536 }
538 elv_rqhash_reposition(q, rq);
540 if (next_sorted) {
541 elv_rqhash_del(q, next);
542 q->nr_sorted--;
543 }
545 q->last_merge = rq;
546 }
548 void elv_bio_merged(struct request_queue *q, struct request *rq,
549 struct bio *bio)
550 {
551 struct elevator_queue *e = q->elevator;
553 if (WARN_ON_ONCE(e->uses_mq))
554 return;
556 if (e->type->ops.sq.elevator_bio_merged_fn)
557 e->type->ops.sq.elevator_bio_merged_fn(q, rq, bio);
558 }
560 #ifdef CONFIG_PM
561 static void blk_pm_requeue_request(struct request *rq)
562 {
563 if (rq->q->dev && !(rq->rq_flags & RQF_PM))
564 rq->q->nr_pending--;
565 }
567 static void blk_pm_add_request(struct request_queue *q, struct request *rq)
568 {
569 if (q->dev && !(rq->rq_flags & RQF_PM) && q->nr_pending++ == 0 &&
570 (q->rpm_status == RPM_SUSPENDED || q->rpm_status == RPM_SUSPENDING))
571 pm_request_resume(q->dev);
572 }
573 #else
574 static inline void blk_pm_requeue_request(struct request *rq) {}
575 static inline void blk_pm_add_request(struct request_queue *q,
576 struct request *rq)
577 {
578 }
579 #endif
581 void elv_requeue_request(struct request_queue *q, struct request *rq)
582 {
583 /*
584 * it already went through dequeue, we need to decrement the
585 * in_flight count again
586 */
587 if (blk_account_rq(rq)) {
588 q->in_flight[rq_is_sync(rq)]--;
589 if (rq->rq_flags & RQF_SORTED)
590 elv_deactivate_rq(q, rq);
591 }
593 rq->rq_flags &= ~RQF_STARTED;
595 blk_pm_requeue_request(rq);
597 __elv_add_request(q, rq, ELEVATOR_INSERT_REQUEUE);
598 }
600 void elv_drain_elevator(struct request_queue *q)
601 {
602 struct elevator_queue *e = q->elevator;
603 static int printed;
605 if (WARN_ON_ONCE(e->uses_mq))
606 return;
608 lockdep_assert_held(q->queue_lock);
610 while (e->type->ops.sq.elevator_dispatch_fn(q, 1))
611 ;
612 if (q->nr_sorted && !blk_queue_is_zoned(q) && printed++ < 10 ) {
613 printk(KERN_ERR "%s: forced dispatching is broken "
614 "(nr_sorted=%u), please report this\n",
615 q->elevator->type->elevator_name, q->nr_sorted);
616 }
617 }
619 void __elv_add_request(struct request_queue *q, struct request *rq, int where)
620 {
621 trace_block_rq_insert(q, rq);
623 blk_pm_add_request(q, rq);
625 rq->q = q;
627 if (rq->rq_flags & RQF_SOFTBARRIER) {
628 /* barriers are scheduling boundary, update end_sector */
629 if (!blk_rq_is_passthrough(rq)) {
630 q->end_sector = rq_end_sector(rq);
631 q->boundary_rq = rq;
632 }
633 } else if (!(rq->rq_flags & RQF_ELVPRIV) &&
634 (where == ELEVATOR_INSERT_SORT ||
635 where == ELEVATOR_INSERT_SORT_MERGE))
636 where = ELEVATOR_INSERT_BACK;
638 switch (where) {
639 case ELEVATOR_INSERT_REQUEUE:
640 case ELEVATOR_INSERT_FRONT:
641 rq->rq_flags |= RQF_SOFTBARRIER;
642 list_add(&rq->queuelist, &q->queue_head);
643 break;
645 case ELEVATOR_INSERT_BACK:
646 rq->rq_flags |= RQF_SOFTBARRIER;
647 elv_drain_elevator(q);
648 list_add_tail(&rq->queuelist, &q->queue_head);
649 /*
650 * We kick the queue here for the following reasons.
651 * - The elevator might have returned NULL previously
652 * to delay requests and returned them now. As the
653 * queue wasn't empty before this request, ll_rw_blk
654 * won't run the queue on return, resulting in hang.
655 * - Usually, back inserted requests won't be merged
656 * with anything. There's no point in delaying queue
657 * processing.
658 */
659 __blk_run_queue(q);
660 break;
662 case ELEVATOR_INSERT_SORT_MERGE:
663 /*
664 * If we succeed in merging this request with one in the
665 * queue already, we are done - rq has now been freed,
666 * so no need to do anything further.
667 */
668 if (elv_attempt_insert_merge(q, rq))
669 break;
670 /* fall through */
671 case ELEVATOR_INSERT_SORT:
672 BUG_ON(blk_rq_is_passthrough(rq));
673 rq->rq_flags |= RQF_SORTED;
674 q->nr_sorted++;
675 if (rq_mergeable(rq)) {
676 elv_rqhash_add(q, rq);
677 if (!q->last_merge)
678 q->last_merge = rq;
679 }
681 /*
682 * Some ioscheds (cfq) run q->request_fn directly, so
683 * rq cannot be accessed after calling
684 * elevator_add_req_fn.
685 */
686 q->elevator->type->ops.sq.elevator_add_req_fn(q, rq);
687 break;
689 case ELEVATOR_INSERT_FLUSH:
690 rq->rq_flags |= RQF_SOFTBARRIER;
691 blk_insert_flush(rq);
692 break;
693 default:
694 printk(KERN_ERR "%s: bad insertion point %d\n",
695 __func__, where);
696 BUG();
697 }
698 }
699 EXPORT_SYMBOL(__elv_add_request);
701 void elv_add_request(struct request_queue *q, struct request *rq, int where)
702 {
703 unsigned long flags;
705 spin_lock_irqsave(q->queue_lock, flags);
706 __elv_add_request(q, rq, where);
707 spin_unlock_irqrestore(q->queue_lock, flags);
708 }
709 EXPORT_SYMBOL(elv_add_request);
711 struct request *elv_latter_request(struct request_queue *q, struct request *rq)
712 {
713 struct elevator_queue *e = q->elevator;
715 if (e->uses_mq && e->type->ops.mq.next_request)
716 return e->type->ops.mq.next_request(q, rq);
717 else if (!e->uses_mq && e->type->ops.sq.elevator_latter_req_fn)
718 return e->type->ops.sq.elevator_latter_req_fn(q, rq);
720 return NULL;
721 }
723 struct request *elv_former_request(struct request_queue *q, struct request *rq)
724 {
725 struct elevator_queue *e = q->elevator;
727 if (e->uses_mq && e->type->ops.mq.former_request)
728 return e->type->ops.mq.former_request(q, rq);
729 if (!e->uses_mq && e->type->ops.sq.elevator_former_req_fn)
730 return e->type->ops.sq.elevator_former_req_fn(q, rq);
731 return NULL;
732 }
734 int elv_set_request(struct request_queue *q, struct request *rq,
735 struct bio *bio, gfp_t gfp_mask)
736 {
737 struct elevator_queue *e = q->elevator;
739 if (WARN_ON_ONCE(e->uses_mq))
740 return 0;
742 if (e->type->ops.sq.elevator_set_req_fn)
743 return e->type->ops.sq.elevator_set_req_fn(q, rq, bio, gfp_mask);
744 return 0;
745 }
747 void elv_put_request(struct request_queue *q, struct request *rq)
748 {
749 struct elevator_queue *e = q->elevator;
751 if (WARN_ON_ONCE(e->uses_mq))
752 return;
754 if (e->type->ops.sq.elevator_put_req_fn)
755 e->type->ops.sq.elevator_put_req_fn(rq);
756 }
758 int elv_may_queue(struct request_queue *q, unsigned int op)
759 {
760 struct elevator_queue *e = q->elevator;
762 if (WARN_ON_ONCE(e->uses_mq))
763 return 0;
765 if (e->type->ops.sq.elevator_may_queue_fn)
766 return e->type->ops.sq.elevator_may_queue_fn(q, op);
768 return ELV_MQUEUE_MAY;
769 }
771 void elv_completed_request(struct request_queue *q, struct request *rq)
772 {
773 struct elevator_queue *e = q->elevator;
775 if (WARN_ON_ONCE(e->uses_mq))
776 return;
778 /*
779 * request is released from the driver, io must be done
780 */
781 if (blk_account_rq(rq)) {
782 q->in_flight[rq_is_sync(rq)]--;
783 if ((rq->rq_flags & RQF_SORTED) &&
784 e->type->ops.sq.elevator_completed_req_fn)
785 e->type->ops.sq.elevator_completed_req_fn(q, rq);
786 }
787 }
789 #define to_elv(atr) container_of((atr), struct elv_fs_entry, attr)
791 static ssize_t
792 elv_attr_show(struct kobject *kobj, struct attribute *attr, char *page)
793 {
794 struct elv_fs_entry *entry = to_elv(attr);
795 struct elevator_queue *e;
796 ssize_t error;
798 if (!entry->show)
799 return -EIO;
801 e = container_of(kobj, struct elevator_queue, kobj);
802 mutex_lock(&e->sysfs_lock);
803 error = e->type ? entry->show(e, page) : -ENOENT;
804 mutex_unlock(&e->sysfs_lock);
805 return error;
806 }
808 static ssize_t
809 elv_attr_store(struct kobject *kobj, struct attribute *attr,
810 const char *page, size_t length)
811 {
812 struct elv_fs_entry *entry = to_elv(attr);
813 struct elevator_queue *e;
814 ssize_t error;
816 if (!entry->store)
817 return -EIO;
819 e = container_of(kobj, struct elevator_queue, kobj);
820 mutex_lock(&e->sysfs_lock);
821 error = e->type ? entry->store(e, page, length) : -ENOENT;
822 mutex_unlock(&e->sysfs_lock);
823 return error;
824 }
826 static const struct sysfs_ops elv_sysfs_ops = {
827 .show = elv_attr_show,
828 .store = elv_attr_store,
829 };
831 static struct kobj_type elv_ktype = {
832 .sysfs_ops = &elv_sysfs_ops,
833 .release = elevator_release,
834 };
836 int elv_register_queue(struct request_queue *q)
837 {
838 struct elevator_queue *e = q->elevator;
839 int error;
841 lockdep_assert_held(&q->sysfs_lock);
843 error = kobject_add(&e->kobj, &q->kobj, "%s", "iosched");
844 if (!error) {
845 struct elv_fs_entry *attr = e->type->elevator_attrs;
846 if (attr) {
847 while (attr->attr.name) {
848 if (sysfs_create_file(&e->kobj, &attr->attr))
849 break;
850 attr++;
851 }
852 }
853 kobject_uevent(&e->kobj, KOBJ_ADD);
854 e->registered = 1;
855 if (!e->uses_mq && e->type->ops.sq.elevator_registered_fn)
856 e->type->ops.sq.elevator_registered_fn(q);
857 }
858 return error;
859 }
861 void elv_unregister_queue(struct request_queue *q)
862 {
863 lockdep_assert_held(&q->sysfs_lock);
865 if (q) {
866 struct elevator_queue *e = q->elevator;
868 kobject_uevent(&e->kobj, KOBJ_REMOVE);
869 kobject_del(&e->kobj);
870 e->registered = 0;
871 /* Re-enable throttling in case elevator disabled it */
872 wbt_enable_default(q);
873 }
874 }
876 int elv_register(struct elevator_type *e)
877 {
878 char *def = "";
880 /* create icq_cache if requested */
881 if (e->icq_size) {
882 if (WARN_ON(e->icq_size < sizeof(struct io_cq)) ||
883 WARN_ON(e->icq_align < __alignof__(struct io_cq)))
884 return -EINVAL;
886 snprintf(e->icq_cache_name, sizeof(e->icq_cache_name),
887 "%s_io_cq", e->elevator_name);
888 e->icq_cache = kmem_cache_create(e->icq_cache_name, e->icq_size,
889 e->icq_align, 0, NULL);
890 if (!e->icq_cache)
891 return -ENOMEM;
892 }
894 /* register, don't allow duplicate names */
895 spin_lock(&elv_list_lock);
896 if (elevator_find(e->elevator_name, e->uses_mq)) {
897 spin_unlock(&elv_list_lock);
898 kmem_cache_destroy(e->icq_cache);
899 return -EBUSY;
900 }
901 list_add_tail(&e->list, &elv_list);
902 spin_unlock(&elv_list_lock);
904 /* print pretty message */
905 if (elevator_match(e, chosen_elevator) ||
906 (!*chosen_elevator &&
907 elevator_match(e, CONFIG_DEFAULT_IOSCHED)))
908 def = " (default)";
910 printk(KERN_INFO "io scheduler %s registered%s\n", e->elevator_name,
911 def);
912 return 0;
913 }
914 EXPORT_SYMBOL_GPL(elv_register);
916 void elv_unregister(struct elevator_type *e)
917 {
918 /* unregister */
919 spin_lock(&elv_list_lock);
920 list_del_init(&e->list);
921 spin_unlock(&elv_list_lock);
923 /*
924 * Destroy icq_cache if it exists. icq's are RCU managed. Make
925 * sure all RCU operations are complete before proceeding.
926 */
927 if (e->icq_cache) {
928 rcu_barrier();
929 kmem_cache_destroy(e->icq_cache);
930 e->icq_cache = NULL;
931 }
932 }
933 EXPORT_SYMBOL_GPL(elv_unregister);
935 int elevator_switch_mq(struct request_queue *q,
936 struct elevator_type *new_e)
937 {
938 int ret;
940 lockdep_assert_held(&q->sysfs_lock);
942 if (q->elevator) {
943 if (q->elevator->registered)
944 elv_unregister_queue(q);
945 ioc_clear_queue(q);
946 elevator_exit(q, q->elevator);
947 }
949 ret = blk_mq_init_sched(q, new_e);
950 if (ret)
951 goto out;
953 if (new_e) {
954 ret = elv_register_queue(q);
955 if (ret) {
956 elevator_exit(q, q->elevator);
957 goto out;
958 }
959 }
961 if (new_e)
962 blk_add_trace_msg(q, "elv switch: %s", new_e->elevator_name);
963 else
964 blk_add_trace_msg(q, "elv switch: none");
966 out:
967 return ret;
968 }
970 /*
971 * For blk-mq devices, we default to using mq-deadline, if available, for single
972 * queue devices. If deadline isn't available OR we have multiple queues,
973 * default to "none".
974 */
975 int elevator_init_mq(struct request_queue *q)
976 {
977 struct elevator_type *e;
978 int err = 0;
980 if (q->nr_hw_queues != 1)
981 return 0;
983 /*
984 * q->sysfs_lock must be held to provide mutual exclusion between
985 * elevator_switch() and here.
986 */
987 mutex_lock(&q->sysfs_lock);
988 if (unlikely(q->elevator))
989 goto out_unlock;
991 e = elevator_get(q, "mq-deadline", false);
992 if (!e)
993 goto out_unlock;
995 err = blk_mq_init_sched(q, e);
996 if (err)
997 elevator_put(e);
998 out_unlock:
999 mutex_unlock(&q->sysfs_lock);
1000 return err;
1001 }
1004 /*
1005 * switch to new_e io scheduler. be careful not to introduce deadlocks -
1006 * we don't free the old io scheduler, before we have allocated what we
1007 * need for the new one. this way we have a chance of going back to the old
1008 * one, if the new one fails init for some reason.
1009 */
1010 static int elevator_switch(struct request_queue *q, struct elevator_type *new_e)
1011 {
1012 struct elevator_queue *old = q->elevator;
1013 bool old_registered = false;
1014 int err;
1016 lockdep_assert_held(&q->sysfs_lock);
1018 if (q->mq_ops) {
1019 blk_mq_freeze_queue(q);
1020 blk_mq_quiesce_queue(q);
1022 err = elevator_switch_mq(q, new_e);
1024 blk_mq_unquiesce_queue(q);
1025 blk_mq_unfreeze_queue(q);
1027 return err;
1028 }
1030 /*
1031 * Turn on BYPASS and drain all requests w/ elevator private data.
1032 * Block layer doesn't call into a quiesced elevator - all requests
1033 * are directly put on the dispatch list without elevator data
1034 * using INSERT_BACK. All requests have SOFTBARRIER set and no
1035 * merge happens either.
1036 */
1037 if (old) {
1038 old_registered = old->registered;
1040 blk_queue_bypass_start(q);
1042 /* unregister and clear all auxiliary data of the old elevator */
1043 if (old_registered)
1044 elv_unregister_queue(q);
1046 ioc_clear_queue(q);
1047 }
1049 /* allocate, init and register new elevator */
1050 err = new_e->ops.sq.elevator_init_fn(q, new_e);
1051 if (err)
1052 goto fail_init;
1054 err = elv_register_queue(q);
1055 if (err)
1056 goto fail_register;
1058 /* done, kill the old one and finish */
1059 if (old) {
1060 elevator_exit(q, old);
1061 blk_queue_bypass_end(q);
1062 }
1064 blk_add_trace_msg(q, "elv switch: %s", new_e->elevator_name);
1066 return 0;
1068 fail_register:
1069 elevator_exit(q, q->elevator);
1070 fail_init:
1071 /* switch failed, restore and re-register old elevator */
1072 if (old) {
1073 q->elevator = old;
1074 elv_register_queue(q);
1075 blk_queue_bypass_end(q);
1076 }
1078 return err;
1079 }
1081 /*
1082 * Switch this queue to the given IO scheduler.
1083 */
1084 static int __elevator_change(struct request_queue *q, const char *name)
1085 {
1086 char elevator_name[ELV_NAME_MAX];
1087 struct elevator_type *e;
1089 /* Make sure queue is not in the middle of being removed */
1090 if (!test_bit(QUEUE_FLAG_REGISTERED, &q->queue_flags))
1091 return -ENOENT;
1093 /*
1094 * Special case for mq, turn off scheduling
1095 */
1096 if (q->mq_ops && !strncmp(name, "none", 4))
1097 return elevator_switch(q, NULL);
1099 strlcpy(elevator_name, name, sizeof(elevator_name));
1100 e = elevator_get(q, strstrip(elevator_name), true);
1101 if (!e)
1102 return -EINVAL;
1104 if (q->elevator && elevator_match(q->elevator->type, elevator_name)) {
1105 elevator_put(e);
1106 return 0;
1107 }
1109 return elevator_switch(q, e);
1110 }
1112 static inline bool elv_support_iosched(struct request_queue *q)
1113 {
1114 if (q->mq_ops && q->tag_set && (q->tag_set->flags &
1115 BLK_MQ_F_NO_SCHED))
1116 return false;
1117 return true;
1118 }
1120 ssize_t elv_iosched_store(struct request_queue *q, const char *name,
1121 size_t count)
1122 {
1123 int ret;
1125 if (!(q->mq_ops || q->request_fn) || !elv_support_iosched(q))
1126 return count;
1128 ret = __elevator_change(q, name);
1129 if (!ret)
1130 return count;
1132 return ret;
1133 }
1135 ssize_t elv_iosched_show(struct request_queue *q, char *name)
1136 {
1137 struct elevator_queue *e = q->elevator;
1138 struct elevator_type *elv = NULL;
1139 struct elevator_type *__e;
1140 bool uses_mq = q->mq_ops != NULL;
1141 int len = 0;
1143 if (!queue_is_rq_based(q))
1144 return sprintf(name, "none\n");
1146 if (!q->elevator)
1147 len += sprintf(name+len, "[none] ");
1148 else
1149 elv = e->type;
1151 spin_lock(&elv_list_lock);
1152 list_for_each_entry(__e, &elv_list, list) {
1153 if (elv && elevator_match(elv, __e->elevator_name) &&
1154 (__e->uses_mq == uses_mq)) {
1155 len += sprintf(name+len, "[%s] ", elv->elevator_name);
1156 continue;
1157 }
1158 if (__e->uses_mq && q->mq_ops && elv_support_iosched(q))
1159 len += sprintf(name+len, "%s ", __e->elevator_name);
1160 else if (!__e->uses_mq && !q->mq_ops)
1161 len += sprintf(name+len, "%s ", __e->elevator_name);
1162 }
1163 spin_unlock(&elv_list_lock);
1165 if (q->mq_ops && q->elevator)
1166 len += sprintf(name+len, "none");
1168 len += sprintf(len+name, "\n");
1169 return len;
1170 }
1172 struct request *elv_rb_former_request(struct request_queue *q,
1173 struct request *rq)
1174 {
1175 struct rb_node *rbprev = rb_prev(&rq->rb_node);
1177 if (rbprev)
1178 return rb_entry_rq(rbprev);
1180 return NULL;
1181 }
1182 EXPORT_SYMBOL(elv_rb_former_request);
1184 struct request *elv_rb_latter_request(struct request_queue *q,
1185 struct request *rq)
1186 {
1187 struct rb_node *rbnext = rb_next(&rq->rb_node);
1189 if (rbnext)
1190 return rb_entry_rq(rbnext);
1192 return NULL;
1193 }
1194 EXPORT_SYMBOL(elv_rb_latter_request);