]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/hwspinlock.git/blob - drivers/dma/dmaengine.c
Merge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/dtor/input
[rpmsg/hwspinlock.git] / drivers / dma / dmaengine.c
1 /*
2  * Copyright(c) 2004 - 2006 Intel Corporation. All rights reserved.
3  *
4  * This program is free software; you can redistribute it and/or modify it
5  * under the terms of the GNU General Public License as published by the Free
6  * Software Foundation; either version 2 of the License, or (at your option)
7  * any later version.
8  *
9  * This program is distributed in the hope that it will be useful, but WITHOUT
10  * ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or
11  * FITNESS FOR A PARTICULAR PURPOSE.  See the GNU General Public License for
12  * more details.
13  *
14  * The full GNU General Public License is included in this distribution in the
15  * file called COPYING.
16  */
18 /*
19  * This code implements the DMA subsystem. It provides a HW-neutral interface
20  * for other kernel code to use asynchronous memory copy capabilities,
21  * if present, and allows different HW DMA drivers to register as providing
22  * this capability.
23  *
24  * Due to the fact we are accelerating what is already a relatively fast
25  * operation, the code goes to great lengths to avoid additional overhead,
26  * such as locking.
27  *
28  * LOCKING:
29  *
30  * The subsystem keeps a global list of dma_device structs it is protected by a
31  * mutex, dma_list_mutex.
32  *
33  * A subsystem can get access to a channel by calling dmaengine_get() followed
34  * by dma_find_channel(), or if it has need for an exclusive channel it can call
35  * dma_request_channel().  Once a channel is allocated a reference is taken
36  * against its corresponding driver to disable removal.
37  *
38  * Each device has a channels list, which runs unlocked but is never modified
39  * once the device is registered, it's just setup by the driver.
40  *
41  * See Documentation/driver-api/dmaengine for more details
42  */
44 #define pr_fmt(fmt) KBUILD_MODNAME ": " fmt
46 #include <linux/platform_device.h>
47 #include <linux/dma-mapping.h>
48 #include <linux/init.h>
49 #include <linux/module.h>
50 #include <linux/mm.h>
51 #include <linux/device.h>
52 #include <linux/dmaengine.h>
53 #include <linux/hardirq.h>
54 #include <linux/spinlock.h>
55 #include <linux/percpu.h>
56 #include <linux/rcupdate.h>
57 #include <linux/mutex.h>
58 #include <linux/jiffies.h>
59 #include <linux/rculist.h>
60 #include <linux/idr.h>
61 #include <linux/slab.h>
62 #include <linux/acpi.h>
63 #include <linux/acpi_dma.h>
64 #include <linux/of_dma.h>
65 #include <linux/mempool.h>
67 static DEFINE_MUTEX(dma_list_mutex);
68 static DEFINE_IDA(dma_ida);
69 static LIST_HEAD(dma_device_list);
70 static long dmaengine_ref_count;
72 /* --- sysfs implementation --- */
74 /**
75  * dev_to_dma_chan - convert a device pointer to the its sysfs container object
76  * @dev - device node
77  *
78  * Must be called under dma_list_mutex
79  */
80 static struct dma_chan *dev_to_dma_chan(struct device *dev)
81 {
82         struct dma_chan_dev *chan_dev;
84         chan_dev = container_of(dev, typeof(*chan_dev), device);
85         return chan_dev->chan;
86 }
88 static ssize_t memcpy_count_show(struct device *dev,
89                                  struct device_attribute *attr, char *buf)
90 {
91         struct dma_chan *chan;
92         unsigned long count = 0;
93         int i;
94         int err;
96         mutex_lock(&dma_list_mutex);
97         chan = dev_to_dma_chan(dev);
98         if (chan) {
99                 for_each_possible_cpu(i)
100                         count += per_cpu_ptr(chan->local, i)->memcpy_count;
101                 err = sprintf(buf, "%lu\n", count);
102         } else
103                 err = -ENODEV;
104         mutex_unlock(&dma_list_mutex);
106         return err;
108 static DEVICE_ATTR_RO(memcpy_count);
110 static ssize_t bytes_transferred_show(struct device *dev,
111                                       struct device_attribute *attr, char *buf)
113         struct dma_chan *chan;
114         unsigned long count = 0;
115         int i;
116         int err;
118         mutex_lock(&dma_list_mutex);
119         chan = dev_to_dma_chan(dev);
120         if (chan) {
121                 for_each_possible_cpu(i)
122                         count += per_cpu_ptr(chan->local, i)->bytes_transferred;
123                 err = sprintf(buf, "%lu\n", count);
124         } else
125                 err = -ENODEV;
126         mutex_unlock(&dma_list_mutex);
128         return err;
130 static DEVICE_ATTR_RO(bytes_transferred);
132 static ssize_t in_use_show(struct device *dev, struct device_attribute *attr,
133                            char *buf)
135         struct dma_chan *chan;
136         int err;
138         mutex_lock(&dma_list_mutex);
139         chan = dev_to_dma_chan(dev);
140         if (chan)
141                 err = sprintf(buf, "%d\n", chan->client_count);
142         else
143                 err = -ENODEV;
144         mutex_unlock(&dma_list_mutex);
146         return err;
148 static DEVICE_ATTR_RO(in_use);
150 static struct attribute *dma_dev_attrs[] = {
151         &dev_attr_memcpy_count.attr,
152         &dev_attr_bytes_transferred.attr,
153         &dev_attr_in_use.attr,
154         NULL,
155 };
156 ATTRIBUTE_GROUPS(dma_dev);
158 static void chan_dev_release(struct device *dev)
160         struct dma_chan_dev *chan_dev;
162         chan_dev = container_of(dev, typeof(*chan_dev), device);
163         if (atomic_dec_and_test(chan_dev->idr_ref)) {
164                 ida_free(&dma_ida, chan_dev->dev_id);
165                 kfree(chan_dev->idr_ref);
166         }
167         kfree(chan_dev);
170 static struct class dma_devclass = {
171         .name           = "dma",
172         .dev_groups     = dma_dev_groups,
173         .dev_release    = chan_dev_release,
174 };
176 /* --- client and device registration --- */
178 #define dma_device_satisfies_mask(device, mask) \
179         __dma_device_satisfies_mask((device), &(mask))
180 static int
181 __dma_device_satisfies_mask(struct dma_device *device,
182                             const dma_cap_mask_t *want)
184         dma_cap_mask_t has;
186         bitmap_and(has.bits, want->bits, device->cap_mask.bits,
187                 DMA_TX_TYPE_END);
188         return bitmap_equal(want->bits, has.bits, DMA_TX_TYPE_END);
191 static struct module *dma_chan_to_owner(struct dma_chan *chan)
193         return chan->device->dev->driver->owner;
196 /**
197  * balance_ref_count - catch up the channel reference count
198  * @chan - channel to balance ->client_count versus dmaengine_ref_count
199  *
200  * balance_ref_count must be called under dma_list_mutex
201  */
202 static void balance_ref_count(struct dma_chan *chan)
204         struct module *owner = dma_chan_to_owner(chan);
206         while (chan->client_count < dmaengine_ref_count) {
207                 __module_get(owner);
208                 chan->client_count++;
209         }
212 /**
213  * dma_chan_get - try to grab a dma channel's parent driver module
214  * @chan - channel to grab
215  *
216  * Must be called under dma_list_mutex
217  */
218 static int dma_chan_get(struct dma_chan *chan)
220         struct module *owner = dma_chan_to_owner(chan);
221         int ret;
223         /* The channel is already in use, update client count */
224         if (chan->client_count) {
225                 __module_get(owner);
226                 goto out;
227         }
229         if (!try_module_get(owner))
230                 return -ENODEV;
232         /* allocate upon first client reference */
233         if (chan->device->device_alloc_chan_resources) {
234                 ret = chan->device->device_alloc_chan_resources(chan);
235                 if (ret < 0)
236                         goto err_out;
237         }
239         if (!dma_has_cap(DMA_PRIVATE, chan->device->cap_mask))
240                 balance_ref_count(chan);
242 out:
243         chan->client_count++;
244         return 0;
246 err_out:
247         module_put(owner);
248         return ret;
251 /**
252  * dma_chan_put - drop a reference to a dma channel's parent driver module
253  * @chan - channel to release
254  *
255  * Must be called under dma_list_mutex
256  */
257 static void dma_chan_put(struct dma_chan *chan)
259         /* This channel is not in use, bail out */
260         if (!chan->client_count)
261                 return;
263         chan->client_count--;
264         module_put(dma_chan_to_owner(chan));
266         /* This channel is not in use anymore, free it */
267         if (!chan->client_count && chan->device->device_free_chan_resources) {
268                 /* Make sure all operations have completed */
269                 dmaengine_synchronize(chan);
270                 chan->device->device_free_chan_resources(chan);
271         }
273         /* If the channel is used via a DMA request router, free the mapping */
274         if (chan->router && chan->router->route_free) {
275                 chan->router->route_free(chan->router->dev, chan->route_data);
276                 chan->router = NULL;
277                 chan->route_data = NULL;
278         }
281 enum dma_status dma_sync_wait(struct dma_chan *chan, dma_cookie_t cookie)
283         enum dma_status status;
284         unsigned long dma_sync_wait_timeout = jiffies + msecs_to_jiffies(5000);
286         dma_async_issue_pending(chan);
287         do {
288                 status = dma_async_is_tx_complete(chan, cookie, NULL, NULL);
289                 if (time_after_eq(jiffies, dma_sync_wait_timeout)) {
290                         dev_err(chan->device->dev, "%s: timeout!\n", __func__);
291                         return DMA_ERROR;
292                 }
293                 if (status != DMA_IN_PROGRESS)
294                         break;
295                 cpu_relax();
296         } while (1);
298         return status;
300 EXPORT_SYMBOL(dma_sync_wait);
302 /**
303  * dma_cap_mask_all - enable iteration over all operation types
304  */
305 static dma_cap_mask_t dma_cap_mask_all;
307 /**
308  * dma_chan_tbl_ent - tracks channel allocations per core/operation
309  * @chan - associated channel for this entry
310  */
311 struct dma_chan_tbl_ent {
312         struct dma_chan *chan;
313 };
315 /**
316  * channel_table - percpu lookup table for memory-to-memory offload providers
317  */
318 static struct dma_chan_tbl_ent __percpu *channel_table[DMA_TX_TYPE_END];
320 static int __init dma_channel_table_init(void)
322         enum dma_transaction_type cap;
323         int err = 0;
325         bitmap_fill(dma_cap_mask_all.bits, DMA_TX_TYPE_END);
327         /* 'interrupt', 'private', and 'slave' are channel capabilities,
328          * but are not associated with an operation so they do not need
329          * an entry in the channel_table
330          */
331         clear_bit(DMA_INTERRUPT, dma_cap_mask_all.bits);
332         clear_bit(DMA_PRIVATE, dma_cap_mask_all.bits);
333         clear_bit(DMA_SLAVE, dma_cap_mask_all.bits);
335         for_each_dma_cap_mask(cap, dma_cap_mask_all) {
336                 channel_table[cap] = alloc_percpu(struct dma_chan_tbl_ent);
337                 if (!channel_table[cap]) {
338                         err = -ENOMEM;
339                         break;
340                 }
341         }
343         if (err) {
344                 pr_err("initialization failure\n");
345                 for_each_dma_cap_mask(cap, dma_cap_mask_all)
346                         free_percpu(channel_table[cap]);
347         }
349         return err;
351 arch_initcall(dma_channel_table_init);
353 /**
354  * dma_find_channel - find a channel to carry out the operation
355  * @tx_type: transaction type
356  */
357 struct dma_chan *dma_find_channel(enum dma_transaction_type tx_type)
359         return this_cpu_read(channel_table[tx_type]->chan);
361 EXPORT_SYMBOL(dma_find_channel);
363 /**
364  * dma_issue_pending_all - flush all pending operations across all channels
365  */
366 void dma_issue_pending_all(void)
368         struct dma_device *device;
369         struct dma_chan *chan;
371         rcu_read_lock();
372         list_for_each_entry_rcu(device, &dma_device_list, global_node) {
373                 if (dma_has_cap(DMA_PRIVATE, device->cap_mask))
374                         continue;
375                 list_for_each_entry(chan, &device->channels, device_node)
376                         if (chan->client_count)
377                                 device->device_issue_pending(chan);
378         }
379         rcu_read_unlock();
381 EXPORT_SYMBOL(dma_issue_pending_all);
383 /**
384  * dma_chan_is_local - returns true if the channel is in the same numa-node as the cpu
385  */
386 static bool dma_chan_is_local(struct dma_chan *chan, int cpu)
388         int node = dev_to_node(chan->device->dev);
389         return node == -1 || cpumask_test_cpu(cpu, cpumask_of_node(node));
392 /**
393  * min_chan - returns the channel with min count and in the same numa-node as the cpu
394  * @cap: capability to match
395  * @cpu: cpu index which the channel should be close to
396  *
397  * If some channels are close to the given cpu, the one with the lowest
398  * reference count is returned. Otherwise, cpu is ignored and only the
399  * reference count is taken into account.
400  * Must be called under dma_list_mutex.
401  */
402 static struct dma_chan *min_chan(enum dma_transaction_type cap, int cpu)
404         struct dma_device *device;
405         struct dma_chan *chan;
406         struct dma_chan *min = NULL;
407         struct dma_chan *localmin = NULL;
409         list_for_each_entry(device, &dma_device_list, global_node) {
410                 if (!dma_has_cap(cap, device->cap_mask) ||
411                     dma_has_cap(DMA_PRIVATE, device->cap_mask))
412                         continue;
413                 list_for_each_entry(chan, &device->channels, device_node) {
414                         if (!chan->client_count)
415                                 continue;
416                         if (!min || chan->table_count < min->table_count)
417                                 min = chan;
419                         if (dma_chan_is_local(chan, cpu))
420                                 if (!localmin ||
421                                     chan->table_count < localmin->table_count)
422                                         localmin = chan;
423                 }
424         }
426         chan = localmin ? localmin : min;
428         if (chan)
429                 chan->table_count++;
431         return chan;
434 /**
435  * dma_channel_rebalance - redistribute the available channels
436  *
437  * Optimize for cpu isolation (each cpu gets a dedicated channel for an
438  * operation type) in the SMP case,  and operation isolation (avoid
439  * multi-tasking channels) in the non-SMP case.  Must be called under
440  * dma_list_mutex.
441  */
442 static void dma_channel_rebalance(void)
444         struct dma_chan *chan;
445         struct dma_device *device;
446         int cpu;
447         int cap;
449         /* undo the last distribution */
450         for_each_dma_cap_mask(cap, dma_cap_mask_all)
451                 for_each_possible_cpu(cpu)
452                         per_cpu_ptr(channel_table[cap], cpu)->chan = NULL;
454         list_for_each_entry(device, &dma_device_list, global_node) {
455                 if (dma_has_cap(DMA_PRIVATE, device->cap_mask))
456                         continue;
457                 list_for_each_entry(chan, &device->channels, device_node)
458                         chan->table_count = 0;
459         }
461         /* don't populate the channel_table if no clients are available */
462         if (!dmaengine_ref_count)
463                 return;
465         /* redistribute available channels */
466         for_each_dma_cap_mask(cap, dma_cap_mask_all)
467                 for_each_online_cpu(cpu) {
468                         chan = min_chan(cap, cpu);
469                         per_cpu_ptr(channel_table[cap], cpu)->chan = chan;
470                 }
473 int dma_get_slave_caps(struct dma_chan *chan, struct dma_slave_caps *caps)
475         struct dma_device *device;
477         if (!chan || !caps)
478                 return -EINVAL;
480         device = chan->device;
482         /* check if the channel supports slave transactions */
483         if (!(test_bit(DMA_SLAVE, device->cap_mask.bits) ||
484               test_bit(DMA_CYCLIC, device->cap_mask.bits)))
485                 return -ENXIO;
487         /*
488          * Check whether it reports it uses the generic slave
489          * capabilities, if not, that means it doesn't support any
490          * kind of slave capabilities reporting.
491          */
492         if (!device->directions)
493                 return -ENXIO;
495         caps->src_addr_widths = device->src_addr_widths;
496         caps->dst_addr_widths = device->dst_addr_widths;
497         caps->directions = device->directions;
498         caps->max_burst = device->max_burst;
499         caps->residue_granularity = device->residue_granularity;
500         caps->descriptor_reuse = device->descriptor_reuse;
501         caps->cmd_pause = !!device->device_pause;
502         caps->cmd_resume = !!device->device_resume;
503         caps->cmd_terminate = !!device->device_terminate_all;
505         return 0;
507 EXPORT_SYMBOL_GPL(dma_get_slave_caps);
509 static struct dma_chan *private_candidate(const dma_cap_mask_t *mask,
510                                           struct dma_device *dev,
511                                           dma_filter_fn fn, void *fn_param)
513         struct dma_chan *chan;
515         if (mask && !__dma_device_satisfies_mask(dev, mask)) {
516                 dev_dbg(dev->dev, "%s: wrong capabilities\n", __func__);
517                 return NULL;
518         }
519         /* devices with multiple channels need special handling as we need to
520          * ensure that all channels are either private or public.
521          */
522         if (dev->chancnt > 1 && !dma_has_cap(DMA_PRIVATE, dev->cap_mask))
523                 list_for_each_entry(chan, &dev->channels, device_node) {
524                         /* some channels are already publicly allocated */
525                         if (chan->client_count)
526                                 return NULL;
527                 }
529         list_for_each_entry(chan, &dev->channels, device_node) {
530                 if (chan->client_count) {
531                         dev_dbg(dev->dev, "%s: %s busy\n",
532                                  __func__, dma_chan_name(chan));
533                         continue;
534                 }
535                 if (fn && !fn(chan, fn_param)) {
536                         dev_dbg(dev->dev, "%s: %s filter said false\n",
537                                  __func__, dma_chan_name(chan));
538                         continue;
539                 }
540                 return chan;
541         }
543         return NULL;
546 static struct dma_chan *find_candidate(struct dma_device *device,
547                                        const dma_cap_mask_t *mask,
548                                        dma_filter_fn fn, void *fn_param)
550         struct dma_chan *chan = private_candidate(mask, device, fn, fn_param);
551         int err;
553         if (chan) {
554                 /* Found a suitable channel, try to grab, prep, and return it.
555                  * We first set DMA_PRIVATE to disable balance_ref_count as this
556                  * channel will not be published in the general-purpose
557                  * allocator
558                  */
559                 dma_cap_set(DMA_PRIVATE, device->cap_mask);
560                 device->privatecnt++;
561                 err = dma_chan_get(chan);
563                 if (err) {
564                         if (err == -ENODEV) {
565                                 dev_dbg(device->dev, "%s: %s module removed\n",
566                                         __func__, dma_chan_name(chan));
567                                 list_del_rcu(&device->global_node);
568                         } else
569                                 dev_dbg(device->dev,
570                                         "%s: failed to get %s: (%d)\n",
571                                          __func__, dma_chan_name(chan), err);
573                         if (--device->privatecnt == 0)
574                                 dma_cap_clear(DMA_PRIVATE, device->cap_mask);
576                         chan = ERR_PTR(err);
577                 }
578         }
580         return chan ? chan : ERR_PTR(-EPROBE_DEFER);
583 /**
584  * dma_get_slave_channel - try to get specific channel exclusively
585  * @chan: target channel
586  */
587 struct dma_chan *dma_get_slave_channel(struct dma_chan *chan)
589         int err = -EBUSY;
591         /* lock against __dma_request_channel */
592         mutex_lock(&dma_list_mutex);
594         if (chan->client_count == 0) {
595                 struct dma_device *device = chan->device;
597                 dma_cap_set(DMA_PRIVATE, device->cap_mask);
598                 device->privatecnt++;
599                 err = dma_chan_get(chan);
600                 if (err) {
601                         dev_dbg(chan->device->dev,
602                                 "%s: failed to get %s: (%d)\n",
603                                 __func__, dma_chan_name(chan), err);
604                         chan = NULL;
605                         if (--device->privatecnt == 0)
606                                 dma_cap_clear(DMA_PRIVATE, device->cap_mask);
607                 }
608         } else
609                 chan = NULL;
611         mutex_unlock(&dma_list_mutex);
614         return chan;
616 EXPORT_SYMBOL_GPL(dma_get_slave_channel);
618 struct dma_chan *dma_get_any_slave_channel(struct dma_device *device)
620         dma_cap_mask_t mask;
621         struct dma_chan *chan;
623         dma_cap_zero(mask);
624         dma_cap_set(DMA_SLAVE, mask);
626         /* lock against __dma_request_channel */
627         mutex_lock(&dma_list_mutex);
629         chan = find_candidate(device, &mask, NULL, NULL);
631         mutex_unlock(&dma_list_mutex);
633         return IS_ERR(chan) ? NULL : chan;
635 EXPORT_SYMBOL_GPL(dma_get_any_slave_channel);
637 /**
638  * __dma_request_channel - try to allocate an exclusive channel
639  * @mask: capabilities that the channel must satisfy
640  * @fn: optional callback to disposition available channels
641  * @fn_param: opaque parameter to pass to dma_filter_fn
642  *
643  * Returns pointer to appropriate DMA channel on success or NULL.
644  */
645 struct dma_chan *__dma_request_channel(const dma_cap_mask_t *mask,
646                                        dma_filter_fn fn, void *fn_param)
648         struct dma_device *device, *_d;
649         struct dma_chan *chan = NULL;
651         /* Find a channel */
652         mutex_lock(&dma_list_mutex);
653         list_for_each_entry_safe(device, _d, &dma_device_list, global_node) {
654                 chan = find_candidate(device, mask, fn, fn_param);
655                 if (!IS_ERR(chan))
656                         break;
658                 chan = NULL;
659         }
660         mutex_unlock(&dma_list_mutex);
662         pr_debug("%s: %s (%s)\n",
663                  __func__,
664                  chan ? "success" : "fail",
665                  chan ? dma_chan_name(chan) : NULL);
667         return chan;
669 EXPORT_SYMBOL_GPL(__dma_request_channel);
671 static const struct dma_slave_map *dma_filter_match(struct dma_device *device,
672                                                     const char *name,
673                                                     struct device *dev)
675         int i;
677         if (!device->filter.mapcnt)
678                 return NULL;
680         for (i = 0; i < device->filter.mapcnt; i++) {
681                 const struct dma_slave_map *map = &device->filter.map[i];
683                 if (!strcmp(map->devname, dev_name(dev)) &&
684                     !strcmp(map->slave, name))
685                         return map;
686         }
688         return NULL;
691 /**
692  * dma_request_chan - try to allocate an exclusive slave channel
693  * @dev:        pointer to client device structure
694  * @name:       slave channel name
695  *
696  * Returns pointer to appropriate DMA channel on success or an error pointer.
697  */
698 struct dma_chan *dma_request_chan(struct device *dev, const char *name)
700         struct dma_device *d, *_d;
701         struct dma_chan *chan = NULL;
703         /* If device-tree is present get slave info from here */
704         if (dev->of_node)
705                 chan = of_dma_request_slave_channel(dev->of_node, name);
707         /* If device was enumerated by ACPI get slave info from here */
708         if (has_acpi_companion(dev) && !chan)
709                 chan = acpi_dma_request_slave_chan_by_name(dev, name);
711         if (chan) {
712                 /* Valid channel found or requester need to be deferred */
713                 if (!IS_ERR(chan) || PTR_ERR(chan) == -EPROBE_DEFER)
714                         return chan;
715         }
717         /* Try to find the channel via the DMA filter map(s) */
718         mutex_lock(&dma_list_mutex);
719         list_for_each_entry_safe(d, _d, &dma_device_list, global_node) {
720                 dma_cap_mask_t mask;
721                 const struct dma_slave_map *map = dma_filter_match(d, name, dev);
723                 if (!map)
724                         continue;
726                 dma_cap_zero(mask);
727                 dma_cap_set(DMA_SLAVE, mask);
729                 chan = find_candidate(d, &mask, d->filter.fn, map->param);
730                 if (!IS_ERR(chan))
731                         break;
732         }
733         mutex_unlock(&dma_list_mutex);
735         return chan ? chan : ERR_PTR(-EPROBE_DEFER);
737 EXPORT_SYMBOL_GPL(dma_request_chan);
739 /**
740  * dma_request_slave_channel - try to allocate an exclusive slave channel
741  * @dev:        pointer to client device structure
742  * @name:       slave channel name
743  *
744  * Returns pointer to appropriate DMA channel on success or NULL.
745  */
746 struct dma_chan *dma_request_slave_channel(struct device *dev,
747                                            const char *name)
749         struct dma_chan *ch = dma_request_chan(dev, name);
750         if (IS_ERR(ch))
751                 return NULL;
753         return ch;
755 EXPORT_SYMBOL_GPL(dma_request_slave_channel);
757 /**
758  * dma_request_chan_by_mask - allocate a channel satisfying certain capabilities
759  * @mask: capabilities that the channel must satisfy
760  *
761  * Returns pointer to appropriate DMA channel on success or an error pointer.
762  */
763 struct dma_chan *dma_request_chan_by_mask(const dma_cap_mask_t *mask)
765         struct dma_chan *chan;
767         if (!mask)
768                 return ERR_PTR(-ENODEV);
770         chan = __dma_request_channel(mask, NULL, NULL);
771         if (!chan) {
772                 mutex_lock(&dma_list_mutex);
773                 if (list_empty(&dma_device_list))
774                         chan = ERR_PTR(-EPROBE_DEFER);
775                 else
776                         chan = ERR_PTR(-ENODEV);
777                 mutex_unlock(&dma_list_mutex);
778         }
780         return chan;
782 EXPORT_SYMBOL_GPL(dma_request_chan_by_mask);
784 void dma_release_channel(struct dma_chan *chan)
786         mutex_lock(&dma_list_mutex);
787         WARN_ONCE(chan->client_count != 1,
788                   "chan reference count %d != 1\n", chan->client_count);
789         dma_chan_put(chan);
790         /* drop PRIVATE cap enabled by __dma_request_channel() */
791         if (--chan->device->privatecnt == 0)
792                 dma_cap_clear(DMA_PRIVATE, chan->device->cap_mask);
793         mutex_unlock(&dma_list_mutex);
795 EXPORT_SYMBOL_GPL(dma_release_channel);
797 /**
798  * dmaengine_get - register interest in dma_channels
799  */
800 void dmaengine_get(void)
802         struct dma_device *device, *_d;
803         struct dma_chan *chan;
804         int err;
806         mutex_lock(&dma_list_mutex);
807         dmaengine_ref_count++;
809         /* try to grab channels */
810         list_for_each_entry_safe(device, _d, &dma_device_list, global_node) {
811                 if (dma_has_cap(DMA_PRIVATE, device->cap_mask))
812                         continue;
813                 list_for_each_entry(chan, &device->channels, device_node) {
814                         err = dma_chan_get(chan);
815                         if (err == -ENODEV) {
816                                 /* module removed before we could use it */
817                                 list_del_rcu(&device->global_node);
818                                 break;
819                         } else if (err)
820                                 dev_dbg(chan->device->dev,
821                                         "%s: failed to get %s: (%d)\n",
822                                         __func__, dma_chan_name(chan), err);
823                 }
824         }
826         /* if this is the first reference and there were channels
827          * waiting we need to rebalance to get those channels
828          * incorporated into the channel table
829          */
830         if (dmaengine_ref_count == 1)
831                 dma_channel_rebalance();
832         mutex_unlock(&dma_list_mutex);
834 EXPORT_SYMBOL(dmaengine_get);
836 /**
837  * dmaengine_put - let dma drivers be removed when ref_count == 0
838  */
839 void dmaengine_put(void)
841         struct dma_device *device;
842         struct dma_chan *chan;
844         mutex_lock(&dma_list_mutex);
845         dmaengine_ref_count--;
846         BUG_ON(dmaengine_ref_count < 0);
847         /* drop channel references */
848         list_for_each_entry(device, &dma_device_list, global_node) {
849                 if (dma_has_cap(DMA_PRIVATE, device->cap_mask))
850                         continue;
851                 list_for_each_entry(chan, &device->channels, device_node)
852                         dma_chan_put(chan);
853         }
854         mutex_unlock(&dma_list_mutex);
856 EXPORT_SYMBOL(dmaengine_put);
858 static bool device_has_all_tx_types(struct dma_device *device)
860         /* A device that satisfies this test has channels that will never cause
861          * an async_tx channel switch event as all possible operation types can
862          * be handled.
863          */
864         #ifdef CONFIG_ASYNC_TX_DMA
865         if (!dma_has_cap(DMA_INTERRUPT, device->cap_mask))
866                 return false;
867         #endif
869         #if IS_ENABLED(CONFIG_ASYNC_MEMCPY)
870         if (!dma_has_cap(DMA_MEMCPY, device->cap_mask))
871                 return false;
872         #endif
874         #if IS_ENABLED(CONFIG_ASYNC_XOR)
875         if (!dma_has_cap(DMA_XOR, device->cap_mask))
876                 return false;
878         #ifndef CONFIG_ASYNC_TX_DISABLE_XOR_VAL_DMA
879         if (!dma_has_cap(DMA_XOR_VAL, device->cap_mask))
880                 return false;
881         #endif
882         #endif
884         #if IS_ENABLED(CONFIG_ASYNC_PQ)
885         if (!dma_has_cap(DMA_PQ, device->cap_mask))
886                 return false;
888         #ifndef CONFIG_ASYNC_TX_DISABLE_PQ_VAL_DMA
889         if (!dma_has_cap(DMA_PQ_VAL, device->cap_mask))
890                 return false;
891         #endif
892         #endif
894         return true;
897 static int get_dma_id(struct dma_device *device)
899         int rc = ida_alloc(&dma_ida, GFP_KERNEL);
901         if (rc < 0)
902                 return rc;
903         device->dev_id = rc;
904         return 0;
907 /**
908  * dma_async_device_register - registers DMA devices found
909  * @device: &dma_device
910  */
911 int dma_async_device_register(struct dma_device *device)
913         int chancnt = 0, rc;
914         struct dma_chan* chan;
915         atomic_t *idr_ref;
917         if (!device)
918                 return -ENODEV;
920         /* validate device routines */
921         if (!device->dev) {
922                 pr_err("DMAdevice must have dev\n");
923                 return -EIO;
924         }
926         if (dma_has_cap(DMA_MEMCPY, device->cap_mask) && !device->device_prep_dma_memcpy) {
927                 dev_err(device->dev,
928                         "Device claims capability %s, but op is not defined\n",
929                         "DMA_MEMCPY");
930                 return -EIO;
931         }
933         if (dma_has_cap(DMA_XOR, device->cap_mask) && !device->device_prep_dma_xor) {
934                 dev_err(device->dev,
935                         "Device claims capability %s, but op is not defined\n",
936                         "DMA_XOR");
937                 return -EIO;
938         }
940         if (dma_has_cap(DMA_XOR_VAL, device->cap_mask) && !device->device_prep_dma_xor_val) {
941                 dev_err(device->dev,
942                         "Device claims capability %s, but op is not defined\n",
943                         "DMA_XOR_VAL");
944                 return -EIO;
945         }
947         if (dma_has_cap(DMA_PQ, device->cap_mask) && !device->device_prep_dma_pq) {
948                 dev_err(device->dev,
949                         "Device claims capability %s, but op is not defined\n",
950                         "DMA_PQ");
951                 return -EIO;
952         }
954         if (dma_has_cap(DMA_PQ_VAL, device->cap_mask) && !device->device_prep_dma_pq_val) {
955                 dev_err(device->dev,
956                         "Device claims capability %s, but op is not defined\n",
957                         "DMA_PQ_VAL");
958                 return -EIO;
959         }
961         if (dma_has_cap(DMA_MEMSET, device->cap_mask) && !device->device_prep_dma_memset) {
962                 dev_err(device->dev,
963                         "Device claims capability %s, but op is not defined\n",
964                         "DMA_MEMSET");
965                 return -EIO;
966         }
968         if (dma_has_cap(DMA_INTERRUPT, device->cap_mask) && !device->device_prep_dma_interrupt) {
969                 dev_err(device->dev,
970                         "Device claims capability %s, but op is not defined\n",
971                         "DMA_INTERRUPT");
972                 return -EIO;
973         }
975         if (dma_has_cap(DMA_CYCLIC, device->cap_mask) && !device->device_prep_dma_cyclic) {
976                 dev_err(device->dev,
977                         "Device claims capability %s, but op is not defined\n",
978                         "DMA_CYCLIC");
979                 return -EIO;
980         }
982         if (dma_has_cap(DMA_INTERLEAVE, device->cap_mask) && !device->device_prep_interleaved_dma) {
983                 dev_err(device->dev,
984                         "Device claims capability %s, but op is not defined\n",
985                         "DMA_INTERLEAVE");
986                 return -EIO;
987         }
990         if (!device->device_tx_status) {
991                 dev_err(device->dev, "Device tx_status is not defined\n");
992                 return -EIO;
993         }
996         if (!device->device_issue_pending) {
997                 dev_err(device->dev, "Device issue_pending is not defined\n");
998                 return -EIO;
999         }
1001         /* note: this only matters in the
1002          * CONFIG_ASYNC_TX_ENABLE_CHANNEL_SWITCH=n case
1003          */
1004         if (device_has_all_tx_types(device))
1005                 dma_cap_set(DMA_ASYNC_TX, device->cap_mask);
1007         idr_ref = kmalloc(sizeof(*idr_ref), GFP_KERNEL);
1008         if (!idr_ref)
1009                 return -ENOMEM;
1010         rc = get_dma_id(device);
1011         if (rc != 0) {
1012                 kfree(idr_ref);
1013                 return rc;
1014         }
1016         atomic_set(idr_ref, 0);
1018         /* represent channels in sysfs. Probably want devs too */
1019         list_for_each_entry(chan, &device->channels, device_node) {
1020                 rc = -ENOMEM;
1021                 chan->local = alloc_percpu(typeof(*chan->local));
1022                 if (chan->local == NULL)
1023                         goto err_out;
1024                 chan->dev = kzalloc(sizeof(*chan->dev), GFP_KERNEL);
1025                 if (chan->dev == NULL) {
1026                         free_percpu(chan->local);
1027                         chan->local = NULL;
1028                         goto err_out;
1029                 }
1031                 chan->chan_id = chancnt++;
1032                 chan->dev->device.class = &dma_devclass;
1033                 chan->dev->device.parent = device->dev;
1034                 chan->dev->chan = chan;
1035                 chan->dev->idr_ref = idr_ref;
1036                 chan->dev->dev_id = device->dev_id;
1037                 atomic_inc(idr_ref);
1038                 dev_set_name(&chan->dev->device, "dma%dchan%d",
1039                              device->dev_id, chan->chan_id);
1041                 rc = device_register(&chan->dev->device);
1042                 if (rc) {
1043                         free_percpu(chan->local);
1044                         chan->local = NULL;
1045                         kfree(chan->dev);
1046                         atomic_dec(idr_ref);
1047                         goto err_out;
1048                 }
1049                 chan->client_count = 0;
1050         }
1052         if (!chancnt) {
1053                 dev_err(device->dev, "%s: device has no channels!\n", __func__);
1054                 rc = -ENODEV;
1055                 goto err_out;
1056         }
1058         device->chancnt = chancnt;
1060         mutex_lock(&dma_list_mutex);
1061         /* take references on public channels */
1062         if (dmaengine_ref_count && !dma_has_cap(DMA_PRIVATE, device->cap_mask))
1063                 list_for_each_entry(chan, &device->channels, device_node) {
1064                         /* if clients are already waiting for channels we need
1065                          * to take references on their behalf
1066                          */
1067                         if (dma_chan_get(chan) == -ENODEV) {
1068                                 /* note we can only get here for the first
1069                                  * channel as the remaining channels are
1070                                  * guaranteed to get a reference
1071                                  */
1072                                 rc = -ENODEV;
1073                                 mutex_unlock(&dma_list_mutex);
1074                                 goto err_out;
1075                         }
1076                 }
1077         list_add_tail_rcu(&device->global_node, &dma_device_list);
1078         if (dma_has_cap(DMA_PRIVATE, device->cap_mask))
1079                 device->privatecnt++;   /* Always private */
1080         dma_channel_rebalance();
1081         mutex_unlock(&dma_list_mutex);
1083         return 0;
1085 err_out:
1086         /* if we never registered a channel just release the idr */
1087         if (atomic_read(idr_ref) == 0) {
1088                 ida_free(&dma_ida, device->dev_id);
1089                 kfree(idr_ref);
1090                 return rc;
1091         }
1093         list_for_each_entry(chan, &device->channels, device_node) {
1094                 if (chan->local == NULL)
1095                         continue;
1096                 mutex_lock(&dma_list_mutex);
1097                 chan->dev->chan = NULL;
1098                 mutex_unlock(&dma_list_mutex);
1099                 device_unregister(&chan->dev->device);
1100                 free_percpu(chan->local);
1101         }
1102         return rc;
1104 EXPORT_SYMBOL(dma_async_device_register);
1106 /**
1107  * dma_async_device_unregister - unregister a DMA device
1108  * @device: &dma_device
1109  *
1110  * This routine is called by dma driver exit routines, dmaengine holds module
1111  * references to prevent it being called while channels are in use.
1112  */
1113 void dma_async_device_unregister(struct dma_device *device)
1115         struct dma_chan *chan;
1117         mutex_lock(&dma_list_mutex);
1118         list_del_rcu(&device->global_node);
1119         dma_channel_rebalance();
1120         mutex_unlock(&dma_list_mutex);
1122         list_for_each_entry(chan, &device->channels, device_node) {
1123                 WARN_ONCE(chan->client_count,
1124                           "%s called while %d clients hold a reference\n",
1125                           __func__, chan->client_count);
1126                 mutex_lock(&dma_list_mutex);
1127                 chan->dev->chan = NULL;
1128                 mutex_unlock(&dma_list_mutex);
1129                 device_unregister(&chan->dev->device);
1130                 free_percpu(chan->local);
1131         }
1133 EXPORT_SYMBOL(dma_async_device_unregister);
1135 static void dmam_device_release(struct device *dev, void *res)
1137         struct dma_device *device;
1139         device = *(struct dma_device **)res;
1140         dma_async_device_unregister(device);
1143 /**
1144  * dmaenginem_async_device_register - registers DMA devices found
1145  * @device: &dma_device
1146  *
1147  * The operation is managed and will be undone on driver detach.
1148  */
1149 int dmaenginem_async_device_register(struct dma_device *device)
1151         void *p;
1152         int ret;
1154         p = devres_alloc(dmam_device_release, sizeof(void *), GFP_KERNEL);
1155         if (!p)
1156                 return -ENOMEM;
1158         ret = dma_async_device_register(device);
1159         if (!ret) {
1160                 *(struct dma_device **)p = device;
1161                 devres_add(device->dev, p);
1162         } else {
1163                 devres_free(p);
1164         }
1166         return ret;
1168 EXPORT_SYMBOL(dmaenginem_async_device_register);
1170 struct dmaengine_unmap_pool {
1171         struct kmem_cache *cache;
1172         const char *name;
1173         mempool_t *pool;
1174         size_t size;
1175 };
1177 #define __UNMAP_POOL(x) { .size = x, .name = "dmaengine-unmap-" __stringify(x) }
1178 static struct dmaengine_unmap_pool unmap_pool[] = {
1179         __UNMAP_POOL(2),
1180         #if IS_ENABLED(CONFIG_DMA_ENGINE_RAID)
1181         __UNMAP_POOL(16),
1182         __UNMAP_POOL(128),
1183         __UNMAP_POOL(256),
1184         #endif
1185 };
1187 static struct dmaengine_unmap_pool *__get_unmap_pool(int nr)
1189         int order = get_count_order(nr);
1191         switch (order) {
1192         case 0 ... 1:
1193                 return &unmap_pool[0];
1194 #if IS_ENABLED(CONFIG_DMA_ENGINE_RAID)
1195         case 2 ... 4:
1196                 return &unmap_pool[1];
1197         case 5 ... 7:
1198                 return &unmap_pool[2];
1199         case 8:
1200                 return &unmap_pool[3];
1201 #endif
1202         default:
1203                 BUG();
1204                 return NULL;
1205         }
1208 static void dmaengine_unmap(struct kref *kref)
1210         struct dmaengine_unmap_data *unmap = container_of(kref, typeof(*unmap), kref);
1211         struct device *dev = unmap->dev;
1212         int cnt, i;
1214         cnt = unmap->to_cnt;
1215         for (i = 0; i < cnt; i++)
1216                 dma_unmap_page(dev, unmap->addr[i], unmap->len,
1217                                DMA_TO_DEVICE);
1218         cnt += unmap->from_cnt;
1219         for (; i < cnt; i++)
1220                 dma_unmap_page(dev, unmap->addr[i], unmap->len,
1221                                DMA_FROM_DEVICE);
1222         cnt += unmap->bidi_cnt;
1223         for (; i < cnt; i++) {
1224                 if (unmap->addr[i] == 0)
1225                         continue;
1226                 dma_unmap_page(dev, unmap->addr[i], unmap->len,
1227                                DMA_BIDIRECTIONAL);
1228         }
1229         cnt = unmap->map_cnt;
1230         mempool_free(unmap, __get_unmap_pool(cnt)->pool);
1233 void dmaengine_unmap_put(struct dmaengine_unmap_data *unmap)
1235         if (unmap)
1236                 kref_put(&unmap->kref, dmaengine_unmap);
1238 EXPORT_SYMBOL_GPL(dmaengine_unmap_put);
1240 static void dmaengine_destroy_unmap_pool(void)
1242         int i;
1244         for (i = 0; i < ARRAY_SIZE(unmap_pool); i++) {
1245                 struct dmaengine_unmap_pool *p = &unmap_pool[i];
1247                 mempool_destroy(p->pool);
1248                 p->pool = NULL;
1249                 kmem_cache_destroy(p->cache);
1250                 p->cache = NULL;
1251         }
1254 static int __init dmaengine_init_unmap_pool(void)
1256         int i;
1258         for (i = 0; i < ARRAY_SIZE(unmap_pool); i++) {
1259                 struct dmaengine_unmap_pool *p = &unmap_pool[i];
1260                 size_t size;
1262                 size = sizeof(struct dmaengine_unmap_data) +
1263                        sizeof(dma_addr_t) * p->size;
1265                 p->cache = kmem_cache_create(p->name, size, 0,
1266                                              SLAB_HWCACHE_ALIGN, NULL);
1267                 if (!p->cache)
1268                         break;
1269                 p->pool = mempool_create_slab_pool(1, p->cache);
1270                 if (!p->pool)
1271                         break;
1272         }
1274         if (i == ARRAY_SIZE(unmap_pool))
1275                 return 0;
1277         dmaengine_destroy_unmap_pool();
1278         return -ENOMEM;
1281 struct dmaengine_unmap_data *
1282 dmaengine_get_unmap_data(struct device *dev, int nr, gfp_t flags)
1284         struct dmaengine_unmap_data *unmap;
1286         unmap = mempool_alloc(__get_unmap_pool(nr)->pool, flags);
1287         if (!unmap)
1288                 return NULL;
1290         memset(unmap, 0, sizeof(*unmap));
1291         kref_init(&unmap->kref);
1292         unmap->dev = dev;
1293         unmap->map_cnt = nr;
1295         return unmap;
1297 EXPORT_SYMBOL(dmaengine_get_unmap_data);
1299 void dma_async_tx_descriptor_init(struct dma_async_tx_descriptor *tx,
1300         struct dma_chan *chan)
1302         tx->chan = chan;
1303         #ifdef CONFIG_ASYNC_TX_ENABLE_CHANNEL_SWITCH
1304         spin_lock_init(&tx->lock);
1305         #endif
1307 EXPORT_SYMBOL(dma_async_tx_descriptor_init);
1309 /* dma_wait_for_async_tx - spin wait for a transaction to complete
1310  * @tx: in-flight transaction to wait on
1311  */
1312 enum dma_status
1313 dma_wait_for_async_tx(struct dma_async_tx_descriptor *tx)
1315         unsigned long dma_sync_wait_timeout = jiffies + msecs_to_jiffies(5000);
1317         if (!tx)
1318                 return DMA_COMPLETE;
1320         while (tx->cookie == -EBUSY) {
1321                 if (time_after_eq(jiffies, dma_sync_wait_timeout)) {
1322                         dev_err(tx->chan->device->dev,
1323                                 "%s timeout waiting for descriptor submission\n",
1324                                 __func__);
1325                         return DMA_ERROR;
1326                 }
1327                 cpu_relax();
1328         }
1329         return dma_sync_wait(tx->chan, tx->cookie);
1331 EXPORT_SYMBOL_GPL(dma_wait_for_async_tx);
1333 /* dma_run_dependencies - helper routine for dma drivers to process
1334  *      (start) dependent operations on their target channel
1335  * @tx: transaction with dependencies
1336  */
1337 void dma_run_dependencies(struct dma_async_tx_descriptor *tx)
1339         struct dma_async_tx_descriptor *dep = txd_next(tx);
1340         struct dma_async_tx_descriptor *dep_next;
1341         struct dma_chan *chan;
1343         if (!dep)
1344                 return;
1346         /* we'll submit tx->next now, so clear the link */
1347         txd_clear_next(tx);
1348         chan = dep->chan;
1350         /* keep submitting up until a channel switch is detected
1351          * in that case we will be called again as a result of
1352          * processing the interrupt from async_tx_channel_switch
1353          */
1354         for (; dep; dep = dep_next) {
1355                 txd_lock(dep);
1356                 txd_clear_parent(dep);
1357                 dep_next = txd_next(dep);
1358                 if (dep_next && dep_next->chan == chan)
1359                         txd_clear_next(dep); /* ->next will be submitted */
1360                 else
1361                         dep_next = NULL; /* submit current dep and terminate */
1362                 txd_unlock(dep);
1364                 dep->tx_submit(dep);
1365         }
1367         chan->device->device_issue_pending(chan);
1369 EXPORT_SYMBOL_GPL(dma_run_dependencies);
1371 static int __init dma_bus_init(void)
1373         int err = dmaengine_init_unmap_pool();
1375         if (err)
1376                 return err;
1377         return class_register(&dma_devclass);
1379 arch_initcall(dma_bus_init);