d33a953c9b55fcfe6ba9c4a0471fdabbc70051b2
1 /*
2 * Copyright(c) 2004 - 2006 Intel Corporation. All rights reserved.
3 *
4 * This program is free software; you can redistribute it and/or modify it
5 * under the terms of the GNU General Public License as published by the Free
6 * Software Foundation; either version 2 of the License, or (at your option)
7 * any later version.
8 *
9 * This program is distributed in the hope that it will be useful, but WITHOUT
10 * ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or
11 * FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public License for
12 * more details.
13 *
14 * The full GNU General Public License is included in this distribution in the
15 * file called COPYING.
16 */
17 #ifndef LINUX_DMAENGINE_H
18 #define LINUX_DMAENGINE_H
20 #include <linux/device.h>
21 #include <linux/err.h>
22 #include <linux/uio.h>
23 #include <linux/bug.h>
24 #include <linux/scatterlist.h>
25 #include <linux/bitmap.h>
26 #include <linux/types.h>
27 #include <asm/page.h>
29 /**
30 * typedef dma_cookie_t - an opaque DMA cookie
31 *
32 * if dma_cookie_t is >0 it's a DMA request cookie, <0 it's an error code
33 */
34 typedef s32 dma_cookie_t;
35 #define DMA_MIN_COOKIE 1
37 static inline int dma_submit_error(dma_cookie_t cookie)
38 {
39 return cookie < 0 ? cookie : 0;
40 }
42 /**
43 * enum dma_status - DMA transaction status
44 * @DMA_COMPLETE: transaction completed
45 * @DMA_IN_PROGRESS: transaction not yet processed
46 * @DMA_PAUSED: transaction is paused
47 * @DMA_ERROR: transaction failed
48 */
49 enum dma_status {
50 DMA_COMPLETE,
51 DMA_IN_PROGRESS,
52 DMA_PAUSED,
53 DMA_ERROR,
54 };
56 /**
57 * enum dma_transaction_type - DMA transaction types/indexes
58 *
59 * Note: The DMA_ASYNC_TX capability is not to be set by drivers. It is
60 * automatically set as dma devices are registered.
61 */
62 enum dma_transaction_type {
63 DMA_MEMCPY,
64 DMA_XOR,
65 DMA_PQ,
66 DMA_XOR_VAL,
67 DMA_PQ_VAL,
68 DMA_MEMSET,
69 DMA_MEMSET_SG,
70 DMA_INTERRUPT,
71 DMA_PRIVATE,
72 DMA_ASYNC_TX,
73 DMA_SLAVE,
74 DMA_CYCLIC,
75 DMA_INTERLEAVE,
76 /* last transaction type for creation of the capabilities mask */
77 DMA_TX_TYPE_END,
78 };
80 /**
81 * enum dma_transfer_direction - dma transfer mode and direction indicator
82 * @DMA_MEM_TO_MEM: Async/Memcpy mode
83 * @DMA_MEM_TO_DEV: Slave mode & From Memory to Device
84 * @DMA_DEV_TO_MEM: Slave mode & From Device to Memory
85 * @DMA_DEV_TO_DEV: Slave mode & From Device to Device
86 */
87 enum dma_transfer_direction {
88 DMA_MEM_TO_MEM,
89 DMA_MEM_TO_DEV,
90 DMA_DEV_TO_MEM,
91 DMA_DEV_TO_DEV,
92 DMA_TRANS_NONE,
93 };
95 /**
96 * Interleaved Transfer Request
97 * ----------------------------
98 * A chunk is collection of contiguous bytes to be transfered.
99 * The gap(in bytes) between two chunks is called inter-chunk-gap(ICG).
100 * ICGs may or maynot change between chunks.
101 * A FRAME is the smallest series of contiguous {chunk,icg} pairs,
102 * that when repeated an integral number of times, specifies the transfer.
103 * A transfer template is specification of a Frame, the number of times
104 * it is to be repeated and other per-transfer attributes.
105 *
106 * Practically, a client driver would have ready a template for each
107 * type of transfer it is going to need during its lifetime and
108 * set only 'src_start' and 'dst_start' before submitting the requests.
109 *
110 *
111 * | Frame-1 | Frame-2 | ~ | Frame-'numf' |
112 * |====....==.===...=...|====....==.===...=...| ~ |====....==.===...=...|
113 *
114 * == Chunk size
115 * ... ICG
116 */
118 /**
119 * struct data_chunk - Element of scatter-gather list that makes a frame.
120 * @size: Number of bytes to read from source.
121 * size_dst := fn(op, size_src), so doesn't mean much for destination.
122 * @icg: Number of bytes to jump after last src/dst address of this
123 * chunk and before first src/dst address for next chunk.
124 * Ignored for dst(assumed 0), if dst_inc is true and dst_sgl is false.
125 * Ignored for src(assumed 0), if src_inc is true and src_sgl is false.
126 * @dst_icg: Number of bytes to jump after last dst address of this
127 * chunk and before the first dst address for next chunk.
128 * Ignored if dst_inc is true and dst_sgl is false.
129 * @src_icg: Number of bytes to jump after last src address of this
130 * chunk and before the first src address for next chunk.
131 * Ignored if src_inc is true and src_sgl is false.
132 */
133 struct data_chunk {
134 size_t size;
135 size_t icg;
136 size_t dst_icg;
137 size_t src_icg;
138 };
140 /**
141 * struct dma_interleaved_template - Template to convey DMAC the transfer pattern
142 * and attributes.
143 * @src_start: Bus address of source for the first chunk.
144 * @dst_start: Bus address of destination for the first chunk.
145 * @dir: Specifies the type of Source and Destination.
146 * @src_inc: If the source address increments after reading from it.
147 * @dst_inc: If the destination address increments after writing to it.
148 * @src_sgl: If the 'icg' of sgl[] applies to Source (scattered read).
149 * Otherwise, source is read contiguously (icg ignored).
150 * Ignored if src_inc is false.
151 * @dst_sgl: If the 'icg' of sgl[] applies to Destination (scattered write).
152 * Otherwise, destination is filled contiguously (icg ignored).
153 * Ignored if dst_inc is false.
154 * @numf: Number of frames in this template.
155 * @frame_size: Number of chunks in a frame i.e, size of sgl[].
156 * @sgl: Array of {chunk,icg} pairs that make up a frame.
157 */
158 struct dma_interleaved_template {
159 dma_addr_t src_start;
160 dma_addr_t dst_start;
161 enum dma_transfer_direction dir;
162 bool src_inc;
163 bool dst_inc;
164 bool src_sgl;
165 bool dst_sgl;
166 size_t numf;
167 size_t frame_size;
168 struct data_chunk sgl[0];
169 };
171 /**
172 * enum dma_ctrl_flags - DMA flags to augment operation preparation,
173 * control completion, and communicate status.
174 * @DMA_PREP_INTERRUPT - trigger an interrupt (callback) upon completion of
175 * this transaction
176 * @DMA_CTRL_ACK - if clear, the descriptor cannot be reused until the client
177 * acknowledges receipt, i.e. has has a chance to establish any dependency
178 * chains
179 * @DMA_PREP_PQ_DISABLE_P - prevent generation of P while generating Q
180 * @DMA_PREP_PQ_DISABLE_Q - prevent generation of Q while generating P
181 * @DMA_PREP_CONTINUE - indicate to a driver that it is reusing buffers as
182 * sources that were the result of a previous operation, in the case of a PQ
183 * operation it continues the calculation with new sources
184 * @DMA_PREP_FENCE - tell the driver that subsequent operations depend
185 * on the result of this operation
186 * @DMA_CTRL_REUSE: client can reuse the descriptor and submit again till
187 * cleared or freed
188 * @DMA_PREP_CMD: tell the driver that the data passed to DMA API is command
189 * data and the descriptor should be in different format from normal
190 * data descriptors.
191 */
192 enum dma_ctrl_flags {
193 DMA_PREP_INTERRUPT = (1 << 0),
194 DMA_CTRL_ACK = (1 << 1),
195 DMA_PREP_PQ_DISABLE_P = (1 << 2),
196 DMA_PREP_PQ_DISABLE_Q = (1 << 3),
197 DMA_PREP_CONTINUE = (1 << 4),
198 DMA_PREP_FENCE = (1 << 5),
199 DMA_CTRL_REUSE = (1 << 6),
200 DMA_PREP_CMD = (1 << 7),
201 };
203 /**
204 * enum sum_check_bits - bit position of pq_check_flags
205 */
206 enum sum_check_bits {
207 SUM_CHECK_P = 0,
208 SUM_CHECK_Q = 1,
209 };
211 /**
212 * enum pq_check_flags - result of async_{xor,pq}_zero_sum operations
213 * @SUM_CHECK_P_RESULT - 1 if xor zero sum error, 0 otherwise
214 * @SUM_CHECK_Q_RESULT - 1 if reed-solomon zero sum error, 0 otherwise
215 */
216 enum sum_check_flags {
217 SUM_CHECK_P_RESULT = (1 << SUM_CHECK_P),
218 SUM_CHECK_Q_RESULT = (1 << SUM_CHECK_Q),
219 };
222 /**
223 * dma_cap_mask_t - capabilities bitmap modeled after cpumask_t.
224 * See linux/cpumask.h
225 */
226 typedef struct { DECLARE_BITMAP(bits, DMA_TX_TYPE_END); } dma_cap_mask_t;
228 /**
229 * struct dma_chan_percpu - the per-CPU part of struct dma_chan
230 * @memcpy_count: transaction counter
231 * @bytes_transferred: byte counter
232 */
234 /**
235 * enum dma_desc_metadata_mode - per descriptor metadata mode types supported
236 * @DESC_METADATA_CLIENT - the metadata buffer is allocated/provided by the
237 * client driver and it is attached (via the dmaengine_desc_attach_metadata()
238 * helper) to the descriptor.
239 *
240 * Client drivers interested to use this mode can follow:
241 * - DMA_MEM_TO_DEV / DEV_MEM_TO_MEM:
242 * 1. prepare the descriptor (dmaengine_prep_*)
243 * construct the metadata in the client's buffer
244 * 2. use dmaengine_desc_attach_metadata() to attach the buffer to the
245 * descriptor
246 * 3. submit the transfer
247 * - DMA_DEV_TO_MEM:
248 * 1. prepare the descriptor (dmaengine_prep_*)
249 * 2. use dmaengine_desc_attach_metadata() to attach the buffer to the
250 * descriptor
251 * 3. submit the transfer
252 * 4. when the transfer is completed, the metadata should be available in the
253 * attached buffer
254 *
255 * @DESC_METADATA_ENGINE - the metadata buffer is allocated/managed by the DMA
256 * driver. The client driver can ask for the pointer, maximum size and the
257 * currently used size of the metadata and can directly update or read it.
258 * dmaengine_desc_get_metadata_ptr() and dmaengine_desc_set_metadata_len() is
259 * provided as helper functions.
260 *
261 * Client drivers interested to use this mode can follow:
262 * - DMA_MEM_TO_DEV / DEV_MEM_TO_MEM:
263 * 1. prepare the descriptor (dmaengine_prep_*)
264 * 2. use dmaengine_desc_get_metadata_ptr() to get the pointer to the engine's
265 * metadata area
266 * 3. update the metadata at the pointer
267 * 4. use dmaengine_desc_set_metadata_len() to tell the DMA engine the amount
268 * of data the client has placed into the metadata buffer
269 * 5. submit the transfer
270 * - DMA_DEV_TO_MEM:
271 * 1. prepare the descriptor (dmaengine_prep_*)
272 * 2. submit the transfer
273 * 3. on transfer completion, use dmaengine_desc_get_metadata_ptr() to get the
274 * pointer to the engine's metadata are
275 * 4. Read out the metadate from the pointer
276 *
277 * Note: the two mode is not compatible and clients must use one mode for a
278 * descriptor.
279 */
280 enum dma_desc_metadata_mode {
281 DESC_METADATA_NONE = 0,
282 DESC_METADATA_CLIENT = BIT(0),
283 DESC_METADATA_ENGINE = BIT(1),
284 };
286 struct dma_chan_percpu {
287 /* stats */
288 unsigned long memcpy_count;
289 unsigned long bytes_transferred;
290 };
292 /**
293 * struct dma_router - DMA router structure
294 * @dev: pointer to the DMA router device
295 * @route_free: function to be called when the route can be disconnected
296 */
297 struct dma_router {
298 struct device *dev;
299 void (*route_free)(struct device *dev, void *route_data);
300 };
302 /**
303 * struct dma_chan - devices supply DMA channels, clients use them
304 * @device: ptr to the dma device who supplies this channel, always !%NULL
305 * @cookie: last cookie value returned to client
306 * @completed_cookie: last completed cookie for this channel
307 * @chan_id: channel ID for sysfs
308 * @dev: class device for sysfs
309 * @device_node: used to add this to the device chan list
310 * @local: per-cpu pointer to a struct dma_chan_percpu
311 * @client_count: how many clients are using this channel
312 * @table_count: number of appearances in the mem-to-mem allocation table
313 * @router: pointer to the DMA router structure
314 * @route_data: channel specific data for the router
315 * @private: private data for certain client-channel associations
316 */
317 struct dma_chan {
318 struct dma_device *device;
319 dma_cookie_t cookie;
320 dma_cookie_t completed_cookie;
322 /* sysfs */
323 int chan_id;
324 struct dma_chan_dev *dev;
326 struct list_head device_node;
327 struct dma_chan_percpu __percpu *local;
328 int client_count;
329 int table_count;
331 /* DMA router */
332 struct dma_router *router;
333 void *route_data;
335 void *private;
336 };
338 /**
339 * struct dma_chan_dev - relate sysfs device node to backing channel device
340 * @chan: driver channel device
341 * @device: sysfs device
342 * @dev_id: parent dma_device dev_id
343 * @idr_ref: reference count to gate release of dma_device dev_id
344 */
345 struct dma_chan_dev {
346 struct dma_chan *chan;
347 struct device device;
348 int dev_id;
349 atomic_t *idr_ref;
350 };
352 /**
353 * enum dma_slave_buswidth - defines bus width of the DMA slave
354 * device, source or target buses
355 */
356 enum dma_slave_buswidth {
357 DMA_SLAVE_BUSWIDTH_UNDEFINED = 0,
358 DMA_SLAVE_BUSWIDTH_1_BYTE = 1,
359 DMA_SLAVE_BUSWIDTH_2_BYTES = 2,
360 DMA_SLAVE_BUSWIDTH_3_BYTES = 3,
361 DMA_SLAVE_BUSWIDTH_4_BYTES = 4,
362 DMA_SLAVE_BUSWIDTH_8_BYTES = 8,
363 DMA_SLAVE_BUSWIDTH_16_BYTES = 16,
364 DMA_SLAVE_BUSWIDTH_32_BYTES = 32,
365 DMA_SLAVE_BUSWIDTH_64_BYTES = 64,
366 };
368 /**
369 * struct dma_slave_config - dma slave channel runtime config
370 * @direction: whether the data shall go in or out on this slave
371 * channel, right now. DMA_MEM_TO_DEV and DMA_DEV_TO_MEM are
372 * legal values. DEPRECATED, drivers should use the direction argument
373 * to the device_prep_slave_sg and device_prep_dma_cyclic functions or
374 * the dir field in the dma_interleaved_template structure.
375 * @src_addr: this is the physical address where DMA slave data
376 * should be read (RX), if the source is memory this argument is
377 * ignored.
378 * @dst_addr: this is the physical address where DMA slave data
379 * should be written (TX), if the source is memory this argument
380 * is ignored.
381 * @src_addr_width: this is the width in bytes of the source (RX)
382 * register where DMA data shall be read. If the source
383 * is memory this may be ignored depending on architecture.
384 * Legal values: 1, 2, 3, 4, 8, 16, 32, 64.
385 * @dst_addr_width: same as src_addr_width but for destination
386 * target (TX) mutatis mutandis.
387 * @src_maxburst: the maximum number of words (note: words, as in
388 * units of the src_addr_width member, not bytes) that can be sent
389 * in one burst to the device. Typically something like half the
390 * FIFO depth on I/O peripherals so you don't overflow it. This
391 * may or may not be applicable on memory sources.
392 * @dst_maxburst: same as src_maxburst but for destination target
393 * mutatis mutandis.
394 * @src_port_window_size: The length of the register area in words the data need
395 * to be accessed on the device side. It is only used for devices which is using
396 * an area instead of a single register to receive the data. Typically the DMA
397 * loops in this area in order to transfer the data.
398 * @dst_port_window_size: same as src_port_window_size but for the destination
399 * port.
400 * @device_fc: Flow Controller Settings. Only valid for slave channels. Fill
401 * with 'true' if peripheral should be flow controller. Direction will be
402 * selected at Runtime.
403 * @slave_id: Slave requester id. Only valid for slave channels. The dma
404 * slave peripheral will have unique id as dma requester which need to be
405 * pass as slave config.
406 *
407 * This struct is passed in as configuration data to a DMA engine
408 * in order to set up a certain channel for DMA transport at runtime.
409 * The DMA device/engine has to provide support for an additional
410 * callback in the dma_device structure, device_config and this struct
411 * will then be passed in as an argument to the function.
412 *
413 * The rationale for adding configuration information to this struct is as
414 * follows: if it is likely that more than one DMA slave controllers in
415 * the world will support the configuration option, then make it generic.
416 * If not: if it is fixed so that it be sent in static from the platform
417 * data, then prefer to do that.
418 */
419 struct dma_slave_config {
420 enum dma_transfer_direction direction;
421 phys_addr_t src_addr;
422 phys_addr_t dst_addr;
423 enum dma_slave_buswidth src_addr_width;
424 enum dma_slave_buswidth dst_addr_width;
425 u32 src_maxburst;
426 u32 dst_maxburst;
427 u32 src_port_window_size;
428 u32 dst_port_window_size;
429 bool device_fc;
430 unsigned int slave_id;
431 };
433 /**
434 * enum dma_residue_granularity - Granularity of the reported transfer residue
435 * @DMA_RESIDUE_GRANULARITY_DESCRIPTOR: Residue reporting is not support. The
436 * DMA channel is only able to tell whether a descriptor has been completed or
437 * not, which means residue reporting is not supported by this channel. The
438 * residue field of the dma_tx_state field will always be 0.
439 * @DMA_RESIDUE_GRANULARITY_SEGMENT: Residue is updated after each successfully
440 * completed segment of the transfer (For cyclic transfers this is after each
441 * period). This is typically implemented by having the hardware generate an
442 * interrupt after each transferred segment and then the drivers updates the
443 * outstanding residue by the size of the segment. Another possibility is if
444 * the hardware supports scatter-gather and the segment descriptor has a field
445 * which gets set after the segment has been completed. The driver then counts
446 * the number of segments without the flag set to compute the residue.
447 * @DMA_RESIDUE_GRANULARITY_BURST: Residue is updated after each transferred
448 * burst. This is typically only supported if the hardware has a progress
449 * register of some sort (E.g. a register with the current read/write address
450 * or a register with the amount of bursts/beats/bytes that have been
451 * transferred or still need to be transferred).
452 */
453 enum dma_residue_granularity {
454 DMA_RESIDUE_GRANULARITY_DESCRIPTOR = 0,
455 DMA_RESIDUE_GRANULARITY_SEGMENT = 1,
456 DMA_RESIDUE_GRANULARITY_BURST = 2,
457 };
459 /**
460 * struct dma_slave_caps - expose capabilities of a slave channel only
461 * @src_addr_widths: bit mask of src addr widths the channel supports.
462 * Width is specified in bytes, e.g. for a channel supporting
463 * a width of 4 the mask should have BIT(4) set.
464 * @dst_addr_widths: bit mask of dst addr widths the channel supports
465 * @directions: bit mask of slave directions the channel supports.
466 * Since the enum dma_transfer_direction is not defined as bit flag for
467 * each type, the dma controller should set BIT(<TYPE>) and same
468 * should be checked by controller as well
469 * @max_burst: max burst capability per-transfer
470 * @cmd_pause: true, if pause is supported (i.e. for reading residue or
471 * for resume later)
472 * @cmd_resume: true, if resume is supported
473 * @cmd_terminate: true, if terminate cmd is supported
474 * @residue_granularity: granularity of the reported transfer residue
475 * @descriptor_reuse: if a descriptor can be reused by client and
476 * resubmitted multiple times
477 */
478 struct dma_slave_caps {
479 u32 src_addr_widths;
480 u32 dst_addr_widths;
481 u32 directions;
482 u32 max_burst;
483 bool cmd_pause;
484 bool cmd_resume;
485 bool cmd_terminate;
486 enum dma_residue_granularity residue_granularity;
487 bool descriptor_reuse;
488 };
490 static inline const char *dma_chan_name(struct dma_chan *chan)
491 {
492 return dev_name(&chan->dev->device);
493 }
495 void dma_chan_cleanup(struct kref *kref);
497 /**
498 * typedef dma_filter_fn - callback filter for dma_request_channel
499 * @chan: channel to be reviewed
500 * @filter_param: opaque parameter passed through dma_request_channel
501 *
502 * When this optional parameter is specified in a call to dma_request_channel a
503 * suitable channel is passed to this routine for further dispositioning before
504 * being returned. Where 'suitable' indicates a non-busy channel that
505 * satisfies the given capability mask. It returns 'true' to indicate that the
506 * channel is suitable.
507 */
508 typedef bool (*dma_filter_fn)(struct dma_chan *chan, void *filter_param);
510 typedef void (*dma_async_tx_callback)(void *dma_async_param);
512 enum dmaengine_tx_result {
513 DMA_TRANS_NOERROR = 0, /* SUCCESS */
514 DMA_TRANS_READ_FAILED, /* Source DMA read failed */
515 DMA_TRANS_WRITE_FAILED, /* Destination DMA write failed */
516 DMA_TRANS_ABORTED, /* Op never submitted / aborted */
517 };
519 struct dmaengine_result {
520 enum dmaengine_tx_result result;
521 u32 residue;
522 };
524 typedef void (*dma_async_tx_callback_result)(void *dma_async_param,
525 const struct dmaengine_result *result);
527 struct dmaengine_unmap_data {
528 #if IS_ENABLED(CONFIG_DMA_ENGINE_RAID)
529 u16 map_cnt;
530 #else
531 u8 map_cnt;
532 #endif
533 u8 to_cnt;
534 u8 from_cnt;
535 u8 bidi_cnt;
536 struct device *dev;
537 struct kref kref;
538 size_t len;
539 dma_addr_t addr[0];
540 };
542 struct dma_async_tx_descriptor;
544 struct dma_descriptor_metadata_ops {
545 int (*attach)(struct dma_async_tx_descriptor *desc, void *data,
546 size_t len);
548 void *(*get_ptr)(struct dma_async_tx_descriptor *desc,
549 size_t *payload_len, size_t *max_len);
550 int (*set_len)(struct dma_async_tx_descriptor *desc,
551 size_t payload_len);
552 };
554 /**
555 * struct dma_async_tx_descriptor - async transaction descriptor
556 * ---dma generic offload fields---
557 * @cookie: tracking cookie for this transaction, set to -EBUSY if
558 * this tx is sitting on a dependency list
559 * @flags: flags to augment operation preparation, control completion, and
560 * communicate status
561 * @phys: physical address of the descriptor
562 * @chan: target channel for this operation
563 * @tx_submit: accept the descriptor, assign ordered cookie and mark the
564 * descriptor pending. To be pushed on .issue_pending() call
565 * @callback: routine to call after this operation is complete
566 * @callback_param: general parameter to pass to the callback routine
567 * @desc_metadata_mode: core managed metadata mode to protect mixed use of
568 * DESC_METADATA_CLIENT or DESC_METADATA_ENGINE. Otherwise
569 * DESC_METADATA_NONE
570 * @metadata_ops: DMA driver provided metadata mode ops, need to be set by the
571 * DMA driver if metadata mode is supported with the descriptor
572 * ---async_tx api specific fields---
573 * @next: at completion submit this descriptor
574 * @parent: pointer to the next level up in the dependency chain
575 * @lock: protect the parent and next pointers
576 */
577 struct dma_async_tx_descriptor {
578 dma_cookie_t cookie;
579 enum dma_ctrl_flags flags; /* not a 'long' to pack with cookie */
580 dma_addr_t phys;
581 struct dma_chan *chan;
582 dma_cookie_t (*tx_submit)(struct dma_async_tx_descriptor *tx);
583 int (*desc_free)(struct dma_async_tx_descriptor *tx);
584 dma_async_tx_callback callback;
585 dma_async_tx_callback_result callback_result;
586 void *callback_param;
587 struct dmaengine_unmap_data *unmap;
588 enum dma_desc_metadata_mode desc_metadata_mode;
589 struct dma_descriptor_metadata_ops *metadata_ops;
590 #ifdef CONFIG_ASYNC_TX_ENABLE_CHANNEL_SWITCH
591 struct dma_async_tx_descriptor *next;
592 struct dma_async_tx_descriptor *parent;
593 spinlock_t lock;
594 #endif
595 };
597 #ifdef CONFIG_DMA_ENGINE
598 static inline void dma_set_unmap(struct dma_async_tx_descriptor *tx,
599 struct dmaengine_unmap_data *unmap)
600 {
601 kref_get(&unmap->kref);
602 tx->unmap = unmap;
603 }
605 struct dmaengine_unmap_data *
606 dmaengine_get_unmap_data(struct device *dev, int nr, gfp_t flags);
607 void dmaengine_unmap_put(struct dmaengine_unmap_data *unmap);
608 #else
609 static inline void dma_set_unmap(struct dma_async_tx_descriptor *tx,
610 struct dmaengine_unmap_data *unmap)
611 {
612 }
613 static inline struct dmaengine_unmap_data *
614 dmaengine_get_unmap_data(struct device *dev, int nr, gfp_t flags)
615 {
616 return NULL;
617 }
618 static inline void dmaengine_unmap_put(struct dmaengine_unmap_data *unmap)
619 {
620 }
621 #endif
623 static inline void dma_descriptor_unmap(struct dma_async_tx_descriptor *tx)
624 {
625 if (tx->unmap) {
626 dmaengine_unmap_put(tx->unmap);
627 tx->unmap = NULL;
628 }
629 }
631 #ifndef CONFIG_ASYNC_TX_ENABLE_CHANNEL_SWITCH
632 static inline void txd_lock(struct dma_async_tx_descriptor *txd)
633 {
634 }
635 static inline void txd_unlock(struct dma_async_tx_descriptor *txd)
636 {
637 }
638 static inline void txd_chain(struct dma_async_tx_descriptor *txd, struct dma_async_tx_descriptor *next)
639 {
640 BUG();
641 }
642 static inline void txd_clear_parent(struct dma_async_tx_descriptor *txd)
643 {
644 }
645 static inline void txd_clear_next(struct dma_async_tx_descriptor *txd)
646 {
647 }
648 static inline struct dma_async_tx_descriptor *txd_next(struct dma_async_tx_descriptor *txd)
649 {
650 return NULL;
651 }
652 static inline struct dma_async_tx_descriptor *txd_parent(struct dma_async_tx_descriptor *txd)
653 {
654 return NULL;
655 }
657 #else
658 static inline void txd_lock(struct dma_async_tx_descriptor *txd)
659 {
660 spin_lock_bh(&txd->lock);
661 }
662 static inline void txd_unlock(struct dma_async_tx_descriptor *txd)
663 {
664 spin_unlock_bh(&txd->lock);
665 }
666 static inline void txd_chain(struct dma_async_tx_descriptor *txd, struct dma_async_tx_descriptor *next)
667 {
668 txd->next = next;
669 next->parent = txd;
670 }
671 static inline void txd_clear_parent(struct dma_async_tx_descriptor *txd)
672 {
673 txd->parent = NULL;
674 }
675 static inline void txd_clear_next(struct dma_async_tx_descriptor *txd)
676 {
677 txd->next = NULL;
678 }
679 static inline struct dma_async_tx_descriptor *txd_parent(struct dma_async_tx_descriptor *txd)
680 {
681 return txd->parent;
682 }
683 static inline struct dma_async_tx_descriptor *txd_next(struct dma_async_tx_descriptor *txd)
684 {
685 return txd->next;
686 }
687 #endif
689 /**
690 * struct dma_tx_state - filled in to report the status of
691 * a transfer.
692 * @last: last completed DMA cookie
693 * @used: last issued DMA cookie (i.e. the one in progress)
694 * @residue: the remaining number of bytes left to transmit
695 * on the selected transfer for states DMA_IN_PROGRESS and
696 * DMA_PAUSED if this is implemented in the driver, else 0
697 */
698 struct dma_tx_state {
699 dma_cookie_t last;
700 dma_cookie_t used;
701 u32 residue;
702 };
704 /**
705 * enum dmaengine_alignment - defines alignment of the DMA async tx
706 * buffers
707 */
708 enum dmaengine_alignment {
709 DMAENGINE_ALIGN_1_BYTE = 0,
710 DMAENGINE_ALIGN_2_BYTES = 1,
711 DMAENGINE_ALIGN_4_BYTES = 2,
712 DMAENGINE_ALIGN_8_BYTES = 3,
713 DMAENGINE_ALIGN_16_BYTES = 4,
714 DMAENGINE_ALIGN_32_BYTES = 5,
715 DMAENGINE_ALIGN_64_BYTES = 6,
716 };
718 /**
719 * struct dma_slave_map - associates slave device and it's slave channel with
720 * parameter to be used by a filter function
721 * @devname: name of the device
722 * @slave: slave channel name
723 * @param: opaque parameter to pass to struct dma_filter.fn
724 */
725 struct dma_slave_map {
726 const char *devname;
727 const char *slave;
728 void *param;
729 };
731 /**
732 * struct dma_filter - information for slave device/channel to filter_fn/param
733 * mapping
734 * @fn: filter function callback
735 * @mapcnt: number of slave device/channel in the map
736 * @map: array of channel to filter mapping data
737 */
738 struct dma_filter {
739 dma_filter_fn fn;
740 int mapcnt;
741 const struct dma_slave_map *map;
742 };
744 /**
745 * struct dma_device - info on the entity supplying DMA services
746 * @chancnt: how many DMA channels are supported
747 * @privatecnt: how many DMA channels are requested by dma_request_channel
748 * @channels: the list of struct dma_chan
749 * @global_node: list_head for global dma_device_list
750 * @filter: information for device/slave to filter function/param mapping
751 * @cap_mask: one or more dma_capability flags
752 * @desc_metadata_modes: supported metadata modes by the DMA device
753 * @max_xor: maximum number of xor sources, 0 if no capability
754 * @max_pq: maximum number of PQ sources and PQ-continue capability
755 * @copy_align: alignment shift for memcpy operations
756 * @xor_align: alignment shift for xor operations
757 * @pq_align: alignment shift for pq operations
758 * @fill_align: alignment shift for memset operations
759 * @dev_id: unique device ID
760 * @dev: struct device reference for dma mapping api
761 * @src_addr_widths: bit mask of src addr widths the device supports
762 * Width is specified in bytes, e.g. for a device supporting
763 * a width of 4 the mask should have BIT(4) set.
764 * @dst_addr_widths: bit mask of dst addr widths the device supports
765 * @directions: bit mask of slave directions the device supports.
766 * Since the enum dma_transfer_direction is not defined as bit flag for
767 * each type, the dma controller should set BIT(<TYPE>) and same
768 * should be checked by controller as well
769 * @max_burst: max burst capability per-transfer
770 * @residue_granularity: granularity of the transfer residue reported
771 * by tx_status
772 * @device_alloc_chan_resources: allocate resources and return the
773 * number of allocated descriptors
774 * @device_free_chan_resources: release DMA channel's resources
775 * @device_prep_dma_memcpy: prepares a memcpy operation
776 * @device_prep_dma_xor: prepares a xor operation
777 * @device_prep_dma_xor_val: prepares a xor validation operation
778 * @device_prep_dma_pq: prepares a pq operation
779 * @device_prep_dma_pq_val: prepares a pqzero_sum operation
780 * @device_prep_dma_memset: prepares a memset operation
781 * @device_prep_dma_memset_sg: prepares a memset operation over a scatter list
782 * @device_prep_dma_interrupt: prepares an end of chain interrupt operation
783 * @device_prep_slave_sg: prepares a slave dma operation
784 * @device_prep_dma_cyclic: prepare a cyclic dma operation suitable for audio.
785 * The function takes a buffer of size buf_len. The callback function will
786 * be called after period_len bytes have been transferred.
787 * @device_prep_interleaved_dma: Transfer expression in a generic way.
788 * @device_prep_dma_imm_data: DMA's 8 byte immediate data to the dst address
789 * @device_config: Pushes a new configuration to a channel, return 0 or an error
790 * code
791 * @device_pause: Pauses any transfer happening on a channel. Returns
792 * 0 or an error code
793 * @device_resume: Resumes any transfer on a channel previously
794 * paused. Returns 0 or an error code
795 * @device_terminate_all: Aborts all transfers on a channel. Returns 0
796 * or an error code
797 * @device_synchronize: Synchronizes the termination of a transfers to the
798 * current context.
799 * @device_tx_status: poll for transaction completion, the optional
800 * txstate parameter can be supplied with a pointer to get a
801 * struct with auxiliary transfer status information, otherwise the call
802 * will just return a simple status code
803 * @device_issue_pending: push pending transactions to hardware
804 * @descriptor_reuse: a submitted transfer can be resubmitted after completion
805 */
806 struct dma_device {
808 unsigned int chancnt;
809 unsigned int privatecnt;
810 struct list_head channels;
811 struct list_head global_node;
812 struct dma_filter filter;
813 dma_cap_mask_t cap_mask;
814 enum dma_desc_metadata_mode desc_metadata_modes;
815 unsigned short max_xor;
816 unsigned short max_pq;
817 enum dmaengine_alignment copy_align;
818 enum dmaengine_alignment xor_align;
819 enum dmaengine_alignment pq_align;
820 enum dmaengine_alignment fill_align;
821 #define DMA_HAS_PQ_CONTINUE (1 << 15)
823 int dev_id;
824 struct device *dev;
826 u32 src_addr_widths;
827 u32 dst_addr_widths;
828 u32 directions;
829 u32 max_burst;
830 bool descriptor_reuse;
831 enum dma_residue_granularity residue_granularity;
833 int (*device_alloc_chan_resources)(struct dma_chan *chan);
834 void (*device_free_chan_resources)(struct dma_chan *chan);
836 struct dma_async_tx_descriptor *(*device_prep_dma_memcpy)(
837 struct dma_chan *chan, dma_addr_t dst, dma_addr_t src,
838 size_t len, unsigned long flags);
839 struct dma_async_tx_descriptor *(*device_prep_dma_xor)(
840 struct dma_chan *chan, dma_addr_t dst, dma_addr_t *src,
841 unsigned int src_cnt, size_t len, unsigned long flags);
842 struct dma_async_tx_descriptor *(*device_prep_dma_xor_val)(
843 struct dma_chan *chan, dma_addr_t *src, unsigned int src_cnt,
844 size_t len, enum sum_check_flags *result, unsigned long flags);
845 struct dma_async_tx_descriptor *(*device_prep_dma_pq)(
846 struct dma_chan *chan, dma_addr_t *dst, dma_addr_t *src,
847 unsigned int src_cnt, const unsigned char *scf,
848 size_t len, unsigned long flags);
849 struct dma_async_tx_descriptor *(*device_prep_dma_pq_val)(
850 struct dma_chan *chan, dma_addr_t *pq, dma_addr_t *src,
851 unsigned int src_cnt, const unsigned char *scf, size_t len,
852 enum sum_check_flags *pqres, unsigned long flags);
853 struct dma_async_tx_descriptor *(*device_prep_dma_memset)(
854 struct dma_chan *chan, dma_addr_t dest, int value, size_t len,
855 unsigned long flags);
856 struct dma_async_tx_descriptor *(*device_prep_dma_memset_sg)(
857 struct dma_chan *chan, struct scatterlist *sg,
858 unsigned int nents, int value, unsigned long flags);
859 struct dma_async_tx_descriptor *(*device_prep_dma_interrupt)(
860 struct dma_chan *chan, unsigned long flags);
862 struct dma_async_tx_descriptor *(*device_prep_slave_sg)(
863 struct dma_chan *chan, struct scatterlist *sgl,
864 unsigned int sg_len, enum dma_transfer_direction direction,
865 unsigned long flags, void *context);
866 struct dma_async_tx_descriptor *(*device_prep_dma_cyclic)(
867 struct dma_chan *chan, dma_addr_t buf_addr, size_t buf_len,
868 size_t period_len, enum dma_transfer_direction direction,
869 unsigned long flags);
870 struct dma_async_tx_descriptor *(*device_prep_interleaved_dma)(
871 struct dma_chan *chan, struct dma_interleaved_template *xt,
872 unsigned long flags);
873 struct dma_async_tx_descriptor *(*device_prep_dma_imm_data)(
874 struct dma_chan *chan, dma_addr_t dst, u64 data,
875 unsigned long flags);
877 int (*device_config)(struct dma_chan *chan,
878 struct dma_slave_config *config);
879 int (*device_pause)(struct dma_chan *chan);
880 int (*device_resume)(struct dma_chan *chan);
881 int (*device_terminate_all)(struct dma_chan *chan);
882 void (*device_synchronize)(struct dma_chan *chan);
884 enum dma_status (*device_tx_status)(struct dma_chan *chan,
885 dma_cookie_t cookie,
886 struct dma_tx_state *txstate);
887 void (*device_issue_pending)(struct dma_chan *chan);
888 };
890 static inline int dmaengine_slave_config(struct dma_chan *chan,
891 struct dma_slave_config *config)
892 {
893 if (chan->device->device_config)
894 return chan->device->device_config(chan, config);
896 return -ENOSYS;
897 }
899 static inline bool is_slave_direction(enum dma_transfer_direction direction)
900 {
901 return (direction == DMA_MEM_TO_DEV) || (direction == DMA_DEV_TO_MEM);
902 }
904 static inline struct dma_async_tx_descriptor *dmaengine_prep_slave_single(
905 struct dma_chan *chan, dma_addr_t buf, size_t len,
906 enum dma_transfer_direction dir, unsigned long flags)
907 {
908 struct scatterlist sg;
909 sg_init_table(&sg, 1);
910 sg_dma_address(&sg) = buf;
911 sg_dma_len(&sg) = len;
913 if (!chan || !chan->device || !chan->device->device_prep_slave_sg)
914 return NULL;
916 return chan->device->device_prep_slave_sg(chan, &sg, 1,
917 dir, flags, NULL);
918 }
920 static inline struct dma_async_tx_descriptor *dmaengine_prep_slave_sg(
921 struct dma_chan *chan, struct scatterlist *sgl, unsigned int sg_len,
922 enum dma_transfer_direction dir, unsigned long flags)
923 {
924 if (!chan || !chan->device || !chan->device->device_prep_slave_sg)
925 return NULL;
927 return chan->device->device_prep_slave_sg(chan, sgl, sg_len,
928 dir, flags, NULL);
929 }
931 #ifdef CONFIG_RAPIDIO_DMA_ENGINE
932 struct rio_dma_ext;
933 static inline struct dma_async_tx_descriptor *dmaengine_prep_rio_sg(
934 struct dma_chan *chan, struct scatterlist *sgl, unsigned int sg_len,
935 enum dma_transfer_direction dir, unsigned long flags,
936 struct rio_dma_ext *rio_ext)
937 {
938 if (!chan || !chan->device || !chan->device->device_prep_slave_sg)
939 return NULL;
941 return chan->device->device_prep_slave_sg(chan, sgl, sg_len,
942 dir, flags, rio_ext);
943 }
944 #endif
946 static inline struct dma_async_tx_descriptor *dmaengine_prep_dma_cyclic(
947 struct dma_chan *chan, dma_addr_t buf_addr, size_t buf_len,
948 size_t period_len, enum dma_transfer_direction dir,
949 unsigned long flags)
950 {
951 if (!chan || !chan->device || !chan->device->device_prep_dma_cyclic)
952 return NULL;
954 return chan->device->device_prep_dma_cyclic(chan, buf_addr, buf_len,
955 period_len, dir, flags);
956 }
958 static inline struct dma_async_tx_descriptor *dmaengine_prep_interleaved_dma(
959 struct dma_chan *chan, struct dma_interleaved_template *xt,
960 unsigned long flags)
961 {
962 if (!chan || !chan->device || !chan->device->device_prep_interleaved_dma)
963 return NULL;
965 return chan->device->device_prep_interleaved_dma(chan, xt, flags);
966 }
968 static inline struct dma_async_tx_descriptor *dmaengine_prep_dma_memset(
969 struct dma_chan *chan, dma_addr_t dest, int value, size_t len,
970 unsigned long flags)
971 {
972 if (!chan || !chan->device || !chan->device->device_prep_dma_memset)
973 return NULL;
975 return chan->device->device_prep_dma_memset(chan, dest, value,
976 len, flags);
977 }
979 static inline struct dma_async_tx_descriptor *dmaengine_prep_dma_memcpy(
980 struct dma_chan *chan, dma_addr_t dest, dma_addr_t src,
981 size_t len, unsigned long flags)
982 {
983 if (!chan || !chan->device || !chan->device->device_prep_dma_memcpy)
984 return NULL;
986 return chan->device->device_prep_dma_memcpy(chan, dest, src,
987 len, flags);
988 }
990 static inline bool dmaengine_is_metadata_mode_supported(struct dma_chan *chan,
991 enum dma_desc_metadata_mode mode)
992 {
993 if (!chan)
994 return false;
996 return !!(chan->device->desc_metadata_modes & mode);
997 }
999 #ifdef CONFIG_DMA_ENGINE
1000 int dmaengine_desc_attach_metadata(struct dma_async_tx_descriptor *desc,
1001 void *data, size_t len);
1002 void *dmaengine_desc_get_metadata_ptr(struct dma_async_tx_descriptor *desc,
1003 size_t *payload_len, size_t *max_len);
1004 int dmaengine_desc_set_metadata_len(struct dma_async_tx_descriptor *desc,
1005 size_t payload_len);
1006 #else /* CONFIG_DMA_ENGINE */
1007 static inline int dmaengine_desc_attach_metadata(
1008 struct dma_async_tx_descriptor *desc, void *data, size_t len)
1009 {
1010 return -EINVAL;
1011 }
1012 static inline void *dmaengine_desc_get_metadata_ptr(
1013 struct dma_async_tx_descriptor *desc, size_t *payload_len,
1014 size_t *max_len)
1015 {
1016 return NULL;
1017 }
1018 static inline int dmaengine_desc_set_metadata_len(
1019 struct dma_async_tx_descriptor *desc, size_t payload_len)
1020 {
1021 return -EINVAL;
1022 }
1023 #endif /* CONFIG_DMA_ENGINE */
1025 /**
1026 * dmaengine_terminate_all() - Terminate all active DMA transfers
1027 * @chan: The channel for which to terminate the transfers
1028 *
1029 * This function is DEPRECATED use either dmaengine_terminate_sync() or
1030 * dmaengine_terminate_async() instead.
1031 */
1032 static inline int dmaengine_terminate_all(struct dma_chan *chan)
1033 {
1034 if (chan->device->device_terminate_all)
1035 return chan->device->device_terminate_all(chan);
1037 return -ENOSYS;
1038 }
1040 /**
1041 * dmaengine_terminate_async() - Terminate all active DMA transfers
1042 * @chan: The channel for which to terminate the transfers
1043 *
1044 * Calling this function will terminate all active and pending descriptors
1045 * that have previously been submitted to the channel. It is not guaranteed
1046 * though that the transfer for the active descriptor has stopped when the
1047 * function returns. Furthermore it is possible the complete callback of a
1048 * submitted transfer is still running when this function returns.
1049 *
1050 * dmaengine_synchronize() needs to be called before it is safe to free
1051 * any memory that is accessed by previously submitted descriptors or before
1052 * freeing any resources accessed from within the completion callback of any
1053 * perviously submitted descriptors.
1054 *
1055 * This function can be called from atomic context as well as from within a
1056 * complete callback of a descriptor submitted on the same channel.
1057 *
1058 * If none of the two conditions above apply consider using
1059 * dmaengine_terminate_sync() instead.
1060 */
1061 static inline int dmaengine_terminate_async(struct dma_chan *chan)
1062 {
1063 if (chan->device->device_terminate_all)
1064 return chan->device->device_terminate_all(chan);
1066 return -EINVAL;
1067 }
1069 /**
1070 * dmaengine_synchronize() - Synchronize DMA channel termination
1071 * @chan: The channel to synchronize
1072 *
1073 * Synchronizes to the DMA channel termination to the current context. When this
1074 * function returns it is guaranteed that all transfers for previously issued
1075 * descriptors have stopped and and it is safe to free the memory assoicated
1076 * with them. Furthermore it is guaranteed that all complete callback functions
1077 * for a previously submitted descriptor have finished running and it is safe to
1078 * free resources accessed from within the complete callbacks.
1079 *
1080 * The behavior of this function is undefined if dma_async_issue_pending() has
1081 * been called between dmaengine_terminate_async() and this function.
1082 *
1083 * This function must only be called from non-atomic context and must not be
1084 * called from within a complete callback of a descriptor submitted on the same
1085 * channel.
1086 */
1087 static inline void dmaengine_synchronize(struct dma_chan *chan)
1088 {
1089 might_sleep();
1091 if (chan->device->device_synchronize)
1092 chan->device->device_synchronize(chan);
1093 }
1095 /**
1096 * dmaengine_terminate_sync() - Terminate all active DMA transfers
1097 * @chan: The channel for which to terminate the transfers
1098 *
1099 * Calling this function will terminate all active and pending transfers
1100 * that have previously been submitted to the channel. It is similar to
1101 * dmaengine_terminate_async() but guarantees that the DMA transfer has actually
1102 * stopped and that all complete callbacks have finished running when the
1103 * function returns.
1104 *
1105 * This function must only be called from non-atomic context and must not be
1106 * called from within a complete callback of a descriptor submitted on the same
1107 * channel.
1108 */
1109 static inline int dmaengine_terminate_sync(struct dma_chan *chan)
1110 {
1111 int ret;
1113 ret = dmaengine_terminate_async(chan);
1114 if (ret)
1115 return ret;
1117 dmaengine_synchronize(chan);
1119 return 0;
1120 }
1122 static inline int dmaengine_pause(struct dma_chan *chan)
1123 {
1124 if (chan->device->device_pause)
1125 return chan->device->device_pause(chan);
1127 return -ENOSYS;
1128 }
1130 static inline int dmaengine_resume(struct dma_chan *chan)
1131 {
1132 if (chan->device->device_resume)
1133 return chan->device->device_resume(chan);
1135 return -ENOSYS;
1136 }
1138 static inline enum dma_status dmaengine_tx_status(struct dma_chan *chan,
1139 dma_cookie_t cookie, struct dma_tx_state *state)
1140 {
1141 return chan->device->device_tx_status(chan, cookie, state);
1142 }
1144 static inline dma_cookie_t dmaengine_submit(struct dma_async_tx_descriptor *desc)
1145 {
1146 return desc->tx_submit(desc);
1147 }
1149 static inline bool dmaengine_check_align(enum dmaengine_alignment align,
1150 size_t off1, size_t off2, size_t len)
1151 {
1152 size_t mask;
1154 if (!align)
1155 return true;
1156 mask = (1 << align) - 1;
1157 if (mask & (off1 | off2 | len))
1158 return false;
1159 return true;
1160 }
1162 static inline bool is_dma_copy_aligned(struct dma_device *dev, size_t off1,
1163 size_t off2, size_t len)
1164 {
1165 return dmaengine_check_align(dev->copy_align, off1, off2, len);
1166 }
1168 static inline bool is_dma_xor_aligned(struct dma_device *dev, size_t off1,
1169 size_t off2, size_t len)
1170 {
1171 return dmaengine_check_align(dev->xor_align, off1, off2, len);
1172 }
1174 static inline bool is_dma_pq_aligned(struct dma_device *dev, size_t off1,
1175 size_t off2, size_t len)
1176 {
1177 return dmaengine_check_align(dev->pq_align, off1, off2, len);
1178 }
1180 static inline bool is_dma_fill_aligned(struct dma_device *dev, size_t off1,
1181 size_t off2, size_t len)
1182 {
1183 return dmaengine_check_align(dev->fill_align, off1, off2, len);
1184 }
1186 static inline void
1187 dma_set_maxpq(struct dma_device *dma, int maxpq, int has_pq_continue)
1188 {
1189 dma->max_pq = maxpq;
1190 if (has_pq_continue)
1191 dma->max_pq |= DMA_HAS_PQ_CONTINUE;
1192 }
1194 static inline bool dmaf_continue(enum dma_ctrl_flags flags)
1195 {
1196 return (flags & DMA_PREP_CONTINUE) == DMA_PREP_CONTINUE;
1197 }
1199 static inline bool dmaf_p_disabled_continue(enum dma_ctrl_flags flags)
1200 {
1201 enum dma_ctrl_flags mask = DMA_PREP_CONTINUE | DMA_PREP_PQ_DISABLE_P;
1203 return (flags & mask) == mask;
1204 }
1206 static inline bool dma_dev_has_pq_continue(struct dma_device *dma)
1207 {
1208 return (dma->max_pq & DMA_HAS_PQ_CONTINUE) == DMA_HAS_PQ_CONTINUE;
1209 }
1211 static inline unsigned short dma_dev_to_maxpq(struct dma_device *dma)
1212 {
1213 return dma->max_pq & ~DMA_HAS_PQ_CONTINUE;
1214 }
1216 /* dma_maxpq - reduce maxpq in the face of continued operations
1217 * @dma - dma device with PQ capability
1218 * @flags - to check if DMA_PREP_CONTINUE and DMA_PREP_PQ_DISABLE_P are set
1219 *
1220 * When an engine does not support native continuation we need 3 extra
1221 * source slots to reuse P and Q with the following coefficients:
1222 * 1/ {00} * P : remove P from Q', but use it as a source for P'
1223 * 2/ {01} * Q : use Q to continue Q' calculation
1224 * 3/ {00} * Q : subtract Q from P' to cancel (2)
1225 *
1226 * In the case where P is disabled we only need 1 extra source:
1227 * 1/ {01} * Q : use Q to continue Q' calculation
1228 */
1229 static inline int dma_maxpq(struct dma_device *dma, enum dma_ctrl_flags flags)
1230 {
1231 if (dma_dev_has_pq_continue(dma) || !dmaf_continue(flags))
1232 return dma_dev_to_maxpq(dma);
1233 else if (dmaf_p_disabled_continue(flags))
1234 return dma_dev_to_maxpq(dma) - 1;
1235 else if (dmaf_continue(flags))
1236 return dma_dev_to_maxpq(dma) - 3;
1237 BUG();
1238 }
1240 static inline size_t dmaengine_get_icg(bool inc, bool sgl, size_t icg,
1241 size_t dir_icg)
1242 {
1243 if (inc) {
1244 if (dir_icg)
1245 return dir_icg;
1246 else if (sgl)
1247 return icg;
1248 }
1250 return 0;
1251 }
1253 static inline size_t dmaengine_get_dst_icg(struct dma_interleaved_template *xt,
1254 struct data_chunk *chunk)
1255 {
1256 return dmaengine_get_icg(xt->dst_inc, xt->dst_sgl,
1257 chunk->icg, chunk->dst_icg);
1258 }
1260 static inline size_t dmaengine_get_src_icg(struct dma_interleaved_template *xt,
1261 struct data_chunk *chunk)
1262 {
1263 return dmaengine_get_icg(xt->src_inc, xt->src_sgl,
1264 chunk->icg, chunk->src_icg);
1265 }
1267 /* --- public DMA engine API --- */
1269 #ifdef CONFIG_DMA_ENGINE
1270 void dmaengine_get(void);
1271 void dmaengine_put(void);
1272 #else
1273 static inline void dmaengine_get(void)
1274 {
1275 }
1276 static inline void dmaengine_put(void)
1277 {
1278 }
1279 #endif
1281 #ifdef CONFIG_ASYNC_TX_DMA
1282 #define async_dmaengine_get() dmaengine_get()
1283 #define async_dmaengine_put() dmaengine_put()
1284 #ifndef CONFIG_ASYNC_TX_ENABLE_CHANNEL_SWITCH
1285 #define async_dma_find_channel(type) dma_find_channel(DMA_ASYNC_TX)
1286 #else
1287 #define async_dma_find_channel(type) dma_find_channel(type)
1288 #endif /* CONFIG_ASYNC_TX_ENABLE_CHANNEL_SWITCH */
1289 #else
1290 static inline void async_dmaengine_get(void)
1291 {
1292 }
1293 static inline void async_dmaengine_put(void)
1294 {
1295 }
1296 static inline struct dma_chan *
1297 async_dma_find_channel(enum dma_transaction_type type)
1298 {
1299 return NULL;
1300 }
1301 #endif /* CONFIG_ASYNC_TX_DMA */
1302 void dma_async_tx_descriptor_init(struct dma_async_tx_descriptor *tx,
1303 struct dma_chan *chan);
1305 static inline void async_tx_ack(struct dma_async_tx_descriptor *tx)
1306 {
1307 tx->flags |= DMA_CTRL_ACK;
1308 }
1310 static inline void async_tx_clear_ack(struct dma_async_tx_descriptor *tx)
1311 {
1312 tx->flags &= ~DMA_CTRL_ACK;
1313 }
1315 static inline bool async_tx_test_ack(struct dma_async_tx_descriptor *tx)
1316 {
1317 return (tx->flags & DMA_CTRL_ACK) == DMA_CTRL_ACK;
1318 }
1320 #define dma_cap_set(tx, mask) __dma_cap_set((tx), &(mask))
1321 static inline void
1322 __dma_cap_set(enum dma_transaction_type tx_type, dma_cap_mask_t *dstp)
1323 {
1324 set_bit(tx_type, dstp->bits);
1325 }
1327 #define dma_cap_clear(tx, mask) __dma_cap_clear((tx), &(mask))
1328 static inline void
1329 __dma_cap_clear(enum dma_transaction_type tx_type, dma_cap_mask_t *dstp)
1330 {
1331 clear_bit(tx_type, dstp->bits);
1332 }
1334 #define dma_cap_zero(mask) __dma_cap_zero(&(mask))
1335 static inline void __dma_cap_zero(dma_cap_mask_t *dstp)
1336 {
1337 bitmap_zero(dstp->bits, DMA_TX_TYPE_END);
1338 }
1340 #define dma_has_cap(tx, mask) __dma_has_cap((tx), &(mask))
1341 static inline int
1342 __dma_has_cap(enum dma_transaction_type tx_type, dma_cap_mask_t *srcp)
1343 {
1344 return test_bit(tx_type, srcp->bits);
1345 }
1347 #define for_each_dma_cap_mask(cap, mask) \
1348 for_each_set_bit(cap, mask.bits, DMA_TX_TYPE_END)
1350 /**
1351 * dma_async_issue_pending - flush pending transactions to HW
1352 * @chan: target DMA channel
1353 *
1354 * This allows drivers to push copies to HW in batches,
1355 * reducing MMIO writes where possible.
1356 */
1357 static inline void dma_async_issue_pending(struct dma_chan *chan)
1358 {
1359 chan->device->device_issue_pending(chan);
1360 }
1362 /**
1363 * dma_async_is_tx_complete - poll for transaction completion
1364 * @chan: DMA channel
1365 * @cookie: transaction identifier to check status of
1366 * @last: returns last completed cookie, can be NULL
1367 * @used: returns last issued cookie, can be NULL
1368 *
1369 * If @last and @used are passed in, upon return they reflect the driver
1370 * internal state and can be used with dma_async_is_complete() to check
1371 * the status of multiple cookies without re-checking hardware state.
1372 */
1373 static inline enum dma_status dma_async_is_tx_complete(struct dma_chan *chan,
1374 dma_cookie_t cookie, dma_cookie_t *last, dma_cookie_t *used)
1375 {
1376 struct dma_tx_state state;
1377 enum dma_status status;
1379 status = chan->device->device_tx_status(chan, cookie, &state);
1380 if (last)
1381 *last = state.last;
1382 if (used)
1383 *used = state.used;
1384 return status;
1385 }
1387 /**
1388 * dma_async_is_complete - test a cookie against chan state
1389 * @cookie: transaction identifier to test status of
1390 * @last_complete: last know completed transaction
1391 * @last_used: last cookie value handed out
1392 *
1393 * dma_async_is_complete() is used in dma_async_is_tx_complete()
1394 * the test logic is separated for lightweight testing of multiple cookies
1395 */
1396 static inline enum dma_status dma_async_is_complete(dma_cookie_t cookie,
1397 dma_cookie_t last_complete, dma_cookie_t last_used)
1398 {
1399 if (last_complete <= last_used) {
1400 if ((cookie <= last_complete) || (cookie > last_used))
1401 return DMA_COMPLETE;
1402 } else {
1403 if ((cookie <= last_complete) && (cookie > last_used))
1404 return DMA_COMPLETE;
1405 }
1406 return DMA_IN_PROGRESS;
1407 }
1409 static inline void
1410 dma_set_tx_state(struct dma_tx_state *st, dma_cookie_t last, dma_cookie_t used, u32 residue)
1411 {
1412 if (st) {
1413 st->last = last;
1414 st->used = used;
1415 st->residue = residue;
1416 }
1417 }
1419 #ifdef CONFIG_DMA_ENGINE
1420 struct dma_chan *dma_find_channel(enum dma_transaction_type tx_type);
1421 enum dma_status dma_sync_wait(struct dma_chan *chan, dma_cookie_t cookie);
1422 enum dma_status dma_wait_for_async_tx(struct dma_async_tx_descriptor *tx);
1423 void dma_issue_pending_all(void);
1424 struct dma_chan *__dma_request_channel(const dma_cap_mask_t *mask,
1425 dma_filter_fn fn, void *fn_param);
1426 struct dma_chan *dma_request_slave_channel(struct device *dev, const char *name);
1428 struct dma_chan *dma_request_chan(struct device *dev, const char *name);
1429 struct dma_chan *dma_request_chan_by_mask(const dma_cap_mask_t *mask);
1431 void dma_release_channel(struct dma_chan *chan);
1432 int dma_get_slave_caps(struct dma_chan *chan, struct dma_slave_caps *caps);
1433 #else
1434 static inline struct dma_chan *dma_find_channel(enum dma_transaction_type tx_type)
1435 {
1436 return NULL;
1437 }
1438 static inline enum dma_status dma_sync_wait(struct dma_chan *chan, dma_cookie_t cookie)
1439 {
1440 return DMA_COMPLETE;
1441 }
1442 static inline enum dma_status dma_wait_for_async_tx(struct dma_async_tx_descriptor *tx)
1443 {
1444 return DMA_COMPLETE;
1445 }
1446 static inline void dma_issue_pending_all(void)
1447 {
1448 }
1449 static inline struct dma_chan *__dma_request_channel(const dma_cap_mask_t *mask,
1450 dma_filter_fn fn, void *fn_param)
1451 {
1452 return NULL;
1453 }
1454 static inline struct dma_chan *dma_request_slave_channel(struct device *dev,
1455 const char *name)
1456 {
1457 return NULL;
1458 }
1459 static inline struct dma_chan *dma_request_chan(struct device *dev,
1460 const char *name)
1461 {
1462 return ERR_PTR(-ENODEV);
1463 }
1464 static inline struct dma_chan *dma_request_chan_by_mask(
1465 const dma_cap_mask_t *mask)
1466 {
1467 return ERR_PTR(-ENODEV);
1468 }
1469 static inline void dma_release_channel(struct dma_chan *chan)
1470 {
1471 }
1472 static inline int dma_get_slave_caps(struct dma_chan *chan,
1473 struct dma_slave_caps *caps)
1474 {
1475 return -ENXIO;
1476 }
1477 #endif
1479 #define dma_request_slave_channel_reason(dev, name) dma_request_chan(dev, name)
1481 static inline int dmaengine_desc_set_reuse(struct dma_async_tx_descriptor *tx)
1482 {
1483 struct dma_slave_caps caps;
1485 dma_get_slave_caps(tx->chan, &caps);
1487 if (caps.descriptor_reuse) {
1488 tx->flags |= DMA_CTRL_REUSE;
1489 return 0;
1490 } else {
1491 return -EPERM;
1492 }
1493 }
1495 static inline void dmaengine_desc_clear_reuse(struct dma_async_tx_descriptor *tx)
1496 {
1497 tx->flags &= ~DMA_CTRL_REUSE;
1498 }
1500 static inline bool dmaengine_desc_test_reuse(struct dma_async_tx_descriptor *tx)
1501 {
1502 return (tx->flags & DMA_CTRL_REUSE) == DMA_CTRL_REUSE;
1503 }
1505 static inline int dmaengine_desc_free(struct dma_async_tx_descriptor *desc)
1506 {
1507 /* this is supported for reusable desc, so check that */
1508 if (dmaengine_desc_test_reuse(desc))
1509 return desc->desc_free(desc);
1510 else
1511 return -EPERM;
1512 }
1514 /* --- DMA device --- */
1516 int dma_async_device_register(struct dma_device *device);
1517 int dmaenginem_async_device_register(struct dma_device *device);
1518 void dma_async_device_unregister(struct dma_device *device);
1519 void dma_run_dependencies(struct dma_async_tx_descriptor *tx);
1520 struct dma_chan *dma_get_slave_channel(struct dma_chan *chan);
1521 struct dma_chan *dma_get_any_slave_channel(struct dma_device *device);
1522 #define dma_request_channel(mask, x, y) __dma_request_channel(&(mask), x, y)
1523 #define dma_request_slave_channel_compat(mask, x, y, dev, name) \
1524 __dma_request_slave_channel_compat(&(mask), x, y, dev, name)
1526 static inline struct dma_chan
1527 *__dma_request_slave_channel_compat(const dma_cap_mask_t *mask,
1528 dma_filter_fn fn, void *fn_param,
1529 struct device *dev, const char *name)
1530 {
1531 struct dma_chan *chan;
1533 chan = dma_request_slave_channel(dev, name);
1534 if (chan)
1535 return chan;
1537 if (!fn || !fn_param)
1538 return NULL;
1540 return __dma_request_channel(mask, fn, fn_param);
1541 }
1542 #endif /* DMAENGINE_H */