1 /*
2 * linux/kernel/softirq.c
3 *
4 * Copyright (C) 1992 Linus Torvalds
5 *
6 * Distribute under GPLv2.
7 *
8 * Rewritten. Old one was good in 2.2, but in 2.3 it was immoral. --ANK (990903)
9 */
11 #define pr_fmt(fmt) KBUILD_MODNAME ": " fmt
13 #include <linux/export.h>
14 #include <linux/kernel_stat.h>
15 #include <linux/interrupt.h>
16 #include <linux/init.h>
17 #include <linux/mm.h>
18 #include <linux/notifier.h>
19 #include <linux/percpu.h>
20 #include <linux/cpu.h>
21 #include <linux/freezer.h>
22 #include <linux/kthread.h>
23 #include <linux/rcupdate.h>
24 #include <linux/ftrace.h>
25 #include <linux/smp.h>
26 #include <linux/smpboot.h>
27 #include <linux/tick.h>
28 #include <linux/irq.h>
30 #define CREATE_TRACE_POINTS
31 #include <trace/events/irq.h>
33 /*
34 - No shared variables, all the data are CPU local.
35 - If a softirq needs serialization, let it serialize itself
36 by its own spinlocks.
37 - Even if softirq is serialized, only local cpu is marked for
38 execution. Hence, we get something sort of weak cpu binding.
39 Though it is still not clear, will it result in better locality
40 or will not.
42 Examples:
43 - NET RX softirq. It is multithreaded and does not require
44 any global serialization.
45 - NET TX softirq. It kicks software netdevice queues, hence
46 it is logically serialized per device, but this serialization
47 is invisible to common code.
48 - Tasklets: serialized wrt itself.
49 */
51 #ifndef __ARCH_IRQ_STAT
52 DEFINE_PER_CPU_ALIGNED(irq_cpustat_t, irq_stat);
53 EXPORT_PER_CPU_SYMBOL(irq_stat);
54 #endif
56 static struct softirq_action softirq_vec[NR_SOFTIRQS] __cacheline_aligned_in_smp;
58 DEFINE_PER_CPU(struct task_struct *, ksoftirqd);
60 const char * const softirq_to_name[NR_SOFTIRQS] = {
61 "HI", "TIMER", "NET_TX", "NET_RX", "BLOCK", "IRQ_POLL",
62 "TASKLET", "SCHED", "HRTIMER", "RCU"
63 };
65 /*
66 * we cannot loop indefinitely here to avoid userspace starvation,
67 * but we also don't want to introduce a worst case 1/HZ latency
68 * to the pending events, so lets the scheduler to balance
69 * the softirq load for us.
70 */
71 static void wakeup_softirqd(void)
72 {
73 /* Interrupts are disabled: no need to stop preemption */
74 struct task_struct *tsk = __this_cpu_read(ksoftirqd);
76 if (tsk && tsk->state != TASK_RUNNING)
77 wake_up_process(tsk);
78 }
80 /*
81 * If ksoftirqd is scheduled, we do not want to process pending softirqs
82 * right now. Let ksoftirqd handle this at its own rate, to get fairness,
83 * unless we're doing some of the synchronous softirqs.
84 */
85 #define SOFTIRQ_NOW_MASK ((1 << HI_SOFTIRQ) | (1 << TASKLET_SOFTIRQ))
86 static bool ksoftirqd_running(unsigned long pending)
87 {
88 struct task_struct *tsk = __this_cpu_read(ksoftirqd);
90 if (pending & SOFTIRQ_NOW_MASK)
91 return false;
92 return tsk && (tsk->state == TASK_RUNNING);
93 }
95 /*
96 * preempt_count and SOFTIRQ_OFFSET usage:
97 * - preempt_count is changed by SOFTIRQ_OFFSET on entering or leaving
98 * softirq processing.
99 * - preempt_count is changed by SOFTIRQ_DISABLE_OFFSET (= 2 * SOFTIRQ_OFFSET)
100 * on local_bh_disable or local_bh_enable.
101 * This lets us distinguish between whether we are currently processing
102 * softirq and whether we just have bh disabled.
103 */
105 /*
106 * This one is for softirq.c-internal use,
107 * where hardirqs are disabled legitimately:
108 */
109 #ifdef CONFIG_TRACE_IRQFLAGS
110 void __local_bh_disable_ip(unsigned long ip, unsigned int cnt)
111 {
112 unsigned long flags;
114 WARN_ON_ONCE(in_irq());
116 raw_local_irq_save(flags);
117 /*
118 * The preempt tracer hooks into preempt_count_add and will break
119 * lockdep because it calls back into lockdep after SOFTIRQ_OFFSET
120 * is set and before current->softirq_enabled is cleared.
121 * We must manually increment preempt_count here and manually
122 * call the trace_preempt_off later.
123 */
124 __preempt_count_add(cnt);
125 /*
126 * Were softirqs turned off above:
127 */
128 if (softirq_count() == (cnt & SOFTIRQ_MASK))
129 trace_softirqs_off(ip);
130 raw_local_irq_restore(flags);
132 if (preempt_count() == cnt) {
133 #ifdef CONFIG_DEBUG_PREEMPT
134 current->preempt_disable_ip = get_lock_parent_ip();
135 #endif
136 trace_preempt_off(CALLER_ADDR0, get_lock_parent_ip());
137 }
138 }
139 EXPORT_SYMBOL(__local_bh_disable_ip);
140 #endif /* CONFIG_TRACE_IRQFLAGS */
142 static void __local_bh_enable(unsigned int cnt)
143 {
144 lockdep_assert_irqs_disabled();
146 if (preempt_count() == cnt)
147 trace_preempt_on(CALLER_ADDR0, get_lock_parent_ip());
149 if (softirq_count() == (cnt & SOFTIRQ_MASK))
150 trace_softirqs_on(_RET_IP_);
152 __preempt_count_sub(cnt);
153 }
155 /*
156 * Special-case - softirqs can safely be enabled by __do_softirq(),
157 * without processing still-pending softirqs:
158 */
159 void _local_bh_enable(void)
160 {
161 WARN_ON_ONCE(in_irq());
162 __local_bh_enable(SOFTIRQ_DISABLE_OFFSET);
163 }
164 EXPORT_SYMBOL(_local_bh_enable);
166 void __local_bh_enable_ip(unsigned long ip, unsigned int cnt)
167 {
168 WARN_ON_ONCE(in_irq());
169 lockdep_assert_irqs_enabled();
170 #ifdef CONFIG_TRACE_IRQFLAGS
171 local_irq_disable();
172 #endif
173 /*
174 * Are softirqs going to be turned on now:
175 */
176 if (softirq_count() == SOFTIRQ_DISABLE_OFFSET)
177 trace_softirqs_on(ip);
178 /*
179 * Keep preemption disabled until we are done with
180 * softirq processing:
181 */
182 preempt_count_sub(cnt - 1);
184 if (unlikely(!in_interrupt() && local_softirq_pending())) {
185 /*
186 * Run softirq if any pending. And do it in its own stack
187 * as we may be calling this deep in a task call stack already.
188 */
189 do_softirq();
190 }
192 preempt_count_dec();
193 #ifdef CONFIG_TRACE_IRQFLAGS
194 local_irq_enable();
195 #endif
196 preempt_check_resched();
197 }
198 EXPORT_SYMBOL(__local_bh_enable_ip);
200 /*
201 * We restart softirq processing for at most MAX_SOFTIRQ_RESTART times,
202 * but break the loop if need_resched() is set or after 2 ms.
203 * The MAX_SOFTIRQ_TIME provides a nice upper bound in most cases, but in
204 * certain cases, such as stop_machine(), jiffies may cease to
205 * increment and so we need the MAX_SOFTIRQ_RESTART limit as
206 * well to make sure we eventually return from this method.
207 *
208 * These limits have been established via experimentation.
209 * The two things to balance is latency against fairness -
210 * we want to handle softirqs as soon as possible, but they
211 * should not be able to lock up the box.
212 */
213 #define MAX_SOFTIRQ_TIME msecs_to_jiffies(2)
214 #define MAX_SOFTIRQ_RESTART 10
216 #ifdef CONFIG_TRACE_IRQFLAGS
217 /*
218 * When we run softirqs from irq_exit() and thus on the hardirq stack we need
219 * to keep the lockdep irq context tracking as tight as possible in order to
220 * not miss-qualify lock contexts and miss possible deadlocks.
221 */
223 static inline bool lockdep_softirq_start(void)
224 {
225 bool in_hardirq = false;
227 if (trace_hardirq_context(current)) {
228 in_hardirq = true;
229 trace_hardirq_exit();
230 }
232 lockdep_softirq_enter();
234 return in_hardirq;
235 }
237 static inline void lockdep_softirq_end(bool in_hardirq)
238 {
239 lockdep_softirq_exit();
241 if (in_hardirq)
242 trace_hardirq_enter();
243 }
244 #else
245 static inline bool lockdep_softirq_start(void) { return false; }
246 static inline void lockdep_softirq_end(bool in_hardirq) { }
247 #endif
249 asmlinkage __visible void __softirq_entry __do_softirq(void)
250 {
251 unsigned long end = jiffies + MAX_SOFTIRQ_TIME;
252 unsigned long old_flags = current->flags;
253 int max_restart = MAX_SOFTIRQ_RESTART;
254 struct softirq_action *h;
255 bool in_hardirq;
256 __u32 pending;
257 int softirq_bit;
259 /*
260 * Mask out PF_MEMALLOC s current task context is borrowed for the
261 * softirq. A softirq handled such as network RX might set PF_MEMALLOC
262 * again if the socket is related to swap
263 */
264 current->flags &= ~PF_MEMALLOC;
266 pending = local_softirq_pending();
267 account_irq_enter_time(current);
269 __local_bh_disable_ip(_RET_IP_, SOFTIRQ_OFFSET);
270 in_hardirq = lockdep_softirq_start();
272 restart:
273 /* Reset the pending bitmask before enabling irqs */
274 set_softirq_pending(0);
276 local_irq_enable();
278 h = softirq_vec;
280 while ((softirq_bit = ffs(pending))) {
281 unsigned int vec_nr;
282 int prev_count;
284 h += softirq_bit - 1;
286 vec_nr = h - softirq_vec;
287 prev_count = preempt_count();
289 kstat_incr_softirqs_this_cpu(vec_nr);
291 trace_softirq_entry(vec_nr);
292 h->action(h);
293 trace_softirq_exit(vec_nr);
294 if (unlikely(prev_count != preempt_count())) {
295 pr_err("huh, entered softirq %u %s %p with preempt_count %08x, exited with %08x?\n",
296 vec_nr, softirq_to_name[vec_nr], h->action,
297 prev_count, preempt_count());
298 preempt_count_set(prev_count);
299 }
300 h++;
301 pending >>= softirq_bit;
302 }
304 rcu_bh_qs();
305 local_irq_disable();
307 pending = local_softirq_pending();
308 if (pending) {
309 if (time_before(jiffies, end) && !need_resched() &&
310 --max_restart)
311 goto restart;
313 wakeup_softirqd();
314 }
316 lockdep_softirq_end(in_hardirq);
317 account_irq_exit_time(current);
318 __local_bh_enable(SOFTIRQ_OFFSET);
319 WARN_ON_ONCE(in_interrupt());
320 current_restore_flags(old_flags, PF_MEMALLOC);
321 }
323 asmlinkage __visible void do_softirq(void)
324 {
325 __u32 pending;
326 unsigned long flags;
328 if (in_interrupt())
329 return;
331 local_irq_save(flags);
333 pending = local_softirq_pending();
335 if (pending && !ksoftirqd_running(pending))
336 do_softirq_own_stack();
338 local_irq_restore(flags);
339 }
341 /*
342 * Enter an interrupt context.
343 */
344 void irq_enter(void)
345 {
346 rcu_irq_enter();
347 if (is_idle_task(current) && !in_interrupt()) {
348 /*
349 * Prevent raise_softirq from needlessly waking up ksoftirqd
350 * here, as softirq will be serviced on return from interrupt.
351 */
352 local_bh_disable();
353 tick_irq_enter();
354 _local_bh_enable();
355 }
357 __irq_enter();
358 }
360 static inline void invoke_softirq(void)
361 {
362 if (ksoftirqd_running(local_softirq_pending()))
363 return;
365 if (!force_irqthreads) {
366 #ifdef CONFIG_HAVE_IRQ_EXIT_ON_IRQ_STACK
367 /*
368 * We can safely execute softirq on the current stack if
369 * it is the irq stack, because it should be near empty
370 * at this stage.
371 */
372 __do_softirq();
373 #else
374 /*
375 * Otherwise, irq_exit() is called on the task stack that can
376 * be potentially deep already. So call softirq in its own stack
377 * to prevent from any overrun.
378 */
379 do_softirq_own_stack();
380 #endif
381 } else {
382 wakeup_softirqd();
383 }
384 }
386 static inline void tick_irq_exit(void)
387 {
388 #ifdef CONFIG_NO_HZ_COMMON
389 int cpu = smp_processor_id();
391 /* Make sure that timer wheel updates are propagated */
392 if ((idle_cpu(cpu) && !need_resched()) || tick_nohz_full_cpu(cpu)) {
393 if (!in_irq())
394 tick_nohz_irq_exit();
395 }
396 #endif
397 }
399 /*
400 * Exit an interrupt context. Process softirqs if needed and possible:
401 */
402 void irq_exit(void)
403 {
404 #ifndef __ARCH_IRQ_EXIT_IRQS_DISABLED
405 local_irq_disable();
406 #else
407 lockdep_assert_irqs_disabled();
408 #endif
409 account_irq_exit_time(current);
410 preempt_count_sub(HARDIRQ_OFFSET);
411 if (!in_interrupt() && local_softirq_pending())
412 invoke_softirq();
414 tick_irq_exit();
415 rcu_irq_exit();
416 trace_hardirq_exit(); /* must be last! */
417 }
419 /*
420 * This function must run with irqs disabled!
421 */
422 inline void raise_softirq_irqoff(unsigned int nr)
423 {
424 __raise_softirq_irqoff(nr);
426 /*
427 * If we're in an interrupt or softirq, we're done
428 * (this also catches softirq-disabled code). We will
429 * actually run the softirq once we return from
430 * the irq or softirq.
431 *
432 * Otherwise we wake up ksoftirqd to make sure we
433 * schedule the softirq soon.
434 */
435 if (!in_interrupt())
436 wakeup_softirqd();
437 }
439 void raise_softirq(unsigned int nr)
440 {
441 unsigned long flags;
443 local_irq_save(flags);
444 raise_softirq_irqoff(nr);
445 local_irq_restore(flags);
446 }
448 void __raise_softirq_irqoff(unsigned int nr)
449 {
450 trace_softirq_raise(nr);
451 or_softirq_pending(1UL << nr);
452 }
454 void open_softirq(int nr, void (*action)(struct softirq_action *))
455 {
456 softirq_vec[nr].action = action;
457 }
459 /*
460 * Tasklets
461 */
462 struct tasklet_head {
463 struct tasklet_struct *head;
464 struct tasklet_struct **tail;
465 };
467 static DEFINE_PER_CPU(struct tasklet_head, tasklet_vec);
468 static DEFINE_PER_CPU(struct tasklet_head, tasklet_hi_vec);
470 static void __tasklet_schedule_common(struct tasklet_struct *t,
471 struct tasklet_head __percpu *headp,
472 unsigned int softirq_nr)
473 {
474 struct tasklet_head *head;
475 unsigned long flags;
477 local_irq_save(flags);
478 head = this_cpu_ptr(headp);
479 t->next = NULL;
480 *head->tail = t;
481 head->tail = &(t->next);
482 raise_softirq_irqoff(softirq_nr);
483 local_irq_restore(flags);
484 }
486 void __tasklet_schedule(struct tasklet_struct *t)
487 {
488 __tasklet_schedule_common(t, &tasklet_vec,
489 TASKLET_SOFTIRQ);
490 }
491 EXPORT_SYMBOL(__tasklet_schedule);
493 void __tasklet_hi_schedule(struct tasklet_struct *t)
494 {
495 __tasklet_schedule_common(t, &tasklet_hi_vec,
496 HI_SOFTIRQ);
497 }
498 EXPORT_SYMBOL(__tasklet_hi_schedule);
500 static void tasklet_action_common(struct softirq_action *a,
501 struct tasklet_head *tl_head,
502 unsigned int softirq_nr)
503 {
504 struct tasklet_struct *list;
506 local_irq_disable();
507 list = tl_head->head;
508 tl_head->head = NULL;
509 tl_head->tail = &tl_head->head;
510 local_irq_enable();
512 while (list) {
513 struct tasklet_struct *t = list;
515 list = list->next;
517 if (tasklet_trylock(t)) {
518 if (!atomic_read(&t->count)) {
519 if (!test_and_clear_bit(TASKLET_STATE_SCHED,
520 &t->state))
521 BUG();
522 t->func(t->data);
523 tasklet_unlock(t);
524 continue;
525 }
526 tasklet_unlock(t);
527 }
529 local_irq_disable();
530 t->next = NULL;
531 *tl_head->tail = t;
532 tl_head->tail = &t->next;
533 __raise_softirq_irqoff(softirq_nr);
534 local_irq_enable();
535 }
536 }
538 static __latent_entropy void tasklet_action(struct softirq_action *a)
539 {
540 tasklet_action_common(a, this_cpu_ptr(&tasklet_vec), TASKLET_SOFTIRQ);
541 }
543 static __latent_entropy void tasklet_hi_action(struct softirq_action *a)
544 {
545 tasklet_action_common(a, this_cpu_ptr(&tasklet_hi_vec), HI_SOFTIRQ);
546 }
548 void tasklet_init(struct tasklet_struct *t,
549 void (*func)(unsigned long), unsigned long data)
550 {
551 t->next = NULL;
552 t->state = 0;
553 atomic_set(&t->count, 0);
554 t->func = func;
555 t->data = data;
556 }
557 EXPORT_SYMBOL(tasklet_init);
559 void tasklet_kill(struct tasklet_struct *t)
560 {
561 if (in_interrupt())
562 pr_notice("Attempt to kill tasklet from interrupt\n");
564 while (test_and_set_bit(TASKLET_STATE_SCHED, &t->state)) {
565 do {
566 yield();
567 } while (test_bit(TASKLET_STATE_SCHED, &t->state));
568 }
569 tasklet_unlock_wait(t);
570 clear_bit(TASKLET_STATE_SCHED, &t->state);
571 }
572 EXPORT_SYMBOL(tasklet_kill);
574 /*
575 * tasklet_hrtimer
576 */
578 /*
579 * The trampoline is called when the hrtimer expires. It schedules a tasklet
580 * to run __tasklet_hrtimer_trampoline() which in turn will call the intended
581 * hrtimer callback, but from softirq context.
582 */
583 static enum hrtimer_restart __hrtimer_tasklet_trampoline(struct hrtimer *timer)
584 {
585 struct tasklet_hrtimer *ttimer =
586 container_of(timer, struct tasklet_hrtimer, timer);
588 tasklet_hi_schedule(&ttimer->tasklet);
589 return HRTIMER_NORESTART;
590 }
592 /*
593 * Helper function which calls the hrtimer callback from
594 * tasklet/softirq context
595 */
596 static void __tasklet_hrtimer_trampoline(unsigned long data)
597 {
598 struct tasklet_hrtimer *ttimer = (void *)data;
599 enum hrtimer_restart restart;
601 restart = ttimer->function(&ttimer->timer);
602 if (restart != HRTIMER_NORESTART)
603 hrtimer_restart(&ttimer->timer);
604 }
606 /**
607 * tasklet_hrtimer_init - Init a tasklet/hrtimer combo for softirq callbacks
608 * @ttimer: tasklet_hrtimer which is initialized
609 * @function: hrtimer callback function which gets called from softirq context
610 * @which_clock: clock id (CLOCK_MONOTONIC/CLOCK_REALTIME)
611 * @mode: hrtimer mode (HRTIMER_MODE_ABS/HRTIMER_MODE_REL)
612 */
613 void tasklet_hrtimer_init(struct tasklet_hrtimer *ttimer,
614 enum hrtimer_restart (*function)(struct hrtimer *),
615 clockid_t which_clock, enum hrtimer_mode mode)
616 {
617 hrtimer_init(&ttimer->timer, which_clock, mode);
618 ttimer->timer.function = __hrtimer_tasklet_trampoline;
619 tasklet_init(&ttimer->tasklet, __tasklet_hrtimer_trampoline,
620 (unsigned long)ttimer);
621 ttimer->function = function;
622 }
623 EXPORT_SYMBOL_GPL(tasklet_hrtimer_init);
625 void __init softirq_init(void)
626 {
627 int cpu;
629 for_each_possible_cpu(cpu) {
630 per_cpu(tasklet_vec, cpu).tail =
631 &per_cpu(tasklet_vec, cpu).head;
632 per_cpu(tasklet_hi_vec, cpu).tail =
633 &per_cpu(tasklet_hi_vec, cpu).head;
634 }
636 open_softirq(TASKLET_SOFTIRQ, tasklet_action);
637 open_softirq(HI_SOFTIRQ, tasklet_hi_action);
638 }
640 static int ksoftirqd_should_run(unsigned int cpu)
641 {
642 return local_softirq_pending();
643 }
645 static void run_ksoftirqd(unsigned int cpu)
646 {
647 local_irq_disable();
648 if (local_softirq_pending()) {
649 /*
650 * We can safely run softirq on inline stack, as we are not deep
651 * in the task stack here.
652 */
653 __do_softirq();
654 local_irq_enable();
655 cond_resched();
656 return;
657 }
658 local_irq_enable();
659 }
661 #ifdef CONFIG_HOTPLUG_CPU
662 /*
663 * tasklet_kill_immediate is called to remove a tasklet which can already be
664 * scheduled for execution on @cpu.
665 *
666 * Unlike tasklet_kill, this function removes the tasklet
667 * _immediately_, even if the tasklet is in TASKLET_STATE_SCHED state.
668 *
669 * When this function is called, @cpu must be in the CPU_DEAD state.
670 */
671 void tasklet_kill_immediate(struct tasklet_struct *t, unsigned int cpu)
672 {
673 struct tasklet_struct **i;
675 BUG_ON(cpu_online(cpu));
676 BUG_ON(test_bit(TASKLET_STATE_RUN, &t->state));
678 if (!test_bit(TASKLET_STATE_SCHED, &t->state))
679 return;
681 /* CPU is dead, so no lock needed. */
682 for (i = &per_cpu(tasklet_vec, cpu).head; *i; i = &(*i)->next) {
683 if (*i == t) {
684 *i = t->next;
685 /* If this was the tail element, move the tail ptr */
686 if (*i == NULL)
687 per_cpu(tasklet_vec, cpu).tail = i;
688 return;
689 }
690 }
691 BUG();
692 }
694 static int takeover_tasklets(unsigned int cpu)
695 {
696 /* CPU is dead, so no lock needed. */
697 local_irq_disable();
699 /* Find end, append list for that CPU. */
700 if (&per_cpu(tasklet_vec, cpu).head != per_cpu(tasklet_vec, cpu).tail) {
701 *__this_cpu_read(tasklet_vec.tail) = per_cpu(tasklet_vec, cpu).head;
702 this_cpu_write(tasklet_vec.tail, per_cpu(tasklet_vec, cpu).tail);
703 per_cpu(tasklet_vec, cpu).head = NULL;
704 per_cpu(tasklet_vec, cpu).tail = &per_cpu(tasklet_vec, cpu).head;
705 }
706 raise_softirq_irqoff(TASKLET_SOFTIRQ);
708 if (&per_cpu(tasklet_hi_vec, cpu).head != per_cpu(tasklet_hi_vec, cpu).tail) {
709 *__this_cpu_read(tasklet_hi_vec.tail) = per_cpu(tasklet_hi_vec, cpu).head;
710 __this_cpu_write(tasklet_hi_vec.tail, per_cpu(tasklet_hi_vec, cpu).tail);
711 per_cpu(tasklet_hi_vec, cpu).head = NULL;
712 per_cpu(tasklet_hi_vec, cpu).tail = &per_cpu(tasklet_hi_vec, cpu).head;
713 }
714 raise_softirq_irqoff(HI_SOFTIRQ);
716 local_irq_enable();
717 return 0;
718 }
719 #else
720 #define takeover_tasklets NULL
721 #endif /* CONFIG_HOTPLUG_CPU */
723 static struct smp_hotplug_thread softirq_threads = {
724 .store = &ksoftirqd,
725 .thread_should_run = ksoftirqd_should_run,
726 .thread_fn = run_ksoftirqd,
727 .thread_comm = "ksoftirqd/%u",
728 };
730 static __init int spawn_ksoftirqd(void)
731 {
732 cpuhp_setup_state_nocalls(CPUHP_SOFTIRQ_DEAD, "softirq:dead", NULL,
733 takeover_tasklets);
734 BUG_ON(smpboot_register_percpu_thread(&softirq_threads));
736 return 0;
737 }
738 early_initcall(spawn_ksoftirqd);
740 /*
741 * [ These __weak aliases are kept in a separate compilation unit, so that
742 * GCC does not inline them incorrectly. ]
743 */
745 int __init __weak early_irq_init(void)
746 {
747 return 0;
748 }
750 int __init __weak arch_probe_nr_irqs(void)
751 {
752 return NR_IRQS_LEGACY;
753 }
755 int __init __weak arch_early_irq_init(void)
756 {
757 return 0;
758 }
760 unsigned int __weak arch_dynirq_lower_bound(unsigned int from)
761 {
762 return from;
763 }