]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/hwspinlock.git/blob - mm/highmem.c
soc: ti: wkup_m3_ipc: Fix race condition with rproc_boot
[rpmsg/hwspinlock.git] / mm / highmem.c
1 // SPDX-License-Identifier: GPL-2.0
2 /*
3  * High memory handling common code and variables.
4  *
5  * (C) 1999 Andrea Arcangeli, SuSE GmbH, andrea@suse.de
6  *          Gerhard Wichert, Siemens AG, Gerhard.Wichert@pdb.siemens.de
7  *
8  *
9  * Redesigned the x86 32-bit VM architecture to deal with
10  * 64-bit physical space. With current x86 CPUs this
11  * means up to 64 Gigabytes physical RAM.
12  *
13  * Rewrote high memory support to move the page cache into
14  * high memory. Implemented permanent (schedulable) kmaps
15  * based on Linus' idea.
16  *
17  * Copyright (C) 1999 Ingo Molnar <mingo@redhat.com>
18  */
20 #include <linux/mm.h>
21 #include <linux/export.h>
22 #include <linux/swap.h>
23 #include <linux/bio.h>
24 #include <linux/pagemap.h>
25 #include <linux/mempool.h>
26 #include <linux/blkdev.h>
27 #include <linux/init.h>
28 #include <linux/hash.h>
29 #include <linux/highmem.h>
30 #include <linux/kgdb.h>
31 #include <asm/tlbflush.h>
34 #if defined(CONFIG_HIGHMEM) || defined(CONFIG_X86_32)
35 DEFINE_PER_CPU(int, __kmap_atomic_idx);
36 #endif
38 /*
39  * Virtual_count is not a pure "count".
40  *  0 means that it is not mapped, and has not been mapped
41  *    since a TLB flush - it is usable.
42  *  1 means that there are no users, but it has been mapped
43  *    since the last TLB flush - so we can't use it.
44  *  n means that there are (n-1) current users of it.
45  */
46 #ifdef CONFIG_HIGHMEM
48 /*
49  * Architecture with aliasing data cache may define the following family of
50  * helper functions in its asm/highmem.h to control cache color of virtual
51  * addresses where physical memory pages are mapped by kmap.
52  */
53 #ifndef get_pkmap_color
55 /*
56  * Determine color of virtual address where the page should be mapped.
57  */
58 static inline unsigned int get_pkmap_color(struct page *page)
59 {
60         return 0;
61 }
62 #define get_pkmap_color get_pkmap_color
64 /*
65  * Get next index for mapping inside PKMAP region for page with given color.
66  */
67 static inline unsigned int get_next_pkmap_nr(unsigned int color)
68 {
69         static unsigned int last_pkmap_nr;
71         last_pkmap_nr = (last_pkmap_nr + 1) & LAST_PKMAP_MASK;
72         return last_pkmap_nr;
73 }
75 /*
76  * Determine if page index inside PKMAP region (pkmap_nr) of given color
77  * has wrapped around PKMAP region end. When this happens an attempt to
78  * flush all unused PKMAP slots is made.
79  */
80 static inline int no_more_pkmaps(unsigned int pkmap_nr, unsigned int color)
81 {
82         return pkmap_nr == 0;
83 }
85 /*
86  * Get the number of PKMAP entries of the given color. If no free slot is
87  * found after checking that many entries, kmap will sleep waiting for
88  * someone to call kunmap and free PKMAP slot.
89  */
90 static inline int get_pkmap_entries_count(unsigned int color)
91 {
92         return LAST_PKMAP;
93 }
95 /*
96  * Get head of a wait queue for PKMAP entries of the given color.
97  * Wait queues for different mapping colors should be independent to avoid
98  * unnecessary wakeups caused by freeing of slots of other colors.
99  */
100 static inline wait_queue_head_t *get_pkmap_wait_queue_head(unsigned int color)
102         static DECLARE_WAIT_QUEUE_HEAD(pkmap_map_wait);
104         return &pkmap_map_wait;
106 #endif
108 unsigned long totalhigh_pages __read_mostly;
109 EXPORT_SYMBOL(totalhigh_pages);
112 EXPORT_PER_CPU_SYMBOL(__kmap_atomic_idx);
114 unsigned int nr_free_highpages (void)
116         struct zone *zone;
117         unsigned int pages = 0;
119         for_each_populated_zone(zone) {
120                 if (is_highmem(zone))
121                         pages += zone_page_state(zone, NR_FREE_PAGES);
122         }
124         return pages;
127 static int pkmap_count[LAST_PKMAP];
128 static  __cacheline_aligned_in_smp DEFINE_SPINLOCK(kmap_lock);
130 pte_t * pkmap_page_table;
132 /*
133  * Most architectures have no use for kmap_high_get(), so let's abstract
134  * the disabling of IRQ out of the locking in that case to save on a
135  * potential useless overhead.
136  */
137 #ifdef ARCH_NEEDS_KMAP_HIGH_GET
138 #define lock_kmap()             spin_lock_irq(&kmap_lock)
139 #define unlock_kmap()           spin_unlock_irq(&kmap_lock)
140 #define lock_kmap_any(flags)    spin_lock_irqsave(&kmap_lock, flags)
141 #define unlock_kmap_any(flags)  spin_unlock_irqrestore(&kmap_lock, flags)
142 #else
143 #define lock_kmap()             spin_lock(&kmap_lock)
144 #define unlock_kmap()           spin_unlock(&kmap_lock)
145 #define lock_kmap_any(flags)    \
146                 do { spin_lock(&kmap_lock); (void)(flags); } while (0)
147 #define unlock_kmap_any(flags)  \
148                 do { spin_unlock(&kmap_lock); (void)(flags); } while (0)
149 #endif
151 struct page *kmap_to_page(void *vaddr)
153         unsigned long addr = (unsigned long)vaddr;
155         if (addr >= PKMAP_ADDR(0) && addr < PKMAP_ADDR(LAST_PKMAP)) {
156                 int i = PKMAP_NR(addr);
157                 return pte_page(pkmap_page_table[i]);
158         }
160         return virt_to_page(addr);
162 EXPORT_SYMBOL(kmap_to_page);
164 static void flush_all_zero_pkmaps(void)
166         int i;
167         int need_flush = 0;
169         flush_cache_kmaps();
171         for (i = 0; i < LAST_PKMAP; i++) {
172                 struct page *page;
174                 /*
175                  * zero means we don't have anything to do,
176                  * >1 means that it is still in use. Only
177                  * a count of 1 means that it is free but
178                  * needs to be unmapped
179                  */
180                 if (pkmap_count[i] != 1)
181                         continue;
182                 pkmap_count[i] = 0;
184                 /* sanity check */
185                 BUG_ON(pte_none(pkmap_page_table[i]));
187                 /*
188                  * Don't need an atomic fetch-and-clear op here;
189                  * no-one has the page mapped, and cannot get at
190                  * its virtual address (and hence PTE) without first
191                  * getting the kmap_lock (which is held here).
192                  * So no dangers, even with speculative execution.
193                  */
194                 page = pte_page(pkmap_page_table[i]);
195                 pte_clear(&init_mm, PKMAP_ADDR(i), &pkmap_page_table[i]);
197                 set_page_address(page, NULL);
198                 need_flush = 1;
199         }
200         if (need_flush)
201                 flush_tlb_kernel_range(PKMAP_ADDR(0), PKMAP_ADDR(LAST_PKMAP));
204 /**
205  * kmap_flush_unused - flush all unused kmap mappings in order to remove stray mappings
206  */
207 void kmap_flush_unused(void)
209         lock_kmap();
210         flush_all_zero_pkmaps();
211         unlock_kmap();
214 static inline unsigned long map_new_virtual(struct page *page)
216         unsigned long vaddr;
217         int count;
218         unsigned int last_pkmap_nr;
219         unsigned int color = get_pkmap_color(page);
221 start:
222         count = get_pkmap_entries_count(color);
223         /* Find an empty entry */
224         for (;;) {
225                 last_pkmap_nr = get_next_pkmap_nr(color);
226                 if (no_more_pkmaps(last_pkmap_nr, color)) {
227                         flush_all_zero_pkmaps();
228                         count = get_pkmap_entries_count(color);
229                 }
230                 if (!pkmap_count[last_pkmap_nr])
231                         break;  /* Found a usable entry */
232                 if (--count)
233                         continue;
235                 /*
236                  * Sleep for somebody else to unmap their entries
237                  */
238                 {
239                         DECLARE_WAITQUEUE(wait, current);
240                         wait_queue_head_t *pkmap_map_wait =
241                                 get_pkmap_wait_queue_head(color);
243                         __set_current_state(TASK_UNINTERRUPTIBLE);
244                         add_wait_queue(pkmap_map_wait, &wait);
245                         unlock_kmap();
246                         schedule();
247                         remove_wait_queue(pkmap_map_wait, &wait);
248                         lock_kmap();
250                         /* Somebody else might have mapped it while we slept */
251                         if (page_address(page))
252                                 return (unsigned long)page_address(page);
254                         /* Re-start */
255                         goto start;
256                 }
257         }
258         vaddr = PKMAP_ADDR(last_pkmap_nr);
259         set_pte_at(&init_mm, vaddr,
260                    &(pkmap_page_table[last_pkmap_nr]), mk_pte(page, kmap_prot));
262         pkmap_count[last_pkmap_nr] = 1;
263         set_page_address(page, (void *)vaddr);
265         return vaddr;
268 /**
269  * kmap_high - map a highmem page into memory
270  * @page: &struct page to map
271  *
272  * Returns the page's virtual memory address.
273  *
274  * We cannot call this from interrupts, as it may block.
275  */
276 void *kmap_high(struct page *page)
278         unsigned long vaddr;
280         /*
281          * For highmem pages, we can't trust "virtual" until
282          * after we have the lock.
283          */
284         lock_kmap();
285         vaddr = (unsigned long)page_address(page);
286         if (!vaddr)
287                 vaddr = map_new_virtual(page);
288         pkmap_count[PKMAP_NR(vaddr)]++;
289         BUG_ON(pkmap_count[PKMAP_NR(vaddr)] < 2);
290         unlock_kmap();
291         return (void*) vaddr;
294 EXPORT_SYMBOL(kmap_high);
296 #ifdef ARCH_NEEDS_KMAP_HIGH_GET
297 /**
298  * kmap_high_get - pin a highmem page into memory
299  * @page: &struct page to pin
300  *
301  * Returns the page's current virtual memory address, or NULL if no mapping
302  * exists.  If and only if a non null address is returned then a
303  * matching call to kunmap_high() is necessary.
304  *
305  * This can be called from any context.
306  */
307 void *kmap_high_get(struct page *page)
309         unsigned long vaddr, flags;
311         lock_kmap_any(flags);
312         vaddr = (unsigned long)page_address(page);
313         if (vaddr) {
314                 BUG_ON(pkmap_count[PKMAP_NR(vaddr)] < 1);
315                 pkmap_count[PKMAP_NR(vaddr)]++;
316         }
317         unlock_kmap_any(flags);
318         return (void*) vaddr;
320 #endif
322 /**
323  * kunmap_high - unmap a highmem page into memory
324  * @page: &struct page to unmap
325  *
326  * If ARCH_NEEDS_KMAP_HIGH_GET is not defined then this may be called
327  * only from user context.
328  */
329 void kunmap_high(struct page *page)
331         unsigned long vaddr;
332         unsigned long nr;
333         unsigned long flags;
334         int need_wakeup;
335         unsigned int color = get_pkmap_color(page);
336         wait_queue_head_t *pkmap_map_wait;
338         lock_kmap_any(flags);
339         vaddr = (unsigned long)page_address(page);
340         BUG_ON(!vaddr);
341         nr = PKMAP_NR(vaddr);
343         /*
344          * A count must never go down to zero
345          * without a TLB flush!
346          */
347         need_wakeup = 0;
348         switch (--pkmap_count[nr]) {
349         case 0:
350                 BUG();
351         case 1:
352                 /*
353                  * Avoid an unnecessary wake_up() function call.
354                  * The common case is pkmap_count[] == 1, but
355                  * no waiters.
356                  * The tasks queued in the wait-queue are guarded
357                  * by both the lock in the wait-queue-head and by
358                  * the kmap_lock.  As the kmap_lock is held here,
359                  * no need for the wait-queue-head's lock.  Simply
360                  * test if the queue is empty.
361                  */
362                 pkmap_map_wait = get_pkmap_wait_queue_head(color);
363                 need_wakeup = waitqueue_active(pkmap_map_wait);
364         }
365         unlock_kmap_any(flags);
367         /* do wake-up, if needed, race-free outside of the spin lock */
368         if (need_wakeup)
369                 wake_up(pkmap_map_wait);
372 EXPORT_SYMBOL(kunmap_high);
373 #endif
375 #if defined(HASHED_PAGE_VIRTUAL)
377 #define PA_HASH_ORDER   7
379 /*
380  * Describes one page->virtual association
381  */
382 struct page_address_map {
383         struct page *page;
384         void *virtual;
385         struct list_head list;
386 };
388 static struct page_address_map page_address_maps[LAST_PKMAP];
390 /*
391  * Hash table bucket
392  */
393 static struct page_address_slot {
394         struct list_head lh;                    /* List of page_address_maps */
395         spinlock_t lock;                        /* Protect this bucket's list */
396 } ____cacheline_aligned_in_smp page_address_htable[1<<PA_HASH_ORDER];
398 static struct page_address_slot *page_slot(const struct page *page)
400         return &page_address_htable[hash_ptr(page, PA_HASH_ORDER)];
403 /**
404  * page_address - get the mapped virtual address of a page
405  * @page: &struct page to get the virtual address of
406  *
407  * Returns the page's virtual address.
408  */
409 void *page_address(const struct page *page)
411         unsigned long flags;
412         void *ret;
413         struct page_address_slot *pas;
415         if (!PageHighMem(page))
416                 return lowmem_page_address(page);
418         pas = page_slot(page);
419         ret = NULL;
420         spin_lock_irqsave(&pas->lock, flags);
421         if (!list_empty(&pas->lh)) {
422                 struct page_address_map *pam;
424                 list_for_each_entry(pam, &pas->lh, list) {
425                         if (pam->page == page) {
426                                 ret = pam->virtual;
427                                 goto done;
428                         }
429                 }
430         }
431 done:
432         spin_unlock_irqrestore(&pas->lock, flags);
433         return ret;
436 EXPORT_SYMBOL(page_address);
438 /**
439  * set_page_address - set a page's virtual address
440  * @page: &struct page to set
441  * @virtual: virtual address to use
442  */
443 void set_page_address(struct page *page, void *virtual)
445         unsigned long flags;
446         struct page_address_slot *pas;
447         struct page_address_map *pam;
449         BUG_ON(!PageHighMem(page));
451         pas = page_slot(page);
452         if (virtual) {          /* Add */
453                 pam = &page_address_maps[PKMAP_NR((unsigned long)virtual)];
454                 pam->page = page;
455                 pam->virtual = virtual;
457                 spin_lock_irqsave(&pas->lock, flags);
458                 list_add_tail(&pam->list, &pas->lh);
459                 spin_unlock_irqrestore(&pas->lock, flags);
460         } else {                /* Remove */
461                 spin_lock_irqsave(&pas->lock, flags);
462                 list_for_each_entry(pam, &pas->lh, list) {
463                         if (pam->page == page) {
464                                 list_del(&pam->list);
465                                 spin_unlock_irqrestore(&pas->lock, flags);
466                                 goto done;
467                         }
468                 }
469                 spin_unlock_irqrestore(&pas->lock, flags);
470         }
471 done:
472         return;
475 void __init page_address_init(void)
477         int i;
479         for (i = 0; i < ARRAY_SIZE(page_address_htable); i++) {
480                 INIT_LIST_HEAD(&page_address_htable[i].lh);
481                 spin_lock_init(&page_address_htable[i].lock);
482         }
485 #endif  /* defined(CONFIG_HIGHMEM) && !defined(WANT_PAGE_VIRTUAL) */