1 // SPDX-License-Identifier: GPL-2.0
2 /*
3 * linux/mm/mincore.c
4 *
5 * Copyright (C) 1994-2006 Linus Torvalds
6 */
8 /*
9 * The mincore() system call.
10 */
11 #include <linux/pagemap.h>
12 #include <linux/gfp.h>
13 #include <linux/mm.h>
14 #include <linux/mman.h>
15 #include <linux/syscalls.h>
16 #include <linux/swap.h>
17 #include <linux/swapops.h>
18 #include <linux/shmem_fs.h>
19 #include <linux/hugetlb.h>
21 #include <linux/uaccess.h>
22 #include <asm/pgtable.h>
24 static int mincore_hugetlb(pte_t *pte, unsigned long hmask, unsigned long addr,
25 unsigned long end, struct mm_walk *walk)
26 {
27 #ifdef CONFIG_HUGETLB_PAGE
28 unsigned char present;
29 unsigned char *vec = walk->private;
31 /*
32 * Hugepages under user process are always in RAM and never
33 * swapped out, but theoretically it needs to be checked.
34 */
35 present = pte && !huge_pte_none(huge_ptep_get(pte));
36 for (; addr != end; vec++, addr += PAGE_SIZE)
37 *vec = present;
38 walk->private = vec;
39 #else
40 BUG();
41 #endif
42 return 0;
43 }
45 /*
46 * Later we can get more picky about what "in core" means precisely.
47 * For now, simply check to see if the page is in the page cache,
48 * and is up to date; i.e. that no page-in operation would be required
49 * at this time if an application were to map and access this page.
50 */
51 static unsigned char mincore_page(struct address_space *mapping, pgoff_t pgoff)
52 {
53 unsigned char present = 0;
54 struct page *page;
56 /*
57 * When tmpfs swaps out a page from a file, any process mapping that
58 * file will not get a swp_entry_t in its pte, but rather it is like
59 * any other file mapping (ie. marked !present and faulted in with
60 * tmpfs's .fault). So swapped out tmpfs mappings are tested here.
61 */
62 #ifdef CONFIG_SWAP
63 if (shmem_mapping(mapping)) {
64 page = find_get_entry(mapping, pgoff);
65 /*
66 * shmem/tmpfs may return swap: account for swapcache
67 * page too.
68 */
69 if (radix_tree_exceptional_entry(page)) {
70 swp_entry_t swp = radix_to_swp_entry(page);
71 page = find_get_page(swap_address_space(swp),
72 swp_offset(swp));
73 }
74 } else
75 page = find_get_page(mapping, pgoff);
76 #else
77 page = find_get_page(mapping, pgoff);
78 #endif
79 if (page) {
80 present = PageUptodate(page);
81 put_page(page);
82 }
84 return present;
85 }
87 static int __mincore_unmapped_range(unsigned long addr, unsigned long end,
88 struct vm_area_struct *vma, unsigned char *vec)
89 {
90 unsigned long nr = (end - addr) >> PAGE_SHIFT;
91 int i;
93 if (vma->vm_file) {
94 pgoff_t pgoff;
96 pgoff = linear_page_index(vma, addr);
97 for (i = 0; i < nr; i++, pgoff++)
98 vec[i] = mincore_page(vma->vm_file->f_mapping, pgoff);
99 } else {
100 for (i = 0; i < nr; i++)
101 vec[i] = 0;
102 }
103 return nr;
104 }
106 static int mincore_unmapped_range(unsigned long addr, unsigned long end,
107 struct mm_walk *walk)
108 {
109 walk->private += __mincore_unmapped_range(addr, end,
110 walk->vma, walk->private);
111 return 0;
112 }
114 static int mincore_pte_range(pmd_t *pmd, unsigned long addr, unsigned long end,
115 struct mm_walk *walk)
116 {
117 spinlock_t *ptl;
118 struct vm_area_struct *vma = walk->vma;
119 pte_t *ptep;
120 unsigned char *vec = walk->private;
121 int nr = (end - addr) >> PAGE_SHIFT;
123 ptl = pmd_trans_huge_lock(pmd, vma);
124 if (ptl) {
125 memset(vec, 1, nr);
126 spin_unlock(ptl);
127 goto out;
128 }
130 if (pmd_trans_unstable(pmd)) {
131 __mincore_unmapped_range(addr, end, vma, vec);
132 goto out;
133 }
135 ptep = pte_offset_map_lock(walk->mm, pmd, addr, &ptl);
136 for (; addr != end; ptep++, addr += PAGE_SIZE) {
137 pte_t pte = *ptep;
139 if (pte_none(pte))
140 __mincore_unmapped_range(addr, addr + PAGE_SIZE,
141 vma, vec);
142 else if (pte_present(pte))
143 *vec = 1;
144 else { /* pte is a swap entry */
145 swp_entry_t entry = pte_to_swp_entry(pte);
147 if (non_swap_entry(entry)) {
148 /*
149 * migration or hwpoison entries are always
150 * uptodate
151 */
152 *vec = 1;
153 } else {
154 #ifdef CONFIG_SWAP
155 *vec = mincore_page(swap_address_space(entry),
156 swp_offset(entry));
157 #else
158 WARN_ON(1);
159 *vec = 1;
160 #endif
161 }
162 }
163 vec++;
164 }
165 pte_unmap_unlock(ptep - 1, ptl);
166 out:
167 walk->private += nr;
168 cond_resched();
169 return 0;
170 }
172 /*
173 * Do a chunk of "sys_mincore()". We've already checked
174 * all the arguments, we hold the mmap semaphore: we should
175 * just return the amount of info we're asked for.
176 */
177 static long do_mincore(unsigned long addr, unsigned long pages, unsigned char *vec)
178 {
179 struct vm_area_struct *vma;
180 unsigned long end;
181 int err;
182 struct mm_walk mincore_walk = {
183 .pmd_entry = mincore_pte_range,
184 .pte_hole = mincore_unmapped_range,
185 .hugetlb_entry = mincore_hugetlb,
186 .private = vec,
187 };
189 vma = find_vma(current->mm, addr);
190 if (!vma || addr < vma->vm_start)
191 return -ENOMEM;
192 mincore_walk.mm = vma->vm_mm;
193 end = min(vma->vm_end, addr + (pages << PAGE_SHIFT));
194 err = walk_page_range(addr, end, &mincore_walk);
195 if (err < 0)
196 return err;
197 return (end - addr) >> PAGE_SHIFT;
198 }
200 /*
201 * The mincore(2) system call.
202 *
203 * mincore() returns the memory residency status of the pages in the
204 * current process's address space specified by [addr, addr + len).
205 * The status is returned in a vector of bytes. The least significant
206 * bit of each byte is 1 if the referenced page is in memory, otherwise
207 * it is zero.
208 *
209 * Because the status of a page can change after mincore() checks it
210 * but before it returns to the application, the returned vector may
211 * contain stale information. Only locked pages are guaranteed to
212 * remain in memory.
213 *
214 * return values:
215 * zero - success
216 * -EFAULT - vec points to an illegal address
217 * -EINVAL - addr is not a multiple of PAGE_SIZE
218 * -ENOMEM - Addresses in the range [addr, addr + len] are
219 * invalid for the address space of this process, or
220 * specify one or more pages which are not currently
221 * mapped
222 * -EAGAIN - A kernel resource was temporarily unavailable.
223 */
224 SYSCALL_DEFINE3(mincore, unsigned long, start, size_t, len,
225 unsigned char __user *, vec)
226 {
227 long retval;
228 unsigned long pages;
229 unsigned char *tmp;
231 /* Check the start address: needs to be page-aligned.. */
232 if (start & ~PAGE_MASK)
233 return -EINVAL;
235 /* ..and we need to be passed a valid user-space range */
236 if (!access_ok(VERIFY_READ, (void __user *) start, len))
237 return -ENOMEM;
239 /* This also avoids any overflows on PAGE_ALIGN */
240 pages = len >> PAGE_SHIFT;
241 pages += (offset_in_page(len)) != 0;
243 if (!access_ok(VERIFY_WRITE, vec, pages))
244 return -EFAULT;
246 tmp = (void *) __get_free_page(GFP_USER);
247 if (!tmp)
248 return -EAGAIN;
250 retval = 0;
251 while (pages) {
252 /*
253 * Do at most PAGE_SIZE entries per iteration, due to
254 * the temporary buffer size.
255 */
256 down_read(¤t->mm->mmap_sem);
257 retval = do_mincore(start, min(pages, PAGE_SIZE), tmp);
258 up_read(¤t->mm->mmap_sem);
260 if (retval <= 0)
261 break;
262 if (copy_to_user(vec, tmp, retval)) {
263 retval = -EFAULT;
264 break;
265 }
266 pages -= retval;
267 vec += retval;
268 start += retval << PAGE_SHIFT;
269 retval = 0;
270 }
271 free_page((unsigned long) tmp);
272 return retval;
273 }