1 ####
2 # kbuild: Generic definitions
4 # Convenient variables
5 comma := ,
6 quote := "
7 squote := '
8 empty :=
9 space := $(empty) $(empty)
10 space_escape := _-_SPACE_-_
11 pound := \#
13 ###
14 # Name of target with a '.' as filename prefix. foo/bar.o => foo/.bar.o
15 dot-target = $(dir $@).$(notdir $@)
17 ###
18 # The temporary file to save gcc -MD generated dependencies must not
19 # contain a comma
20 depfile = $(subst $(comma),_,$(dot-target).d)
22 ###
23 # filename of target with directory and extension stripped
24 basetarget = $(basename $(notdir $@))
26 ###
27 # filename of first prerequisite with directory and extension stripped
28 baseprereq = $(basename $(notdir $<))
30 ###
31 # Escape single quote for use in echo statements
32 escsq = $(subst $(squote),'\$(squote)',$1)
34 ###
35 # Easy method for doing a status message
36 kecho := :
37 quiet_kecho := echo
38 silent_kecho := :
39 kecho := $($(quiet)kecho)
41 ###
42 # filechk is used to check if the content of a generated file is updated.
43 # Sample usage:
44 # define filechk_sample
45 # echo $KERNELRELEASE
46 # endef
47 # version.h : Makefile
48 # $(call filechk,sample)
49 # The rule defined shall write to stdout the content of the new file.
50 # The existing file will be compared with the new one.
51 # - If no file exist it is created
52 # - If the content differ the new file is used
53 # - If they are equal no change, and no timestamp update
54 # - stdin is piped in from the first prerequisite ($<) so one has
55 # to specify a valid file as first prerequisite (often the kbuild file)
56 define filechk
57 $(Q)set -e; \
58 mkdir -p $(dir $@); \
59 $(filechk_$(1)) > $@.tmp; \
60 if [ -r $@ ] && cmp -s $@ $@.tmp; then \
61 rm -f $@.tmp; \
62 else \
63 $(kecho) ' UPD $@'; \
64 mv -f $@.tmp $@; \
65 fi
66 endef
68 ######
69 # gcc support functions
70 # See documentation in Documentation/kbuild/makefiles.txt
72 # cc-cross-prefix
73 # Usage: CROSS_COMPILE := $(call cc-cross-prefix, m68k-linux-gnu- m68k-linux-)
74 # Return first prefix where a prefix$(CC) is found in PATH.
75 # If no $(CC) found in PATH with listed prefixes return nothing
76 cc-cross-prefix = \
77 $(word 1, $(foreach c,$(1), \
78 $(shell set -e; \
79 if (which $(strip $(c))$(CC)) > /dev/null 2>&1 ; then \
80 echo $(c); \
81 fi)))
83 # output directory for tests below
84 TMPOUT := $(if $(KBUILD_EXTMOD),$(firstword $(KBUILD_EXTMOD))/)
86 # try-run
87 # Usage: option = $(call try-run, $(CC)...-o "$$TMP",option-ok,otherwise)
88 # Exit code chooses option. "$$TMP" serves as a temporary file and is
89 # automatically cleaned up.
90 try-run = $(shell set -e; \
91 TMP="$(TMPOUT).$$$$.tmp"; \
92 TMPO="$(TMPOUT).$$$$.o"; \
93 if ($(1)) >/dev/null 2>&1; \
94 then echo "$(2)"; \
95 else echo "$(3)"; \
96 fi; \
97 rm -f "$$TMP" "$$TMPO")
99 # as-option
100 # Usage: cflags-y += $(call as-option,-Wa$(comma)-isa=foo,)
102 as-option = $(call try-run,\
103 $(CC) $(KBUILD_CFLAGS) $(1) -c -x assembler /dev/null -o "$$TMP",$(1),$(2))
105 # as-instr
106 # Usage: cflags-y += $(call as-instr,instr,option1,option2)
108 as-instr = $(call try-run,\
109 printf "%b\n" "$(1)" | $(CC) $(KBUILD_AFLAGS) -c -x assembler -o "$$TMP" -,$(2),$(3))
111 # __cc-option
112 # Usage: MY_CFLAGS += $(call __cc-option,$(CC),$(MY_CFLAGS),-march=winchip-c6,-march=i586)
113 __cc-option = $(call try-run,\
114 $(1) -Werror $(2) $(3) -c -x c /dev/null -o "$$TMP",$(3),$(4))
116 # Do not attempt to build with gcc plugins during cc-option tests.
117 # (And this uses delayed resolution so the flags will be up to date.)
118 CC_OPTION_CFLAGS = $(filter-out $(GCC_PLUGINS_CFLAGS),$(KBUILD_CFLAGS))
120 # cc-option
121 # Usage: cflags-y += $(call cc-option,-march=winchip-c6,-march=i586)
123 cc-option = $(call __cc-option, $(CC),\
124 $(KBUILD_CPPFLAGS) $(CC_OPTION_CFLAGS),$(1),$(2))
126 # hostcc-option
127 # Usage: cflags-y += $(call hostcc-option,-march=winchip-c6,-march=i586)
128 hostcc-option = $(call __cc-option, $(HOSTCC),\
129 $(KBUILD_HOSTCFLAGS) $(HOST_EXTRACFLAGS),$(1),$(2))
131 # cc-option-yn
132 # Usage: flag := $(call cc-option-yn,-march=winchip-c6)
133 cc-option-yn = $(call try-run,\
134 $(CC) -Werror $(KBUILD_CPPFLAGS) $(CC_OPTION_CFLAGS) $(1) -c -x c /dev/null -o "$$TMP",y,n)
136 # cc-disable-warning
137 # Usage: cflags-y += $(call cc-disable-warning,unused-but-set-variable)
138 cc-disable-warning = $(call try-run,\
139 $(CC) -Werror $(KBUILD_CPPFLAGS) $(CC_OPTION_CFLAGS) -W$(strip $(1)) -c -x c /dev/null -o "$$TMP",-Wno-$(strip $(1)))
141 # cc-name
142 # Expands to either gcc or clang
143 cc-name = $(shell $(CC) -v 2>&1 | grep -q "clang version" && echo clang || echo gcc)
145 # cc-version
146 cc-version = $(shell $(CONFIG_SHELL) $(srctree)/scripts/gcc-version.sh $(CC))
148 # cc-fullversion
149 cc-fullversion = $(shell $(CONFIG_SHELL) \
150 $(srctree)/scripts/gcc-version.sh -p $(CC))
152 # cc-ifversion
153 # Usage: EXTRA_CFLAGS += $(call cc-ifversion, -lt, 0402, -O1)
154 cc-ifversion = $(shell [ $(cc-version) $(1) $(2) ] && echo $(3) || echo $(4))
156 # cc-ldoption
157 # Usage: ldflags += $(call cc-ldoption, -Wl$(comma)--hash-style=both)
158 cc-ldoption = $(call try-run,\
159 $(CC) $(1) $(KBUILD_CPPFLAGS) $(CC_OPTION_CFLAGS) -nostdlib -x c /dev/null -o "$$TMP",$(1),$(2))
161 # ld-option
162 # Usage: KBUILD_LDFLAGS += $(call ld-option, -X, -Y)
163 ld-option = $(call try-run, $(LD) $(KBUILD_LDFLAGS) $(1) -v,$(1),$(2),$(3))
165 # ar-option
166 # Usage: KBUILD_ARFLAGS := $(call ar-option,D)
167 # Important: no spaces around options
168 ar-option = $(call try-run, $(AR) rc$(1) "$$TMP",$(1),$(2))
170 # ld-version
171 # Note this is mainly for HJ Lu's 3 number binutil versions
172 ld-version = $(shell $(LD) --version | $(srctree)/scripts/ld-version.sh)
174 # ld-ifversion
175 # Usage: $(call ld-ifversion, -ge, 22252, y)
176 ld-ifversion = $(shell [ $(ld-version) $(1) $(2) ] && echo $(3) || echo $(4))
178 ######
180 ###
181 # Shorthand for $(Q)$(MAKE) -f scripts/Makefile.build obj=
182 # Usage:
183 # $(Q)$(MAKE) $(build)=dir
184 build := -f $(srctree)/scripts/Makefile.build obj
186 ###
187 # Shorthand for $(Q)$(MAKE) -f scripts/Makefile.modbuiltin obj=
188 # Usage:
189 # $(Q)$(MAKE) $(modbuiltin)=dir
190 modbuiltin := -f $(srctree)/scripts/Makefile.modbuiltin obj
192 ###
193 # Shorthand for $(Q)$(MAKE) -f scripts/Makefile.dtbinst obj=
194 # Usage:
195 # $(Q)$(MAKE) $(dtbinst)=dir
196 dtbinst := -f $(if $(KBUILD_SRC),$(srctree)/)scripts/Makefile.dtbinst obj
198 ###
199 # Shorthand for $(Q)$(MAKE) -f scripts/Makefile.clean obj=
200 # Usage:
201 # $(Q)$(MAKE) $(clean)=dir
202 clean := -f $(srctree)/scripts/Makefile.clean obj
204 ###
205 # Shorthand for $(Q)$(MAKE) -f scripts/Makefile.headersinst obj=
206 # Usage:
207 # $(Q)$(MAKE) $(hdr-inst)=dir
208 hdr-inst := -f $(srctree)/scripts/Makefile.headersinst obj
210 # Prefix -I with $(srctree) if it is not an absolute path.
211 # skip if -I has no parameter
212 addtree = $(if $(patsubst -I%,%,$(1)), \
213 $(if $(filter-out -I/% -I./% -I../%,$(1)),$(patsubst -I%,-I$(srctree)/%,$(1)),$(1)),$(1))
215 # Find all -I options and call addtree
216 flags = $(foreach o,$($(1)),$(if $(filter -I%,$(o)),$(call addtree,$(o)),$(o)))
218 # echo command.
219 # Short version is used, if $(quiet) equals `quiet_', otherwise full one.
220 echo-cmd = $(if $($(quiet)cmd_$(1)),\
221 echo ' $(call escsq,$($(quiet)cmd_$(1)))$(echo-why)';)
223 # printing commands
224 cmd = @$(echo-cmd) $(cmd_$(1))
226 # Add $(obj)/ for paths that are not absolute
227 objectify = $(foreach o,$(1),$(if $(filter /%,$(o)),$(o),$(obj)/$(o)))
229 ###
230 # if_changed - execute command if any prerequisite is newer than
231 # target, or command line has changed
232 # if_changed_dep - as if_changed, but uses fixdep to reveal dependencies
233 # including used config symbols
234 # if_changed_rule - as if_changed but execute rule instead
235 # See Documentation/kbuild/makefiles.txt for more info
237 ifneq ($(KBUILD_NOCMDDEP),1)
238 # Check if both arguments are the same including their order. Result is empty
239 # string if equal. User may override this check using make KBUILD_NOCMDDEP=1
240 arg-check = $(filter-out $(subst $(space),$(space_escape),$(strip $(cmd_$@))), \
241 $(subst $(space),$(space_escape),$(strip $(cmd_$1))))
242 else
243 arg-check = $(if $(strip $(cmd_$@)),,1)
244 endif
246 # Replace >$< with >$$< to preserve $ when reloading the .cmd file
247 # (needed for make)
248 # Replace >#< with >$(pound)< to avoid starting a comment in the .cmd file
249 # (needed for make)
250 # Replace >'< with >'\''< to be able to enclose the whole string in '...'
251 # (needed for the shell)
252 make-cmd = $(call escsq,$(subst $(pound),$$(pound),$(subst $$,$$$$,$(cmd_$(1)))))
254 # Find any prerequisites that is newer than target or that does not exist.
255 # PHONY targets skipped in both cases.
256 any-prereq = $(filter-out $(PHONY),$?) $(filter-out $(PHONY) $(wildcard $^),$^)
258 # Execute command if command has changed or prerequisite(s) are updated.
259 if_changed = $(if $(strip $(any-prereq) $(arg-check)), \
260 @set -e; \
261 $(echo-cmd) $(cmd_$(1)); \
262 printf '%s\n' 'cmd_$@ := $(make-cmd)' > $(dot-target).cmd, @:)
264 # Execute the command and also postprocess generated .d dependencies file.
265 if_changed_dep = $(if $(strip $(any-prereq) $(arg-check) ), \
266 @set -e; \
267 $(cmd_and_fixdep), @:)
269 ifndef CONFIG_TRIM_UNUSED_KSYMS
271 cmd_and_fixdep = \
272 $(echo-cmd) $(cmd_$(1)); \
273 scripts/basic/fixdep $(depfile) $@ '$(make-cmd)' > $(dot-target).tmp;\
274 rm -f $(depfile); \
275 mv -f $(dot-target).tmp $(dot-target).cmd;
277 else
279 # Filter out exported kernel symbol names from the preprocessor output.
280 # See also __KSYM_DEPS__ in include/linux/export.h.
281 # We disable the depfile generation here, so as not to overwrite the existing
282 # depfile while fixdep is parsing it.
283 flags_nodeps = $(filter-out -Wp$(comma)-M%, $($(1)))
284 ksym_dep_filter = \
285 case "$(1)" in \
286 cc_*_c|cpp_i_c) \
287 $(CPP) $(call flags_nodeps,c_flags) -D__KSYM_DEPS__ $< ;; \
288 as_*_S|cpp_s_S) \
289 $(CPP) $(call flags_nodeps,a_flags) -D__KSYM_DEPS__ $< ;; \
290 boot*|build*|cpp_its_S|*cpp_lds_S|dtc|host*|vdso*) : ;; \
291 *) echo "Don't know how to preprocess $(1)" >&2; false ;; \
292 esac | tr ";" "\n" | sed -n 's/^.*=== __KSYM_\(.*\) ===.*$$/_\1/p'
294 cmd_and_fixdep = \
295 $(echo-cmd) $(cmd_$(1)); \
296 $(ksym_dep_filter) | \
297 scripts/basic/fixdep -e $(depfile) $@ '$(make-cmd)' \
298 > $(dot-target).tmp; \
299 rm -f $(depfile); \
300 mv -f $(dot-target).tmp $(dot-target).cmd;
302 endif
304 # Usage: $(call if_changed_rule,foo)
305 # Will check if $(cmd_foo) or any of the prerequisites changed,
306 # and if so will execute $(rule_foo).
307 if_changed_rule = $(if $(strip $(any-prereq) $(arg-check) ), \
308 @set -e; \
309 $(rule_$(1)), @:)
311 ###
312 # why - tell why a target got built
313 # enabled by make V=2
314 # Output (listed in the order they are checked):
315 # (1) - due to target is PHONY
316 # (2) - due to target missing
317 # (3) - due to: file1.h file2.h
318 # (4) - due to command line change
319 # (5) - due to missing .cmd file
320 # (6) - due to target not in $(targets)
321 # (1) PHONY targets are always build
322 # (2) No target, so we better build it
323 # (3) Prerequisite is newer than target
324 # (4) The command line stored in the file named dir/.target.cmd
325 # differed from actual command line. This happens when compiler
326 # options changes
327 # (5) No dir/.target.cmd file (used to store command line)
328 # (6) No dir/.target.cmd file and target not listed in $(targets)
329 # This is a good hint that there is a bug in the kbuild file
330 ifeq ($(KBUILD_VERBOSE),2)
331 why = \
332 $(if $(filter $@, $(PHONY)),- due to target is PHONY, \
333 $(if $(wildcard $@), \
334 $(if $(strip $(any-prereq)),- due to: $(any-prereq), \
335 $(if $(arg-check), \
336 $(if $(cmd_$@),- due to command line change, \
337 $(if $(filter $@, $(targets)), \
338 - due to missing .cmd file, \
339 - due to $(notdir $@) not in $$(targets) \
340 ) \
341 ) \
342 ) \
343 ), \
344 - due to target missing \
345 ) \
346 )
348 echo-why = $(call escsq, $(strip $(why)))
349 endif
351 ###############################################################################
352 #
353 # When a Kconfig string contains a filename, it is suitable for
354 # passing to shell commands. It is surrounded by double-quotes, and
355 # any double-quotes or backslashes within it are escaped by
356 # backslashes.
357 #
358 # This is no use for dependencies or $(wildcard). We need to strip the
359 # surrounding quotes and the escaping from quotes and backslashes, and
360 # we *do* need to escape any spaces in the string. So, for example:
361 #
362 # Usage: $(eval $(call config_filename,FOO))
363 #
364 # Defines FOO_FILENAME based on the contents of the CONFIG_FOO option,
365 # transformed as described above to be suitable for use within the
366 # makefile.
367 #
368 # Also, if the filename is a relative filename and exists in the source
369 # tree but not the build tree, define FOO_SRCPREFIX as $(srctree)/ to
370 # be prefixed to *both* command invocation and dependencies.
371 #
372 # Note: We also print the filenames in the quiet_cmd_foo text, and
373 # perhaps ought to have a version specially escaped for that purpose.
374 # But it's only cosmetic, and $(patsubst "%",%,$(CONFIG_FOO)) is good
375 # enough. It'll strip the quotes in the common case where there's no
376 # space and it's a simple filename, and it'll retain the quotes when
377 # there's a space. There are some esoteric cases in which it'll print
378 # the wrong thing, but we don't really care. The actual dependencies
379 # and commands *do* get it right, with various combinations of single
380 # and double quotes, backslashes and spaces in the filenames.
381 #
382 ###############################################################################
383 #
384 define config_filename
385 ifneq ($$(CONFIG_$(1)),"")
386 $(1)_FILENAME := $$(subst \\,\,$$(subst \$$(quote),$$(quote),$$(subst $$(space_escape),\$$(space),$$(patsubst "%",%,$$(subst $$(space),$$(space_escape),$$(CONFIG_$(1)))))))
387 ifneq ($$(patsubst /%,%,$$(firstword $$($(1)_FILENAME))),$$(firstword $$($(1)_FILENAME)))
388 else
389 ifeq ($$(wildcard $$($(1)_FILENAME)),)
390 ifneq ($$(wildcard $$(srctree)/$$($(1)_FILENAME)),)
391 $(1)_SRCPREFIX := $(srctree)/
392 endif
393 endif
394 endif
395 endif
396 endef
397 #
398 ###############################################################################
400 # delete partially updated (i.e. corrupted) files on error
401 .DELETE_ON_ERROR: