================= ARM CPUs bindings ================= The device tree allows to describe the layout of CPUs in a system through the "cpus" node, which in turn contains a number of subnodes (ie "cpu") defining properties for every cpu. Bindings for CPU nodes follow the Devicetree Specification, available from: https://www.devicetree.org/specifications/ with updates for 32-bit and 64-bit ARM systems provided in this document. ================================ Convention used in this document ================================ This document follows the conventions described in the Devicetree Specification, with the addition: - square brackets define bitfields, eg reg[7:0] value of the bitfield in the reg property contained in bits 7 down to 0 ===================================== cpus and cpu node bindings definition ===================================== The ARM architecture, in accordance with the Devicetree Specification, requires the cpus and cpu nodes to be present and contain the properties described below. - cpus node Description: Container of cpu nodes The node name must be "cpus". A cpus node must define the following properties: - #address-cells Usage: required Value type: Definition depends on ARM architecture version and configuration: # On uniprocessor ARM architectures previous to v7 value must be 1, to enable a simple enumeration scheme for processors that do not have a HW CPU identification register. # On 32-bit ARM 11 MPcore, ARM v7 or later systems value must be 1, that corresponds to CPUID/MPIDR registers sizes. # On ARM v8 64-bit systems value should be set to 2, that corresponds to the MPIDR_EL1 register size. If MPIDR_EL1[63:32] value is equal to 0 on all CPUs in the system, #address-cells can be set to 1, since MPIDR_EL1[63:32] bits are not used for CPUs identification. - #size-cells Usage: required Value type: Definition: must be set to 0 - cpu node Description: Describes a CPU in an ARM based system PROPERTIES - device_type Usage: required Value type: Definition: must be "cpu" - reg Usage and definition depend on ARM architecture version and configuration: # On uniprocessor ARM architectures previous to v7 this property is required and must be set to 0. # On ARM 11 MPcore based systems this property is required and matches the CPUID[11:0] register bits. Bits [11:0] in the reg cell must be set to bits [11:0] in CPU ID register. All other bits in the reg cell must be set to 0. # On 32-bit ARM v7 or later systems this property is required and matches the CPU MPIDR[23:0] register bits. Bits [23:0] in the reg cell must be set to bits [23:0] in MPIDR. All other bits in the reg cell must be set to 0. # On ARM v8 64-bit systems this property is required and matches the MPIDR_EL1 register affinity bits. * If cpus node's #address-cells property is set to 2 The first reg cell bits [7:0] must be set to bits [39:32] of MPIDR_EL1. The second reg cell bits [23:0] must be set to bits [23:0] of MPIDR_EL1. * If cpus node's #address-cells property is set to 1 The reg cell bits [23:0] must be set to bits [23:0] of MPIDR_EL1. All other bits in the reg cells must be set to 0. - compatible: Usage: required Value type: Definition: should be one of: "arm,arm710t" "arm,arm720t" "arm,arm740t" "arm,arm7ej-s" "arm,arm7tdmi" "arm,arm7tdmi-s" "arm,arm9es" "arm,arm9ej-s" "arm,arm920t" "arm,arm922t" "arm,arm925" "arm,arm926e-s" "arm,arm926ej-s" "arm,arm940t" "arm,arm946e-s" "arm,arm966e-s" "arm,arm968e-s" "arm,arm9tdmi" "arm,arm1020e" "arm,arm1020t" "arm,arm1022e" "arm,arm1026ej-s" "arm,arm1136j-s" "arm,arm1136jf-s" "arm,arm1156t2-s" "arm,arm1156t2f-s" "arm,arm1176jzf" "arm,arm1176jz-s" "arm,arm1176jzf-s" "arm,arm11mpcore" "arm,cortex-a5" "arm,cortex-a7" "arm,cortex-a8" "arm,cortex-a9" "arm,cortex-a12" "arm,cortex-a15" "arm,cortex-a17" "arm,cortex-a53" "arm,cortex-a57" "arm,cortex-a72" "arm,cortex-a73" "arm,cortex-m0" "arm,cortex-m0+" "arm,cortex-m1" "arm,cortex-m3" "arm,cortex-m4" "arm,cortex-r4" "arm,cortex-r5" "arm,cortex-r7" "brcm,brahma-b15" "brcm,brahma-b53" "brcm,vulcan" "cavium,thunder" "cavium,thunder2" "faraday,fa526" "intel,sa110" "intel,sa1100" "marvell,feroceon" "marvell,mohawk" "marvell,pj4a" "marvell,pj4b" "marvell,sheeva-v5" "nvidia,tegra132-denver" "nvidia,tegra186-denver" "nvidia,tegra194-carmel" "qcom,krait" "qcom,kryo" "qcom,kryo385" "qcom,scorpion" - enable-method Value type: Usage and definition depend on ARM architecture version. # On ARM v8 64-bit this property is required and must be one of: "psci" "spin-table" # On ARM 32-bit systems this property is optional and can be one of: "actions,s500-smp" "allwinner,sun6i-a31" "allwinner,sun8i-a23" "allwinner,sun9i-a80-smp" "amlogic,meson8-smp" "amlogic,meson8b-smp" "arm,realview-smp" "brcm,bcm11351-cpu-method" "brcm,bcm23550" "brcm,bcm2836-smp" "brcm,bcm-nsp-smp" "brcm,brahma-b15" "marvell,armada-375-smp" "marvell,armada-380-smp" "marvell,armada-390-smp" "marvell,armada-xp-smp" "marvell,98dx3236-smp" "mediatek,mt6589-smp" "mediatek,mt81xx-tz-smp" "qcom,gcc-msm8660" "qcom,kpss-acc-v1" "qcom,kpss-acc-v2" "renesas,apmu" "renesas,r9a06g032-smp" "rockchip,rk3036-smp" "rockchip,rk3066-smp" "ste,dbx500-smp" - cpu-release-addr Usage: required for systems that have an "enable-method" property value of "spin-table". Value type: Definition: # On ARM v8 64-bit systems must be a two cell property identifying a 64-bit zero-initialised memory location. - qcom,saw Usage: required for systems that have an "enable-method" property value of "qcom,kpss-acc-v1" or "qcom,kpss-acc-v2" Value type: Definition: Specifies the SAW[1] node associated with this CPU. - qcom,acc Usage: required for systems that have an "enable-method" property value of "qcom,kpss-acc-v1" or "qcom,kpss-acc-v2" Value type: Definition: Specifies the ACC[2] node associated with this CPU. - cpu-idle-states Usage: Optional Value type: Definition: # List of phandles to idle state nodes supported by this cpu [3]. - capacity-dmips-mhz Usage: Optional Value type: Definition: # u32 value representing CPU capacity [4] in DMIPS/MHz, relative to highest capacity-dmips-mhz in the system. - rockchip,pmu Usage: optional for systems that have an "enable-method" property value of "rockchip,rk3066-smp" While optional, it is the preferred way to get access to the cpu-core power-domains. Value type: Definition: Specifies the syscon node controlling the cpu core power domains. - dynamic-power-coefficient Usage: optional Value type: Definition: A u32 value that represents the running time dynamic power coefficient in units of mW/MHz/uV^2. The coefficient can either be calculated from power measurements or derived by analysis. The dynamic power consumption of the CPU is proportional to the square of the Voltage (V) and the clock frequency (f). The coefficient is used to calculate the dynamic power as below - Pdyn = dynamic-power-coefficient * V^2 * f where voltage is in uV, frequency is in MHz. Example 1 (dual-cluster big.LITTLE system 32-bit): cpus { #size-cells = <0>; #address-cells = <1>; cpu@0 { device_type = "cpu"; compatible = "arm,cortex-a15"; reg = <0x0>; }; cpu@1 { device_type = "cpu"; compatible = "arm,cortex-a15"; reg = <0x1>; }; cpu@100 { device_type = "cpu"; compatible = "arm,cortex-a7"; reg = <0x100>; }; cpu@101 { device_type = "cpu"; compatible = "arm,cortex-a7"; reg = <0x101>; }; }; Example 2 (Cortex-A8 uniprocessor 32-bit system): cpus { #size-cells = <0>; #address-cells = <1>; cpu@0 { device_type = "cpu"; compatible = "arm,cortex-a8"; reg = <0x0>; }; }; Example 3 (ARM 926EJ-S uniprocessor 32-bit system): cpus { #size-cells = <0>; #address-cells = <1>; cpu@0 { device_type = "cpu"; compatible = "arm,arm926ej-s"; reg = <0x0>; }; }; Example 4 (ARM Cortex-A57 64-bit system): cpus { #size-cells = <0>; #address-cells = <2>; cpu@0 { device_type = "cpu"; compatible = "arm,cortex-a57"; reg = <0x0 0x0>; enable-method = "spin-table"; cpu-release-addr = <0 0x20000000>; }; cpu@1 { device_type = "cpu"; compatible = "arm,cortex-a57"; reg = <0x0 0x1>; enable-method = "spin-table"; cpu-release-addr = <0 0x20000000>; }; cpu@100 { device_type = "cpu"; compatible = "arm,cortex-a57"; reg = <0x0 0x100>; enable-method = "spin-table"; cpu-release-addr = <0 0x20000000>; }; cpu@101 { device_type = "cpu"; compatible = "arm,cortex-a57"; reg = <0x0 0x101>; enable-method = "spin-table"; cpu-release-addr = <0 0x20000000>; }; cpu@10000 { device_type = "cpu"; compatible = "arm,cortex-a57"; reg = <0x0 0x10000>; enable-method = "spin-table"; cpu-release-addr = <0 0x20000000>; }; cpu@10001 { device_type = "cpu"; compatible = "arm,cortex-a57"; reg = <0x0 0x10001>; enable-method = "spin-table"; cpu-release-addr = <0 0x20000000>; }; cpu@10100 { device_type = "cpu"; compatible = "arm,cortex-a57"; reg = <0x0 0x10100>; enable-method = "spin-table"; cpu-release-addr = <0 0x20000000>; }; cpu@10101 { device_type = "cpu"; compatible = "arm,cortex-a57"; reg = <0x0 0x10101>; enable-method = "spin-table"; cpu-release-addr = <0 0x20000000>; }; cpu@100000000 { device_type = "cpu"; compatible = "arm,cortex-a57"; reg = <0x1 0x0>; enable-method = "spin-table"; cpu-release-addr = <0 0x20000000>; }; cpu@100000001 { device_type = "cpu"; compatible = "arm,cortex-a57"; reg = <0x1 0x1>; enable-method = "spin-table"; cpu-release-addr = <0 0x20000000>; }; cpu@100000100 { device_type = "cpu"; compatible = "arm,cortex-a57"; reg = <0x1 0x100>; enable-method = "spin-table"; cpu-release-addr = <0 0x20000000>; }; cpu@100000101 { device_type = "cpu"; compatible = "arm,cortex-a57"; reg = <0x1 0x101>; enable-method = "spin-table"; cpu-release-addr = <0 0x20000000>; }; cpu@100010000 { device_type = "cpu"; compatible = "arm,cortex-a57"; reg = <0x1 0x10000>; enable-method = "spin-table"; cpu-release-addr = <0 0x20000000>; }; cpu@100010001 { device_type = "cpu"; compatible = "arm,cortex-a57"; reg = <0x1 0x10001>; enable-method = "spin-table"; cpu-release-addr = <0 0x20000000>; }; cpu@100010100 { device_type = "cpu"; compatible = "arm,cortex-a57"; reg = <0x1 0x10100>; enable-method = "spin-table"; cpu-release-addr = <0 0x20000000>; }; cpu@100010101 { device_type = "cpu"; compatible = "arm,cortex-a57"; reg = <0x1 0x10101>; enable-method = "spin-table"; cpu-release-addr = <0 0x20000000>; }; }; -- [1] arm/msm/qcom,saw2.txt [2] arm/msm/qcom,kpss-acc.txt [3] ARM Linux kernel documentation - idle states bindings Documentation/devicetree/bindings/arm/idle-states.txt [4] ARM Linux kernel documentation - cpu capacity bindings Documentation/devicetree/bindings/arm/cpu-capacity.txt