/* * omap_hwmod macros, structures * * Copyright (C) 2009-2011 Nokia Corporation * Copyright (C) 2011-2012 Texas Instruments, Inc. * Paul Walmsley * * Created in collaboration with (alphabetical order): BenoƮt Cousson, * Kevin Hilman, Tony Lindgren, Rajendra Nayak, Vikram Pandita, Sakari * Poussa, Anand Sawant, Santosh Shilimkar, Richard Woodruff * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. * * These headers and macros are used to define OMAP on-chip module * data and their integration with other OMAP modules and Linux. * Copious documentation and references can also be found in the * omap_hwmod code, in arch/arm/mach-omap2/omap_hwmod.c (as of this * writing). * * To do: * - add interconnect error log structures * - init_conn_id_bit (CONNID_BIT_VECTOR) * - implement default hwmod SMS/SDRC flags? * - move Linux-specific data ("non-ROM data") out * */ #ifndef __ARCH_ARM_PLAT_OMAP_INCLUDE_MACH_OMAP_HWMOD_H #define __ARCH_ARM_PLAT_OMAP_INCLUDE_MACH_OMAP_HWMOD_H #include #include #include #include #include struct omap_device; extern struct sysc_regbits omap_hwmod_sysc_type1; extern struct sysc_regbits omap_hwmod_sysc_type2; extern struct sysc_regbits omap_hwmod_sysc_type3; extern struct sysc_regbits omap34xx_sr_sysc_fields; extern struct sysc_regbits omap36xx_sr_sysc_fields; extern struct sysc_regbits omap3_sham_sysc_fields; extern struct sysc_regbits omap3xxx_aes_sysc_fields; extern struct sysc_regbits omap_hwmod_sysc_type_mcasp; extern struct sysc_regbits omap_hwmod_sysc_type_usb_host_fs; /* * OCP SYSCONFIG bit shifts/masks TYPE1. These are for IPs compliant * with the original PRCM protocol defined for OMAP2420 */ #define SYSC_TYPE1_MIDLEMODE_SHIFT 12 #define SYSC_TYPE1_MIDLEMODE_MASK (0x3 << SYSC_TYPE1_MIDLEMODE_SHIFT) #define SYSC_TYPE1_CLOCKACTIVITY_SHIFT 8 #define SYSC_TYPE1_CLOCKACTIVITY_MASK (0x3 << SYSC_TYPE1_CLOCKACTIVITY_SHIFT) #define SYSC_TYPE1_SIDLEMODE_SHIFT 3 #define SYSC_TYPE1_SIDLEMODE_MASK (0x3 << SYSC_TYPE1_SIDLEMODE_SHIFT) #define SYSC_TYPE1_ENAWAKEUP_SHIFT 2 #define SYSC_TYPE1_ENAWAKEUP_MASK (1 << SYSC_TYPE1_ENAWAKEUP_SHIFT) #define SYSC_TYPE1_SOFTRESET_SHIFT 1 #define SYSC_TYPE1_SOFTRESET_MASK (1 << SYSC_TYPE1_SOFTRESET_SHIFT) #define SYSC_TYPE1_AUTOIDLE_SHIFT 0 #define SYSC_TYPE1_AUTOIDLE_MASK (1 << SYSC_TYPE1_AUTOIDLE_SHIFT) /* * OCP SYSCONFIG bit shifts/masks TYPE2. These are for IPs compliant * with the new PRCM protocol defined for new OMAP4 IPs. */ #define SYSC_TYPE2_SOFTRESET_SHIFT 0 #define SYSC_TYPE2_SOFTRESET_MASK (1 << SYSC_TYPE2_SOFTRESET_SHIFT) #define SYSC_TYPE2_SIDLEMODE_SHIFT 2 #define SYSC_TYPE2_SIDLEMODE_MASK (0x3 << SYSC_TYPE2_SIDLEMODE_SHIFT) #define SYSC_TYPE2_MIDLEMODE_SHIFT 4 #define SYSC_TYPE2_MIDLEMODE_MASK (0x3 << SYSC_TYPE2_MIDLEMODE_SHIFT) #define SYSC_TYPE2_DMADISABLE_SHIFT 16 #define SYSC_TYPE2_DMADISABLE_MASK (0x1 << SYSC_TYPE2_DMADISABLE_SHIFT) /* * OCP SYSCONFIG bit shifts/masks TYPE3. * This is applicable for some IPs present in AM33XX */ #define SYSC_TYPE3_SIDLEMODE_SHIFT 0 #define SYSC_TYPE3_SIDLEMODE_MASK (0x3 << SYSC_TYPE3_SIDLEMODE_SHIFT) #define SYSC_TYPE3_MIDLEMODE_SHIFT 2 #define SYSC_TYPE3_MIDLEMODE_MASK (0x3 << SYSC_TYPE3_MIDLEMODE_SHIFT) /* OCP SYSSTATUS bit shifts/masks */ #define SYSS_RESETDONE_SHIFT 0 #define SYSS_RESETDONE_MASK (1 << SYSS_RESETDONE_SHIFT) /* Master standby/slave idle mode flags */ #define HWMOD_IDLEMODE_FORCE (1 << 0) #define HWMOD_IDLEMODE_NO (1 << 1) #define HWMOD_IDLEMODE_SMART (1 << 2) #define HWMOD_IDLEMODE_SMART_WKUP (1 << 3) /* modulemode control type (SW or HW) */ #define MODULEMODE_HWCTRL 1 #define MODULEMODE_SWCTRL 2 #define DEBUG_OMAP2UART1_FLAGS 0 #define DEBUG_OMAP2UART2_FLAGS 0 #define DEBUG_OMAP2UART3_FLAGS 0 #define DEBUG_OMAP3UART3_FLAGS 0 #define DEBUG_OMAP3UART4_FLAGS 0 #define DEBUG_OMAP4UART3_FLAGS 0 #define DEBUG_OMAP4UART4_FLAGS 0 #define DEBUG_TI81XXUART1_FLAGS 0 #define DEBUG_TI81XXUART2_FLAGS 0 #define DEBUG_TI81XXUART3_FLAGS 0 #define DEBUG_AM33XXUART1_FLAGS 0 #define DEBUG_OMAPUART_FLAGS (HWMOD_INIT_NO_IDLE | HWMOD_INIT_NO_RESET) #ifdef CONFIG_OMAP_GPMC_DEBUG #define DEBUG_OMAP_GPMC_HWMOD_FLAGS HWMOD_INIT_NO_RESET #else #define DEBUG_OMAP_GPMC_HWMOD_FLAGS 0 #endif #if defined(CONFIG_DEBUG_OMAP2UART1) #undef DEBUG_OMAP2UART1_FLAGS #define DEBUG_OMAP2UART1_FLAGS DEBUG_OMAPUART_FLAGS #elif defined(CONFIG_DEBUG_OMAP2UART2) #undef DEBUG_OMAP2UART2_FLAGS #define DEBUG_OMAP2UART2_FLAGS DEBUG_OMAPUART_FLAGS #elif defined(CONFIG_DEBUG_OMAP2UART3) #undef DEBUG_OMAP2UART3_FLAGS #define DEBUG_OMAP2UART3_FLAGS DEBUG_OMAPUART_FLAGS #elif defined(CONFIG_DEBUG_OMAP3UART3) #undef DEBUG_OMAP3UART3_FLAGS #define DEBUG_OMAP3UART3_FLAGS DEBUG_OMAPUART_FLAGS #elif defined(CONFIG_DEBUG_OMAP3UART4) #undef DEBUG_OMAP3UART4_FLAGS #define DEBUG_OMAP3UART4_FLAGS DEBUG_OMAPUART_FLAGS #elif defined(CONFIG_DEBUG_OMAP4UART3) #undef DEBUG_OMAP4UART3_FLAGS #define DEBUG_OMAP4UART3_FLAGS DEBUG_OMAPUART_FLAGS #elif defined(CONFIG_DEBUG_OMAP4UART4) #undef DEBUG_OMAP4UART4_FLAGS #define DEBUG_OMAP4UART4_FLAGS DEBUG_OMAPUART_FLAGS #elif defined(CONFIG_DEBUG_TI81XXUART1) #undef DEBUG_TI81XXUART1_FLAGS #define DEBUG_TI81XXUART1_FLAGS DEBUG_OMAPUART_FLAGS #elif defined(CONFIG_DEBUG_TI81XXUART2) #undef DEBUG_TI81XXUART2_FLAGS #define DEBUG_TI81XXUART2_FLAGS DEBUG_OMAPUART_FLAGS #elif defined(CONFIG_DEBUG_TI81XXUART3) #undef DEBUG_TI81XXUART3_FLAGS #define DEBUG_TI81XXUART3_FLAGS DEBUG_OMAPUART_FLAGS #elif defined(CONFIG_DEBUG_AM33XXUART1) #undef DEBUG_AM33XXUART1_FLAGS #define DEBUG_AM33XXUART1_FLAGS DEBUG_OMAPUART_FLAGS #endif /** * struct omap_hwmod_rst_info - IPs reset lines use by hwmod * @name: name of the reset line (module local name) * @rst_shift: Offset of the reset bit * @st_shift: Offset of the reset status bit (OMAP2/3 only) * * @name should be something short, e.g., "cpu0" or "rst". It is defined * locally to the hwmod. */ struct omap_hwmod_rst_info { const char *name; u8 rst_shift; u8 st_shift; }; /** * struct omap_hwmod_opt_clk - optional clocks used by this hwmod * @role: "sys", "32k", "tv", etc -- for use in clk_get() * @clk: opt clock: OMAP clock name * @_clk: pointer to the struct clk (filled in at runtime) * * The module's interface clock and main functional clock should not * be added as optional clocks. */ struct omap_hwmod_opt_clk { const char *role; const char *clk; struct clk *_clk; }; /* omap_hwmod_omap2_firewall.flags bits */ #define OMAP_FIREWALL_L3 (1 << 0) #define OMAP_FIREWALL_L4 (1 << 1) /** * struct omap_hwmod_omap2_firewall - OMAP2/3 device firewall data * @l3_perm_bit: bit shift for L3_PM_*_PERMISSION_* * @l4_fw_region: L4 firewall region ID * @l4_prot_group: L4 protection group ID * @flags: (see omap_hwmod_omap2_firewall.flags macros above) */ struct omap_hwmod_omap2_firewall { u8 l3_perm_bit; u8 l4_fw_region; u8 l4_prot_group; u8 flags; }; /* * omap_hwmod_ocp_if.user bits: these indicate the initiators that use this * interface to interact with the hwmod. Used to add sleep dependencies * when the module is enabled or disabled. */ #define OCP_USER_MPU (1 << 0) #define OCP_USER_SDMA (1 << 1) #define OCP_USER_DSP (1 << 2) #define OCP_USER_IVA (1 << 3) /* omap_hwmod_ocp_if.flags bits */ #define OCPIF_SWSUP_IDLE (1 << 0) #define OCPIF_CAN_BURST (1 << 1) /* omap_hwmod_ocp_if._int_flags possibilities */ #define _OCPIF_INT_FLAGS_REGISTERED (1 << 0) /** * struct omap_hwmod_ocp_if - OCP interface data * @master: struct omap_hwmod that initiates OCP transactions on this link * @slave: struct omap_hwmod that responds to OCP transactions on this link * @addr: address space associated with this link * @clk: interface clock: OMAP clock name * @_clk: pointer to the interface struct clk (filled in at runtime) * @fw: interface firewall data * @width: OCP data width * @user: initiators using this interface (see OCP_USER_* macros above) * @flags: OCP interface flags (see OCPIF_* macros above) * @_int_flags: internal flags (see _OCPIF_INT_FLAGS* macros above) * * It may also be useful to add a tag_cnt field for OCP2.x devices. * * Parameter names beginning with an underscore are managed internally by * the omap_hwmod code and should not be set during initialization. */ struct omap_hwmod_ocp_if { struct omap_hwmod *master; struct omap_hwmod *slave; struct omap_hwmod_addr_space *addr; const char *clk; struct clk *_clk; struct list_head node; union { struct omap_hwmod_omap2_firewall omap2; } fw; u8 width; u8 user; u8 flags; u8 _int_flags; }; /* Macros for use in struct omap_hwmod_sysconfig */ /* Flags for use in omap_hwmod_sysconfig.idlemodes */ #define MASTER_STANDBY_SHIFT 4 #define SLAVE_IDLE_SHIFT 0 #define SIDLE_FORCE (HWMOD_IDLEMODE_FORCE << SLAVE_IDLE_SHIFT) #define SIDLE_NO (HWMOD_IDLEMODE_NO << SLAVE_IDLE_SHIFT) #define SIDLE_SMART (HWMOD_IDLEMODE_SMART << SLAVE_IDLE_SHIFT) #define SIDLE_SMART_WKUP (HWMOD_IDLEMODE_SMART_WKUP << SLAVE_IDLE_SHIFT) #define MSTANDBY_FORCE (HWMOD_IDLEMODE_FORCE << MASTER_STANDBY_SHIFT) #define MSTANDBY_NO (HWMOD_IDLEMODE_NO << MASTER_STANDBY_SHIFT) #define MSTANDBY_SMART (HWMOD_IDLEMODE_SMART << MASTER_STANDBY_SHIFT) #define MSTANDBY_SMART_WKUP (HWMOD_IDLEMODE_SMART_WKUP << MASTER_STANDBY_SHIFT) /* omap_hwmod_sysconfig.sysc_flags capability flags */ #define SYSC_HAS_AUTOIDLE (1 << 0) #define SYSC_HAS_SOFTRESET (1 << 1) #define SYSC_HAS_ENAWAKEUP (1 << 2) #define SYSC_HAS_EMUFREE (1 << 3) #define SYSC_HAS_CLOCKACTIVITY (1 << 4) #define SYSC_HAS_SIDLEMODE (1 << 5) #define SYSC_HAS_MIDLEMODE (1 << 6) #define SYSS_HAS_RESET_STATUS (1 << 7) #define SYSC_NO_CACHE (1 << 8) /* XXX SW flag, belongs elsewhere */ #define SYSC_HAS_RESET_STATUS (1 << 9) #define SYSC_HAS_DMADISABLE (1 << 10) /* omap_hwmod_sysconfig.clockact flags */ #define CLOCKACT_TEST_BOTH 0x0 #define CLOCKACT_TEST_MAIN 0x1 #define CLOCKACT_TEST_ICLK 0x2 #define CLOCKACT_TEST_NONE 0x3 /** * struct omap_hwmod_class_sysconfig - hwmod class OCP_SYS* data * @rev_offs: IP block revision register offset (from module base addr) * @sysc_offs: OCP_SYSCONFIG register offset (from module base addr) * @syss_offs: OCP_SYSSTATUS register offset (from module base addr) * @srst_udelay: Delay needed after doing a softreset in usecs * @idlemodes: One or more of {SIDLE,MSTANDBY}_{OFF,FORCE,SMART} * @sysc_flags: SYS{C,S}_HAS* flags indicating SYSCONFIG bits supported * @clockact: the default value of the module CLOCKACTIVITY bits * * @clockact describes to the module which clocks are likely to be * disabled when the PRCM issues its idle request to the module. Some * modules have separate clockdomains for the interface clock and main * functional clock, and can check whether they should acknowledge the * idle request based on the internal module functionality that has * been associated with the clocks marked in @clockact. This field is * only used if HWMOD_SET_DEFAULT_CLOCKACT is set (see below) * * @sysc_fields: structure containing the offset positions of various bits in * SYSCONFIG register. This can be populated using omap_hwmod_sysc_type1 or * omap_hwmod_sysc_type2 defined in omap_hwmod_common_data.c depending on * whether the device ip is compliant with the original PRCM protocol * defined for OMAP2420 or the new PRCM protocol for new OMAP4 IPs. * If the device follows a different scheme for the sysconfig register , * then this field has to be populated with the correct offset structure. */ struct omap_hwmod_class_sysconfig { s32 rev_offs; s32 sysc_offs; s32 syss_offs; u16 sysc_flags; struct sysc_regbits *sysc_fields; u8 srst_udelay; u8 idlemodes; }; /** * struct omap_hwmod_omap2_prcm - OMAP2/3-specific PRCM data * @module_offs: PRCM submodule offset from the start of the PRM/CM * @idlest_reg_id: IDLEST register ID (e.g., 3 for CM_IDLEST3) * @idlest_idle_bit: register bit shift for CM_IDLEST slave idle bit * * @prcm_reg_id and @module_bit are specific to the AUTOIDLE, WKST, * WKEN, GRPSEL registers. In an ideal world, no extra information * would be needed for IDLEST information, but alas, there are some * exceptions, so @idlest_reg_id, @idlest_idle_bit, @idlest_stdby_bit * are needed for the IDLEST registers (c.f. 2430 I2CHS, 3430 USBHOST) */ struct omap_hwmod_omap2_prcm { s16 module_offs; u8 idlest_reg_id; u8 idlest_idle_bit; }; /* * Possible values for struct omap_hwmod_omap4_prcm.flags * * HWMOD_OMAP4_NO_CONTEXT_LOSS_BIT: Some IP blocks don't have a PRCM * module-level context loss register associated with them; this * flag bit should be set in those cases * HWMOD_OMAP4_ZERO_CLKCTRL_OFFSET: Some IP blocks have a valid CLKCTRL * offset of zero; this flag bit should be set in those cases to * distinguish from hwmods that have no clkctrl offset. * HWMOD_OMAP4_CLKFWK_CLKCTR_CLOCK: Module clockctrl clock is managed * by the common clock framework and not hwmod. */ #define HWMOD_OMAP4_NO_CONTEXT_LOSS_BIT (1 << 0) #define HWMOD_OMAP4_ZERO_CLKCTRL_OFFSET (1 << 1) #define HWMOD_OMAP4_CLKFWK_CLKCTR_CLOCK (1 << 2) /** * struct omap_hwmod_omap4_prcm - OMAP4-specific PRCM data * @clkctrl_offs: offset of the PRCM clock control register * @rstctrl_offs: offset of the XXX_RSTCTRL register located in the PRM * @context_offs: offset of the RM_*_CONTEXT register * @lostcontext_mask: bitmask for selecting bits from RM_*_CONTEXT register * @rstst_reg: (AM33XX only) address of the XXX_RSTST register in the PRM * @submodule_wkdep_bit: bit shift of the WKDEP range * @flags: PRCM register capabilities for this IP block * @modulemode: allowable modulemodes * @context_lost_counter: Count of module level context lost * * If @lostcontext_mask is not defined, context loss check code uses * whole register without masking. @lostcontext_mask should only be * defined in cases where @context_offs register is shared by two or * more hwmods. */ struct omap_hwmod_omap4_prcm { u16 clkctrl_offs; u16 rstctrl_offs; u16 rstst_offs; u16 context_offs; u32 lostcontext_mask; u8 submodule_wkdep_bit; u8 modulemode; u8 flags; int context_lost_counter; }; /* * omap_hwmod.flags definitions * * HWMOD_SWSUP_SIDLE: omap_hwmod code should manually bring module in and out * of idle, rather than relying on module smart-idle * HWMOD_SWSUP_MSTANDBY: omap_hwmod code should manually bring module in and * out of standby, rather than relying on module smart-standby * HWMOD_INIT_NO_RESET: don't reset this module at boot - important for * SDRAM controller, etc. XXX probably belongs outside the main hwmod file * XXX Should be HWMOD_SETUP_NO_RESET * HWMOD_INIT_NO_IDLE: don't idle this module at boot - important for SDRAM * controller, etc. XXX probably belongs outside the main hwmod file * XXX Should be HWMOD_SETUP_NO_IDLE * HWMOD_NO_OCP_AUTOIDLE: disable module autoidle (OCP_SYSCONFIG.AUTOIDLE) * when module is enabled, rather than the default, which is to * enable autoidle * HWMOD_SET_DEFAULT_CLOCKACT: program CLOCKACTIVITY bits at startup * HWMOD_NO_IDLEST: this module does not have idle status - this is the case * only for few initiator modules on OMAP2 & 3. * HWMOD_CONTROL_OPT_CLKS_IN_RESET: Enable all optional clocks during reset. * This is needed for devices like DSS that require optional clocks enabled * in order to complete the reset. Optional clocks will be disabled * again after the reset. * HWMOD_16BIT_REG: Module has 16bit registers * HWMOD_EXT_OPT_MAIN_CLK: The only main functional clock source for * this IP block comes from an off-chip source and is not always * enabled. This prevents the hwmod code from being able to * enable and reset the IP block early. XXX Eventually it should * be possible to query the clock framework for this information. * HWMOD_BLOCK_WFI: Some OMAP peripherals apparently don't work * correctly if the MPU is allowed to go idle while the * peripherals are active. This is apparently true for the I2C on * OMAP2420, and also the EMAC on AM3517/3505. It's unlikely that * this is really true -- we're probably not configuring something * correctly, or this is being abused to deal with some PM latency * issues -- but we're currently suffering from a shortage of * folks who are able to track these issues down properly. * HWMOD_FORCE_MSTANDBY: Always keep MIDLEMODE bits cleared so that device * is kept in force-standby mode. Failing to do so causes PM problems * with musb on OMAP3630 at least. Note that musb has a dedicated register * to control MSTANDBY signal when MIDLEMODE is set to force-standby. * HWMOD_SWSUP_SIDLE_ACT: omap_hwmod code should manually bring the module * out of idle, but rely on smart-idle to the put it back in idle, * so the wakeups are still functional (Only known case for now is UART) * HWMOD_RECONFIG_IO_CHAIN: omap_hwmod code needs to reconfigure wake-up * events by calling _reconfigure_io_chain() when a device is enabled * or idled. * HWMOD_OPT_CLKS_NEEDED: The optional clocks are needed for the module to * operate and they need to be handled at the same time as the main_clk. * HWMOD_NO_IDLE: Do not idle the hwmod at all. Useful to handle certain * IPs like CPSW on DRA7, where clocks to this module cannot be disabled. * HWMOD_CLKDM_NOAUTO: Allows the hwmod's clockdomain to be prevented from * entering HW_AUTO while hwmod is active. This is needed to workaround * some modules which don't function correctly with HW_AUTO. For example, * DCAN on DRA7x SoC needs this to workaround errata i893. */ #define HWMOD_SWSUP_SIDLE (1 << 0) #define HWMOD_SWSUP_MSTANDBY (1 << 1) #define HWMOD_INIT_NO_RESET (1 << 2) #define HWMOD_INIT_NO_IDLE (1 << 3) #define HWMOD_NO_OCP_AUTOIDLE (1 << 4) #define HWMOD_SET_DEFAULT_CLOCKACT (1 << 5) #define HWMOD_NO_IDLEST (1 << 6) #define HWMOD_CONTROL_OPT_CLKS_IN_RESET (1 << 7) #define HWMOD_16BIT_REG (1 << 8) #define HWMOD_EXT_OPT_MAIN_CLK (1 << 9) #define HWMOD_BLOCK_WFI (1 << 10) #define HWMOD_FORCE_MSTANDBY (1 << 11) #define HWMOD_SWSUP_SIDLE_ACT (1 << 12) #define HWMOD_RECONFIG_IO_CHAIN (1 << 13) #define HWMOD_OPT_CLKS_NEEDED (1 << 14) #define HWMOD_NO_IDLE (1 << 15) #define HWMOD_CLKDM_NOAUTO (1 << 16) /* * omap_hwmod._int_flags definitions * These are for internal use only and are managed by the omap_hwmod code. * * _HWMOD_NO_MPU_PORT: no path exists for the MPU to write to this module * _HWMOD_SYSCONFIG_LOADED: set when the OCP_SYSCONFIG value has been cached * _HWMOD_SKIP_ENABLE: set if hwmod enabled during init (HWMOD_INIT_NO_IDLE) - * causes the first call to _enable() to only update the pinmux */ #define _HWMOD_NO_MPU_PORT (1 << 0) #define _HWMOD_SYSCONFIG_LOADED (1 << 1) #define _HWMOD_SKIP_ENABLE (1 << 2) /* * omap_hwmod._state definitions * * INITIALIZED: reset (optionally), initialized, enabled, disabled * (optionally) * * */ #define _HWMOD_STATE_UNKNOWN 0 #define _HWMOD_STATE_REGISTERED 1 #define _HWMOD_STATE_CLKS_INITED 2 #define _HWMOD_STATE_INITIALIZED 3 #define _HWMOD_STATE_ENABLED 4 #define _HWMOD_STATE_IDLE 5 #define _HWMOD_STATE_DISABLED 6 /** * struct omap_hwmod_class - the type of an IP block * @name: name of the hwmod_class * @sysc: device SYSCONFIG/SYSSTATUS register data * @rev: revision of the IP class * @pre_shutdown: ptr to fn to be executed immediately prior to device shutdown * @reset: ptr to fn to be executed in place of the standard hwmod reset fn * @enable_preprogram: ptr to fn to be executed during device enable * @lock: ptr to fn to be executed to lock IP registers * @unlock: ptr to fn to be executed to unlock IP registers * * Represent the class of a OMAP hardware "modules" (e.g. timer, * smartreflex, gpio, uart...) * * @pre_shutdown is a function that will be run immediately before * hwmod clocks are disabled, etc. It is intended for use for hwmods * like the MPU watchdog, which cannot be disabled with the standard * omap_hwmod_shutdown(). The function should return 0 upon success, * or some negative error upon failure. Returning an error will cause * omap_hwmod_shutdown() to abort the device shutdown and return an * error. * * If @reset is defined, then the function it points to will be * executed in place of the standard hwmod _reset() code in * mach-omap2/omap_hwmod.c. This is needed for IP blocks which have * unusual reset sequences - usually processor IP blocks like the IVA. */ struct omap_hwmod_class { const char *name; struct omap_hwmod_class_sysconfig *sysc; u32 rev; int (*pre_shutdown)(struct omap_hwmod *oh); int (*reset)(struct omap_hwmod *oh); int (*enable_preprogram)(struct omap_hwmod *oh); void (*lock)(struct omap_hwmod *oh); void (*unlock)(struct omap_hwmod *oh); }; /** * struct omap_hwmod - integration data for OMAP hardware "modules" (IP blocks) * @name: name of the hwmod * @class: struct omap_hwmod_class * to the class of this hwmod * @od: struct omap_device currently associated with this hwmod (internal use) * @prcm: PRCM data pertaining to this hwmod * @main_clk: main clock: OMAP clock name * @_clk: pointer to the main struct clk (filled in at runtime) * @opt_clks: other device clocks that drivers can request (0..*) * @voltdm: pointer to voltage domain (filled in at runtime) * @dev_attr: arbitrary device attributes that can be passed to the driver * @_sysc_cache: internal-use hwmod flags * @mpu_rt_idx: index of device address space for register target (for DT boot) * @_mpu_rt_va: cached register target start address (internal use) * @_mpu_port: cached MPU register target slave (internal use) * @opt_clks_cnt: number of @opt_clks * @master_cnt: number of @master entries * @slaves_cnt: number of @slave entries * @response_lat: device OCP response latency (in interface clock cycles) * @_int_flags: internal-use hwmod flags * @_state: internal-use hwmod state * @_postsetup_state: internal-use state to leave the hwmod in after _setup() * @flags: hwmod flags (documented below) * @_lock: spinlock serializing operations on this hwmod * @node: list node for hwmod list (internal use) * @parent_hwmod: (temporary) a pointer to the hierarchical parent of this hwmod * * @main_clk refers to this module's "main clock," which for our * purposes is defined as "the functional clock needed for register * accesses to complete." Modules may not have a main clock if the * interface clock also serves as a main clock. * * Parameter names beginning with an underscore are managed internally by * the omap_hwmod code and should not be set during initialization. * * @masters and @slaves are now deprecated. * * @parent_hwmod is temporary; there should be no need for it, as this * information should already be expressed in the OCP interface * structures. @parent_hwmod is present as a workaround until we improve * handling for hwmods with multiple parents (e.g., OMAP4+ DSS with * multiple register targets across different interconnects). */ struct omap_hwmod { const char *name; struct omap_hwmod_class *class; struct omap_device *od; struct omap_hwmod_rst_info *rst_lines; union { struct omap_hwmod_omap2_prcm omap2; struct omap_hwmod_omap4_prcm omap4; } prcm; const char *main_clk; struct clk *_clk; struct omap_hwmod_opt_clk *opt_clks; const char *clkdm_name; struct clockdomain *clkdm; struct list_head slave_ports; /* connect to *_TA */ void *dev_attr; u32 _sysc_cache; void __iomem *_mpu_rt_va; spinlock_t _lock; struct lock_class_key hwmod_key; /* unique lock class */ struct list_head node; struct omap_hwmod_ocp_if *_mpu_port; u32 flags; u8 mpu_rt_idx; u8 response_lat; u8 rst_lines_cnt; u8 opt_clks_cnt; u8 slaves_cnt; u8 hwmods_cnt; u8 _int_flags; u8 _state; u8 _postsetup_state; struct omap_hwmod *parent_hwmod; }; struct device_node; struct omap_hwmod *omap_hwmod_lookup(const char *name); int omap_hwmod_for_each(int (*fn)(struct omap_hwmod *oh, void *data), void *data); int __init omap_hwmod_setup_one(const char *name); int omap_hwmod_parse_module_range(struct omap_hwmod *oh, struct device_node *np, struct resource *res); struct ti_sysc_module_data; struct ti_sysc_cookie; int omap_hwmod_init_module(struct device *dev, const struct ti_sysc_module_data *data, struct ti_sysc_cookie *cookie); int omap_hwmod_enable(struct omap_hwmod *oh); int omap_hwmod_idle(struct omap_hwmod *oh); int omap_hwmod_shutdown(struct omap_hwmod *oh); int omap_hwmod_assert_hardreset(struct omap_hwmod *oh, const char *name); int omap_hwmod_deassert_hardreset(struct omap_hwmod *oh, const char *name); void omap_hwmod_write(u32 v, struct omap_hwmod *oh, u16 reg_offs); u32 omap_hwmod_read(struct omap_hwmod *oh, u16 reg_offs); int omap_hwmod_softreset(struct omap_hwmod *oh); int omap_hwmod_count_resources(struct omap_hwmod *oh, unsigned long flags); int omap_hwmod_fill_resources(struct omap_hwmod *oh, struct resource *res); int omap_hwmod_get_resource_byname(struct omap_hwmod *oh, unsigned int type, const char *name, struct resource *res); struct powerdomain *omap_hwmod_get_pwrdm(struct omap_hwmod *oh); void __iomem *omap_hwmod_get_mpu_rt_va(struct omap_hwmod *oh); int omap_hwmod_enable_wakeup(struct omap_hwmod *oh); int omap_hwmod_disable_wakeup(struct omap_hwmod *oh); int omap_hwmod_for_each_by_class(const char *classname, int (*fn)(struct omap_hwmod *oh, void *user), void *user); int omap_hwmod_set_postsetup_state(struct omap_hwmod *oh, u8 state); int omap_hwmod_get_context_loss_count(struct omap_hwmod *oh); extern void __init omap_hwmod_init(void); const char *omap_hwmod_get_main_clk(struct omap_hwmod *oh); /* * */ extern int omap_hwmod_aess_preprogram(struct omap_hwmod *oh); void omap_hwmod_rtc_unlock(struct omap_hwmod *oh); void omap_hwmod_rtc_lock(struct omap_hwmod *oh); /* * Chip variant-specific hwmod init routines - XXX should be converted * to use initcalls once the initial boot ordering is straightened out */ extern int omap2420_hwmod_init(void); extern int omap2430_hwmod_init(void); extern int omap3xxx_hwmod_init(void); extern int omap44xx_hwmod_init(void); extern int omap54xx_hwmod_init(void); extern int am33xx_hwmod_init(void); extern int dm814x_hwmod_init(void); extern int dm816x_hwmod_init(void); extern int dra7xx_hwmod_init(void); int am43xx_hwmod_init(void); extern int __init omap_hwmod_register_links(struct omap_hwmod_ocp_if **ois); #endif