// SPDX-License-Identifier: GPL-2.0 /* * AM33XX Arch Power Management Routines * * Copyright (C) 2016-2018 Texas Instruments Incorporated - http://www.ti.com/ * Dave Gerlach */ #include #include #include #include #include "cm33xx.h" #include "common.h" #include "control.h" #include "clockdomain.h" #include "iomap.h" #include "omap_hwmod.h" #include "pm.h" #include "powerdomain.h" #include "prm33xx.h" #include "soc.h" #include "sram.h" static struct powerdomain *cefuse_pwrdm, *gfx_pwrdm, *per_pwrdm, *mpu_pwrdm; static struct clockdomain *gfx_l4ls_clkdm; static void __iomem *scu_base; static int __init am43xx_map_scu(void) { scu_base = ioremap(scu_a9_get_base(), SZ_256); if (!scu_base) return -ENOMEM; return 0; } static int amx3_common_init(void) { gfx_pwrdm = pwrdm_lookup("gfx_pwrdm"); per_pwrdm = pwrdm_lookup("per_pwrdm"); mpu_pwrdm = pwrdm_lookup("mpu_pwrdm"); if ((!gfx_pwrdm) || (!per_pwrdm) || (!mpu_pwrdm)) return -ENODEV; (void)clkdm_for_each(omap_pm_clkdms_setup, NULL); /* CEFUSE domain can be turned off post bootup */ cefuse_pwrdm = pwrdm_lookup("cefuse_pwrdm"); if (cefuse_pwrdm) omap_set_pwrdm_state(cefuse_pwrdm, PWRDM_POWER_OFF); else pr_err("PM: Failed to get cefuse_pwrdm\n"); return 0; } static int am33xx_suspend_init(void) { int ret; gfx_l4ls_clkdm = clkdm_lookup("gfx_l4ls_gfx_clkdm"); if (!gfx_l4ls_clkdm) { pr_err("PM: Cannot lookup gfx_l4ls_clkdm clockdomains\n"); return -ENODEV; } ret = amx3_common_init(); return ret; } static int am43xx_suspend_init(void) { int ret = 0; ret = am43xx_map_scu(); if (ret) { pr_err("PM: Could not ioremap SCU\n"); return ret; } ret = amx3_common_init(); return ret; } static void amx3_pre_suspend_common(void) { omap_set_pwrdm_state(gfx_pwrdm, PWRDM_POWER_OFF); } static void amx3_post_suspend_common(void) { int status; /* * Because gfx_pwrdm is the only one under MPU control, * comment on transition status */ status = pwrdm_read_pwrst(gfx_pwrdm); if (status != PWRDM_POWER_OFF) pr_err("PM: GFX domain did not transition: %x\n", status); } static int am33xx_suspend(unsigned int state, int (*fn)(unsigned long)) { int ret = 0; amx3_pre_suspend_common(); ret = cpu_suspend(0, fn); amx3_post_suspend_common(); /* * BUG: GFX_L4LS clock domain needs to be woken up to * ensure thet L4LS clock domain does not get stuck in * transition. If that happens L3 module does not get * disabled, thereby leading to PER power domain * transition failing */ clkdm_wakeup(gfx_l4ls_clkdm); clkdm_sleep(gfx_l4ls_clkdm); return ret; } static int am43xx_suspend(unsigned int state, int (*fn)(unsigned long)) { int ret = 0; amx3_pre_suspend_common(); scu_power_mode(scu_base, SCU_PM_POWEROFF); ret = cpu_suspend(0, fn); scu_power_mode(scu_base, SCU_PM_NORMAL); amx3_post_suspend_common(); return ret; } static struct am33xx_pm_sram_addr *amx3_get_sram_addrs(void) { if (soc_is_am33xx()) return &am33xx_pm_sram; else if (soc_is_am437x()) return &am43xx_pm_sram; else return NULL; } static struct am33xx_pm_platform_data am33xx_ops = { .init = am33xx_suspend_init, .soc_suspend = am33xx_suspend, .get_sram_addrs = amx3_get_sram_addrs, }; static struct am33xx_pm_platform_data am43xx_ops = { .init = am43xx_suspend_init, .soc_suspend = am43xx_suspend, .get_sram_addrs = amx3_get_sram_addrs, }; static struct am33xx_pm_platform_data *am33xx_pm_get_pdata(void) { if (soc_is_am33xx()) return &am33xx_ops; else if (soc_is_am437x()) return &am43xx_ops; else return NULL; } int __init amx3_common_pm_init(void) { struct am33xx_pm_platform_data *pdata; struct platform_device_info devinfo; pdata = am33xx_pm_get_pdata(); memset(&devinfo, 0, sizeof(devinfo)); devinfo.name = "pm33xx"; devinfo.data = pdata; devinfo.size_data = sizeof(*pdata); devinfo.id = -1; platform_device_register_full(&devinfo); return 0; }