#ifndef __ARCH_ARM_MACH_OMAP2_SDRC_H #define __ARCH_ARM_MACH_OMAP2_SDRC_H /* * OMAP2/3 SDRC/SMS macros and prototypes * * Copyright (C) 2007-2008, 2012 Texas Instruments, Inc. * Copyright (C) 2007-2008 Nokia Corporation * * Paul Walmsley * Tony Lindgren * Richard Woodruff * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. */ #undef DEBUG #ifndef __ASSEMBLER__ #include extern void __iomem *omap2_sdrc_base; extern void __iomem *omap2_sms_base; #define OMAP_SDRC_REGADDR(reg) (omap2_sdrc_base + (reg)) #define OMAP_SMS_REGADDR(reg) (omap2_sms_base + (reg)) /* SDRC global register get/set */ static inline void sdrc_write_reg(u32 val, u16 reg) { writel_relaxed(val, OMAP_SDRC_REGADDR(reg)); } static inline u32 sdrc_read_reg(u16 reg) { return readl_relaxed(OMAP_SDRC_REGADDR(reg)); } /* SMS global register get/set */ static inline void sms_write_reg(u32 val, u16 reg) { writel_relaxed(val, OMAP_SMS_REGADDR(reg)); } static inline u32 sms_read_reg(u16 reg) { return readl_relaxed(OMAP_SMS_REGADDR(reg)); } extern void omap2_set_globals_sdrc(void __iomem *sdrc, void __iomem *sms); /** * struct omap_sdrc_params - SDRC parameters for a given SDRC clock rate * @rate: SDRC clock rate (in Hz) * @actim_ctrla: Value to program to SDRC_ACTIM_CTRLA for this rate * @actim_ctrlb: Value to program to SDRC_ACTIM_CTRLB for this rate * @rfr_ctrl: Value to program to SDRC_RFR_CTRL for this rate * @mr: Value to program to SDRC_MR for this rate * * This structure holds a pre-computed set of register values for the * SDRC for a given SDRC clock rate and SDRAM chip. These are * intended to be pre-computed and specified in an array in the board-*.c * files. The structure is keyed off the 'rate' field. */ struct omap_sdrc_params { unsigned long rate; u32 actim_ctrla; u32 actim_ctrlb; u32 rfr_ctrl; u32 mr; }; #ifdef CONFIG_SOC_HAS_OMAP2_SDRC void omap2_sdrc_init(struct omap_sdrc_params *sdrc_cs0, struct omap_sdrc_params *sdrc_cs1); #else static inline void __init omap2_sdrc_init(struct omap_sdrc_params *sdrc_cs0, struct omap_sdrc_params *sdrc_cs1) {}; #endif int omap2_sdrc_get_params(unsigned long r, struct omap_sdrc_params **sdrc_cs0, struct omap_sdrc_params **sdrc_cs1); void omap2_sms_save_context(void); void omap2_sms_restore_context(void); struct memory_timings { u32 m_type; /* ddr = 1, sdr = 0 */ u32 dll_mode; /* use lock mode = 1, unlock mode = 0 */ u32 slow_dll_ctrl; /* unlock mode, dll value for slow speed */ u32 fast_dll_ctrl; /* unlock mode, dll value for fast speed */ u32 base_cs; /* base chip select to use for calculations */ }; extern void omap2xxx_sdrc_init_params(u32 force_lock_to_unlock_mode); struct omap_sdrc_params *rx51_get_sdram_timings(void); u32 omap2xxx_sdrc_dll_is_unlocked(void); u32 omap2xxx_sdrc_reprogram(u32 level, u32 force); #else #define OMAP242X_SDRC_REGADDR(reg) \ OMAP2_L3_IO_ADDRESS(OMAP2420_SDRC_BASE + (reg)) #define OMAP243X_SDRC_REGADDR(reg) \ OMAP2_L3_IO_ADDRESS(OMAP243X_SDRC_BASE + (reg)) #define OMAP34XX_SDRC_REGADDR(reg) \ OMAP2_L3_IO_ADDRESS(OMAP343X_SDRC_BASE + (reg)) #endif /* __ASSEMBLER__ */ /* Minimum frequency that the SDRC DLL can lock at */ #define MIN_SDRC_DLL_LOCK_FREQ 83000000 /* Scale factor for fixed-point arith in omap3_core_dpll_m2_set_rate() */ #define SDRC_MPURATE_SCALE 8 /* 2^SDRC_MPURATE_BASE_SHIFT: MPU MHz that SDRC_MPURATE_LOOPS is defined for */ #define SDRC_MPURATE_BASE_SHIFT 9 /* * SDRC_MPURATE_LOOPS: Number of MPU loops to execute at * 2^MPURATE_BASE_SHIFT MHz for SDRC to stabilize */ #define SDRC_MPURATE_LOOPS 96 /* SDRC register offsets - read/write with sdrc_{read,write}_reg() */ #define SDRC_SYSCONFIG 0x010 #define SDRC_CS_CFG 0x040 #define SDRC_SHARING 0x044 #define SDRC_ERR_TYPE 0x04C #define SDRC_DLLA_CTRL 0x060 #define SDRC_DLLA_STATUS 0x064 #define SDRC_DLLB_CTRL 0x068 #define SDRC_DLLB_STATUS 0x06C #define SDRC_POWER 0x070 #define SDRC_MCFG_0 0x080 #define SDRC_MR_0 0x084 #define SDRC_EMR2_0 0x08c #define SDRC_ACTIM_CTRL_A_0 0x09c #define SDRC_ACTIM_CTRL_B_0 0x0a0 #define SDRC_RFR_CTRL_0 0x0a4 #define SDRC_MANUAL_0 0x0a8 #define SDRC_MCFG_1 0x0B0 #define SDRC_MR_1 0x0B4 #define SDRC_EMR2_1 0x0BC #define SDRC_ACTIM_CTRL_A_1 0x0C4 #define SDRC_ACTIM_CTRL_B_1 0x0C8 #define SDRC_RFR_CTRL_1 0x0D4 #define SDRC_MANUAL_1 0x0D8 #define SDRC_POWER_AUTOCOUNT_SHIFT 8 #define SDRC_POWER_AUTOCOUNT_MASK (0xffff << SDRC_POWER_AUTOCOUNT_SHIFT) #define SDRC_POWER_CLKCTRL_SHIFT 4 #define SDRC_POWER_CLKCTRL_MASK (0x3 << SDRC_POWER_CLKCTRL_SHIFT) #define SDRC_SELF_REFRESH_ON_AUTOCOUNT (0x2 << SDRC_POWER_CLKCTRL_SHIFT) /* * These values represent the number of memory clock cycles between * autorefresh initiation. They assume 1 refresh per 64 ms (JEDEC), 8192 * rows per device, and include a subtraction of a 50 cycle window in the * event that the autorefresh command is delayed due to other SDRC activity. * The '| 1' sets the ARE field to send one autorefresh when the autorefresh * counter reaches 0. * * These represent optimal values for common parts, it won't work for all. * As long as you scale down, most parameters are still work, they just * become sub-optimal. The RFR value goes in the opposite direction. If you * don't adjust it down as your clock period increases the refresh interval * will not be met. Setting all parameters for complete worst case may work, * but may cut memory performance by 2x. Due to errata the DLLs need to be * unlocked and their value needs run time calibration. A dynamic call is * need for that as no single right value exists across production samples. * * Only the FULL speed values are given. Current code is such that rate * changes must be made at DPLLoutx2. The actual value adjustment for low * frequency operation will be handled by omap_set_performance() * * By having the boot loader boot up in the fastest L4 speed available likely * will result in something which you can switch between. */ #define SDRC_RFR_CTRL_165MHz (0x00044c00 | 1) #define SDRC_RFR_CTRL_133MHz (0x0003de00 | 1) #define SDRC_RFR_CTRL_100MHz (0x0002da01 | 1) #define SDRC_RFR_CTRL_110MHz (0x0002da01 | 1) /* Need to calc */ #define SDRC_RFR_CTRL_BYPASS (0x00005000 | 1) /* Need to calc */ /* * SMS register access */ #define OMAP242X_SMS_REGADDR(reg) \ (void __iomem *)OMAP2_L3_IO_ADDRESS(OMAP2420_SMS_BASE + reg) #define OMAP243X_SMS_REGADDR(reg) \ (void __iomem *)OMAP2_L3_IO_ADDRESS(OMAP243X_SMS_BASE + reg) #define OMAP343X_SMS_REGADDR(reg) \ (void __iomem *)OMAP2_L3_IO_ADDRESS(OMAP343X_SMS_BASE + reg) /* SMS register offsets - read/write with sms_{read,write}_reg() */ #define SMS_SYSCONFIG 0x010 /* REVISIT: fill in other SMS registers here */ #endif