# # arch/arm64/Makefile # # This file is included by the global makefile so that you can add your own # architecture-specific flags and dependencies. # # This file is subject to the terms and conditions of the GNU General Public # License. See the file "COPYING" in the main directory of this archive # for more details. # # Copyright (C) 1995-2001 by Russell King LDFLAGS_vmlinux :=--no-undefined -X CPPFLAGS_vmlinux.lds = -DTEXT_OFFSET=$(TEXT_OFFSET) GZFLAGS :=-9 ifeq ($(CONFIG_RELOCATABLE), y) # Pass --no-apply-dynamic-relocs to restore pre-binutils-2.27 behaviour # for relative relocs, since this leads to better Image compression # with the relocation offsets always being zero. LDFLAGS_vmlinux += -pie -shared -Bsymbolic \ $(call ld-option, --no-apply-dynamic-relocs) endif ifeq ($(CONFIG_ARM64_ERRATUM_843419),y) ifeq ($(call ld-option, --fix-cortex-a53-843419),) $(warning ld does not support --fix-cortex-a53-843419; kernel may be susceptible to erratum) else LDFLAGS_vmlinux += --fix-cortex-a53-843419 endif endif KBUILD_DEFCONFIG := defconfig # Check for binutils support for specific extensions lseinstr := $(call as-instr,.arch_extension lse,-DCONFIG_AS_LSE=1) ifeq ($(CONFIG_ARM64_LSE_ATOMICS), y) ifeq ($(lseinstr),) $(warning LSE atomics not supported by binutils) endif endif ifeq ($(CONFIG_ARM64), y) brokengasinst := $(call as-instr,1:\n.inst 0\n.rept . - 1b\n\nnop\n.endr\n,,-DCONFIG_BROKEN_GAS_INST=1) ifneq ($(brokengasinst),) $(warning Detected assembler with broken .inst; disassembly will be unreliable) endif endif KBUILD_CFLAGS += -mgeneral-regs-only $(lseinstr) $(brokengasinst) KBUILD_CFLAGS += -fno-asynchronous-unwind-tables KBUILD_AFLAGS += $(lseinstr) $(brokengasinst) KBUILD_CFLAGS += $(call cc-option,-mabi=lp64) KBUILD_AFLAGS += $(call cc-option,-mabi=lp64) ifeq ($(CONFIG_CPU_BIG_ENDIAN), y) KBUILD_CPPFLAGS += -mbig-endian CHECKFLAGS += -D__AARCH64EB__ AS += -EB # Prefer the baremetal ELF build target, but not all toolchains include # it so fall back to the standard linux version if needed. KBUILD_LDFLAGS += -EB $(call ld-option, -maarch64elfb, -maarch64linuxb) UTS_MACHINE := aarch64_be else KBUILD_CPPFLAGS += -mlittle-endian CHECKFLAGS += -D__AARCH64EL__ AS += -EL # Same as above, prefer ELF but fall back to linux target if needed. KBUILD_LDFLAGS += -EL $(call ld-option, -maarch64elf, -maarch64linux) UTS_MACHINE := aarch64 endif CHECKFLAGS += -D__aarch64__ ifeq ($(CONFIG_ARM64_MODULE_PLTS),y) KBUILD_LDFLAGS_MODULE += -T $(srctree)/arch/arm64/kernel/module.lds endif # Default value head-y := arch/arm64/kernel/head.o # The byte offset of the kernel image in RAM from the start of RAM. ifeq ($(CONFIG_ARM64_RANDOMIZE_TEXT_OFFSET), y) TEXT_OFFSET := $(shell awk "BEGIN {srand(); printf \"0x%06x\n\", \ int(2 * 1024 * 1024 / (2 ^ $(CONFIG_ARM64_PAGE_SHIFT)) * \ rand()) * (2 ^ $(CONFIG_ARM64_PAGE_SHIFT))}") else TEXT_OFFSET := 0x00080000 endif # KASAN_SHADOW_OFFSET = VA_START + (1 << (VA_BITS - KASAN_SHADOW_SCALE_SHIFT)) # - (1 << (64 - KASAN_SHADOW_SCALE_SHIFT)) # in 32-bit arithmetic KASAN_SHADOW_SCALE_SHIFT := 3 KASAN_SHADOW_OFFSET := $(shell printf "0x%08x00000000\n" $$(( \ (0xffffffff & (-1 << ($(CONFIG_ARM64_VA_BITS) - 32))) \ + (1 << ($(CONFIG_ARM64_VA_BITS) - 32 - $(KASAN_SHADOW_SCALE_SHIFT))) \ - (1 << (64 - 32 - $(KASAN_SHADOW_SCALE_SHIFT))) )) ) export TEXT_OFFSET GZFLAGS core-y += arch/arm64/kernel/ arch/arm64/mm/ core-$(CONFIG_NET) += arch/arm64/net/ core-$(CONFIG_KVM) += arch/arm64/kvm/ core-$(CONFIG_XEN) += arch/arm64/xen/ core-$(CONFIG_CRYPTO) += arch/arm64/crypto/ libs-y := arch/arm64/lib/ $(libs-y) core-$(CONFIG_EFI_STUB) += $(objtree)/drivers/firmware/efi/libstub/lib.a # Default target when executing plain make boot := arch/arm64/boot KBUILD_IMAGE := $(boot)/Image.gz KBUILD_DTBS := dtbs all: Image.gz $(KBUILD_DTBS) Image: vmlinux $(Q)$(MAKE) $(build)=$(boot) $(boot)/$@ Image.%: Image $(Q)$(MAKE) $(build)=$(boot) $(boot)/$@ zinstall install: $(Q)$(MAKE) $(build)=$(boot) $@ %.dtb: scripts $(Q)$(MAKE) $(build)=$(boot)/dts $(boot)/dts/$@ PHONY += dtbs dtbs_install dtbs: prepare scripts $(Q)$(MAKE) $(build)=$(boot)/dts dtbs_install: $(Q)$(MAKE) $(dtbinst)=$(boot)/dts PHONY += vdso_install vdso_install: $(Q)$(MAKE) $(build)=arch/arm64/kernel/vdso $@ # We use MRPROPER_FILES and CLEAN_FILES now archclean: $(Q)$(MAKE) $(clean)=$(boot) $(Q)$(MAKE) $(clean)=$(boot)/dts # We need to generate vdso-offsets.h before compiling certain files in kernel/. # In order to do that, we should use the archprepare target, but we can't since # asm-offsets.h is included in some files used to generate vdso-offsets.h, and # asm-offsets.h is built in prepare0, for which archprepare is a dependency. # Therefore we need to generate the header after prepare0 has been made, hence # this hack. prepare: vdso_prepare vdso_prepare: prepare0 $(Q)$(MAKE) $(build)=arch/arm64/kernel/vdso include/generated/vdso-offsets.h define archhelp echo '* Image.gz - Compressed kernel image (arch/$(ARCH)/boot/Image.gz)' echo ' Image - Uncompressed kernel image (arch/$(ARCH)/boot/Image)' echo '* dtbs - Build device tree blobs for enabled boards' echo ' dtbs_install - Install dtbs to $(INSTALL_DTBS_PATH)' echo ' install - Install uncompressed kernel' echo ' zinstall - Install compressed kernel' echo ' Install using (your) ~/bin/installkernel or' echo ' (distribution) /sbin/installkernel or' echo ' install to $$(INSTALL_PATH) and run lilo' endef