/* * Copyright (C) 2014 Texas Instruments Incorporated * Authors: Santosh Shilimkar * Sandeep Nair * Cyril Chemparathy * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License as * published by the Free Software Foundation version 2. * * This program is distributed "as is" WITHOUT ANY WARRANTY of any * kind, whether express or implied; without even the implied warranty * of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. */ #include #include #include #include #include #include #include #include #include #include #include #include #define REG_MASK 0xffffffff #define DMA_LOOPBACK BIT(31) #define DMA_ENABLE BIT(31) #define DMA_TEARDOWN BIT(30) #define DMA_TX_FILT_PSWORDS BIT(29) #define DMA_TX_FILT_EINFO BIT(30) #define DMA_TX_PRIO_SHIFT 0 #define DMA_RX_PRIO_SHIFT 16 #define DMA_PRIO_MASK GENMASK(3, 0) #define DMA_PRIO_DEFAULT 0 #define DMA_RX_TIMEOUT_DEFAULT 17500 /* cycles */ #define DMA_RX_TIMEOUT_MASK GENMASK(16, 0) #define DMA_RX_TIMEOUT_SHIFT 0 #define CHAN_HAS_EPIB BIT(30) #define CHAN_HAS_PSINFO BIT(29) #define CHAN_ERR_RETRY BIT(28) #define CHAN_PSINFO_AT_SOP BIT(25) #define CHAN_SOP_OFF_SHIFT 16 #define CHAN_SOP_OFF_MASK GENMASK(9, 0) #define DESC_TYPE_SHIFT 26 #define DESC_TYPE_MASK GENMASK(2, 0) /* * QMGR & QNUM together make up 14 bits with QMGR as the 2 MSb's in the logical * navigator cloud mapping scheme. * using the 14bit physical queue numbers directly maps into this scheme. */ #define CHAN_QNUM_MASK GENMASK(14, 0) #define DMA_MAX_QMS 4 #define DMA_TIMEOUT 1 /* msecs */ #define DMA_INVALID_ID 0xffff struct reg_global { u32 revision; u32 perf_control; u32 emulation_control; u32 priority_control; u32 qm_base_address[DMA_MAX_QMS]; }; struct reg_chan { u32 control; u32 mode; u32 __rsvd[6]; }; struct reg_tx_sched { u32 prio; }; struct reg_rx_flow { u32 control; u32 tags; u32 tag_sel; u32 fdq_sel[2]; u32 thresh[3]; }; struct knav_dma_pool_device { struct device *dev; struct list_head list; }; struct knav_dma_device { bool loopback, enable_all; unsigned tx_priority, rx_priority, rx_timeout; unsigned logical_queue_managers; unsigned qm_base_address[DMA_MAX_QMS]; struct reg_global __iomem *reg_global; struct reg_chan __iomem *reg_tx_chan; struct reg_rx_flow __iomem *reg_rx_flow; struct reg_chan __iomem *reg_rx_chan; struct reg_tx_sched __iomem *reg_tx_sched; unsigned max_rx_chan, max_tx_chan; unsigned max_rx_flow; char name[32]; atomic_t ref_count; struct list_head list; struct list_head chan_list; spinlock_t lock; }; struct knav_dma_chan { enum dma_transfer_direction direction; struct knav_dma_device *dma; atomic_t ref_count; /* registers */ struct reg_chan __iomem *reg_chan; struct reg_tx_sched __iomem *reg_tx_sched; struct reg_rx_flow __iomem *reg_rx_flow; /* configuration stuff */ unsigned channel, flow; struct knav_dma_cfg cfg; struct list_head list; spinlock_t lock; }; #define chan_number(ch) ((ch->direction == DMA_MEM_TO_DEV) ? \ ch->channel : ch->flow) static struct knav_dma_pool_device *kdev; static bool device_ready; bool knav_dma_device_ready(void) { return device_ready; } EXPORT_SYMBOL_GPL(knav_dma_device_ready); static bool check_config(struct knav_dma_chan *chan, struct knav_dma_cfg *cfg) { if (!memcmp(&chan->cfg, cfg, sizeof(*cfg))) return true; else return false; } static int chan_start(struct knav_dma_chan *chan, struct knav_dma_cfg *cfg) { u32 v = 0; spin_lock(&chan->lock); if ((chan->direction == DMA_MEM_TO_DEV) && chan->reg_chan) { if (cfg->u.tx.filt_pswords) v |= DMA_TX_FILT_PSWORDS; if (cfg->u.tx.filt_einfo) v |= DMA_TX_FILT_EINFO; writel_relaxed(v, &chan->reg_chan->mode); writel_relaxed(DMA_ENABLE, &chan->reg_chan->control); } if (chan->reg_tx_sched) writel_relaxed(cfg->u.tx.priority, &chan->reg_tx_sched->prio); if (chan->reg_rx_flow) { v = 0; if (cfg->u.rx.einfo_present) v |= CHAN_HAS_EPIB; if (cfg->u.rx.psinfo_present) v |= CHAN_HAS_PSINFO; if (cfg->u.rx.err_mode == DMA_RETRY) v |= CHAN_ERR_RETRY; v |= (cfg->u.rx.desc_type & DESC_TYPE_MASK) << DESC_TYPE_SHIFT; if (cfg->u.rx.psinfo_at_sop) v |= CHAN_PSINFO_AT_SOP; v |= (cfg->u.rx.sop_offset & CHAN_SOP_OFF_MASK) << CHAN_SOP_OFF_SHIFT; v |= cfg->u.rx.dst_q & CHAN_QNUM_MASK; writel_relaxed(v, &chan->reg_rx_flow->control); writel_relaxed(0, &chan->reg_rx_flow->tags); writel_relaxed(0, &chan->reg_rx_flow->tag_sel); v = cfg->u.rx.fdq[0] << 16; v |= cfg->u.rx.fdq[1] & CHAN_QNUM_MASK; writel_relaxed(v, &chan->reg_rx_flow->fdq_sel[0]); v = cfg->u.rx.fdq[2] << 16; v |= cfg->u.rx.fdq[3] & CHAN_QNUM_MASK; writel_relaxed(v, &chan->reg_rx_flow->fdq_sel[1]); writel_relaxed(0, &chan->reg_rx_flow->thresh[0]); writel_relaxed(0, &chan->reg_rx_flow->thresh[1]); writel_relaxed(0, &chan->reg_rx_flow->thresh[2]); } /* Keep a copy of the cfg */ memcpy(&chan->cfg, cfg, sizeof(*cfg)); spin_unlock(&chan->lock); return 0; } static int chan_teardown(struct knav_dma_chan *chan) { unsigned long end, value; if (!chan->reg_chan) return 0; /* indicate teardown */ writel_relaxed(DMA_TEARDOWN, &chan->reg_chan->control); /* wait for the dma to shut itself down */ end = jiffies + msecs_to_jiffies(DMA_TIMEOUT); do { value = readl_relaxed(&chan->reg_chan->control); if ((value & DMA_ENABLE) == 0) break; } while (time_after(end, jiffies)); if (readl_relaxed(&chan->reg_chan->control) & DMA_ENABLE) { dev_err(kdev->dev, "timeout waiting for teardown\n"); return -ETIMEDOUT; } return 0; } static void chan_stop(struct knav_dma_chan *chan) { spin_lock(&chan->lock); if (chan->reg_rx_flow) { /* first detach fdqs, starve out the flow */ writel_relaxed(0, &chan->reg_rx_flow->fdq_sel[0]); writel_relaxed(0, &chan->reg_rx_flow->fdq_sel[1]); writel_relaxed(0, &chan->reg_rx_flow->thresh[0]); writel_relaxed(0, &chan->reg_rx_flow->thresh[1]); writel_relaxed(0, &chan->reg_rx_flow->thresh[2]); } /* teardown the dma channel */ chan_teardown(chan); /* then disconnect the completion side */ if (chan->reg_rx_flow) { writel_relaxed(0, &chan->reg_rx_flow->control); writel_relaxed(0, &chan->reg_rx_flow->tags); writel_relaxed(0, &chan->reg_rx_flow->tag_sel); } memset(&chan->cfg, 0, sizeof(struct knav_dma_cfg)); spin_unlock(&chan->lock); dev_dbg(kdev->dev, "channel stopped\n"); } static void dma_hw_enable_all(struct knav_dma_device *dma) { int i; for (i = 0; i < dma->max_tx_chan; i++) { writel_relaxed(0, &dma->reg_tx_chan[i].mode); writel_relaxed(DMA_ENABLE, &dma->reg_tx_chan[i].control); } } static void knav_dma_hw_init(struct knav_dma_device *dma) { unsigned v; int i; spin_lock(&dma->lock); v = dma->loopback ? DMA_LOOPBACK : 0; writel_relaxed(v, &dma->reg_global->emulation_control); v = readl_relaxed(&dma->reg_global->perf_control); v |= ((dma->rx_timeout & DMA_RX_TIMEOUT_MASK) << DMA_RX_TIMEOUT_SHIFT); writel_relaxed(v, &dma->reg_global->perf_control); v = ((dma->tx_priority << DMA_TX_PRIO_SHIFT) | (dma->rx_priority << DMA_RX_PRIO_SHIFT)); writel_relaxed(v, &dma->reg_global->priority_control); /* Always enable all Rx channels. Rx paths are managed using flows */ for (i = 0; i < dma->max_rx_chan; i++) writel_relaxed(DMA_ENABLE, &dma->reg_rx_chan[i].control); for (i = 0; i < dma->logical_queue_managers; i++) writel_relaxed(dma->qm_base_address[i], &dma->reg_global->qm_base_address[i]); spin_unlock(&dma->lock); } static void knav_dma_hw_destroy(struct knav_dma_device *dma) { int i; unsigned v; spin_lock(&dma->lock); v = ~DMA_ENABLE & REG_MASK; for (i = 0; i < dma->max_rx_chan; i++) writel_relaxed(v, &dma->reg_rx_chan[i].control); for (i = 0; i < dma->max_tx_chan; i++) writel_relaxed(v, &dma->reg_tx_chan[i].control); spin_unlock(&dma->lock); } static void dma_debug_show_channels(struct seq_file *s, struct knav_dma_chan *chan) { int i; seq_printf(s, "\t%s %d:\t", ((chan->direction == DMA_MEM_TO_DEV) ? "tx chan" : "rx flow"), chan_number(chan)); if (chan->direction == DMA_MEM_TO_DEV) { seq_printf(s, "einfo - %d, pswords - %d, priority - %d\n", chan->cfg.u.tx.filt_einfo, chan->cfg.u.tx.filt_pswords, chan->cfg.u.tx.priority); } else { seq_printf(s, "einfo - %d, psinfo - %d, desc_type - %d\n", chan->cfg.u.rx.einfo_present, chan->cfg.u.rx.psinfo_present, chan->cfg.u.rx.desc_type); seq_printf(s, "\t\t\tdst_q: [%d], thresh: %d fdq: ", chan->cfg.u.rx.dst_q, chan->cfg.u.rx.thresh); for (i = 0; i < KNAV_DMA_FDQ_PER_CHAN; i++) seq_printf(s, "[%d]", chan->cfg.u.rx.fdq[i]); seq_printf(s, "\n"); } } static void dma_debug_show_devices(struct seq_file *s, struct knav_dma_device *dma) { struct knav_dma_chan *chan; list_for_each_entry(chan, &dma->chan_list, list) { if (atomic_read(&chan->ref_count)) dma_debug_show_channels(s, chan); } } static int dma_debug_show(struct seq_file *s, void *v) { struct knav_dma_device *dma; list_for_each_entry(dma, &kdev->list, list) { if (atomic_read(&dma->ref_count)) { seq_printf(s, "%s : max_tx_chan: (%d), max_rx_flows: (%d)\n", dma->name, dma->max_tx_chan, dma->max_rx_flow); dma_debug_show_devices(s, dma); } } return 0; } static int knav_dma_debug_open(struct inode *inode, struct file *file) { return single_open(file, dma_debug_show, NULL); } static const struct file_operations knav_dma_debug_ops = { .open = knav_dma_debug_open, .read = seq_read, .llseek = seq_lseek, .release = single_release, }; static int of_channel_match_helper(struct device_node *np, const char *name, const char **dma_instance) { struct of_phandle_args args; struct device_node *dma_node; int index; dma_node = of_parse_phandle(np, "ti,navigator-dmas", 0); if (!dma_node) return -ENODEV; *dma_instance = dma_node->name; index = of_property_match_string(np, "ti,navigator-dma-names", name); if (index < 0) { dev_err(kdev->dev, "No 'ti,navigator-dma-names' property\n"); return -ENODEV; } if (of_parse_phandle_with_fixed_args(np, "ti,navigator-dmas", 1, index, &args)) { dev_err(kdev->dev, "Missing the phandle args name %s\n", name); return -ENODEV; } if (args.args[0] < 0) { dev_err(kdev->dev, "Missing args for %s\n", name); return -ENODEV; } return args.args[0]; } /** * knav_dma_open_channel() - try to setup an exclusive slave channel * @dev: pointer to client device structure * @name: slave channel name * @config: dma configuration parameters * * Returns pointer to appropriate DMA channel on success or error. */ void *knav_dma_open_channel(struct device *dev, const char *name, struct knav_dma_cfg *config) { struct knav_dma_chan *chan; struct knav_dma_device *dma; bool found = false; int chan_num = -1; const char *instance; if (!kdev) { pr_err("keystone-navigator-dma driver not registered\n"); return (void *)-EINVAL; } chan_num = of_channel_match_helper(dev->of_node, name, &instance); if (chan_num < 0) { dev_err(kdev->dev, "No DMA instace with name %s\n", name); return (void *)-EINVAL; } dev_dbg(kdev->dev, "initializing %s channel %d from DMA %s\n", config->direction == DMA_MEM_TO_DEV ? "transmit" : config->direction == DMA_DEV_TO_MEM ? "receive" : "unknown", chan_num, instance); if (config->direction != DMA_MEM_TO_DEV && config->direction != DMA_DEV_TO_MEM) { dev_err(kdev->dev, "bad direction\n"); return (void *)-EINVAL; } /* Look for correct dma instance */ list_for_each_entry(dma, &kdev->list, list) { if (!strcmp(dma->name, instance)) { found = true; break; } } if (!found) { dev_err(kdev->dev, "No DMA instace with name %s\n", instance); return (void *)-EINVAL; } /* Look for correct dma channel from dma instance */ found = false; list_for_each_entry(chan, &dma->chan_list, list) { if (config->direction == DMA_MEM_TO_DEV) { if (chan->channel == chan_num) { found = true; break; } } else { if (chan->flow == chan_num) { found = true; break; } } } if (!found) { dev_err(kdev->dev, "channel %d is not in DMA %s\n", chan_num, instance); return (void *)-EINVAL; } if (atomic_read(&chan->ref_count) >= 1) { if (!check_config(chan, config)) { dev_err(kdev->dev, "channel %d config miss-match\n", chan_num); return (void *)-EINVAL; } } if (atomic_inc_return(&chan->dma->ref_count) <= 1) knav_dma_hw_init(chan->dma); if (atomic_inc_return(&chan->ref_count) <= 1) chan_start(chan, config); dev_dbg(kdev->dev, "channel %d opened from DMA %s\n", chan_num, instance); return chan; } EXPORT_SYMBOL_GPL(knav_dma_open_channel); /** * knav_dma_close_channel() - Destroy a dma channel * * channel: dma channel handle * */ void knav_dma_close_channel(void *channel) { struct knav_dma_chan *chan = channel; if (!kdev) { pr_err("keystone-navigator-dma driver not registered\n"); return; } if (atomic_dec_return(&chan->ref_count) <= 0) chan_stop(chan); if (atomic_dec_return(&chan->dma->ref_count) <= 0) knav_dma_hw_destroy(chan->dma); dev_dbg(kdev->dev, "channel %d or flow %d closed from DMA %s\n", chan->channel, chan->flow, chan->dma->name); } EXPORT_SYMBOL_GPL(knav_dma_close_channel); static void __iomem *pktdma_get_regs(struct knav_dma_device *dma, struct device_node *node, unsigned index, resource_size_t *_size) { struct device *dev = kdev->dev; struct resource res; void __iomem *regs; int ret; ret = of_address_to_resource(node, index, &res); if (ret) { dev_err(dev, "Can't translate of node(%s) address for index(%d)\n", node->name, index); return ERR_PTR(ret); } regs = devm_ioremap_resource(kdev->dev, &res); if (IS_ERR(regs)) dev_err(dev, "Failed to map register base for index(%d) node(%s)\n", index, node->name); if (_size) *_size = resource_size(&res); return regs; } static int pktdma_init_rx_chan(struct knav_dma_chan *chan, u32 flow) { struct knav_dma_device *dma = chan->dma; chan->flow = flow; chan->reg_rx_flow = dma->reg_rx_flow + flow; chan->channel = DMA_INVALID_ID; dev_dbg(kdev->dev, "rx flow(%d) (%p)\n", chan->flow, chan->reg_rx_flow); return 0; } static int pktdma_init_tx_chan(struct knav_dma_chan *chan, u32 channel) { struct knav_dma_device *dma = chan->dma; chan->channel = channel; chan->reg_chan = dma->reg_tx_chan + channel; chan->reg_tx_sched = dma->reg_tx_sched + channel; chan->flow = DMA_INVALID_ID; dev_dbg(kdev->dev, "tx channel(%d) (%p)\n", chan->channel, chan->reg_chan); return 0; } static int pktdma_init_chan(struct knav_dma_device *dma, enum dma_transfer_direction dir, unsigned chan_num) { struct device *dev = kdev->dev; struct knav_dma_chan *chan; int ret = -EINVAL; chan = devm_kzalloc(dev, sizeof(*chan), GFP_KERNEL); if (!chan) return -ENOMEM; INIT_LIST_HEAD(&chan->list); chan->dma = dma; chan->direction = DMA_NONE; atomic_set(&chan->ref_count, 0); spin_lock_init(&chan->lock); if (dir == DMA_MEM_TO_DEV) { chan->direction = dir; ret = pktdma_init_tx_chan(chan, chan_num); } else if (dir == DMA_DEV_TO_MEM) { chan->direction = dir; ret = pktdma_init_rx_chan(chan, chan_num); } else { dev_err(dev, "channel(%d) direction unknown\n", chan_num); } list_add_tail(&chan->list, &dma->chan_list); return ret; } static int dma_init(struct device_node *cloud, struct device_node *dma_node) { unsigned max_tx_chan, max_rx_chan, max_rx_flow, max_tx_sched; struct device_node *node = dma_node; struct knav_dma_device *dma; int ret, len, num_chan = 0; resource_size_t size; u32 timeout; u32 i; dma = devm_kzalloc(kdev->dev, sizeof(*dma), GFP_KERNEL); if (!dma) { dev_err(kdev->dev, "could not allocate driver mem\n"); return -ENOMEM; } INIT_LIST_HEAD(&dma->list); INIT_LIST_HEAD(&dma->chan_list); if (!of_find_property(cloud, "ti,navigator-cloud-address", &len)) { dev_err(kdev->dev, "unspecified navigator cloud addresses\n"); return -ENODEV; } dma->logical_queue_managers = len / sizeof(u32); if (dma->logical_queue_managers > DMA_MAX_QMS) { dev_warn(kdev->dev, "too many queue mgrs(>%d) rest ignored\n", dma->logical_queue_managers); dma->logical_queue_managers = DMA_MAX_QMS; } ret = of_property_read_u32_array(cloud, "ti,navigator-cloud-address", dma->qm_base_address, dma->logical_queue_managers); if (ret) { dev_err(kdev->dev, "invalid navigator cloud addresses\n"); return -ENODEV; } dma->reg_global = pktdma_get_regs(dma, node, 0, &size); if (!dma->reg_global) return -ENODEV; if (size < sizeof(struct reg_global)) { dev_err(kdev->dev, "bad size %pa for global regs\n", &size); return -ENODEV; } dma->reg_tx_chan = pktdma_get_regs(dma, node, 1, &size); if (!dma->reg_tx_chan) return -ENODEV; max_tx_chan = size / sizeof(struct reg_chan); dma->reg_rx_chan = pktdma_get_regs(dma, node, 2, &size); if (!dma->reg_rx_chan) return -ENODEV; max_rx_chan = size / sizeof(struct reg_chan); dma->reg_tx_sched = pktdma_get_regs(dma, node, 3, &size); if (!dma->reg_tx_sched) return -ENODEV; max_tx_sched = size / sizeof(struct reg_tx_sched); dma->reg_rx_flow = pktdma_get_regs(dma, node, 4, &size); if (!dma->reg_rx_flow) return -ENODEV; max_rx_flow = size / sizeof(struct reg_rx_flow); dma->rx_priority = DMA_PRIO_DEFAULT; dma->tx_priority = DMA_PRIO_DEFAULT; dma->enable_all = (of_get_property(node, "ti,enable-all", NULL) != NULL); dma->loopback = (of_get_property(node, "ti,loop-back", NULL) != NULL); ret = of_property_read_u32(node, "ti,rx-retry-timeout", &timeout); if (ret < 0) { dev_dbg(kdev->dev, "unspecified rx timeout using value %d\n", DMA_RX_TIMEOUT_DEFAULT); timeout = DMA_RX_TIMEOUT_DEFAULT; } dma->rx_timeout = timeout; dma->max_rx_chan = max_rx_chan; dma->max_rx_flow = max_rx_flow; dma->max_tx_chan = min(max_tx_chan, max_tx_sched); atomic_set(&dma->ref_count, 0); strcpy(dma->name, node->name); spin_lock_init(&dma->lock); for (i = 0; i < dma->max_tx_chan; i++) { if (pktdma_init_chan(dma, DMA_MEM_TO_DEV, i) >= 0) num_chan++; } for (i = 0; i < dma->max_rx_flow; i++) { if (pktdma_init_chan(dma, DMA_DEV_TO_MEM, i) >= 0) num_chan++; } list_add_tail(&dma->list, &kdev->list); /* * For DSP software usecases or userpace transport software, setup all * the DMA hardware resources. */ if (dma->enable_all) { atomic_inc(&dma->ref_count); knav_dma_hw_init(dma); dma_hw_enable_all(dma); } dev_info(kdev->dev, "DMA %s registered %d logical channels, flows %d, tx chans: %d, rx chans: %d%s\n", dma->name, num_chan, dma->max_rx_flow, dma->max_tx_chan, dma->max_rx_chan, dma->loopback ? ", loopback" : ""); return 0; } static int knav_dma_probe(struct platform_device *pdev) { struct device *dev = &pdev->dev; struct device_node *node = pdev->dev.of_node; struct device_node *child; int ret = 0; if (!node) { dev_err(&pdev->dev, "could not find device info\n"); return -EINVAL; } kdev = devm_kzalloc(dev, sizeof(struct knav_dma_pool_device), GFP_KERNEL); if (!kdev) { dev_err(dev, "could not allocate driver mem\n"); return -ENOMEM; } kdev->dev = dev; INIT_LIST_HEAD(&kdev->list); pm_runtime_enable(kdev->dev); ret = pm_runtime_get_sync(kdev->dev); if (ret < 0) { dev_err(kdev->dev, "unable to enable pktdma, err %d\n", ret); return ret; } /* Initialise all packet dmas */ for_each_child_of_node(node, child) { ret = dma_init(node, child); if (ret) { dev_err(&pdev->dev, "init failed with %d\n", ret); break; } } if (list_empty(&kdev->list)) { dev_err(dev, "no valid dma instance\n"); return -ENODEV; } debugfs_create_file("knav_dma", S_IFREG | S_IRUGO, NULL, NULL, &knav_dma_debug_ops); device_ready = true; return ret; } static int knav_dma_remove(struct platform_device *pdev) { struct knav_dma_device *dma; list_for_each_entry(dma, &kdev->list, list) { if (atomic_dec_return(&dma->ref_count) == 0) knav_dma_hw_destroy(dma); } pm_runtime_put_sync(&pdev->dev); pm_runtime_disable(&pdev->dev); return 0; } static struct of_device_id of_match[] = { { .compatible = "ti,keystone-navigator-dma", }, {}, }; MODULE_DEVICE_TABLE(of, of_match); static struct platform_driver knav_dma_driver = { .probe = knav_dma_probe, .remove = knav_dma_remove, .driver = { .name = "keystone-navigator-dma", .of_match_table = of_match, }, }; module_platform_driver(knav_dma_driver); MODULE_LICENSE("GPL v2"); MODULE_DESCRIPTION("TI Keystone Navigator Packet DMA driver"); MODULE_AUTHOR("Sandeep Nair "); MODULE_AUTHOR("Santosh Shilimkar ");