// SPDX-License-Identifier: GPL-2.0 /* * Implement the default iomap interfaces * * (C) Copyright 2004 Linus Torvalds */ #include #include #include #ifdef CONFIG_PCI /** * pci_iomap_range - create a virtual mapping cookie for a PCI BAR * @dev: PCI device that owns the BAR * @bar: BAR number * @offset: map memory at the given offset in BAR * @maxlen: max length of the memory to map * * Using this function you will get a __iomem address to your device BAR. * You can access it using ioread*() and iowrite*(). These functions hide * the details if this is a MMIO or PIO address space and will just do what * you expect from them in the correct way. * * @maxlen specifies the maximum length to map. If you want to get access to * the complete BAR from offset to the end, pass %0 here. * */ void __iomem *pci_iomap_range(struct pci_dev *dev, int bar, unsigned long offset, unsigned long maxlen) { resource_size_t start = pci_resource_start(dev, bar); resource_size_t len = pci_resource_len(dev, bar); unsigned long flags = pci_resource_flags(dev, bar); if (len <= offset || !start) return NULL; len -= offset; start += offset; if (maxlen && len > maxlen) len = maxlen; if (flags & IORESOURCE_IO) return __pci_ioport_map(dev, start, len); if (flags & IORESOURCE_MEM) return ioremap(start, len); /* What? */ return NULL; } EXPORT_SYMBOL(pci_iomap_range); /** * pci_iomap_wc_range - create a virtual WC mapping cookie for a PCI BAR * @dev: PCI device that owns the BAR * @bar: BAR number * @offset: map memory at the given offset in BAR * @maxlen: max length of the memory to map * * Using this function you will get a __iomem address to your device BAR. * You can access it using ioread*() and iowrite*(). These functions hide * the details if this is a MMIO or PIO address space and will just do what * you expect from them in the correct way. When possible write combining * is used. * * @maxlen specifies the maximum length to map. If you want to get access to * the complete BAR from offset to the end, pass %0 here. * */ void __iomem *pci_iomap_wc_range(struct pci_dev *dev, int bar, unsigned long offset, unsigned long maxlen) { resource_size_t start = pci_resource_start(dev, bar); resource_size_t len = pci_resource_len(dev, bar); unsigned long flags = pci_resource_flags(dev, bar); if (flags & IORESOURCE_IO) return NULL; if (len <= offset || !start) return NULL; len -= offset; start += offset; if (maxlen && len > maxlen) len = maxlen; if (flags & IORESOURCE_MEM) return ioremap_wc(start, len); /* What? */ return NULL; } EXPORT_SYMBOL_GPL(pci_iomap_wc_range); /** * pci_iomap - create a virtual mapping cookie for a PCI BAR * @dev: PCI device that owns the BAR * @bar: BAR number * @maxlen: length of the memory to map * * Using this function you will get a __iomem address to your device BAR. * You can access it using ioread*() and iowrite*(). These functions hide * the details if this is a MMIO or PIO address space and will just do what * you expect from them in the correct way. * * @maxlen specifies the maximum length to map. If you want to get access to * the complete BAR without checking for its length first, pass %0 here. * */ void __iomem *pci_iomap(struct pci_dev *dev, int bar, unsigned long maxlen) { return pci_iomap_range(dev, bar, 0, maxlen); } EXPORT_SYMBOL(pci_iomap); /** * pci_iomap_wc - create a virtual WC mapping cookie for a PCI BAR * @dev: PCI device that owns the BAR * @bar: BAR number * @maxlen: length of the memory to map * * Using this function you will get a __iomem address to your device BAR. * You can access it using ioread*() and iowrite*(). These functions hide * the details if this is a MMIO or PIO address space and will just do what * you expect from them in the correct way. When possible write combining * is used. * * @maxlen specifies the maximum length to map. If you want to get access to * the complete BAR without checking for its length first, pass %0 here. * */ void __iomem *pci_iomap_wc(struct pci_dev *dev, int bar, unsigned long maxlen) { return pci_iomap_wc_range(dev, bar, 0, maxlen); } EXPORT_SYMBOL_GPL(pci_iomap_wc); #endif /* CONFIG_PCI */