// SPDX-License-Identifier: GPL-2.0 /* * Variant of atomic_t specialized for reference counts. * * The interface matches the atomic_t interface (to aid in porting) but only * provides the few functions one should use for reference counting. * * It differs in that the counter saturates at UINT_MAX and will not move once * there. This avoids wrapping the counter and causing 'spurious' * use-after-free issues. * * Memory ordering rules are slightly relaxed wrt regular atomic_t functions * and provide only what is strictly required for refcounts. * * The increments are fully relaxed; these will not provide ordering. The * rationale is that whatever is used to obtain the object we're increasing the * reference count on will provide the ordering. For locked data structures, * its the lock acquire, for RCU/lockless data structures its the dependent * load. * * Do note that inc_not_zero() provides a control dependency which will order * future stores against the inc, this ensures we'll never modify the object * if we did not in fact acquire a reference. * * The decrements will provide release order, such that all the prior loads and * stores will be issued before, it also provides a control dependency, which * will order us against the subsequent free(). * * The control dependency is against the load of the cmpxchg (ll/sc) that * succeeded. This means the stores aren't fully ordered, but this is fine * because the 1->0 transition indicates no concurrency. * * Note that the allocator is responsible for ordering things between free() * and alloc(). * */ #include #include #include #include /** * refcount_add_not_zero_checked - add a value to a refcount unless it is 0 * @i: the value to add to the refcount * @r: the refcount * * Will saturate at UINT_MAX and WARN. * * Provides no memory ordering, it is assumed the caller has guaranteed the * object memory to be stable (RCU, etc.). It does provide a control dependency * and thereby orders future stores. See the comment on top. * * Use of this function is not recommended for the normal reference counting * use case in which references are taken and released one at a time. In these * cases, refcount_inc(), or one of its variants, should instead be used to * increment a reference count. * * Return: false if the passed refcount is 0, true otherwise */ bool refcount_add_not_zero_checked(unsigned int i, refcount_t *r) { unsigned int new, val = atomic_read(&r->refs); do { if (!val) return false; if (unlikely(val == UINT_MAX)) return true; new = val + i; if (new < val) new = UINT_MAX; } while (!atomic_try_cmpxchg_relaxed(&r->refs, &val, new)); WARN_ONCE(new == UINT_MAX, "refcount_t: saturated; leaking memory.\n"); return true; } EXPORT_SYMBOL(refcount_add_not_zero_checked); /** * refcount_add_checked - add a value to a refcount * @i: the value to add to the refcount * @r: the refcount * * Similar to atomic_add(), but will saturate at UINT_MAX and WARN. * * Provides no memory ordering, it is assumed the caller has guaranteed the * object memory to be stable (RCU, etc.). It does provide a control dependency * and thereby orders future stores. See the comment on top. * * Use of this function is not recommended for the normal reference counting * use case in which references are taken and released one at a time. In these * cases, refcount_inc(), or one of its variants, should instead be used to * increment a reference count. */ void refcount_add_checked(unsigned int i, refcount_t *r) { WARN_ONCE(!refcount_add_not_zero_checked(i, r), "refcount_t: addition on 0; use-after-free.\n"); } EXPORT_SYMBOL(refcount_add_checked); /** * refcount_inc_not_zero_checked - increment a refcount unless it is 0 * @r: the refcount to increment * * Similar to atomic_inc_not_zero(), but will saturate at UINT_MAX and WARN. * * Provides no memory ordering, it is assumed the caller has guaranteed the * object memory to be stable (RCU, etc.). It does provide a control dependency * and thereby orders future stores. See the comment on top. * * Return: true if the increment was successful, false otherwise */ bool refcount_inc_not_zero_checked(refcount_t *r) { unsigned int new, val = atomic_read(&r->refs); do { new = val + 1; if (!val) return false; if (unlikely(!new)) return true; } while (!atomic_try_cmpxchg_relaxed(&r->refs, &val, new)); WARN_ONCE(new == UINT_MAX, "refcount_t: saturated; leaking memory.\n"); return true; } EXPORT_SYMBOL(refcount_inc_not_zero_checked); /** * refcount_inc_checked - increment a refcount * @r: the refcount to increment * * Similar to atomic_inc(), but will saturate at UINT_MAX and WARN. * * Provides no memory ordering, it is assumed the caller already has a * reference on the object. * * Will WARN if the refcount is 0, as this represents a possible use-after-free * condition. */ void refcount_inc_checked(refcount_t *r) { WARN_ONCE(!refcount_inc_not_zero_checked(r), "refcount_t: increment on 0; use-after-free.\n"); } EXPORT_SYMBOL(refcount_inc_checked); /** * refcount_sub_and_test_checked - subtract from a refcount and test if it is 0 * @i: amount to subtract from the refcount * @r: the refcount * * Similar to atomic_dec_and_test(), but it will WARN, return false and * ultimately leak on underflow and will fail to decrement when saturated * at UINT_MAX. * * Provides release memory ordering, such that prior loads and stores are done * before, and provides a control dependency such that free() must come after. * See the comment on top. * * Use of this function is not recommended for the normal reference counting * use case in which references are taken and released one at a time. In these * cases, refcount_dec(), or one of its variants, should instead be used to * decrement a reference count. * * Return: true if the resulting refcount is 0, false otherwise */ bool refcount_sub_and_test_checked(unsigned int i, refcount_t *r) { unsigned int new, val = atomic_read(&r->refs); do { if (unlikely(val == UINT_MAX)) return false; new = val - i; if (new > val) { WARN_ONCE(new > val, "refcount_t: underflow; use-after-free.\n"); return false; } } while (!atomic_try_cmpxchg_release(&r->refs, &val, new)); return !new; } EXPORT_SYMBOL(refcount_sub_and_test_checked); /** * refcount_dec_and_test_checked - decrement a refcount and test if it is 0 * @r: the refcount * * Similar to atomic_dec_and_test(), it will WARN on underflow and fail to * decrement when saturated at UINT_MAX. * * Provides release memory ordering, such that prior loads and stores are done * before, and provides a control dependency such that free() must come after. * See the comment on top. * * Return: true if the resulting refcount is 0, false otherwise */ bool refcount_dec_and_test_checked(refcount_t *r) { return refcount_sub_and_test_checked(1, r); } EXPORT_SYMBOL(refcount_dec_and_test_checked); /** * refcount_dec_checked - decrement a refcount * @r: the refcount * * Similar to atomic_dec(), it will WARN on underflow and fail to decrement * when saturated at UINT_MAX. * * Provides release memory ordering, such that prior loads and stores are done * before. */ void refcount_dec_checked(refcount_t *r) { WARN_ONCE(refcount_dec_and_test_checked(r), "refcount_t: decrement hit 0; leaking memory.\n"); } EXPORT_SYMBOL(refcount_dec_checked); /** * refcount_dec_if_one - decrement a refcount if it is 1 * @r: the refcount * * No atomic_t counterpart, it attempts a 1 -> 0 transition and returns the * success thereof. * * Like all decrement operations, it provides release memory order and provides * a control dependency. * * It can be used like a try-delete operator; this explicit case is provided * and not cmpxchg in generic, because that would allow implementing unsafe * operations. * * Return: true if the resulting refcount is 0, false otherwise */ bool refcount_dec_if_one(refcount_t *r) { int val = 1; return atomic_try_cmpxchg_release(&r->refs, &val, 0); } EXPORT_SYMBOL(refcount_dec_if_one); /** * refcount_dec_not_one - decrement a refcount if it is not 1 * @r: the refcount * * No atomic_t counterpart, it decrements unless the value is 1, in which case * it will return false. * * Was often done like: atomic_add_unless(&var, -1, 1) * * Return: true if the decrement operation was successful, false otherwise */ bool refcount_dec_not_one(refcount_t *r) { unsigned int new, val = atomic_read(&r->refs); do { if (unlikely(val == UINT_MAX)) return true; if (val == 1) return false; new = val - 1; if (new > val) { WARN_ONCE(new > val, "refcount_t: underflow; use-after-free.\n"); return true; } } while (!atomic_try_cmpxchg_release(&r->refs, &val, new)); return true; } EXPORT_SYMBOL(refcount_dec_not_one); /** * refcount_dec_and_mutex_lock - return holding mutex if able to decrement * refcount to 0 * @r: the refcount * @lock: the mutex to be locked * * Similar to atomic_dec_and_mutex_lock(), it will WARN on underflow and fail * to decrement when saturated at UINT_MAX. * * Provides release memory ordering, such that prior loads and stores are done * before, and provides a control dependency such that free() must come after. * See the comment on top. * * Return: true and hold mutex if able to decrement refcount to 0, false * otherwise */ bool refcount_dec_and_mutex_lock(refcount_t *r, struct mutex *lock) { if (refcount_dec_not_one(r)) return false; mutex_lock(lock); if (!refcount_dec_and_test(r)) { mutex_unlock(lock); return false; } return true; } EXPORT_SYMBOL(refcount_dec_and_mutex_lock); /** * refcount_dec_and_lock - return holding spinlock if able to decrement * refcount to 0 * @r: the refcount * @lock: the spinlock to be locked * * Similar to atomic_dec_and_lock(), it will WARN on underflow and fail to * decrement when saturated at UINT_MAX. * * Provides release memory ordering, such that prior loads and stores are done * before, and provides a control dependency such that free() must come after. * See the comment on top. * * Return: true and hold spinlock if able to decrement refcount to 0, false * otherwise */ bool refcount_dec_and_lock(refcount_t *r, spinlock_t *lock) { if (refcount_dec_not_one(r)) return false; spin_lock(lock); if (!refcount_dec_and_test(r)) { spin_unlock(lock); return false; } return true; } EXPORT_SYMBOL(refcount_dec_and_lock); /** * refcount_dec_and_lock_irqsave - return holding spinlock with disabled * interrupts if able to decrement refcount to 0 * @r: the refcount * @lock: the spinlock to be locked * @flags: saved IRQ-flags if the is acquired * * Same as refcount_dec_and_lock() above except that the spinlock is acquired * with disabled interupts. * * Return: true and hold spinlock if able to decrement refcount to 0, false * otherwise */ bool refcount_dec_and_lock_irqsave(refcount_t *r, spinlock_t *lock, unsigned long *flags) { if (refcount_dec_not_one(r)) return false; spin_lock_irqsave(lock, *flags); if (!refcount_dec_and_test(r)) { spin_unlock_irqrestore(lock, *flags); return false; } return true; } EXPORT_SYMBOL(refcount_dec_and_lock_irqsave);