]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/hwspinlock.git/blobdiff - Documentation/devicetree/bindings/interrupt-controller/ti,sci-inta.txt
Merge branch 'platform-ti-linux-4.19.y' of git://git.ti.com/~rrnayak/ti-linux-kernel...
[rpmsg/hwspinlock.git] / Documentation / devicetree / bindings / interrupt-controller / ti,sci-inta.txt
diff --git a/Documentation/devicetree/bindings/interrupt-controller/ti,sci-inta.txt b/Documentation/devicetree/bindings/interrupt-controller/ti,sci-inta.txt
new file mode 100644 (file)
index 0000000..17b1fbd
--- /dev/null
@@ -0,0 +1,74 @@
+Texas Instruments K3 Interrupt Aggregator
+=========================================
+
+The Interrupt Aggregator (INTA) provides a centralized machine
+which handles the termination of system events to that they can
+be coherently processed by the host(s) in the system. A maximum
+of 64 events can be mapped to a single interrupt.
+
+
+                              Interrupt Aggregator
+                     +-----------------------------------------+
+                     |      Intmap            VINT             |
+                     | +--------------+  +------------+        |
+            m ------>| | vint  | bit  |  | 0 |.....|63| vint0  |
+               .     | +--------------+  +------------+        |       +------+
+               .     |         .               .               |       | HOST |
+Globalevents  ------>|         .               .               |------>| IRQ  |
+               .     |         .               .               |       | CTRL |
+               .     |         .               .               |       +------+
+            n ------>| +--------------+  +------------+        |
+                     | | vint  | bit  |  | 0 |.....|63| vintx  |
+                     | +--------------+  +------------+        |
+                     |                                         |
+                     +-----------------------------------------+
+
+Configuration of these Intmap registers that maps global events to vint is done
+by a system controller (like the Device Memory and Security Controller on K3
+AM654 SoC). Driver should request the system controller to get the range
+of global events and vints assigned to the requesting host. Management
+of these requested resources should be handled by driver and requests
+system controller to map specific global event to vint, bit pair.
+
+Communication between the host processor running an OS and the system
+controller happens through a protocol called TI System Control Interface
+(TISCI protocol). For more details refer:
+Documentation/devicetree/bindings/arm/keystone/ti,sci.txt
+
+TISCI Interrupt Aggregator Node:
+-------------------------------
+- compatible:          Must be "ti,sci-inta".
+- reg:                 Should contain registers location and length.
+- interrupt-controller:        Identifies the node as an interrupt controller
+- #interrupt-cells:    Specifies the number of cells needed to encode an
+                       interrupt source. The value should be 4.
+                       First cell should contain the TISCI device ID of source
+                       Second cell should contain the event source offset
+                       within the device
+                       Third cell specified the interrupt number(vint)
+                       reaching Interrupt aggregator.
+                       Fourth cell specifies the trigger type as defined
+                       in interrupts.txt in this directory.
+- interrupt-parent:    phandle of irq parent for TISCI intr.
+- ti,sci:              Phandle to TI-SCI compatible System controller node.
+- ti,sci-dev-id:       TISCI device ID of the Interrupt Aggregator.
+- ti,sci-rm-range-vint:        TISCI subtype id representing the virtual interrupts
+                       (vints) range within this IA, assigned to the
+                       requesting host context.
+- ti,sci-rm-range-global-event:        TISCI subtype id representing the global
+                       events range reaching this IA and are assigned
+                       to the requesting host context.
+
+Example:
+--------
+main_udmass_inta: interrupt-controller@33d00000 {
+       compatible = "ti,sci-inta";
+       reg = <0x0 0x33d00000 0x0 0x100000>;
+       interrupt-controller;
+       interrupt-parent = <&main_navss_intr>;
+       #interrupt-cells = <4>;
+       ti,sci = <&dmsc>;
+       ti,sci-dev-id = <179>;
+       ti,sci-rm-range-vint = <0x0>;
+       ti,sci-rm-range-global-event = <0x1>;
+};