diff --git a/include/linux/soc/ti/k3-ringacc.h b/include/linux/soc/ti/k3-ringacc.h
--- /dev/null
@@ -0,0 +1,258 @@
+/* SPDX-License-Identifier: GPL-2.0 */
+/*
+ * K3 Ring Accelerator (RA) subsystem interface
+ *
+ * Copyright (C) 2018 Texas Instruments Incorporated - http://www.ti.com
+ */
+
+#ifndef __SOC_TI_K3_RINGACC_API_H_
+#define __SOC_TI_K3_RINGACC_API_H_
+
+/**
+ * enum k3_ring_mode - &struct k3_ring_cfg mode
+ *
+ * RA ring operational modes
+ *
+ * @K3_RINGACC_RING_MODE_RING: Exposed Ring mode for SW direct access
+ * @K3_RINGACC_RING_MODE_MESSAGE: Messaging mode. Messaging mode requires
+ * that all accesses to the queue must go through this IP so that all
+ * accesses to the memory are controlled and ordered. This IP then
+ * controls the entire state of the queue, and SW has no directly control,
+ * such as through doorbells and cannot access the storage memory directly.
+ * This is particularly useful when more than one SW or HW entity can be
+ * the producer and/or consumer at the same time
+ * @K3_RINGACC_RING_MODE_CREDENTIALS: Credentials mode is message mode plus
+ * stores credentials with each message, requiring the element size to be
+ * doubled to fit the credentials. Any exposed memory should be protected
+ * by a firewall from unwanted access
+ * @K3_RINGACC_RING_MODE_QM: Queue manager mode. This takes the credentials
+ * mode and adds packet length per element, along with additional read only
+ * fields for element count and accumulated queue length. The QM mode only
+ * operates with an 8 byte element size (any other element size is
+ * illegal), and like in credentials mode each operation uses 2 element
+ * slots to store the credentials and length fields
+ */
+enum k3_ring_mode {
+ K3_RINGACC_RING_MODE_RING = 0,
+ K3_RINGACC_RING_MODE_MESSAGE,
+ K3_RINGACC_RING_MODE_CREDENTIALS,
+ K3_RINGACC_RING_MODE_QM,
+ K3_RINGACC_RING_MODE_INVALID
+};
+
+/**
+ * enum k3_ring_size - &struct k3_ring_cfg elm_size
+ *
+ * RA ring element's sizes in bytes.
+ */
+enum k3_ring_size {
+ K3_RINGACC_RING_ELSIZE_4 = 0,
+ K3_RINGACC_RING_ELSIZE_8,
+ K3_RINGACC_RING_ELSIZE_16,
+ K3_RINGACC_RING_ELSIZE_32,
+ K3_RINGACC_RING_ELSIZE_64,
+ K3_RINGACC_RING_ELSIZE_128,
+ K3_RINGACC_RING_ELSIZE_256,
+ K3_RINGACC_RING_ELSIZE_INVALID
+};
+
+struct k3_ringacc;
+struct k3_ring;
+
+/**
+ * enum k3_ring_cfg - RA ring configuration structure
+ *
+ * @size: Ring size, number of elements
+ * @elm_size: Ring element size
+ * @mode: Ring operational mode
+ * @flags: Ring configuration flags. Possible values:
+ * @K3_RINGACC_RING_SHARED: when set allows to request the same ring
+ * few times. It's usable when the same ring is used as Free Host PD ring
+ * for different flows, for example.
+ * Note: Locking should be done by consumer if required
+ */
+struct k3_ring_cfg {
+ u32 size;
+ enum k3_ring_size elm_size;
+ enum k3_ring_mode mode;
+#define K3_RINGACC_RING_SHARED BIT(1)
+ u32 flags;
+};
+
+#define K3_RINGACC_RING_ID_ANY (-1)
+
+/**
+ * of_k3_ringacc_get_by_phandle - find a RA by phandle property
+ * @np: device node
+ * @propname: property name containing phandle on RA node
+ *
+ * Returns pointer on the RA - struct k3_ringacc
+ * or -ENODEV if not found,
+ * or -EPROBE_DEFER if not yet registered
+ */
+struct k3_ringacc *of_k3_ringacc_get_by_phandle(struct device_node *np,
+ const char *property);
+
+#define K3_RINGACC_RING_USE_PROXY BIT(1)
+
+/**
+ * k3_ringacc_request_ring - request ring from ringacc
+ * @ringacc: pointer on ringacc
+ * @id: ring id or K3_RINGACC_RING_ID_ANY for any general purpose ring
+ * @flags:
+ * @K3_RINGACC_RING_USE_PROXY: if set - proxy will be allocated and
+ * used to access ring memory. Sopported only for rings in
+ * Message/Credentials/Queue mode.
+ *
+ * Returns pointer on the Ring - struct k3_ring
+ * or NULL in case of failure.
+ */
+struct k3_ring *k3_ringacc_request_ring(struct k3_ringacc *ringacc,
+ int id, u32 flags);
+
+/**
+ * k3_ringacc_get_dev - get pointer on RA device
+ * @ringacc: pointer on RA
+ *
+ * Returns device pointer
+ */
+struct device *k3_ringacc_get_dev(struct k3_ringacc *ringacc);
+
+/**
+ * k3_ringacc_ring_reset - ring reset
+ * @ring: pointer on Ring
+ *
+ * Resets ring internal state ((hw)occ, (hw)idx).
+ * TODO_GS: ? Ring can be reused without reconfiguration
+ */
+void k3_ringacc_ring_reset(struct k3_ring *ring);
+/**
+ * k3_ringacc_ring_reset - ring reset for DMA rings
+ * @ring: pointer on Ring
+ *
+ * Resets ring internal state ((hw)occ, (hw)idx). Should be used for rings
+ * which are read by K3 UDMA, like TX or Free Host PD rings.
+ */
+void k3_ringacc_ring_reset_dma(struct k3_ring *ring, u32 occ);
+
+/**
+ * k3_ringacc_ring_free - ring free
+ * @ring: pointer on Ring
+ *
+ * Resets ring and free all alocated resources.
+ */
+int k3_ringacc_ring_free(struct k3_ring *ring);
+
+/**
+ * k3_ringacc_get_ring_id - Get the Ring ID
+ * @ring: pointer on ring
+ *
+ * Returns the Ring ID
+ */
+u32 k3_ringacc_get_ring_id(struct k3_ring *ring);
+
+/**
+ * k3_ringacc_ring_cfg - ring configure
+ * @ring: pointer on ring
+ * @cfg: Ring configuration parameters (see &struct k3_ring_cfg)
+ *
+ * Configures ring, including ring memory allocation.
+ * Returns 0 on success, errno otherwise.
+ */
+int k3_ringacc_ring_cfg(struct k3_ring *ring, struct k3_ring_cfg *cfg);
+
+/**
+ * k3_ringacc_ring_get_size - get ring size
+ * @ring: pointer on ring
+ *
+ * Returns ring size in number of elements.
+ */
+u32 k3_ringacc_ring_get_size(struct k3_ring *ring);
+
+/**
+ * k3_ringacc_ring_get_free - get free elements
+ * @ring: pointer on ring
+ *
+ * Returns number of free elements in the ring.
+ */
+u32 k3_ringacc_ring_get_free(struct k3_ring *ring);
+
+/**
+ * k3_ringacc_ring_get_occ - get ring occupancy
+ * @ring: pointer on ring
+ *
+ * Returns total number of valid entries on the ring
+ */
+u32 k3_ringacc_ring_get_occ(struct k3_ring *ring);
+
+/**
+ * k3_ringacc_ring_is_full - checks if ring is full
+ * @ring: pointer on ring
+ *
+ * Returns true if the ring is full
+ */
+u32 k3_ringacc_ring_is_full(struct k3_ring *ring);
+
+/**
+ * k3_ringacc_ring_push - push element to the ring tail
+ * @ring: pointer on ring
+ * @elem: pointer on ring element buffer
+ *
+ * Push one ring element to the ring tail. Size of the ring element is
+ * determined by ring configuration &struct k3_ring_cfg elm_size.
+ *
+ * Returns 0 on success, errno otherwise.
+ */
+int k3_ringacc_ring_push(struct k3_ring *ring, void *elem);
+
+/**
+ * k3_ringacc_ring_pop - pop element from the ring head
+ * @ring: pointer on ring
+ * @elem: pointer on ring element buffer
+ *
+ * Push one ring element from the ring head. Size of the ring element is
+ * determined by ring configuration &struct k3_ring_cfg elm_size..
+ *
+ * Returns 0 on success, errno otherwise.
+ */
+int k3_ringacc_ring_pop(struct k3_ring *ring, void *elem);
+
+/**
+ * k3_ringacc_ring_push_head - push element to the ring head
+ * @ring: pointer on ring
+ * @elem: pointer on ring element buffer
+ *
+ * Push one ring element to the ring head. Size of the ring element is
+ * determined by ring configuration &struct k3_ring_cfg elm_size.
+ *
+ * Returns 0 on success, errno otherwise.
+ * Not Supported by ring modes: K3_RINGACC_RING_MODE_RING
+ */
+int k3_ringacc_ring_push_head(struct k3_ring *ring, void *elem);
+
+/**
+ * k3_ringacc_ring_pop_tail - pop element from the ring tail
+ * @ring: pointer on ring
+ * @elem: pointer on ring element buffer
+ *
+ * Push one ring element from the ring tail. Size of the ring element is
+ * determined by ring configuration &struct k3_ring_cfg elm_size.
+ *
+ * Returns 0 on success, errno otherwise.
+ * Not Supported by ring modes: K3_RINGACC_RING_MODE_RING
+ */
+int k3_ringacc_ring_pop_tail(struct k3_ring *ring, void *elem);
+
+u32 k3_ringacc_get_tisci_dev_id(struct k3_ring *ring);
+
+/**
+ * Debugging definitions
+ * TODO: might be removed
+ */
+#ifdef CONFIG_TI_K3_RINGACC_DEBUG
+void k3_ringacc_ring_dump(struct k3_ring *ring);
+#else
+static inline void k3_ringacc_ring_dump(struct k3_ring *ring) {};
+#endif
+
+#endif /* __SOC_TI_K3_RINGACC_API_H_ */