summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 274abd4)
raw | patch | inline | side by side (parent: 274abd4)
author | Andrew F. Davis <afd@ti.com> | |
Tue, 6 Mar 2018 00:18:48 +0000 (16:18 -0800) | ||
committer | Santosh Shilimkar <santosh.shilimkar@oracle.com> | |
Tue, 6 Mar 2018 00:18:48 +0000 (16:18 -0800) |
The keystone_irq node describes a device that is a member of the device
state control module address space. As such, it should not be a member
of soc0 bus but instead a sub-node of device-state-control.
This move also fixes a warning about not having a reg property. Now
that this is a sub-node of device-state-control, a syscon type node,
we add this reg property but relative to the syscon base, this way
when the dt-binding/driver are updated we can drop the non-standard
gpio,syscon-dev property completely and simply use get_resource() in
the driver.
Signed-off-by: Andrew F. Davis <afd@ti.com>
Acked-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Santosh Shilimkar <santosh.shilimkar@oracle.com>
state control module address space. As such, it should not be a member
of soc0 bus but instead a sub-node of device-state-control.
This move also fixes a warning about not having a reg property. Now
that this is a sub-node of device-state-control, a syscon type node,
we add this reg property but relative to the syscon base, this way
when the dt-binding/driver are updated we can drop the non-standard
gpio,syscon-dev property completely and simply use get_resource() in
the driver.
Signed-off-by: Andrew F. Davis <afd@ti.com>
Acked-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Santosh Shilimkar <santosh.shilimkar@oracle.com>
arch/arm/boot/dts/keystone-k2e.dtsi | patch | blob | history |
index 0bcd3f8a9c457d625886e0730f48bb5fd2db4444..085e7326ea8e3c3f2e432acaf8c5743a2d56b3a1 100644 (file)
};
};
- dspgpio0: keystone_dsp_gpio@2620240 {
- compatible = "ti,keystone-dsp-gpio";
- gpio-controller;
- #gpio-cells = <2>;
- gpio,syscon-dev = <&devctrl 0x240>;
+ devctrl: device-state-control@2620000 {
+ dspgpio0: keystone_dsp_gpio@240 {
+ compatible = "ti,keystone-dsp-gpio";
+ reg = <0x240 0x4>;
+ gpio-controller;
+ #gpio-cells = <2>;
+ gpio,syscon-dev = <&devctrl 0x240>;
+ };
};
dsp0: dsp@10800000 {