]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/hwspinlock.git/commitdiff
drivers/gpu/drm/gma500/: change return type to vm_fault_t
authorSouptick Joarder <jrdr.linux@gmail.com>
Fri, 24 Aug 2018 00:01:22 +0000 (17:01 -0700)
committerLinus Torvalds <torvalds@linux-foundation.org>
Fri, 24 Aug 2018 01:48:43 +0000 (18:48 -0700)
Use new return type vm_fault_t for fault handler.  For now, this is just
documenting that the function returns a VM_FAULT value rather than an
errno.  Once all instances are converted, vm_fault_t will become a
distinct type.

Ref-> 1c8f422059ae ("mm: change return type to vm_fault_t")

Previously vm_insert_{pfn,mixed} returns err which driver mapped into
VM_FAULT_* type.  The new function vmf_insert_{pfn,mixed} will replace
this inefficiency by returning VM_FAULT_* type.

vmf_error() is the newly introduce inline function in 4.17-rc6.

Link: http://lkml.kernel.org/r/20180713154541.GA3345@jordon-HP-15-Notebook-PC
Signed-off-by: Souptick Joarder <jrdr.linux@gmail.com>
Reviewed-by: Matthew Wilcox <mawilcox@microsoft.com>
Cc: David Airlie <airlied@linux.ie>
Cc: Arnd Bergmann <arnd@arndb.de>
Cc: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
Cc: Patrik Jakobsson <patrik.r.jakobsson@gmail.com>
Cc: Matthew Wilcox <willy@infradead.org>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
drivers/gpu/drm/gma500/framebuffer.c
drivers/gpu/drm/gma500/gem.c
drivers/gpu/drm/gma500/psb_drv.h

index 2f00a37684a22b22042027adfbdf6358d55ff81f..adefae58b5fcd6e09d513aed236c12d220e406c5 100644 (file)
@@ -108,7 +108,7 @@ static int psbfb_pan(struct fb_var_screeninfo *var, struct fb_info *info)
         return 0;
 }
 
-static int psbfb_vm_fault(struct vm_fault *vmf)
+static vm_fault_t psbfb_vm_fault(struct vm_fault *vmf)
 {
        struct vm_area_struct *vma = vmf->vma;
        struct psb_framebuffer *psbfb = vma->vm_private_data;
@@ -118,7 +118,7 @@ static int psbfb_vm_fault(struct vm_fault *vmf)
        int page_num;
        int i;
        unsigned long address;
-       int ret;
+       vm_fault_t ret = VM_FAULT_SIGBUS;
        unsigned long pfn;
        unsigned long phys_addr = (unsigned long)dev_priv->stolen_base +
                                  gtt->offset;
@@ -131,18 +131,14 @@ static int psbfb_vm_fault(struct vm_fault *vmf)
        for (i = 0; i < page_num; i++) {
                pfn = (phys_addr >> PAGE_SHIFT);
 
-               ret = vm_insert_mixed(vma, address,
+               ret = vmf_insert_mixed(vma, address,
                                __pfn_to_pfn_t(pfn, PFN_DEV));
-               if (unlikely((ret == -EBUSY) || (ret != 0 && i > 0)))
+               if (unlikely(ret & VM_FAULT_ERROR))
                        break;
-               else if (unlikely(ret != 0)) {
-                       ret = (ret == -ENOMEM) ? VM_FAULT_OOM : VM_FAULT_SIGBUS;
-                       return ret;
-               }
                address += PAGE_SIZE;
                phys_addr += PAGE_SIZE;
        }
-       return VM_FAULT_NOPAGE;
+       return ret;
 }
 
 static void psbfb_vm_open(struct vm_area_struct *vma)
index 913bf4c256faffa1fb3324df6b259f052004ba64..576f1b272f23854bf23277520052a03cb2562b9f 100644 (file)
@@ -134,12 +134,13 @@ int psb_gem_dumb_create(struct drm_file *file, struct drm_device *dev,
  *     vma->vm_private_data points to the GEM object that is backing this
  *     mapping.
  */
-int psb_gem_fault(struct vm_fault *vmf)
+vm_fault_t psb_gem_fault(struct vm_fault *vmf)
 {
        struct vm_area_struct *vma = vmf->vma;
        struct drm_gem_object *obj;
        struct gtt_range *r;
-       int ret;
+       int err;
+       vm_fault_t ret;
        unsigned long pfn;
        pgoff_t page_offset;
        struct drm_device *dev;
@@ -158,9 +159,10 @@ int psb_gem_fault(struct vm_fault *vmf)
        /* For now the mmap pins the object and it stays pinned. As things
           stand that will do us no harm */
        if (r->mmapping == 0) {
-               ret = psb_gtt_pin(r);
-               if (ret < 0) {
-                       dev_err(dev->dev, "gma500: pin failed: %d\n", ret);
+               err = psb_gtt_pin(r);
+               if (err < 0) {
+                       dev_err(dev->dev, "gma500: pin failed: %d\n", err);
+                       ret = vmf_error(err);
                        goto fail;
                }
                r->mmapping = 1;
@@ -175,18 +177,9 @@ int psb_gem_fault(struct vm_fault *vmf)
                pfn = (dev_priv->stolen_base + r->offset) >> PAGE_SHIFT;
        else
                pfn = page_to_pfn(r->pages[page_offset]);
-       ret = vm_insert_pfn(vma, vmf->address, pfn);
-
+       ret = vmf_insert_pfn(vma, vmf->address, pfn);
 fail:
        mutex_unlock(&dev_priv->mmap_mutex);
-       switch (ret) {
-       case 0:
-       case -ERESTARTSYS:
-       case -EINTR:
-               return VM_FAULT_NOPAGE;
-       case -ENOMEM:
-               return VM_FAULT_OOM;
-       default:
-               return VM_FAULT_SIGBUS;
-       }
+
+       return ret;
 }
index e8300f50902343957e2967a9cd581244a5bf01ad..93d2f4000d2f90beb943539dd0bdfc0f668c7707 100644 (file)
@@ -21,6 +21,7 @@
 #define _PSB_DRV_H_
 
 #include <linux/kref.h>
+#include <linux/mm_types.h>
 
 #include <drm/drmP.h>
 #include <drm/drm_global.h>
@@ -749,7 +750,7 @@ extern int psb_gem_get_aperture(struct drm_device *dev, void *data,
                        struct drm_file *file);
 extern int psb_gem_dumb_create(struct drm_file *file, struct drm_device *dev,
                        struct drm_mode_create_dumb *args);
-extern int psb_gem_fault(struct vm_fault *vmf);
+extern vm_fault_t psb_gem_fault(struct vm_fault *vmf);
 
 /* psb_device.c */
 extern const struct psb_ops psb_chip_ops;