summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 7db7a8f)
raw | patch | inline | side by side (parent: 7db7a8f)
author | Marc Zyngier <marc.zyngier@arm.com> | |
Fri, 24 Aug 2018 15:06:36 +0000 (16:06 +0100) | ||
committer | Olof Johansson <olof@lixom.net> | |
Fri, 24 Aug 2018 15:50:29 +0000 (08:50 -0700) |
pm_runtime_get_if_in_use can fail: either PM has been disabled
altogether (-EINVAL), or the device hasn't been enabled yet (0).
Sadly, the Rockchip IOMMU driver tends to conflate the two things
by considering a non-zero return value as successful.
This has the consequence of hiding other bugs, so let's handle this
case throughout the driver, with a WARN_ON_ONCE so that we can try
and work out what happened.
Fixes: 0f181d3cf7d98 ("iommu/rockchip: Add runtime PM support")
Reviewed-by: Heiko Stuebner <heiko@sntech.de>
Signed-off-by: Marc Zyngier <marc.zyngier@arm.com>
Signed-off-by: Olof Johansson <olof@lixom.net>
altogether (-EINVAL), or the device hasn't been enabled yet (0).
Sadly, the Rockchip IOMMU driver tends to conflate the two things
by considering a non-zero return value as successful.
This has the consequence of hiding other bugs, so let's handle this
case throughout the driver, with a WARN_ON_ONCE so that we can try
and work out what happened.
Fixes: 0f181d3cf7d98 ("iommu/rockchip: Add runtime PM support")
Reviewed-by: Heiko Stuebner <heiko@sntech.de>
Signed-off-by: Marc Zyngier <marc.zyngier@arm.com>
Signed-off-by: Olof Johansson <olof@lixom.net>
drivers/iommu/rockchip-iommu.c | patch | blob | history |
index 054cd2c8e9c8a670ee2c4fc23fe9ae3a6f78e41a..4e0f9b61cd7fabba7019ad9d9bc697aba7b6f0e2 100644 (file)
u32 int_status;
dma_addr_t iova;
irqreturn_t ret = IRQ_NONE;
- int i;
+ int i, err;
- if (WARN_ON(!pm_runtime_get_if_in_use(iommu->dev)))
- return 0;
+ err = pm_runtime_get_if_in_use(iommu->dev);
+ if (WARN_ON_ONCE(err <= 0))
+ return ret;
if (WARN_ON(clk_bulk_enable(iommu->num_clocks, iommu->clocks)))
goto out;
spin_lock_irqsave(&rk_domain->iommus_lock, flags);
list_for_each(pos, &rk_domain->iommus) {
struct rk_iommu *iommu;
+ int ret;
iommu = list_entry(pos, struct rk_iommu, node);
/* Only zap TLBs of IOMMUs that are powered on. */
- if (pm_runtime_get_if_in_use(iommu->dev)) {
+ ret = pm_runtime_get_if_in_use(iommu->dev);
+ if (WARN_ON_ONCE(ret < 0))
+ continue;
+ if (ret) {
WARN_ON(clk_bulk_enable(iommu->num_clocks,
iommu->clocks));
rk_iommu_zap_lines(iommu, iova, size);
struct rk_iommu *iommu;
struct rk_iommu_domain *rk_domain = to_rk_domain(domain);
unsigned long flags;
+ int ret;
/* Allow 'virtual devices' (eg drm) to detach from domain */
iommu = rk_iommu_from_dev(dev);
list_del_init(&iommu->node);
spin_unlock_irqrestore(&rk_domain->iommus_lock, flags);
- if (pm_runtime_get_if_in_use(iommu->dev)) {
+ ret = pm_runtime_get_if_in_use(iommu->dev);
+ WARN_ON_ONCE(ret < 0);
+ if (ret > 0) {
rk_iommu_disable(iommu);
pm_runtime_put(iommu->dev);
}
list_add_tail(&iommu->node, &rk_domain->iommus);
spin_unlock_irqrestore(&rk_domain->iommus_lock, flags);
- if (!pm_runtime_get_if_in_use(iommu->dev))
+ ret = pm_runtime_get_if_in_use(iommu->dev);
+ if (!ret || WARN_ON_ONCE(ret < 0))
return 0;
ret = rk_iommu_enable(iommu);