]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/hwspinlock.git/commitdiff
RDS: defer the over_batch work to send worker
authorSantosh Shilimkar <santosh.shilimkar@oracle.com>
Thu, 10 Sep 2015 18:57:14 +0000 (11:57 -0700)
committerSantosh Shilimkar <santosh.shilimkar@oracle.com>
Mon, 5 Oct 2015 18:18:45 +0000 (11:18 -0700)
Current process gives up if its send work over the batch limit.
The work queue will get  kicked to finish off any other requests.
This fixes remainder condition from commit 443be0e5affe ("RDS: make
sure not to loop forever inside rds_send_xmit").

The restart condition is only for the case where we reached to
over_batch code for some other reason so just retrying again
before giving up.

While at it, make sure we use already available 'send_batch_count'
parameter instead of magic value. The batch count threshold value
of 1024 came via commit 443be0e5affe ("RDS: make sure not to loop
forever inside rds_send_xmit"). The idea is to process as big a
batch as we can but at the same time we don't hold other waiting
processes for send. Hence back-off after the send_batch_count
limit (1024) to avoid soft-lock ups.

Signed-off-by: Santosh Shilimkar <ssantosh@kernel.org>
Signed-off-by: Santosh Shilimkar <santosh.shilimkar@oracle.com>
net/rds/send.c

index 4df61a515b83da02bd91fc5e247e17ad44246ec2..b0acd45a9d42ae7abc86f3a028aabffe9d6576f4 100644 (file)
@@ -38,6 +38,7 @@
 #include <linux/list.h>
 #include <linux/ratelimit.h>
 #include <linux/export.h>
+#include <linux/sizes.h>
 
 #include "rds.h"
 
@@ -51,7 +52,7 @@
  * it to 0 will restore the old behavior (where we looped until we had
  * drained the queue).
  */
-static int send_batch_count = 64;
+static int send_batch_count = SZ_1K;
 module_param(send_batch_count, int, 0444);
 MODULE_PARM_DESC(send_batch_count, " batch factor when working the send queue");
 
@@ -223,7 +224,7 @@ restart:
                         * through a lot of messages, lets back off and see
                         * if anyone else jumps in
                         */
-                       if (batch_count >= 1024)
+                       if (batch_count >= send_batch_count)
                                goto over_batch;
 
                        spin_lock_irqsave(&conn->c_lock, flags);
@@ -423,7 +424,9 @@ over_batch:
                     !list_empty(&conn->c_send_queue)) &&
                    send_gen == conn->c_send_gen) {
                        rds_stats_inc(s_send_lock_queue_raced);
-                       goto restart;
+                       if (batch_count < send_batch_count)
+                               goto restart;
+                       queue_delayed_work(rds_wq, &conn->c_send_w, 1);
                }
        }
 out: