summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 8d5d8a5)
raw | patch | inline | side by side (parent: 8d5d8a5)
author | Santosh Shilimkar <santosh.shilimkar@oracle.com> | |
Tue, 5 Jul 2016 00:04:37 +0000 (17:04 -0700) | ||
committer | Santosh Shilimkar <santosh.shilimkar@oracle.com> | |
Mon, 2 Jan 2017 22:02:46 +0000 (14:02 -0800) |
The first message to a remote node should prompt a new
connection even if it is RDMA operation. For RDMA operation
the MR mapping can fail because connections is not yet up.
Since the connection establishment is asynchronous,
we make sure the map failure because of unavailable
connection reach to the user by appropriate error code.
Before returning to the user, lets trigger the connection
so that its ready for the next retry.
Signed-off-by: Santosh Shilimkar <santosh.shilimkar@oracle.com>
connection even if it is RDMA operation. For RDMA operation
the MR mapping can fail because connections is not yet up.
Since the connection establishment is asynchronous,
we make sure the map failure because of unavailable
connection reach to the user by appropriate error code.
Before returning to the user, lets trigger the connection
so that its ready for the next retry.
Signed-off-by: Santosh Shilimkar <santosh.shilimkar@oracle.com>
net/rds/send.c | patch | blob | history |
diff --git a/net/rds/send.c b/net/rds/send.c
index bb13c56fc2f8d00b92addb92bad5299cb75236e0..0a6f38b1c8a5cd80dda3d71428fb3960931ae360 100644 (file)
--- a/net/rds/send.c
+++ b/net/rds/send.c
ret = rds_cmsg_rdma_map(rs, rm, cmsg);
if (!ret)
*allocated_mr = 1;
+ else if (ret == -ENODEV)
+ /* Accommodate the get_mr() case which can fail
+ * if connection isn't established yet.
+ */
+ ret = -EAGAIN;
break;
case RDS_CMSG_ATOMIC_CSWP:
case RDS_CMSG_ATOMIC_FADD:
/* Parse any control messages the user may have included. */
ret = rds_cmsg_send(rs, rm, msg, &allocated_mr);
- if (ret)
+ if (ret) {
+ /* Trigger connection so that its ready for the next retry */
+ if (ret == -EAGAIN)
+ rds_conn_connect_if_down(conn);
goto out;
+ }
if (rm->rdma.op_active && !conn->c_trans->xmit_rdma) {
printk_ratelimited(KERN_NOTICE "rdma_op %p conn xmit_rdma %p\n",