dmaengine: Add metadata_ops for dma_async_tx_descriptor
authorPeter Ujfalusi <peter.ujfalusi@ti.com>
Wed, 28 Nov 2018 10:48:08 +0000 (12:48 +0200)
committerTero Kristo <t-kristo@ti.com>
Wed, 28 Nov 2018 10:52:31 +0000 (12:52 +0200)
The metadata is best described as side band data or parameters traveling
alongside the data DMAd by the DMA engine. It is data
which is understood by the peripheral and the peripheral driver only, the
DMA engine see it only as data block and it is not interpreting it in any
way.

The metadata can be different per descriptor as it is a parameter for the
data being transferred.

If the DMA supports per descriptor metadata it can implement the attach,
get_ptr/set_len callbacks.

Client drivers must only use either attach or get_ptr/set_len to avoid
misconfiguration.

Client driver can check if a given metadata mode is supported by the
channel during probe time with
dmaengine_is_metadata_mode_supported(chan, DESC_METADATA_CLIENT);
dmaengine_is_metadata_mode_supported(chan, DESC_METADATA_ENGINE);

and based on this information can use either mode.

Wrappers are also added for the metadata_ops.

To be used in DESC_METADATA_CLIENT mode:
dmaengine_desc_attach_metadata()

To be used in DESC_METADATA_ENGINE mode:
dmaengine_desc_get_metadata_ptr()
dmaengine_desc_set_metadata_len()

Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com>
drivers/dma/dmaengine.c
include/linux/dmaengine.h

index f1a441ab395d7529ebbc4f8d59e891e20c61419d..27b6d7c2d8a07aab4e10aff4e3a6aac5066bfd41 100644 (file)
@@ -1306,6 +1306,79 @@ void dma_async_tx_descriptor_init(struct dma_async_tx_descriptor *tx,
 }
 EXPORT_SYMBOL(dma_async_tx_descriptor_init);
 
+static inline int desc_check_and_set_metadata_mode(
+       struct dma_async_tx_descriptor *desc, enum dma_desc_metadata_mode mode)
+{
+       /* Make sure that the metadata mode is not mixed */
+       if (!desc->desc_metadata_mode) {
+               if (dmaengine_is_metadata_mode_supported(desc->chan, mode))
+                       desc->desc_metadata_mode = mode;
+               else
+                       return -ENOTSUPP;
+       } else if (desc->desc_metadata_mode != mode) {
+               return -EINVAL;
+       }
+
+       return 0;
+}
+
+int dmaengine_desc_attach_metadata(struct dma_async_tx_descriptor *desc,
+                                  void *data, size_t len)
+{
+       int ret;
+
+       if (!desc)
+               return -EINVAL;
+
+       ret = desc_check_and_set_metadata_mode(desc, DESC_METADATA_CLIENT);
+       if (ret)
+               return ret;
+
+       if (!desc->metadata_ops || !desc->metadata_ops->attach)
+               return -ENOTSUPP;
+
+       return desc->metadata_ops->attach(desc, data, len);
+}
+EXPORT_SYMBOL_GPL(dmaengine_desc_attach_metadata);
+
+void *dmaengine_desc_get_metadata_ptr(struct dma_async_tx_descriptor *desc,
+                                     size_t *payload_len, size_t *max_len)
+{
+       int ret;
+
+       if (!desc)
+               return ERR_PTR(-EINVAL);
+
+       ret = desc_check_and_set_metadata_mode(desc, DESC_METADATA_ENGINE);
+       if (ret)
+               return ERR_PTR(ret);
+
+       if (!desc->metadata_ops || !desc->metadata_ops->get_ptr)
+               return ERR_PTR(-ENOTSUPP);
+
+       return desc->metadata_ops->get_ptr(desc, payload_len, max_len);
+}
+EXPORT_SYMBOL_GPL(dmaengine_desc_get_metadata_ptr);
+
+int dmaengine_desc_set_metadata_len(struct dma_async_tx_descriptor *desc,
+                                   size_t payload_len)
+{
+       int ret;
+
+       if (!desc)
+               return -EINVAL;
+
+       ret = desc_check_and_set_metadata_mode(desc, DESC_METADATA_ENGINE);
+       if (ret)
+               return ret;
+
+       if (!desc->metadata_ops || !desc->metadata_ops->set_len)
+               return -ENOTSUPP;
+
+       return desc->metadata_ops->set_len(desc, payload_len);
+}
+EXPORT_SYMBOL_GPL(dmaengine_desc_set_metadata_len);
+
 /* dma_wait_for_async_tx - spin wait for a transaction to complete
  * @tx: in-flight transaction to wait on
  */
index d49ec5c31944863137f044b4046808dab60fe4ea..d33a953c9b55fcfe6ba9c4a0471fdabbc70051b2 100644 (file)
@@ -231,6 +231,58 @@ typedef struct { DECLARE_BITMAP(bits, DMA_TX_TYPE_END); } dma_cap_mask_t;
  * @bytes_transferred: byte counter
  */
 
+/**
+ * enum dma_desc_metadata_mode - per descriptor metadata mode types supported
+ * @DESC_METADATA_CLIENT - the metadata buffer is allocated/provided by the
+ *  client driver and it is attached (via the dmaengine_desc_attach_metadata()
+ *  helper) to the descriptor.
+ *
+ * Client drivers interested to use this mode can follow:
+ * - DMA_MEM_TO_DEV / DEV_MEM_TO_MEM:
+ *   1. prepare the descriptor (dmaengine_prep_*)
+ *     construct the metadata in the client's buffer
+ *   2. use dmaengine_desc_attach_metadata() to attach the buffer to the
+ *     descriptor
+ *   3. submit the transfer
+ * - DMA_DEV_TO_MEM:
+ *   1. prepare the descriptor (dmaengine_prep_*)
+ *   2. use dmaengine_desc_attach_metadata() to attach the buffer to the
+ *     descriptor
+ *   3. submit the transfer
+ *   4. when the transfer is completed, the metadata should be available in the
+ *     attached buffer
+ *
+ * @DESC_METADATA_ENGINE - the metadata buffer is allocated/managed by the DMA
+ *  driver. The client driver can ask for the pointer, maximum size and the
+ *  currently used size of the metadata and can directly update or read it.
+ *  dmaengine_desc_get_metadata_ptr() and dmaengine_desc_set_metadata_len() is
+ *  provided as helper functions.
+ *
+ * Client drivers interested to use this mode can follow:
+ * - DMA_MEM_TO_DEV / DEV_MEM_TO_MEM:
+ *   1. prepare the descriptor (dmaengine_prep_*)
+ *   2. use dmaengine_desc_get_metadata_ptr() to get the pointer to the engine's
+ *     metadata area
+ *   3. update the metadata at the pointer
+ *   4. use dmaengine_desc_set_metadata_len()  to tell the DMA engine the amount
+ *     of data the client has placed into the metadata buffer
+ *   5. submit the transfer
+ * - DMA_DEV_TO_MEM:
+ *   1. prepare the descriptor (dmaengine_prep_*)
+ *   2. submit the transfer
+ *   3. on transfer completion, use dmaengine_desc_get_metadata_ptr() to get the
+ *     pointer to the engine's metadata are
+ *   4. Read out the metadate from the pointer
+ *
+ * Note: the two mode is not compatible and clients must use one mode for a
+ * descriptor.
+ */
+enum dma_desc_metadata_mode {
+       DESC_METADATA_NONE = 0,
+       DESC_METADATA_CLIENT = BIT(0),
+       DESC_METADATA_ENGINE = BIT(1),
+};
+
 struct dma_chan_percpu {
        /* stats */
        unsigned long memcpy_count;
@@ -487,6 +539,18 @@ struct dmaengine_unmap_data {
        dma_addr_t addr[0];
 };
 
+struct dma_async_tx_descriptor;
+
+struct dma_descriptor_metadata_ops {
+       int (*attach)(struct dma_async_tx_descriptor *desc, void *data,
+                     size_t len);
+
+       void *(*get_ptr)(struct dma_async_tx_descriptor *desc,
+                        size_t *payload_len, size_t *max_len);
+       int (*set_len)(struct dma_async_tx_descriptor *desc,
+                      size_t payload_len);
+};
+
 /**
  * struct dma_async_tx_descriptor - async transaction descriptor
  * ---dma generic offload fields---
@@ -500,6 +564,11 @@ struct dmaengine_unmap_data {
  * descriptor pending. To be pushed on .issue_pending() call
  * @callback: routine to call after this operation is complete
  * @callback_param: general parameter to pass to the callback routine
+ * @desc_metadata_mode: core managed metadata mode to protect mixed use of
+ *     DESC_METADATA_CLIENT or DESC_METADATA_ENGINE. Otherwise
+ *     DESC_METADATA_NONE
+ * @metadata_ops: DMA driver provided metadata mode ops, need to be set by the
+ *     DMA driver if metadata mode is supported with the descriptor
  * ---async_tx api specific fields---
  * @next: at completion submit this descriptor
  * @parent: pointer to the next level up in the dependency chain
@@ -516,6 +585,8 @@ struct dma_async_tx_descriptor {
        dma_async_tx_callback_result callback_result;
        void *callback_param;
        struct dmaengine_unmap_data *unmap;
+       enum dma_desc_metadata_mode desc_metadata_mode;
+       struct dma_descriptor_metadata_ops *metadata_ops;
 #ifdef CONFIG_ASYNC_TX_ENABLE_CHANNEL_SWITCH
        struct dma_async_tx_descriptor *next;
        struct dma_async_tx_descriptor *parent;
@@ -678,6 +749,7 @@ struct dma_filter {
  * @global_node: list_head for global dma_device_list
  * @filter: information for device/slave to filter function/param mapping
  * @cap_mask: one or more dma_capability flags
+ * @desc_metadata_modes: supported metadata modes by the DMA device
  * @max_xor: maximum number of xor sources, 0 if no capability
  * @max_pq: maximum number of PQ sources and PQ-continue capability
  * @copy_align: alignment shift for memcpy operations
@@ -739,6 +811,7 @@ struct dma_device {
        struct list_head global_node;
        struct dma_filter filter;
        dma_cap_mask_t  cap_mask;
+       enum dma_desc_metadata_mode desc_metadata_modes;
        unsigned short max_xor;
        unsigned short max_pq;
        enum dmaengine_alignment copy_align;
@@ -914,6 +987,41 @@ static inline struct dma_async_tx_descriptor *dmaengine_prep_dma_memcpy(
                                                    len, flags);
 }
 
+static inline bool dmaengine_is_metadata_mode_supported(struct dma_chan *chan,
+               enum dma_desc_metadata_mode mode)
+{
+       if (!chan)
+               return false;
+
+       return !!(chan->device->desc_metadata_modes & mode);
+}
+
+#ifdef CONFIG_DMA_ENGINE
+int dmaengine_desc_attach_metadata(struct dma_async_tx_descriptor *desc,
+                                  void *data, size_t len);
+void *dmaengine_desc_get_metadata_ptr(struct dma_async_tx_descriptor *desc,
+                                     size_t *payload_len, size_t *max_len);
+int dmaengine_desc_set_metadata_len(struct dma_async_tx_descriptor *desc,
+                                   size_t payload_len);
+#else /* CONFIG_DMA_ENGINE */
+static inline int dmaengine_desc_attach_metadata(
+               struct dma_async_tx_descriptor *desc, void *data, size_t len)
+{
+       return -EINVAL;
+}
+static inline void *dmaengine_desc_get_metadata_ptr(
+               struct dma_async_tx_descriptor *desc, size_t *payload_len,
+               size_t *max_len)
+{
+       return NULL;
+}
+static inline int dmaengine_desc_set_metadata_len(
+               struct dma_async_tx_descriptor *desc, size_t payload_len)
+{
+       return -EINVAL;
+}
+#endif /* CONFIG_DMA_ENGINE */
+
 /**
  * dmaengine_terminate_all() - Terminate all active DMA transfers
  * @chan: The channel for which to terminate the transfers