ARM: OMAP2: Add functions to save and restore omap hwmod context en-masse.
authorRuss Dill <Russ.Dill@ti.com>
Fri, 2 Nov 2018 10:28:00 +0000 (15:58 +0530)
committerTero Kristo <t-kristo@ti.com>
Tue, 6 Nov 2018 13:03:46 +0000 (15:03 +0200)
This is used to support suspend modes like RTC-only and hibernate where
the state of these registers is lost.

After the PRCM loses context in the case of an RTC+DDR cycle omap_hwmod
attempts to return all hwmods to their previous state, however certain
hwmods cannot just be disabled when in their default state, which is why
they need the special handling present in that patch when no driver is
present.

In RTC+DDR mode, even if all drivers are present, the modules are all
returned to their previous state before any driver resume happens so we
will still face the issue described above. This can be prevented by
calling _reidle on all hwmods that need it for any module that is being
disabled to return to it's previous state.

Signed-off-by: Dave Gerlach <d-gerlach@ti.com>
Signed-off-by: Russ Dill <Russ.Dill@ti.com>
Signed-off-by: Keerthy <j-keerthy@ti.com>
arch/arm/mach-omap2/omap_hwmod.c
arch/arm/mach-omap2/omap_hwmod.h

index 56c452db430a3c237e7e439e8afae2336b8029a7..a28950188fb4fbeb7d9ae7b71345775d541f0d07 100644 (file)
@@ -4134,3 +4134,70 @@ const char *omap_hwmod_get_main_clk(struct omap_hwmod *oh)
 
        return oh->main_clk;
 }
+
+/**
+ * omap_hwmod_save_context - Saves the HW reset line state of submodules
+ * @oh: struct omap_hwmod *
+ * @unused: (unused, caller should pass NULL)
+ *
+ * Saves the HW reset line state of all the submodules in the hwmod
+ */
+static int omap_hwmod_save_context(struct omap_hwmod *oh, void *unused)
+{
+       int i;
+
+       for (i = 0; i < oh->rst_lines_cnt; i++)
+               oh->rst_lines[i].context =
+                               _read_hardreset(oh, oh->rst_lines[i].name);
+       return 0;
+}
+
+/**
+ * omap_hwmod_restore_context - Restores the HW reset line state of submodules
+ * @oh: struct omap_hwmod *
+ * @unused: (unused, caller should pass NULL)
+ *
+ * Restores the HW reset line state of all the submodules in the hwmod
+ */
+static int omap_hwmod_restore_context(struct omap_hwmod *oh, void *unused)
+{
+       int i;
+
+       for (i = 0; i < oh->rst_lines_cnt; i++)
+               if (oh->rst_lines[i].context)
+                       _assert_hardreset(oh, oh->rst_lines[i].name);
+               else
+                       _deassert_hardreset(oh, oh->rst_lines[i].name);
+
+       if (oh->_state == _HWMOD_STATE_ENABLED) {
+               if (soc_ops.enable_module)
+                       soc_ops.enable_module(oh);
+       } else {
+               if (oh->flags & HWMOD_NEEDS_REIDLE)
+                       _reidle(oh);
+               else if (soc_ops.disable_module)
+                       soc_ops.disable_module(oh);
+       }
+
+       return 0;
+}
+
+/**
+ * omap_hwmods_save_context - Saves the HW reset line state for all hwmods
+ *
+ * Saves the HW reset line state of all the registered hwmods
+ */
+void omap_hwmods_save_context(void)
+{
+       omap_hwmod_for_each(omap_hwmod_save_context, NULL);
+}
+
+/**
+ * omap_hwmods_restore_context - Restores the HW reset line state for all hwmods
+ *
+ * Restores the HW reset line state of all the registered hwmods
+ */
+void omap_hwmods_restore_context(void)
+{
+       omap_hwmod_for_each(omap_hwmod_restore_context, NULL);
+}
index aea49d8e1e713377ee776ef63f78a8c57750a2cf..997a7d47c04eaef2bcac01c3dbd7162c2f5319f3 100644 (file)
@@ -168,6 +168,7 @@ struct omap_hwmod_rst_info {
        const char      *name;
        u8              rst_shift;
        u8              st_shift;
+       u8              context;
 };
 
 /**
@@ -678,6 +679,9 @@ extern void __init omap_hwmod_init(void);
 
 const char *omap_hwmod_get_main_clk(struct omap_hwmod *oh);
 
+void omap_hwmods_save_context(void);
+void omap_hwmods_restore_context(void);
+
 /*
  *
  */