]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/hwspinlock.git/commitdiff
sched/fair: Fix throttle_list starvation with low CFS quota
authorPhil Auld <pauld@redhat.com>
Mon, 8 Oct 2018 14:36:40 +0000 (10:36 -0400)
committerIngo Molnar <mingo@kernel.org>
Thu, 11 Oct 2018 11:10:18 +0000 (13:10 +0200)
With a very low cpu.cfs_quota_us setting, such as the minimum of 1000,
distribute_cfs_runtime may not empty the throttled_list before it runs
out of runtime to distribute. In that case, due to the change from
c06f04c7048 to put throttled entries at the head of the list, later entries
on the list will starve.  Essentially, the same X processes will get pulled
off the list, given CPU time and then, when expired, get put back on the
head of the list where distribute_cfs_runtime will give runtime to the same
set of processes leaving the rest.

Fix the issue by setting a bit in struct cfs_bandwidth when
distribute_cfs_runtime is running, so that the code in throttle_cfs_rq can
decide to put the throttled entry on the tail or the head of the list.  The
bit is set/cleared by the callers of distribute_cfs_runtime while they hold
cfs_bandwidth->lock.

This is easy to reproduce with a handful of CPU consumers. I use 'crash' on
the live system. In some cases you can simply look at the throttled list and
see the later entries are not changing:

  crash> list cfs_rq.throttled_list -H 0xffff90b54f6ade40 -s cfs_rq.runtime_remaining | paste - - | awk '{print $1"  "$4}' | pr -t -n3
    1     ffff90b56cb2d200  -976050
    2     ffff90b56cb2cc00  -484925
    3     ffff90b56cb2bc00  -658814
    4     ffff90b56cb2ba00  -275365
    5     ffff90b166a45600  -135138
    6     ffff90b56cb2da00  -282505
    7     ffff90b56cb2e000  -148065
    8     ffff90b56cb2fa00  -872591
    9     ffff90b56cb2c000  -84687
   10     ffff90b56cb2f000  -87237
   11     ffff90b166a40a00  -164582

  crash> list cfs_rq.throttled_list -H 0xffff90b54f6ade40 -s cfs_rq.runtime_remaining | paste - - | awk '{print $1"  "$4}' | pr -t -n3
    1     ffff90b56cb2d200  -994147
    2     ffff90b56cb2cc00  -306051
    3     ffff90b56cb2bc00  -961321
    4     ffff90b56cb2ba00  -24490
    5     ffff90b166a45600  -135138
    6     ffff90b56cb2da00  -282505
    7     ffff90b56cb2e000  -148065
    8     ffff90b56cb2fa00  -872591
    9     ffff90b56cb2c000  -84687
   10     ffff90b56cb2f000  -87237
   11     ffff90b166a40a00  -164582

Sometimes it is easier to see by finding a process getting starved and looking
at the sched_info:

  crash> task ffff8eb765994500 sched_info
  PID: 7800   TASK: ffff8eb765994500  CPU: 16  COMMAND: "cputest"
    sched_info = {
      pcount = 8,
      run_delay = 697094208,
      last_arrival = 240260125039,
      last_queued = 240260327513
    },
  crash> task ffff8eb765994500 sched_info
  PID: 7800   TASK: ffff8eb765994500  CPU: 16  COMMAND: "cputest"
    sched_info = {
      pcount = 8,
      run_delay = 697094208,
      last_arrival = 240260125039,
      last_queued = 240260327513
    },

Signed-off-by: Phil Auld <pauld@redhat.com>
Reviewed-by: Ben Segall <bsegall@google.com>
Cc: Linus Torvalds <torvalds@linux-foundation.org>
Cc: Peter Zijlstra <peterz@infradead.org>
Cc: Thomas Gleixner <tglx@linutronix.de>
Cc: stable@vger.kernel.org
Fixes: c06f04c70489 ("sched: Fix potential near-infinite distribute_cfs_runtime() loop")
Link: http://lkml.kernel.org/r/20181008143639.GA4019@pauld.bos.csb
Signed-off-by: Ingo Molnar <mingo@kernel.org>
kernel/sched/fair.c
kernel/sched/sched.h

index 7fc4a371bdd248ee94ffb7f5088bb86b5fa42262..f88e00705b558b04210c86b8198fb3589b94873c 100644 (file)
@@ -4476,9 +4476,13 @@ static void throttle_cfs_rq(struct cfs_rq *cfs_rq)
 
        /*
         * Add to the _head_ of the list, so that an already-started
-        * distribute_cfs_runtime will not see us
+        * distribute_cfs_runtime will not see us. If disribute_cfs_runtime is
+        * not running add to the tail so that later runqueues don't get starved.
         */
-       list_add_rcu(&cfs_rq->throttled_list, &cfs_b->throttled_cfs_rq);
+       if (cfs_b->distribute_running)
+               list_add_rcu(&cfs_rq->throttled_list, &cfs_b->throttled_cfs_rq);
+       else
+               list_add_tail_rcu(&cfs_rq->throttled_list, &cfs_b->throttled_cfs_rq);
 
        /*
         * If we're the first throttled task, make sure the bandwidth
@@ -4622,14 +4626,16 @@ static int do_sched_cfs_period_timer(struct cfs_bandwidth *cfs_b, int overrun)
         * in us over-using our runtime if it is all used during this loop, but
         * only by limited amounts in that extreme case.
         */
-       while (throttled && cfs_b->runtime > 0) {
+       while (throttled && cfs_b->runtime > 0 && !cfs_b->distribute_running) {
                runtime = cfs_b->runtime;
+               cfs_b->distribute_running = 1;
                raw_spin_unlock(&cfs_b->lock);
                /* we can't nest cfs_b->lock while distributing bandwidth */
                runtime = distribute_cfs_runtime(cfs_b, runtime,
                                                 runtime_expires);
                raw_spin_lock(&cfs_b->lock);
 
+               cfs_b->distribute_running = 0;
                throttled = !list_empty(&cfs_b->throttled_cfs_rq);
 
                cfs_b->runtime -= min(runtime, cfs_b->runtime);
@@ -4740,6 +4746,11 @@ static void do_sched_cfs_slack_timer(struct cfs_bandwidth *cfs_b)
 
        /* confirm we're still not at a refresh boundary */
        raw_spin_lock(&cfs_b->lock);
+       if (cfs_b->distribute_running) {
+               raw_spin_unlock(&cfs_b->lock);
+               return;
+       }
+
        if (runtime_refresh_within(cfs_b, min_bandwidth_expiration)) {
                raw_spin_unlock(&cfs_b->lock);
                return;
@@ -4749,6 +4760,9 @@ static void do_sched_cfs_slack_timer(struct cfs_bandwidth *cfs_b)
                runtime = cfs_b->runtime;
 
        expires = cfs_b->runtime_expires;
+       if (runtime)
+               cfs_b->distribute_running = 1;
+
        raw_spin_unlock(&cfs_b->lock);
 
        if (!runtime)
@@ -4759,6 +4773,7 @@ static void do_sched_cfs_slack_timer(struct cfs_bandwidth *cfs_b)
        raw_spin_lock(&cfs_b->lock);
        if (expires == cfs_b->runtime_expires)
                cfs_b->runtime -= min(runtime, cfs_b->runtime);
+       cfs_b->distribute_running = 0;
        raw_spin_unlock(&cfs_b->lock);
 }
 
@@ -4867,6 +4882,7 @@ void init_cfs_bandwidth(struct cfs_bandwidth *cfs_b)
        cfs_b->period_timer.function = sched_cfs_period_timer;
        hrtimer_init(&cfs_b->slack_timer, CLOCK_MONOTONIC, HRTIMER_MODE_REL);
        cfs_b->slack_timer.function = sched_cfs_slack_timer;
+       cfs_b->distribute_running = 0;
 }
 
 static void init_cfs_rq_runtime(struct cfs_rq *cfs_rq)
index 455fa330de0462db774f827a726478aa66abad3b..9683f458aec72823dfed413b5dc0a262836aaf85 100644 (file)
@@ -346,6 +346,8 @@ struct cfs_bandwidth {
        int                     nr_periods;
        int                     nr_throttled;
        u64                     throttled_time;
+
+       bool                    distribute_running;
 #endif
 };