rpmsg/hwspinlock.git
23 months agoarm64: dts: ti: k3-am65-main: Move hwspinlock node to main_navss interconnect hwspinlock-linux-4.19.y
Suman Anna [Fri, 31 May 2019 16:17:49 +0000 (11:17 -0500)]
arm64: dts: ti: k3-am65-main: Move hwspinlock node to main_navss interconnect

The commit c18a938bdbac ("arm64: dts: ti: k3-am65-main: Add hwspinlock
node") had previously added the HwSpinlock node directly under the
cbass_main interconnect node even though it is connected on the Main
NavSS local interconnect. The Main NavSS interconnect is represented
as its own interconnect node, so move this node under the main_navss
interconnect node.

Signed-off-by: Suman Anna <s-anna@ti.com>
2 years agoti_config_fragments: v8_rpmsg: Enable OMAP HwSpinlock driver
Suman Anna [Thu, 8 Mar 2018 00:23:18 +0000 (18:23 -0600)]
ti_config_fragments: v8_rpmsg: Enable OMAP HwSpinlock driver

The OMAP HwSpinlock driver is reused for supporting the HwSpinlock
IP within K3 platforms. So, enable both the HwSpinlock core and the
OMAP HwSpinlock driver in the rpmsg config file. There are currently
no direct users of the HwSpinlock IP, but the built-in is the
preferred choice for this driver.

Signed-off-by: Suman Anna <s-anna@ti.com>
2 years agoarm64: dts: ti: k3-am65-main: Add hwspinlock node
Suman Anna [Fri, 29 Jun 2018 20:27:36 +0000 (15:27 -0500)]
arm64: dts: ti: k3-am65-main: Add hwspinlock node

The Main NavSS block on AM65x SoCs contains a HwSpinlock IP instance
that is similar to the IP on some OMAP SoCs. Add the DT node for this
on AM65x SoCs. The node is present within the NavSS block, and is
added as a child node under the cbass_main node.

NOTE:
The node should be moved into a navss_main interconnect node if the
local interconnect of Main NavSS is represented as a child node of
the cbass_main interconnect node in the future.

Signed-off-by: Suman Anna <s-anna@ti.com>
2 years agohwspinlock/omap: Add support for TI K3 SoCs
Suman Anna [Fri, 29 Jun 2018 22:45:45 +0000 (17:45 -0500)]
hwspinlock/omap: Add support for TI K3 SoCs

The HwSpinlock IP is also present on the newer TI K3 AM65x family of
SoCs. Reuse the existing OMAP Hwspinlock driver to extend the support
for this IP on K3 AM65x SoCs as well.

Signed-off-by: Suman Anna <s-anna@ti.com>
2 years agodt-bindings: hwlock: Update OMAP binding for TI K3 AM65x SoCs
Suman Anna [Wed, 12 Sep 2018 16:03:00 +0000 (11:03 -0500)]
dt-bindings: hwlock: Update OMAP binding for TI K3 AM65x SoCs

The TI K3 AM65x family of SoCs have a HwSpinlock IP that is based
on the existing HwSpinlock IP present in OMAP architecture based
SoCs. Update the existing OMAP HwSpinlock binding for this IP on
TI K3 AM65x SoCs.

Signed-off-by: Suman Anna <s-anna@ti.com>
2 years agohwspinlock/omap: Add a trace during probe
Suman Anna [Thu, 6 Jul 2017 16:49:49 +0000 (11:49 -0500)]
hwspinlock/omap: Add a trace during probe

Add a debug level trace statement in the OMAP HwSpinlock driver
probe function to print a successful registration.

Signed-off-by: Suman Anna <s-anna@ti.com>
2 years agoti_config_fragments: v8_defconfig_map: Add v8 rpmsg config file
Suman Anna [Tue, 11 Dec 2018 16:48:17 +0000 (10:48 -0600)]
ti_config_fragments: v8_defconfig_map: Add v8 rpmsg config file

Add the RPMsg domain config fragment file v8_ipc.cfg file for
all the defconfigs in the v8 defconfig map file, so that the
various RPMsg related drivers can be enabled and built using
the defconfig builder tool for K3 platforms.

Signed-off-by: Suman Anna <s-anna@ti.com>
2 years agoti_config_fragments: v8_rpmsg: Add RPMsg domain config fragment file
Suman Anna [Thu, 18 Jan 2018 00:56:44 +0000 (18:56 -0600)]
ti_config_fragments: v8_rpmsg: Add RPMsg domain config fragment file

Add an initial IPC/RPMsg domain config fragment file specifically for
v8 platforms. This will form the foundation for adding all the RPMsg
related module configurations for TI K3 platforms.

Signed-off-by: Suman Anna <s-anna@ti.com>
2 years agoti_config_fragments: defconfig_map: Include RPMsg config fragment
Suman Anna [Tue, 11 Dec 2018 17:20:41 +0000 (11:20 -0600)]
ti_config_fragments: defconfig_map: Include RPMsg config fragment

Add the RPMsg domain config fragment file ipc.cfg file for all the
defconfigs in the defconfig map file, so that the various RPMsg
related drivers can be enabled and built using the defconfig builder
tool.

Signed-off-by: Suman Anna <s-anna@ti.com>
2 years agoti_config_fragments: rpmsg: Add RPMsg domain config fragment file
Suman Anna [Tue, 11 Dec 2018 17:29:22 +0000 (11:29 -0600)]
ti_config_fragments: rpmsg: Add RPMsg domain config fragment file

Add the initial IPC/RPMsg domain config fragment file. This will
form the foundation for adding all the RPMsg related module
configurations, to be used by the TI Linux integration kernel.

Also, enable the fully upstreamed (on OMAP2+ SoCs) OMAP HwSpinlock
and OMAP Mailbox drivers including the corresponding HwSpinlock and
Mailbox cores. These are chosen to be built-in as it is the preferred
choice for these drivers.

Signed-off-by: Suman Anna <s-anna@ti.com>
2 years agoMerge branch 'platform-ti-linux-4.19.y' of git://git.ti.com/~rrnayak/ti-linux-kernel...
Suman Anna [Tue, 11 Dec 2018 16:17:54 +0000 (10:17 -0600)]
Merge branch 'platform-ti-linux-4.19.y' of git://git.ti.com/~rrnayak/ti-linux-kernel/platform-linux-feature-tree into hwspinlock-linux-4.19.y

Pull in the platform base tree into the hwspinlock feature tree. The
merge pulls in the necessary board support for all the AM65x boards.
All the other boards are already supported on vanilla 4.19 kernel.
It also pulls in the defconfig_builder infrastructure used by TI
Integration kernels. This allows the required IPC driver support to
be added on the TI K3 family of SoCs.

* 'platform-ti-linux-4.19.y' of git://git.ti.com/~rrnayak/ti-linux-kernel/platform-linux-feature-tree: (123 commits)
  dmaengine: ti: k3-udma: Try to use the highest TPL channels for MEM_TO_MEM
  dmaengine: ti: k3-udma: Only allow MEM_TO_MEM transfer on the main UDMA
  ti_config_fragments/defconfig_map.txt: add missing baseport.cfg entries
  ti_config_fragments: v8_baseport: Forward port v8_baseport cfg from 4.14
  arm64: dts: ti: k3-am6: Add NAVSS and PDMA nodes
  dmaengine: ti: k3-udma: Add glue layer for non DMAengine users
  dmaengine: ti: New driver for K3 UDMA
  dmaengine: ti: Add cppi5 header for UDMA
  dt-bindings: dma: ti: Add document for K3 UDMA
  dmaengine: Add function to request slave channel from a dma_device
  dmaengine: Add support for reporting DMA cached data amount
  dmaengine: Add metadata_ops for dma_async_tx_descriptor
  dmaengine: doc: Add sections for per descriptor metadata support
  soc: ti: k3: add navss ringacc driver
  bindings: soc: ti: add documentation for k3 ringacc
  firmware: ti_sci: Add resource management APIs for ringacc, psi-l and udma
  ti_config_fragments: v8_baseport: enable K3 thermal
  arm64: dts: ti: am6: Add VTM node
  arm64: dts: ti: am654: Add thermal zones
  thermal: k3: Add support for bandgap sensors
  ...

Signed-off-by: Suman Anna <s-anna@ti.com>
2 years agodmaengine: ti: k3-udma: Try to use the highest TPL channels for MEM_TO_MEM
Peter Ujfalusi [Thu, 29 Nov 2018 08:06:42 +0000 (10:06 +0200)]
dmaengine: ti: k3-udma: Try to use the highest TPL channels for MEM_TO_MEM

When running memcpy test with big buffers:

echo 800000 > /sys/module/dmatest/parameters/test_buf_size
echo 2000 > /sys/module/dmatest/parameters/timeout
echo 20 > /sys/module/dmatest/parameters/iterations
echo 10 > /sys/module/dmatest/parameters/max_channels
echo 1 > /sys/module/dmatest/parameters/run

The throughput with normal channels is:
dmatest: dma1chan2-copy0: summary 200 tests, 0 failures 87 iops 308840 KB/s (0)

Using High Throughput channel with the same setup:
dmatest: dma1chan2-copy0: summary 200 tests, 0 failures 295 iops 1206172 KB/s (0)

The speed increase is about 4x.

Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com>
2 years agodmaengine: ti: k3-udma: Only allow MEM_TO_MEM transfer on the main UDMA
Peter Ujfalusi [Wed, 28 Nov 2018 13:57:47 +0000 (15:57 +0200)]
dmaengine: ti: k3-udma: Only allow MEM_TO_MEM transfer on the main UDMA

memcpy via the mcu UDMA is much slower compared to main UDMA:

mcu_udma:  dmatest: dma0chan0-copy0: summary 200 tests, 0 failures 41 iops 165997 KB/s (0)
main_udma: dmatest: dma1chan2-copy0: summary 200 tests, 0 failures 87 iops 308840 KB/s (0)

We have enough channels on the main UDMA for memcpy, so disable the support
for MEM_TO_MEM on the mcu side.

Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com>
2 years agoti_config_fragments/defconfig_map.txt: add missing baseport.cfg entries
Sekhar Nori [Thu, 29 Nov 2018 08:46:04 +0000 (14:16 +0530)]
ti_config_fragments/defconfig_map.txt: add missing baseport.cfg entries

baseport.cfg is missing from some defconfig targets. Add it.

Verified that baseport.cfg was present for these targets in
v4.14 based kernel.

Boot tested on DA850 EVM, build tested with ti_sdk_omap2_rt_release
target.

Fixes: 2a38f5aebdae ("ti_config_fragments/defconfig_map.txt: add baseport.cfg")
Signed-off-by: Sekhar Nori <nsekhar@ti.com>
2 years agoti_config_fragments: v8_baseport: Forward port v8_baseport cfg from 4.14
Tero Kristo [Thu, 29 Nov 2018 13:30:10 +0000 (15:30 +0200)]
ti_config_fragments: v8_baseport: Forward port v8_baseport cfg from 4.14

Forward port the v8_baseport config fragment from 4.14 kernel.

Signed-off-by: Tero Kristo <t-kristo@ti.com>
2 years agoarm64: dts: ti: k3-am6: Add NAVSS and PDMA nodes
Peter Ujfalusi [Wed, 28 Nov 2018 10:48:15 +0000 (12:48 +0200)]
arm64: dts: ti: k3-am6: Add NAVSS and PDMA nodes

Add nodes and sub nodes for both NAVSS (main and mcu) and add the PDMA
nodes as well.

Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com>
2 years agodmaengine: ti: k3-udma: Add glue layer for non DMAengine users
Grygorii Strashko [Wed, 28 Nov 2018 10:48:14 +0000 (12:48 +0200)]
dmaengine: ti: k3-udma: Add glue layer for non DMAengine users

Certain users can not use right now the DMAengine API due to missing
features in the core. Prime example is Networking.

These users can use the glue layer interface to avoid misuse of DMAengine
API and when the core gains the needed features they can be converted to
use generic API.

Signed-off-by: Grygorii Strashko <grygorii.strashko@ti.com>
Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com>
2 years agodmaengine: ti: New driver for K3 UDMA
Peter Ujfalusi [Wed, 28 Nov 2018 10:48:13 +0000 (12:48 +0200)]
dmaengine: ti: New driver for K3 UDMA

DMA driver for
Texas Instruments K3 NAVSS Unified DMA – Peripheral Root Complex (UDMA-P)

The UDMA-P is intended to perform similar (but significantly upgraded) functions
as the packet-oriented DMA used on previous SoC devices. The UDMA-P module
supports the transmission and reception of various packet types. The UDMA-P is
architected to facilitate the segmentation and reassembly of SoC DMA data
structure compliant packets to/from smaller data blocks that are natively
compatible with the specific requirements of each connected peripheral. Multiple
Tx and Rx channels are provided within the DMA which allow multiple segmentation
or reassembly operations to be ongoing. The DMA controller maintains state
information for each of the channels which allows packet segmentation and
reassembly operations to be time division multiplexed between channels in order
to share the underlying DMA hardware. An external DMA scheduler is used to
control the ordering and rate at which this multiplexing occurs for Transmit
operations. The ordering and rate of Receive operations is indirectly controlled
by the order in which blocks are pushed into the DMA on the Rx PSI-L interface.

The UDMA-P also supports acting as both a UTC and UDMA-C for its internal
channels. Channels in the UDMA-P can be configured to be either Packet-Based or
Third-Party channels on a channel by channel basis.

The initial driver supports:
- MEM_TO_MEM (TR mode)
- DEV_TO_MEM (Packet / TR mode)
- MEM_TO_DEV (Packet / TR mode)
- Cyclic (Packet / TR mode)
- Metadata for descriptors

Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com>
2 years agodmaengine: ti: Add cppi5 header for UDMA
Peter Ujfalusi [Wed, 28 Nov 2018 10:48:12 +0000 (12:48 +0200)]
dmaengine: ti: Add cppi5 header for UDMA

Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com>
2 years agodt-bindings: dma: ti: Add document for K3 UDMA
Peter Ujfalusi [Wed, 28 Nov 2018 10:48:11 +0000 (12:48 +0200)]
dt-bindings: dma: ti: Add document for K3 UDMA

New binding document for
Texas Instruments K3 NAVSS Unified DMA – Peripheral Root Complex (UDMA-P).

UDMA-P is introduced as part of the K3 architecture and can be found on
AM65x SoC.

Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com>
2 years agodmaengine: Add function to request slave channel from a dma_device
Peter Ujfalusi [Wed, 28 Nov 2018 10:48:10 +0000 (12:48 +0200)]
dmaengine: Add function to request slave channel from a dma_device

dma_get_any_slave_channel() would skip using the filter function, which
in some cases needed to be executed before the alloc_chan_resources
callback to make sure that all parameters are provided for the slave
channel.

Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com>
2 years agodmaengine: Add support for reporting DMA cached data amount
Peter Ujfalusi [Wed, 28 Nov 2018 10:48:09 +0000 (12:48 +0200)]
dmaengine: Add support for reporting DMA cached data amount

A DMA hardware can have big cache or FIFO and the amount of data sitting in
the DMA fabric can be an interest for the clients.

For example in audio we want to know the delay in the data flow and in case
the DMA have significantly large FIFO/cache, it can affect the latenc/delay

Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com>
2 years agodmaengine: Add metadata_ops for dma_async_tx_descriptor
Peter Ujfalusi [Wed, 28 Nov 2018 10:48:08 +0000 (12:48 +0200)]
dmaengine: Add metadata_ops for dma_async_tx_descriptor

The metadata is best described as side band data or parameters traveling
alongside the data DMAd by the DMA engine. It is data
which is understood by the peripheral and the peripheral driver only, the
DMA engine see it only as data block and it is not interpreting it in any
way.

The metadata can be different per descriptor as it is a parameter for the
data being transferred.

If the DMA supports per descriptor metadata it can implement the attach,
get_ptr/set_len callbacks.

Client drivers must only use either attach or get_ptr/set_len to avoid
misconfiguration.

Client driver can check if a given metadata mode is supported by the
channel during probe time with
dmaengine_is_metadata_mode_supported(chan, DESC_METADATA_CLIENT);
dmaengine_is_metadata_mode_supported(chan, DESC_METADATA_ENGINE);

and based on this information can use either mode.

Wrappers are also added for the metadata_ops.

To be used in DESC_METADATA_CLIENT mode:
dmaengine_desc_attach_metadata()

To be used in DESC_METADATA_ENGINE mode:
dmaengine_desc_get_metadata_ptr()
dmaengine_desc_set_metadata_len()

Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com>
2 years agodmaengine: doc: Add sections for per descriptor metadata support
Peter Ujfalusi [Wed, 28 Nov 2018 10:48:07 +0000 (12:48 +0200)]
dmaengine: doc: Add sections for per descriptor metadata support

Update the provider and client documentation with details about the
metadata support.

Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com>
2 years agosoc: ti: k3: add navss ringacc driver
Grygorii Strashko [Wed, 28 Nov 2018 10:48:06 +0000 (12:48 +0200)]
soc: ti: k3: add navss ringacc driver

The Ring Accelerator (RINGACC or RA) provides hardware acceleration to
enable straightforward passing of work between a producer and a consumer.
There is one RINGACC module per NAVSS on TI AM65x SoCs.

The RINGACC converts constant-address read and write accesses to equivalent
read or write accesses to a circular data structure in memory. The RINGACC
eliminates the need for each DMA controller which needs to access ring
elements from having to know the current state of the ring (base address,
current offset). The DMA controller performs a read or write access to a
specific address range (which maps to the source interface on the RINGACC)
and the RINGACC replaces the address for the transaction with a new address
which corresponds to the head or tail element of the ring (head for reads,
tail for writes). Since the RINGACC maintains the state, multiple DMA
controllers or channels are allowed to coherently share the same rings as
applicable. The RINGACC is able to place data which is destined towards
software into cached memory directly.

Supported ring modes:
- Ring Mode
- Messaging Mode
- Credentials Mode
- Queue Manager Mode

TI-SCI integration:

Texas Instrument's System Control Interface (TI-SCI) Message Protocol now
has control over Ringacc module resources management (RM) and Rings
configuration.

The corresponding support of TI-SCI Ringacc module RM protocol
introduced as option through DT parameters:
- ti,sci: phandle on TI-SCI firmware controller DT node
- ti,sci-dev-id: TI-SCI device identifier as per TI-SCI firmware spec

if both parameters present - Ringacc driver will configure/free/reset Rings
using TI-SCI Message Ringacc RM Protocol.

The Ringacc driver manages Rings allocation by itself now and requests
TI-SCI firmware to allocate and configure specific Rings only. It's done
this way because, Linux driver implements two stage Rings allocation and
configuration (allocate ring and configure ring) while I-SCI Message
Protocol supports only one combined operation (allocate+configure).

Grygorii Strashko <grygorii.strashko@ti.com>
Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com>
2 years agobindings: soc: ti: add documentation for k3 ringacc
Grygorii Strashko [Wed, 28 Nov 2018 10:48:05 +0000 (12:48 +0200)]
bindings: soc: ti: add documentation for k3 ringacc

The Ring Accelerator (RINGACC or RA) provides hardware acceleration to
enable straightforward passing of work between a producer and a consumer.
There is one RINGACC module per NAVSS on TI AM65x SoCs.

This patch introduces RINGACC device tree bindings.

Signed-off-by: Grygorii Strashko <grygorii.strashko@ti.com>
2 years agofirmware: ti_sci: Add resource management APIs for ringacc, psi-l and udma
Peter Ujfalusi [Wed, 28 Nov 2018 10:48:04 +0000 (12:48 +0200)]
firmware: ti_sci: Add resource management APIs for ringacc, psi-l and udma

TISCI abstracts the management of NAVSS resources, like UDMA channels,
flows, rings.

Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com>
2 years agoti_config_fragments: v8_baseport: enable K3 thermal
Keerthy [Mon, 26 Nov 2018 07:41:00 +0000 (13:11 +0530)]
ti_config_fragments: v8_baseport: enable K3 thermal

K3 thermal driver is disabled by default, so enable it.

Signed-off-by: Keerthy <j-keerthy@ti.com>
Signed-off-by: Tero Kristo <t-kristo@ti.com>
2 years agoarm64: dts: ti: am6: Add VTM node
Keerthy [Mon, 26 Nov 2018 07:40:59 +0000 (13:10 +0530)]
arm64: dts: ti: am6: Add VTM node

VTM stands for voltage and thermal management. Add the vtm node and
the associated thermal zones on the SoC.

Reviewed-by: Suman Anna <s-anna@ti.com>
Signed-off-by: Keerthy <j-keerthy@ti.com>
2 years agoarm64: dts: ti: am654: Add thermal zones
Keerthy [Mon, 26 Nov 2018 07:40:58 +0000 (13:10 +0530)]
arm64: dts: ti: am654: Add thermal zones

The am654 SoC has three thermal zones namely MPU0, MPU1 and MCU
zones

Reviewed-by: Suman Anna <s-anna@ti.com>
Signed-off-by: Keerthy <j-keerthy@ti.com>
2 years agothermal: k3: Add support for bandgap sensors
Keerthy [Mon, 26 Nov 2018 07:40:57 +0000 (13:10 +0530)]
thermal: k3: Add support for bandgap sensors

Add support for bandgap sensors. Currently reading temperatures
and trend computing is supported.

Reviewed-by: Suman Anna <s-anna@ti.com>
Signed-off-by: Keerthy <j-keerthy@ti.com>
2 years agodt-bindings: thermal: k3: Add VTM bindings documentation
Keerthy [Mon, 26 Nov 2018 07:40:56 +0000 (13:10 +0530)]
dt-bindings: thermal: k3: Add VTM bindings documentation

Add VTM bindings documentation. In the Voltage Thermal
Management Module(VTM), K3 AM654 supplies a voltage
reference and a temperature sensor feature that are gathered in the band
gap voltage and temperature sensor (VBGAPTS) module. The band
gap provides current and voltage reference for its internal
circuits and other analog IP blocks. The analog-to-digital
converter (ADC) produces an output value that is proportional
to the silicon temperature.

Reviewed-by: Suman Anna <s-anna@ti.com>
Signed-off-by: Keerthy <j-keerthy@ti.com>
2 years agoarm64: dts: ti: am654-base-board: Add gpio_keys node
Keerthy [Mon, 26 Nov 2018 07:40:55 +0000 (13:10 +0530)]
arm64: dts: ti: am654-base-board: Add gpio_keys node

There are 2 push buttons: SW5 and SW6 that are basically connected to
WKUP_GPIO0_24 and WKUP_GPIO0_27 respectively. Add the respective
nodes and the pinctrl data to set the mode to GPIO and Input.

Signed-off-by: Keerthy <j-keerthy@ti.com>
2 years agoarm64: configs: Enable GPIO_DAVINCI
Keerthy [Mon, 26 Nov 2018 07:40:54 +0000 (13:10 +0530)]
arm64: configs: Enable GPIO_DAVINCI

Enable GPIO_DAVINCI for K3 platforms.

Signed-off-by: Keerthy <j-keerthy@ti.com>
2 years agoarm64: dts: ti: am6: Add gpio nodes
Keerthy [Mon, 26 Nov 2018 07:40:53 +0000 (13:10 +0530)]
arm64: dts: ti: am6: Add gpio nodes

Add gpio0 and gpio1 nodes under MAIN domain and gpio0
under WAKEUP domain.

Signed-off-by: Keerthy <j-keerthy@ti.com>
Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
2 years agogpio: Davinci: Add K3 Specific dependencies
Keerthy [Mon, 26 Nov 2018 07:40:52 +0000 (13:10 +0530)]
gpio: Davinci: Add K3 Specific dependencies

Add K3 Specific dependencies

Signed-off-by: Keerthy <j-keerthy@ti.com>
2 years agogpio: davinci: Fix the compiler warning with ARM64 config enabled
Keerthy [Mon, 26 Nov 2018 07:40:51 +0000 (13:10 +0530)]
gpio: davinci: Fix the compiler warning with ARM64 config enabled

Fix the compiler warning with ARM64 config enabled

Signed-off-by: Keerthy <j-keerthy@ti.com>
2 years agoarm64: dts: ti: k3-am654-base-board: Add I2C nodes
Vignesh R [Mon, 26 Nov 2018 07:40:50 +0000 (13:10 +0530)]
arm64: dts: ti: k3-am654-base-board: Add I2C nodes

commit e5f4b4ba3d223426cdab582f5a67a841f2b01081 upstream

Add DT entries for I2C instances present in AM654 SoC.

Signed-off-by: Vignesh R <vigneshr@ti.com>
Acked-by: Nishanth Menon <nm@ti.com>
2 years agoarm64: dts: ti: am654-base-board: Add pinmux for main uart0
Vignesh R [Mon, 26 Nov 2018 07:40:49 +0000 (13:10 +0530)]
arm64: dts: ti: am654-base-board: Add pinmux for main uart0

commit 27e0e5f65dd05167283cf707ae89e19630b0289d upstream

Add pinmux for main uart0 that is serves as console on AM654 EVM

Signed-off-by: Vignesh R <vigneshr@ti.com>
Acked-by: Nishanth Menon <nm@ti.com>
2 years agoarm64: dts: ti: k3-am65: Add pinctrl regions
Tero Kristo [Mon, 26 Nov 2018 07:40:48 +0000 (13:10 +0530)]
arm64: dts: ti: k3-am65: Add pinctrl regions

commit ffff31e50509eaeea12df0ea2513fc648359b6bd upstream

Add pinctrl regions for the main and wkup mmr.

The range for main pinctrl region contains a gap
at offset 0x2e4, and because of this, the pinctrl
range is split into two sections.

Signed-off-by: Tero Kristo <t-kristo@ti.com>
Signed-off-by: Vignesh R <vigneshr@ti.com>
Acked-by: Nishanth Menon <nm@ti.com>
2 years agodt-bindings: pinctrl: k3: Introduce pinmux definitions
Vignesh R [Mon, 26 Nov 2018 07:40:47 +0000 (13:10 +0530)]
dt-bindings: pinctrl: k3: Introduce pinmux definitions

commit 4d82c9ec96fd25cb4c126df2e14862df434ee185 upstream

The dt-bindings header for TI K3 AM6 SoCs define a set of macros for
defining pinmux configs in human readable form, instead of raw-coded
hex values.

Signed-off-by: Vignesh R <vigneshr@ti.com>
Acked-by: Linus Walleij <linus.walleij@linaro.org>
Reviewed-by: Rob Herring <robh@kernel.org>
Acked-by: Nishanth Menon <nm@ti.com>
Acked-by: Tony Lindgren <tony@atomide.com>
2 years agoarm64: dts: ti: am654: Add interrupt controller nodes
Lokesh Vutla [Fri, 23 Nov 2018 09:38:05 +0000 (15:08 +0530)]
arm64: dts: ti: am654: Add interrupt controller nodes

Add DT nodes for the interrupt routers and aggregators in the AM65x SoC.

Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com>
2 years agoarm64: dts: ti: am654: Update compatible for dmsc
Lokesh Vutla [Fri, 23 Nov 2018 09:38:04 +0000 (15:08 +0530)]
arm64: dts: ti: am654: Update compatible for dmsc

Use the am654 specific compatible for dmsc. This allows to use
the am654 specific RM mapping table.

Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
2 years agosoc: ti: am6: Enable interrupt controller drivers
Lokesh Vutla [Fri, 23 Nov 2018 09:38:03 +0000 (15:08 +0530)]
soc: ti: am6: Enable interrupt controller drivers

Select all the TISCI dependent interrupt controller drivers
for AM6 SoC.

Suggested-by: Marc Zyngier <marc.zyngier@arm.com>
Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
2 years agoirqchip: ti-sci-inta: Add support for Interrupt Aggregator driver
Lokesh Vutla [Fri, 23 Nov 2018 09:38:02 +0000 (15:08 +0530)]
irqchip: ti-sci-inta: Add support for Interrupt Aggregator driver

Texas Instruments' K3 generation SoCs has an IP Interrupt Aggregator
which is an interrupt controller that does the following:
- Converts events to interrupts that can be understood by
  an interrupt router.
- Allows for multiplexing of events to interrupts.
- Allows for grouping of multiple events to a single interrupt.

Configuration of the interrupt aggregator registers can only be done by
a system co-processor and the driver needs to send a message to this
co processor over TISCI protocol.

Add support for Interrupt Aggregator driver over TISCI protocol.

Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com>
2 years agodt-bindings: irqchip: Introduce TISCI Interrupt Aggregator bindings
Lokesh Vutla [Fri, 23 Nov 2018 09:38:01 +0000 (15:08 +0530)]
dt-bindings: irqchip: Introduce TISCI Interrupt Aggregator bindings

Add the DT binding documentation for Interrupt Aggregator driver.

Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
2 years agoirqchip: ti-sci-intr: Add support for Interrupt Router driver
Lokesh Vutla [Fri, 23 Nov 2018 09:38:00 +0000 (15:08 +0530)]
irqchip: ti-sci-intr: Add support for Interrupt Router driver

Texas Instruments' K3 generation SoCs has an IP Interrupt Router
that does allows for multiplexing of input interrupts to host
interrupt controller. Interrupt Router inputs are either from a
peripheral or from an Interrupt Aggregator which is another
interrupt controller.

Configuration of the interrupt router registers can only be done by
a system co-processor and the driver needs to send a message to this
co processor over TISCI protocol.

Add support for Interrupt Router driver over TISCI protocol.

Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
2 years agodt-bindings: irqchip: Introduce TISCI Interrupt router bindings
Lokesh Vutla [Fri, 23 Nov 2018 09:37:59 +0000 (15:07 +0530)]
dt-bindings: irqchip: Introduce TISCI Interrupt router bindings

Add the DT binding documentation for Interrupt router driver.

Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
2 years agofirmware: ti_sci: Add helper apis to manage resources
Lokesh Vutla [Fri, 23 Nov 2018 09:37:58 +0000 (15:07 +0530)]
firmware: ti_sci: Add helper apis to manage resources

Each resource with in the device can be uniquely identified
by a type and subtype as defined by TISCI. Since this is generic
across the devices, resource allocation also can be made generic
instead of each client driver handling the resource. So add helper
apis to manage the resource.

Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
2 years agofirmware: ti_sci: Add RM mapping table for am654
Peter Ujfalusi [Fri, 23 Nov 2018 09:37:57 +0000 (15:07 +0530)]
firmware: ti_sci: Add RM mapping table for am654

Add the resource mapping table for AM654 SoC as defined
in http://downloads.ti.com/tisci/esd/latest/5_soc_doc/am6x/resasg_types.html
Introduce a new compatible for AM654 "ti,am654-sci" for using
this resource map table.

Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com>
Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
2 years agofirmware: ti_sci: Add support for IRQ management
Lokesh Vutla [Fri, 23 Nov 2018 09:37:56 +0000 (15:07 +0530)]
firmware: ti_sci: Add support for IRQ management

TISCI abstracts the handling of IRQ routes where interrupt sources
are not directly connected to interrupt controller. Add support for
the set of TISCI commands for requesting and releasing IRQs.

Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
2 years agofirmware: ti_sci: Add support for RM core ops
Lokesh Vutla [Fri, 23 Nov 2018 09:37:55 +0000 (15:07 +0530)]
firmware: ti_sci: Add support for RM core ops

TISCI provides support for getting the resources(IRQ, RING etc..)
assigned to a specific device. These resources can be handled by
the client and in turn sends TISCI cmd to configure the resources.

It is very important that client should keep track on usage of these
resources.

Add support for TISCI commands to get resource ranges.

Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com>
2 years agofirmware: ti_sci: Add support to get TISCI handle using of_phandle
Grygorii Strashko [Fri, 23 Nov 2018 09:37:54 +0000 (15:07 +0530)]
firmware: ti_sci: Add support to get TISCI handle using of_phandle

TISCI has been updated to have support for Resource management(likes
interrupts etc..). And there can be multiple device instances of a
resource type in a SoC. So every driver corresponding to a resource type
should get a TISCI handle so that it can make TISCI calls. And each
DT node corresponding to a device should exist under its corresponding
bus node as per the SoC architecture.

But existing apis in TISCI library assumes that all TISCI users are
child nodes of TISCI. Which is not true in the above case. So introduce
(devm_)ti_sci_get_by_phandle() apis that can be used by TISCI users
to get TISCI handle using of phandle property.

Signed-off-by: Grygorii Strashko <grygorii.strashko@ti.com>
Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
2 years agoarm64: enable dtb overlay merging support based on configs provided
Tero Kristo [Sun, 17 Jun 2018 19:30:40 +0000 (22:30 +0300)]
arm64: enable dtb overlay merging support based on configs provided

Add dtb-merger tool support to arm64 TI build. The merged configs are
defined by providing proper .its files.

Signed-off-by: Tero Kristo <t-kristo@ti.com>
2 years agoarm64: enable .dtbo file building for TI arm64 SoCs
Tero Kristo [Sun, 17 Jun 2018 19:30:39 +0000 (22:30 +0300)]
arm64: enable .dtbo file building for TI arm64 SoCs

Add support for building .dtso files into .dtbo binaries. Also change
the base .dtb files to contain symbols for overlay applying purposes.

Signed-off-by: Tero Kristo <t-kristo@ti.com>
2 years agoARM: dts: dt-overlays: add support for am57xx-evm
Tero Kristo [Mon, 27 Nov 2017 09:24:15 +0000 (11:24 +0200)]
ARM: dts: dt-overlays: add support for am57xx-evm

Add support for building FIT image for am57xx-evm. This FIT image
includes support for base am57xx-beagle boards (rev A2 and C) and
AM57xx-evm overlay.

Signed-off-by: Tero Kristo <t-kristo@ti.com>
2 years agoscripts/dtb-merge: add tool for merging DTB overlays
Tero Kristo [Fri, 2 Mar 2018 09:09:16 +0000 (11:09 +0200)]
scripts/dtb-merge: add tool for merging DTB overlays

Add tool for merging DT overlays into single DTB file. This parses
all the available .its files to find out the configuration needed
for the DTB. Once matching config is found, passes the data
to fdtoverlay tool to merge everything into a single .dtb.

Signed-off-by: Tero Kristo <t-kristo@ti.com>
2 years agoscripts/dtc: Bring in upstream version of fdtoverlay tool
Tero Kristo [Fri, 2 Mar 2018 07:21:18 +0000 (09:21 +0200)]
scripts/dtc: Bring in upstream version of fdtoverlay tool

Bring in upstream version v1.4.5.6-gc1e55a5513e9 of the fdtoverlay tool.
Copied over the fdtoverlay.c source as such, and updated the Makefile
to build the tool.

Signed-off-by: Tero Kristo <t-kristo@ti.com>
2 years agoARM: dts: dt-overlays: Add base support for DT overlay building
Tero Kristo [Thu, 22 Nov 2018 15:54:34 +0000 (17:54 +0200)]
ARM: dts: dt-overlays: Add base support for DT overlay building

Add base support for DT overlay building for TI SoCs. Adds support
for building .dtso files into .dtbo, and building .its files into
.itb for FIT image support. Also, add new kernel build target for
building all available FIT images (make itbs.)

Signed-off-by: Tero Kristo <t-kristo@ti.com>
2 years agoARM: dts: dra76x: add support for OPP_PLUS
Tero Kristo [Thu, 29 Mar 2018 05:53:29 +0000 (08:53 +0300)]
ARM: dts: dra76x: add support for OPP_PLUS

Add support for the OPP_PLUS (1.8GHz) for MPU.

Signed-off-by: Tero Kristo <t-kristo@ti.com>
2 years agocpufreq: ti-cpufreq: Add support for OPP_PLUS
Lokesh Vutla [Mon, 31 Jul 2017 05:52:32 +0000 (11:22 +0530)]
cpufreq: ti-cpufreq: Add support for OPP_PLUS

DRA762 SoC introduces OPP_PLUS which runs at 1.8GHz. Add
support for this OPP in ti-cpufreq driver.

Acked-by: Dave Gerlach <d-gerlach@ti.com>
Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
2 years agoti_config_fragments: omap_soc: enable RAS
Tero Kristo [Tue, 20 Nov 2018 10:06:01 +0000 (12:06 +0200)]
ti_config_fragments: omap_soc: enable RAS

Enable reliability, availability and serviceability kernel features.
This is needed as a dependency for EDAC.

Signed-off-by: Tero Kristo <t-kristo@ti.com>
2 years agoARM: dts: am574x-idk: add support for EMIF1 ECC
Tero Kristo [Thu, 5 Oct 2017 12:10:38 +0000 (15:10 +0300)]
ARM: dts: am574x-idk: add support for EMIF1 ECC

EMIF1 has ECC support, so add the DT node with address and interrupt
details to handle this.

Signed-off-by: Tero Kristo <t-kristo@ti.com>
2 years agoarm64: defconfig: Enable SERIAL_8250_OMAP
Lokesh Vutla [Thu, 8 Nov 2018 00:22:36 +0000 (18:22 -0600)]
arm64: defconfig: Enable SERIAL_8250_OMAP

commit d59c774496a2ee824836aaee1975ed23577edfd1 upstream

Enabling CONFIG_SERIAL_8250_OMAP that is used by TI's
AM6 SoC.

Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
Acked-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Arnd Bergmann <arnd@arndb.de>
Signed-off-by: Nishanth Menon <nm@ti.com>
2 years agoarm64: defconfig: Enable TI_SCI related configs
Lokesh Vutla [Thu, 8 Nov 2018 00:22:35 +0000 (18:22 -0600)]
arm64: defconfig: Enable TI_SCI related configs

commit 41925a21cdb58d07d6cad4f30539d1cee7a25d7b upstream

Enable TI System Control Interface (TI_SCI) Message Protocol library
and it's relevant power management drivers using this library.

TI's AM6 SoC uses this TI_SCI library to communicate to its system
controller(DMSC). While at it, enable TI_MESSAGE_MANAGER mailbox driver
using which this communication happens.

Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
Acked-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Arnd Bergmann <arnd@arndb.de>
Signed-off-by: Nishanth Menon <nm@ti.com>
2 years agoarm64: dts: ti: k3-am65-wakeup: Fix wakeup_uart reg address
Vignesh R [Thu, 8 Nov 2018 00:22:34 +0000 (18:22 -0600)]
arm64: dts: ti: k3-am65-wakeup: Fix wakeup_uart reg address

Upstream post: https://patchwork.kernel.org/patch/10617217/

cbass_wakeup interconnect which is the parent of wakeup_uart node
defines address-cells=1 and size-cells=1, therefore fix up reg property
of wakeup_uart node accordingly. Otherwise, this UART instance fails to
probe if enabled.

Fixes: 4201af2544b3 ("arm64: dts: ti: am654: Add uart nodes")
Signed-off-by: Vignesh R <vigneshr@ti.com>
Reviewed-by: Lokesh Vutla <lokeshvutla@ti.com>
Acked-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Nishanth Menon <nm@ti.com>
2 years agoarm64: dts: ti: k3-am6: Add Device Management Security Controller support
Nishanth Menon [Thu, 8 Nov 2018 00:22:33 +0000 (18:22 -0600)]
arm64: dts: ti: k3-am6: Add Device Management Security Controller support

commit 42e54f6467ecc25f464d74c0fcea0c9fab1c2e3b upstream

Add TISCI compatible System controller for AM6 SoCs.

Signed-off-by: Nishanth Menon <nm@ti.com>
Acked-by: Tony Lindgren <tony@atomide.com>
Signed-off-by: Tero Kristo <t-kristo@ti.com>
2 years agoarm64: dts: ti: am654: Add secure proxy instance for main domain
Nishanth Menon [Thu, 8 Nov 2018 00:22:32 +0000 (18:22 -0600)]
arm64: dts: ti: am654: Add secure proxy instance for main domain

commit 77ccbae4f9c8a14d41cb741f1d0a99dee68539fc upstream

Add secure proxy instance for Main domain

Signed-off-by: Nishanth Menon <nm@ti.com>
Acked-by: Tony Lindgren <tony@atomide.com>
Signed-off-by: Tero Kristo <t-kristo@ti.com>
2 years agoarm64: dts: ti: am654: Add uart nodes
Nishanth Menon [Thu, 8 Nov 2018 00:22:31 +0000 (18:22 -0600)]
arm64: dts: ti: am654: Add uart nodes

commit 4201af2544b39782d78ca1d4d59908e3b2502333 upstream

Add uart nodes for AM654 device tree components.

Signed-off-by: Nishanth Menon <nm@ti.com>
Acked-by: Tony Lindgren <tony@atomide.com>
Signed-off-by: Tero Kristo <t-kristo@ti.com>
2 years agoarm64: dts: ti: k3-am65: Change #address-cells and #size-cells of interconnect to 2
Kishon Vijay Abraham I [Thu, 8 Nov 2018 00:22:30 +0000 (18:22 -0600)]
arm64: dts: ti: k3-am65: Change #address-cells and #size-cells of interconnect to 2

commit 3bc1572068e3896b60d86f9c0fb56d1cef28201c upstream

AM65 has two PCIe controllers and each PCIe controller has '2' address
spaces one within the 4GB address space of the SoC and the other above
the 4GB address space of the SoC (cbass_main) in addition to the
register space. The size of the address space above the 4GB SoC address
space is 4GB. These address ranges will be used by CPU/DMA to access
the PCIe address space. In order to represent the address space above
the 4GB SoC address space and to represent the size of this address
space as 4GB, change address-cells and size-cells of interconnect to 2.

Since OSPI has similar need in MCU Domain Memory Map, change
address-cells and size-cells of cbass_mcu interconnect also to 2.

Fixes: ea47eed33a3fe3d919 ("arm64: dts: ti: Add Support for AM654 SoC")
Signed-off-by: Kishon Vijay Abraham I <kishon@ti.com>
Acked-by: Tony Lindgren <tony@atomide.com>
Acked-by: Vignesh R <vigneshr@ti.com>
Acked-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Tero Kristo <t-kristo@ti.com>
Signed-off-by: Nishanth Menon <nm@ti.com>
2 years agoserial: 8250_omap: Make 8250_omap driver driver depend on ARCH_K3
Lokesh Vutla [Thu, 8 Nov 2018 00:22:29 +0000 (18:22 -0600)]
serial: 8250_omap: Make 8250_omap driver driver depend on ARCH_K3

commit c886751465b8e312389d91446b76a00f45a79276 upstream

Allow 8250 omap serial driver to be used for K3 platforms.

Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
Signed-off-by: Nishanth Menon <nm@ti.com>
Acked-by: Tony Lindgren <tony@atomide.com>
Acked-by: Vignesh R <vigneshr@ti.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
2 years agoclk: keystone: Enable TISCI clocks if K3_ARCH
Nishanth Menon [Thu, 8 Nov 2018 00:22:28 +0000 (18:22 -0600)]
clk: keystone: Enable TISCI clocks if K3_ARCH

commit 2f149e6e14bcb5e581e49307b54aafcd6f74a74f upstream

K3_ARCH uses TISCI for clocks as well. Enable the same
for the driver support.

Signed-off-by: Nishanth Menon <nm@ti.com>
Acked-by: Santosh Shilimkar <ssantosh@kernel.org>
Signed-off-by: Stephen Boyd <sboyd@kernel.org>
2 years agodrivers: mailbox: Make ti-msgmr driver depend on ARCH_K3
Nishanth Menon [Thu, 8 Nov 2018 00:22:27 +0000 (18:22 -0600)]
drivers: mailbox: Make ti-msgmr driver depend on ARCH_K3

commit cfc0f7a8ea807bf318a1aa755a6a03d469e02725 upstream

ti-msgmr driver can support K3 platforms as well.

Signed-off-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Jassi Brar <jaswinder.singh@linaro.org>
2 years agofirmware: ti_sci: Provide host-id as an optional dt parameter
Nishanth Menon [Thu, 8 Nov 2018 00:22:26 +0000 (18:22 -0600)]
firmware: ti_sci: Provide host-id as an optional dt parameter

commit e69a35531589a2d3c746b0491d5ad3f77b6a0125 upstream

Texas Instrument's System Control Interface (TISCI) permits the
ability for Operating Systems to running in virtual machines to be
able to independently communicate with the firmware without the need
going through an hypervisor.

The "host-id" in effect is the hardware representation of the
host (example: VMs locked to a core) as identified to the System
Controller.

Provide support as an optional parameter implementation and use the
compatible data as default if one is not provided by device tree.

Signed-off-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Santosh Shilimkar <santosh.shilimkar@oracle.com>
2 years agoDocumentation: dt: keystone: ti-sci: Add optional host-id parameter
Nishanth Menon [Thu, 8 Nov 2018 00:22:25 +0000 (18:22 -0600)]
Documentation: dt: keystone: ti-sci: Add optional host-id parameter

commit 79a79c3a0ec2043711577750d4499abf4155d216 upstream

Texas Instrument's System Control Interface (TISCI) permits
the ability for OSs running in virtual machines to be able to
independently communicate with the firmware without the need going
through an hypervisor.

The "host-id" in effect is the hardware representation of the
host (example: VMs locked to a core) as identified to the System
Controller. Hypervisors can either fill in appropriate host-ids in dt
used for each VM instance OR may use prebuilt blobs where the host-ids
are pre-populated, as appropriate for the OS running in the VMs.

This is introduced as an optional parameter to maintain consistency
with legacy device tree blobs.

Reviewed-by: Rob Herring <robh@kernel.org>
Signed-off-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Santosh Shilimkar <santosh.shilimkar@oracle.com>
2 years agoMAINTAINERS: Drop dt-bindings/genpd/k2g.h
Nishanth Menon [Thu, 8 Nov 2018 00:22:24 +0000 (18:22 -0600)]
MAINTAINERS: Drop dt-bindings/genpd/k2g.h

commit 8abac18fecbd3e6694583227d9b5f337e397f942 upstream.

Drop include/dt-bindings/genpd/k2g.h which disappeared from kernel tree
some time back, however MAINTAINERS file was missed to be updated.

Fixes: d16645054d2f ("dt-bindings: Drop k2g genpd device ID macros")
Cc: Rob Herring <robh@kernel.org>
Cc: Dave Gerlach <d-gerlach@ti.com>
Cc: Santosh Shilimkar <ssantosh@kernel.org>
Cc: Tero Kristo <t-kristo@ti.com>
Reported-by: Joe Perches <joe@perches.com>
Signed-off-by: Nishanth Menon <nm@ti.com>
Acked-by: Santosh Shilimkar <ssantosh@kernel.org>
Signed-off-by: Arnd Bergmann <arnd@arndb.de>
2 years agoHACK: clocksource: kconfig: allow to select arm global timer manually
Grygorii Strashko [Wed, 7 Nov 2018 05:55:17 +0000 (11:25 +0530)]
HACK: clocksource: kconfig: allow to select arm global timer manually

This patch changes definition of ARM_GLOBAL_TIMER so it can be
enabled manually. This is required because ARM Global timer
has some limitations:
 - It is not always-on timer on am437x and it can't be
   used as clocksource device if CPU_IDLE=y
 - It doesn't support CPUfreq now
which can't be resolved properly by using kconfig dependencies
in case of multiplatform build.
For example, ARM_GLOBAL_TIMER can't be selected by default
for TI AM437x SOC, because it expected to support cpuidle
and cpufreq in multiplatform build from one side. From
another side - will cpuidle and cpufreq really work depends
not only from kconfig options, but also from PM driver
which has to be loaded.

LKML version:
 https://patchwork.ozlabs.org/patch/579071/

Signed-off-by: Grygorii Strashko <grygorii.strashko@ti.com>
2 years agoarm: dts: dra72-evm: Add interrupt parent for pcf_lcd
Nikhil Devshatwar [Wed, 7 Nov 2018 05:55:16 +0000 (11:25 +0530)]
arm: dts: dra72-evm: Add interrupt parent for pcf_lcd

On dra72-evm boards, pcf_lcd GPIO expander's interrupt lines
are connected to SoC GPIO as following

GPIO3_30 for dra72-evm
GPIO6_11 for dra72-evm-revc

Add the interrupt-parent property to correctly describe this.

Signed-off-by: Nikhil Devshatwar <nikhil.nd@ti.com>
2 years agoARM: OMAP2+: sleep43xx: Call secure suspend/resume handlers
Andrew F. Davis [Wed, 7 Nov 2018 05:55:15 +0000 (11:25 +0530)]
ARM: OMAP2+: sleep43xx: Call secure suspend/resume handlers

During suspend CPU context may be lost in both non-secure and secure CPU
states. The kernel can handle saving and restoring the non-secure context
but must call into the secure side to allow it to save any context it may
lose. Add these calls here.

Signed-off-by: Andrew F. Davis <afd@ti.com>
Acked-by: Dave Gerlach <d-gerlach@ti.com>
2 years agoregulator: palmas: Disable bypass for ldo1 and ldo2
Kishon Vijay Abraham I [Wed, 7 Nov 2018 05:55:14 +0000 (11:25 +0530)]
regulator: palmas: Disable bypass for ldo1 and ldo2

ldo1 and ldo2 have bypass capability. The regulator framework starts
with assuming that bypass is disabled by default. In this particular
case the bypass OTP is 1. So one cannot disable without first enabling
due to the use count going negative. Hence doing a one time disable at
boot.

Any consumer which wants bypass to be enabled/disabled can use the
bypass_enable/bypass_disable functions to turn on or turn off bypass
subsequently.

Signed-off-by: Kishon Vijay Abraham I <kishon@ti.com>
Signed-off-by: Keerthy <j-keerthy@ti.com>
2 years agopower: opp: ti-opp-supply: Correct the supply in _get_optimal_vdd_voltage call
Keerthy [Wed, 7 Nov 2018 05:55:13 +0000 (11:25 +0530)]
power: opp: ti-opp-supply: Correct the supply in _get_optimal_vdd_voltage call

_get_optimal_vdd_voltage call provides new_supply_vbb->u_volt
as the reference voltage while it should be really new_supply_vdd->u_volt.

Signed-off-by: Keerthy <j-keerthy@ti.com>
Acked-by: Dave Gerlach <d-gerlach@ti.com>
2 years agopower: opp: ti-opp-supply: Dynamically update u_volt_min
Keerthy [Wed, 7 Nov 2018 05:55:12 +0000 (11:25 +0530)]
power: opp: ti-opp-supply: Dynamically update u_volt_min

The voltage range (min, max) provided in the device tree is from
the data manual and is pretty big, catering to a wide range of devices.
On a i2c read/write failure the regulator_set_voltage_triplet function
falls back to set voltage between min and max. The min value from Device
Tree can be lesser than the optimal value and in that case that can lead
to a hang or crash. Hence set the u_volt_min dynamically to the optimal
voltage value.

Signed-off-by: Keerthy <j-keerthy@ti.com>
Acked-by: Dave Gerlach <d-gerlach@ti.com>
2 years agoarm: dts: am57xx-idk-common: Hook smps12 regulator as cpu vdd-supply
Keerthy [Wed, 7 Nov 2018 05:55:11 +0000 (11:25 +0530)]
arm: dts: am57xx-idk-common: Hook smps12 regulator as cpu vdd-supply

commit 5c8a6b9db5e95ea7702ef8d4bb1438537ef63594 upstream

am574x-idk has no cpu vdd-supply at the moment. Hence hook smps12
regulator as cpu vdd-supply in am57xx-idk-common as the same regulator
feeds on to cpu on am571/2/4-idks. So remove all the individual
instances and place that in common place.

Signed-off-by: Keerthy <j-keerthy@ti.com>
2 years agoARM: dts: am437x-gp-evm: Add sleep state for beeper pins
Keerthy [Wed, 7 Nov 2018 05:55:10 +0000 (11:25 +0530)]
ARM: dts: am437x-gp-evm: Add sleep state for beeper pins

Add sleep state for beeper pins. Without this there was a power
increase during the suspend and standby states on V3_3D domain.

Signed-off-by: Keerthy <j-keerthy@ti.com>
2 years agoARM: dts: am335x: Add rtc node as system-power-controller
Keerthy [Wed, 7 Nov 2018 05:55:09 +0000 (11:25 +0530)]
ARM: dts: am335x: Add rtc node as system-power-controller

PMIC_PWR_EN pin of RTC on am335x-evm, bone, and boneblack is connected to
PMIC on board, so flag rtc node as system-power-controller to allow
software to poweroff boards.

Signed-off-by: Dave Gerlach <d-gerlach@ti.com>
Signed-off-by: Keerthy <j-keerthy@ti.com>
2 years agoHACK: arm: keystone: add outer shareable attribute for pages/sections
Murali Karicheri [Wed, 7 Nov 2018 05:55:08 +0000 (11:25 +0530)]
HACK: arm: keystone: add outer shareable attribute for pages/sections

On KS2 devices pages/sections to be used for DMA must have "outer
shareable" attribute. In the upstream kernel, ARM v7 supports only
"inner shareable attribute". This means all memory requests for pages
that are marked inner shareable in the page tables and are writeback
cacheable will be coherent in all caches at the inner domain. However
in Keystone, these are to be marked as "outer shareable" as the keystone
dma coherency hardware implementation use this feature to listen to
maintenance snoop messages to make it coherent with DMA masters. For more
details, please refer to the ARM TRM and Keystone device user guides [1].

[1] MSMC user guide, document id spruhj6

Signed-off-by: Santosh Shilimkar <santosh.shilimkar@ti.com>
Signed-off-by: Vitaly Andrianov <vitalya@ti.com>
Signed-off-by: Murali Karicheri <m-karicheri2@ti.com>
2 years agoARM: dts: keystone-k2g: add timer1 as clocksource
Keerthy [Wed, 7 Nov 2018 05:55:07 +0000 (11:25 +0530)]
ARM: dts: keystone-k2g: add timer1 as clocksource

Add timer1 node as the clocksource.

Signed-off-by: Keerthy <j-keerthy@ti.com>
Signed-off-by: Tero Kristo <t-kristo@ti.com>
2 years agoclocksource: timer-keystone: Add platform probe support to existing code
Keerthy [Wed, 7 Nov 2018 05:55:06 +0000 (11:25 +0530)]
clocksource: timer-keystone: Add platform probe support to existing code

This patch fixes the case for k2g where in clocks are not
available at the time of keystone_timer_init function call.
K2HK/K2L/K2E devices are left untouched and the old way of
keystone_timer_init is preserved since it is init order sensitive.

On top of the existing code a platform driver is introduced so that
if clock is not yet ready probe can be deferred. This enables hres
timers for k2g.

Signed-off-by: Keerthy <j-keerthy@ti.com>
2 years agoHACK: ARM: smccc-call: Use r12 to route secure monitor calls
Harinarayan Bhatta [Mon, 5 Nov 2018 20:54:53 +0000 (14:54 -0600)]
HACK: ARM: smccc-call: Use r12 to route secure monitor calls

Our ROM Secure Monitor(SM) uses the value in r12 to determine which
service is being requested by an SMC call. This goes against he ARM
recommended SMC Calling Convention(SMCCC), which partitions the values
in R0 for this task, OP-TEE's SM follows the ARM recommended convention.

We need a way to signal that a call is for our new SM and not for
the ROM SM in a way that is safe for the ROM SM, in case OP-TEE is
not installed. We do this by putting a value of 0x200 in r12 when the
call is for OP-TEE by modifying the SMCCC caller function.

There are four combinations of events:

If the ROM SM is present and we make a legacy style SMC call, as we
do in early boot, the call will not have r12 set to 0x200 as these
calls go through existing mach-omap2/ SMC handlers, so all is well.

If the ROM SM is present and we make an SMCCC style call, r12 will be
set to 0x200 and ROM SM will see this as an invalid service call and
safely return to the normal world. This should not happen.

If OP-TEE is present and we make a legacy style SMC call, r12 will
not be set to 0x200, and OP-TEE will emulate the functionality that
the call is requesting.

If OP-TEE is present and we make an SMCCC style call, r12 is checked
and as it will be 0x200 we can ignore it and treat the rest of the
registers in the standard SMCCC way.

Using a TI specific calling convention was rejected upstream[0], the
suggested solution was to change all legacy calls to perform runtime
switching based on the DT OP-TEE, this is not a reasonable solution
given how many platforms would be affected, so we will have to keep
this non-upstreamable HACK for now.

[0] https://patchwork.kernel.org/patch/9957687/

Signed-off-by: Harinarayan Bhatta <harinarayan@ti.com>
Signed-off-by: Andrew F. Davis <afd@ti.com>
2 years agoARM: dts: am437x-gp-evm: Add pinmux for gpio0 wake
Dave Gerlach [Fri, 2 Nov 2018 10:31:27 +0000 (16:01 +0530)]
ARM: dts: am437x-gp-evm: Add pinmux for gpio0 wake

Add pinctrl settings so that gpio0 wake from suspend will be supported
using buttons SW4 and SW7. Also, add pinctrl configuration for 0x954,
spi0_d0, which is an unused pin brought out to a header on the board
that in it's default state also connects to the gpio used for wakeup,
gpio0_3, which affects the state of the pin and prevents a working
wakeup unless we set the mux to a different state.

Signed-off-by: Dave Gerlach <d-gerlach@ti.com>
2 years agoARM: dts: am437x-gp-evm: Add uart0 pinctrl default and sleep states
Dave Gerlach [Fri, 2 Nov 2018 10:31:26 +0000 (16:01 +0530)]
ARM: dts: am437x-gp-evm: Add uart0 pinctrl default and sleep states

Currently uart0 uses pinctrl config set by bootloader so
create default state that can be restored after a suspend
event.

Also, modify uart0 pinctrl to include RTS and CTS pins as by
default these are not in a mode for optimal power savings.

Signed-off-by: Dave Gerlach <d-gerlach@ti.com>
2 years agoARM: dts: am437x-gp-evm: Add pinctrl for debugss pins
Dave Gerlach [Fri, 2 Nov 2018 10:31:25 +0000 (16:01 +0530)]
ARM: dts: am437x-gp-evm: Add pinctrl for debugss pins

The pins used by debugss are not configued by default, place pulldowns
on the pins for maximum power savings during sleep.

Signed-off-by: Dave Gerlach <d-gerlach@ti.com>
[t-kristo@ti.com: converted to use AM4372_IOPAD macro]
Signed-off-by: Tero Kristo <t-kristo@ti.com>
2 years agoARM: dts: am437x-gp-evm: Add pinctrl for unused_pins
Dave Gerlach [Fri, 2 Nov 2018 10:31:24 +0000 (16:01 +0530)]
ARM: dts: am437x-gp-evm: Add pinctrl for unused_pins

There are several pins on this EVM that are not in use but they can
still draw power if misconfigured. Create a pinctrl entry for these pins
and configure each one for optimal power savings.

Signed-off-by: Dave Gerlach <d-gerlach@ti.com>
[t-kristo@ti.com: converted to use AM4372_IOPAD macro]
Signed-off-by: Tero Kristo <t-kristo@ti.com>
2 years agoARM: OMAP2+: am43xx: Add lcdc clockdomain
Dave Gerlach [Fri, 2 Nov 2018 10:30:48 +0000 (16:00 +0530)]
ARM: OMAP2+: am43xx: Add lcdc clockdomain

As described in AM437x TRM, spruhl7f, Revised September 2016, there is
an LCDC clockdomain present in the PER power domain. Although it is
entirely unused on AM437x, it should be defined along with the other
clockdomains so it can be shut off by Linux as there are no users.

Reported-by: Munan Xu <munan@ti.com>
Signed-off-by: Dave Gerlach <d-gerlach@ti.com>
2 years agoARM: OMAP2+: timer: Extend pending interrupt ACK for gic
Dave Gerlach [Fri, 2 Nov 2018 10:30:47 +0000 (16:00 +0530)]
ARM: OMAP2+: timer: Extend pending interrupt ACK for gic

The current implementation for preventing timer interrupts from
breaking suspend fully fixes the issue on am335x but the GIC present on
am437x cannot be directly acked using only the irqchip calls as is done
for am335x but requires an additional step.

Calling irqchip->irq_eoi only writes to the GIC_CPU_EOI register but for
an interrupt to be properly cleared by the GIC, a read from
GIC_CPU_INTACK must come first.  The only place the irq-gic driver reads
this is in the actual interrupt handler so we cannot access it from the
driver.

To get around this, let's map the GIC_CPU_BASE and read the
GIC_CPU_INTACK register ourselves before calling irq_eoi to properly ack
late timer interrupts that show up during suspend on am437x.

Signed-off-by: Dave Gerlach <d-gerlach@ti.com>
2 years agoARM: OMAP2+: timer: Ack pending interrupt during suspend
Dave Gerlach [Fri, 2 Nov 2018 10:30:46 +0000 (16:00 +0530)]
ARM: OMAP2+: timer: Ack pending interrupt during suspend

It is possible that when suspending the clock event timer it will generate
an interrupt just before their suspend is completed, but after interrupts have
been disabled. In this case any pending interrupts will prevent suspend, so
ACK the timer interrupt to avoid this.

Signed-off-by: Dave Gerlach <d-gerlach@ti.com>
Signed-off-by: Tero Kristo <t-kristo@ti.com>
2 years agosoc: ti: wkup_m3_ipc: Add debug option to halt m3 in suspend
Dave Gerlach [Fri, 2 Nov 2018 10:30:45 +0000 (16:00 +0530)]
soc: ti: wkup_m3_ipc: Add debug option to halt m3 in suspend

Add a debugfs option to allow configurable halting of the wkup_m3
during suspend at the last possible point before low power mode entry.
This condition can only be resolved through JTAG and advancing beyond
the while loop in a8_lp_ds0_handler. Although this hangs the system it
forces the system to remain active once it has been entirely configured
for low power mode entry, allowing for register inspection through JTAG
to help in debugging transition errors.

Halt mode can be set using the enable_off_mode entry under wkup_m3_ipc
in the debugfs.

Suggested-by: Brad Griffis <bgriffis@ti.com>
Signed-off-by: Dave Gerlach <d-gerlach@ti.com>
2 years agosoc: ti: wkup_m3_ipc: Fix race condition with rproc_boot
Dave Gerlach [Fri, 2 Nov 2018 10:30:43 +0000 (16:00 +0530)]
soc: ti: wkup_m3_ipc: Fix race condition with rproc_boot

Any user of wkup_m3_ipc calls wkup_m3_ipc_get to get a handle and this
checks the value of the static variable m3_ipc_state to see if the
wkup_m3 is ready. Currently this is populated during probe before
rproc_boot has been called, meaning there is a window of time that
wkup_m3_ipc_get can return a valid handle but the wkup_m3 itself is not
ready, leading to invalid IPC calls to the wkup_m3 and system
instability.

To avoid this, move the population of the m3_ipc_state variable until
after rproc_boot has succeeded to guarantee a valid and usable handle
is always returned.

Reported-by: Suman Anna <s-anna@ti.com>
Signed-off-by: Dave Gerlach <d-gerlach@ti.com>
2 years agoARM: dts: am4372: Add idle_states for cpuidle
Dave Gerlach [Fri, 2 Nov 2018 10:29:52 +0000 (15:59 +0530)]
ARM: dts: am4372: Add idle_states for cpuidle

Add idle_states table for CPU on am437x. Currently just add C1 state
which gates the MPU clock domain.

Signed-off-by: Dave Gerlach <d-gerlach@ti.com>
2 years agoARM: dts: am33xx: Add idle_states for cpuidle
Dave Gerlach [Fri, 2 Nov 2018 10:29:51 +0000 (15:59 +0530)]
ARM: dts: am33xx: Add idle_states for cpuidle

Add idle_states table for CPU on am335x. Currently just add C1 state
which gates the MPU clock domain.

Signed-off-by: Dave Gerlach <d-gerlach@ti.com>