author | Andi Kleen <ak@linux.intel.com> | |
Wed, 13 Jun 2018 22:48:26 +0000 (15:48 -0700) | ||
committer | Thomas Gleixner <tglx@linutronix.de> | |
Wed, 20 Jun 2018 17:10:00 +0000 (19:10 +0200) | ||
commit | 17dbca119312b4e8173d4e25ff64262119fcef38 | |
tree | ed81f3bf900f83cdae9739415d0382b1fd303306 | tree | snapshot (tar.xz tar.gz zip) |
parent | 10a70416e1f067f6c4efda6ffd8ea96002ac4223 | commit | diff |
x86/speculation/l1tf: Add sysfs reporting for l1tf
L1TF core kernel workarounds are cheap and normally always enabled, However
they still should be reported in sysfs if the system is vulnerable or
mitigated. Add the necessary CPU feature/bug bits.
- Extend the existing checks for Meltdowns to determine if the system is
vulnerable. All CPUs which are not vulnerable to Meltdown are also not
vulnerable to L1TF
- Check for 32bit non PAE and emit a warning as there is no practical way
for mitigation due to the limited physical address bits
- If the system has more than MAX_PA/2 physical memory the invert page
workarounds don't protect the system against the L1TF attack anymore,
because an inverted physical address will also point to valid
memory. Print a warning in this case and report that the system is
vulnerable.
Add a function which returns the PFN limit for the L1TF mitigation, which
will be used in follow up patches for sanity and range checks.
[ tglx: Renamed the CPU feature bit to L1TF_PTEINV ]
Signed-off-by: Andi Kleen <ak@linux.intel.com>
Signed-off-by: Thomas Gleixner <tglx@linutronix.de>
Reviewed-by: Josh Poimboeuf <jpoimboe@redhat.com>
Acked-by: Dave Hansen <dave.hansen@intel.com>
L1TF core kernel workarounds are cheap and normally always enabled, However
they still should be reported in sysfs if the system is vulnerable or
mitigated. Add the necessary CPU feature/bug bits.
- Extend the existing checks for Meltdowns to determine if the system is
vulnerable. All CPUs which are not vulnerable to Meltdown are also not
vulnerable to L1TF
- Check for 32bit non PAE and emit a warning as there is no practical way
for mitigation due to the limited physical address bits
- If the system has more than MAX_PA/2 physical memory the invert page
workarounds don't protect the system against the L1TF attack anymore,
because an inverted physical address will also point to valid
memory. Print a warning in this case and report that the system is
vulnerable.
Add a function which returns the PFN limit for the L1TF mitigation, which
will be used in follow up patches for sanity and range checks.
[ tglx: Renamed the CPU feature bit to L1TF_PTEINV ]
Signed-off-by: Andi Kleen <ak@linux.intel.com>
Signed-off-by: Thomas Gleixner <tglx@linutronix.de>
Reviewed-by: Josh Poimboeuf <jpoimboe@redhat.com>
Acked-by: Dave Hansen <dave.hansen@intel.com>