author | Dave Gerlach <d-gerlach@ti.com> | |
Fri, 2 Nov 2018 10:31:27 +0000 (16:01 +0530) | ||
committer | Tero Kristo <t-kristo@ti.com> | |
Tue, 6 Nov 2018 13:27:28 +0000 (15:27 +0200) | ||
commit | 2ccf0189a347a47c67135e2e28a1f2e9203214b6 | |
tree | 58c577fc9473d8b08d2e2bcc98e36592248f1c9a | tree | snapshot (tar.xz tar.gz zip) |
parent | b80f06b36f376a221051644aba8b76dfb8e5d086 | commit | diff |
ARM: dts: am437x-gp-evm: Add pinmux for gpio0 wake
Add pinctrl settings so that gpio0 wake from suspend will be supported
using buttons SW4 and SW7. Also, add pinctrl configuration for 0x954,
spi0_d0, which is an unused pin brought out to a header on the board
that in it's default state also connects to the gpio used for wakeup,
gpio0_3, which affects the state of the pin and prevents a working
wakeup unless we set the mux to a different state.
Signed-off-by: Dave Gerlach <d-gerlach@ti.com>
Add pinctrl settings so that gpio0 wake from suspend will be supported
using buttons SW4 and SW7. Also, add pinctrl configuration for 0x954,
spi0_d0, which is an unused pin brought out to a header on the board
that in it's default state also connects to the gpio used for wakeup,
gpio0_3, which affects the state of the pin and prevents a working
wakeup unless we set the mux to a different state.
Signed-off-by: Dave Gerlach <d-gerlach@ti.com>
arch/arm/boot/dts/am437x-gp-evm.dts | diff | blob | history |