summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 06c182c)
raw | patch | inline | side by side (parent: 06c182c)
author | Suman Anna <s-anna@ti.com> | |
Tue, 4 Jun 2019 17:01:45 +0000 (12:01 -0500) | ||
committer | Jassi Brar <jaswinder.singh@linaro.org> | |
Thu, 11 Jul 2019 04:08:43 +0000 (23:08 -0500) |
The TI K3 AM65x and J721E family of SoCs have a new Mailbox IP that
is based on the existing Mailbox IP present in OMAP architecture based
SoCs. Update the existing OMAP Mailbox bindings for this new IP present
on TI K3 AM65x and J721E SoCs. The same compatible from AM65x SoCs is
reused for J721E SoCs.
Signed-off-by: Suman Anna <s-anna@ti.com>
Reviewed-by: Rob Herring <robh@kernel.org>
Signed-off-by: Jassi Brar <jaswinder.singh@linaro.org>
is based on the existing Mailbox IP present in OMAP architecture based
SoCs. Update the existing OMAP Mailbox bindings for this new IP present
on TI K3 AM65x and J721E SoCs. The same compatible from AM65x SoCs is
reused for J721E SoCs.
Signed-off-by: Suman Anna <s-anna@ti.com>
Reviewed-by: Rob Herring <robh@kernel.org>
Signed-off-by: Jassi Brar <jaswinder.singh@linaro.org>
Documentation/devicetree/bindings/mailbox/omap-mailbox.txt | patch | blob | history |
diff --git a/Documentation/devicetree/bindings/mailbox/omap-mailbox.txt b/Documentation/devicetree/bindings/mailbox/omap-mailbox.txt
index 0ef372656a3eac86e8b1be97fc7dc8231936b8e2..35c3f56b7f7bf56b7a2485addbf8140a441cc85a 100644 (file)
-OMAP2+ Mailbox Driver
+OMAP2+ and K3 Mailbox
=====================
The OMAP mailbox hardware facilitates communication between different processors
communication is achieved through a set of registers for message storage and
interrupt configuration registers.
-Each mailbox IP block has a certain number of h/w fifo queues and output
+Each mailbox IP block/cluster has a certain number of h/w fifo queues and output
interrupt lines. An output interrupt line is routed to an interrupt controller
within a processor subsystem, and there can be more than one line going to a
specific processor's interrupt controller. The interrupt line connections are
instance. DRA7xx has multiple instances with different number of h/w fifo queues
and interrupt lines between different instances. The interrupt lines can also be
routed to different processor sub-systems on DRA7xx as they are routed through
-the Crossbar, a kind of interrupt router/multiplexer.
+the Crossbar, a kind of interrupt router/multiplexer. The K3 AM65x and J721E
+SoCs has each of these instances form a cluster and combine multiple clusters
+into a single IP block present within the Main NavSS. The interrupt lines from
+all these clusters are multiplexed and routed to different processor subsystems
+over a limited number of common interrupt output lines of an Interrupt Router.
Mailbox Device Node:
====================
-A Mailbox device node is used to represent a Mailbox IP instance within a SoC.
-The sub-mailboxes are represented as child nodes of this parent node.
+A Mailbox device node is used to represent a Mailbox IP instance/cluster within
+a SoC. The sub-mailboxes are represented as child nodes of this parent node.
Required properties:
--------------------
"ti,omap3-mailbox" for OMAP3430, OMAP3630 SoCs
"ti,omap4-mailbox" for OMAP44xx, OMAP54xx, AM33xx,
AM43xx and DRA7xx SoCs
+ "ti,am654-mailbox" for K3 AM65x and J721E SoCs
- reg: Contains the mailbox register address range (base
address and length)
- interrupts: Contains the interrupt information for the mailbox
device. The format is dependent on which interrupt
- controller the OMAP device uses
-- ti,hwmods: Name of the hwmod associated with the mailbox
+ controller the Mailbox device uses
- #mbox-cells: Common mailbox binding property to identify the number
of cells required for the mailbox specifier. Should be
1
device can interrupt
- ti,mbox-num-fifos: Number of h/w fifo queues within the mailbox IP block
+SoC-specific Required properties:
+---------------------------------
+The following are mandatory properties for the OMAP architecture based SoCs
+only:
+- ti,hwmods: Name of the hwmod associated with the mailbox. This
+ should be defined in the mailbox node only if the node
+ is not defined as a child node of a corresponding sysc
+ interconnect node.
+
+The following are mandatory properties for the K3 AM65x and J721E SoCs only:
+- interrupt-parent: Should contain a phandle to the TI-SCI interrupt
+ controller node that is used to dynamically program
+ the interrupt routes between the IP and the main GIC
+ controllers. See the following binding for additional
+ details,
+ Documentation/devicetree/bindings/interrupt-controller/ti,sci-intr.txt
+
Child Nodes:
============
A child node is used for representing the actual sub-mailbox device that is
Example:
--------
-/* OMAP4 */
+1. /* OMAP4 */
mailbox: mailbox@4a0f4000 {
compatible = "ti,omap4-mailbox";
reg = <0x4a0f4000 0x200>;
...
};
-/* AM33xx */
+2. /* AM33xx */
mailbox: mailbox@480c8000 {
compatible = "ti,omap4-mailbox";
reg = <0x480C8000 0x200>;
ti,mbox-rx = <0 0 3>;
};
};
+
+3. /* AM65x */
+&cbass_main {
+ cbass_main_navss: interconnect0 {
+ mailbox0_cluster0: mailbox@31f80000 {
+ compatible = "ti,am654-mailbox";
+ reg = <0x00 0x31f80000 0x00 0x200>;
+ #mbox-cells = <1>;
+ ti,mbox-num-users = <4>;
+ ti,mbox-num-fifos = <16>;
+ interrupt-parent = <&intr_main_navss>;
+ interrupts = <164 0>;
+
+ mbox_mcu_r5fss0_core0: mbox-mcu-r5fss0-core0 {
+ ti,mbox-tx = <1 0 0>;
+ ti,mbox-rx = <0 0 0>;
+ };
+ };
+ };
+};