net/rpmsg: add support for new rpmsg sockets Add the support for a new socket address and protocol family - remote-processor messaging sockets. This rpmsg protocol driver provides the necessary support to expose a rpmsg communication channel through the socket API to userspace under the AF_RPMSG address family. The usage relies on leveraging the socket API's connect() for Tx sockets and bind() for Rx sockets to exchange messages to/from a remote processor. All message communication is performed using the userspace created sockets, and even though the probed rpmsg proto devices do create an embedded rpmsg endpoint for receiving messages, they are not really designed to process any such unexpected Rx messages. This driver forms the kernel transport portion of the the TI IPC MessageQ stack. The MessageQ stack usage of the AF_RPMSG socket interface is not really designed to handle multiple rpmsg-proto devices published from the same remote processor, so a restriction is imposed to allow only a single rpmsg device even though there are no such restrictions imposed by the rpmsg bus infrastructure. This can be scaled to make it more generic if needed but probably will require some userspace interface adjustments. This patch is based on some quite an old rpmsg socket support patch from Ohad and some work by Rob Tivy. This has been updated rather heavily to work with all the rpmsg framework changes in 4.9+ kernels. Signed-off-by: Ohad Ben Cohen <ohad@wizery.com> [s-anna@ti.com: adapted, improved and modified for latest kernel] Signed-off-by: Suman Anna <s-anna@ti.com>
net: avoid unnecessary sock_flag() check when enable timestamp The sock_flag() check is alreay inside sock_enable_timestamp(), so it is unnecessary checking it in the caller. void sock_enable_timestamp(struct sock *sk, int flag) { if (!sock_flag(sk, flag)) { ... } } Signed-off-by: Yafang Shao <laoar.shao@gmail.com> Signed-off-by: David S. Miller <davem@davemloft.net>
net/socket: remove duplicated init code This refactoring work has been started by David Howells in cdfbabfb2f0c (net: Work around lockdep limitation in sockets that use sockets) but the exact same day in 581319c58600 (net/socket: use per af lockdep classes for sk queues), Paolo Abeni added new classes. This reduces the amount of (nearly) duplicated code and eases the addition of new socket types. Signed-off-by: Matthieu Baerts <matthieu.baerts@tessares.net> Signed-off-by: David S. Miller <davem@davemloft.net>
Merge ra.kernel.org:/pub/scm/linux/kernel/git/davem/net
sock: fix sg page frag coalescing in sk_alloc_sg Current sg coalescing logic in sk_alloc_sg() (latter is used by tls and sockmap) is not quite correct in that we do fetch the previous sg entry, however the subsequent check whether the refilled page frag from the socket is still the same as from the last entry with prior offset and length matching the start of the current buffer is comparing always the first sg list entry instead of the prior one. Fixes: 3c4d7559159b ("tls: kernel TLS support") Signed-off-by: Daniel Borkmann <daniel@iogearbox.net> Acked-by: Dave Watson <davejwatson@fb.com> Signed-off-by: David S. Miller <davem@davemloft.net>
net/sched: Make etf report drops on error_queue Use the socket error queue for reporting dropped packets if the socket has enabled that feature through the SO_TXTIME API. Packets are dropped either on enqueue() if they aren't accepted by the qdisc or on dequeue() if the system misses their deadline. Those are reported as different errors so applications can react accordingly. Userspace can retrieve the errors through the socket error queue and the corresponding cmsg interfaces. A struct sock_extended_err* is used for returning the error data, and the packet's timestamp can be retrieved by adding both ee_data and ee_info fields as e.g.: ((__u64) serr->ee_data << 32) + serr->ee_info This feature is disabled by default and must be explicitly enabled by applications. Enabling it can bring some overhead for the Tx cycles of the application. Signed-off-by: Jesus Sanchez-Palencia <jesus.sanchez-palencia@intel.com> Signed-off-by: David S. Miller <davem@davemloft.net>
net: Add a new socket option for a future transmit time. This patch introduces SO_TXTIME. User space enables this option in order to pass a desired future transmit time in a CMSG when calling sendmsg(2). The argument to this socket option is a 8-bytes long struct provided by the uapi header net_tstamp.h defined as: struct sock_txtime { clockid_t clockid; u32 flags; }; Note that new fields were added to struct sock by filling a 2-bytes hole found in the struct. For that reason, neither the struct size or number of cachelines were altered. Signed-off-by: Richard Cochran <rcochran@linutronix.de> Signed-off-by: Jesus Sanchez-Palencia <jesus.sanchez-palencia@intel.com> Signed-off-by: David S. Miller <davem@davemloft.net>
Merge ra.kernel.org:/pub/scm/linux/kernel/git/davem/net Simple overlapping changes in stmmac driver. Adjust skb_gro_flush_final_remcsum function signature to make GRO list changes in net-next, as per Stephen Rothwell's example merge resolution. Signed-off-by: David S. Miller <davem@davemloft.net>
net: expose sk wmem in sock_exceed_buf_limit tracepoint Currently trace_sock_exceed_buf_limit() only show rmem info, but wmem limit may also be hit. So expose wmem info in this tracepoint as well. Regarding memcg, I think it is better to introduce a new tracepoint(if that is needed), i.e. trace_memcg_limit_hit other than show memcg info in trace_sock_exceed_buf_limit. Signed-off-by: Yafang Shao <laoar.shao@gmail.com> Signed-off-by: David S. Miller <davem@davemloft.net>
net: Record receive queue number for a connection This patch adds a new field to sock_common 'skc_rx_queue_mapping' which holds the receive queue number for the connection. The Rx queue is marked in tcp_finish_connect() to allow a client app to do SO_INCOMING_NAPI_ID after a connect() call to get the right queue association for a socket. Rx queue is also marked in tcp_conn_request() to allow syn-ack to go on the right tx-queue associated with the queue on which syn is received. Signed-off-by: Amritha Nambiar <amritha.nambiar@intel.com> Signed-off-by: Sridhar Samudrala <sridhar.samudrala@intel.com> Signed-off-by: David S. Miller <davem@davemloft.net>
net, mm: account sock objects to kmemcg Currently the kernel accounts the memory for network traffic through mem_cgroup_[un]charge_skmem() interface. However the memory accounted only includes the truesize of sk_buff which does not include the size of sock objects. In our production environment, with opt-out kmem accounting, the sock kmem caches (TCP[v6], UDP[v6], RAW[v6], UNIX) are among the top most charged kmem caches and consume a significant amount of memory which can not be left as system overhead. So, this patch converts the kmem caches of all sock objects to SLAB_ACCOUNT. Signed-off-by: Shakeel Butt <shakeelb@google.com> Suggested-by: Eric Dumazet <edumazet@google.com> Reviewed-by: Kirill Tkhai <ktkhai@virtuozzo.com> Reviewed-by: Eric Dumazet <edumazet@google.com> Signed-off-by: David S. Miller <davem@davemloft.net>
Revert "net: do not allow changing SO_REUSEADDR/SO_REUSEPORT on bound sockets" Revert the patch mentioned in the subject because it breaks at least the Avahi mDNS daemon. That patch namely causes the Ubuntu 18.04 Avahi daemon to fail to start: Jun 12 09:49:24 ubuntu-vm avahi-daemon[529]: Successfully called chroot(). Jun 12 09:49:24 ubuntu-vm avahi-daemon[529]: Successfully dropped remaining capabilities. Jun 12 09:49:24 ubuntu-vm avahi-daemon[529]: No service file found in /etc/avahi/services. Jun 12 09:49:24 ubuntu-vm avahi-daemon[529]: SO_REUSEADDR failed: Structure needs cleaning Jun 12 09:49:24 ubuntu-vm avahi-daemon[529]: SO_REUSEADDR failed: Structure needs cleaning Jun 12 09:49:24 ubuntu-vm avahi-daemon[529]: Failed to create server: No suitable network protocol available Jun 12 09:49:24 ubuntu-vm avahi-daemon[529]: avahi-daemon 0.7 exiting. Jun 12 09:49:24 ubuntu-vm systemd[1]: avahi-daemon.service: Main process exited, code=exited, status=255/n/a Jun 12 09:49:24 ubuntu-vm systemd[1]: avahi-daemon.service: Failed with result 'exit-code'. Jun 12 09:49:24 ubuntu-vm systemd[1]: Failed to start Avahi mDNS/DNS-SD Stack. Fixes: f396922d862a ("net: do not allow changing SO_REUSEADDR/SO_REUSEPORT on bound sockets") Cc: Maciej Żenczykowski <maze@google.com> Cc: Eric Dumazet <edumazet@google.com> Signed-off-by: Bart Van Assche <bart.vanassche@wdc.com> Acked-by: Eric Dumazet <edumazet@google.com> Signed-off-by: David S. Miller <davem@davemloft.net>
Merge git://git.kernel.org/pub/scm/linux/kernel/git/davem/net-next Pull networking updates from David Miller: 1) Add Maglev hashing scheduler to IPVS, from Inju Song. 2) Lots of new TC subsystem tests from Roman Mashak. 3) Add TCP zero copy receive and fix delayed acks and autotuning with SO_RCVLOWAT, from Eric Dumazet. 4) Add XDP_REDIRECT support to mlx5 driver, from Jesper Dangaard Brouer. 5) Add ttl inherit support to vxlan, from Hangbin Liu. 6) Properly separate ipv6 routes into their logically independant components. fib6_info for the routing table, and fib6_nh for sets of nexthops, which thus can be shared. From David Ahern. 7) Add bpf_xdp_adjust_tail helper, which can be used to generate ICMP messages from XDP programs. From Nikita V. Shirokov. 8) Lots of long overdue cleanups to the r8169 driver, from Heiner Kallweit. 9) Add BTF ("BPF Type Format"), from Martin KaFai Lau. 10) Add traffic condition monitoring to iwlwifi, from Luca Coelho. 11) Plumb extack down into fib_rules, from Roopa Prabhu. 12) Add Flower classifier offload support to igb, from Vinicius Costa Gomes. 13) Add UDP GSO support, from Willem de Bruijn. 14) Add documentation for eBPF helpers, from Quentin Monnet. 15) Add TLS tx offload to mlx5, from Ilya Lesokhin. 16) Allow applications to be given the number of bytes available to read on a socket via a control message returned from recvmsg(), from Soheil Hassas Yeganeh. 17) Add x86_32 eBPF JIT compiler, from Wang YanQing. 18) Add AF_XDP sockets, with zerocopy support infrastructure as well. From Björn Töpel. 19) Remove indirect load support from all of the BPF JITs and handle these operations in the verifier by translating them into native BPF instead. From Daniel Borkmann. 20) Add GRO support to ipv6 gre tunnels, from Eran Ben Elisha. 21) Allow XDP programs to do lookups in the main kernel routing tables for forwarding. From David Ahern. 22) Allow drivers to store hardware state into an ELF section of kernel dump vmcore files, and use it in cxgb4. From Rahul Lakkireddy. 23) Various RACK and loss detection improvements in TCP, from Yuchung Cheng. 24) Add TCP SACK compression, from Eric Dumazet. 25) Add User Mode Helper support and basic bpfilter infrastructure, from Alexei Starovoitov. 26) Support ports and protocol values in RTM_GETROUTE, from Roopa Prabhu. 27) Support bulking in ->ndo_xdp_xmit() API, from Jesper Dangaard Brouer. 28) Add lots of forwarding selftests, from Petr Machata. 29) Add generic network device failover driver, from Sridhar Samudrala. * ra.kernel.org:/pub/scm/linux/kernel/git/davem/net-next: (1959 commits) strparser: Add __strp_unpause and use it in ktls. rxrpc: Fix terminal retransmission connection ID to include the channel net: hns3: Optimize PF CMDQ interrupt switching process net: hns3: Fix for VF mailbox receiving unknown message net: hns3: Fix for VF mailbox cannot receiving PF response bnx2x: use the right constant Revert "net: sched: cls: Fix offloading when ingress dev is vxlan" net: dsa: b53: Fix for brcm tag issue in Cygnus SoC enic: fix UDP rss bits netdev-FAQ: clarify DaveM's position for stable backports rtnetlink: validate attributes in do_setlink() mlxsw: Add extack messages for port_{un, }split failures netdevsim: Add extack error message for devlink reload devlink: Add extack to reload and port_{un, }split operations net: metrics: add proper netlink validation ipmr: fix error path when ipmr_new_table fails ip6mr: only set ip6mr_table from setsockopt when ip6mr_new_table succeeds net: hns3: remove unused hclgevf_cfg_func_mta_filter netfilter: provide udp*_lib_lookup for nf_tproxy qed*: Utilize FW 8.37.2.0 ...
net: do not allow changing SO_REUSEADDR/SO_REUSEPORT on bound sockets It is not safe to do so because such sockets are already in the hash tables and changing these options can result in invalidating the tb->fastreuse(port) caching. This can have later far reaching consequences wrt. bind conflict checks which rely on these caches (for optimization purposes). Not to mention that you can currently end up with two identical non-reuseport listening sockets bound to the same local ip:port by clearing reuseport on them after they've already both been bound. There is unfortunately no EISBOUND error or anything similar, and EISCONN seems to be misleading for a bound-but-not-connected socket, so use EUCLEAN 'Structure needs cleaning' which AFAICT is the closest you can get to meaning 'socket in bad state'. (although perhaps EINVAL wouldn't be a bad choice either?) This does unfortunately run the risk of breaking buggy userspace programs... Signed-off-by: Maciej Żenczykowski <maze@google.com> Cc: Eric Dumazet <edumazet@google.com> Change-Id: I77c2b3429b2fdf42671eee0fa7a8ba721c94963b Reviewed-by: Eric Dumazet <edumazet@google.com> Signed-off-by: David S. Miller <davem@davemloft.net>
Merge branch 'work.aio-1' of git://git.kernel.org/pub/scm/linux/kernel/git/viro/vfs Pull aio updates from Al Viro: "Majority of AIO stuff this cycle. aio-fsync and aio-poll, mostly. The only thing I'm holding back for a day or so is Adam's aio ioprio - his last-minute fixup is trivial (missing stub in !CONFIG_BLOCK case), but let it sit in -next for decency sake..." * 'work.aio-1' of git://git.kernel.org/pub/scm/linux/kernel/git/viro/vfs: (46 commits) aio: sanitize the limit checking in io_submit(2) aio: fold do_io_submit() into callers aio: shift copyin of iocb into io_submit_one() aio_read_events_ring(): make a bit more readable aio: all callers of aio_{read,write,fsync,poll} treat 0 and -EIOCBQUEUED the same way aio: take list removal to (some) callers of aio_complete() aio: add missing break for the IOCB_CMD_FDSYNC case random: convert to ->poll_mask timerfd: convert to ->poll_mask eventfd: switch to ->poll_mask pipe: convert to ->poll_mask crypto: af_alg: convert to ->poll_mask net/rxrpc: convert to ->poll_mask net/iucv: convert to ->poll_mask net/phonet: convert to ->poll_mask net/nfc: convert to ->poll_mask net/caif: convert to ->poll_mask net/bluetooth: convert to ->poll_mask net/sctp: convert to ->poll_mask net/tipc: convert to ->poll_mask ...
Merge branch 'hch.procfs' of git://git.kernel.org/pub/scm/linux/kernel/git/viro/vfs Pull procfs updates from Al Viro: "Christoph's proc_create_... cleanups series" * 'hch.procfs' of git://git.kernel.org/pub/scm/linux/kernel/git/viro/vfs: (44 commits) xfs, proc: hide unused xfs procfs helpers isdn/gigaset: add back gigaset_procinfo assignment proc: update SIZEOF_PDE_INLINE_NAME for the new pde fields tty: replace ->proc_fops with ->proc_show ide: replace ->proc_fops with ->proc_show ide: remove ide_driver_proc_write isdn: replace ->proc_fops with ->proc_show atm: switch to proc_create_seq_private atm: simplify procfs code bluetooth: switch to proc_create_seq_data netfilter/x_tables: switch to proc_create_seq_private netfilter/xt_hashlimit: switch to proc_create_{seq,single}_data neigh: switch to proc_create_seq_data hostap: switch to proc_create_{seq,single}_data bonding: switch to proc_create_seq_data rtc/proc: switch to proc_create_single_data drbd: switch to proc_create_single resource: switch to proc_create_seq_data staging/rtl8192u: simplify procfs code jfs: simplify procfs code ...
net: remove sock_no_poll Now that sock_poll handles a NULL ->poll or ->poll_mask there is no need for a stub. Signed-off-by: Christoph Hellwig <hch@lst.de>
Merge git://git.kernel.org/pub/scm/linux/kernel/git/davem/net S390 bpf_jit.S is removed in net-next and had changes in 'net', since that code isn't used any more take the removal. TLS data structures split the TX and RX components in 'net-next', put the new struct members from the bug fix in 'net' into the RX part. The 'net-next' tree had some reworking of how the ERSPAN code works in the GRE tunneling code, overlapping with a one-line headroom calculation fix in 'net'. Overlapping changes in __sock_map_ctx_update_elem(), keep the bits that read the prog members via READ_ONCE() into local variables before using them. Signed-off-by: David S. Miller <davem@davemloft.net>
sock_diag: fix use-after-free read in __sk_free We must not call sock_diag_has_destroy_listeners(sk) on a socket that has no reference on net structure. BUG: KASAN: use-after-free in sock_diag_has_destroy_listeners include/linux/sock_diag.h:75 [inline] BUG: KASAN: use-after-free in __sk_free+0x329/0x340 net/core/sock.c:1609 Read of size 8 at addr ffff88018a02e3a0 by task swapper/1/0 CPU: 1 PID: 0 Comm: swapper/1 Not tainted 4.17.0-rc5+ #54 Hardware name: Google Google Compute Engine/Google Compute Engine, BIOS Google 01/01/2011 Call Trace: <IRQ> __dump_stack lib/dump_stack.c:77 [inline] dump_stack+0x1b9/0x294 lib/dump_stack.c:113 print_address_description+0x6c/0x20b mm/kasan/report.c:256 kasan_report_error mm/kasan/report.c:354 [inline] kasan_report.cold.7+0x242/0x2fe mm/kasan/report.c:412 __asan_report_load8_noabort+0x14/0x20 mm/kasan/report.c:433 sock_diag_has_destroy_listeners include/linux/sock_diag.h:75 [inline] __sk_free+0x329/0x340 net/core/sock.c:1609 sk_free+0x42/0x50 net/core/sock.c:1623 sock_put include/net/sock.h:1664 [inline] reqsk_free include/net/request_sock.h:116 [inline] reqsk_put include/net/request_sock.h:124 [inline] inet_csk_reqsk_queue_drop_and_put net/ipv4/inet_connection_sock.c:672 [inline] reqsk_timer_handler+0xe27/0x10e0 net/ipv4/inet_connection_sock.c:739 call_timer_fn+0x230/0x940 kernel/time/timer.c:1326 expire_timers kernel/time/timer.c:1363 [inline] __run_timers+0x79e/0xc50 kernel/time/timer.c:1666 run_timer_softirq+0x4c/0x70 kernel/time/timer.c:1692 __do_softirq+0x2e0/0xaf5 kernel/softirq.c:285 invoke_softirq kernel/softirq.c:365 [inline] irq_exit+0x1d1/0x200 kernel/softirq.c:405 exiting_irq arch/x86/include/asm/apic.h:525 [inline] smp_apic_timer_interrupt+0x17e/0x710 arch/x86/kernel/apic/apic.c:1052 apic_timer_interrupt+0xf/0x20 arch/x86/entry/entry_64.S:863 </IRQ> RIP: 0010:native_safe_halt+0x6/0x10 arch/x86/include/asm/irqflags.h:54 RSP: 0018:ffff8801d9ae7c38 EFLAGS: 00000282 ORIG_RAX: ffffffffffffff13 RAX: dffffc0000000000 RBX: 1ffff1003b35cf8a RCX: 0000000000000000 RDX: 1ffffffff11a30d0 RSI: 0000000000000001 RDI: ffffffff88d18680 RBP: ffff8801d9ae7c38 R08: ffffed003b5e46c3 R09: 0000000000000000 R10: 0000000000000000 R11: 0000000000000000 R12: 0000000000000001 R13: ffff8801d9ae7cf0 R14: ffffffff897bef20 R15: 0000000000000000 arch_safe_halt arch/x86/include/asm/paravirt.h:94 [inline] default_idle+0xc2/0x440 arch/x86/kernel/process.c:354 arch_cpu_idle+0x10/0x20 arch/x86/kernel/process.c:345 default_idle_call+0x6d/0x90 kernel/sched/idle.c:93 cpuidle_idle_call kernel/sched/idle.c:153 [inline] do_idle+0x395/0x560 kernel/sched/idle.c:262 cpu_startup_entry+0x104/0x120 kernel/sched/idle.c:368 start_secondary+0x426/0x5b0 arch/x86/kernel/smpboot.c:269 secondary_startup_64+0xa5/0xb0 arch/x86/kernel/head_64.S:242 Allocated by task 4557: save_stack+0x43/0xd0 mm/kasan/kasan.c:448 set_track mm/kasan/kasan.c:460 [inline] kasan_kmalloc+0xc4/0xe0 mm/kasan/kasan.c:553 kasan_slab_alloc+0x12/0x20 mm/kasan/kasan.c:490 kmem_cache_alloc+0x12e/0x760 mm/slab.c:3554 kmem_cache_zalloc include/linux/slab.h:691 [inline] net_alloc net/core/net_namespace.c:383 [inline] copy_net_ns+0x159/0x4c0 net/core/net_namespace.c:423 create_new_namespaces+0x69d/0x8f0 kernel/nsproxy.c:107 unshare_nsproxy_namespaces+0xc3/0x1f0 kernel/nsproxy.c:206 ksys_unshare+0x708/0xf90 kernel/fork.c:2408 __do_sys_unshare kernel/fork.c:2476 [inline] __se_sys_unshare kernel/fork.c:2474 [inline] __x64_sys_unshare+0x31/0x40 kernel/fork.c:2474 do_syscall_64+0x1b1/0x800 arch/x86/entry/common.c:287 entry_SYSCALL_64_after_hwframe+0x49/0xbe Freed by task 69: save_stack+0x43/0xd0 mm/kasan/kasan.c:448 set_track mm/kasan/kasan.c:460 [inline] __kasan_slab_free+0x11a/0x170 mm/kasan/kasan.c:521 kasan_slab_free+0xe/0x10 mm/kasan/kasan.c:528 __cache_free mm/slab.c:3498 [inline] kmem_cache_free+0x86/0x2d0 mm/slab.c:3756 net_free net/core/net_namespace.c:399 [inline] net_drop_ns.part.14+0x11a/0x130 net/core/net_namespace.c:406 net_drop_ns net/core/net_namespace.c:405 [inline] cleanup_net+0x6a1/0xb20 net/core/net_namespace.c:541 process_one_work+0xc1e/0x1b50 kernel/workqueue.c:2145 worker_thread+0x1cc/0x1440 kernel/workqueue.c:2279 kthread+0x345/0x410 kernel/kthread.c:240 ret_from_fork+0x3a/0x50 arch/x86/entry/entry_64.S:412 The buggy address belongs to the object at ffff88018a02c140 which belongs to the cache net_namespace of size 8832 The buggy address is located 8800 bytes inside of 8832-byte region [ffff88018a02c140, ffff88018a02e3c0) The buggy address belongs to the page: page:ffffea0006280b00 count:1 mapcount:0 mapping:ffff88018a02c140 index:0x0 compound_mapcount: 0 flags: 0x2fffc0000008100(slab|head) raw: 02fffc0000008100 ffff88018a02c140 0000000000000000 0000000100000001 raw: ffffea00062a1320 ffffea0006268020 ffff8801d9bdde40 0000000000000000 page dumped because: kasan: bad access detected Fixes: b922622ec6ef ("sock_diag: don't broadcast kernel sockets") Signed-off-by: Eric Dumazet <edumazet@google.com> Cc: Craig Gallek <kraig@google.com> Reported-by: syzbot <syzkaller@googlegroups.com> Signed-off-by: David S. Miller <davem@davemloft.net>
proc: introduce proc_create_net{,_data} Variants of proc_create{,_data} that directly take a struct seq_operations and deal with network namespaces in ->open and ->release. All callers of proc_create + seq_open_net converted over, and seq_{open,release}_net are removed entirely. Signed-off-by: Christoph Hellwig <hch@lst.de>