]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - Documentation/DMA-attributes.txt
Merge branch 'rpmsg-linux-4.19.y' of git://git.ti.com/rpmsg/rpmsg into rpmsg-ti-linux...
[rpmsg/rpmsg.git] / Documentation / DMA-attributes.txt
1 ==============
2 DMA attributes
3 ==============
5 This document describes the semantics of the DMA attributes that are
6 defined in linux/dma-mapping.h.
8 DMA_ATTR_WRITE_BARRIER
9 ----------------------
11 DMA_ATTR_WRITE_BARRIER is a (write) barrier attribute for DMA.  DMA
12 to a memory region with the DMA_ATTR_WRITE_BARRIER attribute forces
13 all pending DMA writes to complete, and thus provides a mechanism to
14 strictly order DMA from a device across all intervening busses and
15 bridges.  This barrier is not specific to a particular type of
16 interconnect, it applies to the system as a whole, and so its
17 implementation must account for the idiosyncrasies of the system all
18 the way from the DMA device to memory.
20 As an example of a situation where DMA_ATTR_WRITE_BARRIER would be
21 useful, suppose that a device does a DMA write to indicate that data is
22 ready and available in memory.  The DMA of the "completion indication"
23 could race with data DMA.  Mapping the memory used for completion
24 indications with DMA_ATTR_WRITE_BARRIER would prevent the race.
26 DMA_ATTR_WEAK_ORDERING
27 ----------------------
29 DMA_ATTR_WEAK_ORDERING specifies that reads and writes to the mapping
30 may be weakly ordered, that is that reads and writes may pass each other.
32 Since it is optional for platforms to implement DMA_ATTR_WEAK_ORDERING,
33 those that do not will simply ignore the attribute and exhibit default
34 behavior.
36 DMA_ATTR_WRITE_COMBINE
37 ----------------------
39 DMA_ATTR_WRITE_COMBINE specifies that writes to the mapping may be
40 buffered to improve performance.
42 Since it is optional for platforms to implement DMA_ATTR_WRITE_COMBINE,
43 those that do not will simply ignore the attribute and exhibit default
44 behavior.
46 DMA_ATTR_NON_CONSISTENT
47 -----------------------
49 DMA_ATTR_NON_CONSISTENT lets the platform to choose to return either
50 consistent or non-consistent memory as it sees fit.  By using this API,
51 you are guaranteeing to the platform that you have all the correct and
52 necessary sync points for this memory in the driver.
54 DMA_ATTR_NO_KERNEL_MAPPING
55 --------------------------
57 DMA_ATTR_NO_KERNEL_MAPPING lets the platform to avoid creating a kernel
58 virtual mapping for the allocated buffer. On some architectures creating
59 such mapping is non-trivial task and consumes very limited resources
60 (like kernel virtual address space or dma consistent address space).
61 Buffers allocated with this attribute can be only passed to user space
62 by calling dma_mmap_attrs(). By using this API, you are guaranteeing
63 that you won't dereference the pointer returned by dma_alloc_attr(). You
64 can treat it as a cookie that must be passed to dma_mmap_attrs() and
65 dma_free_attrs(). Make sure that both of these also get this attribute
66 set on each call.
68 Since it is optional for platforms to implement
69 DMA_ATTR_NO_KERNEL_MAPPING, those that do not will simply ignore the
70 attribute and exhibit default behavior.
72 DMA_ATTR_SKIP_CPU_SYNC
73 ----------------------
75 By default dma_map_{single,page,sg} functions family transfer a given
76 buffer from CPU domain to device domain. Some advanced use cases might
77 require sharing a buffer between more than one device. This requires
78 having a mapping created separately for each device and is usually
79 performed by calling dma_map_{single,page,sg} function more than once
80 for the given buffer with device pointer to each device taking part in
81 the buffer sharing. The first call transfers a buffer from 'CPU' domain
82 to 'device' domain, what synchronizes CPU caches for the given region
83 (usually it means that the cache has been flushed or invalidated
84 depending on the dma direction). However, next calls to
85 dma_map_{single,page,sg}() for other devices will perform exactly the
86 same synchronization operation on the CPU cache. CPU cache synchronization
87 might be a time consuming operation, especially if the buffers are
88 large, so it is highly recommended to avoid it if possible.
89 DMA_ATTR_SKIP_CPU_SYNC allows platform code to skip synchronization of
90 the CPU cache for the given buffer assuming that it has been already
91 transferred to 'device' domain. This attribute can be also used for
92 dma_unmap_{single,page,sg} functions family to force buffer to stay in
93 device domain after releasing a mapping for it. Use this attribute with
94 care!
96 DMA_ATTR_FORCE_CONTIGUOUS
97 -------------------------
99 By default DMA-mapping subsystem is allowed to assemble the buffer
100 allocated by dma_alloc_attrs() function from individual pages if it can
101 be mapped as contiguous chunk into device dma address space. By
102 specifying this attribute the allocated buffer is forced to be contiguous
103 also in physical memory.
105 DMA_ATTR_ALLOC_SINGLE_PAGES
106 ---------------------------
108 This is a hint to the DMA-mapping subsystem that it's probably not worth
109 the time to try to allocate memory to in a way that gives better TLB
110 efficiency (AKA it's not worth trying to build the mapping out of larger
111 pages).  You might want to specify this if:
113 - You know that the accesses to this memory won't thrash the TLB.
114   You might know that the accesses are likely to be sequential or
115   that they aren't sequential but it's unlikely you'll ping-pong
116   between many addresses that are likely to be in different physical
117   pages.
118 - You know that the penalty of TLB misses while accessing the
119   memory will be small enough to be inconsequential.  If you are
120   doing a heavy operation like decryption or decompression this
121   might be the case.
122 - You know that the DMA mapping is fairly transitory.  If you expect
123   the mapping to have a short lifetime then it may be worth it to
124   optimize allocation (avoid coming up with large pages) instead of
125   getting the slight performance win of larger pages.
127 Setting this hint doesn't guarantee that you won't get huge pages, but it
128 means that we won't try quite as hard to get them.
130 .. note:: At the moment DMA_ATTR_ALLOC_SINGLE_PAGES is only implemented on ARM,
131           though ARM64 patches will likely be posted soon.
133 DMA_ATTR_NO_WARN
134 ----------------
136 This tells the DMA-mapping subsystem to suppress allocation failure reports
137 (similarly to __GFP_NOWARN).
139 On some architectures allocation failures are reported with error messages
140 to the system logs.  Although this can help to identify and debug problems,
141 drivers which handle failures (eg, retry later) have no problems with them,
142 and can actually flood the system logs with error messages that aren't any
143 problem at all, depending on the implementation of the retry mechanism.
145 So, this provides a way for drivers to avoid those error messages on calls
146 where allocation failures are not a problem, and shouldn't bother the logs.
148 .. note:: At the moment DMA_ATTR_NO_WARN is only implemented on PowerPC.
150 DMA_ATTR_PRIVILEGED
151 -------------------
153 Some advanced peripherals such as remote processors and GPUs perform
154 accesses to DMA buffers in both privileged "supervisor" and unprivileged
155 "user" modes.  This attribute is used to indicate to the DMA-mapping
156 subsystem that the buffer is fully accessible at the elevated privilege
157 level (and ideally inaccessible or at least read-only at the
158 lesser-privileged levels).