1 =====================
2 The Linux IPMI Driver
3 =====================
5 :Author: Corey Minyard <minyard@mvista.com> / <minyard@acm.org>
7 The Intelligent Platform Management Interface, or IPMI, is a
8 standard for controlling intelligent devices that monitor a system.
9 It provides for dynamic discovery of sensors in the system and the
10 ability to monitor the sensors and be informed when the sensor's
11 values change or go outside certain boundaries. It also has a
12 standardized database for field-replaceable units (FRUs) and a watchdog
13 timer.
15 To use this, you need an interface to an IPMI controller in your
16 system (called a Baseboard Management Controller, or BMC) and
17 management software that can use the IPMI system.
19 This document describes how to use the IPMI driver for Linux. If you
20 are not familiar with IPMI itself, see the web site at
21 http://www.intel.com/design/servers/ipmi/index.htm. IPMI is a big
22 subject and I can't cover it all here!
24 Configuration
25 -------------
27 The Linux IPMI driver is modular, which means you have to pick several
28 things to have it work right depending on your hardware. Most of
29 these are available in the 'Character Devices' menu then the IPMI
30 menu.
32 No matter what, you must pick 'IPMI top-level message handler' to use
33 IPMI. What you do beyond that depends on your needs and hardware.
35 The message handler does not provide any user-level interfaces.
36 Kernel code (like the watchdog) can still use it. If you need access
37 from userland, you need to select 'Device interface for IPMI' if you
38 want access through a device driver.
40 The driver interface depends on your hardware. If your system
41 properly provides the SMBIOS info for IPMI, the driver will detect it
42 and just work. If you have a board with a standard interface (These
43 will generally be either "KCS", "SMIC", or "BT", consult your hardware
44 manual), choose the 'IPMI SI handler' option. A driver also exists
45 for direct I2C access to the IPMI management controller. Some boards
46 support this, but it is unknown if it will work on every board. For
47 this, choose 'IPMI SMBus handler', but be ready to try to do some
48 figuring to see if it will work on your system if the SMBIOS/APCI
49 information is wrong or not present. It is fairly safe to have both
50 these enabled and let the drivers auto-detect what is present.
52 You should generally enable ACPI on your system, as systems with IPMI
53 can have ACPI tables describing them.
55 If you have a standard interface and the board manufacturer has done
56 their job correctly, the IPMI controller should be automatically
57 detected (via ACPI or SMBIOS tables) and should just work. Sadly,
58 many boards do not have this information. The driver attempts
59 standard defaults, but they may not work. If you fall into this
60 situation, you need to read the section below named 'The SI Driver' or
61 "The SMBus Driver" on how to hand-configure your system.
63 IPMI defines a standard watchdog timer. You can enable this with the
64 'IPMI Watchdog Timer' config option. If you compile the driver into
65 the kernel, then via a kernel command-line option you can have the
66 watchdog timer start as soon as it initializes. It also have a lot
67 of other options, see the 'Watchdog' section below for more details.
68 Note that you can also have the watchdog continue to run if it is
69 closed (by default it is disabled on close). Go into the 'Watchdog
70 Cards' menu, enable 'Watchdog Timer Support', and enable the option
71 'Disable watchdog shutdown on close'.
73 IPMI systems can often be powered off using IPMI commands. Select
74 'IPMI Poweroff' to do this. The driver will auto-detect if the system
75 can be powered off by IPMI. It is safe to enable this even if your
76 system doesn't support this option. This works on ATCA systems, the
77 Radisys CPI1 card, and any IPMI system that supports standard chassis
78 management commands.
80 If you want the driver to put an event into the event log on a panic,
81 enable the 'Generate a panic event to all BMCs on a panic' option. If
82 you want the whole panic string put into the event log using OEM
83 events, enable the 'Generate OEM events containing the panic string'
84 option. You can also enable these dynamically by setting the module
85 parameter named "panic_op" in the ipmi_msghandler module to "event"
86 or "string". Setting that parameter to "none" disables this function.
88 Basic Design
89 ------------
91 The Linux IPMI driver is designed to be very modular and flexible, you
92 only need to take the pieces you need and you can use it in many
93 different ways. Because of that, it's broken into many chunks of
94 code. These chunks (by module name) are:
96 ipmi_msghandler - This is the central piece of software for the IPMI
97 system. It handles all messages, message timing, and responses. The
98 IPMI users tie into this, and the IPMI physical interfaces (called
99 System Management Interfaces, or SMIs) also tie in here. This
100 provides the kernelland interface for IPMI, but does not provide an
101 interface for use by application processes.
103 ipmi_devintf - This provides a userland IOCTL interface for the IPMI
104 driver, each open file for this device ties in to the message handler
105 as an IPMI user.
107 ipmi_si - A driver for various system interfaces. This supports KCS,
108 SMIC, and BT interfaces. Unless you have an SMBus interface or your
109 own custom interface, you probably need to use this.
111 ipmi_ssif - A driver for accessing BMCs on the SMBus. It uses the
112 I2C kernel driver's SMBus interfaces to send and receive IPMI messages
113 over the SMBus.
115 ipmi_powernv - A driver for access BMCs on POWERNV systems.
117 ipmi_watchdog - IPMI requires systems to have a very capable watchdog
118 timer. This driver implements the standard Linux watchdog timer
119 interface on top of the IPMI message handler.
121 ipmi_poweroff - Some systems support the ability to be turned off via
122 IPMI commands.
124 bt-bmc - This is not part of the main driver, but instead a driver for
125 accessing a BMC-side interface of a BT interface. It is used on BMCs
126 running Linux to provide an interface to the host.
128 These are all individually selectable via configuration options.
130 Much documentation for the interface is in the include files. The
131 IPMI include files are:
133 linux/ipmi.h - Contains the user interface and IOCTL interface for IPMI.
135 linux/ipmi_smi.h - Contains the interface for system management interfaces
136 (things that interface to IPMI controllers) to use.
138 linux/ipmi_msgdefs.h - General definitions for base IPMI messaging.
141 Addressing
142 ----------
144 The IPMI addressing works much like IP addresses, you have an overlay
145 to handle the different address types. The overlay is::
147 struct ipmi_addr
148 {
149 int addr_type;
150 short channel;
151 char data[IPMI_MAX_ADDR_SIZE];
152 };
154 The addr_type determines what the address really is. The driver
155 currently understands two different types of addresses.
157 "System Interface" addresses are defined as::
159 struct ipmi_system_interface_addr
160 {
161 int addr_type;
162 short channel;
163 };
165 and the type is IPMI_SYSTEM_INTERFACE_ADDR_TYPE. This is used for talking
166 straight to the BMC on the current card. The channel must be
167 IPMI_BMC_CHANNEL.
169 Messages that are destined to go out on the IPMB bus use the
170 IPMI_IPMB_ADDR_TYPE address type. The format is::
172 struct ipmi_ipmb_addr
173 {
174 int addr_type;
175 short channel;
176 unsigned char slave_addr;
177 unsigned char lun;
178 };
180 The "channel" here is generally zero, but some devices support more
181 than one channel, it corresponds to the channel as defined in the IPMI
182 spec.
185 Messages
186 --------
188 Messages are defined as::
190 struct ipmi_msg
191 {
192 unsigned char netfn;
193 unsigned char lun;
194 unsigned char cmd;
195 unsigned char *data;
196 int data_len;
197 };
199 The driver takes care of adding/stripping the header information. The
200 data portion is just the data to be send (do NOT put addressing info
201 here) or the response. Note that the completion code of a response is
202 the first item in "data", it is not stripped out because that is how
203 all the messages are defined in the spec (and thus makes counting the
204 offsets a little easier :-).
206 When using the IOCTL interface from userland, you must provide a block
207 of data for "data", fill it, and set data_len to the length of the
208 block of data, even when receiving messages. Otherwise the driver
209 will have no place to put the message.
211 Messages coming up from the message handler in kernelland will come in
212 as::
214 struct ipmi_recv_msg
215 {
216 struct list_head link;
218 /* The type of message as defined in the "Receive Types"
219 defines above. */
220 int recv_type;
222 ipmi_user_t *user;
223 struct ipmi_addr addr;
224 long msgid;
225 struct ipmi_msg msg;
227 /* Call this when done with the message. It will presumably free
228 the message and do any other necessary cleanup. */
229 void (*done)(struct ipmi_recv_msg *msg);
231 /* Place-holder for the data, don't make any assumptions about
232 the size or existence of this, since it may change. */
233 unsigned char msg_data[IPMI_MAX_MSG_LENGTH];
234 };
236 You should look at the receive type and handle the message
237 appropriately.
240 The Upper Layer Interface (Message Handler)
241 -------------------------------------------
243 The upper layer of the interface provides the users with a consistent
244 view of the IPMI interfaces. It allows multiple SMI interfaces to be
245 addressed (because some boards actually have multiple BMCs on them)
246 and the user should not have to care what type of SMI is below them.
249 Watching For Interfaces
250 ^^^^^^^^^^^^^^^^^^^^^^^
252 When your code comes up, the IPMI driver may or may not have detected
253 if IPMI devices exist. So you might have to defer your setup until
254 the device is detected, or you might be able to do it immediately.
255 To handle this, and to allow for discovery, you register an SMI
256 watcher with ipmi_smi_watcher_register() to iterate over interfaces
257 and tell you when they come and go.
260 Creating the User
261 ^^^^^^^^^^^^^^^^^
263 To use the message handler, you must first create a user using
264 ipmi_create_user. The interface number specifies which SMI you want
265 to connect to, and you must supply callback functions to be called
266 when data comes in. The callback function can run at interrupt level,
267 so be careful using the callbacks. This also allows to you pass in a
268 piece of data, the handler_data, that will be passed back to you on
269 all calls.
271 Once you are done, call ipmi_destroy_user() to get rid of the user.
273 From userland, opening the device automatically creates a user, and
274 closing the device automatically destroys the user.
277 Messaging
278 ^^^^^^^^^
280 To send a message from kernel-land, the ipmi_request_settime() call does
281 pretty much all message handling. Most of the parameter are
282 self-explanatory. However, it takes a "msgid" parameter. This is NOT
283 the sequence number of messages. It is simply a long value that is
284 passed back when the response for the message is returned. You may
285 use it for anything you like.
287 Responses come back in the function pointed to by the ipmi_recv_hndl
288 field of the "handler" that you passed in to ipmi_create_user().
289 Remember again, these may be running at interrupt level. Remember to
290 look at the receive type, too.
292 From userland, you fill out an ipmi_req_t structure and use the
293 IPMICTL_SEND_COMMAND ioctl. For incoming stuff, you can use select()
294 or poll() to wait for messages to come in. However, you cannot use
295 read() to get them, you must call the IPMICTL_RECEIVE_MSG with the
296 ipmi_recv_t structure to actually get the message. Remember that you
297 must supply a pointer to a block of data in the msg.data field, and
298 you must fill in the msg.data_len field with the size of the data.
299 This gives the receiver a place to actually put the message.
301 If the message cannot fit into the data you provide, you will get an
302 EMSGSIZE error and the driver will leave the data in the receive
303 queue. If you want to get it and have it truncate the message, us
304 the IPMICTL_RECEIVE_MSG_TRUNC ioctl.
306 When you send a command (which is defined by the lowest-order bit of
307 the netfn per the IPMI spec) on the IPMB bus, the driver will
308 automatically assign the sequence number to the command and save the
309 command. If the response is not receive in the IPMI-specified 5
310 seconds, it will generate a response automatically saying the command
311 timed out. If an unsolicited response comes in (if it was after 5
312 seconds, for instance), that response will be ignored.
314 In kernelland, after you receive a message and are done with it, you
315 MUST call ipmi_free_recv_msg() on it, or you will leak messages. Note
316 that you should NEVER mess with the "done" field of a message, that is
317 required to properly clean up the message.
319 Note that when sending, there is an ipmi_request_supply_msgs() call
320 that lets you supply the smi and receive message. This is useful for
321 pieces of code that need to work even if the system is out of buffers
322 (the watchdog timer uses this, for instance). You supply your own
323 buffer and own free routines. This is not recommended for normal use,
324 though, since it is tricky to manage your own buffers.
327 Events and Incoming Commands
328 ^^^^^^^^^^^^^^^^^^^^^^^^^^^^
330 The driver takes care of polling for IPMI events and receiving
331 commands (commands are messages that are not responses, they are
332 commands that other things on the IPMB bus have sent you). To receive
333 these, you must register for them, they will not automatically be sent
334 to you.
336 To receive events, you must call ipmi_set_gets_events() and set the
337 "val" to non-zero. Any events that have been received by the driver
338 since startup will immediately be delivered to the first user that
339 registers for events. After that, if multiple users are registered
340 for events, they will all receive all events that come in.
342 For receiving commands, you have to individually register commands you
343 want to receive. Call ipmi_register_for_cmd() and supply the netfn
344 and command name for each command you want to receive. You also
345 specify a bitmask of the channels you want to receive the command from
346 (or use IPMI_CHAN_ALL for all channels if you don't care). Only one
347 user may be registered for each netfn/cmd/channel, but different users
348 may register for different commands, or the same command if the
349 channel bitmasks do not overlap.
351 From userland, equivalent IOCTLs are provided to do these functions.
354 The Lower Layer (SMI) Interface
355 -------------------------------
357 As mentioned before, multiple SMI interfaces may be registered to the
358 message handler, each of these is assigned an interface number when
359 they register with the message handler. They are generally assigned
360 in the order they register, although if an SMI unregisters and then
361 another one registers, all bets are off.
363 The ipmi_smi.h defines the interface for management interfaces, see
364 that for more details.
367 The SI Driver
368 -------------
370 The SI driver allows KCS, BT, and SMIC interfaces to be configured
371 in the system. It discovers interfaces through a host of different
372 methods, depending on the system.
374 You can specify up to four interfaces on the module load line and
375 control some module parameters::
377 modprobe ipmi_si.o type=<type1>,<type2>....
378 ports=<port1>,<port2>... addrs=<addr1>,<addr2>...
379 irqs=<irq1>,<irq2>...
380 regspacings=<sp1>,<sp2>,... regsizes=<size1>,<size2>,...
381 regshifts=<shift1>,<shift2>,...
382 slave_addrs=<addr1>,<addr2>,...
383 force_kipmid=<enable1>,<enable2>,...
384 kipmid_max_busy_us=<ustime1>,<ustime2>,...
385 unload_when_empty=[0|1]
386 trydmi=[0|1] tryacpi=[0|1]
387 tryplatform=[0|1] trypci=[0|1]
389 Each of these except try... items is a list, the first item for the
390 first interface, second item for the second interface, etc.
392 The si_type may be either "kcs", "smic", or "bt". If you leave it blank, it
393 defaults to "kcs".
395 If you specify addrs as non-zero for an interface, the driver will
396 use the memory address given as the address of the device. This
397 overrides si_ports.
399 If you specify ports as non-zero for an interface, the driver will
400 use the I/O port given as the device address.
402 If you specify irqs as non-zero for an interface, the driver will
403 attempt to use the given interrupt for the device.
405 The other try... items disable discovery by their corresponding
406 names. These are all enabled by default, set them to zero to disable
407 them. The tryplatform disables openfirmware.
409 The next three parameters have to do with register layout. The
410 registers used by the interfaces may not appear at successive
411 locations and they may not be in 8-bit registers. These parameters
412 allow the layout of the data in the registers to be more precisely
413 specified.
415 The regspacings parameter give the number of bytes between successive
416 register start addresses. For instance, if the regspacing is set to 4
417 and the start address is 0xca2, then the address for the second
418 register would be 0xca6. This defaults to 1.
420 The regsizes parameter gives the size of a register, in bytes. The
421 data used by IPMI is 8-bits wide, but it may be inside a larger
422 register. This parameter allows the read and write type to specified.
423 It may be 1, 2, 4, or 8. The default is 1.
425 Since the register size may be larger than 32 bits, the IPMI data may not
426 be in the lower 8 bits. The regshifts parameter give the amount to shift
427 the data to get to the actual IPMI data.
429 The slave_addrs specifies the IPMI address of the local BMC. This is
430 usually 0x20 and the driver defaults to that, but in case it's not, it
431 can be specified when the driver starts up.
433 The force_ipmid parameter forcefully enables (if set to 1) or disables
434 (if set to 0) the kernel IPMI daemon. Normally this is auto-detected
435 by the driver, but systems with broken interrupts might need an enable,
436 or users that don't want the daemon (don't need the performance, don't
437 want the CPU hit) can disable it.
439 If unload_when_empty is set to 1, the driver will be unloaded if it
440 doesn't find any interfaces or all the interfaces fail to work. The
441 default is one. Setting to 0 is useful with the hotmod, but is
442 obviously only useful for modules.
444 When compiled into the kernel, the parameters can be specified on the
445 kernel command line as::
447 ipmi_si.type=<type1>,<type2>...
448 ipmi_si.ports=<port1>,<port2>... ipmi_si.addrs=<addr1>,<addr2>...
449 ipmi_si.irqs=<irq1>,<irq2>...
450 ipmi_si.regspacings=<sp1>,<sp2>,...
451 ipmi_si.regsizes=<size1>,<size2>,...
452 ipmi_si.regshifts=<shift1>,<shift2>,...
453 ipmi_si.slave_addrs=<addr1>,<addr2>,...
454 ipmi_si.force_kipmid=<enable1>,<enable2>,...
455 ipmi_si.kipmid_max_busy_us=<ustime1>,<ustime2>,...
457 It works the same as the module parameters of the same names.
459 If your IPMI interface does not support interrupts and is a KCS or
460 SMIC interface, the IPMI driver will start a kernel thread for the
461 interface to help speed things up. This is a low-priority kernel
462 thread that constantly polls the IPMI driver while an IPMI operation
463 is in progress. The force_kipmid module parameter will all the user to
464 force this thread on or off. If you force it off and don't have
465 interrupts, the driver will run VERY slowly. Don't blame me,
466 these interfaces suck.
468 Unfortunately, this thread can use a lot of CPU depending on the
469 interface's performance. This can waste a lot of CPU and cause
470 various issues with detecting idle CPU and using extra power. To
471 avoid this, the kipmid_max_busy_us sets the maximum amount of time, in
472 microseconds, that kipmid will spin before sleeping for a tick. This
473 value sets a balance between performance and CPU waste and needs to be
474 tuned to your needs. Maybe, someday, auto-tuning will be added, but
475 that's not a simple thing and even the auto-tuning would need to be
476 tuned to the user's desired performance.
478 The driver supports a hot add and remove of interfaces. This way,
479 interfaces can be added or removed after the kernel is up and running.
480 This is done using /sys/modules/ipmi_si/parameters/hotmod, which is a
481 write-only parameter. You write a string to this interface. The string
482 has the format::
484 <op1>[:op2[:op3...]]
486 The "op"s are::
488 add|remove,kcs|bt|smic,mem|i/o,<address>[,<opt1>[,<opt2>[,...]]]
490 You can specify more than one interface on the line. The "opt"s are::
492 rsp=<regspacing>
493 rsi=<regsize>
494 rsh=<regshift>
495 irq=<irq>
496 ipmb=<ipmb slave addr>
498 and these have the same meanings as discussed above. Note that you
499 can also use this on the kernel command line for a more compact format
500 for specifying an interface. Note that when removing an interface,
501 only the first three parameters (si type, address type, and address)
502 are used for the comparison. Any options are ignored for removing.
504 The SMBus Driver (SSIF)
505 -----------------------
507 The SMBus driver allows up to 4 SMBus devices to be configured in the
508 system. By default, the driver will only register with something it
509 finds in DMI or ACPI tables. You can change this
510 at module load time (for a module) with::
512 modprobe ipmi_ssif.o
513 addr=<i2caddr1>[,<i2caddr2>[,...]]
514 adapter=<adapter1>[,<adapter2>[...]]
515 dbg=<flags1>,<flags2>...
516 slave_addrs=<addr1>,<addr2>,...
517 tryacpi=[0|1] trydmi=[0|1]
518 [dbg_probe=1]
520 The addresses are normal I2C addresses. The adapter is the string
521 name of the adapter, as shown in /sys/class/i2c-adapter/i2c-<n>/name.
522 It is *NOT* i2c-<n> itself. Also, the comparison is done ignoring
523 spaces, so if the name is "This is an I2C chip" you can say
524 adapter_name=ThisisanI2cchip. This is because it's hard to pass in
525 spaces in kernel parameters.
527 The debug flags are bit flags for each BMC found, they are:
528 IPMI messages: 1, driver state: 2, timing: 4, I2C probe: 8
530 The tryxxx parameters can be used to disable detecting interfaces
531 from various sources.
533 Setting dbg_probe to 1 will enable debugging of the probing and
534 detection process for BMCs on the SMBusses.
536 The slave_addrs specifies the IPMI address of the local BMC. This is
537 usually 0x20 and the driver defaults to that, but in case it's not, it
538 can be specified when the driver starts up.
540 Discovering the IPMI compliant BMC on the SMBus can cause devices on
541 the I2C bus to fail. The SMBus driver writes a "Get Device ID" IPMI
542 message as a block write to the I2C bus and waits for a response.
543 This action can be detrimental to some I2C devices. It is highly
544 recommended that the known I2C address be given to the SMBus driver in
545 the smb_addr parameter unless you have DMI or ACPI data to tell the
546 driver what to use.
548 When compiled into the kernel, the addresses can be specified on the
549 kernel command line as::
551 ipmb_ssif.addr=<i2caddr1>[,<i2caddr2>[...]]
552 ipmi_ssif.adapter=<adapter1>[,<adapter2>[...]]
553 ipmi_ssif.dbg=<flags1>[,<flags2>[...]]
554 ipmi_ssif.dbg_probe=1
555 ipmi_ssif.slave_addrs=<addr1>[,<addr2>[...]]
556 ipmi_ssif.tryacpi=[0|1] ipmi_ssif.trydmi=[0|1]
558 These are the same options as on the module command line.
560 The I2C driver does not support non-blocking access or polling, so
561 this driver cannod to IPMI panic events, extend the watchdog at panic
562 time, or other panic-related IPMI functions without special kernel
563 patches and driver modifications. You can get those at the openipmi
564 web page.
566 The driver supports a hot add and remove of interfaces through the I2C
567 sysfs interface.
569 Other Pieces
570 ------------
572 Get the detailed info related with the IPMI device
573 --------------------------------------------------
575 Some users need more detailed information about a device, like where
576 the address came from or the raw base device for the IPMI interface.
577 You can use the IPMI smi_watcher to catch the IPMI interfaces as they
578 come or go, and to grab the information, you can use the function
579 ipmi_get_smi_info(), which returns the following structure::
581 struct ipmi_smi_info {
582 enum ipmi_addr_src addr_src;
583 struct device *dev;
584 union {
585 struct {
586 void *acpi_handle;
587 } acpi_info;
588 } addr_info;
589 };
591 Currently special info for only for SI_ACPI address sources is
592 returned. Others may be added as necessary.
594 Note that the dev pointer is included in the above structure, and
595 assuming ipmi_smi_get_info returns success, you must call put_device
596 on the dev pointer.
599 Watchdog
600 --------
602 A watchdog timer is provided that implements the Linux-standard
603 watchdog timer interface. It has three module parameters that can be
604 used to control it::
606 modprobe ipmi_watchdog timeout=<t> pretimeout=<t> action=<action type>
607 preaction=<preaction type> preop=<preop type> start_now=x
608 nowayout=x ifnum_to_use=n panic_wdt_timeout=<t>
610 ifnum_to_use specifies which interface the watchdog timer should use.
611 The default is -1, which means to pick the first one registered.
613 The timeout is the number of seconds to the action, and the pretimeout
614 is the amount of seconds before the reset that the pre-timeout panic will
615 occur (if pretimeout is zero, then pretimeout will not be enabled). Note
616 that the pretimeout is the time before the final timeout. So if the
617 timeout is 50 seconds and the pretimeout is 10 seconds, then the pretimeout
618 will occur in 40 second (10 seconds before the timeout). The panic_wdt_timeout
619 is the value of timeout which is set on kernel panic, in order to let actions
620 such as kdump to occur during panic.
622 The action may be "reset", "power_cycle", or "power_off", and
623 specifies what to do when the timer times out, and defaults to
624 "reset".
626 The preaction may be "pre_smi" for an indication through the SMI
627 interface, "pre_int" for an indication through the SMI with an
628 interrupts, and "pre_nmi" for a NMI on a preaction. This is how
629 the driver is informed of the pretimeout.
631 The preop may be set to "preop_none" for no operation on a pretimeout,
632 "preop_panic" to set the preoperation to panic, or "preop_give_data"
633 to provide data to read from the watchdog device when the pretimeout
634 occurs. A "pre_nmi" setting CANNOT be used with "preop_give_data"
635 because you can't do data operations from an NMI.
637 When preop is set to "preop_give_data", one byte comes ready to read
638 on the device when the pretimeout occurs. Select and fasync work on
639 the device, as well.
641 If start_now is set to 1, the watchdog timer will start running as
642 soon as the driver is loaded.
644 If nowayout is set to 1, the watchdog timer will not stop when the
645 watchdog device is closed. The default value of nowayout is true
646 if the CONFIG_WATCHDOG_NOWAYOUT option is enabled, or false if not.
648 When compiled into the kernel, the kernel command line is available
649 for configuring the watchdog::
651 ipmi_watchdog.timeout=<t> ipmi_watchdog.pretimeout=<t>
652 ipmi_watchdog.action=<action type>
653 ipmi_watchdog.preaction=<preaction type>
654 ipmi_watchdog.preop=<preop type>
655 ipmi_watchdog.start_now=x
656 ipmi_watchdog.nowayout=x
657 ipmi_watchdog.panic_wdt_timeout=<t>
659 The options are the same as the module parameter options.
661 The watchdog will panic and start a 120 second reset timeout if it
662 gets a pre-action. During a panic or a reboot, the watchdog will
663 start a 120 timer if it is running to make sure the reboot occurs.
665 Note that if you use the NMI preaction for the watchdog, you MUST NOT
666 use the nmi watchdog. There is no reasonable way to tell if an NMI
667 comes from the IPMI controller, so it must assume that if it gets an
668 otherwise unhandled NMI, it must be from IPMI and it will panic
669 immediately.
671 Once you open the watchdog timer, you must write a 'V' character to the
672 device to close it, or the timer will not stop. This is a new semantic
673 for the driver, but makes it consistent with the rest of the watchdog
674 drivers in Linux.
677 Panic Timeouts
678 --------------
680 The OpenIPMI driver supports the ability to put semi-custom and custom
681 events in the system event log if a panic occurs. if you enable the
682 'Generate a panic event to all BMCs on a panic' option, you will get
683 one event on a panic in a standard IPMI event format. If you enable
684 the 'Generate OEM events containing the panic string' option, you will
685 also get a bunch of OEM events holding the panic string.
688 The field settings of the events are:
690 * Generator ID: 0x21 (kernel)
691 * EvM Rev: 0x03 (this event is formatting in IPMI 1.0 format)
692 * Sensor Type: 0x20 (OS critical stop sensor)
693 * Sensor #: The first byte of the panic string (0 if no panic string)
694 * Event Dir | Event Type: 0x6f (Assertion, sensor-specific event info)
695 * Event Data 1: 0xa1 (Runtime stop in OEM bytes 2 and 3)
696 * Event data 2: second byte of panic string
697 * Event data 3: third byte of panic string
699 See the IPMI spec for the details of the event layout. This event is
700 always sent to the local management controller. It will handle routing
701 the message to the right place
703 Other OEM events have the following format:
705 * Record ID (bytes 0-1): Set by the SEL.
706 * Record type (byte 2): 0xf0 (OEM non-timestamped)
707 * byte 3: The slave address of the card saving the panic
708 * byte 4: A sequence number (starting at zero)
709 The rest of the bytes (11 bytes) are the panic string. If the panic string
710 is longer than 11 bytes, multiple messages will be sent with increasing
711 sequence numbers.
713 Because you cannot send OEM events using the standard interface, this
714 function will attempt to find an SEL and add the events there. It
715 will first query the capabilities of the local management controller.
716 If it has an SEL, then they will be stored in the SEL of the local
717 management controller. If not, and the local management controller is
718 an event generator, the event receiver from the local management
719 controller will be queried and the events sent to the SEL on that
720 device. Otherwise, the events go nowhere since there is nowhere to
721 send them.
724 Poweroff
725 --------
727 If the poweroff capability is selected, the IPMI driver will install
728 a shutdown function into the standard poweroff function pointer. This
729 is in the ipmi_poweroff module. When the system requests a powerdown,
730 it will send the proper IPMI commands to do this. This is supported on
731 several platforms.
733 There is a module parameter named "poweroff_powercycle" that may
734 either be zero (do a power down) or non-zero (do a power cycle, power
735 the system off, then power it on in a few seconds). Setting
736 ipmi_poweroff.poweroff_control=x will do the same thing on the kernel
737 command line. The parameter is also available via the proc filesystem
738 in /proc/sys/dev/ipmi/poweroff_powercycle. Note that if the system
739 does not support power cycling, it will always do the power off.
741 The "ifnum_to_use" parameter specifies which interface the poweroff
742 code should use. The default is -1, which means to pick the first one
743 registered.
745 Note that if you have ACPI enabled, the system will prefer using ACPI to
746 power off.