]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - Documentation/Makefile
Revert "HACK: ARM: dts: dra7-ipu-common: Revert to CMA pools for IPU early boots"
[rpmsg/rpmsg.git] / Documentation / Makefile
1 # -*- makefile -*-
2 # Makefile for Sphinx documentation
3 #
5 subdir-y :=
7 # You can set these variables from the command line.
8 SPHINXBUILD   = sphinx-build
9 SPHINXOPTS    =
10 SPHINXDIRS    = .
11 _SPHINXDIRS   = $(patsubst $(srctree)/Documentation/%/conf.py,%,$(wildcard $(srctree)/Documentation/*/conf.py))
12 SPHINX_CONF   = conf.py
13 PAPER         =
14 BUILDDIR      = $(obj)/output
15 PDFLATEX      = xelatex
16 LATEXOPTS     = -interaction=batchmode
18 # User-friendly check for sphinx-build
19 HAVE_SPHINX := $(shell if which $(SPHINXBUILD) >/dev/null 2>&1; then echo 1; else echo 0; fi)
21 ifeq ($(HAVE_SPHINX),0)
23 .DEFAULT:
24         $(warning The '$(SPHINXBUILD)' command was not found. Make sure you have Sphinx installed and in PATH, or set the SPHINXBUILD make variable to point to the full path of the '$(SPHINXBUILD)' executable.)
25         @echo
26         @./scripts/sphinx-pre-install
27         @echo "  SKIP    Sphinx $@ target."
29 else # HAVE_SPHINX
31 # User-friendly check for pdflatex
32 HAVE_PDFLATEX := $(shell if which $(PDFLATEX) >/dev/null 2>&1; then echo 1; else echo 0; fi)
34 # Internal variables.
35 PAPEROPT_a4     = -D latex_paper_size=a4
36 PAPEROPT_letter = -D latex_paper_size=letter
37 KERNELDOC       = $(srctree)/scripts/kernel-doc
38 KERNELDOC_CONF  = -D kerneldoc_srctree=$(srctree) -D kerneldoc_bin=$(KERNELDOC)
39 ALLSPHINXOPTS   =  $(KERNELDOC_CONF) $(PAPEROPT_$(PAPER)) $(SPHINXOPTS)
40 # the i18n builder cannot share the environment and doctrees with the others
41 I18NSPHINXOPTS  = $(PAPEROPT_$(PAPER)) $(SPHINXOPTS) .
43 # commands; the 'cmd' from scripts/Kbuild.include is not *loopable*
44 loop_cmd = $(echo-cmd) $(cmd_$(1)) || exit;
46 # $2 sphinx builder e.g. "html"
47 # $3 name of the build subfolder / e.g. "media", used as:
48 #    * dest folder relative to $(BUILDDIR) and
49 #    * cache folder relative to $(BUILDDIR)/.doctrees
50 # $4 dest subfolder e.g. "man" for man pages at media/man
51 # $5 reST source folder relative to $(srctree)/$(src),
52 #    e.g. "media" for the linux-tv book-set at ./Documentation/media
54 quiet_cmd_sphinx = SPHINX  $@ --> file://$(abspath $(BUILDDIR)/$3/$4)
55       cmd_sphinx = $(MAKE) BUILDDIR=$(abspath $(BUILDDIR)) $(build)=Documentation/media $2 && \
56         PYTHONDONTWRITEBYTECODE=1 \
57         BUILDDIR=$(abspath $(BUILDDIR)) SPHINX_CONF=$(abspath $(srctree)/$(src)/$5/$(SPHINX_CONF)) \
58         $(SPHINXBUILD) \
59         -b $2 \
60         -c $(abspath $(srctree)/$(src)) \
61         -d $(abspath $(BUILDDIR)/.doctrees/$3) \
62         -D version=$(KERNELVERSION) -D release=$(KERNELRELEASE) \
63         $(ALLSPHINXOPTS) \
64         $(abspath $(srctree)/$(src)/$5) \
65         $(abspath $(BUILDDIR)/$3/$4)
67 htmldocs:
68         @+$(foreach var,$(SPHINXDIRS),$(call loop_cmd,sphinx,html,$(var),,$(var)))
70 linkcheckdocs:
71         @$(foreach var,$(SPHINXDIRS),$(call loop_cmd,sphinx,linkcheck,$(var),,$(var)))
73 latexdocs:
74         @+$(foreach var,$(SPHINXDIRS),$(call loop_cmd,sphinx,latex,$(var),latex,$(var)))
76 ifeq ($(HAVE_PDFLATEX),0)
78 pdfdocs:
79         $(warning The '$(PDFLATEX)' command was not found. Make sure you have it installed and in PATH to produce PDF output.)
80         @echo "  SKIP    Sphinx $@ target."
82 else # HAVE_PDFLATEX
84 pdfdocs: latexdocs
85         $(foreach var,$(SPHINXDIRS), $(MAKE) PDFLATEX=$(PDFLATEX) LATEXOPTS="$(LATEXOPTS)" -C $(BUILDDIR)/$(var)/latex || exit;)
87 endif # HAVE_PDFLATEX
89 epubdocs:
90         @+$(foreach var,$(SPHINXDIRS),$(call loop_cmd,sphinx,epub,$(var),epub,$(var)))
92 xmldocs:
93         @+$(foreach var,$(SPHINXDIRS),$(call loop_cmd,sphinx,xml,$(var),xml,$(var)))
95 endif # HAVE_SPHINX
97 # The following targets are independent of HAVE_SPHINX, and the rules should
98 # work or silently pass without Sphinx.
100 refcheckdocs:
101         $(Q)cd $(srctree);scripts/documentation-file-ref-check
103 cleandocs:
104         $(Q)rm -rf $(BUILDDIR)
105         $(Q)$(MAKE) BUILDDIR=$(abspath $(BUILDDIR)) $(build)=Documentation/media clean
107 dochelp:
108         @echo  ' Linux kernel internal documentation in different formats from ReST:'
109         @echo  '  htmldocs        - HTML'
110         @echo  '  latexdocs       - LaTeX'
111         @echo  '  pdfdocs         - PDF'
112         @echo  '  epubdocs        - EPUB'
113         @echo  '  xmldocs         - XML'
114         @echo  '  linkcheckdocs   - check for broken external links (will connect to external hosts)'
115         @echo  '  refcheckdocs    - check for references to non-existing files under Documentation'
116         @echo  '  cleandocs       - clean all generated files'
117         @echo
118         @echo  '  make SPHINXDIRS="s1 s2" [target] Generate only docs of folder s1, s2'
119         @echo  '  valid values for SPHINXDIRS are: $(_SPHINXDIRS)'
120         @echo
121         @echo  '  make SPHINX_CONF={conf-file} [target] use *additional* sphinx-build'
122         @echo  '  configuration. This is e.g. useful to build with nit-picking config.'
123         @echo
124         @echo  '  Default location for the generated documents is Documentation/output'