1 ==============
2 Memory Hotplug
3 ==============
5 :Created: Jul 28 2007
6 :Updated: Add description of notifier of memory hotplug: Oct 11 2007
8 This document is about memory hotplug including how-to-use and current status.
9 Because Memory Hotplug is still under development, contents of this text will
10 be changed often.
12 .. CONTENTS
14 1. Introduction
15 1.1 purpose of memory hotplug
16 1.2. Phases of memory hotplug
17 1.3. Unit of Memory online/offline operation
18 2. Kernel Configuration
19 3. sysfs files for memory hotplug
20 4. Physical memory hot-add phase
21 4.1 Hardware(Firmware) Support
22 4.2 Notify memory hot-add event by hand
23 5. Logical Memory hot-add phase
24 5.1. State of memory
25 5.2. How to online memory
26 6. Logical memory remove
27 6.1 Memory offline and ZONE_MOVABLE
28 6.2. How to offline memory
29 7. Physical memory remove
30 8. Memory hotplug event notifier
31 9. Future Work List
34 .. note::
36 (1) x86_64's has special implementation for memory hotplug.
37 This text does not describe it.
38 (2) This text assumes that sysfs is mounted at /sys.
41 Introduction
42 ============
44 purpose of memory hotplug
45 -------------------------
47 Memory Hotplug allows users to increase/decrease the amount of memory.
48 Generally, there are two purposes.
50 (A) For changing the amount of memory.
51 This is to allow a feature like capacity on demand.
52 (B) For installing/removing DIMMs or NUMA-nodes physically.
53 This is to exchange DIMMs/NUMA-nodes, reduce power consumption, etc.
55 (A) is required by highly virtualized environments and (B) is required by
56 hardware which supports memory power management.
58 Linux memory hotplug is designed for both purpose.
61 Phases of memory hotplug
62 ------------------------
64 There are 2 phases in Memory Hotplug:
66 1) Physical Memory Hotplug phase
67 2) Logical Memory Hotplug phase.
69 The First phase is to communicate hardware/firmware and make/erase
70 environment for hotplugged memory. Basically, this phase is necessary
71 for the purpose (B), but this is good phase for communication between
72 highly virtualized environments too.
74 When memory is hotplugged, the kernel recognizes new memory, makes new memory
75 management tables, and makes sysfs files for new memory's operation.
77 If firmware supports notification of connection of new memory to OS,
78 this phase is triggered automatically. ACPI can notify this event. If not,
79 "probe" operation by system administration is used instead.
80 (see :ref:`memory_hotplug_physical_mem`).
82 Logical Memory Hotplug phase is to change memory state into
83 available/unavailable for users. Amount of memory from user's view is
84 changed by this phase. The kernel makes all memory in it as free pages
85 when a memory range is available.
87 In this document, this phase is described as online/offline.
89 Logical Memory Hotplug phase is triggered by write of sysfs file by system
90 administrator. For the hot-add case, it must be executed after Physical Hotplug
91 phase by hand.
92 (However, if you writes udev's hotplug scripts for memory hotplug, these
93 phases can be execute in seamless way.)
96 Unit of Memory online/offline operation
97 ---------------------------------------
99 Memory hotplug uses SPARSEMEM memory model which allows memory to be divided
100 into chunks of the same size. These chunks are called "sections". The size of
101 a memory section is architecture dependent. For example, power uses 16MiB, ia64
102 uses 1GiB.
104 Memory sections are combined into chunks referred to as "memory blocks". The
105 size of a memory block is architecture dependent and represents the logical
106 unit upon which memory online/offline operations are to be performed. The
107 default size of a memory block is the same as memory section size unless an
108 architecture specifies otherwise. (see :ref:`memory_hotplug_sysfs_files`.)
110 To determine the size (in bytes) of a memory block please read this file:
112 /sys/devices/system/memory/block_size_bytes
115 Kernel Configuration
116 ====================
118 To use memory hotplug feature, kernel must be compiled with following
119 config options.
121 - For all memory hotplug:
122 - Memory model -> Sparse Memory (CONFIG_SPARSEMEM)
123 - Allow for memory hot-add (CONFIG_MEMORY_HOTPLUG)
125 - To enable memory removal, the following are also necessary:
126 - Allow for memory hot remove (CONFIG_MEMORY_HOTREMOVE)
127 - Page Migration (CONFIG_MIGRATION)
129 - For ACPI memory hotplug, the following are also necessary:
130 - Memory hotplug (under ACPI Support menu) (CONFIG_ACPI_HOTPLUG_MEMORY)
131 - This option can be kernel module.
133 - As a related configuration, if your box has a feature of NUMA-node hotplug
134 via ACPI, then this option is necessary too.
136 - ACPI0004,PNP0A05 and PNP0A06 Container Driver (under ACPI Support menu)
137 (CONFIG_ACPI_CONTAINER).
139 This option can be kernel module too.
142 .. _memory_hotplug_sysfs_files:
144 sysfs files for memory hotplug
145 ==============================
147 All memory blocks have their device information in sysfs. Each memory block
148 is described under /sys/devices/system/memory as:
150 /sys/devices/system/memory/memoryXXX
151 (XXX is the memory block id.)
153 For the memory block covered by the sysfs directory. It is expected that all
154 memory sections in this range are present and no memory holes exist in the
155 range. Currently there is no way to determine if there is a memory hole, but
156 the existence of one should not affect the hotplug capabilities of the memory
157 block.
159 For example, assume 1GiB memory block size. A device for a memory starting at
160 0x100000000 is /sys/device/system/memory/memory4::
162 (0x100000000 / 1Gib = 4)
164 This device covers address range [0x100000000 ... 0x140000000)
166 Under each memory block, you can see 5 files:
168 - /sys/devices/system/memory/memoryXXX/phys_index
169 - /sys/devices/system/memory/memoryXXX/phys_device
170 - /sys/devices/system/memory/memoryXXX/state
171 - /sys/devices/system/memory/memoryXXX/removable
172 - /sys/devices/system/memory/memoryXXX/valid_zones
174 =================== ============================================================
175 ``phys_index`` read-only and contains memory block id, same as XXX.
176 ``state`` read-write
178 - at read: contains online/offline state of memory.
179 - at write: user can specify "online_kernel",
181 "online_movable", "online", "offline" command
182 which will be performed on all sections in the block.
183 ``phys_device`` read-only: designed to show the name of physical memory
184 device. This is not well implemented now.
185 ``removable`` read-only: contains an integer value indicating
186 whether the memory block is removable or not
187 removable. A value of 1 indicates that the memory
188 block is removable and a value of 0 indicates that
189 it is not removable. A memory block is removable only if
190 every section in the block is removable.
191 ``valid_zones`` read-only: designed to show which zones this memory block
192 can be onlined to.
194 The first column shows it`s default zone.
196 "memory6/valid_zones: Normal Movable" shows this memoryblock
197 can be onlined to ZONE_NORMAL by default and to ZONE_MOVABLE
198 by online_movable.
200 "memory7/valid_zones: Movable Normal" shows this memoryblock
201 can be onlined to ZONE_MOVABLE by default and to ZONE_NORMAL
202 by online_kernel.
203 =================== ============================================================
205 .. note::
207 These directories/files appear after physical memory hotplug phase.
209 If CONFIG_NUMA is enabled the memoryXXX/ directories can also be accessed
210 via symbolic links located in the /sys/devices/system/node/node* directories.
212 For example:
213 /sys/devices/system/node/node0/memory9 -> ../../memory/memory9
215 A backlink will also be created:
216 /sys/devices/system/memory/memory9/node0 -> ../../node/node0
218 .. _memory_hotplug_physical_mem:
220 Physical memory hot-add phase
221 =============================
223 Hardware(Firmware) Support
224 --------------------------
226 On x86_64/ia64 platform, memory hotplug by ACPI is supported.
228 In general, the firmware (ACPI) which supports memory hotplug defines
229 memory class object of _HID "PNP0C80". When a notify is asserted to PNP0C80,
230 Linux's ACPI handler does hot-add memory to the system and calls a hotplug udev
231 script. This will be done automatically.
233 But scripts for memory hotplug are not contained in generic udev package(now).
234 You may have to write it by yourself or online/offline memory by hand.
235 Please see :ref:`memory_hotplug_how_to_online_memory` and
236 :ref:`memory_hotplug_how_to_offline_memory`.
238 If firmware supports NUMA-node hotplug, and defines an object _HID "ACPI0004",
239 "PNP0A05", or "PNP0A06", notification is asserted to it, and ACPI handler
240 calls hotplug code for all of objects which are defined in it.
241 If memory device is found, memory hotplug code will be called.
244 Notify memory hot-add event by hand
245 -----------------------------------
247 On some architectures, the firmware may not notify the kernel of a memory
248 hotplug event. Therefore, the memory "probe" interface is supported to
249 explicitly notify the kernel. This interface depends on
250 CONFIG_ARCH_MEMORY_PROBE and can be configured on powerpc, sh, and x86
251 if hotplug is supported, although for x86 this should be handled by ACPI
252 notification.
254 Probe interface is located at
255 /sys/devices/system/memory/probe
257 You can tell the physical address of new memory to the kernel by::
259 % echo start_address_of_new_memory > /sys/devices/system/memory/probe
261 Then, [start_address_of_new_memory, start_address_of_new_memory +
262 memory_block_size] memory range is hot-added. In this case, hotplug script is
263 not called (in current implementation). You'll have to online memory by
264 yourself. Please see :ref:`memory_hotplug_how_to_online_memory`.
267 Logical Memory hot-add phase
268 ============================
270 State of memory
271 ---------------
273 To see (online/offline) state of a memory block, read 'state' file::
275 % cat /sys/device/system/memory/memoryXXX/state
278 - If the memory block is online, you'll read "online".
279 - If the memory block is offline, you'll read "offline".
282 .. _memory_hotplug_how_to_online_memory:
284 How to online memory
285 --------------------
287 When the memory is hot-added, the kernel decides whether or not to "online"
288 it according to the policy which can be read from "auto_online_blocks" file::
290 % cat /sys/devices/system/memory/auto_online_blocks
292 The default depends on the CONFIG_MEMORY_HOTPLUG_DEFAULT_ONLINE kernel config
293 option. If it is disabled the default is "offline" which means the newly added
294 memory is not in a ready-to-use state and you have to "online" the newly added
295 memory blocks manually. Automatic onlining can be requested by writing "online"
296 to "auto_online_blocks" file::
298 % echo online > /sys/devices/system/memory/auto_online_blocks
300 This sets a global policy and impacts all memory blocks that will subsequently
301 be hotplugged. Currently offline blocks keep their state. It is possible, under
302 certain circumstances, that some memory blocks will be added but will fail to
303 online. User space tools can check their "state" files
304 (/sys/devices/system/memory/memoryXXX/state) and try to online them manually.
306 If the automatic onlining wasn't requested, failed, or some memory block was
307 offlined it is possible to change the individual block's state by writing to the
308 "state" file::
310 % echo online > /sys/devices/system/memory/memoryXXX/state
312 This onlining will not change the ZONE type of the target memory block,
313 If the memory block doesn't belong to any zone an appropriate kernel zone
314 (usually ZONE_NORMAL) will be used unless movable_node kernel command line
315 option is specified when ZONE_MOVABLE will be used.
317 You can explicitly request to associate it with ZONE_MOVABLE by::
319 % echo online_movable > /sys/devices/system/memory/memoryXXX/state
321 .. note:: current limit: this memory block must be adjacent to ZONE_MOVABLE
323 Or you can explicitly request a kernel zone (usually ZONE_NORMAL) by::
325 % echo online_kernel > /sys/devices/system/memory/memoryXXX/state
327 .. note:: current limit: this memory block must be adjacent to ZONE_NORMAL
329 An explicit zone onlining can fail (e.g. when the range is already within
330 and existing and incompatible zone already).
332 After this, memory block XXX's state will be 'online' and the amount of
333 available memory will be increased.
335 This may be changed in future.
339 Logical memory remove
340 =====================
342 Memory offline and ZONE_MOVABLE
343 -------------------------------
345 Memory offlining is more complicated than memory online. Because memory offline
346 has to make the whole memory block be unused, memory offline can fail if
347 the memory block includes memory which cannot be freed.
349 In general, memory offline can use 2 techniques.
351 (1) reclaim and free all memory in the memory block.
352 (2) migrate all pages in the memory block.
354 In the current implementation, Linux's memory offline uses method (2), freeing
355 all pages in the memory block by page migration. But not all pages are
356 migratable. Under current Linux, migratable pages are anonymous pages and
357 page caches. For offlining a memory block by migration, the kernel has to
358 guarantee that the memory block contains only migratable pages.
360 Now, a boot option for making a memory block which consists of migratable pages
361 is supported. By specifying "kernelcore=" or "movablecore=" boot option, you can
362 create ZONE_MOVABLE...a zone which is just used for movable pages.
363 (See also Documentation/admin-guide/kernel-parameters.rst)
365 Assume the system has "TOTAL" amount of memory at boot time, this boot option
366 creates ZONE_MOVABLE as following.
368 1) When kernelcore=YYYY boot option is used,
369 Size of memory not for movable pages (not for offline) is YYYY.
370 Size of memory for movable pages (for offline) is TOTAL-YYYY.
372 2) When movablecore=ZZZZ boot option is used,
373 Size of memory not for movable pages (not for offline) is TOTAL - ZZZZ.
374 Size of memory for movable pages (for offline) is ZZZZ.
376 .. note::
378 Unfortunately, there is no information to show which memory block belongs
379 to ZONE_MOVABLE. This is TBD.
381 .. _memory_hotplug_how_to_offline_memory:
383 How to offline memory
384 ---------------------
386 You can offline a memory block by using the same sysfs interface that was used
387 in memory onlining::
389 % echo offline > /sys/devices/system/memory/memoryXXX/state
391 If offline succeeds, the state of the memory block is changed to be "offline".
392 If it fails, some error core (like -EBUSY) will be returned by the kernel.
393 Even if a memory block does not belong to ZONE_MOVABLE, you can try to offline
394 it. If it doesn't contain 'unmovable' memory, you'll get success.
396 A memory block under ZONE_MOVABLE is considered to be able to be offlined
397 easily. But under some busy state, it may return -EBUSY. Even if a memory
398 block cannot be offlined due to -EBUSY, you can retry offlining it and may be
399 able to offline it (or not). (For example, a page is referred to by some kernel
400 internal call and released soon.)
402 Consideration:
403 Memory hotplug's design direction is to make the possibility of memory
404 offlining higher and to guarantee unplugging memory under any situation. But
405 it needs more work. Returning -EBUSY under some situation may be good because
406 the user can decide to retry more or not by himself. Currently, memory
407 offlining code does some amount of retry with 120 seconds timeout.
409 Physical memory remove
410 ======================
412 Need more implementation yet....
413 - Notification completion of remove works by OS to firmware.
414 - Guard from remove if not yet.
416 Memory hotplug event notifier
417 =============================
419 Hotplugging events are sent to a notification queue.
421 There are six types of notification defined in include/linux/memory.h:
423 MEM_GOING_ONLINE
424 Generated before new memory becomes available in order to be able to
425 prepare subsystems to handle memory. The page allocator is still unable
426 to allocate from the new memory.
428 MEM_CANCEL_ONLINE
429 Generated if MEMORY_GOING_ONLINE fails.
431 MEM_ONLINE
432 Generated when memory has successfully brought online. The callback may
433 allocate pages from the new memory.
435 MEM_GOING_OFFLINE
436 Generated to begin the process of offlining memory. Allocations are no
437 longer possible from the memory but some of the memory to be offlined
438 is still in use. The callback can be used to free memory known to a
439 subsystem from the indicated memory block.
441 MEM_CANCEL_OFFLINE
442 Generated if MEMORY_GOING_OFFLINE fails. Memory is available again from
443 the memory block that we attempted to offline.
445 MEM_OFFLINE
446 Generated after offlining memory is complete.
448 A callback routine can be registered by calling::
450 hotplug_memory_notifier(callback_func, priority)
452 Callback functions with higher values of priority are called before callback
453 functions with lower values.
455 A callback function must have the following prototype::
457 int callback_func(
458 struct notifier_block *self, unsigned long action, void *arg);
460 The first argument of the callback function (self) is a pointer to the block
461 of the notifier chain that points to the callback function itself.
462 The second argument (action) is one of the event types described above.
463 The third argument (arg) passes a pointer of struct memory_notify::
465 struct memory_notify {
466 unsigned long start_pfn;
467 unsigned long nr_pages;
468 int status_change_nid_normal;
469 int status_change_nid_high;
470 int status_change_nid;
471 }
473 - start_pfn is start_pfn of online/offline memory.
474 - nr_pages is # of pages of online/offline memory.
475 - status_change_nid_normal is set node id when N_NORMAL_MEMORY of nodemask
476 is (will be) set/clear, if this is -1, then nodemask status is not changed.
477 - status_change_nid_high is set node id when N_HIGH_MEMORY of nodemask
478 is (will be) set/clear, if this is -1, then nodemask status is not changed.
479 - status_change_nid is set node id when N_MEMORY of nodemask is (will be)
480 set/clear. It means a new(memoryless) node gets new memory by online and a
481 node loses all memory. If this is -1, then nodemask status is not changed.
483 If status_changed_nid* >= 0, callback should create/discard structures for the
484 node if necessary.
486 The callback routine shall return one of the values
487 NOTIFY_DONE, NOTIFY_OK, NOTIFY_BAD, NOTIFY_STOP
488 defined in include/linux/notifier.h
490 NOTIFY_DONE and NOTIFY_OK have no effect on the further processing.
492 NOTIFY_BAD is used as response to the MEM_GOING_ONLINE, MEM_GOING_OFFLINE,
493 MEM_ONLINE, or MEM_OFFLINE action to cancel hotplugging. It stops
494 further processing of the notification queue.
496 NOTIFY_STOP stops further processing of the notification queue.
498 Future Work
499 ===========
501 - allowing memory hot-add to ZONE_MOVABLE. maybe we need some switch like
502 sysctl or new control file.
503 - showing memory block and physical device relationship.
504 - test and make it better memory offlining.
505 - support HugeTLB page migration and offlining.
506 - memmap removing at memory offline.
507 - physical remove memory.