]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - arch/arc/Makefile
Merge tag 'alloc-args-v4.19-rc8' of https://git.kernel.org/pub/scm/linux/kernel/git...
[rpmsg/rpmsg.git] / arch / arc / Makefile
1 #
2 # Copyright (C) 2004, 2007-2010, 2011-2012 Synopsys, Inc. (www.synopsys.com)
3 #
4 # This program is free software; you can redistribute it and/or modify
5 # it under the terms of the GNU General Public License version 2 as
6 # published by the Free Software Foundation.
7 #
9 KBUILD_DEFCONFIG := nsim_700_defconfig
11 cflags-y        += -fno-common -pipe -fno-builtin -mmedium-calls -D__linux__
12 cflags-$(CONFIG_ISA_ARCOMPACT)  += -mA7
13 cflags-$(CONFIG_ISA_ARCV2)      += -mcpu=hs38
15 ifdef CONFIG_ARC_CURR_IN_REG
16 # For a global register defintion, make sure it gets passed to every file
17 # We had a customer reported bug where some code built in kernel was NOT using
18 # any kernel headers, and missing the r25 global register
19 # Can't do unconditionally because of recursive include issues
20 # due to <linux/thread_info.h>
21 LINUXINCLUDE    +=  -include ${src}/arch/arc/include/asm/current.h
22 endif
24 cflags-y                                += -fsection-anchors
26 cflags-$(CONFIG_ARC_HAS_LLSC)           += -mlock
27 cflags-$(CONFIG_ARC_HAS_SWAPE)          += -mswape
29 ifdef CONFIG_ISA_ARCV2
31 ifndef CONFIG_ARC_HAS_LL64
32 cflags-y                                += -mno-ll64
33 endif
35 ifndef CONFIG_ARC_HAS_DIV_REM
36 cflags-y                                += -mno-div-rem
37 endif
39 endif
41 cfi := $(call as-instr,.cfi_startproc\n.cfi_endproc,-DARC_DW2_UNWIND_AS_CFI)
42 cflags-$(CONFIG_ARC_DW2_UNWIND)         += -fasynchronous-unwind-tables $(cfi)
44 ifndef CONFIG_CC_OPTIMIZE_FOR_SIZE
45 # Generic build system uses -O2, we want -O3
46 # Note: No need to add to cflags-y as that happens anyways
47 #
48 # Disable the false maybe-uninitialized warings gcc spits out at -O3
49 ARCH_CFLAGS += -O3 $(call cc-disable-warning,maybe-uninitialized,)
50 endif
52 # small data is default for elf32 tool-chain. If not usable, disable it
53 # This also allows repurposing GP as scratch reg to gcc reg allocator
54 disable_small_data := y
55 cflags-$(disable_small_data)            += -mno-sdata -fcall-used-gp
57 cflags-$(CONFIG_CPU_BIG_ENDIAN)         += -mbig-endian
58 ldflags-$(CONFIG_CPU_BIG_ENDIAN)        += -EB
60 LIBGCC  = $(shell $(CC) $(cflags-y) --print-libgcc-file-name)
62 # Modules with short calls might break for calls into builtin-kernel
63 KBUILD_CFLAGS_MODULE    += -mlong-calls -mno-millicode
65 # Finally dump eveything into kernel build system
66 KBUILD_CFLAGS   += $(cflags-y)
67 KBUILD_AFLAGS   += $(KBUILD_CFLAGS)
68 KBUILD_LDFLAGS  += $(ldflags-y)
70 head-y          := arch/arc/kernel/head.o
72 # See arch/arc/Kbuild for content of core part of the kernel
73 core-y          += arch/arc/
75 # w/o this dtb won't embed into kernel binary
76 core-y          += arch/arc/boot/dts/
78 core-y                          += arch/arc/plat-sim/
79 core-$(CONFIG_ARC_PLAT_TB10X)   += arch/arc/plat-tb10x/
80 core-$(CONFIG_ARC_PLAT_AXS10X)  += arch/arc/plat-axs10x/
81 core-$(CONFIG_ARC_PLAT_EZNPS)   += arch/arc/plat-eznps/
82 core-$(CONFIG_ARC_SOC_HSDK)     += arch/arc/plat-hsdk/
84 ifdef CONFIG_ARC_PLAT_EZNPS
85 KBUILD_CPPFLAGS += -I$(srctree)/arch/arc/plat-eznps/include
86 endif
88 drivers-$(CONFIG_OPROFILE)      += arch/arc/oprofile/
90 libs-y          += arch/arc/lib/ $(LIBGCC)
92 boot            := arch/arc/boot
94 #default target for make without any arguments.
95 KBUILD_IMAGE    := $(boot)/bootpImage
97 all:    bootpImage
98 bootpImage: vmlinux
100 boot_targets += uImage uImage.bin uImage.gz
102 $(boot_targets): vmlinux
103         $(Q)$(MAKE) $(build)=$(boot) $(boot)/$@
105 %.dtb %.dtb.S %.dtb.o: scripts
106         $(Q)$(MAKE) $(build)=$(boot)/dts $(boot)/dts/$@
108 dtbs: scripts
109         $(Q)$(MAKE) $(build)=$(boot)/dts
111 archclean:
112         $(Q)$(MAKE) $(clean)=$(boot)