1 /*
2 * Based on arch/arm/mm/mmu.c
3 *
4 * Copyright (C) 1995-2005 Russell King
5 * Copyright (C) 2012 ARM Ltd.
6 *
7 * This program is free software; you can redistribute it and/or modify
8 * it under the terms of the GNU General Public License version 2 as
9 * published by the Free Software Foundation.
10 *
11 * This program is distributed in the hope that it will be useful,
12 * but WITHOUT ANY WARRANTY; without even the implied warranty of
13 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
14 * GNU General Public License for more details.
15 *
16 * You should have received a copy of the GNU General Public License
17 * along with this program. If not, see <http://www.gnu.org/licenses/>.
18 */
20 #include <linux/cache.h>
21 #include <linux/export.h>
22 #include <linux/kernel.h>
23 #include <linux/errno.h>
24 #include <linux/init.h>
25 #include <linux/ioport.h>
26 #include <linux/kexec.h>
27 #include <linux/libfdt.h>
28 #include <linux/mman.h>
29 #include <linux/nodemask.h>
30 #include <linux/memblock.h>
31 #include <linux/fs.h>
32 #include <linux/io.h>
33 #include <linux/mm.h>
34 #include <linux/vmalloc.h>
36 #include <asm/barrier.h>
37 #include <asm/cputype.h>
38 #include <asm/fixmap.h>
39 #include <asm/kasan.h>
40 #include <asm/kernel-pgtable.h>
41 #include <asm/sections.h>
42 #include <asm/setup.h>
43 #include <asm/sizes.h>
44 #include <asm/tlb.h>
45 #include <asm/memblock.h>
46 #include <asm/mmu_context.h>
47 #include <asm/ptdump.h>
48 #include <asm/tlbflush.h>
50 #define NO_BLOCK_MAPPINGS BIT(0)
51 #define NO_CONT_MAPPINGS BIT(1)
53 u64 idmap_t0sz = TCR_T0SZ(VA_BITS);
54 u64 idmap_ptrs_per_pgd = PTRS_PER_PGD;
56 u64 kimage_voffset __ro_after_init;
57 EXPORT_SYMBOL(kimage_voffset);
59 /*
60 * Empty_zero_page is a special page that is used for zero-initialized data
61 * and COW.
62 */
63 unsigned long empty_zero_page[PAGE_SIZE / sizeof(unsigned long)] __page_aligned_bss;
64 EXPORT_SYMBOL(empty_zero_page);
66 static pte_t bm_pte[PTRS_PER_PTE] __page_aligned_bss;
67 static pmd_t bm_pmd[PTRS_PER_PMD] __page_aligned_bss __maybe_unused;
68 static pud_t bm_pud[PTRS_PER_PUD] __page_aligned_bss __maybe_unused;
70 pgprot_t phys_mem_access_prot(struct file *file, unsigned long pfn,
71 unsigned long size, pgprot_t vma_prot)
72 {
73 if (!pfn_valid(pfn))
74 return pgprot_noncached(vma_prot);
75 else if (file->f_flags & O_SYNC)
76 return pgprot_writecombine(vma_prot);
77 return vma_prot;
78 }
79 EXPORT_SYMBOL(phys_mem_access_prot);
81 static phys_addr_t __init early_pgtable_alloc(void)
82 {
83 phys_addr_t phys;
84 void *ptr;
86 phys = memblock_alloc(PAGE_SIZE, PAGE_SIZE);
88 /*
89 * The FIX_{PGD,PUD,PMD} slots may be in active use, but the FIX_PTE
90 * slot will be free, so we can (ab)use the FIX_PTE slot to initialise
91 * any level of table.
92 */
93 ptr = pte_set_fixmap(phys);
95 memset(ptr, 0, PAGE_SIZE);
97 /*
98 * Implicit barriers also ensure the zeroed page is visible to the page
99 * table walker
100 */
101 pte_clear_fixmap();
103 return phys;
104 }
106 static bool pgattr_change_is_safe(u64 old, u64 new)
107 {
108 /*
109 * The following mapping attributes may be updated in live
110 * kernel mappings without the need for break-before-make.
111 */
112 static const pteval_t mask = PTE_PXN | PTE_RDONLY | PTE_WRITE | PTE_NG;
114 /* creating or taking down mappings is always safe */
115 if (old == 0 || new == 0)
116 return true;
118 /* live contiguous mappings may not be manipulated at all */
119 if ((old | new) & PTE_CONT)
120 return false;
122 /* Transitioning from Non-Global to Global is unsafe */
123 if (old & ~new & PTE_NG)
124 return false;
126 return ((old ^ new) & ~mask) == 0;
127 }
129 static void init_pte(pmd_t *pmdp, unsigned long addr, unsigned long end,
130 phys_addr_t phys, pgprot_t prot)
131 {
132 pte_t *ptep;
134 ptep = pte_set_fixmap_offset(pmdp, addr);
135 do {
136 pte_t old_pte = READ_ONCE(*ptep);
138 set_pte(ptep, pfn_pte(__phys_to_pfn(phys), prot));
140 /*
141 * After the PTE entry has been populated once, we
142 * only allow updates to the permission attributes.
143 */
144 BUG_ON(!pgattr_change_is_safe(pte_val(old_pte),
145 READ_ONCE(pte_val(*ptep))));
147 phys += PAGE_SIZE;
148 } while (ptep++, addr += PAGE_SIZE, addr != end);
150 pte_clear_fixmap();
151 }
153 static void alloc_init_cont_pte(pmd_t *pmdp, unsigned long addr,
154 unsigned long end, phys_addr_t phys,
155 pgprot_t prot,
156 phys_addr_t (*pgtable_alloc)(void),
157 int flags)
158 {
159 unsigned long next;
160 pmd_t pmd = READ_ONCE(*pmdp);
162 BUG_ON(pmd_sect(pmd));
163 if (pmd_none(pmd)) {
164 phys_addr_t pte_phys;
165 BUG_ON(!pgtable_alloc);
166 pte_phys = pgtable_alloc();
167 __pmd_populate(pmdp, pte_phys, PMD_TYPE_TABLE);
168 pmd = READ_ONCE(*pmdp);
169 }
170 BUG_ON(pmd_bad(pmd));
172 do {
173 pgprot_t __prot = prot;
175 next = pte_cont_addr_end(addr, end);
177 /* use a contiguous mapping if the range is suitably aligned */
178 if ((((addr | next | phys) & ~CONT_PTE_MASK) == 0) &&
179 (flags & NO_CONT_MAPPINGS) == 0)
180 __prot = __pgprot(pgprot_val(prot) | PTE_CONT);
182 init_pte(pmdp, addr, next, phys, __prot);
184 phys += next - addr;
185 } while (addr = next, addr != end);
186 }
188 static void init_pmd(pud_t *pudp, unsigned long addr, unsigned long end,
189 phys_addr_t phys, pgprot_t prot,
190 phys_addr_t (*pgtable_alloc)(void), int flags)
191 {
192 unsigned long next;
193 pmd_t *pmdp;
195 pmdp = pmd_set_fixmap_offset(pudp, addr);
196 do {
197 pmd_t old_pmd = READ_ONCE(*pmdp);
199 next = pmd_addr_end(addr, end);
201 /* try section mapping first */
202 if (((addr | next | phys) & ~SECTION_MASK) == 0 &&
203 (flags & NO_BLOCK_MAPPINGS) == 0) {
204 pmd_set_huge(pmdp, phys, prot);
206 /*
207 * After the PMD entry has been populated once, we
208 * only allow updates to the permission attributes.
209 */
210 BUG_ON(!pgattr_change_is_safe(pmd_val(old_pmd),
211 READ_ONCE(pmd_val(*pmdp))));
212 } else {
213 alloc_init_cont_pte(pmdp, addr, next, phys, prot,
214 pgtable_alloc, flags);
216 BUG_ON(pmd_val(old_pmd) != 0 &&
217 pmd_val(old_pmd) != READ_ONCE(pmd_val(*pmdp)));
218 }
219 phys += next - addr;
220 } while (pmdp++, addr = next, addr != end);
222 pmd_clear_fixmap();
223 }
225 static void alloc_init_cont_pmd(pud_t *pudp, unsigned long addr,
226 unsigned long end, phys_addr_t phys,
227 pgprot_t prot,
228 phys_addr_t (*pgtable_alloc)(void), int flags)
229 {
230 unsigned long next;
231 pud_t pud = READ_ONCE(*pudp);
233 /*
234 * Check for initial section mappings in the pgd/pud.
235 */
236 BUG_ON(pud_sect(pud));
237 if (pud_none(pud)) {
238 phys_addr_t pmd_phys;
239 BUG_ON(!pgtable_alloc);
240 pmd_phys = pgtable_alloc();
241 __pud_populate(pudp, pmd_phys, PUD_TYPE_TABLE);
242 pud = READ_ONCE(*pudp);
243 }
244 BUG_ON(pud_bad(pud));
246 do {
247 pgprot_t __prot = prot;
249 next = pmd_cont_addr_end(addr, end);
251 /* use a contiguous mapping if the range is suitably aligned */
252 if ((((addr | next | phys) & ~CONT_PMD_MASK) == 0) &&
253 (flags & NO_CONT_MAPPINGS) == 0)
254 __prot = __pgprot(pgprot_val(prot) | PTE_CONT);
256 init_pmd(pudp, addr, next, phys, __prot, pgtable_alloc, flags);
258 phys += next - addr;
259 } while (addr = next, addr != end);
260 }
262 static inline bool use_1G_block(unsigned long addr, unsigned long next,
263 unsigned long phys)
264 {
265 if (PAGE_SHIFT != 12)
266 return false;
268 if (((addr | next | phys) & ~PUD_MASK) != 0)
269 return false;
271 return true;
272 }
274 static void alloc_init_pud(pgd_t *pgdp, unsigned long addr, unsigned long end,
275 phys_addr_t phys, pgprot_t prot,
276 phys_addr_t (*pgtable_alloc)(void),
277 int flags)
278 {
279 unsigned long next;
280 pud_t *pudp;
281 pgd_t pgd = READ_ONCE(*pgdp);
283 if (pgd_none(pgd)) {
284 phys_addr_t pud_phys;
285 BUG_ON(!pgtable_alloc);
286 pud_phys = pgtable_alloc();
287 __pgd_populate(pgdp, pud_phys, PUD_TYPE_TABLE);
288 pgd = READ_ONCE(*pgdp);
289 }
290 BUG_ON(pgd_bad(pgd));
292 pudp = pud_set_fixmap_offset(pgdp, addr);
293 do {
294 pud_t old_pud = READ_ONCE(*pudp);
296 next = pud_addr_end(addr, end);
298 /*
299 * For 4K granule only, attempt to put down a 1GB block
300 */
301 if (use_1G_block(addr, next, phys) &&
302 (flags & NO_BLOCK_MAPPINGS) == 0) {
303 pud_set_huge(pudp, phys, prot);
305 /*
306 * After the PUD entry has been populated once, we
307 * only allow updates to the permission attributes.
308 */
309 BUG_ON(!pgattr_change_is_safe(pud_val(old_pud),
310 READ_ONCE(pud_val(*pudp))));
311 } else {
312 alloc_init_cont_pmd(pudp, addr, next, phys, prot,
313 pgtable_alloc, flags);
315 BUG_ON(pud_val(old_pud) != 0 &&
316 pud_val(old_pud) != READ_ONCE(pud_val(*pudp)));
317 }
318 phys += next - addr;
319 } while (pudp++, addr = next, addr != end);
321 pud_clear_fixmap();
322 }
324 static void __create_pgd_mapping(pgd_t *pgdir, phys_addr_t phys,
325 unsigned long virt, phys_addr_t size,
326 pgprot_t prot,
327 phys_addr_t (*pgtable_alloc)(void),
328 int flags)
329 {
330 unsigned long addr, length, end, next;
331 pgd_t *pgdp = pgd_offset_raw(pgdir, virt);
333 /*
334 * If the virtual and physical address don't have the same offset
335 * within a page, we cannot map the region as the caller expects.
336 */
337 if (WARN_ON((phys ^ virt) & ~PAGE_MASK))
338 return;
340 phys &= PAGE_MASK;
341 addr = virt & PAGE_MASK;
342 length = PAGE_ALIGN(size + (virt & ~PAGE_MASK));
344 end = addr + length;
345 do {
346 next = pgd_addr_end(addr, end);
347 alloc_init_pud(pgdp, addr, next, phys, prot, pgtable_alloc,
348 flags);
349 phys += next - addr;
350 } while (pgdp++, addr = next, addr != end);
351 }
353 static phys_addr_t pgd_pgtable_alloc(void)
354 {
355 void *ptr = (void *)__get_free_page(PGALLOC_GFP);
356 if (!ptr || !pgtable_page_ctor(virt_to_page(ptr)))
357 BUG();
359 /* Ensure the zeroed page is visible to the page table walker */
360 dsb(ishst);
361 return __pa(ptr);
362 }
364 /*
365 * This function can only be used to modify existing table entries,
366 * without allocating new levels of table. Note that this permits the
367 * creation of new section or page entries.
368 */
369 static void __init create_mapping_noalloc(phys_addr_t phys, unsigned long virt,
370 phys_addr_t size, pgprot_t prot)
371 {
372 if (virt < VMALLOC_START) {
373 pr_warn("BUG: not creating mapping for %pa at 0x%016lx - outside kernel range\n",
374 &phys, virt);
375 return;
376 }
377 __create_pgd_mapping(init_mm.pgd, phys, virt, size, prot, NULL,
378 NO_CONT_MAPPINGS);
379 }
381 void __init create_pgd_mapping(struct mm_struct *mm, phys_addr_t phys,
382 unsigned long virt, phys_addr_t size,
383 pgprot_t prot, bool page_mappings_only)
384 {
385 int flags = 0;
387 BUG_ON(mm == &init_mm);
389 if (page_mappings_only)
390 flags = NO_BLOCK_MAPPINGS | NO_CONT_MAPPINGS;
392 __create_pgd_mapping(mm->pgd, phys, virt, size, prot,
393 pgd_pgtable_alloc, flags);
394 }
396 static void update_mapping_prot(phys_addr_t phys, unsigned long virt,
397 phys_addr_t size, pgprot_t prot)
398 {
399 if (virt < VMALLOC_START) {
400 pr_warn("BUG: not updating mapping for %pa at 0x%016lx - outside kernel range\n",
401 &phys, virt);
402 return;
403 }
405 __create_pgd_mapping(init_mm.pgd, phys, virt, size, prot, NULL,
406 NO_CONT_MAPPINGS);
408 /* flush the TLBs after updating live kernel mappings */
409 flush_tlb_kernel_range(virt, virt + size);
410 }
412 static void __init __map_memblock(pgd_t *pgdp, phys_addr_t start,
413 phys_addr_t end, pgprot_t prot, int flags)
414 {
415 __create_pgd_mapping(pgdp, start, __phys_to_virt(start), end - start,
416 prot, early_pgtable_alloc, flags);
417 }
419 void __init mark_linear_text_alias_ro(void)
420 {
421 /*
422 * Remove the write permissions from the linear alias of .text/.rodata
423 */
424 update_mapping_prot(__pa_symbol(_text), (unsigned long)lm_alias(_text),
425 (unsigned long)__init_begin - (unsigned long)_text,
426 PAGE_KERNEL_RO);
427 }
429 static void __init map_mem(pgd_t *pgdp)
430 {
431 phys_addr_t kernel_start = __pa_symbol(_text);
432 phys_addr_t kernel_end = __pa_symbol(__init_begin);
433 struct memblock_region *reg;
434 int flags = 0;
436 if (debug_pagealloc_enabled())
437 flags = NO_BLOCK_MAPPINGS | NO_CONT_MAPPINGS;
439 /*
440 * Take care not to create a writable alias for the
441 * read-only text and rodata sections of the kernel image.
442 * So temporarily mark them as NOMAP to skip mappings in
443 * the following for-loop
444 */
445 memblock_mark_nomap(kernel_start, kernel_end - kernel_start);
446 #ifdef CONFIG_KEXEC_CORE
447 if (crashk_res.end)
448 memblock_mark_nomap(crashk_res.start,
449 resource_size(&crashk_res));
450 #endif
452 /* map all the memory banks */
453 for_each_memblock(memory, reg) {
454 phys_addr_t start = reg->base;
455 phys_addr_t end = start + reg->size;
457 if (start >= end)
458 break;
459 if (memblock_is_nomap(reg))
460 continue;
462 __map_memblock(pgdp, start, end, PAGE_KERNEL, flags);
463 }
465 /*
466 * Map the linear alias of the [_text, __init_begin) interval
467 * as non-executable now, and remove the write permission in
468 * mark_linear_text_alias_ro() below (which will be called after
469 * alternative patching has completed). This makes the contents
470 * of the region accessible to subsystems such as hibernate,
471 * but protects it from inadvertent modification or execution.
472 * Note that contiguous mappings cannot be remapped in this way,
473 * so we should avoid them here.
474 */
475 __map_memblock(pgdp, kernel_start, kernel_end,
476 PAGE_KERNEL, NO_CONT_MAPPINGS);
477 memblock_clear_nomap(kernel_start, kernel_end - kernel_start);
479 #ifdef CONFIG_KEXEC_CORE
480 /*
481 * Use page-level mappings here so that we can shrink the region
482 * in page granularity and put back unused memory to buddy system
483 * through /sys/kernel/kexec_crash_size interface.
484 */
485 if (crashk_res.end) {
486 __map_memblock(pgdp, crashk_res.start, crashk_res.end + 1,
487 PAGE_KERNEL,
488 NO_BLOCK_MAPPINGS | NO_CONT_MAPPINGS);
489 memblock_clear_nomap(crashk_res.start,
490 resource_size(&crashk_res));
491 }
492 #endif
493 }
495 void mark_rodata_ro(void)
496 {
497 unsigned long section_size;
499 /*
500 * mark .rodata as read only. Use __init_begin rather than __end_rodata
501 * to cover NOTES and EXCEPTION_TABLE.
502 */
503 section_size = (unsigned long)__init_begin - (unsigned long)__start_rodata;
504 update_mapping_prot(__pa_symbol(__start_rodata), (unsigned long)__start_rodata,
505 section_size, PAGE_KERNEL_RO);
507 debug_checkwx();
508 }
510 static void __init map_kernel_segment(pgd_t *pgdp, void *va_start, void *va_end,
511 pgprot_t prot, struct vm_struct *vma,
512 int flags, unsigned long vm_flags)
513 {
514 phys_addr_t pa_start = __pa_symbol(va_start);
515 unsigned long size = va_end - va_start;
517 BUG_ON(!PAGE_ALIGNED(pa_start));
518 BUG_ON(!PAGE_ALIGNED(size));
520 __create_pgd_mapping(pgdp, pa_start, (unsigned long)va_start, size, prot,
521 early_pgtable_alloc, flags);
523 if (!(vm_flags & VM_NO_GUARD))
524 size += PAGE_SIZE;
526 vma->addr = va_start;
527 vma->phys_addr = pa_start;
528 vma->size = size;
529 vma->flags = VM_MAP | vm_flags;
530 vma->caller = __builtin_return_address(0);
532 vm_area_add_early(vma);
533 }
535 static int __init parse_rodata(char *arg)
536 {
537 return strtobool(arg, &rodata_enabled);
538 }
539 early_param("rodata", parse_rodata);
541 #ifdef CONFIG_UNMAP_KERNEL_AT_EL0
542 static int __init map_entry_trampoline(void)
543 {
544 pgprot_t prot = rodata_enabled ? PAGE_KERNEL_ROX : PAGE_KERNEL_EXEC;
545 phys_addr_t pa_start = __pa_symbol(__entry_tramp_text_start);
547 /* The trampoline is always mapped and can therefore be global */
548 pgprot_val(prot) &= ~PTE_NG;
550 /* Map only the text into the trampoline page table */
551 memset(tramp_pg_dir, 0, PGD_SIZE);
552 __create_pgd_mapping(tramp_pg_dir, pa_start, TRAMP_VALIAS, PAGE_SIZE,
553 prot, pgd_pgtable_alloc, 0);
555 /* Map both the text and data into the kernel page table */
556 __set_fixmap(FIX_ENTRY_TRAMP_TEXT, pa_start, prot);
557 if (IS_ENABLED(CONFIG_RANDOMIZE_BASE)) {
558 extern char __entry_tramp_data_start[];
560 __set_fixmap(FIX_ENTRY_TRAMP_DATA,
561 __pa_symbol(__entry_tramp_data_start),
562 PAGE_KERNEL_RO);
563 }
565 return 0;
566 }
567 core_initcall(map_entry_trampoline);
568 #endif
570 /*
571 * Create fine-grained mappings for the kernel.
572 */
573 static void __init map_kernel(pgd_t *pgdp)
574 {
575 static struct vm_struct vmlinux_text, vmlinux_rodata, vmlinux_inittext,
576 vmlinux_initdata, vmlinux_data;
578 /*
579 * External debuggers may need to write directly to the text
580 * mapping to install SW breakpoints. Allow this (only) when
581 * explicitly requested with rodata=off.
582 */
583 pgprot_t text_prot = rodata_enabled ? PAGE_KERNEL_ROX : PAGE_KERNEL_EXEC;
585 /*
586 * Only rodata will be remapped with different permissions later on,
587 * all other segments are allowed to use contiguous mappings.
588 */
589 map_kernel_segment(pgdp, _text, _etext, text_prot, &vmlinux_text, 0,
590 VM_NO_GUARD);
591 map_kernel_segment(pgdp, __start_rodata, __inittext_begin, PAGE_KERNEL,
592 &vmlinux_rodata, NO_CONT_MAPPINGS, VM_NO_GUARD);
593 map_kernel_segment(pgdp, __inittext_begin, __inittext_end, text_prot,
594 &vmlinux_inittext, 0, VM_NO_GUARD);
595 map_kernel_segment(pgdp, __initdata_begin, __initdata_end, PAGE_KERNEL,
596 &vmlinux_initdata, 0, VM_NO_GUARD);
597 map_kernel_segment(pgdp, _data, _end, PAGE_KERNEL, &vmlinux_data, 0, 0);
599 if (!READ_ONCE(pgd_val(*pgd_offset_raw(pgdp, FIXADDR_START)))) {
600 /*
601 * The fixmap falls in a separate pgd to the kernel, and doesn't
602 * live in the carveout for the swapper_pg_dir. We can simply
603 * re-use the existing dir for the fixmap.
604 */
605 set_pgd(pgd_offset_raw(pgdp, FIXADDR_START),
606 READ_ONCE(*pgd_offset_k(FIXADDR_START)));
607 } else if (CONFIG_PGTABLE_LEVELS > 3) {
608 /*
609 * The fixmap shares its top level pgd entry with the kernel
610 * mapping. This can really only occur when we are running
611 * with 16k/4 levels, so we can simply reuse the pud level
612 * entry instead.
613 */
614 BUG_ON(!IS_ENABLED(CONFIG_ARM64_16K_PAGES));
615 pud_populate(&init_mm,
616 pud_set_fixmap_offset(pgdp, FIXADDR_START),
617 lm_alias(bm_pmd));
618 pud_clear_fixmap();
619 } else {
620 BUG();
621 }
623 kasan_copy_shadow(pgdp);
624 }
626 /*
627 * paging_init() sets up the page tables, initialises the zone memory
628 * maps and sets up the zero page.
629 */
630 void __init paging_init(void)
631 {
632 phys_addr_t pgd_phys = early_pgtable_alloc();
633 pgd_t *pgdp = pgd_set_fixmap(pgd_phys);
635 map_kernel(pgdp);
636 map_mem(pgdp);
638 /*
639 * We want to reuse the original swapper_pg_dir so we don't have to
640 * communicate the new address to non-coherent secondaries in
641 * secondary_entry, and so cpu_switch_mm can generate the address with
642 * adrp+add rather than a load from some global variable.
643 *
644 * To do this we need to go via a temporary pgd.
645 */
646 cpu_replace_ttbr1(__va(pgd_phys));
647 memcpy(swapper_pg_dir, pgdp, PGD_SIZE);
648 cpu_replace_ttbr1(lm_alias(swapper_pg_dir));
650 pgd_clear_fixmap();
651 memblock_free(pgd_phys, PAGE_SIZE);
653 /*
654 * We only reuse the PGD from the swapper_pg_dir, not the pud + pmd
655 * allocated with it.
656 */
657 memblock_free(__pa_symbol(swapper_pg_dir) + PAGE_SIZE,
658 __pa_symbol(swapper_pg_end) - __pa_symbol(swapper_pg_dir)
659 - PAGE_SIZE);
660 }
662 /*
663 * Check whether a kernel address is valid (derived from arch/x86/).
664 */
665 int kern_addr_valid(unsigned long addr)
666 {
667 pgd_t *pgdp;
668 pud_t *pudp, pud;
669 pmd_t *pmdp, pmd;
670 pte_t *ptep, pte;
672 if ((((long)addr) >> VA_BITS) != -1UL)
673 return 0;
675 pgdp = pgd_offset_k(addr);
676 if (pgd_none(READ_ONCE(*pgdp)))
677 return 0;
679 pudp = pud_offset(pgdp, addr);
680 pud = READ_ONCE(*pudp);
681 if (pud_none(pud))
682 return 0;
684 if (pud_sect(pud))
685 return pfn_valid(pud_pfn(pud));
687 pmdp = pmd_offset(pudp, addr);
688 pmd = READ_ONCE(*pmdp);
689 if (pmd_none(pmd))
690 return 0;
692 if (pmd_sect(pmd))
693 return pfn_valid(pmd_pfn(pmd));
695 ptep = pte_offset_kernel(pmdp, addr);
696 pte = READ_ONCE(*ptep);
697 if (pte_none(pte))
698 return 0;
700 return pfn_valid(pte_pfn(pte));
701 }
702 #ifdef CONFIG_SPARSEMEM_VMEMMAP
703 #if !ARM64_SWAPPER_USES_SECTION_MAPS
704 int __meminit vmemmap_populate(unsigned long start, unsigned long end, int node,
705 struct vmem_altmap *altmap)
706 {
707 return vmemmap_populate_basepages(start, end, node);
708 }
709 #else /* !ARM64_SWAPPER_USES_SECTION_MAPS */
710 int __meminit vmemmap_populate(unsigned long start, unsigned long end, int node,
711 struct vmem_altmap *altmap)
712 {
713 unsigned long addr = start;
714 unsigned long next;
715 pgd_t *pgdp;
716 pud_t *pudp;
717 pmd_t *pmdp;
719 do {
720 next = pmd_addr_end(addr, end);
722 pgdp = vmemmap_pgd_populate(addr, node);
723 if (!pgdp)
724 return -ENOMEM;
726 pudp = vmemmap_pud_populate(pgdp, addr, node);
727 if (!pudp)
728 return -ENOMEM;
730 pmdp = pmd_offset(pudp, addr);
731 if (pmd_none(READ_ONCE(*pmdp))) {
732 void *p = NULL;
734 p = vmemmap_alloc_block_buf(PMD_SIZE, node);
735 if (!p)
736 return -ENOMEM;
738 pmd_set_huge(pmdp, __pa(p), __pgprot(PROT_SECT_NORMAL));
739 } else
740 vmemmap_verify((pte_t *)pmdp, node, addr, next);
741 } while (addr = next, addr != end);
743 return 0;
744 }
745 #endif /* CONFIG_ARM64_64K_PAGES */
746 void vmemmap_free(unsigned long start, unsigned long end,
747 struct vmem_altmap *altmap)
748 {
749 }
750 #endif /* CONFIG_SPARSEMEM_VMEMMAP */
752 static inline pud_t * fixmap_pud(unsigned long addr)
753 {
754 pgd_t *pgdp = pgd_offset_k(addr);
755 pgd_t pgd = READ_ONCE(*pgdp);
757 BUG_ON(pgd_none(pgd) || pgd_bad(pgd));
759 return pud_offset_kimg(pgdp, addr);
760 }
762 static inline pmd_t * fixmap_pmd(unsigned long addr)
763 {
764 pud_t *pudp = fixmap_pud(addr);
765 pud_t pud = READ_ONCE(*pudp);
767 BUG_ON(pud_none(pud) || pud_bad(pud));
769 return pmd_offset_kimg(pudp, addr);
770 }
772 static inline pte_t * fixmap_pte(unsigned long addr)
773 {
774 return &bm_pte[pte_index(addr)];
775 }
777 /*
778 * The p*d_populate functions call virt_to_phys implicitly so they can't be used
779 * directly on kernel symbols (bm_p*d). This function is called too early to use
780 * lm_alias so __p*d_populate functions must be used to populate with the
781 * physical address from __pa_symbol.
782 */
783 void __init early_fixmap_init(void)
784 {
785 pgd_t *pgdp, pgd;
786 pud_t *pudp;
787 pmd_t *pmdp;
788 unsigned long addr = FIXADDR_START;
790 pgdp = pgd_offset_k(addr);
791 pgd = READ_ONCE(*pgdp);
792 if (CONFIG_PGTABLE_LEVELS > 3 &&
793 !(pgd_none(pgd) || pgd_page_paddr(pgd) == __pa_symbol(bm_pud))) {
794 /*
795 * We only end up here if the kernel mapping and the fixmap
796 * share the top level pgd entry, which should only happen on
797 * 16k/4 levels configurations.
798 */
799 BUG_ON(!IS_ENABLED(CONFIG_ARM64_16K_PAGES));
800 pudp = pud_offset_kimg(pgdp, addr);
801 } else {
802 if (pgd_none(pgd))
803 __pgd_populate(pgdp, __pa_symbol(bm_pud), PUD_TYPE_TABLE);
804 pudp = fixmap_pud(addr);
805 }
806 if (pud_none(READ_ONCE(*pudp)))
807 __pud_populate(pudp, __pa_symbol(bm_pmd), PMD_TYPE_TABLE);
808 pmdp = fixmap_pmd(addr);
809 __pmd_populate(pmdp, __pa_symbol(bm_pte), PMD_TYPE_TABLE);
811 /*
812 * The boot-ioremap range spans multiple pmds, for which
813 * we are not prepared:
814 */
815 BUILD_BUG_ON((__fix_to_virt(FIX_BTMAP_BEGIN) >> PMD_SHIFT)
816 != (__fix_to_virt(FIX_BTMAP_END) >> PMD_SHIFT));
818 if ((pmdp != fixmap_pmd(fix_to_virt(FIX_BTMAP_BEGIN)))
819 || pmdp != fixmap_pmd(fix_to_virt(FIX_BTMAP_END))) {
820 WARN_ON(1);
821 pr_warn("pmdp %p != %p, %p\n",
822 pmdp, fixmap_pmd(fix_to_virt(FIX_BTMAP_BEGIN)),
823 fixmap_pmd(fix_to_virt(FIX_BTMAP_END)));
824 pr_warn("fix_to_virt(FIX_BTMAP_BEGIN): %08lx\n",
825 fix_to_virt(FIX_BTMAP_BEGIN));
826 pr_warn("fix_to_virt(FIX_BTMAP_END): %08lx\n",
827 fix_to_virt(FIX_BTMAP_END));
829 pr_warn("FIX_BTMAP_END: %d\n", FIX_BTMAP_END);
830 pr_warn("FIX_BTMAP_BEGIN: %d\n", FIX_BTMAP_BEGIN);
831 }
832 }
834 /*
835 * Unusually, this is also called in IRQ context (ghes_iounmap_irq) so if we
836 * ever need to use IPIs for TLB broadcasting, then we're in trouble here.
837 */
838 void __set_fixmap(enum fixed_addresses idx,
839 phys_addr_t phys, pgprot_t flags)
840 {
841 unsigned long addr = __fix_to_virt(idx);
842 pte_t *ptep;
844 BUG_ON(idx <= FIX_HOLE || idx >= __end_of_fixed_addresses);
846 ptep = fixmap_pte(addr);
848 if (pgprot_val(flags)) {
849 set_pte(ptep, pfn_pte(phys >> PAGE_SHIFT, flags));
850 } else {
851 pte_clear(&init_mm, addr, ptep);
852 flush_tlb_kernel_range(addr, addr+PAGE_SIZE);
853 }
854 }
856 void *__init __fixmap_remap_fdt(phys_addr_t dt_phys, int *size, pgprot_t prot)
857 {
858 const u64 dt_virt_base = __fix_to_virt(FIX_FDT);
859 int offset;
860 void *dt_virt;
862 /*
863 * Check whether the physical FDT address is set and meets the minimum
864 * alignment requirement. Since we are relying on MIN_FDT_ALIGN to be
865 * at least 8 bytes so that we can always access the magic and size
866 * fields of the FDT header after mapping the first chunk, double check
867 * here if that is indeed the case.
868 */
869 BUILD_BUG_ON(MIN_FDT_ALIGN < 8);
870 if (!dt_phys || dt_phys % MIN_FDT_ALIGN)
871 return NULL;
873 /*
874 * Make sure that the FDT region can be mapped without the need to
875 * allocate additional translation table pages, so that it is safe
876 * to call create_mapping_noalloc() this early.
877 *
878 * On 64k pages, the FDT will be mapped using PTEs, so we need to
879 * be in the same PMD as the rest of the fixmap.
880 * On 4k pages, we'll use section mappings for the FDT so we only
881 * have to be in the same PUD.
882 */
883 BUILD_BUG_ON(dt_virt_base % SZ_2M);
885 BUILD_BUG_ON(__fix_to_virt(FIX_FDT_END) >> SWAPPER_TABLE_SHIFT !=
886 __fix_to_virt(FIX_BTMAP_BEGIN) >> SWAPPER_TABLE_SHIFT);
888 offset = dt_phys % SWAPPER_BLOCK_SIZE;
889 dt_virt = (void *)dt_virt_base + offset;
891 /* map the first chunk so we can read the size from the header */
892 create_mapping_noalloc(round_down(dt_phys, SWAPPER_BLOCK_SIZE),
893 dt_virt_base, SWAPPER_BLOCK_SIZE, prot);
895 if (fdt_magic(dt_virt) != FDT_MAGIC)
896 return NULL;
898 *size = fdt_totalsize(dt_virt);
899 if (*size > MAX_FDT_SIZE)
900 return NULL;
902 if (offset + *size > SWAPPER_BLOCK_SIZE)
903 create_mapping_noalloc(round_down(dt_phys, SWAPPER_BLOCK_SIZE), dt_virt_base,
904 round_up(offset + *size, SWAPPER_BLOCK_SIZE), prot);
906 return dt_virt;
907 }
909 void *__init fixmap_remap_fdt(phys_addr_t dt_phys)
910 {
911 void *dt_virt;
912 int size;
914 dt_virt = __fixmap_remap_fdt(dt_phys, &size, PAGE_KERNEL_RO);
915 if (!dt_virt)
916 return NULL;
918 memblock_reserve(dt_phys, size);
919 return dt_virt;
920 }
922 int __init arch_ioremap_pud_supported(void)
923 {
924 /* only 4k granule supports level 1 block mappings */
925 return IS_ENABLED(CONFIG_ARM64_4K_PAGES);
926 }
928 int __init arch_ioremap_pmd_supported(void)
929 {
930 return 1;
931 }
933 int pud_set_huge(pud_t *pudp, phys_addr_t phys, pgprot_t prot)
934 {
935 pgprot_t sect_prot = __pgprot(PUD_TYPE_SECT |
936 pgprot_val(mk_sect_prot(prot)));
937 pud_t new_pud = pfn_pud(__phys_to_pfn(phys), sect_prot);
939 /* Only allow permission changes for now */
940 if (!pgattr_change_is_safe(READ_ONCE(pud_val(*pudp)),
941 pud_val(new_pud)))
942 return 0;
944 BUG_ON(phys & ~PUD_MASK);
945 set_pud(pudp, new_pud);
946 return 1;
947 }
949 int pmd_set_huge(pmd_t *pmdp, phys_addr_t phys, pgprot_t prot)
950 {
951 pgprot_t sect_prot = __pgprot(PMD_TYPE_SECT |
952 pgprot_val(mk_sect_prot(prot)));
953 pmd_t new_pmd = pfn_pmd(__phys_to_pfn(phys), sect_prot);
955 /* Only allow permission changes for now */
956 if (!pgattr_change_is_safe(READ_ONCE(pmd_val(*pmdp)),
957 pmd_val(new_pmd)))
958 return 0;
960 BUG_ON(phys & ~PMD_MASK);
961 set_pmd(pmdp, new_pmd);
962 return 1;
963 }
965 int pud_clear_huge(pud_t *pudp)
966 {
967 if (!pud_sect(READ_ONCE(*pudp)))
968 return 0;
969 pud_clear(pudp);
970 return 1;
971 }
973 int pmd_clear_huge(pmd_t *pmdp)
974 {
975 if (!pmd_sect(READ_ONCE(*pmdp)))
976 return 0;
977 pmd_clear(pmdp);
978 return 1;
979 }
981 int pmd_free_pte_page(pmd_t *pmdp, unsigned long addr)
982 {
983 pte_t *table;
984 pmd_t pmd;
986 pmd = READ_ONCE(*pmdp);
988 if (!pmd_present(pmd))
989 return 1;
990 if (!pmd_table(pmd)) {
991 VM_WARN_ON(!pmd_table(pmd));
992 return 1;
993 }
995 table = pte_offset_kernel(pmdp, addr);
996 pmd_clear(pmdp);
997 __flush_tlb_kernel_pgtable(addr);
998 pte_free_kernel(NULL, table);
999 return 1;
1000 }
1002 int pud_free_pmd_page(pud_t *pudp, unsigned long addr)
1003 {
1004 pmd_t *table;
1005 pmd_t *pmdp;
1006 pud_t pud;
1007 unsigned long next, end;
1009 pud = READ_ONCE(*pudp);
1011 if (!pud_present(pud))
1012 return 1;
1013 if (!pud_table(pud)) {
1014 VM_WARN_ON(!pud_table(pud));
1015 return 1;
1016 }
1018 table = pmd_offset(pudp, addr);
1019 pmdp = table;
1020 next = addr;
1021 end = addr + PUD_SIZE;
1022 do {
1023 pmd_free_pte_page(pmdp, next);
1024 } while (pmdp++, next += PMD_SIZE, next != end);
1026 pud_clear(pudp);
1027 __flush_tlb_kernel_pgtable(addr);
1028 pmd_free(NULL, table);
1029 return 1;
1030 }