]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - arch/sparc/kernel/of_device_32.c
Merge tag 'alloc-args-v4.19-rc8' of https://git.kernel.org/pub/scm/linux/kernel/git...
[rpmsg/rpmsg.git] / arch / sparc / kernel / of_device_32.c
1 // SPDX-License-Identifier: GPL-2.0
2 #include <linux/string.h>
3 #include <linux/kernel.h>
4 #include <linux/of.h>
5 #include <linux/init.h>
6 #include <linux/mod_devicetable.h>
7 #include <linux/slab.h>
8 #include <linux/errno.h>
9 #include <linux/irq.h>
10 #include <linux/of_device.h>
11 #include <linux/of_platform.h>
12 #include <linux/dma-mapping.h>
13 #include <asm/leon.h>
14 #include <asm/leon_amba.h>
16 #include "of_device_common.h"
17 #include "irq.h"
19 /*
20  * PCI bus specific translator
21  */
23 static int of_bus_pci_match(struct device_node *np)
24 {
25         if (!strcmp(np->type, "pci") || !strcmp(np->type, "pciex")) {
26                 /* Do not do PCI specific frobbing if the
27                  * PCI bridge lacks a ranges property.  We
28                  * want to pass it through up to the next
29                  * parent as-is, not with the PCI translate
30                  * method which chops off the top address cell.
31                  */
32                 if (!of_find_property(np, "ranges", NULL))
33                         return 0;
35                 return 1;
36         }
38         return 0;
39 }
41 static void of_bus_pci_count_cells(struct device_node *np,
42                                    int *addrc, int *sizec)
43 {
44         if (addrc)
45                 *addrc = 3;
46         if (sizec)
47                 *sizec = 2;
48 }
50 static int of_bus_pci_map(u32 *addr, const u32 *range,
51                           int na, int ns, int pna)
52 {
53         u32 result[OF_MAX_ADDR_CELLS];
54         int i;
56         /* Check address type match */
57         if ((addr[0] ^ range[0]) & 0x03000000)
58                 return -EINVAL;
60         if (of_out_of_range(addr + 1, range + 1, range + na + pna,
61                             na - 1, ns))
62                 return -EINVAL;
64         /* Start with the parent range base.  */
65         memcpy(result, range + na, pna * 4);
67         /* Add in the child address offset, skipping high cell.  */
68         for (i = 0; i < na - 1; i++)
69                 result[pna - 1 - i] +=
70                         (addr[na - 1 - i] -
71                          range[na - 1 - i]);
73         memcpy(addr, result, pna * 4);
75         return 0;
76 }
78 static unsigned long of_bus_pci_get_flags(const u32 *addr, unsigned long flags)
79 {
80         u32 w = addr[0];
82         /* For PCI, we override whatever child busses may have used.  */
83         flags = 0;
84         switch((w >> 24) & 0x03) {
85         case 0x01:
86                 flags |= IORESOURCE_IO;
87                 break;
89         case 0x02: /* 32 bits */
90         case 0x03: /* 64 bits */
91                 flags |= IORESOURCE_MEM;
92                 break;
93         }
94         if (w & 0x40000000)
95                 flags |= IORESOURCE_PREFETCH;
96         return flags;
97 }
99 static unsigned long of_bus_sbus_get_flags(const u32 *addr, unsigned long flags)
101         return IORESOURCE_MEM;
104  /*
105  * AMBAPP bus specific translator
106  */
108 static int of_bus_ambapp_match(struct device_node *np)
110         return !strcmp(np->type, "ambapp");
113 static void of_bus_ambapp_count_cells(struct device_node *child,
114                                       int *addrc, int *sizec)
116         if (addrc)
117                 *addrc = 1;
118         if (sizec)
119                 *sizec = 1;
122 static int of_bus_ambapp_map(u32 *addr, const u32 *range,
123                              int na, int ns, int pna)
125         return of_bus_default_map(addr, range, na, ns, pna);
128 static unsigned long of_bus_ambapp_get_flags(const u32 *addr,
129                                              unsigned long flags)
131         return IORESOURCE_MEM;
134 /*
135  * Array of bus specific translators
136  */
138 static struct of_bus of_busses[] = {
139         /* PCI */
140         {
141                 .name = "pci",
142                 .addr_prop_name = "assigned-addresses",
143                 .match = of_bus_pci_match,
144                 .count_cells = of_bus_pci_count_cells,
145                 .map = of_bus_pci_map,
146                 .get_flags = of_bus_pci_get_flags,
147         },
148         /* SBUS */
149         {
150                 .name = "sbus",
151                 .addr_prop_name = "reg",
152                 .match = of_bus_sbus_match,
153                 .count_cells = of_bus_sbus_count_cells,
154                 .map = of_bus_default_map,
155                 .get_flags = of_bus_sbus_get_flags,
156         },
157         /* AMBA */
158         {
159                 .name = "ambapp",
160                 .addr_prop_name = "reg",
161                 .match = of_bus_ambapp_match,
162                 .count_cells = of_bus_ambapp_count_cells,
163                 .map = of_bus_ambapp_map,
164                 .get_flags = of_bus_ambapp_get_flags,
165         },
166         /* Default */
167         {
168                 .name = "default",
169                 .addr_prop_name = "reg",
170                 .match = NULL,
171                 .count_cells = of_bus_default_count_cells,
172                 .map = of_bus_default_map,
173                 .get_flags = of_bus_default_get_flags,
174         },
175 };
177 static struct of_bus *of_match_bus(struct device_node *np)
179         int i;
181         for (i = 0; i < ARRAY_SIZE(of_busses); i ++)
182                 if (!of_busses[i].match || of_busses[i].match(np))
183                         return &of_busses[i];
184         BUG();
185         return NULL;
188 static int __init build_one_resource(struct device_node *parent,
189                                      struct of_bus *bus,
190                                      struct of_bus *pbus,
191                                      u32 *addr,
192                                      int na, int ns, int pna)
194         const u32 *ranges;
195         unsigned int rlen;
196         int rone;
198         ranges = of_get_property(parent, "ranges", &rlen);
199         if (ranges == NULL || rlen == 0) {
200                 u32 result[OF_MAX_ADDR_CELLS];
201                 int i;
203                 memset(result, 0, pna * 4);
204                 for (i = 0; i < na; i++)
205                         result[pna - 1 - i] =
206                                 addr[na - 1 - i];
208                 memcpy(addr, result, pna * 4);
209                 return 0;
210         }
212         /* Now walk through the ranges */
213         rlen /= 4;
214         rone = na + pna + ns;
215         for (; rlen >= rone; rlen -= rone, ranges += rone) {
216                 if (!bus->map(addr, ranges, na, ns, pna))
217                         return 0;
218         }
220         return 1;
223 static int __init use_1to1_mapping(struct device_node *pp)
225         /* If we have a ranges property in the parent, use it.  */
226         if (of_find_property(pp, "ranges", NULL) != NULL)
227                 return 0;
229         /* Some SBUS devices use intermediate nodes to express
230          * hierarchy within the device itself.  These aren't
231          * real bus nodes, and don't have a 'ranges' property.
232          * But, we should still pass the translation work up
233          * to the SBUS itself.
234          */
235         if (!strcmp(pp->name, "dma") ||
236             !strcmp(pp->name, "espdma") ||
237             !strcmp(pp->name, "ledma") ||
238             !strcmp(pp->name, "lebuffer"))
239                 return 0;
241         return 1;
244 static int of_resource_verbose;
246 static void __init build_device_resources(struct platform_device *op,
247                                           struct device *parent)
249         struct platform_device *p_op;
250         struct of_bus *bus;
251         int na, ns;
252         int index, num_reg;
253         const void *preg;
255         if (!parent)
256                 return;
258         p_op = to_platform_device(parent);
259         bus = of_match_bus(p_op->dev.of_node);
260         bus->count_cells(op->dev.of_node, &na, &ns);
262         preg = of_get_property(op->dev.of_node, bus->addr_prop_name, &num_reg);
263         if (!preg || num_reg == 0)
264                 return;
266         /* Convert to num-cells.  */
267         num_reg /= 4;
269         /* Conver to num-entries.  */
270         num_reg /= na + ns;
272         op->resource = op->archdata.resource;
273         op->num_resources = num_reg;
274         for (index = 0; index < num_reg; index++) {
275                 struct resource *r = &op->resource[index];
276                 u32 addr[OF_MAX_ADDR_CELLS];
277                 const u32 *reg = (preg + (index * ((na + ns) * 4)));
278                 struct device_node *dp = op->dev.of_node;
279                 struct device_node *pp = p_op->dev.of_node;
280                 struct of_bus *pbus, *dbus;
281                 u64 size, result = OF_BAD_ADDR;
282                 unsigned long flags;
283                 int dna, dns;
284                 int pna, pns;
286                 size = of_read_addr(reg + na, ns);
288                 memcpy(addr, reg, na * 4);
290                 flags = bus->get_flags(reg, 0);
292                 if (use_1to1_mapping(pp)) {
293                         result = of_read_addr(addr, na);
294                         goto build_res;
295                 }
297                 dna = na;
298                 dns = ns;
299                 dbus = bus;
301                 while (1) {
302                         dp = pp;
303                         pp = dp->parent;
304                         if (!pp) {
305                                 result = of_read_addr(addr, dna);
306                                 break;
307                         }
309                         pbus = of_match_bus(pp);
310                         pbus->count_cells(dp, &pna, &pns);
312                         if (build_one_resource(dp, dbus, pbus, addr,
313                                                dna, dns, pna))
314                                 break;
316                         flags = pbus->get_flags(addr, flags);
318                         dna = pna;
319                         dns = pns;
320                         dbus = pbus;
321                 }
323         build_res:
324                 memset(r, 0, sizeof(*r));
326                 if (of_resource_verbose)
327                         printk("%s reg[%d] -> %llx\n",
328                                op->dev.of_node->full_name, index,
329                                result);
331                 if (result != OF_BAD_ADDR) {
332                         r->start = result & 0xffffffff;
333                         r->end = result + size - 1;
334                         r->flags = flags | ((result >> 32ULL) & 0xffUL);
335                 }
336                 r->name = op->dev.of_node->name;
337         }
340 static struct platform_device * __init scan_one_device(struct device_node *dp,
341                                                  struct device *parent)
343         struct platform_device *op = kzalloc(sizeof(*op), GFP_KERNEL);
344         const struct linux_prom_irqs *intr;
345         struct dev_archdata *sd;
346         int len, i;
348         if (!op)
349                 return NULL;
351         sd = &op->dev.archdata;
352         sd->op = op;
354         op->dev.of_node = dp;
356         intr = of_get_property(dp, "intr", &len);
357         if (intr) {
358                 op->archdata.num_irqs = len / sizeof(struct linux_prom_irqs);
359                 for (i = 0; i < op->archdata.num_irqs; i++)
360                         op->archdata.irqs[i] =
361                             sparc_config.build_device_irq(op, intr[i].pri);
362         } else {
363                 const unsigned int *irq =
364                         of_get_property(dp, "interrupts", &len);
366                 if (irq) {
367                         op->archdata.num_irqs = len / sizeof(unsigned int);
368                         for (i = 0; i < op->archdata.num_irqs; i++)
369                                 op->archdata.irqs[i] =
370                                     sparc_config.build_device_irq(op, irq[i]);
371                 } else {
372                         op->archdata.num_irqs = 0;
373                 }
374         }
376         build_device_resources(op, parent);
378         op->dev.parent = parent;
379         op->dev.bus = &platform_bus_type;
380         if (!parent)
381                 dev_set_name(&op->dev, "root");
382         else
383                 dev_set_name(&op->dev, "%08x", dp->phandle);
385         op->dev.coherent_dma_mask = DMA_BIT_MASK(32);
386         op->dev.dma_mask = &op->dev.coherent_dma_mask;
388         if (of_device_register(op)) {
389                 printk("%s: Could not register of device.\n",
390                        dp->full_name);
391                 kfree(op);
392                 op = NULL;
393         }
395         return op;
398 static void __init scan_tree(struct device_node *dp, struct device *parent)
400         while (dp) {
401                 struct platform_device *op = scan_one_device(dp, parent);
403                 if (op)
404                         scan_tree(dp->child, &op->dev);
406                 dp = dp->sibling;
407         }
410 static int __init scan_of_devices(void)
412         struct device_node *root = of_find_node_by_path("/");
413         struct platform_device *parent;
415         parent = scan_one_device(root, NULL);
416         if (!parent)
417                 return 0;
419         scan_tree(root->child, &parent->dev);
420         return 0;
422 postcore_initcall(scan_of_devices);
424 static int __init of_debug(char *str)
426         int val = 0;
428         get_option(&str, &val);
429         if (val & 1)
430                 of_resource_verbose = 1;
431         return 1;
434 __setup("of_debug=", of_debug);