1 /*
2 * Copyright 2006 Andi Kleen, SUSE Labs.
3 * Subject to the GNU Public License, v.2
4 *
5 * Fast user context implementation of clock_gettime, gettimeofday, and time.
6 *
7 * 32 Bit compat layer by Stefani Seibold <stefani@seibold.net>
8 * sponsored by Rohde & Schwarz GmbH & Co. KG Munich/Germany
9 *
10 * The code should have no internal unresolved relocations.
11 * Check with readelf after changing.
12 */
14 #include <uapi/linux/time.h>
15 #include <asm/vgtod.h>
16 #include <asm/vvar.h>
17 #include <asm/unistd.h>
18 #include <asm/msr.h>
19 #include <asm/pvclock.h>
20 #include <asm/mshyperv.h>
21 #include <linux/math64.h>
22 #include <linux/time.h>
23 #include <linux/kernel.h>
25 #define gtod (&VVAR(vsyscall_gtod_data))
27 extern int __vdso_clock_gettime(clockid_t clock, struct timespec *ts);
28 extern int __vdso_gettimeofday(struct timeval *tv, struct timezone *tz);
29 extern time_t __vdso_time(time_t *t);
31 #ifdef CONFIG_PARAVIRT_CLOCK
32 extern u8 pvclock_page
33 __attribute__((visibility("hidden")));
34 #endif
36 #ifdef CONFIG_HYPERV_TSCPAGE
37 extern u8 hvclock_page
38 __attribute__((visibility("hidden")));
39 #endif
41 #ifndef BUILD_VDSO32
43 notrace static long vdso_fallback_gettime(long clock, struct timespec *ts)
44 {
45 long ret;
46 asm ("syscall" : "=a" (ret), "=m" (*ts) :
47 "0" (__NR_clock_gettime), "D" (clock), "S" (ts) :
48 "memory", "rcx", "r11");
49 return ret;
50 }
52 notrace static long vdso_fallback_gtod(struct timeval *tv, struct timezone *tz)
53 {
54 long ret;
56 asm ("syscall" : "=a" (ret), "=m" (*tv), "=m" (*tz) :
57 "0" (__NR_gettimeofday), "D" (tv), "S" (tz) :
58 "memory", "rcx", "r11");
59 return ret;
60 }
63 #else
65 notrace static long vdso_fallback_gettime(long clock, struct timespec *ts)
66 {
67 long ret;
69 asm (
70 "mov %%ebx, %%edx \n"
71 "mov %[clock], %%ebx \n"
72 "call __kernel_vsyscall \n"
73 "mov %%edx, %%ebx \n"
74 : "=a" (ret), "=m" (*ts)
75 : "0" (__NR_clock_gettime), [clock] "g" (clock), "c" (ts)
76 : "memory", "edx");
77 return ret;
78 }
80 notrace static long vdso_fallback_gtod(struct timeval *tv, struct timezone *tz)
81 {
82 long ret;
84 asm (
85 "mov %%ebx, %%edx \n"
86 "mov %[tv], %%ebx \n"
87 "call __kernel_vsyscall \n"
88 "mov %%edx, %%ebx \n"
89 : "=a" (ret), "=m" (*tv), "=m" (*tz)
90 : "0" (__NR_gettimeofday), [tv] "g" (tv), "c" (tz)
91 : "memory", "edx");
92 return ret;
93 }
95 #endif
97 #ifdef CONFIG_PARAVIRT_CLOCK
98 static notrace const struct pvclock_vsyscall_time_info *get_pvti0(void)
99 {
100 return (const struct pvclock_vsyscall_time_info *)&pvclock_page;
101 }
103 static notrace u64 vread_pvclock(int *mode)
104 {
105 const struct pvclock_vcpu_time_info *pvti = &get_pvti0()->pvti;
106 u64 ret;
107 u64 last;
108 u32 version;
110 /*
111 * Note: The kernel and hypervisor must guarantee that cpu ID
112 * number maps 1:1 to per-CPU pvclock time info.
113 *
114 * Because the hypervisor is entirely unaware of guest userspace
115 * preemption, it cannot guarantee that per-CPU pvclock time
116 * info is updated if the underlying CPU changes or that that
117 * version is increased whenever underlying CPU changes.
118 *
119 * On KVM, we are guaranteed that pvti updates for any vCPU are
120 * atomic as seen by *all* vCPUs. This is an even stronger
121 * guarantee than we get with a normal seqlock.
122 *
123 * On Xen, we don't appear to have that guarantee, but Xen still
124 * supplies a valid seqlock using the version field.
125 *
126 * We only do pvclock vdso timing at all if
127 * PVCLOCK_TSC_STABLE_BIT is set, and we interpret that bit to
128 * mean that all vCPUs have matching pvti and that the TSC is
129 * synced, so we can just look at vCPU 0's pvti.
130 */
132 do {
133 version = pvclock_read_begin(pvti);
135 if (unlikely(!(pvti->flags & PVCLOCK_TSC_STABLE_BIT))) {
136 *mode = VCLOCK_NONE;
137 return 0;
138 }
140 ret = __pvclock_read_cycles(pvti, rdtsc_ordered());
141 } while (pvclock_read_retry(pvti, version));
143 /* refer to vread_tsc() comment for rationale */
144 last = gtod->cycle_last;
146 if (likely(ret >= last))
147 return ret;
149 return last;
150 }
151 #endif
152 #ifdef CONFIG_HYPERV_TSCPAGE
153 static notrace u64 vread_hvclock(int *mode)
154 {
155 const struct ms_hyperv_tsc_page *tsc_pg =
156 (const struct ms_hyperv_tsc_page *)&hvclock_page;
157 u64 current_tick = hv_read_tsc_page(tsc_pg);
159 if (current_tick != U64_MAX)
160 return current_tick;
162 *mode = VCLOCK_NONE;
163 return 0;
164 }
165 #endif
167 notrace static u64 vread_tsc(void)
168 {
169 u64 ret = (u64)rdtsc_ordered();
170 u64 last = gtod->cycle_last;
172 if (likely(ret >= last))
173 return ret;
175 /*
176 * GCC likes to generate cmov here, but this branch is extremely
177 * predictable (it's just a function of time and the likely is
178 * very likely) and there's a data dependence, so force GCC
179 * to generate a branch instead. I don't barrier() because
180 * we don't actually need a barrier, and if this function
181 * ever gets inlined it will generate worse code.
182 */
183 asm volatile ("");
184 return last;
185 }
187 notrace static inline u64 vgetsns(int *mode)
188 {
189 u64 v;
190 cycles_t cycles;
192 if (gtod->vclock_mode == VCLOCK_TSC)
193 cycles = vread_tsc();
194 #ifdef CONFIG_PARAVIRT_CLOCK
195 else if (gtod->vclock_mode == VCLOCK_PVCLOCK)
196 cycles = vread_pvclock(mode);
197 #endif
198 #ifdef CONFIG_HYPERV_TSCPAGE
199 else if (gtod->vclock_mode == VCLOCK_HVCLOCK)
200 cycles = vread_hvclock(mode);
201 #endif
202 else
203 return 0;
204 v = (cycles - gtod->cycle_last) & gtod->mask;
205 return v * gtod->mult;
206 }
208 /* Code size doesn't matter (vdso is 4k anyway) and this is faster. */
209 notrace static int __always_inline do_realtime(struct timespec *ts)
210 {
211 unsigned long seq;
212 u64 ns;
213 int mode;
215 do {
216 seq = gtod_read_begin(gtod);
217 mode = gtod->vclock_mode;
218 ts->tv_sec = gtod->wall_time_sec;
219 ns = gtod->wall_time_snsec;
220 ns += vgetsns(&mode);
221 ns >>= gtod->shift;
222 } while (unlikely(gtod_read_retry(gtod, seq)));
224 ts->tv_sec += __iter_div_u64_rem(ns, NSEC_PER_SEC, &ns);
225 ts->tv_nsec = ns;
227 return mode;
228 }
230 notrace static int __always_inline do_monotonic(struct timespec *ts)
231 {
232 unsigned long seq;
233 u64 ns;
234 int mode;
236 do {
237 seq = gtod_read_begin(gtod);
238 mode = gtod->vclock_mode;
239 ts->tv_sec = gtod->monotonic_time_sec;
240 ns = gtod->monotonic_time_snsec;
241 ns += vgetsns(&mode);
242 ns >>= gtod->shift;
243 } while (unlikely(gtod_read_retry(gtod, seq)));
245 ts->tv_sec += __iter_div_u64_rem(ns, NSEC_PER_SEC, &ns);
246 ts->tv_nsec = ns;
248 return mode;
249 }
251 notrace static void do_realtime_coarse(struct timespec *ts)
252 {
253 unsigned long seq;
254 do {
255 seq = gtod_read_begin(gtod);
256 ts->tv_sec = gtod->wall_time_coarse_sec;
257 ts->tv_nsec = gtod->wall_time_coarse_nsec;
258 } while (unlikely(gtod_read_retry(gtod, seq)));
259 }
261 notrace static void do_monotonic_coarse(struct timespec *ts)
262 {
263 unsigned long seq;
264 do {
265 seq = gtod_read_begin(gtod);
266 ts->tv_sec = gtod->monotonic_time_coarse_sec;
267 ts->tv_nsec = gtod->monotonic_time_coarse_nsec;
268 } while (unlikely(gtod_read_retry(gtod, seq)));
269 }
271 notrace int __vdso_clock_gettime(clockid_t clock, struct timespec *ts)
272 {
273 switch (clock) {
274 case CLOCK_REALTIME:
275 if (do_realtime(ts) == VCLOCK_NONE)
276 goto fallback;
277 break;
278 case CLOCK_MONOTONIC:
279 if (do_monotonic(ts) == VCLOCK_NONE)
280 goto fallback;
281 break;
282 case CLOCK_REALTIME_COARSE:
283 do_realtime_coarse(ts);
284 break;
285 case CLOCK_MONOTONIC_COARSE:
286 do_monotonic_coarse(ts);
287 break;
288 default:
289 goto fallback;
290 }
292 return 0;
293 fallback:
294 return vdso_fallback_gettime(clock, ts);
295 }
296 int clock_gettime(clockid_t, struct timespec *)
297 __attribute__((weak, alias("__vdso_clock_gettime")));
299 notrace int __vdso_gettimeofday(struct timeval *tv, struct timezone *tz)
300 {
301 if (likely(tv != NULL)) {
302 if (unlikely(do_realtime((struct timespec *)tv) == VCLOCK_NONE))
303 return vdso_fallback_gtod(tv, tz);
304 tv->tv_usec /= 1000;
305 }
306 if (unlikely(tz != NULL)) {
307 tz->tz_minuteswest = gtod->tz_minuteswest;
308 tz->tz_dsttime = gtod->tz_dsttime;
309 }
311 return 0;
312 }
313 int gettimeofday(struct timeval *, struct timezone *)
314 __attribute__((weak, alias("__vdso_gettimeofday")));
316 /*
317 * This will break when the xtime seconds get inaccurate, but that is
318 * unlikely
319 */
320 notrace time_t __vdso_time(time_t *t)
321 {
322 /* This is atomic on x86 so we don't need any locks. */
323 time_t result = READ_ONCE(gtod->wall_time_sec);
325 if (t)
326 *t = result;
327 return result;
328 }
329 time_t time(time_t *t)
330 __attribute__((weak, alias("__vdso_time")));