1 // SPDX-License-Identifier: GPL-2.0
3 /*
4 * Hyper-V specific APIC code.
5 *
6 * Copyright (C) 2018, Microsoft, Inc.
7 *
8 * Author : K. Y. Srinivasan <kys@microsoft.com>
9 *
10 * This program is free software; you can redistribute it and/or modify it
11 * under the terms of the GNU General Public License version 2 as published
12 * by the Free Software Foundation.
13 *
14 * This program is distributed in the hope that it will be useful, but
15 * WITHOUT ANY WARRANTY; without even the implied warranty of
16 * MERCHANTABILITY OR FITNESS FOR A PARTICULAR PURPOSE, GOOD TITLE or
17 * NON INFRINGEMENT. See the GNU General Public License for more
18 * details.
19 *
20 */
22 #include <linux/types.h>
23 #include <linux/version.h>
24 #include <linux/vmalloc.h>
25 #include <linux/mm.h>
26 #include <linux/clockchips.h>
27 #include <linux/hyperv.h>
28 #include <linux/slab.h>
29 #include <linux/cpuhotplug.h>
30 #include <asm/hypervisor.h>
31 #include <asm/mshyperv.h>
32 #include <asm/apic.h>
34 #include <asm/trace/hyperv.h>
36 static struct apic orig_apic;
38 static u64 hv_apic_icr_read(void)
39 {
40 u64 reg_val;
42 rdmsrl(HV_X64_MSR_ICR, reg_val);
43 return reg_val;
44 }
46 static void hv_apic_icr_write(u32 low, u32 id)
47 {
48 u64 reg_val;
50 reg_val = SET_APIC_DEST_FIELD(id);
51 reg_val = reg_val << 32;
52 reg_val |= low;
54 wrmsrl(HV_X64_MSR_ICR, reg_val);
55 }
57 static u32 hv_apic_read(u32 reg)
58 {
59 u32 reg_val, hi;
61 switch (reg) {
62 case APIC_EOI:
63 rdmsr(HV_X64_MSR_EOI, reg_val, hi);
64 return reg_val;
65 case APIC_TASKPRI:
66 rdmsr(HV_X64_MSR_TPR, reg_val, hi);
67 return reg_val;
69 default:
70 return native_apic_mem_read(reg);
71 }
72 }
74 static void hv_apic_write(u32 reg, u32 val)
75 {
76 switch (reg) {
77 case APIC_EOI:
78 wrmsr(HV_X64_MSR_EOI, val, 0);
79 break;
80 case APIC_TASKPRI:
81 wrmsr(HV_X64_MSR_TPR, val, 0);
82 break;
83 default:
84 native_apic_mem_write(reg, val);
85 }
86 }
88 static void hv_apic_eoi_write(u32 reg, u32 val)
89 {
90 wrmsr(HV_X64_MSR_EOI, val, 0);
91 }
93 /*
94 * IPI implementation on Hyper-V.
95 */
96 static bool __send_ipi_mask_ex(const struct cpumask *mask, int vector)
97 {
98 struct hv_send_ipi_ex **arg;
99 struct hv_send_ipi_ex *ipi_arg;
100 unsigned long flags;
101 int nr_bank = 0;
102 int ret = 1;
104 if (!(ms_hyperv.hints & HV_X64_EX_PROCESSOR_MASKS_RECOMMENDED))
105 return false;
107 local_irq_save(flags);
108 arg = (struct hv_send_ipi_ex **)this_cpu_ptr(hyperv_pcpu_input_arg);
110 ipi_arg = *arg;
111 if (unlikely(!ipi_arg))
112 goto ipi_mask_ex_done;
114 ipi_arg->vector = vector;
115 ipi_arg->reserved = 0;
116 ipi_arg->vp_set.valid_bank_mask = 0;
118 if (!cpumask_equal(mask, cpu_present_mask)) {
119 ipi_arg->vp_set.format = HV_GENERIC_SET_SPARSE_4K;
120 nr_bank = cpumask_to_vpset(&(ipi_arg->vp_set), mask);
121 }
122 if (nr_bank < 0)
123 goto ipi_mask_ex_done;
124 if (!nr_bank)
125 ipi_arg->vp_set.format = HV_GENERIC_SET_ALL;
127 ret = hv_do_rep_hypercall(HVCALL_SEND_IPI_EX, 0, nr_bank,
128 ipi_arg, NULL);
130 ipi_mask_ex_done:
131 local_irq_restore(flags);
132 return ((ret == 0) ? true : false);
133 }
135 static bool __send_ipi_mask(const struct cpumask *mask, int vector)
136 {
137 int cur_cpu, vcpu;
138 struct hv_send_ipi ipi_arg;
139 int ret = 1;
141 trace_hyperv_send_ipi_mask(mask, vector);
143 if (cpumask_empty(mask))
144 return true;
146 if (!hv_hypercall_pg)
147 return false;
149 if ((vector < HV_IPI_LOW_VECTOR) || (vector > HV_IPI_HIGH_VECTOR))
150 return false;
152 /*
153 * From the supplied CPU set we need to figure out if we can get away
154 * with cheaper HVCALL_SEND_IPI hypercall. This is possible when the
155 * highest VP number in the set is < 64. As VP numbers are usually in
156 * ascending order and match Linux CPU ids, here is an optimization:
157 * we check the VP number for the highest bit in the supplied set first
158 * so we can quickly find out if using HVCALL_SEND_IPI_EX hypercall is
159 * a must. We will also check all VP numbers when walking the supplied
160 * CPU set to remain correct in all cases.
161 */
162 if (hv_cpu_number_to_vp_number(cpumask_last(mask)) >= 64)
163 goto do_ex_hypercall;
165 ipi_arg.vector = vector;
166 ipi_arg.cpu_mask = 0;
168 for_each_cpu(cur_cpu, mask) {
169 vcpu = hv_cpu_number_to_vp_number(cur_cpu);
170 if (vcpu == VP_INVAL)
171 return false;
173 /*
174 * This particular version of the IPI hypercall can
175 * only target upto 64 CPUs.
176 */
177 if (vcpu >= 64)
178 goto do_ex_hypercall;
180 __set_bit(vcpu, (unsigned long *)&ipi_arg.cpu_mask);
181 }
183 ret = hv_do_fast_hypercall16(HVCALL_SEND_IPI, ipi_arg.vector,
184 ipi_arg.cpu_mask);
185 return ((ret == 0) ? true : false);
187 do_ex_hypercall:
188 return __send_ipi_mask_ex(mask, vector);
189 }
191 static bool __send_ipi_one(int cpu, int vector)
192 {
193 struct cpumask mask = CPU_MASK_NONE;
195 cpumask_set_cpu(cpu, &mask);
196 return __send_ipi_mask(&mask, vector);
197 }
199 static void hv_send_ipi(int cpu, int vector)
200 {
201 if (!__send_ipi_one(cpu, vector))
202 orig_apic.send_IPI(cpu, vector);
203 }
205 static void hv_send_ipi_mask(const struct cpumask *mask, int vector)
206 {
207 if (!__send_ipi_mask(mask, vector))
208 orig_apic.send_IPI_mask(mask, vector);
209 }
211 static void hv_send_ipi_mask_allbutself(const struct cpumask *mask, int vector)
212 {
213 unsigned int this_cpu = smp_processor_id();
214 struct cpumask new_mask;
215 const struct cpumask *local_mask;
217 cpumask_copy(&new_mask, mask);
218 cpumask_clear_cpu(this_cpu, &new_mask);
219 local_mask = &new_mask;
220 if (!__send_ipi_mask(local_mask, vector))
221 orig_apic.send_IPI_mask_allbutself(mask, vector);
222 }
224 static void hv_send_ipi_allbutself(int vector)
225 {
226 hv_send_ipi_mask_allbutself(cpu_online_mask, vector);
227 }
229 static void hv_send_ipi_all(int vector)
230 {
231 if (!__send_ipi_mask(cpu_online_mask, vector))
232 orig_apic.send_IPI_all(vector);
233 }
235 static void hv_send_ipi_self(int vector)
236 {
237 if (!__send_ipi_one(smp_processor_id(), vector))
238 orig_apic.send_IPI_self(vector);
239 }
241 void __init hv_apic_init(void)
242 {
243 if (ms_hyperv.hints & HV_X64_CLUSTER_IPI_RECOMMENDED) {
244 pr_info("Hyper-V: Using IPI hypercalls\n");
245 /*
246 * Set the IPI entry points.
247 */
248 orig_apic = *apic;
250 apic->send_IPI = hv_send_ipi;
251 apic->send_IPI_mask = hv_send_ipi_mask;
252 apic->send_IPI_mask_allbutself = hv_send_ipi_mask_allbutself;
253 apic->send_IPI_allbutself = hv_send_ipi_allbutself;
254 apic->send_IPI_all = hv_send_ipi_all;
255 apic->send_IPI_self = hv_send_ipi_self;
256 }
258 if (ms_hyperv.hints & HV_X64_APIC_ACCESS_RECOMMENDED) {
259 pr_info("Hyper-V: Using MSR based APIC access\n");
260 apic_set_eoi_write(hv_apic_eoi_write);
261 apic->read = hv_apic_read;
262 apic->write = hv_apic_write;
263 apic->icr_write = hv_apic_icr_write;
264 apic->icr_read = hv_apic_icr_read;
265 }
266 }