1 /* SPDX-License-Identifier: GPL-2.0 */
2 #ifndef _ASM_X86_PGTABLE_H
3 #define _ASM_X86_PGTABLE_H
5 #include <linux/mem_encrypt.h>
6 #include <asm/page.h>
7 #include <asm/pgtable_types.h>
9 /*
10 * Macro to mark a page protection value as UC-
11 */
12 #define pgprot_noncached(prot) \
13 ((boot_cpu_data.x86 > 3) \
14 ? (__pgprot(pgprot_val(prot) | \
15 cachemode2protval(_PAGE_CACHE_MODE_UC_MINUS))) \
16 : (prot))
18 /*
19 * Macros to add or remove encryption attribute
20 */
21 #define pgprot_encrypted(prot) __pgprot(__sme_set(pgprot_val(prot)))
22 #define pgprot_decrypted(prot) __pgprot(__sme_clr(pgprot_val(prot)))
24 #ifndef __ASSEMBLY__
25 #include <asm/x86_init.h>
27 extern pgd_t early_top_pgt[PTRS_PER_PGD];
28 int __init __early_make_pgtable(unsigned long address, pmdval_t pmd);
30 void ptdump_walk_pgd_level(struct seq_file *m, pgd_t *pgd);
31 void ptdump_walk_pgd_level_debugfs(struct seq_file *m, pgd_t *pgd, bool user);
32 void ptdump_walk_pgd_level_checkwx(void);
33 void ptdump_walk_user_pgd_level_checkwx(void);
35 #ifdef CONFIG_DEBUG_WX
36 #define debug_checkwx() ptdump_walk_pgd_level_checkwx()
37 #define debug_checkwx_user() ptdump_walk_user_pgd_level_checkwx()
38 #else
39 #define debug_checkwx() do { } while (0)
40 #define debug_checkwx_user() do { } while (0)
41 #endif
43 /*
44 * ZERO_PAGE is a global shared page that is always zero: used
45 * for zero-mapped memory areas etc..
46 */
47 extern unsigned long empty_zero_page[PAGE_SIZE / sizeof(unsigned long)]
48 __visible;
49 #define ZERO_PAGE(vaddr) (virt_to_page(empty_zero_page))
51 extern spinlock_t pgd_lock;
52 extern struct list_head pgd_list;
54 extern struct mm_struct *pgd_page_get_mm(struct page *page);
56 extern pmdval_t early_pmd_flags;
58 #ifdef CONFIG_PARAVIRT
59 #include <asm/paravirt.h>
60 #else /* !CONFIG_PARAVIRT */
61 #define set_pte(ptep, pte) native_set_pte(ptep, pte)
62 #define set_pte_at(mm, addr, ptep, pte) native_set_pte_at(mm, addr, ptep, pte)
64 #define set_pte_atomic(ptep, pte) \
65 native_set_pte_atomic(ptep, pte)
67 #define set_pmd(pmdp, pmd) native_set_pmd(pmdp, pmd)
69 #ifndef __PAGETABLE_P4D_FOLDED
70 #define set_pgd(pgdp, pgd) native_set_pgd(pgdp, pgd)
71 #define pgd_clear(pgd) (pgtable_l5_enabled() ? native_pgd_clear(pgd) : 0)
72 #endif
74 #ifndef set_p4d
75 # define set_p4d(p4dp, p4d) native_set_p4d(p4dp, p4d)
76 #endif
78 #ifndef __PAGETABLE_PUD_FOLDED
79 #define p4d_clear(p4d) native_p4d_clear(p4d)
80 #endif
82 #ifndef set_pud
83 # define set_pud(pudp, pud) native_set_pud(pudp, pud)
84 #endif
86 #ifndef __PAGETABLE_PUD_FOLDED
87 #define pud_clear(pud) native_pud_clear(pud)
88 #endif
90 #define pte_clear(mm, addr, ptep) native_pte_clear(mm, addr, ptep)
91 #define pmd_clear(pmd) native_pmd_clear(pmd)
93 #define pgd_val(x) native_pgd_val(x)
94 #define __pgd(x) native_make_pgd(x)
96 #ifndef __PAGETABLE_P4D_FOLDED
97 #define p4d_val(x) native_p4d_val(x)
98 #define __p4d(x) native_make_p4d(x)
99 #endif
101 #ifndef __PAGETABLE_PUD_FOLDED
102 #define pud_val(x) native_pud_val(x)
103 #define __pud(x) native_make_pud(x)
104 #endif
106 #ifndef __PAGETABLE_PMD_FOLDED
107 #define pmd_val(x) native_pmd_val(x)
108 #define __pmd(x) native_make_pmd(x)
109 #endif
111 #define pte_val(x) native_pte_val(x)
112 #define __pte(x) native_make_pte(x)
114 #define arch_end_context_switch(prev) do {} while(0)
116 #endif /* CONFIG_PARAVIRT */
118 /*
119 * The following only work if pte_present() is true.
120 * Undefined behaviour if not..
121 */
122 static inline int pte_dirty(pte_t pte)
123 {
124 return pte_flags(pte) & _PAGE_DIRTY;
125 }
128 static inline u32 read_pkru(void)
129 {
130 if (boot_cpu_has(X86_FEATURE_OSPKE))
131 return __read_pkru();
132 return 0;
133 }
135 static inline void write_pkru(u32 pkru)
136 {
137 if (boot_cpu_has(X86_FEATURE_OSPKE))
138 __write_pkru(pkru);
139 }
141 static inline int pte_young(pte_t pte)
142 {
143 return pte_flags(pte) & _PAGE_ACCESSED;
144 }
146 static inline int pmd_dirty(pmd_t pmd)
147 {
148 return pmd_flags(pmd) & _PAGE_DIRTY;
149 }
151 static inline int pmd_young(pmd_t pmd)
152 {
153 return pmd_flags(pmd) & _PAGE_ACCESSED;
154 }
156 static inline int pud_dirty(pud_t pud)
157 {
158 return pud_flags(pud) & _PAGE_DIRTY;
159 }
161 static inline int pud_young(pud_t pud)
162 {
163 return pud_flags(pud) & _PAGE_ACCESSED;
164 }
166 static inline int pte_write(pte_t pte)
167 {
168 return pte_flags(pte) & _PAGE_RW;
169 }
171 static inline int pte_huge(pte_t pte)
172 {
173 return pte_flags(pte) & _PAGE_PSE;
174 }
176 static inline int pte_global(pte_t pte)
177 {
178 return pte_flags(pte) & _PAGE_GLOBAL;
179 }
181 static inline int pte_exec(pte_t pte)
182 {
183 return !(pte_flags(pte) & _PAGE_NX);
184 }
186 static inline int pte_special(pte_t pte)
187 {
188 return pte_flags(pte) & _PAGE_SPECIAL;
189 }
191 /* Entries that were set to PROT_NONE are inverted */
193 static inline u64 protnone_mask(u64 val);
195 static inline unsigned long pte_pfn(pte_t pte)
196 {
197 phys_addr_t pfn = pte_val(pte);
198 pfn ^= protnone_mask(pfn);
199 return (pfn & PTE_PFN_MASK) >> PAGE_SHIFT;
200 }
202 static inline unsigned long pmd_pfn(pmd_t pmd)
203 {
204 phys_addr_t pfn = pmd_val(pmd);
205 pfn ^= protnone_mask(pfn);
206 return (pfn & pmd_pfn_mask(pmd)) >> PAGE_SHIFT;
207 }
209 static inline unsigned long pud_pfn(pud_t pud)
210 {
211 phys_addr_t pfn = pud_val(pud);
212 pfn ^= protnone_mask(pfn);
213 return (pfn & pud_pfn_mask(pud)) >> PAGE_SHIFT;
214 }
216 static inline unsigned long p4d_pfn(p4d_t p4d)
217 {
218 return (p4d_val(p4d) & p4d_pfn_mask(p4d)) >> PAGE_SHIFT;
219 }
221 static inline unsigned long pgd_pfn(pgd_t pgd)
222 {
223 return (pgd_val(pgd) & PTE_PFN_MASK) >> PAGE_SHIFT;
224 }
226 static inline int p4d_large(p4d_t p4d)
227 {
228 /* No 512 GiB pages yet */
229 return 0;
230 }
232 #define pte_page(pte) pfn_to_page(pte_pfn(pte))
234 static inline int pmd_large(pmd_t pte)
235 {
236 return pmd_flags(pte) & _PAGE_PSE;
237 }
239 #ifdef CONFIG_TRANSPARENT_HUGEPAGE
240 static inline int pmd_trans_huge(pmd_t pmd)
241 {
242 return (pmd_val(pmd) & (_PAGE_PSE|_PAGE_DEVMAP)) == _PAGE_PSE;
243 }
245 #ifdef CONFIG_HAVE_ARCH_TRANSPARENT_HUGEPAGE_PUD
246 static inline int pud_trans_huge(pud_t pud)
247 {
248 return (pud_val(pud) & (_PAGE_PSE|_PAGE_DEVMAP)) == _PAGE_PSE;
249 }
250 #endif
252 #define has_transparent_hugepage has_transparent_hugepage
253 static inline int has_transparent_hugepage(void)
254 {
255 return boot_cpu_has(X86_FEATURE_PSE);
256 }
258 #ifdef __HAVE_ARCH_PTE_DEVMAP
259 static inline int pmd_devmap(pmd_t pmd)
260 {
261 return !!(pmd_val(pmd) & _PAGE_DEVMAP);
262 }
264 #ifdef CONFIG_HAVE_ARCH_TRANSPARENT_HUGEPAGE_PUD
265 static inline int pud_devmap(pud_t pud)
266 {
267 return !!(pud_val(pud) & _PAGE_DEVMAP);
268 }
269 #else
270 static inline int pud_devmap(pud_t pud)
271 {
272 return 0;
273 }
274 #endif
276 static inline int pgd_devmap(pgd_t pgd)
277 {
278 return 0;
279 }
280 #endif
281 #endif /* CONFIG_TRANSPARENT_HUGEPAGE */
283 static inline pte_t pte_set_flags(pte_t pte, pteval_t set)
284 {
285 pteval_t v = native_pte_val(pte);
287 return native_make_pte(v | set);
288 }
290 static inline pte_t pte_clear_flags(pte_t pte, pteval_t clear)
291 {
292 pteval_t v = native_pte_val(pte);
294 return native_make_pte(v & ~clear);
295 }
297 static inline pte_t pte_mkclean(pte_t pte)
298 {
299 return pte_clear_flags(pte, _PAGE_DIRTY);
300 }
302 static inline pte_t pte_mkold(pte_t pte)
303 {
304 return pte_clear_flags(pte, _PAGE_ACCESSED);
305 }
307 static inline pte_t pte_wrprotect(pte_t pte)
308 {
309 return pte_clear_flags(pte, _PAGE_RW);
310 }
312 static inline pte_t pte_mkexec(pte_t pte)
313 {
314 return pte_clear_flags(pte, _PAGE_NX);
315 }
317 static inline pte_t pte_mkdirty(pte_t pte)
318 {
319 return pte_set_flags(pte, _PAGE_DIRTY | _PAGE_SOFT_DIRTY);
320 }
322 static inline pte_t pte_mkyoung(pte_t pte)
323 {
324 return pte_set_flags(pte, _PAGE_ACCESSED);
325 }
327 static inline pte_t pte_mkwrite(pte_t pte)
328 {
329 return pte_set_flags(pte, _PAGE_RW);
330 }
332 static inline pte_t pte_mkhuge(pte_t pte)
333 {
334 return pte_set_flags(pte, _PAGE_PSE);
335 }
337 static inline pte_t pte_clrhuge(pte_t pte)
338 {
339 return pte_clear_flags(pte, _PAGE_PSE);
340 }
342 static inline pte_t pte_mkglobal(pte_t pte)
343 {
344 return pte_set_flags(pte, _PAGE_GLOBAL);
345 }
347 static inline pte_t pte_clrglobal(pte_t pte)
348 {
349 return pte_clear_flags(pte, _PAGE_GLOBAL);
350 }
352 static inline pte_t pte_mkspecial(pte_t pte)
353 {
354 return pte_set_flags(pte, _PAGE_SPECIAL);
355 }
357 static inline pte_t pte_mkdevmap(pte_t pte)
358 {
359 return pte_set_flags(pte, _PAGE_SPECIAL|_PAGE_DEVMAP);
360 }
362 static inline pmd_t pmd_set_flags(pmd_t pmd, pmdval_t set)
363 {
364 pmdval_t v = native_pmd_val(pmd);
366 return native_make_pmd(v | set);
367 }
369 static inline pmd_t pmd_clear_flags(pmd_t pmd, pmdval_t clear)
370 {
371 pmdval_t v = native_pmd_val(pmd);
373 return native_make_pmd(v & ~clear);
374 }
376 static inline pmd_t pmd_mkold(pmd_t pmd)
377 {
378 return pmd_clear_flags(pmd, _PAGE_ACCESSED);
379 }
381 static inline pmd_t pmd_mkclean(pmd_t pmd)
382 {
383 return pmd_clear_flags(pmd, _PAGE_DIRTY);
384 }
386 static inline pmd_t pmd_wrprotect(pmd_t pmd)
387 {
388 return pmd_clear_flags(pmd, _PAGE_RW);
389 }
391 static inline pmd_t pmd_mkdirty(pmd_t pmd)
392 {
393 return pmd_set_flags(pmd, _PAGE_DIRTY | _PAGE_SOFT_DIRTY);
394 }
396 static inline pmd_t pmd_mkdevmap(pmd_t pmd)
397 {
398 return pmd_set_flags(pmd, _PAGE_DEVMAP);
399 }
401 static inline pmd_t pmd_mkhuge(pmd_t pmd)
402 {
403 return pmd_set_flags(pmd, _PAGE_PSE);
404 }
406 static inline pmd_t pmd_mkyoung(pmd_t pmd)
407 {
408 return pmd_set_flags(pmd, _PAGE_ACCESSED);
409 }
411 static inline pmd_t pmd_mkwrite(pmd_t pmd)
412 {
413 return pmd_set_flags(pmd, _PAGE_RW);
414 }
416 static inline pud_t pud_set_flags(pud_t pud, pudval_t set)
417 {
418 pudval_t v = native_pud_val(pud);
420 return native_make_pud(v | set);
421 }
423 static inline pud_t pud_clear_flags(pud_t pud, pudval_t clear)
424 {
425 pudval_t v = native_pud_val(pud);
427 return native_make_pud(v & ~clear);
428 }
430 static inline pud_t pud_mkold(pud_t pud)
431 {
432 return pud_clear_flags(pud, _PAGE_ACCESSED);
433 }
435 static inline pud_t pud_mkclean(pud_t pud)
436 {
437 return pud_clear_flags(pud, _PAGE_DIRTY);
438 }
440 static inline pud_t pud_wrprotect(pud_t pud)
441 {
442 return pud_clear_flags(pud, _PAGE_RW);
443 }
445 static inline pud_t pud_mkdirty(pud_t pud)
446 {
447 return pud_set_flags(pud, _PAGE_DIRTY | _PAGE_SOFT_DIRTY);
448 }
450 static inline pud_t pud_mkdevmap(pud_t pud)
451 {
452 return pud_set_flags(pud, _PAGE_DEVMAP);
453 }
455 static inline pud_t pud_mkhuge(pud_t pud)
456 {
457 return pud_set_flags(pud, _PAGE_PSE);
458 }
460 static inline pud_t pud_mkyoung(pud_t pud)
461 {
462 return pud_set_flags(pud, _PAGE_ACCESSED);
463 }
465 static inline pud_t pud_mkwrite(pud_t pud)
466 {
467 return pud_set_flags(pud, _PAGE_RW);
468 }
470 #ifdef CONFIG_HAVE_ARCH_SOFT_DIRTY
471 static inline int pte_soft_dirty(pte_t pte)
472 {
473 return pte_flags(pte) & _PAGE_SOFT_DIRTY;
474 }
476 static inline int pmd_soft_dirty(pmd_t pmd)
477 {
478 return pmd_flags(pmd) & _PAGE_SOFT_DIRTY;
479 }
481 static inline int pud_soft_dirty(pud_t pud)
482 {
483 return pud_flags(pud) & _PAGE_SOFT_DIRTY;
484 }
486 static inline pte_t pte_mksoft_dirty(pte_t pte)
487 {
488 return pte_set_flags(pte, _PAGE_SOFT_DIRTY);
489 }
491 static inline pmd_t pmd_mksoft_dirty(pmd_t pmd)
492 {
493 return pmd_set_flags(pmd, _PAGE_SOFT_DIRTY);
494 }
496 static inline pud_t pud_mksoft_dirty(pud_t pud)
497 {
498 return pud_set_flags(pud, _PAGE_SOFT_DIRTY);
499 }
501 static inline pte_t pte_clear_soft_dirty(pte_t pte)
502 {
503 return pte_clear_flags(pte, _PAGE_SOFT_DIRTY);
504 }
506 static inline pmd_t pmd_clear_soft_dirty(pmd_t pmd)
507 {
508 return pmd_clear_flags(pmd, _PAGE_SOFT_DIRTY);
509 }
511 static inline pud_t pud_clear_soft_dirty(pud_t pud)
512 {
513 return pud_clear_flags(pud, _PAGE_SOFT_DIRTY);
514 }
516 #endif /* CONFIG_HAVE_ARCH_SOFT_DIRTY */
518 /*
519 * Mask out unsupported bits in a present pgprot. Non-present pgprots
520 * can use those bits for other purposes, so leave them be.
521 */
522 static inline pgprotval_t massage_pgprot(pgprot_t pgprot)
523 {
524 pgprotval_t protval = pgprot_val(pgprot);
526 if (protval & _PAGE_PRESENT)
527 protval &= __supported_pte_mask;
529 return protval;
530 }
532 static inline pgprotval_t check_pgprot(pgprot_t pgprot)
533 {
534 pgprotval_t massaged_val = massage_pgprot(pgprot);
536 /* mmdebug.h can not be included here because of dependencies */
537 #ifdef CONFIG_DEBUG_VM
538 WARN_ONCE(pgprot_val(pgprot) != massaged_val,
539 "attempted to set unsupported pgprot: %016llx "
540 "bits: %016llx supported: %016llx\n",
541 (u64)pgprot_val(pgprot),
542 (u64)pgprot_val(pgprot) ^ massaged_val,
543 (u64)__supported_pte_mask);
544 #endif
546 return massaged_val;
547 }
549 static inline pte_t pfn_pte(unsigned long page_nr, pgprot_t pgprot)
550 {
551 phys_addr_t pfn = (phys_addr_t)page_nr << PAGE_SHIFT;
552 pfn ^= protnone_mask(pgprot_val(pgprot));
553 pfn &= PTE_PFN_MASK;
554 return __pte(pfn | check_pgprot(pgprot));
555 }
557 static inline pmd_t pfn_pmd(unsigned long page_nr, pgprot_t pgprot)
558 {
559 phys_addr_t pfn = (phys_addr_t)page_nr << PAGE_SHIFT;
560 pfn ^= protnone_mask(pgprot_val(pgprot));
561 pfn &= PHYSICAL_PMD_PAGE_MASK;
562 return __pmd(pfn | check_pgprot(pgprot));
563 }
565 static inline pud_t pfn_pud(unsigned long page_nr, pgprot_t pgprot)
566 {
567 phys_addr_t pfn = (phys_addr_t)page_nr << PAGE_SHIFT;
568 pfn ^= protnone_mask(pgprot_val(pgprot));
569 pfn &= PHYSICAL_PUD_PAGE_MASK;
570 return __pud(pfn | check_pgprot(pgprot));
571 }
573 static inline pmd_t pmd_mknotpresent(pmd_t pmd)
574 {
575 return pfn_pmd(pmd_pfn(pmd),
576 __pgprot(pmd_flags(pmd) & ~(_PAGE_PRESENT|_PAGE_PROTNONE)));
577 }
579 static inline pud_t pud_mknotpresent(pud_t pud)
580 {
581 return pfn_pud(pud_pfn(pud),
582 __pgprot(pud_flags(pud) & ~(_PAGE_PRESENT|_PAGE_PROTNONE)));
583 }
585 static inline u64 flip_protnone_guard(u64 oldval, u64 val, u64 mask);
587 static inline pte_t pte_modify(pte_t pte, pgprot_t newprot)
588 {
589 pteval_t val = pte_val(pte), oldval = val;
591 /*
592 * Chop off the NX bit (if present), and add the NX portion of
593 * the newprot (if present):
594 */
595 val &= _PAGE_CHG_MASK;
596 val |= check_pgprot(newprot) & ~_PAGE_CHG_MASK;
597 val = flip_protnone_guard(oldval, val, PTE_PFN_MASK);
598 return __pte(val);
599 }
601 static inline pmd_t pmd_modify(pmd_t pmd, pgprot_t newprot)
602 {
603 pmdval_t val = pmd_val(pmd), oldval = val;
605 val &= _HPAGE_CHG_MASK;
606 val |= check_pgprot(newprot) & ~_HPAGE_CHG_MASK;
607 val = flip_protnone_guard(oldval, val, PHYSICAL_PMD_PAGE_MASK);
608 return __pmd(val);
609 }
611 /* mprotect needs to preserve PAT bits when updating vm_page_prot */
612 #define pgprot_modify pgprot_modify
613 static inline pgprot_t pgprot_modify(pgprot_t oldprot, pgprot_t newprot)
614 {
615 pgprotval_t preservebits = pgprot_val(oldprot) & _PAGE_CHG_MASK;
616 pgprotval_t addbits = pgprot_val(newprot);
617 return __pgprot(preservebits | addbits);
618 }
620 #define pte_pgprot(x) __pgprot(pte_flags(x))
621 #define pmd_pgprot(x) __pgprot(pmd_flags(x))
622 #define pud_pgprot(x) __pgprot(pud_flags(x))
623 #define p4d_pgprot(x) __pgprot(p4d_flags(x))
625 #define canon_pgprot(p) __pgprot(massage_pgprot(p))
627 static inline pgprot_t arch_filter_pgprot(pgprot_t prot)
628 {
629 return canon_pgprot(prot);
630 }
632 static inline int is_new_memtype_allowed(u64 paddr, unsigned long size,
633 enum page_cache_mode pcm,
634 enum page_cache_mode new_pcm)
635 {
636 /*
637 * PAT type is always WB for untracked ranges, so no need to check.
638 */
639 if (x86_platform.is_untracked_pat_range(paddr, paddr + size))
640 return 1;
642 /*
643 * Certain new memtypes are not allowed with certain
644 * requested memtype:
645 * - request is uncached, return cannot be write-back
646 * - request is write-combine, return cannot be write-back
647 * - request is write-through, return cannot be write-back
648 * - request is write-through, return cannot be write-combine
649 */
650 if ((pcm == _PAGE_CACHE_MODE_UC_MINUS &&
651 new_pcm == _PAGE_CACHE_MODE_WB) ||
652 (pcm == _PAGE_CACHE_MODE_WC &&
653 new_pcm == _PAGE_CACHE_MODE_WB) ||
654 (pcm == _PAGE_CACHE_MODE_WT &&
655 new_pcm == _PAGE_CACHE_MODE_WB) ||
656 (pcm == _PAGE_CACHE_MODE_WT &&
657 new_pcm == _PAGE_CACHE_MODE_WC)) {
658 return 0;
659 }
661 return 1;
662 }
664 pmd_t *populate_extra_pmd(unsigned long vaddr);
665 pte_t *populate_extra_pte(unsigned long vaddr);
667 #ifdef CONFIG_PAGE_TABLE_ISOLATION
668 pgd_t __pti_set_user_pgtbl(pgd_t *pgdp, pgd_t pgd);
670 /*
671 * Take a PGD location (pgdp) and a pgd value that needs to be set there.
672 * Populates the user and returns the resulting PGD that must be set in
673 * the kernel copy of the page tables.
674 */
675 static inline pgd_t pti_set_user_pgtbl(pgd_t *pgdp, pgd_t pgd)
676 {
677 if (!static_cpu_has(X86_FEATURE_PTI))
678 return pgd;
679 return __pti_set_user_pgtbl(pgdp, pgd);
680 }
681 #else /* CONFIG_PAGE_TABLE_ISOLATION */
682 static inline pgd_t pti_set_user_pgtbl(pgd_t *pgdp, pgd_t pgd)
683 {
684 return pgd;
685 }
686 #endif /* CONFIG_PAGE_TABLE_ISOLATION */
688 #endif /* __ASSEMBLY__ */
691 #ifdef CONFIG_X86_32
692 # include <asm/pgtable_32.h>
693 #else
694 # include <asm/pgtable_64.h>
695 #endif
697 #ifndef __ASSEMBLY__
698 #include <linux/mm_types.h>
699 #include <linux/mmdebug.h>
700 #include <linux/log2.h>
701 #include <asm/fixmap.h>
703 static inline int pte_none(pte_t pte)
704 {
705 return !(pte.pte & ~(_PAGE_KNL_ERRATUM_MASK));
706 }
708 #define __HAVE_ARCH_PTE_SAME
709 static inline int pte_same(pte_t a, pte_t b)
710 {
711 return a.pte == b.pte;
712 }
714 static inline int pte_present(pte_t a)
715 {
716 return pte_flags(a) & (_PAGE_PRESENT | _PAGE_PROTNONE);
717 }
719 #ifdef __HAVE_ARCH_PTE_DEVMAP
720 static inline int pte_devmap(pte_t a)
721 {
722 return (pte_flags(a) & _PAGE_DEVMAP) == _PAGE_DEVMAP;
723 }
724 #endif
726 #define pte_accessible pte_accessible
727 static inline bool pte_accessible(struct mm_struct *mm, pte_t a)
728 {
729 if (pte_flags(a) & _PAGE_PRESENT)
730 return true;
732 if ((pte_flags(a) & _PAGE_PROTNONE) &&
733 mm_tlb_flush_pending(mm))
734 return true;
736 return false;
737 }
739 static inline int pmd_present(pmd_t pmd)
740 {
741 /*
742 * Checking for _PAGE_PSE is needed too because
743 * split_huge_page will temporarily clear the present bit (but
744 * the _PAGE_PSE flag will remain set at all times while the
745 * _PAGE_PRESENT bit is clear).
746 */
747 return pmd_flags(pmd) & (_PAGE_PRESENT | _PAGE_PROTNONE | _PAGE_PSE);
748 }
750 #ifdef CONFIG_NUMA_BALANCING
751 /*
752 * These work without NUMA balancing but the kernel does not care. See the
753 * comment in include/asm-generic/pgtable.h
754 */
755 static inline int pte_protnone(pte_t pte)
756 {
757 return (pte_flags(pte) & (_PAGE_PROTNONE | _PAGE_PRESENT))
758 == _PAGE_PROTNONE;
759 }
761 static inline int pmd_protnone(pmd_t pmd)
762 {
763 return (pmd_flags(pmd) & (_PAGE_PROTNONE | _PAGE_PRESENT))
764 == _PAGE_PROTNONE;
765 }
766 #endif /* CONFIG_NUMA_BALANCING */
768 static inline int pmd_none(pmd_t pmd)
769 {
770 /* Only check low word on 32-bit platforms, since it might be
771 out of sync with upper half. */
772 unsigned long val = native_pmd_val(pmd);
773 return (val & ~_PAGE_KNL_ERRATUM_MASK) == 0;
774 }
776 static inline unsigned long pmd_page_vaddr(pmd_t pmd)
777 {
778 return (unsigned long)__va(pmd_val(pmd) & pmd_pfn_mask(pmd));
779 }
781 /*
782 * Currently stuck as a macro due to indirect forward reference to
783 * linux/mmzone.h's __section_mem_map_addr() definition:
784 */
785 #define pmd_page(pmd) pfn_to_page(pmd_pfn(pmd))
787 /*
788 * the pmd page can be thought of an array like this: pmd_t[PTRS_PER_PMD]
789 *
790 * this macro returns the index of the entry in the pmd page which would
791 * control the given virtual address
792 */
793 static inline unsigned long pmd_index(unsigned long address)
794 {
795 return (address >> PMD_SHIFT) & (PTRS_PER_PMD - 1);
796 }
798 /*
799 * Conversion functions: convert a page and protection to a page entry,
800 * and a page entry and page directory to the page they refer to.
801 *
802 * (Currently stuck as a macro because of indirect forward reference
803 * to linux/mm.h:page_to_nid())
804 */
805 #define mk_pte(page, pgprot) pfn_pte(page_to_pfn(page), (pgprot))
807 /*
808 * the pte page can be thought of an array like this: pte_t[PTRS_PER_PTE]
809 *
810 * this function returns the index of the entry in the pte page which would
811 * control the given virtual address
812 */
813 static inline unsigned long pte_index(unsigned long address)
814 {
815 return (address >> PAGE_SHIFT) & (PTRS_PER_PTE - 1);
816 }
818 static inline pte_t *pte_offset_kernel(pmd_t *pmd, unsigned long address)
819 {
820 return (pte_t *)pmd_page_vaddr(*pmd) + pte_index(address);
821 }
823 static inline int pmd_bad(pmd_t pmd)
824 {
825 return (pmd_flags(pmd) & ~_PAGE_USER) != _KERNPG_TABLE;
826 }
828 static inline unsigned long pages_to_mb(unsigned long npg)
829 {
830 return npg >> (20 - PAGE_SHIFT);
831 }
833 #if CONFIG_PGTABLE_LEVELS > 2
834 static inline int pud_none(pud_t pud)
835 {
836 return (native_pud_val(pud) & ~(_PAGE_KNL_ERRATUM_MASK)) == 0;
837 }
839 static inline int pud_present(pud_t pud)
840 {
841 return pud_flags(pud) & _PAGE_PRESENT;
842 }
844 static inline unsigned long pud_page_vaddr(pud_t pud)
845 {
846 return (unsigned long)__va(pud_val(pud) & pud_pfn_mask(pud));
847 }
849 /*
850 * Currently stuck as a macro due to indirect forward reference to
851 * linux/mmzone.h's __section_mem_map_addr() definition:
852 */
853 #define pud_page(pud) pfn_to_page(pud_pfn(pud))
855 /* Find an entry in the second-level page table.. */
856 static inline pmd_t *pmd_offset(pud_t *pud, unsigned long address)
857 {
858 return (pmd_t *)pud_page_vaddr(*pud) + pmd_index(address);
859 }
861 static inline int pud_large(pud_t pud)
862 {
863 return (pud_val(pud) & (_PAGE_PSE | _PAGE_PRESENT)) ==
864 (_PAGE_PSE | _PAGE_PRESENT);
865 }
867 static inline int pud_bad(pud_t pud)
868 {
869 return (pud_flags(pud) & ~(_KERNPG_TABLE | _PAGE_USER)) != 0;
870 }
871 #else
872 static inline int pud_large(pud_t pud)
873 {
874 return 0;
875 }
876 #endif /* CONFIG_PGTABLE_LEVELS > 2 */
878 static inline unsigned long pud_index(unsigned long address)
879 {
880 return (address >> PUD_SHIFT) & (PTRS_PER_PUD - 1);
881 }
883 #if CONFIG_PGTABLE_LEVELS > 3
884 static inline int p4d_none(p4d_t p4d)
885 {
886 return (native_p4d_val(p4d) & ~(_PAGE_KNL_ERRATUM_MASK)) == 0;
887 }
889 static inline int p4d_present(p4d_t p4d)
890 {
891 return p4d_flags(p4d) & _PAGE_PRESENT;
892 }
894 static inline unsigned long p4d_page_vaddr(p4d_t p4d)
895 {
896 return (unsigned long)__va(p4d_val(p4d) & p4d_pfn_mask(p4d));
897 }
899 /*
900 * Currently stuck as a macro due to indirect forward reference to
901 * linux/mmzone.h's __section_mem_map_addr() definition:
902 */
903 #define p4d_page(p4d) pfn_to_page(p4d_pfn(p4d))
905 /* Find an entry in the third-level page table.. */
906 static inline pud_t *pud_offset(p4d_t *p4d, unsigned long address)
907 {
908 return (pud_t *)p4d_page_vaddr(*p4d) + pud_index(address);
909 }
911 static inline int p4d_bad(p4d_t p4d)
912 {
913 unsigned long ignore_flags = _KERNPG_TABLE | _PAGE_USER;
915 if (IS_ENABLED(CONFIG_PAGE_TABLE_ISOLATION))
916 ignore_flags |= _PAGE_NX;
918 return (p4d_flags(p4d) & ~ignore_flags) != 0;
919 }
920 #endif /* CONFIG_PGTABLE_LEVELS > 3 */
922 static inline unsigned long p4d_index(unsigned long address)
923 {
924 return (address >> P4D_SHIFT) & (PTRS_PER_P4D - 1);
925 }
927 #if CONFIG_PGTABLE_LEVELS > 4
928 static inline int pgd_present(pgd_t pgd)
929 {
930 if (!pgtable_l5_enabled())
931 return 1;
932 return pgd_flags(pgd) & _PAGE_PRESENT;
933 }
935 static inline unsigned long pgd_page_vaddr(pgd_t pgd)
936 {
937 return (unsigned long)__va((unsigned long)pgd_val(pgd) & PTE_PFN_MASK);
938 }
940 /*
941 * Currently stuck as a macro due to indirect forward reference to
942 * linux/mmzone.h's __section_mem_map_addr() definition:
943 */
944 #define pgd_page(pgd) pfn_to_page(pgd_pfn(pgd))
946 /* to find an entry in a page-table-directory. */
947 static inline p4d_t *p4d_offset(pgd_t *pgd, unsigned long address)
948 {
949 if (!pgtable_l5_enabled())
950 return (p4d_t *)pgd;
951 return (p4d_t *)pgd_page_vaddr(*pgd) + p4d_index(address);
952 }
954 static inline int pgd_bad(pgd_t pgd)
955 {
956 unsigned long ignore_flags = _PAGE_USER;
958 if (!pgtable_l5_enabled())
959 return 0;
961 if (IS_ENABLED(CONFIG_PAGE_TABLE_ISOLATION))
962 ignore_flags |= _PAGE_NX;
964 return (pgd_flags(pgd) & ~ignore_flags) != _KERNPG_TABLE;
965 }
967 static inline int pgd_none(pgd_t pgd)
968 {
969 if (!pgtable_l5_enabled())
970 return 0;
971 /*
972 * There is no need to do a workaround for the KNL stray
973 * A/D bit erratum here. PGDs only point to page tables
974 * except on 32-bit non-PAE which is not supported on
975 * KNL.
976 */
977 return !native_pgd_val(pgd);
978 }
979 #endif /* CONFIG_PGTABLE_LEVELS > 4 */
981 #endif /* __ASSEMBLY__ */
983 /*
984 * the pgd page can be thought of an array like this: pgd_t[PTRS_PER_PGD]
985 *
986 * this macro returns the index of the entry in the pgd page which would
987 * control the given virtual address
988 */
989 #define pgd_index(address) (((address) >> PGDIR_SHIFT) & (PTRS_PER_PGD - 1))
991 /*
992 * pgd_offset() returns a (pgd_t *)
993 * pgd_index() is used get the offset into the pgd page's array of pgd_t's;
994 */
995 #define pgd_offset_pgd(pgd, address) (pgd + pgd_index((address)))
996 /*
997 * a shortcut to get a pgd_t in a given mm
998 */
999 #define pgd_offset(mm, address) pgd_offset_pgd((mm)->pgd, (address))
1000 /*
1001 * a shortcut which implies the use of the kernel's pgd, instead
1002 * of a process's
1003 */
1004 #define pgd_offset_k(address) pgd_offset(&init_mm, (address))
1007 #define KERNEL_PGD_BOUNDARY pgd_index(PAGE_OFFSET)
1008 #define KERNEL_PGD_PTRS (PTRS_PER_PGD - KERNEL_PGD_BOUNDARY)
1010 #ifndef __ASSEMBLY__
1012 extern int direct_gbpages;
1013 void init_mem_mapping(void);
1014 void early_alloc_pgt_buf(void);
1015 extern void memblock_find_dma_reserve(void);
1017 #ifdef CONFIG_X86_64
1018 /* Realmode trampoline initialization. */
1019 extern pgd_t trampoline_pgd_entry;
1020 static inline void __meminit init_trampoline_default(void)
1021 {
1022 /* Default trampoline pgd value */
1023 trampoline_pgd_entry = init_top_pgt[pgd_index(__PAGE_OFFSET)];
1024 }
1025 # ifdef CONFIG_RANDOMIZE_MEMORY
1026 void __meminit init_trampoline(void);
1027 # else
1028 # define init_trampoline init_trampoline_default
1029 # endif
1030 #else
1031 static inline void init_trampoline(void) { }
1032 #endif
1034 /* local pte updates need not use xchg for locking */
1035 static inline pte_t native_local_ptep_get_and_clear(pte_t *ptep)
1036 {
1037 pte_t res = *ptep;
1039 /* Pure native function needs no input for mm, addr */
1040 native_pte_clear(NULL, 0, ptep);
1041 return res;
1042 }
1044 static inline pmd_t native_local_pmdp_get_and_clear(pmd_t *pmdp)
1045 {
1046 pmd_t res = *pmdp;
1048 native_pmd_clear(pmdp);
1049 return res;
1050 }
1052 static inline pud_t native_local_pudp_get_and_clear(pud_t *pudp)
1053 {
1054 pud_t res = *pudp;
1056 native_pud_clear(pudp);
1057 return res;
1058 }
1060 static inline void native_set_pte_at(struct mm_struct *mm, unsigned long addr,
1061 pte_t *ptep , pte_t pte)
1062 {
1063 native_set_pte(ptep, pte);
1064 }
1066 static inline void set_pmd_at(struct mm_struct *mm, unsigned long addr,
1067 pmd_t *pmdp, pmd_t pmd)
1068 {
1069 native_set_pmd(pmdp, pmd);
1070 }
1072 static inline void set_pud_at(struct mm_struct *mm, unsigned long addr,
1073 pud_t *pudp, pud_t pud)
1074 {
1075 native_set_pud(pudp, pud);
1076 }
1078 /*
1079 * We only update the dirty/accessed state if we set
1080 * the dirty bit by hand in the kernel, since the hardware
1081 * will do the accessed bit for us, and we don't want to
1082 * race with other CPU's that might be updating the dirty
1083 * bit at the same time.
1084 */
1085 struct vm_area_struct;
1087 #define __HAVE_ARCH_PTEP_SET_ACCESS_FLAGS
1088 extern int ptep_set_access_flags(struct vm_area_struct *vma,
1089 unsigned long address, pte_t *ptep,
1090 pte_t entry, int dirty);
1092 #define __HAVE_ARCH_PTEP_TEST_AND_CLEAR_YOUNG
1093 extern int ptep_test_and_clear_young(struct vm_area_struct *vma,
1094 unsigned long addr, pte_t *ptep);
1096 #define __HAVE_ARCH_PTEP_CLEAR_YOUNG_FLUSH
1097 extern int ptep_clear_flush_young(struct vm_area_struct *vma,
1098 unsigned long address, pte_t *ptep);
1100 #define __HAVE_ARCH_PTEP_GET_AND_CLEAR
1101 static inline pte_t ptep_get_and_clear(struct mm_struct *mm, unsigned long addr,
1102 pte_t *ptep)
1103 {
1104 pte_t pte = native_ptep_get_and_clear(ptep);
1105 return pte;
1106 }
1108 #define __HAVE_ARCH_PTEP_GET_AND_CLEAR_FULL
1109 static inline pte_t ptep_get_and_clear_full(struct mm_struct *mm,
1110 unsigned long addr, pte_t *ptep,
1111 int full)
1112 {
1113 pte_t pte;
1114 if (full) {
1115 /*
1116 * Full address destruction in progress; paravirt does not
1117 * care about updates and native needs no locking
1118 */
1119 pte = native_local_ptep_get_and_clear(ptep);
1120 } else {
1121 pte = ptep_get_and_clear(mm, addr, ptep);
1122 }
1123 return pte;
1124 }
1126 #define __HAVE_ARCH_PTEP_SET_WRPROTECT
1127 static inline void ptep_set_wrprotect(struct mm_struct *mm,
1128 unsigned long addr, pte_t *ptep)
1129 {
1130 clear_bit(_PAGE_BIT_RW, (unsigned long *)&ptep->pte);
1131 }
1133 #define flush_tlb_fix_spurious_fault(vma, address) do { } while (0)
1135 #define mk_pmd(page, pgprot) pfn_pmd(page_to_pfn(page), (pgprot))
1137 #define __HAVE_ARCH_PMDP_SET_ACCESS_FLAGS
1138 extern int pmdp_set_access_flags(struct vm_area_struct *vma,
1139 unsigned long address, pmd_t *pmdp,
1140 pmd_t entry, int dirty);
1141 extern int pudp_set_access_flags(struct vm_area_struct *vma,
1142 unsigned long address, pud_t *pudp,
1143 pud_t entry, int dirty);
1145 #define __HAVE_ARCH_PMDP_TEST_AND_CLEAR_YOUNG
1146 extern int pmdp_test_and_clear_young(struct vm_area_struct *vma,
1147 unsigned long addr, pmd_t *pmdp);
1148 extern int pudp_test_and_clear_young(struct vm_area_struct *vma,
1149 unsigned long addr, pud_t *pudp);
1151 #define __HAVE_ARCH_PMDP_CLEAR_YOUNG_FLUSH
1152 extern int pmdp_clear_flush_young(struct vm_area_struct *vma,
1153 unsigned long address, pmd_t *pmdp);
1156 #define pmd_write pmd_write
1157 static inline int pmd_write(pmd_t pmd)
1158 {
1159 return pmd_flags(pmd) & _PAGE_RW;
1160 }
1162 #define __HAVE_ARCH_PMDP_HUGE_GET_AND_CLEAR
1163 static inline pmd_t pmdp_huge_get_and_clear(struct mm_struct *mm, unsigned long addr,
1164 pmd_t *pmdp)
1165 {
1166 return native_pmdp_get_and_clear(pmdp);
1167 }
1169 #define __HAVE_ARCH_PUDP_HUGE_GET_AND_CLEAR
1170 static inline pud_t pudp_huge_get_and_clear(struct mm_struct *mm,
1171 unsigned long addr, pud_t *pudp)
1172 {
1173 return native_pudp_get_and_clear(pudp);
1174 }
1176 #define __HAVE_ARCH_PMDP_SET_WRPROTECT
1177 static inline void pmdp_set_wrprotect(struct mm_struct *mm,
1178 unsigned long addr, pmd_t *pmdp)
1179 {
1180 clear_bit(_PAGE_BIT_RW, (unsigned long *)pmdp);
1181 }
1183 #define pud_write pud_write
1184 static inline int pud_write(pud_t pud)
1185 {
1186 return pud_flags(pud) & _PAGE_RW;
1187 }
1189 #ifndef pmdp_establish
1190 #define pmdp_establish pmdp_establish
1191 static inline pmd_t pmdp_establish(struct vm_area_struct *vma,
1192 unsigned long address, pmd_t *pmdp, pmd_t pmd)
1193 {
1194 if (IS_ENABLED(CONFIG_SMP)) {
1195 return xchg(pmdp, pmd);
1196 } else {
1197 pmd_t old = *pmdp;
1198 WRITE_ONCE(*pmdp, pmd);
1199 return old;
1200 }
1201 }
1202 #endif
1203 /*
1204 * Page table pages are page-aligned. The lower half of the top
1205 * level is used for userspace and the top half for the kernel.
1206 *
1207 * Returns true for parts of the PGD that map userspace and
1208 * false for the parts that map the kernel.
1209 */
1210 static inline bool pgdp_maps_userspace(void *__ptr)
1211 {
1212 unsigned long ptr = (unsigned long)__ptr;
1214 return (((ptr & ~PAGE_MASK) / sizeof(pgd_t)) < PGD_KERNEL_START);
1215 }
1217 static inline int pgd_large(pgd_t pgd) { return 0; }
1219 #ifdef CONFIG_PAGE_TABLE_ISOLATION
1220 /*
1221 * All top-level PAGE_TABLE_ISOLATION page tables are order-1 pages
1222 * (8k-aligned and 8k in size). The kernel one is at the beginning 4k and
1223 * the user one is in the last 4k. To switch between them, you
1224 * just need to flip the 12th bit in their addresses.
1225 */
1226 #define PTI_PGTABLE_SWITCH_BIT PAGE_SHIFT
1228 /*
1229 * This generates better code than the inline assembly in
1230 * __set_bit().
1231 */
1232 static inline void *ptr_set_bit(void *ptr, int bit)
1233 {
1234 unsigned long __ptr = (unsigned long)ptr;
1236 __ptr |= BIT(bit);
1237 return (void *)__ptr;
1238 }
1239 static inline void *ptr_clear_bit(void *ptr, int bit)
1240 {
1241 unsigned long __ptr = (unsigned long)ptr;
1243 __ptr &= ~BIT(bit);
1244 return (void *)__ptr;
1245 }
1247 static inline pgd_t *kernel_to_user_pgdp(pgd_t *pgdp)
1248 {
1249 return ptr_set_bit(pgdp, PTI_PGTABLE_SWITCH_BIT);
1250 }
1252 static inline pgd_t *user_to_kernel_pgdp(pgd_t *pgdp)
1253 {
1254 return ptr_clear_bit(pgdp, PTI_PGTABLE_SWITCH_BIT);
1255 }
1257 static inline p4d_t *kernel_to_user_p4dp(p4d_t *p4dp)
1258 {
1259 return ptr_set_bit(p4dp, PTI_PGTABLE_SWITCH_BIT);
1260 }
1262 static inline p4d_t *user_to_kernel_p4dp(p4d_t *p4dp)
1263 {
1264 return ptr_clear_bit(p4dp, PTI_PGTABLE_SWITCH_BIT);
1265 }
1266 #endif /* CONFIG_PAGE_TABLE_ISOLATION */
1268 /*
1269 * clone_pgd_range(pgd_t *dst, pgd_t *src, int count);
1270 *
1271 * dst - pointer to pgd range anwhere on a pgd page
1272 * src - ""
1273 * count - the number of pgds to copy.
1274 *
1275 * dst and src can be on the same page, but the range must not overlap,
1276 * and must not cross a page boundary.
1277 */
1278 static inline void clone_pgd_range(pgd_t *dst, pgd_t *src, int count)
1279 {
1280 memcpy(dst, src, count * sizeof(pgd_t));
1281 #ifdef CONFIG_PAGE_TABLE_ISOLATION
1282 if (!static_cpu_has(X86_FEATURE_PTI))
1283 return;
1284 /* Clone the user space pgd as well */
1285 memcpy(kernel_to_user_pgdp(dst), kernel_to_user_pgdp(src),
1286 count * sizeof(pgd_t));
1287 #endif
1288 }
1290 #define PTE_SHIFT ilog2(PTRS_PER_PTE)
1291 static inline int page_level_shift(enum pg_level level)
1292 {
1293 return (PAGE_SHIFT - PTE_SHIFT) + level * PTE_SHIFT;
1294 }
1295 static inline unsigned long page_level_size(enum pg_level level)
1296 {
1297 return 1UL << page_level_shift(level);
1298 }
1299 static inline unsigned long page_level_mask(enum pg_level level)
1300 {
1301 return ~(page_level_size(level) - 1);
1302 }
1304 /*
1305 * The x86 doesn't have any external MMU info: the kernel page
1306 * tables contain all the necessary information.
1307 */
1308 static inline void update_mmu_cache(struct vm_area_struct *vma,
1309 unsigned long addr, pte_t *ptep)
1310 {
1311 }
1312 static inline void update_mmu_cache_pmd(struct vm_area_struct *vma,
1313 unsigned long addr, pmd_t *pmd)
1314 {
1315 }
1316 static inline void update_mmu_cache_pud(struct vm_area_struct *vma,
1317 unsigned long addr, pud_t *pud)
1318 {
1319 }
1321 #ifdef CONFIG_HAVE_ARCH_SOFT_DIRTY
1322 static inline pte_t pte_swp_mksoft_dirty(pte_t pte)
1323 {
1324 return pte_set_flags(pte, _PAGE_SWP_SOFT_DIRTY);
1325 }
1327 static inline int pte_swp_soft_dirty(pte_t pte)
1328 {
1329 return pte_flags(pte) & _PAGE_SWP_SOFT_DIRTY;
1330 }
1332 static inline pte_t pte_swp_clear_soft_dirty(pte_t pte)
1333 {
1334 return pte_clear_flags(pte, _PAGE_SWP_SOFT_DIRTY);
1335 }
1337 #ifdef CONFIG_ARCH_ENABLE_THP_MIGRATION
1338 static inline pmd_t pmd_swp_mksoft_dirty(pmd_t pmd)
1339 {
1340 return pmd_set_flags(pmd, _PAGE_SWP_SOFT_DIRTY);
1341 }
1343 static inline int pmd_swp_soft_dirty(pmd_t pmd)
1344 {
1345 return pmd_flags(pmd) & _PAGE_SWP_SOFT_DIRTY;
1346 }
1348 static inline pmd_t pmd_swp_clear_soft_dirty(pmd_t pmd)
1349 {
1350 return pmd_clear_flags(pmd, _PAGE_SWP_SOFT_DIRTY);
1351 }
1352 #endif
1353 #endif
1355 #define PKRU_AD_BIT 0x1
1356 #define PKRU_WD_BIT 0x2
1357 #define PKRU_BITS_PER_PKEY 2
1359 static inline bool __pkru_allows_read(u32 pkru, u16 pkey)
1360 {
1361 int pkru_pkey_bits = pkey * PKRU_BITS_PER_PKEY;
1362 return !(pkru & (PKRU_AD_BIT << pkru_pkey_bits));
1363 }
1365 static inline bool __pkru_allows_write(u32 pkru, u16 pkey)
1366 {
1367 int pkru_pkey_bits = pkey * PKRU_BITS_PER_PKEY;
1368 /*
1369 * Access-disable disables writes too so we need to check
1370 * both bits here.
1371 */
1372 return !(pkru & ((PKRU_AD_BIT|PKRU_WD_BIT) << pkru_pkey_bits));
1373 }
1375 static inline u16 pte_flags_pkey(unsigned long pte_flags)
1376 {
1377 #ifdef CONFIG_X86_INTEL_MEMORY_PROTECTION_KEYS
1378 /* ifdef to avoid doing 59-bit shift on 32-bit values */
1379 return (pte_flags & _PAGE_PKEY_MASK) >> _PAGE_BIT_PKEY_BIT0;
1380 #else
1381 return 0;
1382 #endif
1383 }
1385 static inline bool __pkru_allows_pkey(u16 pkey, bool write)
1386 {
1387 u32 pkru = read_pkru();
1389 if (!__pkru_allows_read(pkru, pkey))
1390 return false;
1391 if (write && !__pkru_allows_write(pkru, pkey))
1392 return false;
1394 return true;
1395 }
1397 /*
1398 * 'pteval' can come from a PTE, PMD or PUD. We only check
1399 * _PAGE_PRESENT, _PAGE_USER, and _PAGE_RW in here which are the
1400 * same value on all 3 types.
1401 */
1402 static inline bool __pte_access_permitted(unsigned long pteval, bool write)
1403 {
1404 unsigned long need_pte_bits = _PAGE_PRESENT|_PAGE_USER;
1406 if (write)
1407 need_pte_bits |= _PAGE_RW;
1409 if ((pteval & need_pte_bits) != need_pte_bits)
1410 return 0;
1412 return __pkru_allows_pkey(pte_flags_pkey(pteval), write);
1413 }
1415 #define pte_access_permitted pte_access_permitted
1416 static inline bool pte_access_permitted(pte_t pte, bool write)
1417 {
1418 return __pte_access_permitted(pte_val(pte), write);
1419 }
1421 #define pmd_access_permitted pmd_access_permitted
1422 static inline bool pmd_access_permitted(pmd_t pmd, bool write)
1423 {
1424 return __pte_access_permitted(pmd_val(pmd), write);
1425 }
1427 #define pud_access_permitted pud_access_permitted
1428 static inline bool pud_access_permitted(pud_t pud, bool write)
1429 {
1430 return __pte_access_permitted(pud_val(pud), write);
1431 }
1433 #define __HAVE_ARCH_PFN_MODIFY_ALLOWED 1
1434 extern bool pfn_modify_allowed(unsigned long pfn, pgprot_t prot);
1436 static inline bool arch_has_pfn_modify_check(void)
1437 {
1438 return boot_cpu_has_bug(X86_BUG_L1TF);
1439 }
1441 #include <asm-generic/pgtable.h>
1442 #endif /* __ASSEMBLY__ */
1444 #endif /* _ASM_X86_PGTABLE_H */