]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/blob - arch/x86/kernel/cpu/amd.c
Merge tag 'xfs-fixes-for-4.19-rc7' of git://git.kernel.org/pub/scm/fs/xfs/xfs-linux
[rpmsg/rpmsg.git] / arch / x86 / kernel / cpu / amd.c
1 #include <linux/export.h>
2 #include <linux/bitops.h>
3 #include <linux/elf.h>
4 #include <linux/mm.h>
6 #include <linux/io.h>
7 #include <linux/sched.h>
8 #include <linux/sched/clock.h>
9 #include <linux/random.h>
10 #include <asm/processor.h>
11 #include <asm/apic.h>
12 #include <asm/cacheinfo.h>
13 #include <asm/cpu.h>
14 #include <asm/spec-ctrl.h>
15 #include <asm/smp.h>
16 #include <asm/pci-direct.h>
17 #include <asm/delay.h>
19 #ifdef CONFIG_X86_64
20 # include <asm/mmconfig.h>
21 # include <asm/set_memory.h>
22 #endif
24 #include "cpu.h"
26 static const int amd_erratum_383[];
27 static const int amd_erratum_400[];
28 static bool cpu_has_amd_erratum(struct cpuinfo_x86 *cpu, const int *erratum);
30 /*
31  * nodes_per_socket: Stores the number of nodes per socket.
32  * Refer to Fam15h Models 00-0fh BKDG - CPUID Fn8000_001E_ECX
33  * Node Identifiers[10:8]
34  */
35 static u32 nodes_per_socket = 1;
37 static inline int rdmsrl_amd_safe(unsigned msr, unsigned long long *p)
38 {
39         u32 gprs[8] = { 0 };
40         int err;
42         WARN_ONCE((boot_cpu_data.x86 != 0xf),
43                   "%s should only be used on K8!\n", __func__);
45         gprs[1] = msr;
46         gprs[7] = 0x9c5a203a;
48         err = rdmsr_safe_regs(gprs);
50         *p = gprs[0] | ((u64)gprs[2] << 32);
52         return err;
53 }
55 static inline int wrmsrl_amd_safe(unsigned msr, unsigned long long val)
56 {
57         u32 gprs[8] = { 0 };
59         WARN_ONCE((boot_cpu_data.x86 != 0xf),
60                   "%s should only be used on K8!\n", __func__);
62         gprs[0] = (u32)val;
63         gprs[1] = msr;
64         gprs[2] = val >> 32;
65         gprs[7] = 0x9c5a203a;
67         return wrmsr_safe_regs(gprs);
68 }
70 /*
71  *      B step AMD K6 before B 9730xxxx have hardware bugs that can cause
72  *      misexecution of code under Linux. Owners of such processors should
73  *      contact AMD for precise details and a CPU swap.
74  *
75  *      See     http://www.multimania.com/poulot/k6bug.html
76  *      and     section 2.6.2 of "AMD-K6 Processor Revision Guide - Model 6"
77  *              (Publication # 21266  Issue Date: August 1998)
78  *
79  *      The following test is erm.. interesting. AMD neglected to up
80  *      the chip setting when fixing the bug but they also tweaked some
81  *      performance at the same time..
82  */
84 extern __visible void vide(void);
85 __asm__(".globl vide\n"
86         ".type vide, @function\n"
87         ".align 4\n"
88         "vide: ret\n");
90 static void init_amd_k5(struct cpuinfo_x86 *c)
91 {
92 #ifdef CONFIG_X86_32
93 /*
94  * General Systems BIOSen alias the cpu frequency registers
95  * of the Elan at 0x000df000. Unfortunately, one of the Linux
96  * drivers subsequently pokes it, and changes the CPU speed.
97  * Workaround : Remove the unneeded alias.
98  */
99 #define CBAR            (0xfffc) /* Configuration Base Address  (32-bit) */
100 #define CBAR_ENB        (0x80000000)
101 #define CBAR_KEY        (0X000000CB)
102         if (c->x86_model == 9 || c->x86_model == 10) {
103                 if (inl(CBAR) & CBAR_ENB)
104                         outl(0 | CBAR_KEY, CBAR);
105         }
106 #endif
109 static void init_amd_k6(struct cpuinfo_x86 *c)
111 #ifdef CONFIG_X86_32
112         u32 l, h;
113         int mbytes = get_num_physpages() >> (20-PAGE_SHIFT);
115         if (c->x86_model < 6) {
116                 /* Based on AMD doc 20734R - June 2000 */
117                 if (c->x86_model == 0) {
118                         clear_cpu_cap(c, X86_FEATURE_APIC);
119                         set_cpu_cap(c, X86_FEATURE_PGE);
120                 }
121                 return;
122         }
124         if (c->x86_model == 6 && c->x86_stepping == 1) {
125                 const int K6_BUG_LOOP = 1000000;
126                 int n;
127                 void (*f_vide)(void);
128                 u64 d, d2;
130                 pr_info("AMD K6 stepping B detected - ");
132                 /*
133                  * It looks like AMD fixed the 2.6.2 bug and improved indirect
134                  * calls at the same time.
135                  */
137                 n = K6_BUG_LOOP;
138                 f_vide = vide;
139                 OPTIMIZER_HIDE_VAR(f_vide);
140                 d = rdtsc();
141                 while (n--)
142                         f_vide();
143                 d2 = rdtsc();
144                 d = d2-d;
146                 if (d > 20*K6_BUG_LOOP)
147                         pr_cont("system stability may be impaired when more than 32 MB are used.\n");
148                 else
149                         pr_cont("probably OK (after B9730xxxx).\n");
150         }
152         /* K6 with old style WHCR */
153         if (c->x86_model < 8 ||
154            (c->x86_model == 8 && c->x86_stepping < 8)) {
155                 /* We can only write allocate on the low 508Mb */
156                 if (mbytes > 508)
157                         mbytes = 508;
159                 rdmsr(MSR_K6_WHCR, l, h);
160                 if ((l&0x0000FFFF) == 0) {
161                         unsigned long flags;
162                         l = (1<<0)|((mbytes/4)<<1);
163                         local_irq_save(flags);
164                         wbinvd();
165                         wrmsr(MSR_K6_WHCR, l, h);
166                         local_irq_restore(flags);
167                         pr_info("Enabling old style K6 write allocation for %d Mb\n",
168                                 mbytes);
169                 }
170                 return;
171         }
173         if ((c->x86_model == 8 && c->x86_stepping > 7) ||
174              c->x86_model == 9 || c->x86_model == 13) {
175                 /* The more serious chips .. */
177                 if (mbytes > 4092)
178                         mbytes = 4092;
180                 rdmsr(MSR_K6_WHCR, l, h);
181                 if ((l&0xFFFF0000) == 0) {
182                         unsigned long flags;
183                         l = ((mbytes>>2)<<22)|(1<<16);
184                         local_irq_save(flags);
185                         wbinvd();
186                         wrmsr(MSR_K6_WHCR, l, h);
187                         local_irq_restore(flags);
188                         pr_info("Enabling new style K6 write allocation for %d Mb\n",
189                                 mbytes);
190                 }
192                 return;
193         }
195         if (c->x86_model == 10) {
196                 /* AMD Geode LX is model 10 */
197                 /* placeholder for any needed mods */
198                 return;
199         }
200 #endif
203 static void init_amd_k7(struct cpuinfo_x86 *c)
205 #ifdef CONFIG_X86_32
206         u32 l, h;
208         /*
209          * Bit 15 of Athlon specific MSR 15, needs to be 0
210          * to enable SSE on Palomino/Morgan/Barton CPU's.
211          * If the BIOS didn't enable it already, enable it here.
212          */
213         if (c->x86_model >= 6 && c->x86_model <= 10) {
214                 if (!cpu_has(c, X86_FEATURE_XMM)) {
215                         pr_info("Enabling disabled K7/SSE Support.\n");
216                         msr_clear_bit(MSR_K7_HWCR, 15);
217                         set_cpu_cap(c, X86_FEATURE_XMM);
218                 }
219         }
221         /*
222          * It's been determined by AMD that Athlons since model 8 stepping 1
223          * are more robust with CLK_CTL set to 200xxxxx instead of 600xxxxx
224          * As per AMD technical note 27212 0.2
225          */
226         if ((c->x86_model == 8 && c->x86_stepping >= 1) || (c->x86_model > 8)) {
227                 rdmsr(MSR_K7_CLK_CTL, l, h);
228                 if ((l & 0xfff00000) != 0x20000000) {
229                         pr_info("CPU: CLK_CTL MSR was %x. Reprogramming to %x\n",
230                                 l, ((l & 0x000fffff)|0x20000000));
231                         wrmsr(MSR_K7_CLK_CTL, (l & 0x000fffff)|0x20000000, h);
232                 }
233         }
235         /* calling is from identify_secondary_cpu() ? */
236         if (!c->cpu_index)
237                 return;
239         /*
240          * Certain Athlons might work (for various values of 'work') in SMP
241          * but they are not certified as MP capable.
242          */
243         /* Athlon 660/661 is valid. */
244         if ((c->x86_model == 6) && ((c->x86_stepping == 0) ||
245             (c->x86_stepping == 1)))
246                 return;
248         /* Duron 670 is valid */
249         if ((c->x86_model == 7) && (c->x86_stepping == 0))
250                 return;
252         /*
253          * Athlon 662, Duron 671, and Athlon >model 7 have capability
254          * bit. It's worth noting that the A5 stepping (662) of some
255          * Athlon XP's have the MP bit set.
256          * See http://www.heise.de/newsticker/data/jow-18.10.01-000 for
257          * more.
258          */
259         if (((c->x86_model == 6) && (c->x86_stepping >= 2)) ||
260             ((c->x86_model == 7) && (c->x86_stepping >= 1)) ||
261              (c->x86_model > 7))
262                 if (cpu_has(c, X86_FEATURE_MP))
263                         return;
265         /* If we get here, not a certified SMP capable AMD system. */
267         /*
268          * Don't taint if we are running SMP kernel on a single non-MP
269          * approved Athlon
270          */
271         WARN_ONCE(1, "WARNING: This combination of AMD"
272                 " processors is not suitable for SMP.\n");
273         add_taint(TAINT_CPU_OUT_OF_SPEC, LOCKDEP_NOW_UNRELIABLE);
274 #endif
277 #ifdef CONFIG_NUMA
278 /*
279  * To workaround broken NUMA config.  Read the comment in
280  * srat_detect_node().
281  */
282 static int nearby_node(int apicid)
284         int i, node;
286         for (i = apicid - 1; i >= 0; i--) {
287                 node = __apicid_to_node[i];
288                 if (node != NUMA_NO_NODE && node_online(node))
289                         return node;
290         }
291         for (i = apicid + 1; i < MAX_LOCAL_APIC; i++) {
292                 node = __apicid_to_node[i];
293                 if (node != NUMA_NO_NODE && node_online(node))
294                         return node;
295         }
296         return first_node(node_online_map); /* Shouldn't happen */
298 #endif
300 /*
301  * Fix up cpu_core_id for pre-F17h systems to be in the
302  * [0 .. cores_per_node - 1] range. Not really needed but
303  * kept so as not to break existing setups.
304  */
305 static void legacy_fixup_core_id(struct cpuinfo_x86 *c)
307         u32 cus_per_node;
309         if (c->x86 >= 0x17)
310                 return;
312         cus_per_node = c->x86_max_cores / nodes_per_socket;
313         c->cpu_core_id %= cus_per_node;
317 static void amd_get_topology_early(struct cpuinfo_x86 *c)
319         if (cpu_has(c, X86_FEATURE_TOPOEXT))
320                 smp_num_siblings = ((cpuid_ebx(0x8000001e) >> 8) & 0xff) + 1;
323 /*
324  * Fixup core topology information for
325  * (1) AMD multi-node processors
326  *     Assumption: Number of cores in each internal node is the same.
327  * (2) AMD processors supporting compute units
328  */
329 static void amd_get_topology(struct cpuinfo_x86 *c)
331         u8 node_id;
332         int cpu = smp_processor_id();
334         /* get information required for multi-node processors */
335         if (boot_cpu_has(X86_FEATURE_TOPOEXT)) {
336                 int err;
337                 u32 eax, ebx, ecx, edx;
339                 cpuid(0x8000001e, &eax, &ebx, &ecx, &edx);
341                 node_id  = ecx & 0xff;
343                 if (c->x86 == 0x15)
344                         c->cu_id = ebx & 0xff;
346                 if (c->x86 >= 0x17) {
347                         c->cpu_core_id = ebx & 0xff;
349                         if (smp_num_siblings > 1)
350                                 c->x86_max_cores /= smp_num_siblings;
351                 }
353                 /*
354                  * In case leaf B is available, use it to derive
355                  * topology information.
356                  */
357                 err = detect_extended_topology(c);
358                 if (!err)
359                         c->x86_coreid_bits = get_count_order(c->x86_max_cores);
361                 cacheinfo_amd_init_llc_id(c, cpu, node_id);
363         } else if (cpu_has(c, X86_FEATURE_NODEID_MSR)) {
364                 u64 value;
366                 rdmsrl(MSR_FAM10H_NODE_ID, value);
367                 node_id = value & 7;
369                 per_cpu(cpu_llc_id, cpu) = node_id;
370         } else
371                 return;
373         if (nodes_per_socket > 1) {
374                 set_cpu_cap(c, X86_FEATURE_AMD_DCM);
375                 legacy_fixup_core_id(c);
376         }
379 /*
380  * On a AMD dual core setup the lower bits of the APIC id distinguish the cores.
381  * Assumes number of cores is a power of two.
382  */
383 static void amd_detect_cmp(struct cpuinfo_x86 *c)
385         unsigned bits;
386         int cpu = smp_processor_id();
388         bits = c->x86_coreid_bits;
389         /* Low order bits define the core id (index of core in socket) */
390         c->cpu_core_id = c->initial_apicid & ((1 << bits)-1);
391         /* Convert the initial APIC ID into the socket ID */
392         c->phys_proc_id = c->initial_apicid >> bits;
393         /* use socket ID also for last level cache */
394         per_cpu(cpu_llc_id, cpu) = c->phys_proc_id;
397 u16 amd_get_nb_id(int cpu)
399         return per_cpu(cpu_llc_id, cpu);
401 EXPORT_SYMBOL_GPL(amd_get_nb_id);
403 u32 amd_get_nodes_per_socket(void)
405         return nodes_per_socket;
407 EXPORT_SYMBOL_GPL(amd_get_nodes_per_socket);
409 static void srat_detect_node(struct cpuinfo_x86 *c)
411 #ifdef CONFIG_NUMA
412         int cpu = smp_processor_id();
413         int node;
414         unsigned apicid = c->apicid;
416         node = numa_cpu_node(cpu);
417         if (node == NUMA_NO_NODE)
418                 node = per_cpu(cpu_llc_id, cpu);
420         /*
421          * On multi-fabric platform (e.g. Numascale NumaChip) a
422          * platform-specific handler needs to be called to fixup some
423          * IDs of the CPU.
424          */
425         if (x86_cpuinit.fixup_cpu_id)
426                 x86_cpuinit.fixup_cpu_id(c, node);
428         if (!node_online(node)) {
429                 /*
430                  * Two possibilities here:
431                  *
432                  * - The CPU is missing memory and no node was created.  In
433                  *   that case try picking one from a nearby CPU.
434                  *
435                  * - The APIC IDs differ from the HyperTransport node IDs
436                  *   which the K8 northbridge parsing fills in.  Assume
437                  *   they are all increased by a constant offset, but in
438                  *   the same order as the HT nodeids.  If that doesn't
439                  *   result in a usable node fall back to the path for the
440                  *   previous case.
441                  *
442                  * This workaround operates directly on the mapping between
443                  * APIC ID and NUMA node, assuming certain relationship
444                  * between APIC ID, HT node ID and NUMA topology.  As going
445                  * through CPU mapping may alter the outcome, directly
446                  * access __apicid_to_node[].
447                  */
448                 int ht_nodeid = c->initial_apicid;
450                 if (__apicid_to_node[ht_nodeid] != NUMA_NO_NODE)
451                         node = __apicid_to_node[ht_nodeid];
452                 /* Pick a nearby node */
453                 if (!node_online(node))
454                         node = nearby_node(apicid);
455         }
456         numa_set_node(cpu, node);
457 #endif
460 static void early_init_amd_mc(struct cpuinfo_x86 *c)
462 #ifdef CONFIG_SMP
463         unsigned bits, ecx;
465         /* Multi core CPU? */
466         if (c->extended_cpuid_level < 0x80000008)
467                 return;
469         ecx = cpuid_ecx(0x80000008);
471         c->x86_max_cores = (ecx & 0xff) + 1;
473         /* CPU telling us the core id bits shift? */
474         bits = (ecx >> 12) & 0xF;
476         /* Otherwise recompute */
477         if (bits == 0) {
478                 while ((1 << bits) < c->x86_max_cores)
479                         bits++;
480         }
482         c->x86_coreid_bits = bits;
483 #endif
486 static void bsp_init_amd(struct cpuinfo_x86 *c)
489 #ifdef CONFIG_X86_64
490         if (c->x86 >= 0xf) {
491                 unsigned long long tseg;
493                 /*
494                  * Split up direct mapping around the TSEG SMM area.
495                  * Don't do it for gbpages because there seems very little
496                  * benefit in doing so.
497                  */
498                 if (!rdmsrl_safe(MSR_K8_TSEG_ADDR, &tseg)) {
499                         unsigned long pfn = tseg >> PAGE_SHIFT;
501                         pr_debug("tseg: %010llx\n", tseg);
502                         if (pfn_range_is_mapped(pfn, pfn + 1))
503                                 set_memory_4k((unsigned long)__va(tseg), 1);
504                 }
505         }
506 #endif
508         if (cpu_has(c, X86_FEATURE_CONSTANT_TSC)) {
510                 if (c->x86 > 0x10 ||
511                     (c->x86 == 0x10 && c->x86_model >= 0x2)) {
512                         u64 val;
514                         rdmsrl(MSR_K7_HWCR, val);
515                         if (!(val & BIT(24)))
516                                 pr_warn(FW_BUG "TSC doesn't count with P0 frequency!\n");
517                 }
518         }
520         if (c->x86 == 0x15) {
521                 unsigned long upperbit;
522                 u32 cpuid, assoc;
524                 cpuid    = cpuid_edx(0x80000005);
525                 assoc    = cpuid >> 16 & 0xff;
526                 upperbit = ((cpuid >> 24) << 10) / assoc;
528                 va_align.mask     = (upperbit - 1) & PAGE_MASK;
529                 va_align.flags    = ALIGN_VA_32 | ALIGN_VA_64;
531                 /* A random value per boot for bit slice [12:upper_bit) */
532                 va_align.bits = get_random_int() & va_align.mask;
533         }
535         if (cpu_has(c, X86_FEATURE_MWAITX))
536                 use_mwaitx_delay();
538         if (boot_cpu_has(X86_FEATURE_TOPOEXT)) {
539                 u32 ecx;
541                 ecx = cpuid_ecx(0x8000001e);
542                 nodes_per_socket = ((ecx >> 8) & 7) + 1;
543         } else if (boot_cpu_has(X86_FEATURE_NODEID_MSR)) {
544                 u64 value;
546                 rdmsrl(MSR_FAM10H_NODE_ID, value);
547                 nodes_per_socket = ((value >> 3) & 7) + 1;
548         }
550         if (!boot_cpu_has(X86_FEATURE_AMD_SSBD) &&
551             !boot_cpu_has(X86_FEATURE_VIRT_SSBD) &&
552             c->x86 >= 0x15 && c->x86 <= 0x17) {
553                 unsigned int bit;
555                 switch (c->x86) {
556                 case 0x15: bit = 54; break;
557                 case 0x16: bit = 33; break;
558                 case 0x17: bit = 10; break;
559                 default: return;
560                 }
561                 /*
562                  * Try to cache the base value so further operations can
563                  * avoid RMW. If that faults, do not enable SSBD.
564                  */
565                 if (!rdmsrl_safe(MSR_AMD64_LS_CFG, &x86_amd_ls_cfg_base)) {
566                         setup_force_cpu_cap(X86_FEATURE_LS_CFG_SSBD);
567                         setup_force_cpu_cap(X86_FEATURE_SSBD);
568                         x86_amd_ls_cfg_ssbd_mask = 1ULL << bit;
569                 }
570         }
573 static void early_detect_mem_encrypt(struct cpuinfo_x86 *c)
575         u64 msr;
577         /*
578          * BIOS support is required for SME and SEV.
579          *   For SME: If BIOS has enabled SME then adjust x86_phys_bits by
580          *            the SME physical address space reduction value.
581          *            If BIOS has not enabled SME then don't advertise the
582          *            SME feature (set in scattered.c).
583          *   For SEV: If BIOS has not enabled SEV then don't advertise the
584          *            SEV feature (set in scattered.c).
585          *
586          *   In all cases, since support for SME and SEV requires long mode,
587          *   don't advertise the feature under CONFIG_X86_32.
588          */
589         if (cpu_has(c, X86_FEATURE_SME) || cpu_has(c, X86_FEATURE_SEV)) {
590                 /* Check if memory encryption is enabled */
591                 rdmsrl(MSR_K8_SYSCFG, msr);
592                 if (!(msr & MSR_K8_SYSCFG_MEM_ENCRYPT))
593                         goto clear_all;
595                 /*
596                  * Always adjust physical address bits. Even though this
597                  * will be a value above 32-bits this is still done for
598                  * CONFIG_X86_32 so that accurate values are reported.
599                  */
600                 c->x86_phys_bits -= (cpuid_ebx(0x8000001f) >> 6) & 0x3f;
602                 if (IS_ENABLED(CONFIG_X86_32))
603                         goto clear_all;
605                 rdmsrl(MSR_K7_HWCR, msr);
606                 if (!(msr & MSR_K7_HWCR_SMMLOCK))
607                         goto clear_sev;
609                 return;
611 clear_all:
612                 clear_cpu_cap(c, X86_FEATURE_SME);
613 clear_sev:
614                 clear_cpu_cap(c, X86_FEATURE_SEV);
615         }
618 static void early_init_amd(struct cpuinfo_x86 *c)
620         u64 value;
621         u32 dummy;
623         early_init_amd_mc(c);
625 #ifdef CONFIG_X86_32
626         if (c->x86 == 6)
627                 set_cpu_cap(c, X86_FEATURE_K7);
628 #endif
630         if (c->x86 >= 0xf)
631                 set_cpu_cap(c, X86_FEATURE_K8);
633         rdmsr_safe(MSR_AMD64_PATCH_LEVEL, &c->microcode, &dummy);
635         /*
636          * c->x86_power is 8000_0007 edx. Bit 8 is TSC runs at constant rate
637          * with P/T states and does not stop in deep C-states
638          */
639         if (c->x86_power & (1 << 8)) {
640                 set_cpu_cap(c, X86_FEATURE_CONSTANT_TSC);
641                 set_cpu_cap(c, X86_FEATURE_NONSTOP_TSC);
642         }
644         /* Bit 12 of 8000_0007 edx is accumulated power mechanism. */
645         if (c->x86_power & BIT(12))
646                 set_cpu_cap(c, X86_FEATURE_ACC_POWER);
648 #ifdef CONFIG_X86_64
649         set_cpu_cap(c, X86_FEATURE_SYSCALL32);
650 #else
651         /*  Set MTRR capability flag if appropriate */
652         if (c->x86 == 5)
653                 if (c->x86_model == 13 || c->x86_model == 9 ||
654                     (c->x86_model == 8 && c->x86_stepping >= 8))
655                         set_cpu_cap(c, X86_FEATURE_K6_MTRR);
656 #endif
657 #if defined(CONFIG_X86_LOCAL_APIC) && defined(CONFIG_PCI)
658         /*
659          * ApicID can always be treated as an 8-bit value for AMD APIC versions
660          * >= 0x10, but even old K8s came out of reset with version 0x10. So, we
661          * can safely set X86_FEATURE_EXTD_APICID unconditionally for families
662          * after 16h.
663          */
664         if (boot_cpu_has(X86_FEATURE_APIC)) {
665                 if (c->x86 > 0x16)
666                         set_cpu_cap(c, X86_FEATURE_EXTD_APICID);
667                 else if (c->x86 >= 0xf) {
668                         /* check CPU config space for extended APIC ID */
669                         unsigned int val;
671                         val = read_pci_config(0, 24, 0, 0x68);
672                         if ((val >> 17 & 0x3) == 0x3)
673                                 set_cpu_cap(c, X86_FEATURE_EXTD_APICID);
674                 }
675         }
676 #endif
678         /*
679          * This is only needed to tell the kernel whether to use VMCALL
680          * and VMMCALL.  VMMCALL is never executed except under virt, so
681          * we can set it unconditionally.
682          */
683         set_cpu_cap(c, X86_FEATURE_VMMCALL);
685         /* F16h erratum 793, CVE-2013-6885 */
686         if (c->x86 == 0x16 && c->x86_model <= 0xf)
687                 msr_set_bit(MSR_AMD64_LS_CFG, 15);
689         /*
690          * Check whether the machine is affected by erratum 400. This is
691          * used to select the proper idle routine and to enable the check
692          * whether the machine is affected in arch_post_acpi_init(), which
693          * sets the X86_BUG_AMD_APIC_C1E bug depending on the MSR check.
694          */
695         if (cpu_has_amd_erratum(c, amd_erratum_400))
696                 set_cpu_bug(c, X86_BUG_AMD_E400);
698         early_detect_mem_encrypt(c);
700         /* Re-enable TopologyExtensions if switched off by BIOS */
701         if (c->x86 == 0x15 &&
702             (c->x86_model >= 0x10 && c->x86_model <= 0x6f) &&
703             !cpu_has(c, X86_FEATURE_TOPOEXT)) {
705                 if (msr_set_bit(0xc0011005, 54) > 0) {
706                         rdmsrl(0xc0011005, value);
707                         if (value & BIT_64(54)) {
708                                 set_cpu_cap(c, X86_FEATURE_TOPOEXT);
709                                 pr_info_once(FW_INFO "CPU: Re-enabling disabled Topology Extensions Support.\n");
710                         }
711                 }
712         }
714         amd_get_topology_early(c);
717 static void init_amd_k8(struct cpuinfo_x86 *c)
719         u32 level;
720         u64 value;
722         /* On C+ stepping K8 rep microcode works well for copy/memset */
723         level = cpuid_eax(1);
724         if ((level >= 0x0f48 && level < 0x0f50) || level >= 0x0f58)
725                 set_cpu_cap(c, X86_FEATURE_REP_GOOD);
727         /*
728          * Some BIOSes incorrectly force this feature, but only K8 revision D
729          * (model = 0x14) and later actually support it.
730          * (AMD Erratum #110, docId: 25759).
731          */
732         if (c->x86_model < 0x14 && cpu_has(c, X86_FEATURE_LAHF_LM)) {
733                 clear_cpu_cap(c, X86_FEATURE_LAHF_LM);
734                 if (!rdmsrl_amd_safe(0xc001100d, &value)) {
735                         value &= ~BIT_64(32);
736                         wrmsrl_amd_safe(0xc001100d, value);
737                 }
738         }
740         if (!c->x86_model_id[0])
741                 strcpy(c->x86_model_id, "Hammer");
743 #ifdef CONFIG_SMP
744         /*
745          * Disable TLB flush filter by setting HWCR.FFDIS on K8
746          * bit 6 of msr C001_0015
747          *
748          * Errata 63 for SH-B3 steppings
749          * Errata 122 for all steppings (F+ have it disabled by default)
750          */
751         msr_set_bit(MSR_K7_HWCR, 6);
752 #endif
753         set_cpu_bug(c, X86_BUG_SWAPGS_FENCE);
756 static void init_amd_gh(struct cpuinfo_x86 *c)
758 #ifdef CONFIG_MMCONF_FAM10H
759         /* do this for boot cpu */
760         if (c == &boot_cpu_data)
761                 check_enable_amd_mmconf_dmi();
763         fam10h_check_enable_mmcfg();
764 #endif
766         /*
767          * Disable GART TLB Walk Errors on Fam10h. We do this here because this
768          * is always needed when GART is enabled, even in a kernel which has no
769          * MCE support built in. BIOS should disable GartTlbWlk Errors already.
770          * If it doesn't, we do it here as suggested by the BKDG.
771          *
772          * Fixes: https://bugzilla.kernel.org/show_bug.cgi?id=33012
773          */
774         msr_set_bit(MSR_AMD64_MCx_MASK(4), 10);
776         /*
777          * On family 10h BIOS may not have properly enabled WC+ support, causing
778          * it to be converted to CD memtype. This may result in performance
779          * degradation for certain nested-paging guests. Prevent this conversion
780          * by clearing bit 24 in MSR_AMD64_BU_CFG2.
781          *
782          * NOTE: we want to use the _safe accessors so as not to #GP kvm
783          * guests on older kvm hosts.
784          */
785         msr_clear_bit(MSR_AMD64_BU_CFG2, 24);
787         if (cpu_has_amd_erratum(c, amd_erratum_383))
788                 set_cpu_bug(c, X86_BUG_AMD_TLB_MMATCH);
791 #define MSR_AMD64_DE_CFG        0xC0011029
793 static void init_amd_ln(struct cpuinfo_x86 *c)
795         /*
796          * Apply erratum 665 fix unconditionally so machines without a BIOS
797          * fix work.
798          */
799         msr_set_bit(MSR_AMD64_DE_CFG, 31);
802 static void init_amd_bd(struct cpuinfo_x86 *c)
804         u64 value;
806         /*
807          * The way access filter has a performance penalty on some workloads.
808          * Disable it on the affected CPUs.
809          */
810         if ((c->x86_model >= 0x02) && (c->x86_model < 0x20)) {
811                 if (!rdmsrl_safe(MSR_F15H_IC_CFG, &value) && !(value & 0x1E)) {
812                         value |= 0x1E;
813                         wrmsrl_safe(MSR_F15H_IC_CFG, value);
814                 }
815         }
818 static void init_amd_zn(struct cpuinfo_x86 *c)
820         set_cpu_cap(c, X86_FEATURE_ZEN);
821         /*
822          * Fix erratum 1076: CPB feature bit not being set in CPUID. It affects
823          * all up to and including B1.
824          */
825         if (c->x86_model <= 1 && c->x86_stepping <= 1)
826                 set_cpu_cap(c, X86_FEATURE_CPB);
829 static void init_amd(struct cpuinfo_x86 *c)
831         early_init_amd(c);
833         /*
834          * Bit 31 in normal CPUID used for nonstandard 3DNow ID;
835          * 3DNow is IDd by bit 31 in extended CPUID (1*32+31) anyway
836          */
837         clear_cpu_cap(c, 0*32+31);
839         if (c->x86 >= 0x10)
840                 set_cpu_cap(c, X86_FEATURE_REP_GOOD);
842         /* get apicid instead of initial apic id from cpuid */
843         c->apicid = hard_smp_processor_id();
845         /* K6s reports MCEs but don't actually have all the MSRs */
846         if (c->x86 < 6)
847                 clear_cpu_cap(c, X86_FEATURE_MCE);
849         switch (c->x86) {
850         case 4:    init_amd_k5(c); break;
851         case 5:    init_amd_k6(c); break;
852         case 6:    init_amd_k7(c); break;
853         case 0xf:  init_amd_k8(c); break;
854         case 0x10: init_amd_gh(c); break;
855         case 0x12: init_amd_ln(c); break;
856         case 0x15: init_amd_bd(c); break;
857         case 0x17: init_amd_zn(c); break;
858         }
860         /*
861          * Enable workaround for FXSAVE leak on CPUs
862          * without a XSaveErPtr feature
863          */
864         if ((c->x86 >= 6) && (!cpu_has(c, X86_FEATURE_XSAVEERPTR)))
865                 set_cpu_bug(c, X86_BUG_FXSAVE_LEAK);
867         cpu_detect_cache_sizes(c);
869         amd_detect_cmp(c);
870         amd_get_topology(c);
871         srat_detect_node(c);
873         init_amd_cacheinfo(c);
875         if (cpu_has(c, X86_FEATURE_XMM2)) {
876                 unsigned long long val;
877                 int ret;
879                 /*
880                  * A serializing LFENCE has less overhead than MFENCE, so
881                  * use it for execution serialization.  On families which
882                  * don't have that MSR, LFENCE is already serializing.
883                  * msr_set_bit() uses the safe accessors, too, even if the MSR
884                  * is not present.
885                  */
886                 msr_set_bit(MSR_F10H_DECFG,
887                             MSR_F10H_DECFG_LFENCE_SERIALIZE_BIT);
889                 /*
890                  * Verify that the MSR write was successful (could be running
891                  * under a hypervisor) and only then assume that LFENCE is
892                  * serializing.
893                  */
894                 ret = rdmsrl_safe(MSR_F10H_DECFG, &val);
895                 if (!ret && (val & MSR_F10H_DECFG_LFENCE_SERIALIZE)) {
896                         /* A serializing LFENCE stops RDTSC speculation */
897                         set_cpu_cap(c, X86_FEATURE_LFENCE_RDTSC);
898                 } else {
899                         /* MFENCE stops RDTSC speculation */
900                         set_cpu_cap(c, X86_FEATURE_MFENCE_RDTSC);
901                 }
902         }
904         /*
905          * Family 0x12 and above processors have APIC timer
906          * running in deep C states.
907          */
908         if (c->x86 > 0x11)
909                 set_cpu_cap(c, X86_FEATURE_ARAT);
911         /* 3DNow or LM implies PREFETCHW */
912         if (!cpu_has(c, X86_FEATURE_3DNOWPREFETCH))
913                 if (cpu_has(c, X86_FEATURE_3DNOW) || cpu_has(c, X86_FEATURE_LM))
914                         set_cpu_cap(c, X86_FEATURE_3DNOWPREFETCH);
916         /* AMD CPUs don't reset SS attributes on SYSRET, Xen does. */
917         if (!cpu_has(c, X86_FEATURE_XENPV))
918                 set_cpu_bug(c, X86_BUG_SYSRET_SS_ATTRS);
921 #ifdef CONFIG_X86_32
922 static unsigned int amd_size_cache(struct cpuinfo_x86 *c, unsigned int size)
924         /* AMD errata T13 (order #21922) */
925         if (c->x86 == 6) {
926                 /* Duron Rev A0 */
927                 if (c->x86_model == 3 && c->x86_stepping == 0)
928                         size = 64;
929                 /* Tbird rev A1/A2 */
930                 if (c->x86_model == 4 &&
931                         (c->x86_stepping == 0 || c->x86_stepping == 1))
932                         size = 256;
933         }
934         return size;
936 #endif
938 static void cpu_detect_tlb_amd(struct cpuinfo_x86 *c)
940         u32 ebx, eax, ecx, edx;
941         u16 mask = 0xfff;
943         if (c->x86 < 0xf)
944                 return;
946         if (c->extended_cpuid_level < 0x80000006)
947                 return;
949         cpuid(0x80000006, &eax, &ebx, &ecx, &edx);
951         tlb_lld_4k[ENTRIES] = (ebx >> 16) & mask;
952         tlb_lli_4k[ENTRIES] = ebx & mask;
954         /*
955          * K8 doesn't have 2M/4M entries in the L2 TLB so read out the L1 TLB
956          * characteristics from the CPUID function 0x80000005 instead.
957          */
958         if (c->x86 == 0xf) {
959                 cpuid(0x80000005, &eax, &ebx, &ecx, &edx);
960                 mask = 0xff;
961         }
963         /* Handle DTLB 2M and 4M sizes, fall back to L1 if L2 is disabled */
964         if (!((eax >> 16) & mask))
965                 tlb_lld_2m[ENTRIES] = (cpuid_eax(0x80000005) >> 16) & 0xff;
966         else
967                 tlb_lld_2m[ENTRIES] = (eax >> 16) & mask;
969         /* a 4M entry uses two 2M entries */
970         tlb_lld_4m[ENTRIES] = tlb_lld_2m[ENTRIES] >> 1;
972         /* Handle ITLB 2M and 4M sizes, fall back to L1 if L2 is disabled */
973         if (!(eax & mask)) {
974                 /* Erratum 658 */
975                 if (c->x86 == 0x15 && c->x86_model <= 0x1f) {
976                         tlb_lli_2m[ENTRIES] = 1024;
977                 } else {
978                         cpuid(0x80000005, &eax, &ebx, &ecx, &edx);
979                         tlb_lli_2m[ENTRIES] = eax & 0xff;
980                 }
981         } else
982                 tlb_lli_2m[ENTRIES] = eax & mask;
984         tlb_lli_4m[ENTRIES] = tlb_lli_2m[ENTRIES] >> 1;
987 static const struct cpu_dev amd_cpu_dev = {
988         .c_vendor       = "AMD",
989         .c_ident        = { "AuthenticAMD" },
990 #ifdef CONFIG_X86_32
991         .legacy_models = {
992                 { .family = 4, .model_names =
993                   {
994                           [3] = "486 DX/2",
995                           [7] = "486 DX/2-WB",
996                           [8] = "486 DX/4",
997                           [9] = "486 DX/4-WB",
998                           [14] = "Am5x86-WT",
999                           [15] = "Am5x86-WB"
1000                   }
1001                 },
1002         },
1003         .legacy_cache_size = amd_size_cache,
1004 #endif
1005         .c_early_init   = early_init_amd,
1006         .c_detect_tlb   = cpu_detect_tlb_amd,
1007         .c_bsp_init     = bsp_init_amd,
1008         .c_init         = init_amd,
1009         .c_x86_vendor   = X86_VENDOR_AMD,
1010 };
1012 cpu_dev_register(amd_cpu_dev);
1014 /*
1015  * AMD errata checking
1016  *
1017  * Errata are defined as arrays of ints using the AMD_LEGACY_ERRATUM() or
1018  * AMD_OSVW_ERRATUM() macros. The latter is intended for newer errata that
1019  * have an OSVW id assigned, which it takes as first argument. Both take a
1020  * variable number of family-specific model-stepping ranges created by
1021  * AMD_MODEL_RANGE().
1022  *
1023  * Example:
1024  *
1025  * const int amd_erratum_319[] =
1026  *      AMD_LEGACY_ERRATUM(AMD_MODEL_RANGE(0x10, 0x2, 0x1, 0x4, 0x2),
1027  *                         AMD_MODEL_RANGE(0x10, 0x8, 0x0, 0x8, 0x0),
1028  *                         AMD_MODEL_RANGE(0x10, 0x9, 0x0, 0x9, 0x0));
1029  */
1031 #define AMD_LEGACY_ERRATUM(...)         { -1, __VA_ARGS__, 0 }
1032 #define AMD_OSVW_ERRATUM(osvw_id, ...)  { osvw_id, __VA_ARGS__, 0 }
1033 #define AMD_MODEL_RANGE(f, m_start, s_start, m_end, s_end) \
1034         ((f << 24) | (m_start << 16) | (s_start << 12) | (m_end << 4) | (s_end))
1035 #define AMD_MODEL_RANGE_FAMILY(range)   (((range) >> 24) & 0xff)
1036 #define AMD_MODEL_RANGE_START(range)    (((range) >> 12) & 0xfff)
1037 #define AMD_MODEL_RANGE_END(range)      ((range) & 0xfff)
1039 static const int amd_erratum_400[] =
1040         AMD_OSVW_ERRATUM(1, AMD_MODEL_RANGE(0xf, 0x41, 0x2, 0xff, 0xf),
1041                             AMD_MODEL_RANGE(0x10, 0x2, 0x1, 0xff, 0xf));
1043 static const int amd_erratum_383[] =
1044         AMD_OSVW_ERRATUM(3, AMD_MODEL_RANGE(0x10, 0, 0, 0xff, 0xf));
1047 static bool cpu_has_amd_erratum(struct cpuinfo_x86 *cpu, const int *erratum)
1049         int osvw_id = *erratum++;
1050         u32 range;
1051         u32 ms;
1053         if (osvw_id >= 0 && osvw_id < 65536 &&
1054             cpu_has(cpu, X86_FEATURE_OSVW)) {
1055                 u64 osvw_len;
1057                 rdmsrl(MSR_AMD64_OSVW_ID_LENGTH, osvw_len);
1058                 if (osvw_id < osvw_len) {
1059                         u64 osvw_bits;
1061                         rdmsrl(MSR_AMD64_OSVW_STATUS + (osvw_id >> 6),
1062                             osvw_bits);
1063                         return osvw_bits & (1ULL << (osvw_id & 0x3f));
1064                 }
1065         }
1067         /* OSVW unavailable or ID unknown, match family-model-stepping range */
1068         ms = (cpu->x86_model << 4) | cpu->x86_stepping;
1069         while ((range = *erratum++))
1070                 if ((cpu->x86 == AMD_MODEL_RANGE_FAMILY(range)) &&
1071                     (ms >= AMD_MODEL_RANGE_START(range)) &&
1072                     (ms <= AMD_MODEL_RANGE_END(range)))
1073                         return true;
1075         return false;
1078 void set_dr_addr_mask(unsigned long mask, int dr)
1080         if (!boot_cpu_has(X86_FEATURE_BPEXT))
1081                 return;
1083         switch (dr) {
1084         case 0:
1085                 wrmsr(MSR_F16H_DR0_ADDR_MASK, mask, 0);
1086                 break;
1087         case 1:
1088         case 2:
1089         case 3:
1090                 wrmsr(MSR_F16H_DR1_ADDR_MASK - 1 + dr, mask, 0);
1091                 break;
1092         default:
1093                 break;
1094         }