1 # SPDX-License-Identifier: GPL-2.0
2 #
3 # Block layer core configuration
4 #
5 menuconfig BLOCK
6 bool "Enable the block layer" if EXPERT
7 default y
8 select SBITMAP
9 select SRCU
10 help
11 Provide block layer support for the kernel.
13 Disable this option to remove the block layer support from the
14 kernel. This may be useful for embedded devices.
16 If this option is disabled:
18 - block device files will become unusable
19 - some filesystems (such as ext3) will become unavailable.
21 Also, SCSI character devices and USB storage will be disabled since
22 they make use of various block layer definitions and facilities.
24 Say Y here unless you know you really don't want to mount disks and
25 suchlike.
27 if BLOCK
29 config LBDAF
30 bool "Support for large (2TB+) block devices and files"
31 depends on !64BIT
32 default y
33 help
34 Enable block devices or files of size 2TB and larger.
36 This option is required to support the full capacity of large
37 (2TB+) block devices, including RAID, disk, Network Block Device,
38 Logical Volume Manager (LVM) and loopback.
40 This option also enables support for single files larger than
41 2TB.
43 The ext4 filesystem requires that this feature be enabled in
44 order to support filesystems that have the huge_file feature
45 enabled. Otherwise, it will refuse to mount in the read-write
46 mode any filesystems that use the huge_file feature, which is
47 enabled by default by mke2fs.ext4.
49 The GFS2 filesystem also requires this feature.
51 If unsure, say Y.
53 config BLK_SCSI_REQUEST
54 bool
56 config BLK_DEV_BSG
57 bool "Block layer SG support v4"
58 default y
59 select BLK_SCSI_REQUEST
60 help
61 Saying Y here will enable generic SG (SCSI generic) v4 support
62 for any block device.
64 Unlike SG v3 (aka block/scsi_ioctl.c drivers/scsi/sg.c), SG v4
65 can handle complicated SCSI commands: tagged variable length cdbs
66 with bidirectional data transfers and generic request/response
67 protocols (e.g. Task Management Functions and SMP in Serial
68 Attached SCSI).
70 This option is required by recent UDEV versions to properly
71 access device serial numbers, etc.
73 If unsure, say Y.
75 config BLK_DEV_BSGLIB
76 bool "Block layer SG support v4 helper lib"
77 default n
78 select BLK_DEV_BSG
79 select BLK_SCSI_REQUEST
80 help
81 Subsystems will normally enable this if needed. Users will not
82 normally need to manually enable this.
84 If unsure, say N.
86 config BLK_DEV_INTEGRITY
87 bool "Block layer data integrity support"
88 select CRC_T10DIF if BLK_DEV_INTEGRITY
89 ---help---
90 Some storage devices allow extra information to be
91 stored/retrieved to help protect the data. The block layer
92 data integrity option provides hooks which can be used by
93 filesystems to ensure better data integrity.
95 Say yes here if you have a storage device that provides the
96 T10/SCSI Data Integrity Field or the T13/ATA External Path
97 Protection. If in doubt, say N.
99 config BLK_DEV_ZONED
100 bool "Zoned block device support"
101 ---help---
102 Block layer zoned block device support. This option enables
103 support for ZAC/ZBC host-managed and host-aware zoned block devices.
105 Say yes here if you have a ZAC or ZBC storage device.
107 config BLK_DEV_THROTTLING
108 bool "Block layer bio throttling support"
109 depends on BLK_CGROUP=y
110 default n
111 ---help---
112 Block layer bio throttling support. It can be used to limit
113 the IO rate to a device. IO rate policies are per cgroup and
114 one needs to mount and use blkio cgroup controller for creating
115 cgroups and specifying per device IO rate policies.
117 See Documentation/cgroup-v1/blkio-controller.txt for more information.
119 config BLK_DEV_THROTTLING_LOW
120 bool "Block throttling .low limit interface support (EXPERIMENTAL)"
121 depends on BLK_DEV_THROTTLING
122 default n
123 ---help---
124 Add .low limit interface for block throttling. The low limit is a best
125 effort limit to prioritize cgroups. Depending on the setting, the limit
126 can be used to protect cgroups in terms of bandwidth/iops and better
127 utilize disk resource.
129 Note, this is an experimental interface and could be changed someday.
131 config BLK_CMDLINE_PARSER
132 bool "Block device command line partition parser"
133 default n
134 ---help---
135 Enabling this option allows you to specify the partition layout from
136 the kernel boot args. This is typically of use for embedded devices
137 which don't otherwise have any standardized method for listing the
138 partitions on a block device.
140 See Documentation/block/cmdline-partition.txt for more information.
142 config BLK_WBT
143 bool "Enable support for block device writeback throttling"
144 default n
145 ---help---
146 Enabling this option enables the block layer to throttle buffered
147 background writeback from the VM, making it more smooth and having
148 less impact on foreground operations. The throttling is done
149 dynamically on an algorithm loosely based on CoDel, factoring in
150 the realtime performance of the disk.
152 config BLK_CGROUP_IOLATENCY
153 bool "Enable support for latency based cgroup IO protection"
154 depends on BLK_CGROUP=y
155 default n
156 ---help---
157 Enabling this option enables the .latency interface for IO throttling.
158 The IO controller will attempt to maintain average IO latencies below
159 the configured latency target, throttling anybody with a higher latency
160 target than the victimized group.
162 Note, this is an experimental interface and could be changed someday.
164 config BLK_WBT_SQ
165 bool "Single queue writeback throttling"
166 default n
167 depends on BLK_WBT
168 ---help---
169 Enable writeback throttling by default on legacy single queue devices
171 config BLK_WBT_MQ
172 bool "Multiqueue writeback throttling"
173 default y
174 depends on BLK_WBT
175 ---help---
176 Enable writeback throttling by default on multiqueue devices.
177 Multiqueue currently doesn't have support for IO scheduling,
178 enabling this option is recommended.
180 config BLK_DEBUG_FS
181 bool "Block layer debugging information in debugfs"
182 default y
183 depends on DEBUG_FS
184 ---help---
185 Include block layer debugging information in debugfs. This information
186 is mostly useful for kernel developers, but it doesn't incur any cost
187 at runtime.
189 Unless you are building a kernel for a tiny system, you should
190 say Y here.
192 config BLK_DEBUG_FS_ZONED
193 bool
194 default BLK_DEBUG_FS && BLK_DEV_ZONED
196 config BLK_SED_OPAL
197 bool "Logic for interfacing with Opal enabled SEDs"
198 ---help---
199 Builds Logic for interfacing with Opal enabled controllers.
200 Enabling this option enables users to setup/unlock/lock
201 Locking ranges for SED devices using the Opal protocol.
203 menu "Partition Types"
205 source "block/partitions/Kconfig"
207 endmenu
209 endif # BLOCK
211 config BLOCK_COMPAT
212 bool
213 depends on BLOCK && COMPAT
214 default y
216 config BLK_MQ_PCI
217 bool
218 depends on BLOCK && PCI
219 default y
221 config BLK_MQ_VIRTIO
222 bool
223 depends on BLOCK && VIRTIO
224 default y
226 config BLK_MQ_RDMA
227 bool
228 depends on BLOCK && INFINIBAND
229 default y
231 source block/Kconfig.iosched