1 /*
2 * drm kms/fb cma (contiguous memory allocator) helper functions
3 *
4 * Copyright (C) 2012 Analog Device Inc.
5 * Author: Lars-Peter Clausen <lars@metafoo.de>
6 *
7 * Based on udl_fbdev.c
8 * Copyright (C) 2012 Red Hat
9 *
10 * This program is free software; you can redistribute it and/or
11 * modify it under the terms of the GNU General Public License
12 * as published by the Free Software Foundation; either version 2
13 * of the License, or (at your option) any later version.
14 * This program is distributed in the hope that it will be useful,
15 * but WITHOUT ANY WARRANTY; without even the implied warranty of
16 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
17 * GNU General Public License for more details.
18 */
20 #include <drm/drmP.h>
21 #include <drm/drm_client.h>
22 #include <drm/drm_fb_helper.h>
23 #include <drm/drm_framebuffer.h>
24 #include <drm/drm_gem_cma_helper.h>
25 #include <drm/drm_gem_framebuffer_helper.h>
26 #include <drm/drm_fb_cma_helper.h>
27 #include <drm/drm_print.h>
28 #include <linux/module.h>
30 struct drm_fbdev_cma {
31 struct drm_fb_helper fb_helper;
32 };
34 /**
35 * DOC: framebuffer cma helper functions
36 *
37 * Provides helper functions for creating a cma (contiguous memory allocator)
38 * backed framebuffer.
39 *
40 * drm_gem_fb_create() is used in the &drm_mode_config_funcs.fb_create
41 * callback function to create a cma backed framebuffer.
42 *
43 * An fbdev framebuffer backed by cma is also available by calling
44 * drm_fb_cma_fbdev_init(). drm_fb_cma_fbdev_fini() tears it down.
45 */
47 static inline struct drm_fbdev_cma *to_fbdev_cma(struct drm_fb_helper *helper)
48 {
49 return container_of(helper, struct drm_fbdev_cma, fb_helper);
50 }
52 /**
53 * drm_fb_cma_get_gem_obj() - Get CMA GEM object for framebuffer
54 * @fb: The framebuffer
55 * @plane: Which plane
56 *
57 * Return the CMA GEM object for given framebuffer.
58 *
59 * This function will usually be called from the CRTC callback functions.
60 */
61 struct drm_gem_cma_object *drm_fb_cma_get_gem_obj(struct drm_framebuffer *fb,
62 unsigned int plane)
63 {
64 struct drm_gem_object *gem;
66 gem = drm_gem_fb_get_obj(fb, plane);
67 if (!gem)
68 return NULL;
70 return to_drm_gem_cma_obj(gem);
71 }
72 EXPORT_SYMBOL_GPL(drm_fb_cma_get_gem_obj);
74 /**
75 * drm_fb_cma_get_gem_addr() - Get physical address for framebuffer
76 * @fb: The framebuffer
77 * @state: Which state of drm plane
78 * @plane: Which plane
79 * Return the CMA GEM address for given framebuffer.
80 *
81 * This function will usually be called from the PLANE callback functions.
82 */
83 dma_addr_t drm_fb_cma_get_gem_addr(struct drm_framebuffer *fb,
84 struct drm_plane_state *state,
85 unsigned int plane)
86 {
87 struct drm_gem_cma_object *obj;
88 dma_addr_t paddr;
90 obj = drm_fb_cma_get_gem_obj(fb, plane);
91 if (!obj)
92 return 0;
94 paddr = obj->paddr + fb->offsets[plane];
95 paddr += fb->format->cpp[plane] * (state->src_x >> 16);
96 paddr += fb->pitches[plane] * (state->src_y >> 16);
98 return paddr;
99 }
100 EXPORT_SYMBOL_GPL(drm_fb_cma_get_gem_addr);
102 /**
103 * drm_fb_cma_fbdev_init() - Allocate and initialize fbdev emulation
104 * @dev: DRM device
105 * @preferred_bpp: Preferred bits per pixel for the device.
106 * @dev->mode_config.preferred_depth is used if this is zero.
107 * @max_conn_count: Maximum number of connectors.
108 * @dev->mode_config.num_connector is used if this is zero.
109 *
110 * Returns:
111 * Zero on success or negative error code on failure.
112 */
113 int drm_fb_cma_fbdev_init(struct drm_device *dev, unsigned int preferred_bpp,
114 unsigned int max_conn_count)
115 {
116 struct drm_fbdev_cma *fbdev_cma;
118 /* dev->fb_helper will indirectly point to fbdev_cma after this call */
119 fbdev_cma = drm_fbdev_cma_init(dev, preferred_bpp, max_conn_count);
120 if (IS_ERR(fbdev_cma))
121 return PTR_ERR(fbdev_cma);
123 return 0;
124 }
125 EXPORT_SYMBOL_GPL(drm_fb_cma_fbdev_init);
127 /**
128 * drm_fb_cma_fbdev_fini() - Teardown fbdev emulation
129 * @dev: DRM device
130 */
131 void drm_fb_cma_fbdev_fini(struct drm_device *dev)
132 {
133 if (dev->fb_helper)
134 drm_fbdev_cma_fini(to_fbdev_cma(dev->fb_helper));
135 }
136 EXPORT_SYMBOL_GPL(drm_fb_cma_fbdev_fini);
138 static const struct drm_fb_helper_funcs drm_fb_cma_helper_funcs = {
139 .fb_probe = drm_fb_helper_generic_probe,
140 };
142 /**
143 * drm_fbdev_cma_init() - Allocate and initializes a drm_fbdev_cma struct
144 * @dev: DRM device
145 * @preferred_bpp: Preferred bits per pixel for the device
146 * @max_conn_count: Maximum number of connectors
147 *
148 * Returns a newly allocated drm_fbdev_cma struct or a ERR_PTR.
149 */
150 struct drm_fbdev_cma *drm_fbdev_cma_init(struct drm_device *dev,
151 unsigned int preferred_bpp, unsigned int max_conn_count)
152 {
153 struct drm_fbdev_cma *fbdev_cma;
154 struct drm_fb_helper *fb_helper;
155 int ret;
157 fbdev_cma = kzalloc(sizeof(*fbdev_cma), GFP_KERNEL);
158 if (!fbdev_cma)
159 return ERR_PTR(-ENOMEM);
161 fb_helper = &fbdev_cma->fb_helper;
163 ret = drm_client_init(dev, &fb_helper->client, "fbdev", NULL);
164 if (ret)
165 goto err_free;
167 ret = drm_fb_helper_fbdev_setup(dev, fb_helper, &drm_fb_cma_helper_funcs,
168 preferred_bpp, max_conn_count);
169 if (ret)
170 goto err_client_put;
172 drm_client_add(&fb_helper->client);
174 return fbdev_cma;
176 err_client_put:
177 drm_client_release(&fb_helper->client);
178 err_free:
179 kfree(fbdev_cma);
181 return ERR_PTR(ret);
182 }
183 EXPORT_SYMBOL_GPL(drm_fbdev_cma_init);
185 /**
186 * drm_fbdev_cma_fini() - Free drm_fbdev_cma struct
187 * @fbdev_cma: The drm_fbdev_cma struct
188 */
189 void drm_fbdev_cma_fini(struct drm_fbdev_cma *fbdev_cma)
190 {
191 drm_fb_helper_unregister_fbi(&fbdev_cma->fb_helper);
192 /* All resources have now been freed by drm_fbdev_fb_destroy() */
193 }
194 EXPORT_SYMBOL_GPL(drm_fbdev_cma_fini);
196 /**
197 * drm_fbdev_cma_restore_mode() - Restores initial framebuffer mode
198 * @fbdev_cma: The drm_fbdev_cma struct, may be NULL
199 *
200 * This function is usually called from the &drm_driver.lastclose callback.
201 */
202 void drm_fbdev_cma_restore_mode(struct drm_fbdev_cma *fbdev_cma)
203 {
204 if (fbdev_cma)
205 drm_fb_helper_restore_fbdev_mode_unlocked(&fbdev_cma->fb_helper);
206 }
207 EXPORT_SYMBOL_GPL(drm_fbdev_cma_restore_mode);
209 /**
210 * drm_fbdev_cma_hotplug_event() - Poll for hotpulug events
211 * @fbdev_cma: The drm_fbdev_cma struct, may be NULL
212 *
213 * This function is usually called from the &drm_mode_config.output_poll_changed
214 * callback.
215 */
216 void drm_fbdev_cma_hotplug_event(struct drm_fbdev_cma *fbdev_cma)
217 {
218 if (fbdev_cma)
219 drm_fb_helper_hotplug_event(&fbdev_cma->fb_helper);
220 }
221 EXPORT_SYMBOL_GPL(drm_fbdev_cma_hotplug_event);
223 /**
224 * drm_fbdev_cma_set_suspend - wrapper around drm_fb_helper_set_suspend
225 * @fbdev_cma: The drm_fbdev_cma struct, may be NULL
226 * @state: desired state, zero to resume, non-zero to suspend
227 *
228 * Calls drm_fb_helper_set_suspend, which is a wrapper around
229 * fb_set_suspend implemented by fbdev core.
230 */
231 void drm_fbdev_cma_set_suspend(struct drm_fbdev_cma *fbdev_cma, bool state)
232 {
233 if (fbdev_cma)
234 drm_fb_helper_set_suspend(&fbdev_cma->fb_helper, state);
235 }
236 EXPORT_SYMBOL(drm_fbdev_cma_set_suspend);
238 /**
239 * drm_fbdev_cma_set_suspend_unlocked - wrapper around
240 * drm_fb_helper_set_suspend_unlocked
241 * @fbdev_cma: The drm_fbdev_cma struct, may be NULL
242 * @state: desired state, zero to resume, non-zero to suspend
243 *
244 * Calls drm_fb_helper_set_suspend, which is a wrapper around
245 * fb_set_suspend implemented by fbdev core.
246 */
247 void drm_fbdev_cma_set_suspend_unlocked(struct drm_fbdev_cma *fbdev_cma,
248 bool state)
249 {
250 if (fbdev_cma)
251 drm_fb_helper_set_suspend_unlocked(&fbdev_cma->fb_helper,
252 state);
253 }
254 EXPORT_SYMBOL(drm_fbdev_cma_set_suspend_unlocked);